S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
1. Build the project. a. Select the build configuration. (optional) b. Click on Build. c. Check there are no compiler errors. 2. Configure the debug configuration to start a debug session. a. Click down arrow next to Debug button. b. Select 'Debug Configurations…' c. Select the debug configuration associated with your current build configuration. d. Select whether to rebuild code each time debug session start is requested. e. Click on Debugger tab. f. Verify proper interface and port. 3. Click Debug
記事全体を表示
Getting started with APEX2 S32DS: Getting Started - APEX2 Graph Tool Tutorial  Getting started with ISP S32DS: Getting Started - ISP Graph Tool Tutorial 
記事全体を表示
Online update In standard situation update can be started by clicking on message box appeared after S32DS Launch: If you don't see such message - you can check for updates/update your S32DS Installation manually. On main menu bar click on Help -> S32DS Extensions and Updates  Select from available items, then click "Install/Update" button  Offline update   Download update package from Updated/Patches (for S32DS 3.x - S32 Design Studio | NXP , for ARM S32DS - S32 Design Studio IDE for Arm® based MCUs|NXP, for Power Architecture S32DS - S32 Design Studio IDE for Power Architecture based MCUs | NXP ). Click on Help -> S32DS Extensions and Updates and choose Go to Preferences.   Click Add... Click Archive... and locate the zip file you downloaded and click OK Select the packages and updates then start the installation with the Install/Update button. 
記事全体を表示
PEmicro’s debug configuration allows user to modify JTAG communication shift frequency between debug interface and the target. By default, this frequency is set to a maximum value of 5000KHz, to take advantage of the fastest run control and FLASH programming experience: At the same time, not every PowerPC processor might be able to support highest debug shift frequencies with all PEmicro debug interfaces. For example, debug frequency for MPC5634M board used in conjunction with Multilink Universal FX RevC , needs to be lowered to 4000Khz in order to succeed. Hence, if debug session fails to successfully start up or fails on FLASH programming, lowering a debug shift frequency by a factor of 2 or 4 is the first trouble shooting recommendation. To get to PEmicro’s debug configuration window, one should select “Debug Configuration” from the menu next to a debug icon, and switch over to the Debug tab, within “Debug Configuration” menu pop- up.
記事全体を表示
Building Projects There is already a significant amount of information already available on this topic. Please explore the external references listed below for detailed information. External References Building Projects with Eclipse Build Several CDT C++ projects from command line With the following command line, it is possible to build the project KEA128: eclipsec -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data C:\Users\username\workspaceS32DS.ARM2.0 -build KEA128/Release   The project was located in workspace - C:\Users\username\workspaceS32DS.ARM2.0 Project Name is: KEA128 Build Configuration is: Release Emitting Source Code S32 Design Studio for Vision Emitting the source code from the command line: There are 2 sections in the Reference Manual, one for each of the ISP and APEX2 Visual Graph Tools. Processor Expert Software - S32 Design Studio There is a section in the Processor Expert User Guide titled 'Command Line Interface'
記事全体を表示
To install updates and additional packages to S32 Design Studio: 1) Download the Update from the S32 Design Studio page at NXP.com. 2) From S32 Design Studio, got to Help – S32DS Extensions and Updates. 3) Click on ‘Manage Sites’ link. 4) Select 'Add...' 5) Select 'Archive...', locate the downloaded update: 6) Click OK. 7) Click Apply and Close on the Preferences menu 😎 Notice the S32DS Extensions and Updates menu displays the new content. 9) Check the box next to the new package and click Install/Update. 10) Accept license terms and click Finish. 11) After the installation is complete, restart S32 Design Studio.
記事全体を表示
This Example demonstrates an alternative way to multi-core projects. This is basically a single eclipse project that generates the single elf file for dual core MCU (MPC5777C) See the project structure below where the sources for each core are separated into a core specific source folder: Main core0 [e200z7_0] performs basic initialization (Clocks, ports..) Each core initializes the interrupt controller in order to service interrupts generated by PIT (Periodic Interrupt Timer): Core 0 (e200z7_0) services PIT channel 0 interrupts generated once per second. Core 1 (e200z7_1) services PIT channel 2 interrupts generated once per two seconds.
記事全体を表示
The Image Vector Table (IVT) image is a set of pointers to other images which are required by the BootROM. It typically contains the following images, though not all are required to create a valid IVT image: DCD Self-Test DCD HSE Application Bootloader The IVT Tool enables configuration and generation of the IVT image as specified in the BootROM reference manual. Prerequisites Before using the IVT Tool, it will be useful to have already generated the binary image from your application project, it will be an input to the IVT. It may also be necessary to include a DCD image, for example, to initialize the SRAM. For application bootloader image, follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file, selecting 'Raw binary' option. For DCD image, follow the steps in HOWTO: Use DCD Tool To Create A Device Configuration Data Image . Procedure With desired project open in project explorer (C/C++ perspective), switch to IVT perspective. Click on 'Open IVT'. In the Boot Configuration section, check that the correct Boot Target is selected. For the demonstration here, M7_0 is the correct selection. Check the 'Interface selection' section. If your intended boot device is SD, MMC or eMMC, then change the setting from QuadSPI Serial Flash. If your intended boot device is QuadSPI AND you do not have a QuadSPI parameter file to specify, then uncheck the box for 'Configure QuadSPI parameters'. QuadSPI parameters change some flash registers' settings away from the default setting and are generally required for larger memory sizes (for ex. applications over 1 MB in size, for some supported devices). From the Image Table section, depending on your configuration, turn off all unused images. For the demonstration here, the following will be changed to Reserved: Self-Test DCD, Self-Test DCD (backup), DCD (backup), Application bootloader (backup). The following images will remain enabled: DCD, Application bootloader. In DCD section of the Image Table, click 'Browse File' and select the DCD binary file. Some of the fields may become red shaded after the file is loaded. This is OK as it is showing the memory layout is no longer aligned. This will be resolved in a later step.  Scroll down to the Application bootloader section, again use  'Browse File' and select the application binary. When the application boot image is loaded, the tool processes the file to check if it contains the header for the application bootloader image. If the header is not found, it means that the file is only the raw code (the bin generated by S32 Design Studio) and it will be necessary to provide the values for RAM start & entry addresses (code length is automatically calculated), as noted with the expanded view and red shading. To set the RAM start pointer and entry pointer addresses, from to the C/C++ perspective: From Project Explorer on the C/C++ perspective, open the linker file (in this case: hello_world\Project_Settings\Linker_Files\<device_name>_common_ram.ld) and locate the RAM start address and enter it in both the RAM start pointer AND RAM entry pointer fields in the IVT Tool. Use copy and paste to add the values to the Application Boot Image settings. Since the application binary file which was loaded for this example is just a raw binary file, it is necessary to generate the full application bootloader image. The Export Image function takes the values entered for the RAM start & entry pointers and the automatically calculated Code length, then generates the Application bootloader header. This header is added to the raw binary file producing a new image, the full application bootloader image file. Within the Application bootloader section, click 'Export Image' and enter a meaningful name for the image file. In addition to being a necessary source component of the IVT image, this file can more easily be shared or re-used to as an input to other IVT images. After the file has been generated, you will notice that the address settings section has collapsed. This is because it has replaced the file you originally selected with the newly generated one and the tool has recognized that the file contains the required header information. Before the Blob image can be generated, all of the images must be properly aligned within the memory map. You will likely also see error messages regarding segment overlaps, but even without this error it is good to check that the alignment is correct. In the Automatic Align section, if you have a dedicated area of the memory you can specify the start address and then click 'Align'. If you don't have a dedicated area, then use the default automatic align start address of 0x0 (QSPI), or 0x1000 (SD, MMC, eMMC). Click 'Align' to automatically align the images to this address. Upon successful completion of the alignment, all of the red shading will be removed. Click 'Export Blob Image' to generate the blob image file. This is what will be flashed to the target. Now that the Blob Image is generated, the 'Flash Image' button could be used to program the image to the target over serial connection, or use the S32 Flash Tool.
記事全体を表示
IVT - short for Image Vector Table, is an image with a set of pointers to other images which are required at boot by the embedded BootROM. This video will explain using S32V chip how IVT tool works and covers create and flash SDK's PIT example.
記事全体を表示
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the ability to access the flash programming and debugging of the S32 Debug Probe via GDB command line. This document provides only the necessary commands specific to launching a debug session on NXP devices. It does not cover general GDB command line operations, these are covered in detail in the GNU communities and other public websites which are not associated with NXP.   Preparation Setup the software tools Install S32 Design Studio for S32 Platform  Install the Development Package for the device you are debugging. In this case, the S32G2xx development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for initialization of the cores. Setup the hardware Confirm the setup of the S32G274A evaluation board.  Configure the JTAG. The S32G274A evaluation board supports both 10- and 20- pin JTAG connections. The default board configuration is set to 20-pin, change the position of the jumper J59 from 2-3(default)  to 1-2, if you are using the 10 Pin JTAG interface. Both are supported by the S32 Debugger and S32 Debug Probe. Connect the power supply cable Setup the S32 Debug Probe Connect the S32 Debug Probe to the evaluation board via JTAG cable. Refer to the S32 Debug Probe User Manual for installation instructions. Use the JTAG connection as was confirmed in the previous step. Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard.     Procedure As separate debug threads need to be started for each core to be debugged, and the method for launching a debug thread differs depending upon whether it is a primary core or secondary core and if the executable image will be loaded or if the executable is already running and the debugger just needs to be attached. These scenarios will be covered by the following 3 sections: Primary Core Load Image and Run: The application image will be loaded directly to memory by the debugger and then initialized and started. The primary core will launch any secondary cores used by the application. Secondary Cores: The primary core has launched a secondary core, it is now running and the debugger will connect through the attach method. Primary Core Image Already In Memory and Running: The primary core has already been initialized and launched by other means, such as via a Linux OS on the target, so the debugger will connect through the attach method without initializing or loading the image to memory.   Please proceed with the section which applies to the core for which you are starting a debug thread.   Primary Core Load Image and Run Prepare the initialization script for the core(s) to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx\s32g2xx_generic_bareboard_all_cores.py Uncomment the following lines: #_JTAG_SPEED = 16000 #_PROBE_IP = "10.112.101.91" #_GDB_SERVER_PORT = 45000 #_CORE_NAME = 'M7_0' #_RESET_TYPE = "default" #_RESET_DELAY = 1 #_REMOTE_TIMEOUT = 60 #_IS_LOGGING_ENABLED = True This file is used by the S32 Debugger within the S32 Design Studio IDE where the settings are provided from the GUI, so these lines are commented out in order to allow the GUI settings to have control. The commented lines are provided so the script could more easily be run by the command line method. Update the IP address line (_PROBE_IP) to match the IP address of the S32 Debug Probe which is connected to your PC. See the user guide for the S32 Debug Probe for details on how to obtain the IP address.  Update the core name (_CORE_NAME), if necessary. See s32g2xx_context.py for complete list of supported cores. Save the file with a new name to preserve the original. For example, s32g2xx_gen_bb_all_c_my_probe.py. This ensures the S32 Debugger will still function correctly.   Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe  Should see a window appear like this:   Ensure Environment Variable for Python is set. From command prompt, run the command:  set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window:   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32g2xx\\s32g2xx_gen_bb_all_c_my_probe.py This specifies the script for initialization. py board_init() This initializes the board. It should only be called for the initial core. In a multicore debugging workflow, the debugger launch for additional cores would omit this step. py core_init() This initializes the core specified in the initialization script in step 1.   Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\New_S32G_Project\\New_S32G_Project_M7_0\\Debug_RAM\\New_S32G_Project_M7_0.elf load   Secondary Cores After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. Some additional steps will need to be performed from within the primary core GDB session, enter the following commands: set *0x34100000 = 0x34200000  set *0x34100004 = 0x34100025 set *0x34100024 = 0xFFFEF7FF set *0x34200000 = 0x34300000 set *0x34200004 = 0x34200025 set *0x34200024 = 0xFFFEF7FF b main c   These lines prepare the environment for launching debugging on secondary cores. This will allow for multicore debugging in the case of separate ELF files for each core. These can be found in the Run Commands field of the Startup tab on the Debug Configuration for the primary core within S32 Design Studio IDE, of any multicore project created from the New Application Project Wizard. Note: If there is just one ELF file for all cores, then these 'set *0x... = 0x...' commands should be skipped. In general, it will be correct to set the break-point at main, as shown, but this might need to be changed depending on when the secondary cores are started within the project. Prepare the initialization script for the secondary core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx\s32g2xx_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: #_JTAG_SPEED = 14000 #_GDB_SERVER_PORT = "127.0.0.1:45000" #_RESET_TYPE = "default" #_PROBE_IP = "s32dbg:10.222.24.64" #_CORE_NAME = 'M7' #_RESET_DELAY = 1 #_CMD_TIMEOUT = 7200 #_REMOTE_TIMEOUT = 60 #_IS_LOGGING_ENABLED = True #_SOC_NAME = "S32G274A" Make the following changes to the lines: _JTAG_SPEED = 14000 ->  None _GDB_SERVER_PORT = "127.0.0.1:45000" -> 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg:10.222.24.64" -> None _CORE_NAME = 'M7' -> 'M7_1' (this should be set to match the name of the core to be debugged, see s32g2xx_context.py for complete list) _RESET_DELAY = 1 _CMD_TIMEOUT = 7200 _REMOTE_TIMEOUT = 60 _IS_LOGGING_ENABLED = True _SOC_NAME = "S32G274A" Save the file with a new name to preserve the original. For example, s32g2xx_attach_my_probe_core1.py. This ensures the S32 Debugger will still function correctly. The existing GTA server is used, so do not launch a new one. Open an new command window and follow similar steps as done for the primary core. Setup the Python environment variable, if not done globally set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Start GDB Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window:   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32g2xx\\s32g2xx_attach_my_probe_core1.py This specifies the script for initialization. We will not execute the py board_init() as this was already done for the primary core. py core_init() This initializes the core specified in the initialization script in step 2.   Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\S32G_MultiCore\\S32G_MultiCore_M7_1\\Debug_RAM\\S32G_MultiCore_M7_1.elf load   Repeat 3-6 for each additional core. Primary Core Image Already in Memory and Running The core is running and does not need to be initialized. Prepare the initialization script for the core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx\s32g2xx_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: #_JTAG_SPEED = 14000 #_GDB_SERVER_PORT = "127.0.0.1:45000" #_RESET_TYPE = "default" #_PROBE_IP = "s32dbg:10.222.24.64" #_CORE_NAME = 'M7' #_RESET_DELAY = 1 #_CMD_TIMEOUT = 7200 #_REMOTE_TIMEOUT = 60 #_IS_LOGGING_ENABLED = True #_SOC_NAME = "S32G274A" Make the following changes to the lines: _JTAG_SPEED = 14000 _GDB_SERVER_PORT = "127.0.0.1:45000" -> 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg:10.222.24.64" -> (enter the IP address of your probe) _CORE_NAME = 'M7' -> 'M7_0' (this should be set to match the name of the core to be debugged, see s32g2xx_context.py for complete list) _RESET_DELAY = 1 _CMD_TIMEOUT = 7200 _REMOTE_TIMEOUT = 60 _IS_LOGGING_ENABLED = True _SOC_NAME = "S32G274A" Save the file with a new name to preserve the original. For example, s32g2xx_attach_my_probe_core0.py. This ensures the S32 Debugger will still function correctly.   Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe Should see a window appear like this:   Ensure Environment Variable for Python is set. From command prompt, run the command: set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window:   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32g2xx\\s32g2xx_attach_my_probe_core0.py This specifies the script for debugger initialization. Do not execute the py board_init() as this will initialize the board, and reset the currently executing application, which is not desired for this case. py core_init() This initializes the debugger connection to the core specified in the initialization script in step 1.   Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\S32G_Multicore\\S32G_Multicore_M7_0\ \Debug_RAM\\S32G_Multicore_M7_0.elf load   After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. See section ‘Secondary Cores’ for each additional core to be debugged.
記事全体を表示
If your EVB with OpenSDA debugger can't start debug session - you can try to update OpenSDA firmware on your board.  Go to PE Micro web pages - http://www.pemicro.com/opensda/ and get the latest firmware archive.  Extract .SDA file related to your EVB - for example            DEBUG-OPENSDA-E200_Pemicro_v110.SDA for DEVKIT-MPC5748G            MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA for S32K144EVB  Press and hold SW3 (Reset for S32K144EVB) button and connect OpenSDA connector on EVB to PC. New BOOTLOADER Drive should appear on your PC.  Copy .SDA file in BOOTLOADER drive Reset EVB.   More details you can find in "Updating the OpenSDA Firmware.pdf" file. It is part of downloaded zip file from PE Micro web pages. 
記事全体を表示
The release notes of S32K RTD usually mention which dependent software packages need to be installed. Taking SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_ReleaseNotes.pdf as an example, we can see that the following software packages need to be installed: You must be logged into your account on NXP.com to gain access to the download link. 1. Download and install S32Design Studio 3.5: Click S32 Design Studio 3.5 – Windows/Linux -> 3.5 S32 Design Studio for S32 Platform v.3.5 -> S32DS.3.5_b220726_win32.x86_64.exe Note: For Windows OS, the user account designated for installing S32 Design Studio for the S32 Platform must be a member of the local Administrators security group.   2. Download and Install S32 Design Studio 3.5 Update 8 D2311: SW32_S32DS_3.5.8_D2311.zip (com.nxp.s32ds.update_3.5.8.20231116041033.zip) Since the SW32K3_S32DS_3.5.8_D2311.zip downloaded in step3 already contains the files of the SW32_S32DS_3.5.8_D2311.zip in the step2, we will skip this step here.   3. Click S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio Download and Install S32 Design Studio 3.5.8 Development Package with support for S32K3xx devices (3.5.8_D2311): SW32K3_S32DS_3.5.8_D2311.zip  (com.nxp.s32ds.s32k3xx.update_3.5.8.20231116045533.zip) Unchecking Contact all update sites during install to find required software can complete offline installation faster.   4. Download and install S32 Design Studio 3.5.6 RTM with support for S32K39x devices(3.5.6_D2309): SW32K39x_S32DS_3.5.6_D2309.zip   5. For users who need to use S32M27x(Otherwise, go to step 6), please click S32M2 Standard Software -> Automotive SW - S32M2 - S32 Design Studio Download and Install S32 Design Studio 3.5.8 Development Package with support for S32M2xx devices(3.5.8_D2311): SW32M2_S32DS_3.5.8_D2311.zip (com.nxp.s32ds.s32m2.update_3.5.8.20231116044631.zip)   6. Click S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M Select and install one of the updatesite for S32K3 RTD 4.0.0.  The latest S32K3 RTD version is usually recommended. However, if you need to use Reference Software or Premium Software (such as FreeRTOS, LIN Stack, TCP/IP Stack, AWS Libraries for S32K3, S32 Safety Software Framework (SAF) for S32K3xx, Structural Core Self-Test (SCST), HSE Premium Firmware, ISELED Driver), it is recommended to install the specific version of S32K3 RTD according to their release notes. Since there are many versions of S32K3 RTD 4.0.0, only one version of RTD will be installed here. Download and install S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 4.0.0: SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip Then in S32DS v3.5, click File -> New -> S32DS Project from Examples and you should be able to see the example projects for S32K3 RTD 4.0.0.
記事全体を表示
The Quick Start describes how to use the S32 Design Studio to create, build, and debug a project. Starting S32DS Design Studio for S32 Platform 3.5 To start S32 Design Studio and begin to work with it: Launch S32 Design Studio : locate the shortcut depending on your selection during the installation, and double-click the product icon. The Eclipse Launcher dialog box appears to let you define the location of your workspace.   Note: A workspace is the folder where S32 Design Studio stores projects that you create or import. Select a folder for your workspace. It is recommended to create a new workspace for each product instance. To choose the default location, click OK. To use a different location, click Browse. In the Select Workspace Directory dialog box, select the preferred folder or click Make New Folder to create a new folder for storing your projects. Click OK. S32 Design Studio is launched. Browse through the Getting Started tab and close it. The workbench appears:   Creating and building a project   To create and build a project: Click File > New > S32DS Application Project or S32DS Library Project on the menu bar. The first page of the wizard appears. Specify the name of the new project in the Project name text box. Note: The Location field shows the default project location. If you want to change this location, clear the Use default location check box, click Browse and specify a different location. Click OK. Select the target processor from the Processors panel. Click Next. The second page of the wizard appears. Check the project settings, select the cores and parameters. Click Finish. The new project appears in the Project Explorer view. Note: The wizard creates one or multiple projects, depending on the number of selected cores. To build your project, do any of the following: Right-click the project in the Project Explorer view and click Build Project Select the project in the Project Explorer view, then click Project > Build Project on the menu Select the project in the Project Explorer view and click on the tool icon on the toolbar.        The build process starts.   If a build generates any errors or warnings, you can see them in the Problems view. Read through the build messages in the Console view to make sure that the project is built successfully.   Debugging a project   To debug a project: Set the debug configuration for your project. Select the project in the Project Explorer view. Open the debug configuration in any of these ways: Right-click the project and select Debug as > Debug Configurations… from the context menu. Choose Run > Debug Configurations… from the menu bar. Click an arrow next to Debug picture on the toolbar and select DebugConfigurations…. In the Debug Configurations dialog box, select the required debug configuration. The name of the debug configuration is composed of the project name, debugging interface and build configuration. The configuration settings appear on the tabs.   Modify the configuration settings where required and click Apply to save the changes. Click Debug. The debugger downloads the program to the memory of the target processor. The Debug perspective is displayed. The execution halts at the first statement of the main() function. The program counter icon on the marker bar points the next statement to be executed.   To set and run to a breakpoint: Double-click on the marker bar next to a statement. The breakpoint indicator (blue dot) appears next to the statement. From the Debug view, select Run > Resume on the menu bar. The debugger executes all statements up to (but not including) the breakpoint statement. To control the program: From the Debug view, select Run > Step Over from the menu bar. The debugger executes the breakpoint statement and halts at the next statement. From the Debug view, select Run > Resume from the menu bar. The debugger resumes the program execution. From the Debug view, select Run > Terminate. The debug session ends.
記事全体を表示
Before you can start debugging an S32DS for Vision project for S32V234 Cortex-A53 APEX2/ISP Linux target on the S32V234-EVB, we must first setup the hardware connections and start the Linux BSP OS. 1) Connect (1) S32V234 USB Micro B port to (2) USB A port on your PC. This allow you to connect to the Linux BSP OS via a terminal program to issue commands and to obtain the IP address. 2) Insert microSDHC card (with U-boot, Linux kernel, devicetree, and root file system loaded*) into (3) the S32V234 SD card slot   3) Connect (1) Ethernet port on S32V234 daughter card to (2) LAN**. This will allow S32DS to communicate with the Linux BSP OS for flashing and GDB debugging.   4) Connect the power supply to (3) S234V234 EVB 5) Turn on the (4) power switch, this will start the Linux BSP OS *Instructions for preparing the SD card are provided in the VisionSDK document: ..\S32DS_Vision_v2.0\S234DS\s234v234_sdk\docs\vsdk\S32V234-EVB_SetupGuide.pdf or refer to https://community.nxp.com/docs/DOC-335023  **Ensure PC is connected to LAN as well (either hardwired or wireless)
記事全体を表示
This simple example shows how to attach GPIO Interrupt handler to particular GPIO Pin. Example is for S32K148 EVB and uses SW4 connected to PTC 13 and Green LED connected to PTE 22. Pressing SW4 invoke interrupt and Interrupt handler toggles Green LED. 
記事全体を表示
  The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the capability to access the flash programming capabilities of the S32 Debug Probe via the S32 Debugger. Note: currently only QSPI flashing is supported. Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. In this case, the S32G2xx development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for performing the flash programming operations.   Open the application project containing the application to be programmed to the flash memory device. Follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file , selecting the 'Raw Binary' option. Build the project, generating the binary executable. This will be our application binary input to the IVT Tool. The IVT Tool must be used to generate the BLOB image which can be programmed to flash memory device and loaded to the RAM by the BootROM. Follow the steps in HOWTO: Use IVT Tool To Create A BLOB Image S32G274A. The resulting BLOB image file is what can be flashed to the device.   Procedure Open Debug Configuration menu Select 'S32 Debugger Flash Programmer', then right-click and select New. Enter an name for the new configuration and click Add... to add the file to be flashed. Click Browse... to select the project from the workspace where the application binary is located Select the project and click OK By default, the ELF file is found. Click Search in project to select the binary file. Select the .bin file and click OK Now we must enter the base address. Typically, this could be 0, but you may have other requirements. Click OK. Just the memory required by the new image needs to be cleared, so only check the box 'Erase all flash memory' if truly needed. Now we are ready to configure the debugger connection settings. Click on the Debugger tab. Starting from the top and working our way down, click on Select device. Select the device and click OK The correct Initialization script will automatically be set. Set the Debug Probe Connection settings to match your setup. When done, click Apply To start the flashing, click Debug When complete, the Debug perspective will show at terminated thread.   Happy flashing with GDB!   Note, to debug this application since it will be subsequently started by the BootROM: use 's32gxx_attach.py' in the Initialization script field on the debugger tab of the Debug Configurations menu Make the following adjustments on the Startup tab within the Debug Configurations menu: Uncheck "Load image"  Check "Set program counter at:" and enter the value "Reset_Handler"  
記事全体を表示
S32 Platform Download and Install S32 Design Studio for S32 Platform v3.6  S32 Design Studio 3.6 Main Features Download and Install S32 Design Studio for S32 Platform v3.4    S32K1 Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2 A demonstration of the use of the Migration wizard in S32 Design Studio 3.4 to migrate S32K1 projects from S32 Design Studio for Arm and S32 SDK 3.0.x to S32 Design Studio 3.4 and S32 SDK 4.0.2   S32G2 Getting Started: Pins Tool Getting Started: DCD Tool Getting Started: IVT Tool Getting Started: DDR Tool   S32R45 Install S32R45 Development Package Install S32R45 Radar Extension Package Creating And Building A Project on the S32R45 for A53, LAX and SPT Cores in S32 Design Studio   S32V2 Create From Example 1 | Create an ISP project from example  A demonstration of how to load an example ISP image processing application project featuring RGB, YUV, and GS8 image formats, in the S32 Design Studio. 2 | Create an APEX2 project from example  A demonstration of how to load an example ORB-based APEX2 image processing application project in the S32 Design Studio. Create New Project 3 | Create a new ISP application  A demonstration of how to create a new Debayer-based ISP image processing application project in the S32 Design Studio. 4 | Create a new APEX2 application  A demonstration of how to create a new APEX2 image processing application project featuring upscaling and downscaling in the S32 Design Studio. Debug 5 | ISP Debugging w/S32 Debug Probe   A demonstration of how to setup and debug an ISP application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 6 | APEX2 debugging w/S32 Debug Probe  A demonstration of how to setup and debug an APEX2 application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 7 | APEX2 debugging with Emulator  A demonstration of how to debug an emulated-APEX2 image processing application project in the S32 Design Studio. 8 | Debug a Linux A53 project  A demonstration of how to debug a Linux A53 application project in the S32 Design Studio for Vision version 2.0. The example shown also includes code for APEX, but currently GDB Remote Linux only supports debug of the A53 code.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 2          What is new? S32 SDK for Power Architecture 0.9.0 BETA for MPC574x-B-C-G and MPC574xP derivatives (see attached release notes for more details) S32 SDK  Power Architecture v0.9.0  BETA Examples - "Create S32DS Project from Example" Updated version of GNU Build tools for e200 (see the release notes attached below) Support of GHS compiler in New Project Wizard - please contact GreenHills support to obtain toolchain plugin compatible with Eclipse Neon version Updated P&E Plugin (v1.7.3.201803261737) and drivers (v12.7.0) Fixed Defects • S32DS-3506 - [e200][MPC5744P] unable to connect to secured device - addressed by adding unsecure support for MPC5744P devices • S32DS-7326 - [e200][MPC5634M] Exception occurs when accessing peripheral A registers - MMU init script error is resolved by updating the script • S32DS-7991 - [e200 2017.R1] Semihosting disabling interrupts is resolved by not disabling interrupts when stepping over specific instruction • S32DS-7177 - [MPC5634M] unable to access RAM in the debug session • S32DS-7896 - [e200] default linker sections (.got2, .jsr...) are missing in the linker script file • S32DS-3681 - [S32DS E200 B170421] Project build fail with Library support = newlib, the startup.S update to add section _fini Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
CAN communication is supported in the latest version of MPC5777C Bootloader .rbf file (attached below) + Supported UART0/eSCI_0(J20 on DB): GPIO89-90 pins(Speed: 115200b/s) + Supported  MCAN0(J5 on MB):  GPIO83-84 pins(Speed: 500Kb/s)   Tested on the dev board:   Motherboard MPC57xxMB Development Board X-MPC5777C-516DS Processor SPC5777CDMMO3 3N45H Also included is a version of the .rbf file where the delay before app start is 1 second (instead of 3 seconds)
記事全体を表示
In this document, the steps to create a new S32 Design Studio project from example will be detailed. 1. Launch S32 Design Studio 2. Use quick S32DS Project from Example button from Dashboard.  or select File -> New -> S32DS Project From Example   3. Select one of the projects, for example, S32K58_PI_MonteCarlo_BM. Click Finish.     4. The project is added to the current workspace. It is ready to be built and can be executed on the target.  
記事全体を表示