S32 Design Studio知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio Knowledge Base

讨论

排序依据:
S32 Design Studio (S32DS) supports Lauterbach’s “loos coupling” version of Eclipse plug-in to debug S32DS projects via a Lauterbach probe + TRACE32 standalone application. This configuration uses Eclipse IDE for development and standalone TRACE32 for debugging.    This plug-in supports the features below: Start TRACE32 from an Eclipse launch configuration Support for multiple projects (multi-core) Synchronization of breakpoints between Eclipse and TRACE32 Open source file' functionality from TRACE32 to Eclipse and vice versa See the Lauterbach document for additional information about the plug-in.   Installation instructions First of all make sure you have TRACE32 installed. Now let's proceed to eclipse plug-in installation.   First of all make sure you have TRACE32 installed. Now let's proceed to eclipse plug-in installation.   go to menu "Help" -> "Install New Software"    Click on the arrow to bring up the list.  Select ‘LauterbachGmbHUpdateSite - http://www.lauterbach.com/eclipse‘                 Check the box next to the Lauterbach TRACE32 Eclipse Loose Coupling and click "Next"   Check "I Accept the terms of the license agreement" and Select all Lauterbach certificates to trust. Finally you proceed to the installation. When the plugin is installed you will be asked to restart S32DS   Now you should be able to use the New Project Wizard create an application project with Lauterbach Debugger support:     Or manage (create, delete, adjust) Lauterbach eclipse debug configurations:   Enjoy debugging with TRACE32 Eclipse plug-in in S32DS!  
查看全文
So you have created a project in S32DS for Vision with target of S32V234 Cortex-A53 APEX2/ISP Linux . You have built the project and now want to execute it on the S32V234-EVB, which is running the Linux BSP from the VSDK on a SD card. There are many ways to do this, however, the simplest is to use the built-in support within S32DS to run and/or debug over an Ethernet connection to the Linux BSP OS running on the EVB. In order for S32DS to connect to the Linux BSP OS, the following steps should be followed: 1) First, we must complete the steps to Setup S32V234 EVB for debugging with Linux BSP. 2) With the Linux running on the EVB, start a terminal program (for ex. PuTTY) on your PC 3) Set Connection type to Serial 4) Set speed to 115200, Data bits 8, Stop bits 1, Parity None 5) Set Serial line to the COM port associated with the USB port setup in step 1 of this document. (for ex. COM3) 6) Click Open to start the terminal session 7) Press enter key to bring up login prompt 😎 Log into Linux (login name is "root") 10) Get IP address, enter command:    ifconfig       Make note of the IP address 11) Launch S32DS for Vision. From the C/C++ Perspective, select Run->Debug Configurations... 12) From 'C/C++ Remote Application'. Select '<project_name>_Remote_Linux' debug configuration. 13) Select New to create new debug connection. 14) Select SSH 15) Enter the IP address noted earlier 16) Enter user ID as "root". The Linux BSP uses Password based authentication, but by default, no password is set. So the password can be left blank. 17) Select Finish 19) Select Apply, and then if you wish, Debug
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2.2  Update 1          What is new? SDK S32K1xx RTM SR 3.0.3 (Patch for SDK S32K1xx RTM 3.0.0) AMMCLIB version 1.1.19 for KEAx, for S32K11x, for S32K14x AMMCLIB version 1.1.20 for KEAx, for S32K11x, for S32K14x Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  online installation: go to menu "Help" -> "S32DS Extensions and Updates" dialog check boxes next to "S32K1xx development package", "S32K1xx SDK 3.0.3 pakage" and "S32 Design Studio for ARM Devices development package" click "Install/Update 3 item(s)" offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file go to menu "Help" -> "S32DS Extensions and Updates" dialog select "Go to Preferences" Add a new Software Site Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step check boxes next to "S32K1xx development package" and "S32 Design Studio for ARM Devices development package" click "Install/Update 2 item(s)" This will start the update installation process.
查看全文
S32 Design Studio (S32DS) for ARM supports IAR Plugin, and the user can use IAR specific features in S32DS with IAR toolchain for ARM. This document describes the way to convert S32DS project to IAR EW based project using project exporting wizard in S32DS. This guidance is based on the NXP S32K144 microcontroller, and compatible with S32K14x / S32K11x family.   The version of each IDE which is used for this document is as follows: S32 Design Studio for Arm 2018.R1 IAR Embedded Workbench for ARM 8.32.1.18631     1. Install IAR Plugin using IAR Embedded Workbench plugin manager on S32DS Help - Install New Software   Put "IAR Embedded Workbench for Eclipse " as the repository for new installation of software.     Help - IAR Embedded Workbench Plugin Manager     Install IAR Plugin which is matched with your IAR version.         2. Create S32DS Project File - New - S32DS Application Project   The tool chain should be chosen as IAR Toolchain. Be noted that the IAR 7.x toolchain is different from the IAR 8.x.   The project is created as follows.     3. Export S32DS Application Project File - Export   Choose S32 Design Studio - Project Info Export Wizard   Now "ProjectInfo.xml" was created. "ProjectInfo.xml" should be used for creating a project in the IAR EW.   4. Create IAR EW Project The way to create IAR project as described below. The snapshots are based on IAR EW 8.32.1. Details may vary.   5. Connect the Project Use the menu - Project - Add Project Connection, and choose "Freescale Processor Expert".   Select the "ProjectInfo.xml" file which was created at step #3.    Now, the project which had been created in IAR was connected to the S32DS project.   The created IAR project should be modified if the user wants to use the project with S32DS SDK to build and debug under IAR EW environment as follows.   1. Modify the Linker configuration and remove ProjectInfo.xml Remove "ProjectInfo.xml"   Linker configuration from the project Options   Even though the user modified the linker configuration, a definition in IAR EW  for "device_registers.h" from SDK will cause build error when trying building the project.   This error will be eliminated by inserting Chip specific definition into IAR project. If you take a look into the "device_register.h", you can find the definition as follows.   2. Define symbols  Right mouse click on the Project name - Options   Write the symbols referred from "device_register.h". The symbols may vary (e.g., CPU_S32K146, CPU_S32K142, ...).   3. Build and Debugger configuration Options - Debugger   I used PE micro's OpenSDA on S32K144EVB for this document. After choosing debugger and clicking Download and Debug (Ctrl+D), you can see the P&E Configuration Manager as follows. Just choose appropriate configuration, and select the correct part number of S32K by clicking Select New Device.   Finally, you can download and debug the converted IAR EW project with S32DS SDK.
查看全文
S32 Design Studio for S32 Platform - 3.6.x releases   Date Version Release content/NPI support Download link Notes March 31, 2025 S32DS 3.6.1 S32K1 S32K3 S32M2 S32G S32ZE S32N S32J S32R41 S32R45 SAF85 SAF86 S32R43/R47 Flexera Win/Linux installer and updater for S32DS 3.6.1 with all public NPI's  integrated Nov 29, 2024 S32DS 3.6.0 S32K1 S32K3 S32M2 S32G S32ZE S32N S32J S32R41 S32R45 SAF85 SAF86 S32R43/R47 Flexera Win/Linux installer for S32DS 3.6 with all public NPI's  integrated   S32 Design Studio for S32 Platform 3.6.0 Release Announcement  S32 Design Studio for S32 Platform - 3.5.x releases   Date Version Release content/NPI support Download link Notes July  29, 2022 S32DS 3.5 base/platform package Flexera Win/Linux installer for S32DS 3.5  Sep 30, 2024 S32DS 3.5.14 Update 14 with support for S32Z2/E2 SPF2 Add-On 1.5.0 download offline package installable on previous S32DS 3.5.x installations via S32DS Extensions and Updates (see installation Note* from below) Jul 31, 2024 S32DS 3.5.13 Update 13 with support for: S32R45 Development Package 3.5.13 S32Z2/E2 Development Package 3.5.13 S32K3xx Development Package 3.5.13 S32K39x Development Package 3.5.13 S32M2xx Development Package 3.5.13 S32R45 Radar Extension 1.5.0 S32R45 BBE32 Add-On 1.5.0 S32Z2/E2 SPF2 Add-On 1.4.0 download May 31, 2024 S32DS 3.5.12 Update 12 with support for: S32N5 Development Package 3.5.12 SAF85xx and SAF86xx Development Package 3.5.12 SAF85xx Radar Extension Package 1.2.0 SAF85xx and SAF86xx BBE32 Add-On 1.3.0 download Mar 29, 2024 S32DS 3.5.11 Update 11 with support for: S32Z2/E2 SPF2 Add-On 1.3.0 SAF86xx Development Package 3.5.11 SAF86xx BBE32 Add-On 1.2.0 download Jan 31, 2024 S32DS 3.5.10  Update 10 download Dec 20, 2023 S32DS 3.5.9  Update 9 download Nov 29, 2023 S32DS 3.5.8 Update 8 with support for: S32K3xx Development Package 3.5.8 S32M2xx Development Package 3.5.8 download Sep 29, 2023 S32DS 3.5.6 Update 6 with support for: S32Z2/E2 Development Package 3.5.6 S32Z2/E2 SPF2 Add-on package for  1.2.0 S32K39x Development Package 3.5.6 download Aug 31, 2023 S32DS 3.5.5 Update 5 with support for: S32R45 Development Package 3.5.5 Radar Extension and BBE32 Add-on package for S32R45 1.4.0 S32V2 Development Package 3.5.5 download Jul 31, 2023 S32DS 3.5.4 Update 4 with support for: S32K1 Development Package 3.5.4 download Jun 30, 2023 S32DS 3.5.3 Update 3 with support for: S32Z27/E27 Development Package S32R41 Development Package S32R41 Radar Extension Package S32R41 BBE32 Add-on download Feb 28, 2023 S32DS 3.5.2 Update 2 with support for: S32G, S32R41, S32V2 Development Packages download (Note*) Installation procedure for platform update/development/extended/add-on packages: Install S32 Design Studio v3.5 (base/platform) version using Win/Linux installer Download the archive files for platform/dev/ext/add-on package. Start S32 Design Studio v3.5 and install the application package. Go to  Help > S32DS Extensions and Updates. In the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to  S32DS Extensions and Updates and can use this dialog to select desired packages. Q: How to install S32DS 3.5.6 ? A: install S32DS 3.5 base/platform using Win/Linux installer and apply Update 6 or apply Update 6 on existing S32DS 3.5.1-5 installation S32 Design Studio for S32 Platform - legacy versions   S32 Design Studio for S32 Platform 3.4 (Windows/Linux) S32 Design Studio for S32 Platform 3.4 Update 1 (for S32G2) S32 Design Studio for S32 Platform 3.3 (Windows/Linux)  S32 Design Studio for S32 Platform 3.2 (Windows/Linux)  S32 Design Studio 3.2 - Update 191226 S32 Design Studio 3.2 - Update 191219 S32 Design Studio 3.1 (Windows/Linux) S32 Design Studio 3.1 - Update 2    S32 Design Studio 3.1 - Update 190708  S32 Design Studio 3.1 - Update 190508  S32 Design Studio 2018.R1 (Windows/Linux)   Development packages S32K1 Service Pack 1 (S32 Design Studio 3.4) S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0 (S32 Design Studio 3.3) Extension packages Vision Extension Package for S32V234 1.2.0 (S32 Design Studio 3.3) Vision Extension Package for S32V2xx 1.0.0 (for S32 Design Studio 3.1)   S32DS for Arm S32 Design Studio for Arm 2.2 (Windows/Linux)  S32 Design Studio for Arm 2.2 - Update 1 S32 Design Studio for Arm 2018.R1 (Windows/Linux)  S32 Design Studio for Arm 2018.R1 - Update 11  S32 Design Studio for Arm 2018.R1 - Update 10  S32 Design Studio for Arm 2018.R1 - Update 9  S32 Design Studio for Arm 2018.R1 - Update 8  S32 Design Studio for Arm 2018.R1 - Update 7 S32 Design Studio for Arm 2018.R1 - Update 6  S32 Design Studio for Arm 2018.R1 - Update 5 S32 Design Studio for Arm 2018.R1 - Update 4  S32 Design Studio for Arm 2018.R1 - Update 3 S32 Design Studio for Arm 2018.R1 - Update 2 S32 Design Studio for Arm 2018.R1 - Update 1 S32 Design Studio for Arm v2.0 (Windows/Linux) S32 Design Studio for Arm v2.0 - Update 3 S32 Design Studio for Arm v2.0 - Update 2 S32 Design Studio for Arm v2.0 - Update 1 S32 Design Studio for Arm v1.3 (Windows/Linux)  S32 Design Studio for Arm v1.3 - Update 3 &amp; 4 S32 Design Studio for Arm v1.3 - Update 2 S32 Design Studio for Arm v1.3 - Update 1 S32 Design Studio for ARM v1.2 (Windows/Linux)    S32DS for Power S32 Design Studio for Power Architecture v2.1 (Windows/Linux)  S32 Design Studio for Power Architecture v2.1 - Update 14 S32 Design Studio for Power Architecture v2.1 - Update 13 S32 Design Studio for Power Architecture v2.1 - Update 12 S32 Design Studio for Power Architecture v2.1 - Update 10  S32 Design Studio for Power Architecture v2.1 - Update 8  S32 Design Studio for Power Architecture v2.1 - Update 7  S32 Design Studio for Power Architecture v2.1 - Update 2  S32 Design Studio for Power Architecture v2.1 - Update 1  S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux)  S32 Design Studio for Power Architecture 2017.R1 - Update 11  S32 Design Studio for Power Architecture 2017.R1 - Update 10  S32 Design Studio for Power Architecture 2017.R1 - Update 9 S32 Design Studio for Power Architecture 2017.R1 - Update 8 S32 Design Studio for Power Architecture 2017.R1 - Update 7  S32 Design Studio for Power Architecture 2017.R1 - Updates 5 and 6  S32 Design Studio for Power Architecture 2017.R1 - Update 4 S32 Design Studio for Power Architecture 2017.R1 - Update 3  S32 Design Studio for Power Architecture 2017.R1 - Update 2 S32 Design Studio for Power Architecture 2017.R1 - Update 1 S32 Design Studio for Power v1.2 (Windows/Linux)   S32 Design Studio for Power v1.2 - Update 3 S32 Design Studio for Power v1.2 - Update 2 S32 Design Studio for Power v1.2 - Update 1 S32 Design Studio for Power v1.1 (Windows, Linux)  S32 Design Studio for Power v1.1 - Update 1 S32 Design Studio for Power v1.0 (Windows)    Other Hot Fixes S32 Design Studio Offline activation issue hot fix 
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1         The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Power Architecture version v2.1. It is the successor of S32 Design Studio for Power 2017.R1. - the versioning scheme has changed. Release content (What is new?) Eclipse Neon 4.6 Framework GNU Build Tools for e200 processors bld=1607 rev=gceb1328 (support VLE and BookE ISA, based on gcc 4.9.4 [1.February 2019], binutils 2.28 and gdb 7.8.2) - see the complete GCC release notes Libraries included: newlib, newlib-nano and Freescale EWL2 P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v1.7.2.201709281658) New Project wizards to create application and library projects and projects from project examples for supported devices Peripherals Register and Special Purpose Registers View Fully integrated S32 SDK RTM v.3.0.0 (Windows only). For the details on the feature set of SDK please refer to SDK Release notes attached and Reference Manuals (Please note that SDK has Early Access Release status, which means that there could be some limitations and/or issues. Also note, the SDK is available for Windows host only). SDK management included: o FreeMASTER Serial Communication driver (v2.0 August 31th 2016) o Automotive Math and Motor Control Libraries(v1.1.15) o Support for importing MCAL configuration to a custom SDK o An SDK can be attached to a library project using the project wizard Windriver Diab, and GreenHills compiler support by new project wizard (The Green Hills Software (GHS) compiler support depends on the availability of the Eclipse plug-in integrating GHS compiler compatible with the Eclipse Neon. Full support for the Green Hills Software compiler Eclipse Neon-compatible plug-in within S32DS for PA 2.1 was not validated in time for this release.) Lauterbach, iSystem, and PLS debuggers support by new project wizard (The plugins to support Diab, iSystem, Lauterbach, and GreenHills are not included and have to be installed from the corresponding update site or installation.) Kernel Aware debugging for FreeRTOS, eCOS, OSEK Devices supported: S32R274 S32R372 MPC5775B, MPC5775E MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5744B, MPC5745B, MPC5746B, MPC5744C, MPC5745C, MPC5746C MPC5744P, MPC5743P, MPC5742P, MPC5741P MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A, MPC5642A MPC5643L MPC5676R MPC5632M, MPC5633M, MPC5634M MPC5674F MPC5673K, MPC5674K, MPC5675K Collateral Getting Started page The S32DS Extensions and Updates tool Migration guide to help migrate projects from an earlier version to S32 Design Studio for Power Architecture 2. Bug Fixes For detailed list of the GNU Tools bug fixes, refer to the release notes located in S32DS/ build_tools/powerpc-eabivle-4_9/ Fixed the semihosting issues with the EWL and NewLib libraries Fixed the FLASH programming algorithm for MPC5744P Added missing linker script sections for MPC5748G Fixed reading values from the peripheral bridge A registers for MPC5634M Fixed access to the RAM memory for MPC5634M Removed unavailable addresses from the MPC574xB linker files Added the -fstrict-volatile-bitfield compiler option to the project settings Fixed secure connection to MPC5744P Disabled RTTI for EWL library due to incompatibility with the GNU tools Fixed importing/exporting projectinfo.xml with library settings Complete S32 Design Studio for Power Architecture v2.1 release notes are available here Installation Notes To download the installer please visit the S32DS for Power Architecture product page: downloads section. The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the installer downloading process: Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space: https://community.nxp.com/community/s32/s32ds    
查看全文
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe 2. Download and Install S32 Design Studio 3.5 Update 2 D2302: SW32_S32DS_3.5.2_D2302.zip  (com.nxp.s32ds.update_3.5.2.20230227110156)   3. Click S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio Download and Install S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices(3.5.0_D2303): SW32K3xx_S32DS_3.5.0_D2303.zip  (com.nxp.s32ds.sp1.s32k3xx.update_3.5.0.20230405175452)   4. For users who need to install S32K396 RTD for development, please download and install S32 Design Studio Service Pack 1 RTM with support for S32K39x devices(3.5.0_D2303): SW32K39x_S32DS_3.5.0_D2303.zip (com.nxp.s32ds.sp1.s32k396.update_3.5.0.20230330)   5.a) For users who need to install S32M276 RTD in S32K3 RTD 3.0.0\P01\P01 HF01\P01 HF02 for development, please download and install S32 Design Studio Service Pack 2 CD with support for S32M2xx devices (3.5.0_D2302😞 SW32M2xx_S32DS_3.5.0_D2302.zip(com.nxp.s32ds.s32m2.update_3.5.0.20230222151347)  Note: Please contact your local FAE to enable for you download the S32M276 development package. 5.b) For users who need to install S32M276 RTD in S32K3 RTD 3.0.0 P07 for development, , please download and install S32 Design Studio Service Pack 2 EAR2 with support for S32M2xx devices(3.5.0_D2303😞 SW32M2xx_S32DS_3.5.0_D2303.zip(com.nxp.s32ds.s32m2.update_3.5.0.20230328160305)   6. S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M Select and install one of the following updatesite for S32K3 RTD 3.0.0: 6.a) Download and install S32K3 Real-Time Drivers Version 3.0.0: SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip   6.b) Download and install S32K3 Real-Time Drivers Version 3.0.0 P01 : SW32K3_RTD_4.4_3.0.0_P01_D2303_DS_updatesite.zip   6.c) Download and install S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 (3.0.0_P01_HF02😞 SW32K3_RTD_4.4_3.0.0_P01_HF02_DS_updatesite_D2305.zip   6.d) Download and install S32K3_M27X Real-Time Drivers Version 3.0.0 P07: SW32K3_RTD_R21-11_3.0.0 _P07_D2307.zip  
查看全文
Sometimes you need an output file other than the standard ELF, like a FLASH image. This instruction shows how to setup the selected build type to generate an additional output from the supported file types.   Go to Project Properties Right click on the Project name in Project Explorer -> Properties, OR Select the Project name in Project Explorer, select from pulldown menu Project -> Properties Navigate to C/C++ Build -> Settings -> Cross Settings, check the box for ‘Create flash image’. Be sure to take note that the build configuration set in the Configuration field is correct one. The change you make here will only apply to the selected configuration. Scroll the window down until you can see the ‘Apply’ button, then click on it. You can specify output in newly appeared option Standard S32DS Create flash image Build the project. The new output file is generated.
查看全文
Included in the S32DS for ARM is a set of example projects, which include one called 'hello'. This example shows a basic application which activates an LED when a button is pressed on the S32K144EVB-Q100 evaluation board. The S32K SDK is not used in this example. In this HOWTO, we will show how to load the project into the workspace, build, download to the target, and run debug. 1. Create Project a. File -> New -> New S32DS Project from Example   OR from the Dashboard b. Select S32DS Example Projects -> S32K144 -> hello 2. Examine the code a. Locate the project in C/C++ Projects view b. Expand 'hello', then 'src' c. Double-click on 'hello.c', to open the file in the editor 3. Build the project a. Click to select hello project, this is to ensure that the tool knows which project you wish to build. b. Click Build button. By default, the standard 'Debug' build configuration will be used. Projects created using either the New S32DS Project from Example, or New S32DS Project wizard are setup with 3 build configurations: Debug, Debug_RAM, and Release. The 'Debug' configuration contains settings to build the project with the lowest compiler optimization setting and to occupy the Flash memory space on the target. The 'Debug_RAM' configuration is very similar to the 'Debug' configuration with one exception. It is set to occupy the RAM memory space on the target. The 'Release' configuration will build the project with the highest optimization setting and to occupy the Flash memory space on the target. c. From the console tab, the build status output is displayed. Check here to confirm the build completed and there were no errors. 4. Setup Debug Configuration a. Click Run -> Debug Configurations… OR from the Debug button menu b. Expand the 'GDB PEMicro Interface Debugging' group. c. Select the configuration which matches the build configuration you just used to build the project. For each build configuration generated by the new project wizard, it also generates a matching debug configuration. d. Select the Debugger tab. The debug configuration was created with the 'PE Micro GDB server' option selected, but there are several hardware options for this. Select the option which matches your hardware setup. For example, for the S32K144, most likely you have the standard evaluation board, which has OpenSDA integrated. In this case, you would use the OpenSDA interface option. For other MCUs, you may have hardware which requires the USB Multilink or Cyclone. e. Click Refresh to ensure the correct port is selected. 5. Click Debug to start the debugger launch sequence. It is not necessary to click on the 'Apply' button unless setting changes are being made without intention to launch the debugger. The scripts behind the Debug button include the actions of the script behind the Apply button. 6. When the launch sequence completes, the application is executed until the start of main(), where a breakpoint was automatically set. 7. It is now possible to run or step through the code, view variables and registers. 8. Click Resume and when Button 0 is pressed, the LED will turn on as Blue, and when Button 0 is released, the LED turns off. 9. To end the debug session, click the 'Terminate' button. It is a good idea to also click on 'Remove All Terminated Launches', before starting another debug session.
查看全文
This document describes how to link a binary file(s) with an existing project in S32 Design Studio using GCC build tools. Let's demonstrate this on S32K144 project in S32DS for ARM. Nevertheless it should work with any other GCC based development tools. The first step is to add the binary file(s) into your project folder in the workspace. In the example below I created two binary files "my_bin.bin" and "my_bin2.bin" and added them into a custom folder "bin_files". I also entered 10 characters into each file. my_bin.bin: 0x41 0x41 0x41 0x41 0x41 0x41 0x41 0x41 0x41 0x41  (represents 10 characters "A") my_bin2.bin: 0x42 0x42 0x42 0x42 0x42 0x42 0x42 0x42 0x42 0x42  (represents 10 characters "B") The next step is to modify the linker configuration file (.ld) in order to specify input file format and path to the binary files (see the line 14-17) /* Specify the memory areas */ MEMORY { /* Flash */ m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400 m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010 m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0 /* SRAM_L */ m_data (RW) : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000 /* SRAM_U */ m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00007000 } TARGET(binary) /* specify the file format of binary file */ INPUT (..\bin_files\my_bin.bin) /* first bin file path (relative to the output folder)*/ INPUT (..\bin_files\my_bin2.bin) /* second bin file path (relative to the output folder)*/ OUTPUT_FORMAT(default) /* restore the out file format */ /* Define output sections */ SECTIONS { ... ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Finally, in the SECTIONS block of .ld file specify where to place the binary files (in the example it is placed at the end of .text section - see the line 37,38). /* Define output sections */ SECTIONS { /* The startup code goes first into internal flash */ .interrupts : { __VECTOR_TABLE = .; __interrupts_start__ = .; . = ALIGN(4); KEEP(*(.isr_vector)) /* Startup code */ __interrupts_end__ = .; . = ALIGN(4); } > m_interrupts .flash_config : { . = ALIGN(4); KEEP(*(.FlashConfig)) /* Flash Configuration Field (FCF) */ . = ALIGN(4); }> m_flash_config /* The program code and other data goes into internal flash */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ *(.text*) /* .text* sections (code) */ *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); ..\bin_files\my_bin.bin /* First binary file */ ..\bin_files\my_bin2.bin /* Second binary file */ } > m_text ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ After successful compilation and link let's check map and s-record file (HOWTO: Generate S-Record/Intel HEX/Binary file ) to confirm the binary files have been linked correctly: .glue_7t 0x0000080c 0x0 linker stubs *(.eh_frame) *(.init) *(.fini) 0x0000080c . = ALIGN (0x4) ..\bin_files\my_bin.bin() .data 0x0000080c 0xa ..\bin_files\my_bin.bin 0x0000080c _binary____bin_files_my_bin_bin_start 0x00000816 _binary____bin_files_my_bin_bin_end ..\bin_files\my_bin2.bin() .data 0x00000816 0xa ..\bin_files\my_bin2.bin 0x00000816 _binary____bin_files_my_bin2_bin_start 0x00000820 _binary____bin_files_my_bin2_bin_end .vfp11_veneer 0x00000820 0x0 .vfp11_veneer 0x00000820 0x0 linker stubs‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ If you need a reference to the binary file block start/end address in your code you can use the linker symbols generated automatically or you can define your own symbols in the linker script. /* declare symbols from linker script file */ extern unsigned int _binary____bin_files_my_bin_bin_start; extern unsigned int _binary____bin_files_my_bin_bin_end; int main(void) { #define COUNTER_LIMIT 100 unsigned int counter = 0; unsigned int * bin_start_ptr; unsigned int * bin_end_ptr; bin_start_ptr = &_binary____bin_files_my_bin_bin_start; bin_end_ptr = &_binary____bin_files_my_bin_bin_end; for(;;) { counter++; counter = *(bin_start_ptr); /*loads 0x4141_4141 into counter*/ if(counter > COUNTER_LIMIT) { counter = 0; } } return 0; }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note: if it is intended to place the binary file at specific absolute address (e.g. if binary file that represent bootloader) you have to create a separate custom MEMORY and SECTION block in .ld file. /* Specify the memory areas */ MEMORY { /* Flash */ m_bootloader (RX) : ORIGIN = 0x001000, LENGTH = 0x00010000 /* section for bootloadeer*/ m_text (RX) : ORIGIN = 0x00011000, LENGTH = 0x0040000 /*section for application code*/ ... } TARGET(binary) /* specify the file format of binary file */ INPUT (..\bin_files\my_booloader.bin) /* bootloader bin file path (relative to the output folder)*/ OUTPUT_FORMAT(default) /* restore the out file format */ /* Define output sections */ SECTIONS { /* place the bootloader binary into 0x0..0x10000 */ .bootloader : { ..\binary_files\my_bootloader.bin /* place the binary file here */ } > m_bootloader ... ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Enjoy linking binaries in S32 Design Studio!
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1         The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Power Architecture version 2017.R1. It is the successor of S32 Design Studio for Power v1.2. - the versioning scheme has changed. Release content (What is new?) Eclipse Neon 4.6 Framework GNU Build Tools for e200 processors (support VLE and BookE ISA, based on gcc 4.9.4 [7.October 2017], binutils 2.28 and gdb 7.8.2) - see the complete GCC release notes Libraries included: newlib, newlib-nano and Freescale EWL2 P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v1.7.2.201709281658) New Project wizard to create application and library projects for supported devices Peripherals Register and Special Purpose Registers View Fully integrated MPC5748G/MPC5746C SDK EAR v.0.8.1. For the details on the feature set of SDK please refer to SDK Release notes attached and Reference Manuals (Please note that SDK has Early Access Release status, which means that there could be some limitations and/or issues. Also note, the SDK is available for Windows host only). SDK management included: o FreeMASTER Serial Communication driver (v2.0 August 31th 2016) o Automotive Math and Motor Control Libraries(v1.1.9) Windriver Diab compiler support by new project wizard Lauterbach, iSystem, and PLS debuggers support by new project wizard (The plugins to support Diab, iSystem, Lauterbach are not included and have to be installed from the corresponding update site or installation. The current version of the GreenHills plugin is not compatible with Eclipse Neon version, so it should not be used with this release) Kernel Aware debugging for FreeRTOS, eCOS, OSEK Devices supported: S32R274 S32R372 MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5744B, MPC5745B, MPC5746B, MPC5744C, MPC5745C, MPC5746C MPC5744P, MPC5743P, MPC5742P, MPC5741P MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A, MPC5642A MPC5643L MPC5676R MPC5632M, MPC5633M, MPC5634M MPC5674F MPC5673K, MPC5674K, MPC5675K Collateral Getting Started page Bug Fixes C preprocessor tool added for C++ projects configuration The makefile generation is updated to fix and issue with building a project on the Korean version of Windows - Code page switch command cannot be executed. The Rename Project functionality is improved to cover referenced projects and launch configurations Complete S32 Design Studio for Power Architecture 2017.R1 release notes are available here Installation Notes To download the installer please visit the S32DS for Power Architecture product page: downloads section. The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the installer downloading process: Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space: https://community.nxp.com/community/s32/s32ds    
查看全文
S32 Design Studio (S32DS) supports Wind River Eclipse plug-in which integrates Wind River Diab tool chain for e200 (PowerPC architecture) into Eclipse IDE. S32DS integration by a new project wizard that allows to create a new project with Wind River Diab build tools. The generated executable can be then debugged by any supported debugger plug-in (PEMicro, iSystem, PLS, Lauterbach) S32 Design Studio versions that support Wind River Diab plugin: S32DS Power v1.1+   Installation instructions First of all make sure you have Wind River Diab tools installed on your machine.  You can start with Wind River Diab Compiler 5.9.6 Evaluation  Anyway, after your evaluation period expires you need a valid license from Wind River to be able to use this plug-in in S32DS. The plug-in is available with the Diab compiler and it's located here: "<WindRiver home folder>\compilers\eclipse_cdt"   1. Run S32 Design Studio and go to menu "Help" -> "Install New Software" and  click on "Add..." button. Enter the local location to the folder above. 2. select the "Diab Compiler Support for Eclipse C/C++ IDE " and click "Next"   3. Read and Tick " I Accept the terms of the license agreement" and agree with installation of the unsigned content. 4. When the plug-in is successfully installed you will be asked to restart S32DS.     5. Set the path to the Diab compiler for your workspace (S32DS_DIAB_PATH environment variable) in the Window->Preferences->C/C++->Build->Build Variables (Show System Variables). If you switch the workspace you will need to enter this path again. Now you should be able to create a new project with Wind River Diab toolchain available: The created project includes Diab specific files such as "dld", startup code as well as tools specific setup in the project properties (Project Properties->C/C++ Build->Settings (Tools Settings Tab)    Enjoy building with Wind River Diab plug-in in S32DS!
查看全文
Hello,   The new official release of S32DS for ARM v1.2 is available in the download section of S32DS web page: http://www.nxp.com/s32ds       To  install the product the Activation Code is needed. You can Find it under "License keys" tab.   S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB), and other open-source software. This release supports Windows 7/8/8.1/10 (32/64 bit) and Linux versions as well.   S32DS ARM v1.2 main features Free of charge tool with no code size limitation (no license file required) Eclipse Luna 4.4 Framework GNU Tools for ARM embedded processors (launchpad, based on gcc 4.9.3) and ARM64: 4.9.3 20141031 Linaro Libraries included: newlib, newlib-nano and Freescale EWL2 (ewl and ewl-nano) SEGGER J-Link (with SEGGER GDB Server), P&E Multilink (with P&E GDB Server) Fully integrated S32 SDK for S32K144 EAR release v.0.8.1 SDK management included (KEA drivers, FreeMASTER for KEA, AMMCLIB for KEA and S32K) CodeWarrior/KDS project importer GreenHills/IAR compiler support by the new Project Wizard iSystem/Lauterbach debuggers support by the new Project Wizard Kernel Aware Debugging FreeRTOS, OSEK. Devices supported SKEAZN8, SKEAZN16, SKEAZN32, SKEAZN64, SKEAZ128, SKEAZ64 S32K144 S32V234 MAC57D54H   Technical Support S32 Design Studio is supported by NXP community - https://community.freescale.com/community/s32/s32ds/ For more details see the attached release notes.     * Red items are the new features   Regards, Stanislav  
查看全文
     This summary records my process of using J-LINK Plus in S32 Design Studio for S32 Platform, hoping to help people who use the same tool.   1.Download the latest package: https://www.segger.com/downloads/jlink/   2.Install the downloaded package and some note will show like this.   3.Open J-Link GDB Server V7.8 , if you current firmware version is too low, you will be prompted to upgrade to the latest firmware version.       At this point ,if you use the default configuration to debug the application, the following error will appear.   Modified the "Debug configurations" for S32 Design Studio platform V3.4   Change the highlighted part to the path below. C:\Program Files (x86)\SEGGER\JLink\JLinkGDBServerCL.exe C:\NXP\S32DS.3.4\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb.exe   Modified the "Debug configurations" for S32 Design Studio platform V3.5 Change the highlight part to the path below. C:\Program Files (x86)\SEGGER\JLink\JLinkGDBServerCL.exe C:\NXP\S32DS.3.5\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb.exe   For now, you may debug your project with SEGGER J-Link Plus Tools. Hope it works for you!
查看全文
There are situations that require debugging multiple executable files within one debug session. Typical example is debugging the bootloader + application together where each one is a separate executable elf file or S32DS eclipse project. S32DS project loads the debug information of the generated executable file by default. Anyway GDB supports command to add additional elf files debug information into same debug session. If the executable source files are present on the same machine then the source level debugging of all the elf files is possible. Let's assume there are two elf files (bootloader and application) and both are built with debug information enabled - build configuration is named "Debug". Generation of the debug information for GCC compiler could be set in the Project Properties -> C/C++ Build -> Settings -> Standard  S32DS C Compiler -> Debug Level  Each debug configuration in S32 Design Studio supports loading or ignoring debug information. "Load symbols" loads just the debug information whereas "Load executable" basically loads program/code/data sections into MCU memory without debug information. Both options are enabled by default. Before starting the debugger it's necessary to load both executable files into your MCU memory. This could be easily achieved in S32DS (GDB) debug configuration where you specify to add the additional object files. In this specific case we need just 1 additional file - bootloader elf. The bootloader project in this example is actually another project in the same workspace (workspace relative path to elf file entered). After starting debugger the Debugger Console view now shows the details about programming of two elf files instead of one including load address of each section. When loading is finished the debug information for bootloader is not yet available ("No source available..." message displayed in the source level debug view) In order to display source and symbols for the bootloader elf please enter "add-symbol-file"  GDB command into Debugger Console View: add-symbol-file "C:/Users/NXA21306/workspaceS32DS.ARM.2018.R1/s32K144_Bootloader/Debug/s32K144_Bootloader.elf" 0x0000000‍‍‍‍‍ The GDB client command could be executed automatically when launching a debug session: The first argument is path to the elf file and the second argument (0x00000000) is the load address of the elf file (see the first bootloader load address ). Finally the debug session needs to be refreshed in order to display changes from just added symbol file. The refresh can be forced by performing a single step or issuing the target reset from the debugger.
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power v1.2             S32 Design Studio for Power v1.2 (Windows/Linux) has been released. This is a complete installer which does not require any previous version to be installed. To download the installer please visit download section: www.nxp.com/s32ds What is new? New devices: • MPC5632M, MPC5633M, MPC5634M • MPC5642A • MPC5674F • MPC5673K, MPC5674K, MPC5675K • S32R372 New features: • Compiler update – see details in compiler release notes attached below • View for the Special Purpose Registers added • Improvements for Peripherals Register view • Added support for Semihosting/Debug console for single core devices • RESET functionality added, the hardware reset2 is executed for main/boot core and individual core reset for secondary cores. • Improvements for SPT diagram to display instruction labels and key parameters • SDK mechanism improvements to support SDK per build configuration • FreeMaster Serial Communication driver 2.0 integrated • iSystem debugger support added to New Project Wizard • SPT assembler update • Updated P&E debug plugins and drivers to the latest and greatest versions Note: The plugins to support GreenHills, IAR, iSystem, Lauterbach are not included and have to be installed from corresponding update site or installation. S32DS release notes are available here. GCC Build tools release notes are here.   Installation Notes The installer requires NEW Activation ID to be entered during the installation. You should receive an email including the Activation ID after starting the download process e.g:    
查看全文
Introduction In this document, we will discuss the S32DS Extensions & Updates tool and how to use it to install the device support you need.   S32 Design Studio for S32 Platform has been designed to allow users to customize their installation, enabling them to integrate support for just the NXP devices they need and just the tools they need. With the new modular design, parts of the tool have been moved into one of 4 different package types. The Platform and Tools Packages are default packages which are included as part of the base install, cannot be uninstalled, however, they can be updated.   The Platform package contains the base components of the IDE, modular installer, general documentation and integration mechanisms. The Tools Package contains the compilers, debuggers, and MSYS2. The Development Package contains hardware specific support such as New Project Wizard, S32 Configuration Tools, SDKs and Libraries. The Extension Package contains Accelerator Compiler, Debugger, Graph Tool and advanced SDKs.   Downloading the various components from our cloud-based update server, allows you to assemble and complete the customized installation of the tools and software to meet your development needs. It is also via the update server that the updates and bug fixes will be provided. And of course, all of these will be available as downloads from our product page for users who are installing to an offline PC. S32DS Extensions and Updates Menu When you first launch the S32 Design Studio for S32 Platform, you are presented with the S32DS Extensions and Updates menu. This menu provides a listing of the add-on packages which have been installed, those that are available to be installed, and those which have updates available to be installed. In the panel to the right is displayed detailed information specific to the package which is selected in the panel to the left. If there is an update available for the selected package, the currently installed version number will be shown on the left and the update version number will be shown on the right.       Online Package Installation Setup If your PC is connected to the internet, then it will link to NXP's update server (http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_3.5) and any new or updated packages will be automatically added to the list. See Package Installation section below for installation procedure and details.       Offline Package Installation Setup If your PC is not connected to the internet, you must first download the desired packages from the NXP website, in the form of an archive file, to a separate PC and have them transferred to your target PC. Then you would select the link 'Go to Preferences' and add each downloaded archive file as a separate software site. After selecting OK, you will see the new packages contained within the archive files listed.   Procedure: Go to S32 Design Studio for S32 Platformdownload page and select Download for the package or update you need. Once the file is downloaded, it must be installed within S32 Design Studio. Launch S32DS and wait for the S32DS Extensions and Updates window to appear. Then select the 'Manage Sites' link. The Preferences window appears. Select the 'Add...' button to add a new software site to the list. The file you downloaded will be a software site. Now the Add Site window appears. Since the downloaded file is an archive of type ZIP, the 'Archive...' button should be used to select it. Navigate to the location where the file was saved. Now the downloaded file has been added as a new site. Select OK to return to the main S32DS Extensions and Updates window. Now the new package(s) will appear in the S32DS Extensions and Updates window, just as it would from the update server. See Package Installation section below for installation procedure and details.   Package Installation To install the new packages or updates, check the box to the left of the desired package in the left panel and select 'Install/Update'. The tool will automatically detect any dependencies on other packages and select them to meet all requirements for the installation.     Follow the prompts and the packages will be installed, followed by a request to restart S32 Design Studio.     Dependencies and Errors If there are dependencies between two or more updates, the tool will detect this and inform you of the package which cannot yet be installed. If you try to install a package which is not compatible with the version of S32 Design Studio you have installed, a notice will appear, and the package will not be listed in the S32DS Extensions and Updates menu.   Uninstalling Unwanted Packages If you no longer need a particular package or installed one by mistake, just check the box next to the package and select 'Uninstall'.       Reinstalling Packages If you believe your installed package has become corrupted, if you accidentally deleted part of it (such as an example project, etc.), or if for any reason you need to restore the package, just check the box next to the package and select 'Reinstall'.   Additional Information If you wish to not see the S32DS Extensions and Updates menu at startup, you can uncheck the box at the lower left. For internet connected PCs, the update server will still be linked and checked for new packages at S32DS startup, but you will no longer see the S32DS Extensions and Updates menu. However, you will still see a notice at the lower right of the tool at startup when new packages are detected.      
查看全文
******************************************************************************** * Detailed Description: * This example shows, how to use printf function in project. * Files uart_console_io.c, uart.c and uart.h was added. These files contain * necessary functions for correct printf() functionality * * * Test HW:         FRDMPK144-Q100 * MCU:             PS32K144HFVLL 0N77P * Terminal:        9600-8-no parity-1 stop bit-no flow control on LPUART1 * Fsys:            160 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS *                  OpenSDA embedded debug * Target:          internal_FLASH, internal RAM * EVB connection:  default
查看全文
There are 2 errors which produce the FNP error 0 message for which we have identified solutions:   1) That activation request yields no right to a license If you receive the following error message following an attempt to activate S32 Design Studio, this is a known issue and we have a solution.     This issue is due to a recent event. On October 1st, 2019, Flexera made this change. Since NXP uses Flexera for product activations, we were affected.   The solution to the issue is to enable support for TLS 1.2 within your Internet Properties.   2) com.acresso.activation.handler.ServerException If you receive the following error message following an attempt to activate S32 Design Studio, this is a known issue and we have a solution. This issue is known to occur on older releases of S32 Design Studio.     The version of FlexNet Publisher (FNP) used to activate the S32 Design Studio on your PC has an issue on some users machines. While we don't fully understand what change is happening to cause this issue, we have determined that an update to the version of FNP will resolve it. We have incorporated a newer version in the 3.5 release of S32 Design Studio.   Attached is a package of files (Activation.7z) which will allow you to update the version of FNP on your machine.   Enter the following command replacing the paths as noted. It should be possible to execute from CMD window located at any path. Make sure to use the ‘/’ instead of ‘\’ and if you have any paths with spaces, then enclose the full path with “.   For 64-bit OS: C:/NXP/S32DS.3.5/jre/bin/java  -Djava.library.path="{path to where you extracted the activation.zip}/Activation/cll/x64"  -jar "{path to where you extracted the activation.zip}/Activation/license.jar" activateUI   For 32-bit OS: C:/NXP/S32DS.3.5/jre/bin/java -Djava.library.path="{path to where you extracted the activation.zip}/Activation/cll/i86" -jar "{path to where you extracted the activation.zip}/Activation/license.jar" activateUI   If you have no existing S32DS installation from which to use Java, then please use the attached package (CLL_FNP.11.18.0.2.zip) and follow the instructions in the included .txt file. This package only works on Windows OS 64-bit.
查看全文
This document describes two ways how to add a static library file (*.a) into your S32 Design Studio GCC project. These methods differs from each other in sense how a library update is reflected into project build process. Adding a static library WITHOUT dependency to executable (elf) file This approach assumes a library does not change. An update of the library does not trigger project rebuild process. If the library changes the project needs to be manually cleaned (assuming no other source file has changed) and next build links the updated library. The path to the library and the library name shall be entered into Project Properties -> C/C++ Build -> Settings -> Standard S32DS C Linker -> Libraries Please note that GCC adds prefix "lib" and the extension ".a"  to the library name entered into the above dialog by default. GCC linker will search for the library file named: "libtestlib.a" in the folder "c:\my_libs" In the example above. In case a library cannot be found the linker error occurs e.g. one depicted below. The linker library file name option "-ltestlib.a" is expanded into file name "libtestlib.a.a" which does not exist. 10:28:53 **** Incremental Build of configuration Debug for project S32K144_Project_with_library **** make -j8 all Building target: S32K144_Project_with_library.elf Executing target #5 S32K144_Project_with_library.elf Invoking: Standard S32DS C Linker arm-none-eabi-gcc -o "S32K144_Project_with_library.elf" "@S32K144_Project_with_library.args" c:/nxp/s32ds_arm_v2.0/cross_tools/gcc-arm-none-eabi-4_9/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -ltestlib.a collect2.exe: error: ld returned 1 exit status make: *** [makefile:49: S32K144_Project_with_library.elf] Error 1 10:28:54 Build Finished (took 1s.332ms)‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ For a custom library name add colon character ":" at the beginning of the library name to disable the default prefix/extension expansion. GCC linker now searches for file name "testlib.lib" in the example below:   Adding a static library WITH dependency to executable (elf) file If a static library has changed - "touched"  it is sometimes desired to trigger project rebuild. In this scenario the library shall be added into a different project dialog: Project Properties -> C/C++ Build -> Settings -> Standard S32DS C Linker -> Miscellaneous -> Other objects The items from "Other objects" list is propagated into USER_OBJS makefile variable which is prerequisite for auto-generated makefile rule that build the target (elf): Enjoy linking static libraries in S32DS!
查看全文