S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released!

cancel
Showing results for 
Search instead for 
Did you mean: 

S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released!

No ratings

S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released!

 

 

 

nxp.png 

Product Release Announcement

Automotive Microcontrollers and Processors

S32 Design Studio for Power Architecture

2017.R1

S32DS_Logo_official_2016_scaled.png

 

 

 

 

The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Power Architecture version 2017.R1.

It is the successor of S32 Design Studio for Power v1.2. - the versioning scheme has changed.

Release content (What is new?)

  • Eclipse Neon 4.6 Framework
  • GNU Build Tools for e200 processors (support VLE and BookE ISA, based on gcc 4.9.4 [7.October 2017], binutils 2.28 and gdb 7.8.2) - see the complete GCC release notes
  • Libraries included: newlib, newlib-nano and Freescale EWL2
  • P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v1.7.2.201709281658)
  • New Project wizard to create application and library projects for supported devices
  • Peripherals Register and Special Purpose Registers View
  • Fully integrated MPC5748G/MPC5746C SDK EAR v.0.8.1. For the details on the feature set of SDK please refer to SDK Release notes attached and Reference Manuals (Please note that SDK has Early Access Release status, which means that there could be some limitations and/or issues. Also note, the SDK is available for Windows host only).
  • SDK management included:

o FreeMASTER Serial Communication driver (v2.0 August 31th 2016)

o Automotive Math and Motor Control Libraries(v1.1.9)

  • Windriver Diab compiler support by new project wizard
  • Lauterbach, iSystem, and PLS debuggers support by new project wizard (The plugins to support Diab, iSystem, Lauterbach are not included and have to be installed from the corresponding update site or installation. The current version of the GreenHills plugin is not compatible with Eclipse Neon version, so it should not be used with this release)
  • Kernel Aware debugging for FreeRTOS, eCOS, OSEK
  • Devices supported:
    • S32R274
    • S32R372
    • MPC5775K, MPC5774K
    • MPC5746R, MPC5745R, MPC5743R
    • MPC5777M
    • MPC5777C
    • MPC5748G, MPC5747G, MPC5746G
    • MPC5744B, MPC5745B, MPC5746B, MPC5744C, MPC5745C, MPC5746C
    • MPC5744P, MPC5743P, MPC5742P, MPC5741P
    • MPC5601P, MPC5602P, MPC5603P, MPC5604P
    • MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C
    • MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B
    • MPC5606S
    • MPC5604E
    • MPC5644A, MPC5642A
    • MPC5643L
    • MPC5676R
    • MPC5632M, MPC5633M, MPC5634M
    • MPC5674F
    • MPC5673K, MPC5674K, MPC5675K
  • Collateral Getting Started pagepastedImage_25.png

Bug Fixes

  • C preprocessor tool added for C++ projects configuration
  • The makefile generation is updated to fix and issue with building a project on the Korean version of Windows - Code page switch command cannot be executed.
  • The Rename Project functionality is improved to cover referenced projects and launch configurations

Complete S32 Design Studio for Power Architecture 2017.R1 release notes are available here

Installation Notes

To download the installer please visit the S32DS for Power Architecture product page: downloads section.

The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the installer downloading process:

pastedImage_7.png

Technical Support

S32 Design Studio issues are tracked through the S32DS Public NXP Community space:

https://community.nxp.com/community/s32/s32ds

 

 

Labels (1)
Attachments
Comments

Hello,

Do I need to install this new version ? 

Doesn't it has patches , so that When I run CHeck for Updates in s32 v1.2 , I get the latest version as well ?

Thanks

Vrushali

Hello,

The latest version release 2017.R1 includes the new version of Eclipse IDE (neon) - it is not possible to update it via eclipse updater.

Therefore there is no a patch to v1.2 available.

Anyway you can have multiple installations of S32DS installed on your computer - they will work simultaneously.

Hope it helps,

Stan

GCC source code? For a company so concerned with licensing and letting lawyers dictate what we are allowed to see (even when the community could help) you have a habit of glossing over the important bits of other licenses.https://www.gnu.org/licenses/gpl-violation.en.html" title="https://www.gnu.org/licenses/gpl-violatio...

Why open yourself up to litigation over something so trivial? Violations of the GNU Licenses- GNU Project - Free Software Foundation 

GNU GENERAL PUBLIC LICENSE

Our General Public Licenses are designed to make sure that you have the freedom to distribute copies of free software (and charge for them if you wish), that you receive source code or can get it if you want it, that you can change the software or use pieces of it in new free programs, and that you know you can do these things.

For example, if you distribute copies of such a program, whether gratis or for a fee, you must pass on to the recipients the same freedoms that you received. You must make sure that they, too, receive or can get the source code. And you must show them these terms so they know their rights.

1. Source Code.

The “Corresponding Source” for a work in object code form means all the source code needed to generate, install, and (for an executable work) run the object code and to modify the work, including scripts to control those activities. However, it does not include the work's System Libraries, or general-purpose tools or generally available free programs which are used unmodified in performing those activities but which are not part of the work. For example, Corresponding Source includes interface definition files associated with source files for the work, and the source code for shared libraries and dynamically linked subprograms that the work is specifically designed to require, such as by intimate data communication or control flow between those subprograms and other parts of the work.

- Full body of the GPLv3: https://www.gnu.org/licenses/gpl-3.0.en.html

Hello Jed,

Thanks for pointing us to this issue.

I'd like to ensure you we do respect our GNU licensing obligations seriously.

The delay between release the binary and GCC source package wasn't intended and does not mean we are trying to bypass these obligations in any sense.

This was caused purely by a human factor.

Therefore I've escalated the issue to appropriate team to prevent this kind of issues in a future releases.

The GCC Source package is now available for download:

https://www.nxp.com/lgfiles/updates/S32DS/S32DS_PA_2017.R1_GCC.tar 

pastedImage_1.png

Thank you for your valuable comments on nxp community!

Stan

Therefore I've escalated the issue to appropriate team to prevent this kind of issues in a future releases.

Thank you.

Version history
Revision #:
1 of 1
Last update:
‎10-31-2017 09:10 AM
Updated by: