NFC Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Knowledge Base

Discussions

Sort by:
As NFC reader library 5.12 also supports PN5180, switching the NFC frontend from CLRC663 to PN5180 is quite easy based on previous porting. The porting also includes the hardware settings and software modification. Hardware Setup for porting: a) Remove resistors on PNEV5180B to disconnect the onboard lpc1769 from PN5180, following steps on page 16 of https://www.nxp.com/docs/en/application-note/AN11908.pdf  b) Connect LPCXpresso board for LPC11U37 with PNEV5180 as below: Software Modification for porting: 1. Make a copy of Board_Lpc11u37Rc663.h , and change its name to "Board_Lpc11u37Pn5180.h", and import it into the DAL/boards folder. 2.Change the source code in the header file as below: 3. Add two more pins' definition and configuration for BUSY and DWL pins of PN5180, and new configuration for reset pin. and modify the reset logic: 4.Change the IRQ interrupt trigger type to rising edge. 5.Include this header file in BoardSelection.h 6.Add this new configuration in ph_NxpBuild_App.h 7.Add this new configuration in phApp_Init.h 8.Add this new configuration in ph_NxpBuild_Platform.h 9.Add this new configuration in Settings. 10.Building result: Testing result:
View full article
This document provides a step by step guide of how to use the CLRC663 plus with i.MX RT1050. For this purpose, we need to port the NFC Reader Library to i.MX RT1050.  There are two zip files attached to this document: 1. "NFCReaderLibrary_IMXRT1050_Porting Guide +DAL_IMXRT1050_BLE-NFC-V2.zip" : This folder is pre-configured for those who want to use BLE-NFC-v2 board with i.MX RT1050. 2. "NFCReaderLibrary_IMXRT1050_Porting Guide +DAL_IMXRT1050_CLEV6630B.zip" : This folder is pre-configured for those who want to use CLEV6630B board with i.MX RT1050. A video describing how to use i.MX RT1050 with CLRC663 Plus Family is available by clicking this link (Using i.MX RT 1050 with CLRC663 plus family |NXP ) as well. 
View full article
This post provides guidance on how to port the example projects from the NXP NCI 2.0 NFC library to the MCXW71 Wireless MCU using SPI interface to communicate with PN7160 SPI EVK. To follow this guide, please use the following environment: MCUXpresso IDE 25.06.136. FRDM-MCXW71 SDK v25.12.00 (last available for MCUXpresso IDE). FRDM-MCXW71. OM27160B1 (PN7160 SPI EVK). Hardware Setup. The MCXW71 complies with the Arduino header standard as the OM27160B1 board, therefore you can connect directly the shield over the FRDM-MCXW71 as the pin connection match among both, allowing an easy connection between the devices. Take into consideration that this setup forces us to use the LPSPI1 instance of the MCXW71, it is possible to use another instance, but we would not be able to connect the boards directly, rather we would need to do the connections with jumpers. Downloading base projects and adapting for MCXW71 port. To start with the porting work, download the NXP-NCI example project from this page. This compressed file contains the base project for different boards that will allow us to do the required modifications to add support for the MCXW71. Once downloaded, extract the SW6705 file into a known path (e.g. the Downloads folder) to later import the project to the IDE. The extracted folder should contain a .zip file with the examples that we will later import to the IDE. Download the FRDM-MCXW71's SDK from the SDK Builder page, make sure to select the 25.12.00 version, as it is the latest SDK available to use along the MCUXpresso IDE. Now we have to import the NXP-NCI2.0_MCUXpresso_examples.zip file we previously extracted to the IDE's workspace, to do so, click on the Import project(s) from file system and in the Project archive (zip) tab, browse for the extracted file of step 1 (NXP-NCI2.0_MCUXpresso_examples.zip) and click on Next >. NOTE: Don’t worry if the IDE shows an error message for not having the SDKs of the default boards (iMXRT1170, LPC55S6x, LPC82x) or having a different version, close the warning message, we only need these examples to copy the NCI library and example files. Your workspace should now look like the following image: Import the hello_world example from the FRDM-MCXW71 SDK: Add the SPI drivers to the imported project by right clicking over the project, hover the cursor over the SDK Management option and select the option Manage SDK Components: Select the driver, click Ok and if you are asked to refresh files accept it, after this you should be able to see the driver in the "drivers" folder of the project. Copy the contents of the source folder of the iMXRT1170 project, as well as the NfcLibrary folder and paste them into the imported hello_world project:          Make sure to delete the hello_world.c and hello_word.mex files as we won't need it again.             After this process your project should look like the following image: To avoid compiling issues, exclude from the build the files nfc_example_P2P.c and nfc_example_RW.c, to do so right click on the file, go to Resource Configurations and select Exclude from Build… and select for all configurations. Do this for each file. Add the preprocessor macro: BOARD_NXPNCI_INTERFACE_SPI, as this is used by the example to select the interface with the board. To do this, right-click on the project and select Properties, then drop-down the C/C++ Build option and go to the Settings tab. Here, add the macro in the Preprocessor option, click on Apply and accept the index rebuild. Add the root folder in C/C++ General > Paths and Symbols > Source Location tab, click on Ok and then Apply: Still in Paths and Symbols, go to the Includes tab and add the source, TML and tool folders from workspace, click Ok and Apply. Make sure to add them one by one. Now, go to C/C++ Build > Settings > Includes and add the following folders from Workspace. You can select all of them and add them at the same time or also do it one by one. Once done, click on Apply and Apply and Close. If you are asked to rebuild the index, do it. "${workspace_loc:/${ProjName}/source/TML}" "${workspace_loc:/${ProjName}/source/tool}" "${workspace_loc:/${ProjName}/NfcLibrary}" "${workspace_loc:/${ProjName}/NfcLibrary/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary/src}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20/src}" Source Code Changes. In the board folder, open the board.h file and add the following definitions to refer to the peripherals and clocks to be used. Please notice that you may change the LPSPI instance, however you would need to connect jumpers instead of connecting directly the shield over the FRDM. #ifdef BOARD_NXPNCI_INTERFACE_SPI #define BOARD_NXPNCI_SPI_CLOCK (CLOCK_GetIpFreq(kCLOCK_Lpspi1)) #define BOARD_NXPNCI_SPI_INSTANCE (LPSPI1) #define BOARD_NXPNCI_SPI_BAUDRATE (400000) #endif #define BOARD_NXPNCI_IRQ_PORT (GPIOC) // J2.10 - GPIO0 [PN7160] - IRQ -> J2.10 GPIOC0 [MCXW71] #define BOARD_NXPNCI_VEN_PORT (GPIOA) // J4.1 - GPIO1 [PN7160] - VEN -> J1.8 GPIOA21 [MCXW71] #define BOARD_NXPNCI_DWL_PORT (GPIOA) // J4.2 - GPIO2 [PN7160] - REQ -> J1.7 GPIOA20 [MCXW71] #define BOARD_NXPNCI_IRQ_PIN (0U) #define BOARD_NXPNCI_VEN_PIN (21U) #define BOARD_NXPNCI_DWL_PIN (20U)   Now we need to add the required clock, peripheral and pin initialization for our board. To do this, go to the hardware_init.c file inside the board folder, and overwrite the BOARD_InitHardware function with the following: void BOARD_InitHardware(void) { BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); CLOCK_SetIpSrc(kCLOCK_Lpspi1, kCLOCK_IpSrcFro192M); CLOCK_SetIpSrcDiv(kCLOCK_Lpspi1, kSCG_SysClkDivBy16); }   To add the correct pin multiplexing and configuration for our SPI and GPIO pins, go to the pin_mux.c file (also in the board folder) and overwrite the BOARD_InitPins function with the following: void BOARD_InitPins(void) { /* Clock Configuration: Peripheral clocks are enabled; module does not stall low power mode entry */ CLOCK_EnableClock(kCLOCK_GpioA); CLOCK_EnableClock(kCLOCK_GpioC); CLOCK_EnableClock(kCLOCK_PortA); CLOCK_EnableClock(kCLOCK_PortB); CLOCK_EnableClock(kCLOCK_PortC); /*IF SHORTING SH11, SH12, SH13, SH14 needed for LPSPI1*/ const port_pin_config_t portb0_pin46_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_PCS0 */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB0 (pin 46) is configured as LPSPI1_PCS0 */ PORT_SetPinConfig(PORTB, 0U, &portb0_pin46_config); const port_pin_config_t portb1_pin47_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SIN */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB1 (pin 47) is configured as LPSPI1_SIN */ PORT_SetPinConfig(PORTB, 1U, &portb1_pin47_config); const port_pin_config_t portb3_pin1_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SOUT */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB3 (pin 1) is configured as LPSPI1_SOUT */ PORT_SetPinConfig(PORTB, 3U, &portb3_pin1_config); const port_pin_config_t portb2_pin48_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SCK */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA19 (pin 14) is configured as LPSPI1_SCK */ PORT_SetPinConfig(PORTB, 2U, &portb2_pin48_config); /*IF SHORTING SH11, SH12, SH13, SH14 needed for LPSPI1*/ const port_pin_config_t irq_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTC0 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC0 (pin 37) is configured as PTC0 */ PORT_SetPinConfig(PORTC, 0U, &irq_pin); const port_pin_config_t ven_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTA20 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA20 (pin 17) is configured as PTA20 */ PORT_SetPinConfig(PORTA, 20U, &ven_pin); const port_pin_config_t req_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTA21 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA21 (pin 18) is configured as PTA21 */ PORT_SetPinConfig(PORTA, 21U, &req_pin); const port_pin_config_t portc2_pin39_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART1_RX */ (uint16_t)kPORT_MuxAlt3, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC2 (pin 39) is configured as LPUART1_RX */ PORT_SetPinConfig(PORTC, 2U, &portc2_pin39_config); const port_pin_config_t portc3_pin40_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART1_TX */ (uint16_t)kPORT_MuxAlt3, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC3 (pin 40) is configured as LPUART1_TX */ PORT_SetPinConfig(PORTC, 3U, &portc3_pin40_config); }   To add the required interfacing APIs specific of our chip, we need to modify the tml.c file from the TML folder, in this file overwrite the functions: INTF_INIT, INTF_WRITE and INTF_READ with the following: static void INTF_INIT(void) { lpspi_master_config_t userConfig; uint32_t srcFreq = 0; /*SPI configuration*/ LPSPI_MasterGetDefaultConfig(&userConfig); userConfig.baudRate = BOARD_NXPNCI_SPI_BAUDRATE; srcFreq = BOARD_NXPNCI_SPI_CLOCK; userConfig.whichPcs = (lpspi_which_pcs_t)kLPSPI_Pcs0; userConfig.pcsActiveHighOrLow = (lpspi_pcs_polarity_config_t)kLPSPI_PcsActiveLow; /*Initialize SPI*/ LPSPI_MasterInit(BOARD_NXPNCI_SPI_INSTANCE, &userConfig, srcFreq); } static status_t INTF_WRITE(uint8_t *pBuff, uint16_t buffLen) { uint8_t temp[1000]; temp[0] = 0x7F; memcpy(temp+1, pBuff, buffLen); masterXfer.txData = temp; masterXfer.rxData = NULL; masterXfer.dataSize = buffLen+1; masterXfer.configFlags = kLPSPI_MasterPcs0 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;; return LPSPI_MasterTransferBlocking(BOARD_NXPNCI_SPI_INSTANCE, &masterXfer); } static status_t INTF_READ(uint8_t *pBuff, uint16_t buffLen) { status_t status; uint8_t temp[257]; temp[0] = 0xFF; masterXfer.txData = temp; masterXfer.rxData = temp; masterXfer.dataSize = buffLen+1; masterXfer.configFlags = kLPSPI_MasterPcs0 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;; status = LPSPI_MasterTransferBlocking(BOARD_NXPNCI_SPI_INSTANCE, &masterXfer); if(status == kStatus_Success) memcpy(pBuff, temp+1, buffLen); SDK_DelayAtLeastUs(10, SDK_DEVICE_MAXIMUM_CPU_CLOCK_FREQUENCY); return status; } #endif   We also need to overwrite the functions: tml_Init, tml_DeInit and tml_Reset to adapt them to use the specific APIs for the GPIOs of our board. static Status tml_Init(void) { gpio_pin_config_t in_config = {kGPIO_DigitalInput, 0}; gpio_pin_config_t out_config = {kGPIO_DigitalOutput, 0}; GPIO_PinInit(BOARD_NXPNCI_IRQ_PORT, BOARD_NXPNCI_IRQ_PIN, &in_config); GPIO_PinInit(BOARD_NXPNCI_VEN_PORT, BOARD_NXPNCI_VEN_PIN, &out_config); GPIO_PinInit(BOARD_NXPNCI_DWL_PORT, BOARD_NXPNCI_DWL_PIN, &out_config); INTF_INIT(); return SUCCESS; } static Status tml_DeInit(void) { GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); return SUCCESS; } static Status tml_Reset(void) { /* Set DWL_REQ low for NCI protocol */ GPIO_PortClear(BOARD_NXPNCI_DWL_PORT, 1U << BOARD_NXPNCI_DWL_PIN); GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); GPIO_PortSet(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); return SUCCESS; }   Finally, modify the main file so it uses the APIs to initialize our board clocks and pins: #include <stdio.h> #include <string.h> #include "app.h" #include "board.h" #include "pin_mux.h" #include "fsl_debug_console.h" extern void nfc_example (void); int main(void) { BOARD_InitHardware(); #ifdef BOARD_NXPNCI_INTERFACE_I2C PRINTF("\nRunning the NXP-NCI2.0 example (I2C interface)\n"); #else PRINTF("\nRunning the NXP-NCI2.0 example (SPI interface)\n"); #endif nfc_example(); } Testing the example. At this point we have everything set to build and flash our example with SPI interface, you may proceed to build and debug/flash the example by pressing the blue beetle button: Once the example is flashed, open a serial terminal such as Teraterm with the following settings: Baudrate: 115200. Data: 8 bits. Parity: None. Stop bits: 1 bit. No flow control. While running, the example should output the following logs to the terminal: When a tag is placed near the antenna, the example should print the tag information in the terminal as shown:  
View full article
PN5190-NTAG X DNA High Speed Communication Demo: This article describes important feature of these two chips when interacting with each other at contactless interface: Passthrough demonstrator at high bit rates for ISO/IEC14443-A between PN5190 and NTAG X DNA Scope of demonstrator: ▪ Demonstrating a unique feature of NXP Semiconductors. High bit rates for ISO14443 communication (up to 848 kbps) between a PN5190 reader IC and an NTAG X DNA when connected to MCXA153 host MCU, when simulating the transmission of a dummy file as big as 101 kbytes. ▪ Through MCUXpresso console, the user can configure the contactless bit rate: 106 kbps 212 kbps 424 kbps or 848 kbps The amount of data is fixed in this demo. ▪ transmission mode is implemented from NFC reader library at K82 MCU built in the PNEV5190BP evaluation kit. On the other side, NTAG X DNA + Level shifter (represented by evaluation kit NTAG-X-DNA-EVAL) is connected to a Freedom Board, equipped with MCXA153 - FRDM-MCXA153). ▪ The PN5190 prints on the MCUXpresso console (debug mode) the outcome of the transaction and average baud rate achieved. ▪ In order to handle full file transmission from K82 to MCXA153 (MCU <-> MCU communication), we are using NTAG X DNA GPIO wires as well as proper settings on the NTAG X DNA <-> MCXA153 side and hard coded timeout on the PN5190 + MCU side. For more details, please open attached file PN5190_NTAGXDNA_MCXA153_DualInterface_HBR_Demo_SetupInstructions_Q32025.pdf. Required hardware and software enablement: Hardware ▪ PNEV5190BP Development Board ▪ FRDM-MCXA153 Development Board ▪ NTAG X DNA Development Board ▪ 2 x USB micro cables (for PNEV5190BP dev. br., one for DC power, other for Jlink debug on MCUxpresso IDE) ▪ 1 x USB-C cable (for FRDM-MCXA153 dev. br., only for DC power) Software ▪ MCUxpresso project (firmware Source Code) for PNEV5190BP is attached to this article, containing keywork pn5190: pn5190-ntagxdna-highspeed-demo1.zip. Instructions will be given in from future release of NFC Reader Library public v07.14.00 (NxpNfcRdLib_PN5190_v07.14.00_Pub.zip). ▪ SDK_2.x_FRDM-K82F is already included in bundle mentioned above. ▪ Firmware Source Code for FRDM-MCXA153 is attached to this article, containing keyword MCXA153: MCXA153.zip ▪ MCUXpresso IDE recent version, for instance v24.12.148 or above. Demonstrator bring up: Hardware assembly for FRDM-MCXA153: • Connect NTAG X DNA to level shifter (see Fig. 1) • Connect bundle NTAG X DNA+ level shifter bundle to flat cable (contained in demokit box) to FRDM-MCXA153 according to Fig. 2. • Make sure each wire is connected to proper position in Arduino socket: - black wire IO2 goes to J1-14 - white wire IO1 goes to J1-16 - gray wire SCL goes to J2-20 - violet wire SDA goes to J2-18 - blue wire GND goes to J3-14 - green wire VCC goes to J3-8 • Connect FRDM-MCXA153 via J15 (MCU-Link) to your computer (Debug Link Input), for the first time that you have to flash binary in it. Then after storing binary, you may just connect USB-C cable from a power supply to J6 port (named Ext-debugger). • No additional power source is needed. Hardware assembly for PNEV5190B: • Connect two USB micro cables to PNEV5190B board for power, flashing firmware and UART connection (see Fig. 3): • microUSB on J7 is necessary for DC power. Check that jumper J9 is in the position USB dc supply • microUSB on J20 is the Jlink debug port, and it will be connected to your Windows computer, where MCUxpresso has been installed. • Red LED indicates power is enabled • Green LED debugging/UART status Alternatively, if you have a DC power supply (voltage above 7 V), you may change Jumper J9 to Ext power supply, and avoid using second microUSB cable. Software loading on FRDM-MCXA153: 1. Create a new workspace for MCXA153 MCUxpresso example: 2. Make sure you have installed MCXA153 SDK: - install MCXA153 SDK which can be downloaded from: https://mcuxpresso.nxp.com/  3. Unzip "MCXA153.zip" file in local C: directory, with reasonable path length. 4. Import existing projects from file system, into MCUXpresso IDE: 5. Select proper root directory (keyword is MCXA153): 6. Click "Finish" 7. If you get this warning, simply click "OK": 8. Highlight project, click "build", and check that there are no errors: Finished building target: MCXA153_NTAGXDNA_DualInterface_DataRead_Demo.axf Performing post-build steps arm-none-eabi-size "MCXA153_NTAGXDNA_DualInterface_DataRead_Demo.axf"; # arm-none-eabi-objcopy -v -O binary "MCXA153_NTAGXDNA_DualInterface_DataRead_Demo.axf" "MCXA153_NTAGXDNA_DualInterface_DataRead_Demo.bin" ; # checksum -p MCXA153 -d "MCXA153_NTAGXDNA_DualInterface_DataRead_Demo.bin";    text        data         bss         dec         hex     filename   23524          20        3684       27228        6a5c      MCXA153_NTAGXDNA_DualInterface_DataRead_Demo.axf 16:27:26 Build Finished. 0 errors, 0 warnings. (took 5s.787ms) 9. Now, flash the binary into MCXA153 MCU using GUI Flash tool; select suitable  MCUxpresso probe (CMSIS-DAP). Make sure USB-c cable is connected to J15 in Freedom board (MCU-link port for flashing FW). 10. Select binary file *.axf as indicated below: It may happen that your MCXA153 has outdated FW on CMSIS-DAP, but you can continue, it will make no harm; click then Ok to flash. 11. After flashing, reboot your board. Following LEDs should be on: - D15 RGB led should be "white" lit. - D7 should be blinking "red" - D8 and D4 should be "green" lit. D15 will blink "white" only during file transmission. You may disconnect USB-c from J15 (the one used with MCUxpresso for flah and connect it to J8. Then, plug the other cable tip to any USB  5 volt battery charger. Now your Freedom board FRDM-MCXA153 is ready to receive data from PNEV5190 board, once project will be imported too in MCUxpresso. Software loading on PNEV5190BP: 1. Unzip *.zip file in directory with reasonable path length. 2. Import existing projects from file system 3. Select Example 12 "NfcrdlibEx12_NTAGXDNA" 4. Uncheck the choice "copy projects into workspace" 5. Install SDK_2.x_FRDM-K82F if not yet done. Such SDK is included in project file tree: • ...Examples\Platform\SDK_2.x_FRDM-K82F • This specific SDK can be obtained from https://mcuxpresso.nxp.com/ by selecting following K82F tab related "PN5180" : • FRDM-K82F-PN5180 (MK82FN256xxx15) • SDK 2.0 is no longer officially available, but SDK 2.2 and newer are backward compatible and recommended by NXP • Build project and check that there are no errors ("warnings" are allowed). • Start Debug session to see available bitrate options on the console. Hardware combination of PNEV5190B and NTAG X DNA connected to FRDM-MCXA153: Under MCUXpresso: 1. Click "Debug" icon on quick access left panel. Accept agreement in case of J-Link tool: 2. Click on icon "Run" on top side of MCUxpresso, and observe the following on "Console" tab: [MCUXpresso Semihosting Telnet console for 'NfcrdlibEx12_NTAGXDNA_mcux JLink DebugFRDMK82F' started on port 59973 @ 127.0.0.1] SEGGER J-Link GDB Server V8.12a - Terminal output channel *** NTAG X DNA Example *** Please place NTAG X DNA Card and Select Demo option. 1 : Perform Data Read Write using AES128 Key Authentication 2 : Perform Data Read Write using ECC Sigma-I Authentication Host as Initiator with NIST P-256 Curve, session key AES128 3 : Perform Data Read Write using ECC Sigma-I Authentication Host as Responder with NIST P-256 Curve, session key AES128 4 : Perform HBR transfer to Microcontroller through NTAG X DNA. 5 : Configure NTAG X DNA for HBR transfer Enter your option : Menu options when two boards have NFC antennas facing each other: There are 5 options in console menu as soon as you "Run" the debug. 1 - options from 1 until and including 3 are related to crypto functionality (symmetric and asymmetric) and are out of the scope of this article. 2 - Then option 5 is used for the first time that you are configuring your NTAG X DNA product. It will set registers and GPIO properly for High bit rate transfer. Once you have run option 5, then go to option 4: 3 - Four options of bitrate are available for transfer a fixed amount of data from host (K82) to NTAG X DNA MCU (MCXA153) using PN5190 as tunnel: Please configure the required baud rate 1 : 106 Kbps 2 : 212 Kbps 3 : 424 Kbps 4 : 848 Kbps Enter your option : Demonstration flow: Once one of these option is selected, reader is ready to detect a tag. ▪ When tag is detected, reader configures selected bitrate and starts data exchange. ▪ Blinking RGB LED D15 indicates transfer ongoing and the console shows a progress. Here are some results of transaction at the different bit rates and data sizes offered by this demonstrator: 1 - 106 Kbps - Baud rate 7.6 kBytes/s - elapsed time: 13.99 s Type A Tag is discovered. ***** Perform Transfer sequence ******* Select Application Successful Select File Successful Data transferring NFC -> NTAG X DNA -> Microcontroller... Amount of data exchanged 101200 Bytes, Baudrate (total) = 7.6 kB/s, Time = 13.99 s Please Remove the Card   After removing the card, K82 firmware starts again prompting for a new selection, in the previous menu. First select 4 again and then chose again another new baud rate: 2 - 212 Kbps - Baud rate 10.51 kBytes/s - elapsed time: 9.39 s 3 - 424 Kbps - Baud rate 13.92 kBytes/s - elapsed time: 7.90 s 4 - 848 Kbps - Baud rate 16.60 kBytes/s - elapse time: 5.95 s   Using Example 12 of NFC Reader Library v.07.14.00 to prepare High Speed demo on PNEV5190BP and NTAG X DNA: 1. Go to https://nxp.com web site and type "NFC Reader Library" in Search tab. Follow the instructions until you get to this screenshot: 2. Start by downloading NFC Reader library V.07.14.00 from NXP website; agree with Terms and Conditions. Then download the bundle to your local C: drive: 3. Click on “down arrow” to download version 07.14.00. Once zip file is received, unzip previous bundle to a local drive directory.   4. Start a new workspace, then choose "Import from Existing Projects into Workspace": 5. De-select all useless Examples and keep only example 12; please including all other essential items; click "Finish": 6. If you find this error, it means you need to install K82F SDK: 7. Click install, then MCUxpresso SDKs pages will open. Select K82F from Processor tab: Click “Install” button; after installation is completed, you will get a screen showing all installed sdk's. Afterwards you may get the prompt "Make SDK persistent"; just click ok. 8. Highlight project NfcrdlibEx12_NTAGXDNA_mcux and click build; check if there are errors: Finished building target: NfcrdlibEx12_NTAGXDNA_mcux.axf Performing post-build steps arm-none-eabi-size "NfcrdlibEx12_NTAGXDNA_mcux.axf" ; arm-none-eabi-objcopy -O binary "NfcrdlibEx12_NTAGXDNA_mcux.axf" "NfcrdlibEx12_NTAGXDNA_mcux.bin" ; #checksum -p MK82FN256xxx15 -d "NfcrdlibEx12_NTAGXDNA_mcux.bin"    text        data         bss         dec         hex     filename  222400          92       86816     309308       4b83c      NfcrdlibEx12_NTAGXDNA_mcux.axf 17:32:59 Build Finished. 0 errors, 3 warnings. (took 33s.718ms) 9. Now, check in MCUxpresso the tab Windows > Preferences > Run/Debug. Untick the box related to General Options Build (if required) before launching; it will save you much time! Then, click button “Apply and Close”. 10. Using this Example 12 as it is given by NXP in this library, when you will debug it, you will realize that there are only 3 Menu options related to NTAG X DNA cryptography (and no high speed options). In order to “unlock” the high-speed demo option, please do the following. 11. Go to Quick Settings → Defined Symbols and open it in a new window: Now add after last symbol, the following line: "PH_EX12_ENABLE_DUALINTERFACE_HBR", by clicking on “add button” ("+" shown in green) on top right side of above window; add it manually then click OK two times. Now, build Ex12 again and check that there are no errors. 12. Debug Example 12, then press Run button and check if Console has 5 options in its Menu: Please place NTAG X DNA Card and Select Demo option. 1 : Perform Data Read Write using AES128 Key Authentication 2 : Perform Data Read Write using ECC Sigma-I Authentication Host as Initiator     with NIST P-256 Curve, session key AES128 3 : Perform Data Read Write using ECC Sigma-I Authentication Host as Responder     with NIST P-256 Curve, session key AES128 4 : Perform HBR transfer to Microcontroller through NTAG X DNA. 5 : Configure NTAG X DNA for HBR transfer Enter your option : 13. Let's focus on the last two options: 4 – perform HBR (high bit rate) transfer, and 5 – Configure your NTAG X DNA for HBR. 14. If this is the first time you are using this NTAG X DNA connected to MCXA153, then choose option 5 so that PN5190 will write proper configuration data to NTAG X DNA next to it. For this reason, turn on NTAG X DNA connected to FRDM-MCXA153 board (after powering it up with a simple 5V-USB source), and place NTAG X DNA antenna over PNEV5190BP board antenna (connected to MCUxpresso), as in picture shown above. Enter your option : 5 Ready to detect Type A Tag is discovered.       Select NDEF Application Successful       Authenticate Application Successful       SetConfig Successful       StdDataFile with File ID 0xE106 already exists. Please Remove the Card 15. Remove NTAG X DNA antenna from PN5190 antenna, until you get back to initial menu. Then, choose option 4 on previous menu: 4 : Perform HBR transfer to Microcontroller through NTAG X DNA. 5 : Configure NTAG X DNA for HBR transfer Enter your option : 4  Please configure the required baud rate 1 : 106 Kbps 2 : 212 Kbps 3 : 424 Kbps 4 : 848 Kbps Enter your option : 16. Now, choose the lowest speed "1"; check final result: Ready to detect Type A Tag is discovered. ***** Perform Transfer sequence *******       Select Application Successful       Select File Successful       Data transferring NFC -> NTAG X DNA -> Microcontroller...       Amount of data exchanged 101200 Bytes, Baudrate (total) = 5.72 kB/s, Time = 17.25 s Please Remove the Card 17. Separate both antennas, and then, choose option "2"; check final result: Enter your option : 2 Ready to detect Type A Tag is discovered. ***** Perform Transfer sequence *******       Select Application Successful       Select File Successful       Data transferring NFC -> NTAG X DNA -> Microcontroller… Amount of data exchanged 101200 Bytes, Baudrate (total) = 10.49 kB/s, Time = 9.41 s 18. Separate both antennas, and then, choose option "3"; check final result: Enter your option : 3 Ready to detect Type A Tag is discovered. ***** Perform Transfer sequence *******       Select Application Successful       Select File Successful       Data transferring NFC -> NTAG X DNA -> Microcontroller...       Amount of data exchanged 101200 Bytes, Baudrate (total) = 13.89 kB/s, Time = 7.11 s Please Remove the Card 19. Separate both antennas, and then, choose option "4"; check final result:  Enter your option : 4 Ready to detect Type A Tag is discovered. ***** Perform Transfer sequence *******       Select Application Successful       Select File Successful       Data transferring NFC -> NTAG X DNA -> Microcontroller...       Amount of data exchanged 101200 Bytes, Baudrate (total) = 16.57 kB/s, Time = 5.96 s Please Remove the Card Conclusions: This demonstrator HW & SW can show that high speed interaction can be achieved between PN5190 (NFC Front end) and NTAG X DNA (NFC connected tag), making use of available commands described in its product support package (https://www.nxp.com/products/NTAG-X-DNA). Disclaimer:All SW available here is aimed only for evaluation purposes and NXP disclaims any direct or indirect liability damages, since referred SW bundles are not yet official part of PN5190/NTAG X DNA standard product support packages currently available at nxp.com.  
View full article
  Some customers are trying to update the user firmware on PN7642 through host interface and using “DownloadLibEx1” demo,  and they are using SFWUMaker to create .esfwu file from .bin followed the readme file but failed to do a firmware update. Here is a step-by-step guide to do it. I will use the SDK led blinky demo,  and generate an Esfwu file , and program it into PN7642 board with LPC5516 host.  Led blinky demo is in PN7642_MCUXpresso_SDK_02-15-00_PUB.  You can download it from PN7642 product page.  Single-Chip Solution with High-Performance NFC Reader, Customizable MCU and Security Toolbox | NXP Semiconductors Step 1: compile pnev7642fama_led_blinky demo Please make sure the flash size is 180KB.  By default,  the output flash size is 180KB with MCUXpresso IDE.     Step 2: Bin file generation The binary (.bin) file is not generated by default, we can do it manually by doing following: Build your target application Open the debug/release folder in MCUXpresso Right-click on the *.axf file Choose 'Binary Utilities' → 'Create binary' in the menu The .bin should appear   Step 3: Make an ESFWU file To convert a bin file to an ESFWU file, we can use the ESFWU Maker Utility (sw810311). It can be downloaded from PN7642 product page. It is a secure file, and you need to have an active NDA to get it.  To run this utility, the toml file is very important.  You need to change the output name and binary name according to your project ,  and  you need to use the correct aes_root_key. For other parameters, we left them unchanged.   3.1   change the output name and binary name   3.2 set the correct aes_root_key The application flashed via SWD is a bin file and NOT encrypted neither is it flashed with our bootloader. The .esfwu file via host interface is encrypted and flashed by our own bootloader.  The keys have to be valid, else the bootloader will not be able to decrypt the received file. Please make sure we are using the right keys to create the user application firmware.  This is crucial and without it, it won’t work anyways. The default keys are mentioned in the datasheet as transport keys. See below picture.  But it is highly recommended to provision your own keys!  Please have a look at the secure key mode application note for further information on that.        If you are not sure whether you have provisioned the root key or not, you can check the SKM state by running SKM demo. if the root key is provisioned, please use the provisioned root key.  From below picture, I can see that the app_root_key is  not provisioned, so I use the default transport key.     3.3  use the EsfwuMaker command to generate the Esfwu file.     After this command, we can get the esfwu file.       Step 4: Secure firmware download   We use the firmware download example to update the PN7642 firmware.  It is in the host software package, it  holds examples to be used with LPC55S16 and MCUXpresso, to interact with the PN7642. The LPC55S16 Host Software can be download from PN7642 product page. LPC55S16 Host Software Version 02.01.00 (nxp.com) To run the demo, we need to edit the firmware location.  In file DownloadLibEx1.c,  about line 60.       Please set the correct hardware settings as below.  we have to stack the PNEV7642A Rev-B development board on top of the LPC55S16-EVK board. Align Pin.1 of J36 of the PNEV7642A Rev-B development board with Pin.1 of J9 of the LPC55 board. The last 4 pins, 17 - 20, of J12 of the LPC board are not connected. As well as pin 1-4 of J10 stay unconnected, as below picture shows.       Run the firmware download Demo with LPC55s16,  see the log output below.  Choose option “6” to update your application firmware. The update may take a while.  At the end, a successful update is indicated by the prompt of “Successful firmware upload ”.         To verify it is successful, we can run this demo, please keep J65 open.  you will see the D7 (RED LED) blinky (0.5 HZ rate). If you need the pnev7642fama_led_blinky.esfwu, please let me know.    
View full article
Using an alternative clock source to set up PN7462's contact interface clock , so that we have more options of the clock frequency.
View full article
A Quick Solution for link issue of "missing --end-group" when you use the latest MCUXpresso IDE to compile the NFC reader library projects.
View full article
Example sends Wi-Fi credentials from phone to IoT device, so it can join the Wi-Fi network.  Using: iOS and Android phone with NXP's TagWriter app PN7462 NFC Reader device on PNEV7462B eval board, part of kit OM27462CDK Host Card Emulation mode example based on NfcrdlibEx8_HCE_T4T example from NFC Reader Library Example will also print out other NDEF messages received.  NDEF formats include: Contacts / Business Cards URL link Wi-Fi network and credentials Bluetooth MAC address for pairing Email address Phone number Geo location Launch application on host OS Plain text SMS (sorry the audio is horrible)
View full article
The NFC reader library is supporting multiple frontends. For a customer this might become a more difficult to use, if only the part for one of the frontend chips is needed. To enhance the readability and usability, you can remove the support for not used reader ICs by simply removing the folders below NxpRdLib/comps/phhalHw/src. For instance: if you only want to use the RC663, you could simply delete the folders Pn5180, Rc523. The result would be a library that only supports RC663. This short screen recording shows the steps to reduce the number of supported Frontends.
View full article
Based on NFC reader library porting guide for LPC11u37h(Ver 5.12) ,We have a partial ported NFC reader library like below: Now, it is time to port other demos in this project. You may choose any demo, but here NfcrdlibEx2_AdvancedDiscoveryLoop is selected. and similar with before, the first step is creating a new build configuration: then in the project references, choose the LPCopen library for LPC11u37 instead. Change the MCU settings: Change the build settings: Change FreeRTOS portable to cortex M0: Search "PHDRIVER_LPC1769RC663_BOARD" in the source code of "NfcrdlibEx2_AdvancedDiscoveryLoop" project, and you may simply replace it with "PHDRIVER_LPC11U37RC663_BOARD", and there are only two places needs to be fixed. Search "PHDRIVER_LPC1769" in the source code of "NfcrdlibEx2_AdvancedDiscoveryLoop" project, and you may simply replace it with "PHDRIVER_LPC11U37". Most changes are in phApp_Init.c. Also please don't forget to enable optimization for size. Building result: Demo testing result:
View full article
This page contains information about the supported NXP MCU/MPU and NXP NFC product combinations which have ready to use packages. These can be used as a reference. The table below contains link to where you can find the projects as well.    MCU ↓   NFC IC →  NTAG I²C  plus NTAG 5 PN7150 CLRC663 plus family* PN5180 i.MX RT1050 i.MX RT1050 + NTAG I²C plus i.MX RT1050 + CLRC663 plus   Video: Using i.MX RT1050 with CLRC663 plus family and the NFC Reader Library | NXP  i.MX RT1060 i.MX RT1060 + NTAG I²C plus  i.MX RT1060 + PN7150 i.MX 8M Mini i.MX 8M Mini + PN7150 (Andriod) i.MX 8M Mini + PN7150 (linux-yocto) i.MX 7 Dual Sabre i.MX7 Dual Sabre + PN5180 LPC1769 LPC1769 + CLRC663 plus LPC1769 + PN5180 LPC55S69 LPC55S69 + NTAG I²C plus LPC55S69 + NTAG 5 LPC55S69 + PN7150 LPC55S69 + CLRC663 plus LPC55S69 + CLRC663 plus + SE050 (smart lock) LPC11u37h LPC11u37 + PN7150 LPC11u37h + CLRC663 plus LPC11u68 LPC11u68 + PN7150 LPC82X LPC82X + PN7150 LPC845 LPC845 + CLRC663 plus Kinetis K82F K82F + CLRC663 plus K82F + PN5180 Kinetis K64F K64F + PN7150 K64F + CLRC663 plus Kinetis K63 K63 + PN7150 Kinetis K24 K24 + PN7150 KW41Z KW41Z + NTAG I²C plus KW41Z + NTAG 5 KW41Z + PN7150 *CLRC663 plus family: CLRC663 plus, MFRC630 plus, MFRC631 plus, SLRC610 plus For more information on the NFC products, please visit https://www.nxp.com/nfc
View full article
The latest NXP-NCI example is rev 1.6, and when you run this demo with the lpc11xx board, for example, lpc1115 rev A, and the OM5577, you may meet the following issue: The problem is due to two aspects: one is hardware and the other is software. For hardware solution, besides following what is described in AN11658 section 2.4 LPC11xx, you have to do one more thing: a) The I2C lines are not pulled-up: LPC11xx doesn't offer internal pull-up setting of the I2C lines so external pull-up resistors must be added. For software solution, the function of Sleep()( in tool.c) was optimized too much, and it didn't meet the timing requirement of OM5577, so we should let the IDE ignore it. The solution I use is as below: __attribute__((optimize("O0"))) void my_func() { blah } You may check the attachment for details. The result is shown as below: Original Attachment has been moved to: tool.c.zip
View full article
Hello NFC community, MIFARE® Ultralight-based tickets offer an ideal solution for low-cost, high-volume applications such as public transport, loyalty cards and event ticketing. They serve as a perfect contactless replacement for magnetic stripe, barcode, or QR-code systems. The introduction of the contactless MIFARE Ultralight® ICs for limited-use applications can lead to reduced system installation and maintenance costs. As you may know the MIFARE family has the Ultralight C tag which is a contactless IC supporting 3DES cryptography is mostly used in limited use applications such smart ticketing, this tag complies with ISO 14443-3 type A and it is defined as type 2 tag, in this document I want to show you the procedure to change the default key to a custom key also to protect certain areas in the tag so the authentication is needed to perform a read or write operation. --------------------------------------------------------------------------------------------------- For this document I used : MFEV710: PEGODA Contactless Smart Card Reader RFIDDiscover Software Lite version  Full Version Available in Docstore Mifare Ultralight c --------------------------------------------------------------------------------------------------- Information Old Key : 49454D4B41455242214E4143554F5946 New Key : 88776655443322117766554433221199 Data sheet ---------------------------------------------------------------------------------------------------- First we start with the procedure to activate the tag and the anticollision procedure explained in the ISO/IEC 14443-3. Command Direction    ">" this direction is command send from PCD (Reader) to PICC(Ultralight c)    "<" this direction is command send from PICC (Ultralight c) to PCD (Reader)    "=" Prepare this command before sending Command   Data message REQA =  Request Command, Type A >  26 ATQA = Answer To Request, Type A  <  4400 SEL + NVB = SEL (Select code for cascade level ) 93, NVB (Number of Valid bits) 20 >  9320 ANTICOLLISION START <  8804598356   >  93708804598356 SAK (Select Acknowledge) = indicates additional cascade level <  x04   >  9520   <  E1ED2580A9   >  9570E1ED2580A9   <  x00 UID = 045983E1ED2580  ** the following procedure is explained in section 7.5.5 from the datasheet** Command   Data message Authenticate Part 1  (command 1A) >  1A00   <  AFA1ED1D682E5101422CC7 Authenticate Part 2 (command AF) >  AF2970D895F186D0302970D895F186D030188AAF4DAF68C5B9   <  006BD027CEC3E04EBC6919 [AUTHENTICATED] Then according to  section 7.5.7 of the datasheet the sections  where the 3DES key are saved are the 2C (Page 44) to the 2F (Page 47). We proceed to  write our new key using the A2 (WRITE command) Command   Data message DATA = byte 07,06,05,04 = 11223344 WRITE to page 44 (2C) >  A22C11223344 Positive acknowledge (ACK) <  0A DATA = byte 03,02,01,00 = 55667788 WRITE to page 45 (2D) >  A22D55667788  Positive acknowledge (ACK) <  0A DATA = byte 0F,0E,0D,0C = 99112233 WRITE to page 46 (2E) >  A22E99112233  Positive acknowledge (ACK) <  0A DATA = byte 0B,0A,09,08 = 44556677 WRITE to page 47 (2F) >  A22F44556677  Positive acknowledge (ACK) <  0A [RESET FIELD] [Authenticate with new key] Command   Data message Authenticate Part 1  (command 1A >  1A00   <  AFFAE2EFF17FAAD69862E7 Authenticate Part 2 (command AF) >  AFFD5794F2D4EA1B19FD5794F2D4EA1B196CF420CD4D9E8104   <  0030922228601939B8FA18 [AUTENTICATED WITH NEW KEY] we proceed to define from which sector the authentication is needed in order to read or write, to do this we use a write command to the AUTH0 (AUTH0 defines the page address from which the authentication is required. Valid address values for byte AUTH0 are from 03h to 30h.) the AUTH0 is located on the section 2A please check table 5 from #datasheet. **for this example we will define that from page 6 (06) we will need authentication to perform a read or write operation** Command   Data message WRITE command (A2) to AUTH0 (2A) from page 6 (06) >  A22A06000000 Positive acknowledge (ACK) <  0A Now the Read capabilities from page 06  require an Authentication in order to be read or written. Hope you find this document useful to get a better understanding of the behavior of the Ultralight C and how its security features can help you in your applications. Have a great day! BR Jonathan
View full article
The latest NFC reader library for CLRC663 just supports LPCXpresso1769 and FRDM-K82 boards, so when customers want to porting the library to other host controller, they have to make a custom board at first, or use OM26630FDK and make a little hardware modification by following the steps described in https://www.nxp.com/docs/en/training-reference-material/NFC-READER-K64F.pdf?fsrch=1&sr=3&pageNum=1 to connect the frontend board with host controller board, but today we will discuss an alternative way. The CLEV663B Blueboard is a pure NFC frontend board, and it supports connecting with LPCXpresso board not limited with LPC1769, the main difference with OM26630FDK is the reader IC, which is CLRC663 not CLRC663 plus, but fortunately they are pin to pin compatible, so we may replace it with CLRC663 plus, and use that board for porting purpose. Before: After: please forgive my poor soldering skill... With this new board and LPC1769 Xpresso board, you may run the latest 5.12 NFC reader library, for example, the NfcrdlibEx1_BasicDiscoveryLoop demo. but you might have the following issue: This is due to ver 5.12 use another set of IO pins to connect with the reader IC, modify pin definitions in Board_Lpc1769Rc663.h can fix this issue. The final result is as below: Please note, it is recommended using NFC reader library ver 4.03 to test the hardware including CLEV663B and LPC1769Xpresso before replacing with CLRC663 plus, and you know, CLEV663B Blueboard is just optimized for CLRC663 , so the matching circuit is not the best for CLRC663 plus, it is just good enough to run the demo, so that we may know if the porting is successful, but if you want to have the best performance with CLRC663 plus, you have to redo the antenna tuning, and you may refer to https://community.nxp.com/docs/DOC-335545 for more details on that topic.
View full article
SPIM module is one of the master interfaces provided by PN7462 , which is a 32-bit ARM Cortex-M0-based NFC microcontroller, and users may use this interface to connect with up to two SPI slave devices. The NFC reader library provides SPIM driver code in phHal/phhalSPIM, and users may directly use the following APIs in their application to implement simple SPI transaction, just like what is done  in the demo of "PN7462AU_ex_phExHif". While this demo has limitation with some SPI nor flash devices, which need a write-read operation in one NSS session, for example, the SPI nor flash device on OM27462 as below: Please note to solder R202 and connect it to 3V3 to make sure nHold pin has pull-up out of POR. The following is one of the command sets this device supports: This command contains 1 write(9F) followed by 3 read operations in one NSS session, but if you implement it with phhalSPIM_Transmit() and phhalSPIM_Receive() as below: status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 2, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, data_length, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);" You will have the following result: expected: NSS   \__________________________/ MOSI     CMD A7-A0 MISO                            DATA       actual:                         NSS   \____________||______________/ MOSI     CMD A7-A0 MISO                           DATA so the pulse between the write and read is the problem, and here we have to handle the NSS line manually, with the help of NSS_VAL and NSS_CONTROL bits in SPIM_CONFIG_REG. so the code should be like this:   Assert NSS   status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 2, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, data_length, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);"   De-assert NSS The NSS line assert and de-assert function can be implemented with register bit level APIs, just like below:             PH_REG_SET_BIT(SPIM_CONFIG_REG, NSS_VAL);//de-assert NSS             PH_REG_SET_BIT(SPIM_CONFIG_REG, NSS_CTRL);             PH_REG_CLEAR_BIT(SPIM_CONFIG_REG, NSS_VAL);//assert NSS Please also include the following header files in your application code. #include "ph_Reg.h" #include "PN7462AU/PN7462AU_spim.h" Please notice that phhalSPIM_Transmit() and phhalSPIM_Receive() are Rom based function, which clear NSS_CTRL bit by default. We can not change ROM API's behave but fortunately we have phhalSPIM_TransmitContinue() and phhalSPIM_ReceiveContinue() instead. so the final solution will be like below: Assert NSS   status = phhalSPIM_TransmitContinue(1, cmd_buf);    status = phhalSPIM_ReceiveContinue(3, dst);   De-assert NSS This doesn't mean phhalSPIM_Transmit() and phhalSPIM_Receive() are useless, because they can also help up to configure the SPI master interface, if you don't want to use register bit level API to initial the SPIM module manually. Please note to use 1 byte for write/read length to make these two functions work properly. so the whole pseudo code is like below: phhalSPIM_Init(PH_HW_SPIM_TIMEOUT) ; phhalSPIM_Configure(PH_HW_SPIM_SLAVE, PH_HW_SPIM_MSB_FIRST,                 \                                     PH_HW_SPIM_MODE, PH_HW_SPIM_BAUDRATE,  \                                     PH_HW_SPIM_NSSPULSE, PH_HW_SPIM_NSSPOL) ; status = phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);    status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);" Assert NSS   status = phhalSPIM_TransmitContinue(1, cmd_buf);    status = phhalSPIM_ReceiveContinue(3, dst);   De-assert NSS The following steps show how to create a new project based on NFC reader library, please refer to https://www.nxp.com/docs/en/user-guide/UM10883.pdf  on how to import the NFC reader library. 1. Create a new project after importing the NFC reader library. 2. if you installed PN7462 support package, you will see this: 3. add a link to NFC reader lib: 4. add path and enable NFC reader lib in the project: 5. delete cr_startup.c and create the main code as well as the header file: 6. Build result: 7.Debug result: To fetch the ready demo, please submit a private ticket via the guide of https://community.nxp.com/docs/DOC-329745 . Hope that helps, Best regards, Kan
View full article
The latest NFC reader library supports lpc1769 which is a cortex M3 controller with LPCopen lib supports, so in theory , it should supports other controllers supported by LPCopen, but we have to test this, so we choose , for example, lpc11u37, a cortex M0 based controller for this porting. Platform for this porting: LPC11u37h-Xpresso Rev A: CLRC663 plus based CLEV663B Blueboard 3.0. Please refer to Prepare CLEV663B board for NFC reader library porting  for details. They are connected via LPCXpresso ports. Now we may start the porting, the IDE we use in this porting is MCUXpresso 10.1.1 1. Download and import the latest NFC reader library for CLEV6630B, as it supports CLRC663 plus. For how to import the project, please refer to https://www.nxp.com/docs/en/application-note/AN11211.pdf . 2. Download LPCopen for LPC11u37h and import it as well. 3. Now we may choose some demo in the NFC reader library, for example, the NfcrdlibEx1_BasicDiscoveryLoop, and create new build configuration for lpc11u37h. 4.Select the correct MCU 5.Modify build settings Here we find LPC1769RC663 is defined, so we have to find what is related with this definition in the code and change it/them. Fortunately they are not too many. you may find they are just related with board header file including or something like that, so it is not difficult to modify them. 6. Add new header file for the new board definition 7. add the new board definition 8. As we now use LPCopen lib for LPC11u37h instead, so we have to change the including path. As LPC11u37h is cortex M3 based, so we have to setup FreeRTOS for M0 support: and add the source code for building: 9.Change the link libraries and including path 10.Set the correct ref projects to use LPCopen for LPC11u37h. 11. Some changes in LPCopen library: 1)enable semihosting debug 2) add startup source code for the demo, this C file can be reused/imported from the some lpcopen project. 12. After the above steps, we still have to change the source code in DAL: You know , due to different version of LPCopen library,  some function definition might be changed, and different LPCXpresso boards has different pin connection to the LPCXpresso ports, so it is recommended checking the board schematics and the examples in lpcopen project , find the proper function calls to implement the source codes in the DAL folder. When you finished , the porting is done. 13. As the final image size is greater than 128K, we have enable optimization for size. 14.Demo test ok. Now , we know lpc11u37 can be supported by the latest NFC reader library, so the porting should also be applied for other Cortex M0 controllers, and it is recommended the controller with large internal flash size, better greater than 128K, but anyway, in this porting, I didn't enable the size optimization for LPCopen library, so there might be possibility to have a smaller size image at last...
View full article