Make the NFC reader library easier to read, by removing folders for the frontend ICs not needed in a project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Make the NFC reader library easier to read, by removing folders for the frontend ICs not needed in a project

No ratings

Make the NFC reader library easier to read, by removing folders for the frontend ICs not needed in a project

The NFC reader library is supporting multiple frontends. For a customer this might become a more difficult to use, if only the part for one of the frontend chips is needed.

To enhance the readability and usability, you can remove the support for not used reader ICs by simply removing the folders below NxpRdLib/comps/phhalHw/src. For instance: if you only want to use the RC663, you could simply delete the folders Pn5180, Rc523. The result would be a library that only supports RC663.

This short screen recording shows the steps to reduce the number of supported Frontends.

Version history
Last update:
‎04-14-2016 05:44 AM
Updated by: