Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
S32K344/358/388 SWO Printf が動作しないのは S32DS3.6 です チームの皆さん、こんにちは。 この手順に従って、PEマルチリンクとS32DS3.6を使用してSWOのprintf関数をテストしました。S32K3の公式EVBを使用し、SWOピンが正常に伸びていることを確認しました。S32K311、312 SWOは正常に動作しますが、S32K344、358、388は印刷できません。ソフトウェアに何らかの隠れた設定があるはずです。テストして試していただけますか? S32DS3.6.1、3.6.2をテストしました。3.6.3、3.6.5.すべて同じように動作します。311/312は正常に動作しますが、344、358、388は動作しません。 優先度:高 S32DS Re: S32K344/358/388 SWO Printf not work is S32DS3.6 S32K344と312のSWOルーティングに関するRMを確認しました。344はより複雑です。ソフトウェアによって追加のスイッチをオンにする必要があるのかもしれません。 よろしくお願いいたします。 ジェレミー Re: S32K344/358/388 SWO Printf not work is S32DS3.6 こんにちは、ジェレミーさん。 あなたの問題を調べてみます。以前は既知のバグでしたが、現在は修正されていることを願っています。最新のPE Microプラグインを使用していますか? Re: S32K344/358/388 SWO Printf not work is S32DS3.6 こんにちは、ジリさん。 これは私のPEマイクロプラグインです Re: S32K344/358/388 SWO Printf not work is S32DS3.6 こんにちは、ジェレミーさん。 最新のPE Microプラグイン(v6.1.8)をお試しください。 Re: S32K344/358/388 SWO Printf not work is S32DS3.6 こんにちは、ジリさん。 後で時間ができたら試してみますか?バージョン6.1.8は試してみましたか? よろしくお願いいたします。 ジェレミー Re: S32K344/358/388 SWO Printf not work is S32DS3.6 こんにちは、Jiriさん。この問題は私の方ではまだ解決していません。そちらでは何か進展はありますか? よろしくお願いいたします。 ジェレミー
查看全文
NXP iMX8MP: WFI-based CPU idle in U-Boot never wakes Dear NXP Support Team, We are investigating a low-power waiting mechanism in U-Boot for a i.MX8M Plus based product and have reached a point where we would appreciate guidance from NXP. Software versions SoC: NXP i.MX8M Plus BSP: ATF: lf_v2.10_android-15.0.0_1.2.0 U-Boot: lf_v2024.04_android-15.0.0_1.2.0 Based on the public NXP BSP (Variscite fork contains no relevant modifications in the ATF/GIC code paths) Goal The application needs to remain in U-Boot for several minutes while a deeply discharged battery charges before Android is started. A busy-loop based on mdelay() consumes unnecessary power and generates additional heat, so we are trying to periodically enter a low-power idle state and wake using the ARM Generic Timer (CNTP, PPI 30). Initial implementation configure CNTP timer enable PPI 30 execute a raw wfi() from EL2 The processor never wakes from wfi(). UART output simply stops with no exception or crash. PSCI implementation PSCI_VERSION returns 1.1 PSCI_FEATURES(CPU_SUSPEND) returns 0 (supported) invoke CPU_SUSPEND requesting the Standby power state This reaches the ATF standby implementation imx_cpu_standby(), but the system hangs in exactly the same way: no exception, no UART output, and execution never resumes. Therefore, both: raw wfi() executed at EL2 wfi() executed through ATF via PSCI produce identical behavior. What have been already verified CPU and timer U-Boot executes at EL2. CNTP timer is correctly programmed. CNTP_TVAL_EL0 counts down correctly. CNTP_CTL_EL0 shows: ENABLE = 1 IMASK = 0 ISTATUS = 0 immediately after arming. CPU interface ICC_PMR_EL1 is configured correctly. ICC_IGRPEN1_EL1 is enabled. Virtualization HCR_EL2 has: IMO = 0 FMO = 0 so interrupt routing through EL2 virtualization is not involved. Interrupt security classification From the ATF sources we verified that: all PPIs are initially configured as Group 1 Non-secure by the generic GICv3 helper code, only SGI8 (and optionally SDEI SGIs) are reconfigured as Secure, PPI 30 is **not** present in the secure interrupt property table. Therefore the Generic Timer interrupt appears to remain Group 1 Non-secure as expected. SCR_EL3.TWE We originally suspected that non-secure wfi() might be trapped to EL3 via SCR_EL3.TWE, but this now seems unlikely because the same behavior occurs when wfi() is executed inside ATF itself through PSCI. Additional investigation While tracing the ATF GIC initialization we noticed that gicv3_distif_init() clears the Distributor EnableGrp bits and only re-enables those requested by the secure interrupt property table. Since the helper only produces Group0 and Group1 Secure properties, it appears that EnableGrp1NS is never explicitly re-enabled. To verify this we: read GICD_CTLR observed EnableGrp1NS = 0 attempted to set EnableGrp1NS ourselves from EL2. Unexpectedly: the write completes without fault, RWP behaves normally, but EnableGrp1NS remains 0 after readback. We also verified: GICD_CTLR.DS == 0 RDC protection for the GIC memory regions is disabled (ENA = 0) RDC violation registers remain zero. Therefore RDC does not appear to be preventing the write. Remaining question At this point we have eliminated: timer programming, CPU interface configuration, interrupt priority masking, interrupt group classification, SCR_EL3.TWE trapping, PSCI vs raw WFI execution, RDC protection. The remaining unexplained behavior is that an architecturally Non-secure writable Distributor control bit (EnableGrp1NS) does not appear to accept writes on this platform, and consequently neither raw wfi() nor PSCI CPU_SUSPEND ever wake using the Generic Timer interrupt. Is this behavior expected on the i.MX8M Plus Android 15 BSP? Is there any platform-specific initialization missing outside the public ATF sources that is required before the Generic Timer PPI can wake a CPU from wfi()? Is EnableGrp1NS intentionally prevented from being modified by non-secure software on this platform? Has anyone successfully implemented periodic wake-up from U-Boot using either: raw wfi(), or PSCI CPU_SUSPEND  driven by the ARM Generic Timer? Any insight into the expected initialization sequence or platform-specific behavior would be greatly appreciated. Thanks Best Regards Pier
查看全文
使用 flex-installer "lsdk2606" 版本在 Debian "imx95-15x15-frdm" 系统上发布 "Weston.Service" 你好, 我使用 flex-installer 版本“ lsdk2606 ”安装了 Debian 镜像。 剧透 (高亮部分可供阅读) sudo flex-installer -i auto -d /dev/sdX -m imx95-15x15-frdm sudo flex-installer -i auto -d /dev/sdX -m imx95-15x15-frdm 我的imx95-15x15-frdm 然后,我按照标准流程继续安装。 剧透 (高亮部分可供阅读) debian-post-install-pkg debian-post-install-pkg 安装完所有软件包并重启后,启动时出现以下错误: 剧透 (高亮部分可供阅读) [失败] 启动 weston.service - W…nd compositor 作为系统服务失败。 [失败] 启动 weston.service - W…nd compositor 作为系统服务失败。 剧透 (高亮部分可供阅读) root@imx95-15x15-frdm:~# systemctl status weston.service × weston.service - Weston,一个 Wayland 排版器,作为系统服务 已加载: 已加载 (/usr/lib/systemd/system/weston.service;已启用;预设:已启用) 活动状态:失败(结果:退出代码),自 2026 年 7 月 20 日星期一 13:51:20 UTC 起;19 秒前 调用:67b22b0fa1484ce681d8b2acdc107add 触发者:● weston.socket 文档:man:weston(1) man:weston.ini(5) http://wayland.freedesktop.org/ 进程:408 ExecStart=/usr/bin/weston --log= ${XDG_RUNTIME_DIR} /weston.log --modules=systemd-notify.so (code=exited, status=1/FAILURE) 主进程 ID:408(退出代码=1,状态=1/失败) 内存峰值:3.5M CPU:49毫秒 7月20日 13:51:19 imx95-15x15-frdm systemd[1]: 正在启动 weston.service - Weston,一个 Wayland 合成器,作为系统服务... 7 月 20 日 13:51:19 imx95-15x15-frdm (weston)[408]: pam_unix(weston-autologin:session): 用户 root(uid=0) 的会话已由 (uid=0) 打开 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:主进程已退出,代码=已退出,状态=1/失败 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:失败,结果为“退出代码”。 7 月 20 日 13:51:20 imx95-15x15-frdm systemd[1]: 启动 weston.service 失败 - Weston,一个 Wayland 合成器,作为系统服务。 root@imx95-15x15-frdm:~# systemctl status weston.service×weston.service - Weston,一个 Wayland 合成器,作为系统服务已加载:已加载 (/usr/lib/systemd/system/weston.service;已启用;预设:已启用)活动状态:失败(结果:退出代码)自 2026 年 7 月 20 日星期一 13:51:20 UTC 起;19 秒前 调用:67b22b0fa1484ce681d8b2acdc107add 触发者:● weston.socket文档: man:weston(1) man:weston.ini(5) http://wayland.freedesktop.org/进程:408 ExecStart=/usr/bin/weston --log= ${XDG_RUNTIME_DIR} /weston.log --modules=systemd-notify.so (code=exited, status=1/FAILURE) 主进程 ID:408 (code=exited, status=1/FAILURE) 内存峰值:3.5M CPU:49ms 7月20日 13:51:19 imx95-15x15-frdm systemd[1]: 正在启动 weston.service - Weston,一个 Wayland 合成器,作为系统服务... 7月20日 13:51:19 imx95-15x15-frdm (weston)[408]: pam_unix(weston-autologin:session): 用户 root(uid=0) 的会话已由 (uid=0) 打开 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:主进程已退出,代码=已退出,状态=1/失败 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:失败,结果为“退出代码”。7 月 20 日 13:51:20 imx95-15x15-frdm systemd[1]: 启动 weston.service 失败 - Weston,一个 Wayland 合成器,作为系统服务。 剧透 (高亮部分可供阅读) root@imx95-15x15-frdm:~# cat /run/user/0/weston.log 日期:2026年7月20日 UTC [12:34:22.150]韦斯顿 14.0.2 https://wayland.freedesktop.org 错误报告请提交至: https://gitlab.freedesktop.org/wayland/weston/issues/ 版本:LSDK-25.12_DEBIAN-13_LF-6.12.20-168-g2ddc741+ [12:34:22.153]命令行:/usr/bin/weston --log=/run/user/0/weston.log --modules=systemd-notify.so [12:34:22.153]操作系统:Linux,6.12.49,#5 SMP PREEMPT 2026年5月28日星期四 13:07:26 KST,aarch64 [12:34:22.153]飞行记录仪:已启用 [12:34:22.155]使用配置文件“/etc/xdg/weston/weston.ini” [12:34:22.156]输出重绘窗口最大为 16 毫秒。 [12:34:22.158]正在加载模块“/usr/lib/libweston-14/drm-backend.so” [12:34:22.162]模块加载失败:libdisplay-info.so.1:无法打开共享对象文件:没有该文件或目录 [12:34:22.162]致命错误:创建合成器后端失败 root@imx95-15x15-frdm:~# cat /run/user/0/weston.logDate:2026-07-20 UTC[12:34:22.150]weston 14.0.2https://wayland.freedesktop.org错误报告至:https://gitlab.freedesktop.org/wayland/weston/issues/Build:LSDK-25.12_DEBIAN-13_LF-6.12.20-168-g2ddc741+[12:34:22.153]命令行:/usr/bin/weston --log=/run/user/0/weston.log --modules=systemd-notify.so[12:34:22.153]操作系统:Linux,6.12.49,#5 SMP PREEMPT 2026 年 5 月 28 日星期四 13:07:26 KST,aarch64[12:34:22.153]飞行记录仪:已启用[12:34:22.155]使用配置文件“/etc/xdg/weston/weston.ini”[12:34:22.156]输出重绘窗口最大为 16 毫秒。[12:34:22.158]正在加载模块“/usr/lib/libweston-14/drm-backend.so”[12:34:22.162]模块加载失败:libdisplay-info.so.1:无法打开共享对象文件:没有该文件或目录[12:34:22.162]致命错误:创建合成器后端失败 我也遇到了同样的错误(我不知道是否相关),但是我的屏幕上什么都没显示。 剧透 (高亮部分可供阅读) it6263 3-004c:未能清除 DDC FIFO it6263 3-004c:读取 EDID 失败 it6263 3-004c:清除 DDC FIFO 失败;it6263 3-004c:读取 EDID 失败 Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe root@imx95-15x15-frdm:~# ldd /usr/lib/libweston-14/drm-backend.so linux-vdso.so.1 (0x0000ffffac56c000) libweston-14.so.0 => /usr/lib/libweston-14.so.0 (0x0000ffffac410000) libwayland-client.so.0 => /lib/aarch64-linux-gnu/libwayland-client.so.0 (0x0000ffffac3e0000) libpixman-1.so.0 => /lib/aarch64-linux-gnu/libpixman-1.so.0 (0x0000ffffac330000) libwayland-server.so.0 => /lib/aarch64-linux-gnu/libwayland-server.so.0 (0x0000ffffac2f0000) libdrm.so.2 => /usr/lib/libdrm.so.2 (0x0000ffffac2b0000) libudev.so.1 => /lib/aarch64-linux-gnu/libudev.so.1 (0x0000ffffac250000) libdisplay-info.so.1 => 未找到 libgbm.so.1 => /usr/lib/libgbm.so.1 (0x0000ffffac220000) libseat.so.1 => /lib/aarch64-linux-gnu/libseat.so.1 (0x0000ffffac1f0000) libinput.so.10 => /lib/aarch64-linux-gnu/libinput.so.10 (0x0000ffffac170000) libc.so.6 => /lib/aarch64-linux-gnu/libc.so.6 (0x0000ffffabfb0000) /lib/ld-linux-aarch64.so.1 (0x0000ffffac520000) libxkbcommon.so.0 => /lib/aarch64-linux-gnu/libxkbcommon.so.0 (0x0000ffffabf40000) libffi.so.8 => /lib/aarch64-linux-gnu/libffi.so.8 (0x0000ffffabf10000) libm.so.6 => /lib/aarch64-linux-gnu/libm.so.6 (0x0000ffffabe60000) libcap.so.2 => /lib/aarch64-linux-gnu/libcap.so.2 (0x0000ffffabe30000) libsystemd.so.0 => /lib/aarch64-linux-gnu/libsystemd.so.0 (0x0000ffffabd00000) libmtdev.so.1 => /lib/aarch64-linux-gnu/libmtdev.so.1 (0x0000ffffabcd0000) libevdev.so.2 => /lib/aarch64-linux-gnu/libevdev.so.2 (0x0000ffffabc90000) libwacom.so.9 => /lib/aarch64-linux-gnu/libwacom.so.9 (0x0000ffffabc60000) libgudev-1.0.so.0 => /lib/aarch64-linux-gnu/libgudev-1.0.so.0 (0x0000ffffabc30000) libgobject-2.0.so.0 => /lib/aarch64-linux-gnu/libgobject-2.0.so.0 (0x0000ffffabba0000) libglib-2.0.so.0 => /lib/aarch64-linux-gnu/libglib-2.0.so.0 (0x0000ffffaba10000) libatomic.so.1 => /lib/aarch64-linux-gnu/libatomic.so.1 (0x0000ffffab9e0000) libpcre2-8.so.0 => /lib/aarch64-linux-gnu/libpcre2-8.so.0 (0x0000ffffab920000) Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe Hello root@imx95-15x15-frdm:~# find /usr -name "libdisplay-info*" /usr/lib/aarch64-linux-gnu/libdisplay-info.so.2 /usr/lib/aarch64-linux-gnu/libdisplay-info.so.0.2.0 /usr/share/doc/libdisplay-info2 Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe 请运行以下命令并分享输出结果? 查找 /usr -name "libdisplay-info*" 谢谢! Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe 谢谢你的更新。 我可以看到 libdisplay-info 存在于系统中,但是 Weston 日志正在查找 libdisplay-info.so.1,而安装的库似乎是 libdisplay-info.so.2。 请运行以下命令并分享输出结果? ldd /usr/lib/libweston-14/drm-backend.so 这将有助于验证是否存在库版本不匹配或其他缺失的依赖项。
查看全文
S32K344/358/388 SWO Printf 在 S32DS3.6 中不起作用 嗨,团队、 我按照这个步骤用 pe multilink 和 S32DS3.6 测试了 SWO printf 函数。 我使用了 S32K3 官方 EVB 并检查了 SWO 引脚是否成功伸出。S32K311,312 SWO 可以正常工作,但 S32K344,358,388 无法打印出来。肯定有一些隐藏设置需要在软件中完成,您能帮忙测试并尝试一下吗? 我已经测试了 S32DS3.6.1、3.6.2、3.6.3,3.6.5.所有情况都一样,311/312 可以正常工作,而 344、358、388 则无法工作。 优先级:高 S32DS Re: S32K344/358/388 SWO Printf not work is S32DS3.6 我已经检查了 S32K344 和 312 的 SWO 路线的 RM。344 则更为复杂。 也许需要用软件打开一些额外的开关。 顺祝商祺! 杰里米 Re: S32K344/358/388 SWO Printf not work is S32DS3.6 嗨,杰里米、 我来看看你的问题。过去这是一个已知的错误,但希望现在已经修复。您使用的是最新的 PE Micro 插件吗? Re: S32K344/358/388 SWO Printf not work is S32DS3.6 嗨,吉瑞、 这是我的 PE 微型插件 Re: S32K344/358/388 SWO Printf not work is S32DS3.6 嗨,杰里米、 请尝试使用最新的 PE Micro 插件(v6.1.8 Re: S32K344/358/388 SWO Printf not work is S32DS3.6 嗨,吉日、 有时间的话,我会测试一下。您试过这个 v6.1.8 版本吗? 顺祝商祺! 杰里米 Re: S32K344/358/388 SWO Printf not work is S32DS3.6 Jiri,你好,我这边这个问题仍然存在,你那边有什么进展吗? 顺祝商祺! 杰米
查看全文
MPC5746C FXOSC 出力周波数 パーツ:MPC5746C(Power Architecture Z4、SDK:NXP MPC57xxプラットフォームSDK)。 MPC5746Cのマニュアルには、FXOSCは8~40MHzの出力周波数を提供すると記載されています。以下の構成におけるFXOSCの出力周波数を特定するのを手伝ってください。 1. FXOSC_CTL: OSCBYP = 0 かつ OSCM = LCP 2. FXOSC_CTL: OSCBYP = 0 かつ OSCM = FSP 3. FXOSC_CTL: OSCBYP = 1 かつ OSCM = LCP 4. FXOSC_CTL: OSCBYP = 1 かつ OSCM = FSP 他のレジスタ項目についてもデフォルト値を検討してください。ありがとう。 Re: MPC5746C FXOSC output frequency @petervlna さん、ご回答ありがとうございます。 クリスタル/共振器(OSCBYP = 0)と外部クロック(OSCBYP = 1)が提供する周波数はどのように見つければよいのでしょうか? Re: MPC5746C FXOSC output frequency こんにちは、 FXOSCモジュールは、OSCBYPおよびOSCMの設定に基づいて特定の周波数を生成しません。FXOSCの出力周波数は常にFXOSCに接続された外部ソースの周波数(OSCBYP=0のクリスタル/共振器、OSCBYP=1の時は外部クロック)と等しく、8〜40 MHzのサポート範囲内で行われます。 したがって、記載されている4つの構成すべてにおいて、FXOSCの出力周波数は外部入力周波数と全く同じになります。OSCMの設定(LCP/FSP)は発振器の動作モードに影響を与えますが、クロック周波数は変更しません。 よろしくお願いいたします。 ピーター Re: MPC5746C FXOSC output frequency @petervlna上記のFXOSCの問い合わせについてサポートいただければ幸いです。 Re: MPC5746C FXOSC output frequency クリスタル/共振器(OSCBYP = 0)と外部クロック(OSCBYP = 1)が提供する周波数はどのように見つければよいのでしょうか? 上記の質問について、 @petervlna さんにお知らせください。FXOSCをタイマーのクロックソースとして使用したい。提供される周波数に基づいて、カウント値をタイマーレジスタに読み込めます Re: MPC5746C FXOSC output frequency こんにちは、 MPC5746Cには、FXOSCレジスタからFXOSC周波数を測定または判定する方法がありません。周波数はハードウェア設計から知られている必要があります: OSCBYP = 0: FXOSC周波数は、基板に取り付けられた外部水晶発振器/共振器の周波数と等しい。 OSCBYP = 1: FXOSC周波数は、FXOSC入力ピンに印加される外部クロック信号の周波数と等しくなります。 FXOSCをタイマークロックソースとして使用するには、タイマーカウント値を計算する際に基板の回路図やクロックデザインで指定された周波数(例:8 MHz、16 MHz、40 MHzなど)を使用する必要があります。OSCBYPとOSCMの設定は、周波数自体には影響しません。 よろしくお願いいたします。 ピーター
查看全文
S32K344/358/388 SWO Printf not work is S32DS3.6 Hi Team, I have tested the SWO printf function with pe multilink and S32DS3.6 following this step.  I have used the S32K3 official EVB and checked the SWO pin have extended out successfully. The S32K311,312 SWO can work fine, but S32K344,358,388 can't print out. There must be some hidden settings which needs to be done in the software, Could you help to test and try? I have tested S32DS3.6.1, 3.6.2, 3.6.3, 3.6.5. All behaves the same, 311/312 can work fine and 344,358,388 can't work. Priority: HIGH S32DS Re: S32K344/358/388 SWO Printf not work is S32DS3.6 I have checked the RM for the SWO routing for S32K344 and 312. 344 is more complex.  Maybe some extra switch need to be swited on by software. Best Regards, Jeremy Re: S32K344/358/388 SWO Printf not work is S32DS3.6 Hi Jeremy,  I'll look at your issue. In past it was known bug, but hope that it is fixed now. Are you using latest PE Micro plugin?  Re: S32K344/358/388 SWO Printf not work is S32DS3.6 Hi jiri, This is my PE micro plugin Re: S32K344/358/388 SWO Printf not work is S32DS3.6 Hi Jiri, I will test it when I get time lator? Have you tried this  v6.1.8 version?  Best Regards, Jeremy Re: S32K344/358/388 SWO Printf not work is S32DS3.6 Hi Jeremy,  please try to use the latest PE Micro plugin which is v6.1.8 Re: S32K344/358/388 SWO Printf not work is S32DS3.6 Hi Jiri, this issue still exists at my side, any update on your side? Best Regards, Jermey
查看全文
サポート要望:i.MX8MプラスLVDS出力を用いたHD-SDIインターフェース 拝啓、 私たちは NXP i.MX8M Plus プロセッサをベースにしたシステムを設計しており 、 HD-SDIインターフェース の実装について皆様のご指導をいただきたい と考えています。 私たちの要件は、3つのHD-SDI出力をサポートすることです。 i.MX8M PlusのLVDSインターフェースを使用し、以下のデバイスを使ってHD-SDIに変換する予定です。 LMH0340SQE/NOPB – LVDS-HD-SDIシリアライザ LMH0324RTWT 1対3 HD-SDI分配アンプ 2台 i.MX8M PlusのLVDSインターフェース が 、3つのHD-SDI出力を生成するこのアーキテクチャに対応している か確認していただけます か? もしこの方法が推奨されない場合やサポートされていない場合、i.MX8M Plusプロセッサを使い続けながら3つのHD-SDIインターフェースを実装する代替案をご提案いただけます か?私たちはi.MX8M Plusをデザインに残したいと考えています。なぜなら、他のシステム要件をすべて満たすからです。 このインターフェースを成功裏に実装するためのリファレンス・デザインやアプリケーションノートのご提案をいただけるとありがたいです。 サポートありがとうございます。ご指導をお待ちしております。 よろしくお願いいたします。 サムドラランカイア・ジャンパニ アナログ(ADC|CMP|DAC|OpAmp) ボード設計 MCXA MCX C Re: Support Request: HD-SDI Interface Using i.MX8M Plus LVDS Output こんにちは、 残念ながら、私はこの種の使い方にあまり慣れていません。あなたが共有した部分を調べたところ、FPGAで使うことが期待されているようで、LVDSチャネルでは使えそうでないようで、このインターフェースがその用途に使えるかはわかりません。 i.MX8MPの別のブリッジや他のインターフェース、あるいはその間の別のレイヤー(FPGA)を使うのが解決策かもしれません。 よろしくお願いいたします。 アルド。
查看全文
如何调整功放MD8LC925NR1的偏置电压? 你好, 我们目前正在设计一个使用MD8LC925NR1功率放大器的系统。我们恳请您推荐合适的偏置电路或专用电源管理元器件,以便为该功率放大器提供正确的偏置。 请问您能否提供一些推荐的参考设计、应用笔记或具体零件编号? 谢谢你的帮助。 Re: How to bias the amp MD8LC925NR1? 你好, 感谢您对恩智浦半导体产品的关注,也感谢您给我们提供支持的机会。 提供的零件编号似乎有误。MDL8LC925NR1不是 NXP 可订购的有效零件编号。最接近的匹配设备是MD8IC925N。请注意,该设备目前已停产,这意味着它不再受支持,也不再接受新的购买。 以下NXP文档提供了详细的设计信息,包括电路原理图、元器件清单和特性数据: MD8IC925N 数据手册 AN1977 –射频集成电路系列中的静态电流热跟踪电路 AN1987 – 射频集成电路设备系列的静态电流控制(包括两种偏置电路拓扑结构及完整的元器件清单) AN1955 – 射频功率放大器的热测量方法 遗憾的是,MD8IC925N 没有直接的替代品。此外,许多涵盖100 MHz 至 1000 MHz频率范围的射频产品即将停产,目前还没有宣布推出新的替代设备。 如果您需要我们根据您的具体频率、功率和供电电压要求,协助您寻找替代解决方案,请与我们联系。 顺祝商祺!
查看全文
NXP iMX8MP:基于WFI的CPU在U-Boot中处于空闲状态时不会唤醒 尊敬的恩智浦技术支持团队: 我们正在研究基于 i.MX8M Plus 的产品的 U-Boot 中的低功耗等待机制,现在我们希望得到 NXP 的指导。 软件版本 SoC:NXP i.MX8M Plus BSP: ATF:lf_v2.10_android-15.0.0_1.2.0 U-Boot:lf_v2024.04_android-15.0.0_1.2.0 基于公开的 NXP 电路板支持包(Variscite 分支对 ATF/GIC 代码路径没有相关的修改) 目标 在 Android 系统启动之前,应用程序需要在 U-Boot 模式下停留几分钟,以便为深度放电的电池充电。 基于 mdelay() 的忙循环会消耗不必要的功率并产生额外的热量,因此我们正在尝试定期进入低功耗空闲状态,并使用 ARM 通用定时器 (CNTP, PPI 30) 唤醒。 初始实施 配置 CNTP 定时器 启用 PPI 30 从 EL2 执行原始 wfi() 处理器永远不会从 wfi() 中唤醒。UART 输出突然停止,没有任何异常或崩溃。 PSCI 实现 PSCI_VERSION 返回 1.1 PSCI_FEATURES(CPU_SUSPEND) 返回 0(支持) 调用 CPU_SUSPEND 请求进入待机电源状态 程序会执行 ATF 备用程序实现 imx_cpu_standby(),但系统会以完全相同的方式挂起:没有异常,没有 UART 输出,执行永远不会恢复。 因此,两者: 在 EL2 级别执行原始 wfi() 函数 wfi() 通过 ATF 经由 PSCI 执行 产生相同的行为。 已经核实的内容 CPU 和定时器 U-Boot 在 EL2 层执行。 CNTP定时器已正确编程。 CNTP_TVAL_EL0 倒计时正常。 CNTP_CTL_EL0 显示: 启用 = 1 IMASK = 0 布防后,ISTATUS = 0。 CPU接口 ICC_PMR_EL1 配置正确。 ICC_IGRPEN1_EL1 已启用。 虚拟化 HCR_EL2 具有: IMO = 0 FMO = 0 因此,中断路由不会通过 EL2 虚拟化进行。 中断网络安全分类 我们从美国烟酒枪炮及爆炸物管理局(ATF)的消息来源证实: 所有PPI最初都由通用GICv3辅助代码配置为第1组非安全设备。 只有 SGI8(以及可选的 SDEI SGI)被重新配置为安全模式。 PPI 30 不在安全中断属性表中。 因此,通用定时器中断似乎仍如预期那样保持为第 1 组非安全状态。 SCR_EL3.TWE 我们最初怀疑不安全的 wfi() 可能会通过 SCR_EL3.TWE 被困到 EL3,但现在看来不太可能,因为当 wfi() 通过 PSCI 在 ATF 内部执行时,也会发生同样的行为。 进一步调查 在跟踪 ATF GIC 初始化时,我们注意到 gicv3_distif_init() 会清除 Distributor EnableGrp 位,并且只会重新启用安全中断属性表请求的那些位。 由于该辅助程序只生成 Group0 和 Group1 Secure 属性,因此 EnableGrp1NS 似乎永远不会被显式地重新启用。 为了验证这一点,我们: 读取 GICD_CTLR 观察到 EnableGrp1NS = 0 尝试从 EL2 自行设置 EnableGrp1NS。 不料: 写入操作顺利完成,没有出现任何错误。 RWP运行正常 但读取后 EnableGrp1NS 仍然为 0。 我们还核实了: GICD_CTLR.DS == 0 GIC 内存区域的 RDC 保护已禁用(ENA = 0) RDC违规登记数量仍为零。 因此,RDC 似乎并没有阻止写入操作。 剩余问题 至此,我们已经排除了: 定时器编程 CPU接口配置, 中断优先级掩码 中断组分类, SCR_EL3.TWE 捕获, PSCI 与原始 WFI 执行方式对比, RDC保护。 剩下的未解释的行为是,架构上不安全的可写分发器控制位(EnableGrp1NS)似乎不接受此平台上的写入,因此原始 wfi() 和 PSCI CPU_SUSPEND 都无法使用通用定时器中断唤醒。 i.MX8M Plus Android 15 电路板支持包。 出现这种现象是否正常? 在公共 ATF 源代码之外,是否存在任何平台特定的初始化缺失,导致通用定时器 PPI 无法通过 wfi() 唤醒 CPU? EnableGrp1NS 是否被有意阻止在此平台上被不安全的软件修改? 有没有人成功地使用以下两种方法之一实现了从 U-Boot 定期唤醒: 原始 wfi(),或 PSCI CPU_SUSPEND 由 ARM 通用定时器驱动? 非常感谢您能提供任何关于预期初始化顺序或平台特定行为的见解。 谢谢! 顺祝商祺! 码头
查看全文
PN7221 无法检测到 ISO 14443-3B 我们按照文档AN14880 PN7160/PN7220 - Android 16 移植指南移植了 PN7221。测试过程中,无法检测到 ISO 14443-3B (NfcB) 卡。此外,轻触此类卡片后,NFC 功能出现故障,无法识别任何卡片。需要将 NFC 关闭再重新打开才能恢复正常运行。相关日志附在下方,供您分析。 ❯ 07-16 09:24:28.515 530 6384 D NxpTml : PN72xx - I2C 读取成功..... 07-16 09:24:28.515 530 6384 D NxpNciR : len = 26 > 61051701010001FF010C0B00000000D103860500808001000000 07-16 09:24:28.515 530 6384 D NxpTml : PN72xx - 正在发布已读消息..... 07-16 09:24:28.516 530 6387 D NxpHal : 读取成功 状态 = 0x0 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: RF接口 = 帧 RF 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: 协议 = 未知 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: 模式 = B 被动轮询 07-16 09:24:28.516 530 6387 D NxpHal : NCI NTF: RF_DEACTIVATED len=26 type=1 07-16 09:24:28.517 530 6384 D NxpTml : PN72xx - 读取请求..... 07-16 09:24:28.517 530 6384 D NxpTml : PN72xx - 调用 I2C 读取..... 07-16 09:24:28.517 1599 6381 D libnfc_nci: rw_t4t_send_to_lower: conn_id 已发送至 lower =0 07-16 09:24:28.517 530 542 I android.hardware.nfc2-service.nxp:写 07-16 09:24:28.517 530 6385 D NxpTml : PN72xx - 写入请求..... 07-16 09:24:28.517 530 6385 D NxpTml : PN72xx - 调用 I2C 写入..... 07-16 09:24:28.519 530 6385 D NxpNciX : 长度 = 12 > 0000091D0000000000080100 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - I2C 写入成功..... 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - 发布新消息..... 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - Tml 写入线程正在运行................ 07-16 09:24:28.519 530 6387 D NxpHal : 写入成功 状态 = 0x0 07-16 09:24:28.520 530 6384 D NxpTml : PN72xx - I2C 读取成功..... 07-16 09:24:28.520 530 6384 D NxpNciR:长度 = 6 > 600603010001 07-16 09:24:28.520 530 6384 D NxpTml : PN72xx - 正在发布已读消息..... 07-16 09:24:28.521 530 6387 D NxpHal : 读取成功 状态 = 0x0 07-16 09:24:28.521 530 6387 D NxpHal : NCI NTF: CORE_GENERIC_ERROR len=6 07-16 09:24:28.521 530 6384 D NxpTml : PN72xx - 读取请求..... 07-16 09:24:28.521 530 6384 D NxpTml : PN72xx - 调用 I2C 读取..... 07-16 09:24:28.523 530 6384 D NxpTml : PN72xx - I2C 读取成功..... 07-16 09:24:28.523 530 6384 D NxpNciR:长度 = 5 > 0000020000 07-16 09:24:28.523 530 6384 D NxpTml : PN72xx - 正在发布已读消息..... 07-16 09:24:28.523 530 6387 D NxpHal : 读取成功 状态 = 0x0 07-16 09:24:28.524 1599 6381 I libnfc_nci: rw_t3Bt_sm_get_id (): sub_state:WAIT_ENDEF_FILE_CTRL_TLV (17) 07-16 09:24:28.524 1599 6381 D libnfc_nci: rw_t4t_send_to_lower: conn_id 已发送至 lower =0 07-16 09:24:28.524 530 542 I android.hardware.nfc2-service.nxp:写 07-16 09:24:28.524 530 6385 D NxpTml : PN72xx - 写入请求..... 07-16 09:24:28.524 530 6385 D NxpTml : PN72xx - 调用 I2C 写入..... 07-16 09:24:28.524 530 6384 D NxpTml : PN72xx - 读取请求..... 07-16 09:24:28.524 530 6384 D NxpTml : PN72xx - 调用 I2C 读取..... 07-16 09:24:28.525 530 6385 D NxpNciX : 长度 = 8 > 0000050036000008 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - I2C 写入成功..... 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - 发布新消息..... 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - Tml 写入线程正在运行................ 07-16 09:24:28.525 530 6387 D NxpHal : 写入成功 状态 = 0x0 07-16 09:24:28.527 530 6384 D NxpTml : PN72xx - I2C 读取成功..... 07-16 09:24:28.527 530 6384 D NxpNciR:长度 = 6 > 600603010001 07-16 09:24:28.528 530 6384 D NxpTml : PN72xx - 正在发布已读消息..... 07-16 09:24:28.528 530 6387 D NxpHal : 读取成功 状态 = 0x0 07-16 09:24:28.528 530 6387 D NxpHal : NCI NTF: CORE_GENERIC_ERROR len=6 07-16 09:24:28.530 530 6384 D NxpTml : PN72xx - 读取请求..... 07-16 09:24:28.530 530 6384 D NxpTml : PN72xx - 调用 I2C 读取..... 07-16 09:24:28.531 530 6384 D NxpTml : PN72xx - I2C 读取成功..... 07-16 09:24:28.532 530 6384 D NxpNciR : len = 14 > 00000B21CBA4729CB97166900000 07-16 09:24:28.532 530 6384 D NxpTml : PN72xx - 正在发布已读消息..... 07-16 09:24:28.532 530 6387 D NxpHal : 读取成功 状态 = 0x0 07-16 09:24:28.533 1599 6381 I libnfc_nci: rw_t3Bt_sm_get_id (): sub_state:???? 未知子状态 (18) 07-16 09:24:28.533 1599 6381 我 libnfc_nci: nfa_rw_update_pupi_id: 07-16 09:24:28.534 530 6384 D NxpTml : PN72xx - 读取请求..... 07-16 09:24:28.534 530 6384 D NxpTml : PN72xx - 调用 I2C 读取..... Re: PN7221 fails to detect ISO 14443-3B 我们已经升级到 3.2.5 版本,但测试结果仍然没有改变。 07-17 01:13:52.157 533 542 D NxpHal : 设备上检测到的固件版本 = 0x30205 Re: PN7221 fails to detect ISO 14443-3B 你好@zhangkai 请更新至 3.2.5 版本,您可以通过以下路径获取固件文件: nfc-NXPNFCC_FW/InfraFW/pn7220 at master · NXP/nfc-NXPNFCC_FW Re: PN7221 fails to detect ISO 14443-3B 06-24 10:20:33.259 390 401 D NxpHal : 设备上检测到的固件版本 = 0x302c4 Re: PN7221 fails to detect ISO 14443-3B 你好@zhangkai 固件版本是多少?如果版本低于 3.2.5,请更新到最新版本并再次测试。 如果还有疑问,请向我们提供完整日志。 Re: PN7221 fails to detect ISO 14443-3B 你好@zhangkai 能否提供 libnfc-nci.conf 和 libnfc-nxp.conf 文件? Re: PN7221 fails to detect ISO 14443-3B Hello @zhangkai  此问题可能与A16的变更有关。具体而言:在A15之前,NXP的MW依赖NFA_PROTOCOL_T3BT(80)来支持身份证,但A16通过Google已将中国身份证直接纳入其支持范围。然而,PN7xxx的MW仍保留了该代码。因此,客户尝试将T3BT逻辑从PN7xxx MW中完全移除,并直接使用Google的原生逻辑。 Re: PN7221 fails to detect ISO 14443-3B 配置文件已上传。
查看全文
How to bias the amp MD8LC925NR1? Hello, We are currently designing a system using the MD8LC925NR1 Power Amplifier. We would appreciate your recommendation for a suitable bias circuit or a dedicated power management component to properly bias this PA. Could you please provide any reference designs, application notes, or specific part numbers that you recommend for this purpose? Thank you for your assistance. Re: How to bias the amp MD8LC925NR1? Hello, Thank you for your interest in NXP Semiconductors products and for the opportunity to support you. There appears to be a typo in the part number provided. MDL8LC925NR1 is not a valid NXP orderable part number. The closest matching device is MD8IC925N. Please note that this device is currently End of Life, meaning it is no longer supported and is no longer available for new purchases. The following NXP documents provide detailed design information, including circuit schematics, component lists, and characterization data: MD8IC925N Datasheet AN1977 – Quiescent Current Thermal Tracking Circuit in the RF Integrated Circuit Family AN1987 – Quiescent Current Control for the RF Integrated Circuit Device Family (includes both bias circuit topologies with complete component lists) AN1955 – Thermal Measurement Methodology of RF Power Amplifiers Unfortunately, there is no direct replacement available for the MD8IC925N. In addition, many RF products covering the 100 MHz to 1000 MHz frequency range are approaching EOL status, and no new replacement devices have been announced at this time. Please let us know if you would like assistance identifying alternative solutions based on your specific frequency, power, and supply voltage requirements. Best regards
查看全文
PN7221はISO 14443-3Bを検出できません PN7221は PN7160/PN7220 - Android 16移植ガイドAN14880文書に従って移植しました。テスト中、ISO 14443-3B(NfcB)カードは検出できません。さらに、そのようなカードをタップすると、NFC機能が誤作動を起こし、どのカードも認識しなくなります。正常な動作に戻すには、NFC機能を一度オフにしてから再度オンにする必要があります。分析に必要な関連ログを以下に添付いたします。 ❯ 07-16 09:24:28.515 530 6384 D NxpTml : PN72xx - I2C読み込み成功..... 07-16 09:24:28.515 530 6384 D NxpNciR : len = 26 > 61051701010001FF010C0B00000000D103860500808001000000 07-16 09:24:28.515 530 6384 D NxpTml : PN72xx - 既読メッセージを投稿中..... 07-16 09:24:28.516 530 6387 D NxpHal : read 成功状態 = 0x0 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: RF インターフェース = フレームRF 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: プロトコル = 不明 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: Mode = B パッシブ投票 07-16 09:24:28.516 530 6387 D NxpHal : NCI NTF: RF_DEACTIVATED len=26 タイプ=1 07-16 09:24:28.517 530 6384 D NxpTml : PN72xx - 読書リクエスト..... 07-16 09:24:28.517 530 6384 D NxpTml : PN72xx - I2Cリードの呼び出し..... 07-16 09:24:28.517 1599 6381 D libnfc_nci: rw_t4t_send_to_lower: conn_id 下層へ送信 =0 07-16 09:24:28.517 530 542 I android.hardware.nfc2-service.nxp:書く 07-16 09:24:28.517 530 6385 D NxpTml : PN72xx - 書き込みリクエスト..... 07-16 09:24:28.517 530 6385 D NxpTml : PN72xx - I2C Writeの呼び出し..... 07-16 09:24:28.519 530 6385 D NxpNciX : len = 12 > 00000091D000000000000080100 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - I2C 書き込み成功..... 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - 新しい書き込みメッセージの投稿中..... 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - Tml Writer Thread実行中................ 07-16 09:24:28.519 530 6387 D NxpHal : write true status = 0x0 07-16 09:24:28.520 530 6384 D NxpTml : PN72xx - I2C読み取り成功..... 07-16 09:24:28.520 530 6384 D NxpNciR : len = 6 > 600603010001 07-16 09:24:28.520 530 6384 D NxpTml : PN72xx - 既読メッセージを投稿中..... 07-16 09:24:28.521 530 6387 D NxpHal : read, 成功した状態 = 0x0 07-16 09:24:28.521 530 6387 D NxpHal : NCI NTF: CORE_GENERIC_ERROR len=6 07-16 09:24:28.521 530 6384 D NxpTml : PN72xx - 読書リクエスト中..... 07-16 09:24:28.521 530 6384 D NxpTml : PN72xx - I2Cリードの呼び出し..... 07-16 09:24:28.523 530 6384 D NxpTml : PN72xx - I2C読み取り成功..... 07-16 09:24:28.523 530 6384 D NxpNciR : len = 5 > 0000020000 07-16 09:24:28.523 530 6384 D NxpTml : PN72xx - 既読メッセージの投稿..... 07-16 09:24:28.523 530 6387 D NxpHal : read 成功状態 = 0x0 07-16 09:24:28.524 1599 6381 I libnfc_nci: rw_t3Bt_sm_get_id (): sub_state:WAIT_ENDEF_FILE_CTRL_TLV (17) 07-16 09:24:28.524 1599 6381 D libnfc_nci: rw_t4t_send_to_lower: conn_id 下層へ送信 =0 07-16 09:24:28.524 530 542 I android.hardware.nfc2-service.nxp:書く 07-16 09:24:28.524 530 6385 D NxpTml : PN72xx - 書き込みリクエスト..... 07-16 09:24:28.524 530 6385 D NxpTml : PN72xx - I2C Write..... 07-16 09:24:28.524 530 6384 D NxpTml : PN72xx - 読書リクエスト中..... 07-16 09:24:28.524 530 6384 D NxpTml : PN72xx - I2Cリードの呼び出し..... 07-16 09:24:28.525 530 6385 D NxpNciX : len = 8 > 0000050036000008 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - I2C 書き込み成功..... 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - 新しい書き込みメッセージの投稿中..... 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - TMLライターThread実行中................ 07-16 09:24:28.525 530 6387 D NxpHal : write failed status = 0x0 07-16 09:24:28.527 530 6384 D NxpTml : PN72xx - I2C読み込み成功..... 07-16 09:24:28.527 530 6384 D NxpNciR : len = 6 > 600603010001 07-16 09:24:28.528 530 6384 D NxpTml : PN72xx - 既読メッセージを投稿中..... 07-16 09:24:28.528 530 6387 D NxpHal : read 成功状態 = 0x0 07-16 09:24:28.528 530 6387 D NxpHal : NCI NTF: CORE_GENERIC_ERROR len=6 07-16 09:24:28.530 530 6384 D NxpTml : PN72xx - 読書リクエスト..... 07-16 09:24:28.530 530 6384 D NxpTml : PN72xx - I2Cリードの呼び出し..... 07-16 09:24:28.531 530 6384 D NxpTml : PN72xx - I2C読み取り成功..... 07-16 09:24:28.532 530 6384 D NxpNciR : len = 14 > 00000B21CBA4729CB971669000000 07-16 09:24:28.532 530 6384 D NxpTml : PN72xx - 既読メッセージを投稿中..... 07-16 09:24:28.532 530 6387 D NxpHal : read 成功状態 = 0x0 07-16 09:24:28.533 1599 6381 I libnfc_nci: rw_t3Bt_sm_get_id (): sub_state:????不明のサブステート(18歳) 07-16 09:24:28.533 1599 6381 I libnfc_nci: nfa_rw_update_pupi_id: 07-16 09:24:28.534 530 6384 D NxpTml : PN72xx - 読書リクエスト..... 07-16 09:24:28.534 530 6384 D NxpTml : PN72xx - I2Cリードの呼び出し..... Re: PN7221 fails to detect ISO 14443-3B バージョン3.2.5にアップグレードしましたが、テスト結果は変わりません。 07-17 01:13:52.157 533 542 D NxpHal : デバイスで見つかったファームウェアバージョン = 0x30205 Re: PN7221 fails to detect ISO 14443-3B こんにちは、 @zhangkai さん。 3.2.5にアップデートしてください。fwファイルは以下のサイトから入手できます:nfc-NXPNFCC_FW/InfraFW/pn7220 at master ·NXP/NFC-NXPNFCC_FW Re: PN7221 fails to detect ISO 14443-3B 06-24 10:20:33.259 390 401 D NxpHal : デバイスで見つかったファームウェアバージョン = 0x302c4 Re: PN7221 fails to detect ISO 14443-3B こんにちは、 @zhangkai さん。 ファームウェアのバージョンは何ですか?もし3.2.5のような低いバージョンであれば、最新バージョンにアップデートして再度テストしてください。 それでもご不明な点がある場合は、ログ全体をご提供ください。 Re: PN7221 fails to detect ISO 14443-3B こんにちは、 @zhangkai さん。 libnfc-nci.confとlibnfc-nxp.confのファイルを提供してもらえますか? Re: PN7221 fails to detect ISO 14443-3B こんにちは、 @zhangkai さん。 この問題は、A16の変更に関連している可能性があります。具体的には、A15以前のNXP製モバイルMWは、IDカードのサポートにNFA_PROTOCOL_T3BT(80)を使用していましたが、A16ではGoogleを通じて中国のIDカードがサポート対象に直接含まれるようになりました。しかし、PN7xxx MWには依然としてこのコードが残っています。そのため、顧客はPN7xxx MWからT3BTロジックを完全に削除し、Googleのネイティブロジックを直接使用しようとしています。 Re: PN7221 fails to detect ISO 14443-3B 設定ファイルがアップロードされました。
查看全文
HID(W):LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 早安 ! 我正在试用 FRDM i.MX 93 入门指南:指南 我下载了FRDM-IMX93 演示镜像(尝试了 REV.1.0 和 REV4.0),但一直收到相同的错误信息。 尝试了指南中的命令:.\uuu.exe -b sd_all imx-image-full-imx93frdm.rootfs.wic.zst 用于 nxp imx 芯片的 uuu(通用更新实用程序) -- libuuu_1.5.243-0-g230f1b1 版本 in config: Pctl Chip Vid Pid BcdVersion Serial_No ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDPS: MX93 0x1fc9 0x014e SDPS: MX91 0x1fc9 0x0159 SDPS: MX95 0x1fc9 0x015d SDPS: MX95 0x1fc9 0x015c SDPS: MX943 0x1fc9 0x0027 SDPS: MX952 0x1fc9 0x0028 SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 FB: 0x0483 0x0afb 运行内置脚本: uuu_version 1.4.149 # @_flash.bin | 引导加载程序,可从 wic 映像中提取 # @_image [_flash.bin] | wic 映像刻录到 emmc。 # 此命令将在 i.mx6/7 i.mx8MM、i.mx8MQ SDP: 启动-f imx-image-full-imx-image-full-imx93frdm.rootfs.wic.zst/*-scanlimited 0x 800000 时运行 # 此命令将在 ROM 支持直播模式时运行 # i.MX8QXP, i.MX8QM SDPS: 启动 -scanterm -f imx-image-full-imx93frdm.rootfs.wic.zst/* -scanlimited 0x800000 # 这些命令将在使用 SPL 时运行,如果不使用 SPL,则跳过这些命令。 # SDPU 将被弃用,请使用 SDPV 代替 SDPU # { SDPU: delay 1000 SDPU: write -f imx-image-full-imx93frdm.rootfs.wic.zst/* -offset 0x57c00 -scanlimited 0x800000 SDPU: jump -scanlimited 0x800000 # } # 使用 SPL 时将运行这些命令,如果不支持,则跳过这些命令。 # 如果(SPL 支持 SDPV) # { SDPV:延迟 1000 SDPV: write -f imx-image-full-imx93frdm.rootfs.wic.zst/* -skipspl -scanterm -scanlimited 0x800000 SDPV: 跳转 -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev${sd_dev} FB: ucmd mmc dev${sd_dev} FB: flash -raw2sparse all imx-image-full-imx93frdm.rootfs.wic.zst/* FB: flash -scanterm -scanlimited 0x800000 引导加载程序 imx-image-full-imx93frdm.rootfs.wic.zst/* FB: 已完成 等待已知的 USB 设备出现... 4:2-23 连接新的 USB 设备 F11C6A09B54230 4 :2-23 F11C6A09B54230 > 启动 cmd: SDPS:boot-scanterm-f imx-image-full-imx93frdm.rootfs.wic.zst/*-scanlimited 0x800000 解压缩文件:> imx-image-full-imx9 3frdm.rootfs.wic.zst 14%4:2-23F11C6A09B54230>Fail HID(W):LIBUSB_ERROR_TIMEOUT (-7)(20.15s) 然后我试了一下。\ uuu.exe-v-b emmc_all。\ imx-boot-imx93frdm-sd.bin-flash_singleboot。\ imx-image-full-imx93frdm.rootfs.wic.zst,但也得到了同样的错误信息: 用于 nxp imx 芯片的 uuu(通用更新实用程序) -- libuuu_1.5.243-0-g230f1b1 版本 in config: Pctl Chip Vid Pid BcdVersion Serial_No ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDPS: MX93 0x1fc9 0x014e SDPS: MX91 0x1fc9 0x0159 SDPS: MX95 0x1fc9 0x015d SDPS: MX95 0x1fc9 0x015c SDPS: MX943 0x1fc9 0x0027 SDPS: MX952 0x1fc9 0x0028 SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 FB: 0x0483 0x0afb 运行内置脚本: uuu_version 1.4.149 # @_flash.bin | 引导加载程序,可从 wic 映像中提取 # @_image [_flash.bin] | wic 映像刻录到 emmc。 # 此命令将在 i.mx6/7 i.mx8MM、i.mx8MQ SDP: 启动-f 时运行 。 \ imx-boot-imx93frdm-sd.bin-flash_singleboot-Scanlimited 0x800000 # 此命令将在 ROM 支持直播模式时运行 # i.mx8QXP,i.mx8QM SDPS:启动-scanterm- f。\ imx-boot-imx93frdm-sd.bin-flash_singleboot-Scanlimited 0x800000 # 这些命令将在使用 SPL 时运行,如果不弃用 spl # SDPU,则将跳过 这些命令。请使用 SDPV 代替 SDPU # { SDPU: delay 1000 SDPU: write-f。 \ imx-boot-imx93frdm-sd.bin-flash_singleboot-offset 0x57c00 SDPU:jump-scanlimited 0x800000 #} # 这些命令将在使用 SPL 时运行,如果没有 spl 则会跳过 # if(SPL 支持 SDPV) # { SDPV: delay 1000 SDP V: write-f。 \ imx-boot-imx93frdm-sd.bin-flash_singleboot-skipspl-scanterm-scanlimited 0x800000 SDPV:跳跃-scanlimited 0x800000 #} FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev${emmc_dev} FB: ucmd mmc dev${emmc_dev} FB: flash -raw2sparse all .\imx-image-full-imx93frdm.rootfs.wic.zst/* FB:flash-scanterm-scanlimited 0x800000 引导加载程序。 \ imx-boot-imx93frdm-sd.bin-flash_singleboot FB: 如果环境存在 ucmd emmc_ack;那么;否则 setenv emmc_ack 0;fi; FB:ucmd mmc partc onf${emmc_dev}${emmc_ack} 1 0 FB:完成 等待已知的 USB 设备出现... 在 4:2-4:2 连接新的 USB 设备- > 启动 Cmd:SDPS: 启动-scanterm-f。 \ imx-boot-imx93frdm-sd.bin-flash_singleboot-scanlimited 0x800000 4:2-> 失败 HID (W):LIBUSB_ERROR_TIMEOUT (-7) (20.02s) 我使用的是最新的 uuu.exe 版本。 Windows上还有新的驱动程序。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 我也一样。我尝试使用 Ubuntu 20.04,也出现了同样的错误。 sudo ~/uuu-ubuntu20.04 -lsusb uuu(通用更新实用程序),用于 nxp imx 芯片 -- libuu_1.5.243-0-g230f1b1 已连接的已知 USB 设备 路径芯片 Pro Vid Pid BCD 版本序列号_否 ===================================================================================== 8214D79A2FFA4708 sudo ~/uuuu-ubuntu20.04-b emmc_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singlebootimx-image-core-imx93-11x11-lpddr4x-frdm.rootfs-20260608162024.wic.zst 用于 nxp imx 芯片的 uuu(通用更新实用程序) -- libuuu_1.5.243-0-g230f1b1 成功 0 失败 1 1:3-8214 D79A 1/ 1 [HID (W):LIBUSB_ERROR_TIMEOUT (-7)] SDPS:启动-scanterm-f imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash... 我尝试了 MACHINE=imx93frdm 和 MACHINE=imx93-11x11-lpddr4x-frdm,结果相同。我刚刚在 UART 上看到了这个日志 DEBUG: U-Boot SPL 2024.04+gde16f4f1722+p0(Sep 02 2024 - 10:44:35 +0000) SOC: 0xa1009300 LC: 0x2040010 PMIC: PCA9451A PMIC: Over Drive Voltage Mode DDR: 3733MTS DDR: 3733MTS M33 prepare ok 没有任何解决方案,也没有人提供帮助。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 你好, 请从这里尝试使用标准电路板支持包版本: https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX 另外,我建议不要使用压缩的 rootfs,请解压缩(un-zst)后再试一次。 致以最崇高的敬意/问候, Aldo。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 嗨, ,我也遇到了同样的问题。 板从 emmc 启动正常,但是当我尝试以任何方式刷新 SD 卡时它都不起作用。 我试过刷新 imx93 FRDM 主页上的一张预建图像(压缩和未压缩) 使用uuu 我也用过dd: zstd -d imx-image-full-imx93frdm.rootfs.wic.zst -c | sudo dd of=/dev/mmcblk0 bs=4M status=progress conv=fsync 然后当我从 SD 卡启动主板时它无法完全启动并停在那里 U-Boot SPL 2024.04+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000) SOC: 0xa1009300 LC: 0x2040010 PMIC: PCA9451A PMIC: Over Drive Voltage Mode DDR: 3733MTS DDR: 3733MTS M33 prepare ok 当我尝试使用 flex-installer 用基于 Debian 的镜像刷新 SD 卡时,启动后我遇到了同样的输出。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 另外,请更新我在第一篇帖子中链接的指南,以便帮助其他人 :)。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 你好!! 关于第一个问题,请注意,您不仅需要 rootfs,还需要引导加载程序,因此您需要运行类似以下的命令: ./uuu-b emmc_all flash.bin imx-image-full-imx93frdm.rootfs.wic 关于它使用 dd 这一问题,情况相同,请不要使用压缩的 rootfs(un-zst) 此致, 阿尔多。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 嗯,我觉得用你提供的最新软件和以下命令应该能行:.\uuu.exe -v uuu.auto-imx93-11x11-lpddr4x-frdm 但我不知道这是否是最好的解决方案,因为现在我的主板自称是 " imx93evk " 不是 imx93frdm。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 你好, 很高兴它现在可以运行了,我会仔细检查脚本,也许它使用了不同的引导加载程序,是的,我们正在改进 FRDM 板的文档,感谢你的评论。 致以最崇高的敬意/问候, Aldo。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 正如我之前所说,这行不通,请查看我上面的评论。 要让它正常运行的唯一方法是:.\uuu.exe -v uuu.auto-imx93-11x11-lpddr4x-frdm Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 你好, 我在试用 i.MX 93 FRDM 开发板时也遇到了这个问题。我找到的培训指南是错误的,具有误导性;演示固件包包含大量文件,但没有任何信息说明每个文件是什么;即使阅读了手册,‘uuu’实用程序的用法也几乎无法理解(至少对我来说是这样!)。 以下是我弄明白的情况。如果我理解有误,请指正。 我下载了演示固件包“ LF_v6.18.20-2.0.0_images_IMX93EVK.zip ”。我想测试将固件映像写入 uSD 卡和/或内置 eMMC 的过程。 以下方法奏效了: 我认为名称类似“ imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot ”的文件是特定板卡和不同配置的引导加载程序镜像。我选择这个是为了向我板上的uSD卡写入数据。 我认为“ imx-image-full-imx93evk.wic ”是Linux镜像(rootfs等)。只有一个,所以我猜所有支持的开发板都一样? * 根据以上评论,请勿尝试使用压缩版本“imx-image-full-imx93evk.tar.zst”? 写入uSD卡: * 关闭板电源 * 插入uSD卡 * 通过 USB-C 线缆将板的“USB1_C”端口连接到笔记本电脑。 * 将启动开关设置为[3:0] 0001以进入串行下载模式 * 使用固件文件夹中的uuu命令: # 仅将引导加载程序复制到 SD 卡: uuu -b sd imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot 或者:复制引导加载程序和 Linux 镜像: uuu -b sd_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singlebootimx-image-full-imx93evk.wic * 板上电源。UUU 应该会自动检测主板并开始下载。 要将文件写入 eMMC,您可以使用以下命令: # 仅限引导加载程序: uuu -b emcc imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot # 或者:引导加载程序和镜像: uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singlebootimx-image-full-imx93evk.wic 我不知道各种启动加载程序文件之间有什么区别。 @Kapixxx你的方法可能确实奏效了。我认为所有板都使用相同的 Linux 根文件系统,所以它们的主机名都是“imx93evk”。然而,我还没有弄明白如何使用 uuu 脚本(例如)。" uuu.auto-imx93-11x11-lpddr4x-frdm ")写入到uSD卡而不是eMMC。提供的命令行参数、内置脚本和提供的脚本文件之间的关系尚不明确。
查看全文
HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 おはよう ! FRDM i.MX 93 の入門ガイドを使って準備を進めています。 FRDM-IMX93のデモイメージをダウンロードしましたが(REV.1.0とREV4.0を試しました)、同じエラーメッセージが表示され続けます。 ガイドに記載されているコマンドを試しました: .\uuu.exe -b sd_all imx-image-full-imx93frdm.rootfs.wic.zst NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 設定ファイルに含める: PctlチップビデオPID Bcdバージョンシリアル番号 ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDPS: MX93 0x1fc9 0x014e SDPS: MX91 0x1fc9 0x0159 SDPS: MX95 0x1fc9 0x015d SDPS: MX95 0x1fc9 0x015c SDPS: MX943 0x1fc9 0x0027 SDPS: MX952 0x1fc9 0x0028 SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 FB: 0x0483 0x0afb 組み込みスクリプトを実行します: uuu_version 1.4.149 # @_flash.bin | wicイメージから抽出できるブートローダー # @_image [_flash.bin] | wic イメージを emmc に書き込みます。 # このコマンドは、i.MX6/7、i.MX8MM、i.MX8MQ の場合に実行されます SDP: boot -f imx-image-full-imx93frdm.rootfs.wic.zst/* -scanlimited 0x800000 # このコマンドは、ROMがストリームモードをサポートしている場合に実行されます # i.MX8QXP、i.MX8QM SDPS: boot -scanterm -f imx-image-full-imx93frdm.rootfs.wic.zst/* -scanlimited 0x800000 # これらのコマンドはSPLを使用する場合に実行され、SPLを使用しない場合はスキップされます # SDPU は非推奨になります。SDPU の代わりに SDPV を使用してください。 # ヤミン・アメックス SDPU: 遅延 1000 SDPU: write -f imx-image-full-imx93frdm.rootfs.wic.zst/* -offset 0x57c00 -scanlimited 0x800000 SDPU: ジャンプ -scanlimited 0x800000 # } # これらのコマンドはSPLを使用する場合に実行され、SPLを使用しない場合はスキップされます # if (SPLがSDPVをサポートしている場合) # ヤミン・アメックス SDPV: 遅延 1000 SDPV: write -f imx-image-full-imx93frdm.rootfs.wic.zst/* -skipspl -scanterm -scanlimited 0x800000 SDPV: ジャンプ -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${sd_dev} FB: ucmd mmc dev ${sd_dev} FB: flash -raw2sparse all imx-image-full-imx93frdm.rootfs.wic.zst/* FB: flash -scanterm -scanlimited 0x800000 bootloader imx-image-full-imx93frdm.rootfs.wic.zst/* FB: 完了 既知のUSBデバイスが表示されるまでお待ちください... 新しいUSBデバイスが4:2-23F11C6A09B54230に接続されました 4:2-23F11C6A09B54230>開始コマンド:SDPS: boot -scanterm -f imx-image-full-imx93frdm.rootfs.wic.zst/* -scanlimited 0x800000 ファイルの解凍:>imx-image-full-imx93frdm.rootfs.wic.zst 14%4:2-23F11C6A09B54230>HID(W)エラー: LIBUSB_ERROR_TIMEOUT (-7)(20.15秒) 次に、.\uuu.exe -v -b emmc_all .\imx-boot-imx93frdm-sd.bin-flash_singleboot .\imx-image-full-imx93frdm.rootfs.wic.zst を試しました。しかし、同じエラーメッセージも表示されました。 NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 設定ファイルに含める: PctlチップビデオPID Bcdバージョンシリアル番号 ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDPS: MX93 0x1fc9 0x014e SDPS: MX91 0x1fc9 0x0159 SDPS: MX95 0x1fc9 0x015d SDPS: MX95 0x1fc9 0x015c SDPS: MX943 0x1fc9 0x0027 SDPS: MX952 0x1fc9 0x0028 SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 FB: 0x0483 0x0afb 組み込みスクリプトを実行します: uuu_version 1.4.149 # @_flash.bin | wicイメージから抽出できるブートローダー # @_image [_flash.bin] | wic イメージを emmc に書き込みます。 # このコマンドは、i.MX6/7、i.MX8MM、i.MX8MQ の場合に実行されます SDP: boot -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -scanlimited 0x800000 # このコマンドは、ROMがストリームモードをサポートしている場合に実行されます # i.MX8QXP、i.MX8QM SDPS: boot -scanterm -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -scanlimited 0x800000 # これらのコマンドはSPLを使用する場合に実行され、SPLを使用しない場合はスキップされます # SDPU は非推奨になります。SDPU の代わりに SDPV を使用してください。 # ヤミン・アメックス SDPU: 遅延 1000 SDPU: write -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -offset 0x57c00 SDPU: ジャンプ -scanlimited 0x800000 # } # これらのコマンドはSPLを使用する場合に実行され、SPLを使用しない場合はスキップされます # if (SPLがSDPVをサポートしている場合) # ヤミン・アメックス SDPV: 遅延 1000 SDPV: write -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -skipspl -scanterm -scanlimited 0x800000 SDPV: ジャンプ -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all .\imx-image-full-imx93frdm.rootfs.wic.zst/* FB: flash -scanterm -scanlimited 0x800000 bootloader .\imx-boot-imx93frdm-sd.bin-flash_singleboot FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: 完了 既知のUSBデバイスが表示されるまでお待ちください... 新しいUSBデバイスが4:2に接続されました。 4:2->開始コマンド:SDPS: boot -scanterm -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -scanlimited 0x800000 4:2->HID(W)エラー: LIBUSB_ERROR_TIMEOUT (-7)(20.02秒) 最新バージョンのuuu.exeを使用しています。また、Windowsには新しいドライバもインストールされています。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 こっちも一緒。Ubuntu 20.04で試してみましたが、同じエラーが発生しました。 sudo ~/uuu-ubuntu20.04 -lsusb NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 コネクテッド Known USB Devices パス チップ プロ ビデオ Pid BcdVersion シリアル番号 ==================================================================== 1:3 MX93 SDPS: 0x1FC9 0x014E 0x0001 8214D79A2FFA4708 sudo ~/uuu-ubuntu20.04 -b emmc_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singlebootimx-image-core-imx93-11x11-lpddr4x-frdm.rootfs-20260608162024.wic.zst NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 成功 0 失敗 1 1:3-8214D79A 1/1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -scanterm -f imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash... MACHINE=imx93frdmとMACHINE=imx93-11x11-lpddr4x-frdmの両方を試しましたが、結果は同じでした。UART DEBUGに以下のログが表示されました。 U-Boot SPL 2024.04+gde16f4f1722+p0(2024年9月2日 10:44:35 +0000) SOC: 0xa1009300 LC: 0x2040010 PMIC: PCA9451A PMIC: オーバードライブ電圧モード DDR: 3733MTS DDR: 3733MTS M33準備OK どこにも解決策はなく、誰も助けてくれない。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 こんにちは、 こちらの標準BSPリリースをお試しください。 https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX また、圧縮されたルートファイルシステムは使用せず、解凍(un-zst)してから再度試すことをお勧めします。 よろしくお願いいたします。 アルド。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 こんにちは、 私も同じ問題に直面しています。 ボードはeMMCから正常に起動するのですが、SDカードに何らかの方法で書き込もうとしても動作しません。 imx93 FRDMのメインページにある、あらかじめビルドされたイメージ(圧縮版と非圧縮版)のいずれかをフラッシュしてみました。 uuuを使用しています 私もddを使いました: zstd -d imx-image-full-imx93frdm.rootfs.wic.zst -c | sudo dd of=/dev/mmcblk0 bs=4M status=progress conv=fsync SDカードからボードを起動しても、完全に起動せず、そこで停止します。 U-Boot SPL 2024.04+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000) SOC: 0xa1009300 LC: 0x2040010 PMIC: PCA9451A PMIC: Over Drive Voltage Mode DDR: 3733MTS DDR: 3733MTS M33 prepare ok そして、flex-installerを使ってDebianベースのイメージをSDカードに書き込もうとしたところ、起動後に同じ出力が表示されました。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 こんにちは、 動作するようになってよかったです。スクリプトをもう一度確認してみます。もしかしたら別のブートローダーを使っているかもしれません。FRDMボードのドキュメントの改善に取り組んでいますので、ご意見ありがとうございます。 よろしくお願いいたします。 アルド。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 ええと、あなたがリンクした最新のソフトウェアとコマンド「.\uuu.exe -v uuu.auto-imx93-11x11-lpddr4x-frdm」でうまくいったと思います。 しかし、これが最善の解決策かどうかはわかりません。なぜなら、私のボードは現在、imx93frdmではなく「imx93evk」として認識されるからです。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 こんにちは!! 最初の問題については、rootfsだけでなくブートローダーも必要となるため、次のようなコマンドを実行する必要があることにご注意ください。 ./uuu-b emmc_all flash.bin imx-image-full-imx93frdm.rootfs.wic ddを使用するという問題については、圧縮されたrootfs(un-zst)を使用しないでください。 よろしくお願いいたします。 アルド。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 また、他の人の役に立つよう、最初の投稿でリンクしたガイドを更新してください。 Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 先ほど申し上げた通り、うまくいっていません。上記の私のコメントをご確認ください。 これを機能させる唯一の方法は、次のコマンドを実行することです。.\uuu.exe -v uuu.auto-imx93-11x11-lpddr4x-frdm Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 こんにちは、 私も同じ問題に直面しました。i.MX 93年の開発ボードを試しているときに。見つけたトレーニングガイドは誤っていて誤解を招くものでしたし、デモのファームウェアパッケージには何が何であるかの情報がほとんどないファイルが山のように入っていて、「uuu」というユーティリティの使い方は(少なくとも私には)ほとんど理解できません。マニュアルを読んでもそうです。 私が分かったことは以下のとおりです。もし私の理解が間違っていたら、どなたか訂正してください。 デモ版のファームウェアパッケージ「LF_v6.18.20-2.0.0_images_IMX93EVK.zip」をダウンロードしました。uSDカードや内蔵eMMCにファームウェアイメージを書き込むプロセスをテストしたいと思いました。 効果があったのは以下のとおりです。 * 「 imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot 」のような名前のファイルは、特定のボードや異なる構成用のブートローダーイメージだと思います。このモデルはボードのuSDカードに書き込みするために選びました。 * 「imx-image-full-imx93evk.wic」はLinuxのイメージ(rootfsなど)だと思います。一つしかないので、サポートされている開発ボードは全て同じだと思います。 * 上記のコメントにあるように、圧縮版の「imx-image-full-imx93evk.tar.zst」を使用しないでください。 uSDカードに書き込むには: * ボードの電源がオフになっています * uSDカードを挿入してください * ボードの「USB1_C」ポートをUSB-CケーブルでノートPCに接続 * シリアルダウンロードモード用にブートスイッチを [3:0] 0001 に設定 * ファームウェアフォルダから以下のuuuコマンドを使用してください。 # ブートローダーのみをSDカードにコピーします。 uuu -b sd imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot # または:ブートローダーとLinuxイメージをコピーしてください: uuu -b sd_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singlebootimx-image-full-imx93evk.wic * ボード上の電源。UUUは自動的にボードを検出し、ダウンロードを開始するはずです。 eMMCにファイルを書き込むには、以下のコマンドを使用します。 # ブートローダーのみ: uuu -b emcc imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot # または: ブートローダーとイメージ: uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singlebootimx-image-full-imx93evk.wic 様々なブートローダーファイルの違いが分かりません。 @Kapixxx  あなたの方法はおそらく効果があったでしょう。すべてのボードは同じLinuxのrootfsを使っているので、ホスト名はすべて「imx93evk」になっていると思います。しかし、uuuスクリプトの使い方がわかりません(例:"uuu.auto-imx93-11x11-lpddr4x-frdm")eMMCではなくuSDカードに書き込みをする。指定されたコマンドラインパラメータ、組み込みスクリプト、および指定されたスクリプトファイル間の関係は不明瞭である。
查看全文
HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Good Morning ! I am trying to get ready with FRDM i.MX 93 with getting started guide: Guide I downloaded FRDM-IMX93 Demo Images (tried REV.1.0 and REV4.0), but keep getting same error message.  Tried command from guide: .\uuu.exe -b sd_all imx-image-full-imx93frdm.rootfs.wic.zst uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Build in config: Pctl Chip Vid Pid BcdVersion Serial_No ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDPS: MX93 0x1fc9 0x014e SDPS: MX91 0x1fc9 0x0159 SDPS: MX95 0x1fc9 0x015d SDPS: MX95 0x1fc9 0x015c SDPS: MX943 0x1fc9 0x0027 SDPS: MX952 0x1fc9 0x0028 SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 FB: 0x0483 0x0afb Run built-in script: uuu_version 1.4.149 # @_flash.bin | bootloader, which can extract from wic image # @_image [_flash.bin] | wic image burn to emmc. # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f imx-image-full-imx93frdm.rootfs.wic.zst/* -scanlimited 0x800000 # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM SDPS: boot -scanterm -f imx-image-full-imx93frdm.rootfs.wic.zst/* -scanlimited 0x800000 # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f imx-image-full-imx93frdm.rootfs.wic.zst/* -offset 0x57c00 -scanlimited 0x800000 SDPU: jump -scanlimited 0x800000 # } # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f imx-image-full-imx93frdm.rootfs.wic.zst/* -skipspl -scanterm -scanlimited 0x800000 SDPV: jump -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${sd_dev} FB: ucmd mmc dev ${sd_dev} FB: flash -raw2sparse all imx-image-full-imx93frdm.rootfs.wic.zst/* FB: flash -scanterm -scanlimited 0x800000 bootloader imx-image-full-imx93frdm.rootfs.wic.zst/* FB: done Wait for Known USB Device Appear... New USB Device Attached at 4:2-23F11C6A09B54230 4:2-23F11C6A09B54230>Start Cmd:SDPS: boot -scanterm -f imx-image-full-imx93frdm.rootfs.wic.zst/* -scanlimited 0x800000 Decompress file:>imx-image-full-imx93frdm.rootfs.wic.zst 14%4:2-23F11C6A09B54230>Fail HID(W): LIBUSB_ERROR_TIMEOUT (-7)(20.15s) Then I tried .\uuu.exe -v -b emmc_all .\imx-boot-imx93frdm-sd.bin-flash_singleboot .\imx-image-full-imx93frdm.rootfs.wic.zst, but also got same error meassage: uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Build in config: Pctl Chip Vid Pid BcdVersion Serial_No ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDPS: MX93 0x1fc9 0x014e SDPS: MX91 0x1fc9 0x0159 SDPS: MX95 0x1fc9 0x015d SDPS: MX95 0x1fc9 0x015c SDPS: MX943 0x1fc9 0x0027 SDPS: MX952 0x1fc9 0x0028 SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 FB: 0x0483 0x0afb Run built-in script: uuu_version 1.4.149 # @_flash.bin | bootloader, which can extract from wic image # @_image [_flash.bin] | wic image burn to emmc. # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -scanlimited 0x800000 # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM SDPS: boot -scanterm -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -scanlimited 0x800000 # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -offset 0x57c00 SDPU: jump -scanlimited 0x800000 # } # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -skipspl -scanterm -scanlimited 0x800000 SDPV: jump -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all .\imx-image-full-imx93frdm.rootfs.wic.zst/* FB: flash -scanterm -scanlimited 0x800000 bootloader .\imx-boot-imx93frdm-sd.bin-flash_singleboot FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: done Wait for Known USB Device Appear... New USB Device Attached at 4:2- 4:2->Start Cmd:SDPS: boot -scanterm -f .\imx-boot-imx93frdm-sd.bin-flash_singleboot -scanlimited 0x800000 4:2->Fail HID(W): LIBUSB_ERROR_TIMEOUT (-7)(20.02s) I am using latest uuu.exe version. Also with new drivers on windows. Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Same here. I'm trying with Ubuntu 20.04 and same error occured. sudo ~/uuu-ubuntu20.04 -lsusb uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Connected Known USB Devices Path Chip Pro Vid Pid BcdVersion Serial_no ==================================================================== 1:3 MX93 SDPS: 0x1FC9 0x014E 0x0001 8214D79A2FFA4708 sudo ~/uuu-ubuntu20.04 -b emmc_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot imx-image-core-imx93-11x11-lpddr4x-frdm.rootfs-20260608162024.wic.zst uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Success 0 Failure 1 1:3-8214D79A 1/ 1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -scanterm -f imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash... I tried both with MACHINE=imx93frdm and MACHINE=imx93-11x11-lpddr4x-frdm and same result. I just see this log on UART DEBUG: U-Boot SPL 2024.04+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000) SOC: 0xa1009300 LC: 0x2040010 PMIC: PCA9451A PMIC: Over Drive Voltage Mode DDR: 3733MTS DDR: 3733MTS M33 prepare ok There's no solution anywhere and no one is helping. Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Hello, Please try with the standard BSP release from here: https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX Also, I would rather recommend to not use the compressed rootfs, please uncompress (un-zst) and try again. Best regards/Saludos, Aldo. Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Hi,  I am facing the same problem.  The board is booting fine from the emmc but when I try to flash the SD card in any way it does not work. I tried flashing one of the pre-built images on the imx93 FRDM main page (compressed and un-compressed) using uuu I also used dd:  zstd -d imx-image-full-imx93frdm.rootfs.wic.zst -c | sudo dd of=/dev/mmcblk0 bs=4M status=progress conv=fsync then when I boot the board from the SD card it does not fully boot and stops there U-Boot SPL 2024.04+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000) SOC: 0xa1009300 LC: 0x2040010 PMIC: PCA9451A PMIC: Over Drive Voltage Mode DDR: 3733MTS DDR: 3733MTS M33 prepare ok And I faced this same output after booting up when I tried flashing the SD card with the Debian-based image using flex-installer. Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Hello!! For the first issue, please note that you'll need the bootloader not only the rootfs, so you'll need to run a command like the following: ./uuu -b emmc_all flash.bin imx-image-full-imx93frdm.rootfs.wic For the issue that it uses dd, is the same please do not use compressed rootfs (un-zst) Best regards/Saludos, Aldo. Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Also please update the guide I linked in first post to help others :). Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Hello, Glad that it is now working, I will double check the script maybe it uses a different bootloader, and yes we are working on improvingthe documentation for the FRDM boards we apreciate your comments. Best regards/Saludos, Aldo. Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Well I think it worked with the latest software You linked and command: .\uuu.exe -v uuu.auto-imx93-11x11-lpddr4x-frdm But I don't know is it the best solution, because now my board introduces itself as "imx93evk" not imx93frdm. Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 As I told it is not working, check my comment above. The only way to make it work is: .\uuu.exe -v uuu.auto-imx93-11x11-lpddr4x-frdm Re: HID(W): LIBUSB_ERROR_TIMEOUT (-7) FRDM i.MX 93 Hi, I have run into this problem as well, trying out a i.MX 93 FRDM development board. The training guide I found was wrong and misleading, the demo firmware package contains a pile of files with no info as to what each one is, and the usage of the "uuu" utility is almost incomprehensible (at least to me!), even after reading the manual for it.  Here's what I have figured out.  Someone please correct me if I got this wrong. I downloaded the demo firmware package "LF_v6.18.20-2.0.0_images_IMX93EVK.zip". I wanted to test the process of writing a firmware image to the uSD card and/or the built-in eMMC. Here is what worked: * I think files with names like "imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot" are bootloader images for specific boards and different configurations. I chose this one for writing to uSD card on my board. * I think "imx-image-full-imx93evk.wic" is the Linux image (rootfs, etc). There is only one, so I guess it's the same for all supported dev boards? * As per comments above, don't try to use the zipped version "imx-image-full-imx93evk.tar.zst"? To write to uSD card: * Power off board * Insert uSD card * Connect board "USB1_C" port to laptop via USB-C cable * Set boot switches to [3:0] 0001 for serial download mode * Use this uuu command from the firmware folder: # Copy BOOTLOADER ONLY to the SD card: uuu -b sd imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot # OR: Copy bootloader and linux image: uuu -b sd_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot imx-image-full-imx93evk.wic * Power on the board. UUU should automatically detect the board and start the download. For writing the files to eMMC, you use these commands: # Bootloader Only: uuu -b emcc imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot # OR: Bootloader and Image: uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-frdm-sd.bin-flash_singleboot imx-image-full-imx93evk.wic I don't know what the difference is between the various boot loader files. @Kapixxx   Your method probably did work. I think all the boards use the same Linux rootfs so they all have the host name "imx93evk". However, I have not figured out how to use a uuu script (e.g. "uuu.auto-imx93-11x11-lpddr4x-frdm") to write to uSD card rather than eMMC. The relationship between the supplied command line parameters, built-in scripts, and supplied script files is unclear.
查看全文
UG10215 lists imx708 as supported — which kernel driver should be used? Hi, I'm working on integrating a Raspberry Pi Sony IMX708 camera on an i.MX 95 based board, following UG10215 (i.MX 95 Camera Porting Guide). The document's "List of camera sensors modules supported" table lists the Raspberry Pi Sony imx708 as a supported reference camera module. However, I couldn't find a corresponding driver (e.g. imx708.c) in the linux-imx repository (branch lf-6.18.y😞 https://github.com/nxp-imx/linux-imx/commits/lf-6.18.y/drivers/media/i2c Could you clarify which kernel driver is expected to be used for the imx708 sensor on the i.MX 95? Is the IMX708 driver included in the public BSP? Thanks in advance. Re: UG10215 lists imx708 as supported — which kernel driver should be used? Hello, We do not have it officially supported yet in our standard BSP, you can take the driver from raspberry sources and use it: https://github.com/raspberrypi/linux/blob/rpi-6.12.y/drivers/media/i2c/imx708.c Best regards/Saludos, Aldo. Re: UG10215 lists imx708 as supported — which kernel driver should be used? Hi Aldo, thanks for your reply. We do not have it officially supported yet in our standard BSP Will it be supported in the future? Why is the IMX708 camera listed in UG10215 if support is not included in the standard BSP? Thanks again Diego Re: UG10215 lists imx708 as supported — which kernel driver should be used? Hello, Yes it is planned to be added but, unfortunately, I do not have a due date/version when its going to be added to the standard BSP release. The reason that it appears in the guide is because is one of the cameras that was tested in early development but was not fully supported in our BSP. Best regards/Saludos, Aldo.
查看全文
SPI用のDMAを設定する必要があります 私はS32DS IDEとRTD 3.0を使っています。SPIでDMAを起動する方法や、ステップバイステップの手順や、もしあれば他の例コードがあれば教えてもらえますか? Re: I need to configure DMA for SPI ご回答ありがとうございます。 この作業はs32k322 MCUで行ってください Re: I need to configure DMA for SPI こんにちは@ershi RTDにはDMAを用いたSPI通信用の2つの例コードが付属しており、1つは低レベルドライバ(Ip)を用い、もう1つは高レベルドライバ(MCAL)を使用します。例のインポート方法については、HOWTO: S32 Design Studio - Create a New S32DS Project from Example Threadを参照してください。 また、スレッドの 例であるS32K31 SPI Multiple Packet Transmit and Receive: Solution for DMA Cache Issueの例を参照することもできます。 BR、VaneB Re: I need to configure DMA for SPI こんにちは@ershi これらの例はS32K322向けに特別に設計されているわけではありませんが、リファレンス・マニュアルに特に記載されていない限り、S32K3 ファミリ全体で機能性は概ね同じです。したがって、このプロジェクトを実装の参考として活用し、必要に応じてデバイスに合わせて調整することができます。 Re: I need to configure DMA for SPI すべて設定しましたが、最初は動作せず、(Lpspi_Ip_AsyncTransmit)でLPSPI_IP_STATUS_SUCCESSとして返され、2回目は失敗と表示されますLPSPI_IP_STATUS_FAIL、DMAなしでこのAPIを使ってデータをSPI経由で送信できますLpspi_Ip_SyncTransmit()いくつかの設定スクリーンショットを添付しました。 Re: I need to configure DMA for SPI こんにちは@ershi RMやIntCtrl_Ipドライバーの設定画像も共有してもらえますか? Re: I need to configure DMA for SPI こんにちは、 @VaneBさん RMとIntCtrl_IPドライバの設定のスクリーンショットと、詳細な参考のために短い動画クリップを添付しました。 LPSPIの設定ページで1つの違いに気づきました。SPI GeneralタブのSpi_Phy_TxDmaChannelの項目で、TX設定とRX設定で名前が異なっています。 追加情報が必要な場合はお知らせください。 InterruptsInterruptsInterruptsInterruptsInterruptsInterruptsInterrupts割り込み RMRMRMRMRMRMRMRM Re: I need to configure DMA for SPI こんにちは@ershi 情報を共有していただきありがとうございます。 一つだけ気づいたことがあります。Dma_Ipドライバー構成では、DMA_SPI_CALLBACK_0を割り込みコールバックとして定義しています。しかし、LPSPI DMAのコールバックはドライバーから既に提供されており、Lpspi_Ip_Irq.cで見つけることができますファイル。 LPSPI2の場合、設定するコールバックは以下のとおりです。 TX DMAチャネルのLpspi_Ip_LPSPI_2_IrqTxDmaHandler RX DMAチャネルのLpspi_Ip_LPSPI_2_IrqRxDmaHandler Re: I need to configure DMA for SPI こんにちは、 @VaneBさん ご説明いただきありがとうございます。 Dma_Ip設定を更新し、LPSPI2ではTXとRX DMAチャネルがLpspi_Ip_Irq.cからのコールバックを使うようになりました。 TX DMAチャネルのLpspi_Ip_LPSPI_2_IrqTxDmaHandler RX DMAチャネルnxpのLpspi_Ip_LPSPI_2_IrqRxDmaHandler しかしながら、私の環境ではDMAベースのLPSPI転送が期待通りに動作していません。参考までに、現在の設定画面のスクリーンショットを添付しました。他に調整すべき設定があれば教えてください。 Re: I need to configure DMA for SPI こんにちは@ershi SPIコミュニケーションをどのように実装しているのか教えていただけますか?また、以前共有したサンプルコードをテストしてみましたか? Re: I need to configure DMA for SPI こんにちは、 @VaneBさん 以前の設定を削除し、SPIデータはDMA経由で送信されるようになりましたが、データが一致しないという問題が発生しています。 #define RX_MSG_SIZE (15U) #define TX_MSG_SIZE (15U) uint8_t txBuffer_check[TX_MSG_SIZE] = {0x48,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x10,0x11,0x12,0x13,0x14,0x15}; uint8_t rxBuffer_check[]={0}; if(Lpspi_Ip_AsyncTransmit(&Lpspi_Ip_DeviceAttributes_SpiExternalDevice_1_Instance_2_BOARD_InitPeripherals,txBuffer_check,rxBuffer_check,TX_MSG_SIZE,spi_DMA_Function) == LPSPI_IP_STATUS_SUCCESS) { Dma_Ip_ReturnType status = {0},status1 = {0}; Dma_Ip_LogicChannelStatusType channelStatus ={0},channelStatus1 ={0}; status = Dma_Ip_GetLogicChannelStatus(DMA_LOGIC_CH_0,&channelStatus); status1 = Dma_Ip_GetLogicChannelStatus(DMA_LOGIC_CH_1,&channelStatus1);   return SYS_SUCCESS; } Re: I need to configure DMA for SPI こんにちは@ershi LPSPI2のSOUT信号をSINに直接接続していますか、それともロジックアナライザを使用して送受信データを検証していますか? Re: I need to configure DMA for SPI こんにちは、 @VaneB さん。 コードを書き直したところ、今は完璧に動作しています。データは正しく入力されています。 ご協力ありがとうございました。
查看全文
Ara240 16GB M.2 模块 Ara240 16GB M.2 模块官方支持哪些量化精度?(INT4、8、16) Re: Ara240 16GB M.2 Module 根据Ara240 离散神经处理单元数据表 精确测量 官方文件支持 INT4 未找到相关文档支持 INT8 支持 INT16 支持 INT32 虽然不在您的 INT4/8/16 列表中,但已支持。
查看全文
SDAファームウェアに関する質問 FRDM-A-S32K358の開発ボードを購入し、Open SDAを担当するMK26チップのファームウェアを変更するためにJTAGポートを確認しました。もし誤ってJ13にファームウェアをインストールしてしまった場合、Open SDAのファームウェアを入手する必要があります。この場合、サポートチケットを通じてファームウェアを入手できますか? Re: Open SDA Firmware Question こんにちは、 @wj_kwak MK26 OpenSDAデバイスがJ13経由で上書きされた場合、正常に動作するOpenSDAブートローダーを前提としているため、標準のOpenSDAアップデート手順は適用できなくなる可能性があります。OpenSDAのリカバリファームウェアは、通常、単体のプログラミングイメージとしては配布されていません。 OpenSDAのファームウェアとブートローダーは、NXPが開発したソフトウェアではなくPEmicro技術です。PEmicroはOpenSDAのファームウェアアップデート、ブートローダー更新アプリケーション、関連サポートを提供しています。 したがって、MK26がJTAG/SWDで消去または再プログラムされ、OpenSDAブートローダーが機能しなくなった場合、回復案内やファームウェアの入手は主にPEmicroが担当となります。 https://www.pemicro.com/support/index.cfm よろしくお願いいたします。 ルーカス
查看全文
ライブラリを追加する CodeWarriorから移行したばかりで、新しいiMacにMCUXをインストールしたばかりです。私は赤外線リモコンを含む新しいプロジェクトに取り組んでおり、IRemoteライブラリ(GitHubから入手)を使用したいと考えています。ライブラリファイルはダウンロードしましたが、SDK_2.x_LPCXpresso824MAX(私が使っている開発ボード)には追加できません。「静的ライブラリの作成と使用方法」というドキュメントの手順に従ったのですが、手順とスクリーンショットは私のものよりかなり古いバージョンのもののようです。 私の問題を解決してくれるような「初心者向けガイド」を持っている人はいませんか? Re: Add a library こんにちは、 ライブラリにはどのようなファイル形式がありますか?拡張子は.aですか、それとも.hですか? 「ユーザーアプリケーションにユーザー静的ライブラリを追加する」第2章( MCUXpresso IDEで静的ライブラリの作成と使用 方法)の5ページで述べた手順は、新しいバージョンのMCUXpresso IDEにも引き続き適用されます。ガイドに示されているウィンドウは最近のMCUXpressoバージョンでも同じです。手順に問題がありますか? また、どのバージョンを使っているのか確認してもらえますか? SDKに関しては、「SDK_2.x_」と書いたのですね。どの古いバージョンを使っているか確認してもらえますか?最新のSDKバージョン26.06を使うようにアップデートすることもできます。SDK Builderからダウンロードできます 敬具、ルイス Re: Add a library これは私の問題の一部です。ファイルには拡張子がなく、単に「IRemote-4.7.1」という名前で、ダウンロードフォルダ内ではフォルダとして表示されます。古いバージョンのSDKを使っているとは思いません。バージョンは26.06.00です。もしかすると、実際のIRemoteライブラリを読み込んでいないのかもしれません。ただダウンロードボタンを押してしまっただけかもしれません Re: Add a library Hello おそらくライブラリのGithubフォルダ全体をダウンロードしていると思います。通常、Githubユーザーは.h/.c/.hpp/.cppを保存します。srcフォルダ内のなど。 必要な.h/.aファイルだけをsrcフォルダからダウンロードするか、Githubで検索するだけで、Githubプロジェクト全体をダウンロードせずに、ガイドに従ってライブラリとリンクへのパスを追加できます。 敬具、ルイス
查看全文