Problem with DDRv tool on LS1088A Hi, I am trying to validate a new type of DDR4 SO-DIMM on a custom board based on LS1088A SoC, but I am encountering problems with DDRv. I have already validated several other models of DDR4 in the past, and I did not encounter any problems. The new model of DDR that I am trying to validate is IMM2G72D4SOD8AG-B075I from Memphis. Its speed-grade is 2,666, but we would like to run it at 2,100 MT/s. I have created a new QorQ configuration project and successfully read DDR configuration via SPD. However, the first step (Centering the clock) consistently fails at 0.04%, on the 'Auto search & detect for write leveling start values' part. In the Test Results summary, I see that the test failed with the reason: "DDR interface is failing due to an issue other than WRLVL_START values, please investigate HW issues on the board." In the Logs section, I see the following information: #################### Result for: wrlvl_searcher ###### Run 1 ###################################### Test result: [ ============================================================ Updated: WRLVL_CNTL = 0x86550605, WRLVL_CNTL_2 = 0x00000000, WRLVL_CNTL_3 = 0x00000000, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x86550607, WRLVL_CNTL_2 = 0x09060C0F, WRLVL_CNTL_3 = 0x0E110B0E, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x86550607, WRLVL_CNTL_2 = 0x09050C0F, WRLVL_CNTL_3 = 0x1611130E, SDRAM_CLK_CNTL = 0x02800000 DDR interface is failing due to an issue other than WRLVL_START values, please investigate HW issues on the board. < > {{DDR interface is failing due to an issue other than WRLVL_START values, please investigate HW issues on the board.}} Err. capture registers: 0xE20, 0x00000000 0xE24, 0x00000000 0xE28, 0x00000000 0xE40, 0x00000080 0xE44, 0x00000000 0xE48, 0x0000001D 0xE4C, 0x00000000 0xE50, 0x00000000 0xE54, 0x00000000 0xE58, 0x00010000 Dump: 0xF00, 0x00000000 0xF04, 0x00001002 0xF08, 0x0000000A 0xF0C, 0x14000C20 0xF10, 0x00000000 0xF14, 0x00000000 0xF18, 0x00000000 0xF1C, 0x00000000 0xF20, 0x00000000 0xF24, 0x2F003500 0xF28, 0x2A003600 0xF2C, 0x3E004A00 0xF30, 0x44004600 0xF34, 0x3A007000 0xF38, 0x00000000 0xF3C, 0x00000000 0xF40, 0x00000000 0xF44, 0x00000000 0xF48, 0x00000001 0xF4C, 0x94000000 0xF50, 0x0F001300 0xF54, 0x0C001800 0xF58, 0x1F002C00 0xF5C, 0x22002700 0xF60, 0x1C000000 0xF64, 0x00009000 0xF68, 0x00000020 0xF6C, 0x00000000 0xF70, 0x0060007B 0xF74, 0x00000000 0xF78, 0x00000000 0xF7C, 0x00000000 0xF80, 0x00000000 0xF84, 0x00000000 0xF88, 0x00000000 0xF8C, 0x00000000 0xF90, 0x00000000 0xF94, 0x80000000 0xF98, 0x00000000 0xF9C, 0x29002B00 0xFA0, 0x2B002B00 0xFA4, 0x27002D00 0xFA8, 0x28002E00 0xFAC, 0x27000000 0xFB0, 0x10000003 0xFB4, 0x42344241 0xFB8, 0x40334332 0xFBC, 0x43404150 0xFC0, 0x00004133 0xFC4, 0x44424444 0xFC8, 0x44415134 0xFCC, 0x51414251 0xFD0, 0x42414241 0xFD4, 0x50434252 0xFD8, 0x50444342 0xFDC, 0x42413444 0xFE0, 0x43514340 0xFE4, 0x44424444 0xFE8, 0x42514441 0xFEC, 0x40423443 0xFF0, 0x43424342 0xFF4, 0x43415042 0xFF8, 0x51415341 0xFFC, 0x54000D0D Data: 0x00000005 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 ] I have attached the verbose CCS log from the failed validation procedure as well. Could you please explain what this means and how we can debug the issue? QorIQ LS1 Devices Re: Problem with DDRv tool on LS1088A Compare with new type of DDR4 SO-DIMM, what kind of SODIMM used before? Any change between the new one and the old one Re: Problem with DDRv tool on LS1088A Hello,
For your specific dump, the most actionable interpretation is: the controller raised an automatic calibration error ( ACE ) during training, and DDRv’s write-leveling search could not find a valid operating region by adjusting WRLVL_START . That points first to reset/clock/configuration/DQ-map/SI checks, with DDR reset and DQn_MAP high on the list because both are repeatedly tied to this exact DDRv failure class in NXP debug history. So, verify DDR clock/RCW, DDR reset timing, SPD-derived rank/geometry, DQ mapping, and power/SI before tuning margins.
Regards
查看全文