Hi. I'm looking for the schematic for S32K144EVB-Q100 Rev D. I cannot seem to make the board send any CAN messages. Is there sample code available to send message on CAN 0 on that board? I was able to use SPI and confirm the CAN transceiver is in forced normal mode so CAN should be working.
You may check the sample code at S32DS for S32K144EVB... Please share if any since i can not found it...
Hello @rosejp03,
I've sent you a private message on the community regarding the design files.
Regarding the CAN functionality, Rev. C (the current board I am using) & Rev. D have the same exact CAN design and transceiver (UJA1169):
S32K144EVB-Q100 Rev. DS32K144EVB-Q100 Rev. DS32K144EVB-Q100 Rev. D
S32K144EVB Rev. C1S32K144EVB Rev. C1S32K144EVB Rev. C1
Are you using any existing example? Either the AN5413: S32K1xx Series Cookbook or the ones included through the RTD package?
Are you using the 12V jack connector? Change J107 position to 1-2 and power the board with 12V.
How are you testing CAN communication? Are you using another EVB, a CAN analyzer, or anything else? Can you try scoping the bus?
Best regards,
Julián
Hi @db16122,
If you also need the design files for S32K144EVB Rev. D, please let me know.
Best regards,
Julián