Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
GUI Guider画面(i.MX RT)で短いループ状の製品動画を表示する i.MX RTボード上で動作するGUI Guiderプロジェクトのアイドル画面で、約10秒ほどの短いループ状の製品デモクリップをお見せしたいと思います。これらのクリップは、Nereo( https://www.nereo.io/ )などのAIビデオツールを使用して作成された短いマーケティングビデオです。したがって、ソースは通常のH.264 MP4です。 質問: GUI Guiderでは、MP4を画像シーケンスに変換してアニメーション画像ウィジェットを使用する方法が推奨されていますか?それとも、より適切な方法(例えばMJPEG/AVIプレーヤーなど)はありますか? RT1170 / RT1060 i.MX タッチの応答性に影響を与えずに現実的なフレームレートと解像度はどれくらいでしょうか? この用途でフレームを外部フラッシュに保存するのとSDカードで保存する方法について、何かアドバイスはありますか? 参考になる例やアプリの説明書などがあれば教えていただけると助かります。 Re: Showing a short looping product video on a GUI Guider screen (i.MX RT) こんにちは、 @nereostudio さん。 1.このような用途には推奨される方法です。 2. 期待されるFPSや解像度は、ディスプレイインターフェースの帯域幅や色深度、選択したMCUコアと周波数、グラフィックスパイプラインでアクセラレータの使用状況、表示される追加ウィジェット数やウィジェットの複雑さなど、多くの変数に依存します。とはいえ、RT1170は明らかにRT1060よりも性能が優れているので、安定した30fpsを維持したいならRT1170を選ぶことをおすすめします。さらに、望ましい仕様に達していない場合に性能を確保するための多くの方法があり、それらはユーザーガイドの以下のセクションで説明されています:パフォーマンス最適化 — GUI Guiderドキュメント 3. GUI Guiderはデフォルトで画像を.cファイルに変換します。GUIの他の部分と一緒に1つのバイナリファイルとして構築され、フラッシュに保存されるファイルなので、特に心配する必要はありません。
View full article
Huge power consumption on RTC ofLPCXpresso54S018M EVB. I use are LPCXpresso54S018M EVB. I need the RTC in the LPC54018 to work after the main power supply is removed. I initialized and enabled the RTC in my firmware. I powered the VBATT line (J10:11) with a coin cell battery CR2032. While the main power is present, the VBATT line consumption is == 0. It's Ok. However, after removing the main power supply, the VBATT line consumption increases up to ~41 uA! According to the datasheet, consumption should be less than 1 uA. Why? How can I achieve current consumption of 1 µA or less? LPC54xxx Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. Hi @jcxz  The ~41 µA is most likely leakage through the RESETN circuitry , not RTC consumption. When main power is removed, VBAT > VDD; If VBAT> VDD, the external reset pin must be floating to prevent high VBAT leakage. The LPCXpresso54S018M-EVK connects RESETN to its pushbutton/debug circuitry, so the unmodified EVK does not satisfy that measurement condition. To reduce the current: Isolate the MCU’s RESETN pin from the EVK reset network. BR Harry Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. I read about this requirement in the datasheet (If VBAT> VDD, the external reset pin must be floating to prevent high VBAT leakage). But I don't understand how to achieve this? I'm not talking about a EVB schematic. EVB - only for prototyping. But in our working device's circuit, MCU RESETN will be connected direct to the RST output of the external WDT-chip (TPS3823-33DBVR). Can you recommend: How to correct the connection MCU.RESETN <-> WDT.RST connection's schematic so, that the VBAT current consumption does not exceed 1 µA? I am attaching a schematic of the WDT <-> MCU.RESETN interconnection in my device: In this picture, the wire named "Reset" is connected to the RESETN pin of the LPC54005JBD100. Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. Hi @jcxz  "Floating" here means that RESETN should have no external DC path during battery-only operation (VBAT present, VDD removed). The MCU's internal reset pull-up does not need to be disabled; the datasheet already accounts for that condition. In the proposed watchdog circuit, RESETN remains connected to the unpowered TPS3823 output as well as the external RC network. Therefore, the datasheet condition of a floating RESETN pin is not met. This is a plausible explanation for the observed ~41 µA current, although the exact leakage path has not yet been experimentally verified. To meet the datasheet condition, we recommend inserting a normally-open isolation switch between the watchdog reset output and the MCU RESETN pin. All external reset components (pull-up resistor, capacitor, watchdog output, etc.) should remain on the watchdog side of the switch, while the MCU side should not contain any external pull-up, pull-down, capacitor, or other DC connection. The selected switch should explicitly support a low-leakage, high-impedance state when its supply voltage is removed. BR Harry Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. Thanks for your help, Harry_Zhang! Following your recommendations, we created the following circuit: Do you think - this circuit is correct? Will the LPC54005's power consumption with this RESETN circuit be less than 1 μA (from VBAT pin)?
View full article
S32K344 EVB HDQFP172 的 ADC 配置 您好, 我想执行连接到板载电位器的 ADC 通道ADC0_P7 ,并将转换后的值用于调暗板载 LED( GPIO29 )。 配置完成后,显示如下内容: 错误: platform.driver.pins 此外,在配置完成后构建项目时,我们遇到了以下编译错误:image(error_Adc) 我还附上了下面的配置设置。 注:我已添加了示例中的项目。 请解决此问题。 谢谢! 拉基 Re: ADC Configuration for S32K344 EVB HDQFP172 您好, 请尝试按照提示解决“问题”窗口中显示的错误。 大部分个人驱动程序可能不会添加到工具链中。在较新的 S32DS 中,通常在通过配置工具更新代码后,此功能就会消失。或者您需要通过“管理 SDK 元器件”手动添加它。 请确保已选择使用的元器件,然后再次更新代码。 对于 Siul2_Port 元器件,可能出现 2 个错误。 - Pin 工具配置了 2 个引脚,而 Siul2_port 只配置了 1 个引脚,两者设置不匹配。 对于 ADC 输入,无需进行引脚设置,模拟路径始终启用,您可以从引脚工具中删除它。 - 另一个可能是引脚工具中的功能组命名。 如果遇到问题,请分享您的完整项目。 BR,彼得 Re: ADC Configuration for S32K344 EVB HDQFP172 您好, 添加 Siul2_Port 后出现此错误。 我的引脚配置如下: 非常感谢您抽出时间回复。 BR, 拉基 Re: ADC Configuration for S32K344 EVB HDQFP172 您好, 添加 Siul2_Port 元器件,更新代码,并构建。 BR,彼得 Re: ADC Configuration for S32K344 EVB HDQFP172 嗨@PetrS , 谢谢你的关注。 附件如下。 Br, 拉基 Re: ADC Configuration for S32K344 EVB HDQFP172 您好, 您没有上传任何文件或截图。 您可以参考以下使用电位器进行ADC采样的示例: 示例 S32K312 ADC IP 连续扫描 DMA (S32DS 3.6, RTD 6.0.0) RTD400 LLD K344 ADC 软件/硬件触发示例 BR,Petr Re: ADC Configuration for S32K344 EVB HDQFP172 嗨,Petrs, 感谢您的支持。 您能否提供一些关于AUTOSAR版本的资源供我尝试? 我尝试了示例中的项目。但却不起作用。 请帮忙。 BR, 拉基
View full article
LPCXpresso54S018M EVBのRTCは消費電力が非常に大きい。 私が使用しているのはLPCXpresso54S018M EVBです。LPC54018に内蔵されているRTCは、主電源が切断された後も動作する必要があります。ファームウェア内でRTCを初期化し、有効化しました。VBATTライン(J10:11)には、CR2032というコイン型電池で電源を供給しました。主電源が供給されている間は、VBATTラインの消費電力は0です。問題ありません。しかし、主電源を取り外すと、VBATTラインの消費電流が約41μAまで増加します。データシートによると、消費電流は1μA未満であるはずです。なぜ?電流消費電力を1μA以下にするにはどうすればよいですか? LPC54xxx Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. データシートでこの要件について読みました(VBAT>VDDの場合、高VBATリークを防ぐために外部リセットピンはフローティング状態にする必要があります)。 でも、どうすればそれが実現できるのか分かりません。 私はEVBの回路図について話しているわけではありません。EVB - プロトタイプ作成専用。しかし、動作中の機器の回路では、MCU RESETNが外部WDTチップ(TPS3823-33DBVR)のRST出力に直接接続されます。 おすすめはありますか:接続MCUの修正方法。リセット<->WDT。RST接続の回路図はVBATの電流消費が1μAを超えないようにしていますか? WDT <-> MCUの回路図を添付します。私のデバイスにおけるRESETN相互接続: この図では、「Reset」と名付けられた配線がLPC54005JBD100のRESETNピンに接続されています。 Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. こんにちは、 @jcxzさん 約41μAは、RTCの消費電流ではなく、RESETN回路からのリーク電流である可能性が最も高い。主電源が切断されたとき、VBAT > VDD となります。VBAT > VDD の場合、高 VBAT リークを防ぐために外部リセットピンはフローティング状態にする必要があります。 LPCXpresso54S018M-EVKはRESETNをプッシュボタン/デバッグ回路に接続するため、未改造のEVKはその測定条件を満たしません。 電流を減らすには: MCUのRESETNピンをEVKリセットネットワークから分離してください。 BR ハリー Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. こんにちは、 @jcxzさん ここでいう「フローティング」とは、バッテリーのみでの動作時(VBATが存在し、VDDが除去されている状態)には、RESETNに外部DC経路が存在しないことを意味します。MCUの内部リセットプルアップは無効化する必要はありません。データシートにはすでにその条件が記載されています。 提案された監視回線では、RESETNは電源のないTPS3823出力および外部RCネットワークに接続されたままです。したがって、データシートに記載されているRESETNピンのフローティング状態という条件は満たされていません。これは観測された約41μAの電流に対するもっともらしい説明であるが、正確な漏洩経路はまだ実験的に検証されていない。 データシート条件を満たすために、ウォッチドッグリセット出力とMCU RESETNピンの間に通常開閉のアイソレーションスイッチを挿入することを推奨します。すべての外部リセット部品(プルアップ抵抗、コンデンサ、ウォッチドッグ出力など)はウォッチドッグ側に留め、MCU側には外部プルアップ、プルダウン、コンデンサ、その他の直流接続は含まれてはいけません。 選択したスイッチは、供給電圧が除去された際に低漏れ・高インピーダンス状態を明示的にサポートしている必要があります。 BR ハリー Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. Harry_Zhangさん、ご協力ありがとうございました! ご提案いただいた内容に基づき、以下の回路を作成しました。 この回路は正しいと思いますか?このRESETN回路を使用した場合、LPC54005の消費電力は1μA未満になりますか(VBATピンからの消費電流)?
View full article
MCSPTE1AK144 – MATLABホストモデル起動直後のモーター故障 MATLAB/Simulinkで提供されている開ループおよび閉ループのサンプルを使用してMCSPTE1AK144キットを制御する際に問題が発生しています。 ターゲットモデルが構築され、生成されたファイルは S32K144に正常にフラッシュされます。MATLABはOpenSDA CDCシリアルポートも検出し、ホストモデルは通信を確立できます。 しかし、ホストモデルを起動してモーターをオンにすると、モーターシャフトが一瞬ピクピク動くか、動かず、D11の赤いLEDがすぐに点灯・点滅し、故障を示しています。するとモーターが反応しなくなる。 基本的なボード通信は、LPUART Hello Worldサンプルを使用して別途検証されており、OpenSDAシリアルポートを介して正常にビルド、フラッシュ、通信が行われます。 MATLABホストモデルから制御開始直後にモーター制御アプリケーションが故障に入る原因や、根本原因を特定するためにどの故障/ステータス変数をチェックすべきか教えていただけますか? ハードウェア:MCSPTE1AK144(S32K144-EVB + DEVKIT-MOTORGD) モーター:Sunrise 42BLY3A78-24110 MATLAB/SimulinkとNXP MBDT ありがとうございます。 ホットフィックス
View full article
IMX8ulp 中的猎鹰模式启动问题 大家好, 我在以 Falcon 模式 启动主板时遇到问题 。 我将meta-imx-fastboot层克隆到我的 Yocto 源代码目录中。 在构建过程中,我遇到了一些与 imx-boot 和设备树 相关的问题 ,因为我使用的是需要加载到我们开发板上的自定义 DTS。为了解决这个问题,我在 machine.conf 文件中配置了 Falcon 模式参数, 如下所示: FALCON_KERNEL_DEVICETREE = "imx8ulp-custom" 完成此配置后,我能够按照 Falcon 模式步骤中所述生成imx8ulp_no_uboot加载器。 我正在使用 fitImage KERNEL_IMAGETYPE = "fitImage" KERNEL_CLASSES:append = " kernel-fitimage" IMAGE_BOOT_FILES = "fitImage" 然后我使用以下命令对开发板进行了烧录: sudo uuu -b emmc_all *.wic sudo uuu -b emmc 刷写固件后,启动开发板时,启动失败并出现以下错误: U-Boot SPL 2025.04-gb9f705c183f0(2025年6月4日 - 09:48:20 +0000) 正常启动 ELE固件版本2.0.2-85b63cb9 upower_apd_inst_isr:入口 upower_init: soc_id=48 upower_init:版本:11.11.13 upower_init:启动 uPower RAM 服务 user_upwr_rdy_callb: soc=b user_upwr_rdy_callb:内存版本:12.18 打开开关…… 打开开关,没问题 唤醒记忆…… 打开记忆功能 清除DDR数据保留... 清除DDR数据保留正常 SEC0:RNG 实例化 尝试从 MMC1 启动 设备 0 上的分区 1 无效 spl_register_fat_device:fat 设备寄存器错误 -1 设备 0 上的分区 1 无效 spl_register_fat_device:fat 设备寄存器错误 -1 spl_load_image_fat:读取镜像 u-boot-atf-container.img 时出错,错误代码 -1 错误:-2 SPL:无法从所有引导设备启动 # ## ERROR ## # 请 RESET 该板 ### 请问您能否帮我了解一下这个错误的原因,并建议一下如何解决 Falcon 模式启动问题? Re: Falcon Mode Boot Issue in IMX8ulp 你好@elgin_1950 如果将 DTS 内容和 defconfig 同步到 Falcon 默认支持的 EVK 代码,是否还会出现任何问题? 此致, 志明 Re: Falcon Mode Boot Issue in IMX8ulp 您好@Zhiming_Liu,抱歉回复晚了。 我已经解决了这个问题,因为 Falcon 模式使用的是普通内核图像而不是fitImage 。 但是,有没有办法通过 Falcon 模式加载fitImage ?
View full article
ADC Configuration for S32K344 EVB HDQFP172 Hi, I want to execute ADC channel ADC0_P7 which is connected to board's Potentiometer, and converted value is used to dim board's LED (GPIO29). After configuration, it is showing: Error:  platform.driver.pins Additionally, when building the project after the configuration, we encountered the following compilation error: image(error_Adc) I also attached the configuration settings below. NOTE: I have added the project from Example. Kindly resolve the issue. Thanks, Raky Re: ADC Configuration for S32K344 EVB HDQFP172 Hi, try to follow hints and resolve errors indicated in Problems window. Most probabbly indiovidual drivers are not added to the toolchain. In newer S32DS this commonly disappear after you Update Code in config tool. Or you need to add it manually through Manage SDK components be sure used components are selecected then Update Code again For the Siul2_Port component, 2 things can be wrong. - Pin tool have 2 pins configured, Siul2_port just 1 and there is missmatch in setting.  Fore ADC input, no pin setting is needed, analog path is always enabled, you can delete it from Pins tool. - another could be naming of Functional group in Pins tool. If you have issue still share your full project. BR, Petr Re: ADC Configuration for S32K344 EVB HDQFP172 Hi, After adding Siul2_Port I got this error. My pin configuration is: I really appreciate taking your time to reply, thanks. BR, Raky Re: ADC Configuration for S32K344 EVB HDQFP172 Hi, add Siul2_Port component, Update Code, and build. BR, Petr Re: ADC Configuration for S32K344 EVB HDQFP172 Hi @PetrS , Thanks for noticing. Here is the attached file below. Br, Raky Re: ADC Configuration for S32K344 EVB HDQFP172 Hi, You did not attach any files or screenshots. You can refer to the following examples that use ADC sampling with a potentiometer: Example S32K312 ADC IP Continuous Scan DMA (S32DS 3.6, RTD 6.0.0) RTD400 LLD K344 ADC SW/HW Trigger Example BR, Petr  Re: ADC Configuration for S32K344 EVB HDQFP172 Hi Petrs, Thanks for the support. Can you also give any resource to try for AUTOSAR version. I tried with the project from example. But not working. Kindly help. BR, Raky 
View full article
S32K344 EVB HDQFP172のADC構成 こんにちは、 基板のポテンショメーターに接続されたADC チャネル ADC0_P7 を実行し、変換した値を基板のLED(GPIO29)を暗めるために使いたいです。 設定後、以下のように表示されます。 エラー: platform.driver.pins さらに、設定後にプロジェクトを構築する際に、以下のコンパイルエラーに遭遇しました:image(error_Adc) 設定ファイルも下記に添付しました。 注:Exampleからプロジェクトを追加しました。 問題を解決してください。 ありがとうございます ラキー Re: ADC Configuration for S32K344 EVB HDQFP172 こんにちは、 「問題」ウィンドウに表示されるヒントに従って、エラーを解決してみてください。 おそらくほとんどの独立ドライバはツールチェーンに追加されません。新しいS32DSでは、設定ツールでコードを更新すると、この問題は通常解消されます。あるいは、Manage SDKコンポーネントから手動で追加する必要があります 使用済みのコンポーネントが選択されていることを確認してから、再度コードを更新してください。 Siul2_Portコンポーネントについては、2つの誤りがあります。 Pinツールでは2つのピンが設定されていますが、Siul2_portでは1つしか設定されておらず、設定に不一致があります。 前方ADC入力ではピン設定は不要で、アナログパスは常に有効で、ピンツールから削除できます。 - もう一つは、ピンツールで機能グループの名前を付けることです。 それでも問題が解決しない場合は、プロジェクト全体を共有してください。 BR、ペトル Re: ADC Configuration for S32K344 EVB HDQFP172 こんにちは、 Siul2_Portを追加した後、このエラーが発生しました。 私のPIN設定は以下のとおりです。 お返事をいただき、本当にありがとうございます。 BR、 ラキー Re: ADC Configuration for S32K344 EVB HDQFP172 こんにちは、 Siul2_Portコンポーネントを追加し、コードを更新してビルドします。 BR、ペトル Re: ADC Configuration for S32K344 EVB HDQFP172 こんにちは、 @PetrS さん。 気づいてくれてありがとう。 添付ファイルは以下のとおりです。 Br、 ラキー Re: ADC Configuration for S32K344 EVB HDQFP172 こんにちは、 ファイルやスクリーンショットが添付されていませんでした。 ポテンショメーターでADCサンプリングを用いる以下の例を参照できます: 例S32K312 ADC IP連続スキャンDMA(S32DS 3.6、RTD 6.0.0) RTD400 LLD K344 ADC ソフトウェア/ハードウェアトリガーの例 BR、ペトル Re: ADC Configuration for S32K344 EVB HDQFP172 こんにちは、ペトルスさん。 サポートありがとうございます。 AUTOSAR版で試せるリソースも教えてもらえますか? サンプルプロジェクトを使って試してみました。しかし、うまくいかない。 どうか助けてください。 BR、 ラキー
View full article
LPCXpresso54S018M EVB 的 RTC 功耗巨大。 我使用的是 LPCXpresso54S018M EVB。我需要 LPC54018 中的 RTC 在主电源断开后仍然能够工作。我在固件中初始化并启用了实时时钟 (RTC)。我用一枚纽扣电池 CR2032 为 VBATT 线 (J10:11) 供电。主电源正常时,VBATT 线路功耗为 0。没问题。然而,移除主电源后,VBATT 线功耗增加到约 41 uA!根据数据手册,功耗应小于 1 uA。为什么?如何才能实现1µA或更低的电流消耗? LPC54xxx Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. 我在数据手册中读到了这个要求(如果 VBAT> VDD,则外部复位引脚必须悬空,以防止 VBAT 漏电流过高)。 但我不知道该如何实现这一点? 我说的不是EVB原理图。EVB——仅用于原型制作。但在我们的工作设备电路中,MCU RESETN 将直接连接到外部 WDT 芯片 (TPS3823-33DBVR) 的 RST 输出。 请问如何修正MCU.RESETN <-> WDT.RST连接的原理图,才能使VBAT电流消耗不超过1 µA? 我附上设备中 WDT <-> MCU.RESETN 互连的原理图: 在这张图中,名为“Reset”的导线连接到 LPC54005JBD100 的 RESETN 引脚。 Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. 嗨@jcxz ~41 µA 很可能是 RESETN 电路的漏电流,而不是 RTC 的功耗。主电源断开时,VBAT > VDD;如果 VBAT > VDD,则外部复位引脚必须浮空,以防止 VBAT 漏电流过高。 LPCXpresso54S018M-EVK 将 RESETN 连接到其按钮/调试电路,因此未修改的 EVK 不满足该测量条件。 为了降低电流: 将 MCU 的 RESETN 引脚与 EVK 复位网络隔离。 BR 哈里 Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. 嗨@jcxz “浮空”在此表示 RESETN 在仅使用电池供电时(VBAT 存在,VDD 移除)不应有外部直流通路。MCU 的内部 RESET 上拉电阻无需禁用;数据手册已经考虑到了这种情况。 在所提出的看门狗电路中,RESETN 仍然连接到未通电的 TPS3823 输出以及外部 RC 网络。因此,数据手册中关于 RESETN 引脚浮空的条件不满足。对于观察到的 ~41 µA 电流,这是一种合理的解释,尽管确切的泄漏路径尚未通过实验验证。 为了满足数据手册的要求,我们建议在看门狗复位输出和 MCU RESETN 引脚之间插入一个常开隔离开关。所有外部复位元器件(上拉电阻、电容、看门狗输出等)都应保留在开关的看门狗侧,而 MCU 侧不应包含任何外部上拉、下拉、电容或其他直流连接。 所选开关应明确支持在电源电压移除时处于低漏电、高阻抗状态。 BR 哈里 Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. 谢谢你的帮助, Harry_Zhang ! 根据您的建议,我们设计了以下电路: 你认为这个电路图正确吗?采用此 RESETN 电路后,LPC54005 的功耗(从 VBAT 引脚)是否会小于 1 μA ?
View full article
S32G3 EB AUTOCORE LICENSE Hello Team, We are facing issue in the activation code within EB Client License Administrator to start EB tresos AutoCore: 7FCB-75DF-0F6E-4E7A (valid until 12/30/2026),saying its expired. Please see the below attachment Re: S32G3 EB AUTOCORE LICENSE Hi, Please try signing in with an account from a colleague that has not access the license in the past. This should help you get the most updated license. Please do not share passwords, licenses other sensitive information in the community post.
View full article
Falcon Mode Boot Issue in IMX8ulp Hi Team, I am facing an issue while booting the board in Falcon Mode. I cloned the meta-imx-fastboot layer into my Yocto source directory. While building, I encountered some issues related to imx-boot and the device tree because I am using a custom DTS that needs to be loaded onto our board. To address this, I configured the Falcon Mode arguments in my machine.conf as follows: FALCON_KERNEL_DEVICETREE = "imx8ulp-custom" After this configuration, I was able to generate the imx8ulp_no_uboot loader as described in the Falcon Mode steps. I am using fitImage KERNEL_IMAGETYPE = "fitImage" KERNEL_CLASSES:append = " kernel-fitimage" IMAGE_BOOT_FILES = "fitImage" I then flashed the board using the following commands: sudo uuu -b emmc_all *.wic sudo uuu -b emmc After flashing, when I boot the board, it fails to boot and generates the following error: U-Boot SPL 2025.04-gb9f705c183f0 (Jun 04 2025 - 09:48:20 +0000) Normal Boot ELE firmware version 2.0.2-85b63cb9 upower_apd_inst_isr: entry upower_init: soc_id=48 upower_init: version:11.11.13 upower_init: start uPower RAM service user_upwr_rdy_callb: soc=b user_upwr_rdy_callb: RAM version:12.18 Turning on switches... Turn on switches ok Turning on memories... Turn on memories ok Clearing DDR retention... Clear DDR retention ok SEC0: RNG instantiated Trying to boot from MMC1 Partition 1 invalid on device 0 spl_register_fat_device: fat register err - -1 Partition 1 invalid on device 0 spl_register_fat_device: fat register err - -1 spl_load_image_fat: error reading image u-boot-atf-container.img, err - -1 Error: -2 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ### Could you please help me understand the cause of this error and suggest how I can resolve the Falcon Mode boot issue? Re: Falcon Mode Boot Issue in IMX8ulp Hi @elgin_1950  If you sync your DTS content and defconfig to the EVK code that Falcon supports by default, will there still be any issues? Best Regards, Zhiming Re: Falcon Mode Boot Issue in IMX8ulp Hi @Zhiming_Liu sorry for late reply  I have fixed the issue, as Falcon mode was taking the normal kernel images instead of the fitImage. However, is there a way to load the fitImage through Falcon mode?
View full article
Re: i.MX RT1064 - PEmicro Connection Assistant Error Hi, This is a follow up to a previously raised query. The link has been attached to the previous query, and the link has the required details which was requested. Kindly reply and help us address the issue at the earliest. Thanks and Regards Subhasri https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1064-PEmicro-Connection-Assistant-Error-and-Boot/m-p/2412530#M37152 i.MXRT 106x Re: i.MX RT1064 - PEmicro Connection Assistant Error Hi @Subhasri_S, On the measurements you shared, are the pull-up voltages powered before POR_B is released? In your application, is there any point at which the MCU enters a low-power state? Does any fault or error occur before the issue appears? Best Regards, Pablo Re: i.MX RT1064 - PEmicro Connection Assistant Error Hi @Pablo_Ramos , thank you for your response. The pull-up voltages are not powered before POR_B is released. Signals of the pull -up wrt. POR_B behavior is attached below. There is no point in our application where MCU Enters low power mode.  Also, no fault or error occurs before this issue. I would also like to know whether there is any way to recover the board through software when this issue occurs. Thanks and Regards Subhasri Re: i.MX RT1064 - PEmicro Connection Assistant Error Hi When this behavior occurs, you mentioned that you are unable to flash or debug the device. If you try to attach a debugger, are you able to do so? If you are able to attach the debugger, what is the last instruction that was executed? One possible explanation is described in the following knowledge base article: Knowledge Base: RT board recovery for debugger connect issues "When the flash contains an abnormal application (for example, accessing non-existent memory, memory corruption, clock misconfiguration, etc.), the board may enter an unknown state, preventing the debugger from taking control of the core. However, when the device is placed in Serial Downloader mode, the core is forced into a known state, allowing the debugger to take control. Therefore, when encountering debugger connection issues on an RT board, try performing a mass erase of the external flash while the device is in Serial Downloader mode. This should restore normal debugger operation." You mentioned that this issue occurs on both a custom board and the EVK. Does the issue also occur when running a standard SDK example? For the EVK where this behavior is observed, have any hardware modifications been made? Best Regards, Pablo Re: i.MX RT1064 - PEmicro Connection Assistant Error Hello @Pablo_Ramos  This is just  a gentle follow up on the same. Thank you  Regards  Subhasri Re: i.MX RT1064 - PEmicro Connection Assistant Error Hi  , thank you for the response. No, I am unable to flash the device with the debugger - PE Micro. The screenshot with the last instruction executed has been attached below. If any code results in a hard fault/ bus fault, after build itself the board becomes inaccessible. Once the board has entered this state, I am unable to flash any other code including NXP Example codes. I am also not able to Erase the flash in internal boot mode, I am not able to access the board unless I manually change the boot mode to serial download on the hardware and erase the flash. We observed the same behavior on the EVK as well. On the EVK, recovery was relatively straightforward because it has physical switches to change the boot mode. However, our custom board does not have these switches, so recovering the board requires a much more involved process. This makes it risky to proceed with production, as a firmware fault could potentially leave the board inaccessible and require a manual recovery procedure that is not practical for the production hardware. Is there any other way to recover the board using the debugger/PEmicro when it is in this state, without switching to Serial Download mode and is the issue caused by hardware or software ? What could be causing the MCU to enter this unrecoverable state which can be consciously avoided by us? Thanks and Regards  Subhasri
View full article
功耗管理 鉴于能源价格目前已飙升至天价,并且在接下来的几个月里,它们的目标是达到太阳的高度,那么问题在于,我们可以采取哪些措施来最大限度地减少其影响。 我相信你们中的许多人也和我一样,公司一直以来的“政策”(或者说惯例)是让所有设备始终保持开启状态,无论是为了系统维护、远程访问还是其他任何原因。 今天早上,我读了一篇关于“由于能源价格上涨,很大一部分公司可能无法生存”的文章后,想到我们可以通过在公司范围内制定严格的电源管理单元政策来积极应对这种情况。 所以现在我想知道,你们都是怎么做的?如果你们以前成功解决过这个问题,你们觉得最好的方法是什么? 电源设置组策略?第三方应用程序/系统?先好好跟用户说,让他们下班时把所有设备都关掉,然后用定期殴打来强制执行? 那些长期从事这项工作的人有什么经验分享吗? 电源解决方案 Re: Power consumption management 您提出的问题——如何实施公司范围内的电源管理单元策略以降低能源成本——属于一般的 IT 和设施管理主题,超出了 NXP 产品技术支持的范围。
View full article
Power consumption management Given that the energy prices are now through the roof and in the next few months they are aiming to reach the Sun, there is a question what can be done to minimise the impact. I am sure many of you are also in the same position as I am where at the company the "policy" or rather custom was so far to keep everything switched on all the time, for system maintenance, remote access or for any other reasons. Today morning, after reading an article about "High percentage of companies may not make it due to the energy prices" it occurred to me we can proactively do something about it by setting strict power management policies across the company. So now I wonder, what are you all doing about this, and if you did manage this before, what did you find the best way of going with this? Power settings group policies? A third party application/system? Ask the users nicely to turn everything off when they leave for the day and then enforce it with regular beatings? Any insights from those who are already doing this for a long time? Power solution Re: Power consumption management The question you have raised - how to implement company-wide power management policies to reduce energy costs - is a general IT and facilities management topic and falls outside the scope of NXP product technical support.
View full article
MCSPTE1AK144 – Motor Faults Immediately After Starting MATLAB Host Model I am facing an issue while controlling the MCSPTE1AK144 kit using the MATLAB/Simulink open-loop and closed loop examples available. The target model builds and the generated file can be flashed to the S32K144 successfully. MATLAB also detects the OpenSDA CDC serial port and the host model is able to establish communication. However, whenever I start the host model and switch the motor ON, the motor shaft either twitches briefly or does not run, and the D11 red LED immediately turns ON/flashes, indicating a fault. The motor then stops responding. Basic board communication has been verified separately using the LPUART Hello World example, which builds, flashes, and communicates successfully through the OpenSDA serial port. Could you please advise what could cause the motor-control application to enter a fault immediately after starting control from the MATLAB host model, and which fault/status variables should be checked to identify the root cause? Hardware: MCSPTE1AK144 (S32K144-EVB + DEVKIT-MOTORGD) Motor: Sunrise 42BLY3A78-24110 MATLAB/Simulink with NXP MBDT Thanks. HotFix
View full article
回复:i.MX RT1064 - PEmicro 连接助手错误 您好, 这是对之前提出的一个问题的后续跟进。链接已附加到之前的查询中,链接中包含所要求的详细信息。请尽快回复,并协助我们解决问题。 谢谢并致以诚挚的问候 苏巴斯里 https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/i-MX-RT1064-PEmicro-Connection-Assistant-Error-and-Boot/m-p/2412530#M37152 i.MX RT106x Re: i.MX RT1064 - PEmicro Connection Assistant Error 你好@Subhasri_S , 根据您分享的测量结果,上拉电压是在 POR_B 释放之前供电的吗? 在您的应用中,MCU 是否会在某个时刻进入低功耗状态? 在出现问题之前是否发生过任何故障或错误? 此致, 巴勃罗 Re: i.MX RT1064 - PEmicro Connection Assistant Error @Pablo_Ramos你好,谢谢你的回复。 在 POR_B 释放之前,上拉电压不会通电。上拉信号与。POR_B 行为如下所示。 我们的应用程序中没有任何环节会让MCU进入低功耗模式。 此外,在此问题出现之前没有发生任何故障或错误。 我还想知道,当出现这种问题时,是否可以通过软件恢复主板。 谢谢并致以诚挚的问候 苏巴斯里 Re: i.MX RT1064 - PEmicro Connection Assistant Error 你好@Pablo_Ramos 这只是对之前内容的温和跟进。 谢谢 此致敬礼 苏巴斯里 Re: i.MX RT1064 - PEmicro Connection Assistant Error HI 当出现这种现象时,您提到无法刷写固件或调试设备。如果尝试附加调试器,是否可以成功? 如果可以连接调试器,请问执行的最后一条指令是什么? 以下知识库文章描述了一种可能的解释: 知识库: RT板恢复调试器连接问题 “当闪存中包含异常应用程序(例如,访问不存在的内存、内存损坏、时钟配置错误等)时,板可能会进入未知状态,从而阻止调试器控制内核。但是,当设备处于串行下载器模式时,内核会被强制进入已知状态,从而允许调试器接管控制权。 因此,当 RT 板上出现调试器连接问题时,请尝试在设备处于串行下载器模式时对外部闪存进行批量擦除。这样应该可以恢复调试器的正常运行。 您提到这个问题在定制板和 EVK 上都会出现。运行标准 SDK 示例时也会出现此问题吗? 对于出现这种现象的 EVK,是否进行了任何硬件修改? 顺祝商祺! 巴勃罗 Re: i.MX RT1064 - PEmicro Connection Assistant Error 您好,谢谢您的回复。 不,我无法使用调试器 PE Micro 烧录设备。 下面附上最后一条指令执行完毕的屏幕截图。如果任何代码导致硬故障/总线故障,则在版本完成后,板将无法访问。一旦板进入这种状态,我就无法刷入任何其他代码,包括 NXP 示例代码。我也无法在内部启动模式下擦除闪存,除非我手动将硬件上的启动模式更改为串行下载并擦除闪存,否则我无法访问该板。 我们在 EVK 上也观察到了同样的现象。在 EVK 上,恢复过程相对简单,因为它有物理开关来改变启动模式。但是,我们的定制板没有这些开关,因此恢复板需要更加复杂的过程。 这使得继续生产存在风险,因为固件故障可能会导致板无法访问,需要手动恢复程序,这对于生产硬件来说是不切实际的。 当板处于这种状态时,除了切换到串行下载模式之外,还有其他方法可以使用调试器/PEmicro 来恢复板吗?这个问题是由硬件还是软件引起的? 是什么原因导致MCU进入这种我们本可以避免的不可恢复状态? 感谢并致意 苏巴斯里
View full article
S32G3 EB AUTOCORE 许可证 各位团队成员,大家好! 我们在 EB Client License Administrator 中遇到激活码问题,无法启动 EB tresos AutoCore: 7FCB-75DF-0F6E-4E7A(有效期至 2026 年 12 月 30 日),提示已过期。 请参阅以下附件。 Re: S32G3 EB AUTOCORE LICENSE 你好, 请尝试使用之前未曾访问过该许可证的同事的帐户登录。这应该有助于您获得最新许可证。 请勿在社区帖子中分享密码、许可证或其他敏感信息。
View full article
S32K2x8EVB-Q289 QSPI(S26KL512Sバリアントが誤っている) こんにちは、 現在、S32K3x8EVB-Q289ボードを使用しており、オンボードのS26KL512SDABHV030フラッシュとQSPIを連携させることを試みています。 徹底的なデバッグを行った結果、行き詰まってしまい、何が起こっているのか分からなくなってしまいました。そこで、解決したい点を見つけたので、ここに報告します。 EVBのユーザーガイドと回路図には、S26KL512SDABHV030が基板上にハンダ付けされていると記載されています。部品を検査した結果、刻印は以下のとおりであることが確認されました。 6KL512SDAHV03は03バリアント(DCARSバリアント)です。 S26K512Sのデータシートを読んだところ、DCARSはPSC信号を使用してRWDS(読み取りに必要な信号)を生成すると記載されていました。しかし、EVBの回路図では、PSCは(テストパッドTPAD21を除いて)どこにも配線されていません。PSC#は3VバリアントではRFUなので、必要ありません。 ロジックアナライザを見ると、レイテンシ期間(戻るデータを観察すべき時刻)後にRWDSが切り替える様子は見られず、転送は最終的にタイムアウトします。 フラッシュメモリが動作せず、EVBに誤ったバージョンのフラッシュメモリが搭載されているのではないかと考えています。 ご助言ありがとうございます。 ミハル Re: S32K2x8EVB-Q289 QSPI with wrong S26KL512S variant 中古ボードのリビジョンを具体的に教えてもらえますか?ボードユーザーマニュアルには以下の訂正が明記されています: Re: S32K2x8EVB-Q289 QSPI with wrong S26KL512S variant もう一つ最新情報をお伝えします。 PSCをSCKに接続した後、RWDS信号が得られました。 これは以下のことを裏付けています。 03(DCARS)バージョンでは、データが利用可能になったことを示すためにPSC信号が必要となります。現在、Rev C EVBにはコネクテッドされていません。 02(非DCARS)バリアントは、インストールされるべきICです。 PSC信号に遅延がないため、RWDSトグルはデータ変化エッジに非常に近い位置にあり、読み取り値にばらつきが生じます(現在はデバイスIDの読み取り値でテストしています)。 S32K358の内部DQSを利用すると、データの変更と正しく整合していない可能性があるため、データの読み取り方法が信頼できるとは言えません。 お知らせ下さい ミハル Re: S32K2x8EVB-Q289 QSPI with wrong S26KL512S variant 当社にはRev Cバージョンの基板があります。 したがって、その訂正は私たちのケースには適用されませんし、さらに、回路図上でPSCピンが入れ替わっていても、PSCピンは切断されたままになります(SCKピンだけが接続されているため)。 S26KL5152Sのデータシートを読むと、SCKピンをPSCに接続すればメモリが02(DCARS以外の)バリアントのように振る舞うと書かれています。基板を再設計してこの接続を追加し、それで問題が解決するかどうか確認してみます。 他に解決策があれば、ぜひお知らせください。 ミハル Re: S32K2x8EVB-Q289 QSPI with wrong S26KL512S variant こんにちは、ミハルさん。 ご意見ありがとうございます。デバイス識別と関連するInfineonのドキュメントを再確認しましたが、あなたの結論に同意します。プロピュレーションS26KL512SDABHV030 DCARSバリアントはPSC信号を必要としますが、Rev. Cボードにはコネクテッドされていません。 この問題はアプリケーションエンジニアリングチームに報告し、さらなる調査を依頼します。 よろしくお願いします、 デビッド
View full article
MCSPTE1AK144 – 启动 MATLAB 主机模型后立即出现电机故障 我在使用 MATLAB/Simulink 提供的开环和闭环示例控制 MCSPTE1AK144 套件时遇到了问题。 目标模型构建成功,生成的文件可以成功烧录到S32K144。MATLAB也能检测到OpenSDA CDC串口,主机模型能够建立通信。 但是,每当我启动主机模型并打开电机时,电机轴要么短暂地抽动一下,要么根本不运转,D11 红色 LED 灯立即亮起/闪烁,表明出现故障。随后电机停止响应。 已使用 LPUART Hello World 示例单独验证了基本板通信,该示例可以成功版本、烧录并通过 OpenSDA 串行端口进行通信。 请问是什么原因导致电机控制应用程序在从 MATLAB 主机模型启动控制后立即出现故障?应该检查哪些故障/状态变量来确定根本原因? 硬件:MCSPTE1AK144(S32K144-EVB + DEVKIT-MOTORGD) 电机:Sunrise 42BLY3A78-24110 MATLAB/Simulink 与 NXP MBDT 谢谢。 热修复
View full article
IMX8ulpにおけるファルコンモード起動の問題 チームの皆さん、こんにちは。 Falconモード でボードを起動する際に問題が発生しています 。 meta-imx-fastboot レイヤーをYoctoのソースディレクトリに クローンしました 。 構築中に imx-boot やデバイスツリー に関する問題に直面しました 。カスタムDTSを使っていて、それをボードに読み込む必要があるからです。これに対処するために、machine.confのFalcon Mode引数を 次のように 設定しました: FALCON_KERNEL_DEVICETREE = "imx8ulp-custom" この設定後、 Falcon Modeの手順で説明されているとおり、 imx8ulp_no_ubootローダーを生成することができました。 fitImageを使用しています KERNEL_IMAGETYPE = "fitImage" KERNEL_CLASSES:append = " kernel-fitimage" IMAGE_BOOT_FILES = "fitImage" 次に、以下のコマンドを使用してボードにファームウェアを書き込みました。 sudo uuu -b emmc_all *.wic sudo uuu -b emmc ファームウェアの書き込み後、ボードを起動すると、起動に失敗し、以下のエラーが発生します。 U-Boot SPL 2025.04-gb9f705c183f0(2025年6月4日 09:48:20 +0000) 通常起動 ELEファームウェアバージョン2.0.2-85b63cb9 upower_apd_inst_isr: エントリ upower_init: soc_id=48 upower_init: バージョン:11.11.13 upower_init: uPower RAMサービスを開始します user_upwr_rdy_callb: soc=b user_upwr_rdy_callb: RAMバージョン:12.18 スイッチを入れる... スイッチを入れてみて、OK 記憶を起動する... メモリーをオンにして DDRの保持をクリアします... DDRの保持はクリアです 第0節:RNGのインスタンス化 MMC1からの起動を試みています パーティション1がデバイス0で無効 spl_register_fat_device:ファットレジスター err - -1 パーティション1がデバイス0で無効 spl_register_fat_device:ファットレジスター err - -1 spl_load_image_fat: error reading image u-boot-atf-container.img, err - -1 誤差:-2 SPL:すべての起動デバイスから起動に失敗 ### ERROR ### ボードをリセットしてください### このエラーの原因を理解し、Falcon Modeの起動問題を解決する方法を教えていただけませんか? Re: Falcon Mode Boot Issue in IMX8ulp こんにちは@elgin_1950  もしDTSコンテンツとdefconfigをFalconがデフォルトでサポートしているEVKコードに同期した場合、問題は起きるのでしょうか? よろしくお願いします、 志明 Re: Falcon Mode Boot Issue in IMX8ulp @Zhiming_Liuさん、返信が遅れて申し訳ありません。 FalconモードでfitImageではなく通常のカーネルイメージが使用されていたため、問題を修正しました。 しかし、 Falconモードを通してfitImageを読み込む方法はありますか?
View full article