Hi Team,
I am facing an issue while booting the board in Falcon Mode.
I cloned the meta-imx-fastboot layer into my Yocto source directory.
While building, I encountered some issues related to imx-boot and the device tree because I am using a custom DTS that needs to be loaded onto our board. To address this, I configured the Falcon Mode arguments in my machine.conf as follows:
FALCON_KERNEL_DEVICETREE = "imx8ulp-custom"
After this configuration, I was able to generate the imx8ulp_no_uboot loader as described in the Falcon Mode steps.
I am using fitImage
KERNEL_IMAGETYPE = "fitImage"
KERNEL_CLASSES:append = " kernel-fitimage"
IMAGE_BOOT_FILES = "fitImage"
I then flashed the board using the following commands:
sudo uuu -b emmc_all
*.wic
sudo uuu -b emmc
After flashing, when I boot the board, it fails to boot and generates the following error:
U-Boot SPL 2025.04-gb9f705c183f0 (Jun 04 2025 - 09:48:20 +0000)
Normal Boot
ELE firmware version 2.0.2-85b63cb9
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.18
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0: RNG instantiated
Trying to boot from MMC1
Partition 1 invalid on device 0
spl_register_fat_device: fat register err - -1
Partition 1 invalid on device 0
spl_register_fat_device: fat register err - -1
spl_load_image_fat: error reading image u-boot-atf-container.img, err - -1
Error: -2
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
Could you please help me understand the cause of this error and suggest how I can resolve the Falcon Mode boot issue?
Hi @elgin_1950
If you sync your DTS content and defconfig to the EVK code that Falcon supports by default, will there still be any issues?
Best Regards,
Zhiming