Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Regarding the consistency of LPC-Link2 serial numbers I would like to ask how to change the serial number of several LPC-Link2 chips if they are identical. Thank you. Re: 关于lpc-link2 SN码一致 Hi @chenwei97 This serial number cannot be modified. If you are connecting multiple LPC-LINK2 devices simultaneously, it is recommended to update to the CMSIS-DAP firmware. This will give each debugger a unique ID number. BR Alice
View full article
RT1176 PWM startup failed I am using PWM + fault + QTimer to implement motor pulse control, but the PWM3 submodule 0 PWM_A channel occasionally fails to start, where after the first high level it remains constant and subsequent pulses do not appear.After the inspection, it was found that the "run" bit of the pwm was not correctly set. Even though repeated startup operations were added in the program later, this anomaly still occurred. liu626_0-1782287927569.png Re: RT1176 PWM startup failed Hi @liu626, Are you using a custom board or an EVK? If you are using the EVK, did you make any rework to it? Could you share the configuration you are using for PWM3? Are you using an example as a reference? If so, which one? If you try to replicate the issue using a project with only PWM3, does the problem persist? Does this only happen with PWM3 submodule 0 PWM_A channel? Has this occurred on other PWM modules or submodules? Is there any other task or interrupt that manipulates PWM3 registers and could affect or overwrite the run bit? Best Regards, Pablo Re: RT1176 PWM startup failed hi,I used a custom circuit board. I didn't refer to any examples. This was a problem that was discovered during the official development of the project. I configured six PWM channels for pulse control. Only this channel had problems, while no such issue occurred on the other sub-modules. I checked and found that only this channel was using the PWM3 module. No other interfering factors were detected. Below is my configuration. static axis_ctrl_t g_axes[AXIS_NUM] = { { .id = AXIS_X1, .name = "X1", .pwmBase = PWM1, .pwmModule = kPWM_Module_0, .pwmChannel = kPWM_PwmA, .tmrBase = TMR3, .lowCh = kQTMR_Channel_2, .highCh = kQTMR_Channel_3, .tmrInputsrc=kQTMR_ClockCounter2InputPin, .cascadePcs = 6U, .faultNum = 0U, .hwExactSupported = true, .outTrigMask = kPWM_ValueRegisterMask_3, }, { .id = AXIS_X2, .name = "X2", .pwmBase = PWM2, .pwmModule = kPWM_Module_0, .pwmChannel = kPWM_PwmA, .tmrBase = TMR2, .lowCh = kQTMR_Channel_0, .highCh = kQTMR_Channel_1, .tmrInputsrc=kQTMR_ClockCounter0InputPin, .cascadePcs = 4U, .faultNum = 0U, .hwExactSupported = true, .outTrigMask = kPWM_ValueRegisterMask_3, }, { .id = AXIS_Y, .name = "Y", .pwmBase = PWM3, .pwmModule = kPWM_Module_0, .pwmChannel = kPWM_PwmA, .tmrBase = TMR3, .lowCh = kQTMR_Channel_0, .highCh = kQTMR_Channel_1, .tmrInputsrc=kQTMR_ClockCounter0InputPin, .cascadePcs = 4U, .faultNum = 0U, .hwExactSupported = true, .outTrigMask = kPWM_ValueRegisterMask_3, }, { .id = AXIS_Z, .name = "Z", .pwmBase = PWM4, .pwmModule = kPWM_Module_0, .pwmChannel = kPWM_PwmA, .tmrBase = TMR1, .lowCh = kQTMR_Channel_0, .highCh = kQTMR_Channel_1, .tmrInputsrc=kQTMR_ClockCounter0InputPin, .cascadePcs = 4U, .faultNum = 0U, .hwExactSupported = true, .outTrigMask = kPWM_ValueRegisterMask_3, }, { .id = AXIS_EX1, .name = "EX1", .pwmBase = PWM1, .pwmModule = kPWM_Module_1, .pwmChannel = kPWM_PwmA, .tmrBase = TMR1, .lowCh = kQTMR_Channel_2, .highCh = kQTMR_Channel_3, .tmrInputsrc=kQTMR_ClockCounter2InputPin, .cascadePcs = 6U, .faultNum = 1U, .hwExactSupported = true, .outTrigMask = kPWM_ValueRegisterMask_3, }, { .id = AXIS_EX2, .name = "EX2", .pwmBase = PWM2, .pwmModule = kPWM_Module_1, .pwmChannel = kPWM_PwmA, .tmrBase = TMR2, .lowCh = kQTMR_Channel_2, .highCh = kQTMR_Channel_3, .tmrInputsrc=kQTMR_ClockCounter2InputPin, .cascadePcs = 6U, .faultNum = 1U, .hwExactSupported = true, .outTrigMask = kPWM_ValueRegisterMask_3, }, };static void APP_Init_PWM_QTMR(void) { pwm_config_t pwmConfig; pwm_fault_param_t faultConfig; qtmr_config_t qtmrConfig; PWM_GetDefaultConfig(&pwmConfig); pwmConfig.pairOperation = kPWM_Independent; pwmConfig.reloadLogic = kPWM_ReloadImmediate; PWM_FaultDefaultConfig(&faultConfig); faultConfig.faultLevel = true; faultConfig.enableCombinationalPath = false; faultConfig.faultClearingMode = kPWM_ManualSafety; faultConfig.recoverMode = kPWM_NoRecovery; QTMR_GetDefaultConfig(&qtmrConfig); CLOCK_EnableClock(kCLOCK_Qtimer1); CLOCK_EnableClock(kCLOCK_Qtimer2); CLOCK_EnableClock(kCLOCK_Qtimer3); PWM_StopTimer(PWM1, 0x0FU); PWM_StopTimer(PWM2, 0x0FU); PWM_StopTimer(PWM3, 0x0FU); PWM_StopTimer(PWM4, 0x0FU); pwm_fault_input_filter_param_t faultFilter; faultFilter.faultFilterPeriod = 255U; faultFilter.faultFilterCount = 7U; faultFilter.faultGlitchStretch = false; /* 记录每个 PWM 实例上已配置的 fault channel,避免重复设置 */ uint16_t pwm1FaultDone = 0U, pwm2FaultDone = 0U, pwm3FaultDone = 0U, pwm4FaultDone = 0U; for (uint8_t i = 0U; i < AXIS_NUM; i++) { axis_ctrl_t *ax = &g_axes[i]; PWM_Init(ax->pwmBase, ax->pwmModule, &pwmConfig); PWM_SetupFaults(ax->pwmBase, (pwm_fault_input_t)ax->faultNum, &faultConfig); /* 故障滤波(每个 PWM 实例的每个 fault channel 只设一次) */ { uint16_t *faultDone; if (ax->pwmBase == PWM1) faultDone = &pwm1FaultDone; else if (ax->pwmBase == PWM2) faultDone = &pwm2FaultDone; else if (ax->pwmBase == PWM3) faultDone = &pwm3FaultDone; else faultDone = &pwm4FaultDone; uint16_t faultBit = (uint16_t)(1U << ax->faultNum); if ((*faultDone & faultBit) == 0U) { PWM_SetupFaultInputFilterExt(ax->pwmBase, (pwm_fault_channels_t)ax->faultNum, &faultFilter); *faultDone |= faultBit; } } /* Fault 时输出低电平 */ ax->pwmBase->SM[ax->pwmModule].OCTRL &= ~(PWM_OCTRL_PWMAFS_MASK | PWM_OCTRL_PWMBFS_MASK); APP_PWM_Unmap_Selected_Fault(ax); APP_PWM_ClearFault_Safe(ax); ax->pwmBase->SM[ax->pwmModule].INIT = 0U; ax->pwmBase->SM[ax->pwmModule].VAL0 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL1 = 1U; ax->pwmBase->SM[ax->pwmModule].VAL2 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL3 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL4 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL5 = 0U; ax->pwmBase->SM[ax->pwmModule].TCTRL = PWM_TCTRL_OUT_TRIG_EN(ax->outTrigMask); APP_PWM_Disable_Output(ax); if (ax->hwExactSupported) { qtmrConfig.primarySource = ax->tmrInputSrc; QTMR_Init(ax->tmrBase, ax->lowCh, &qtmrConfig); QTMR_Init(ax->tmrBase, ax->highCh, &qtmrConfig); ax->tmrBase->CHANNEL[ax->lowCh].CTRL = TMR_CTRL_CM(kQTMR_PriSrcRiseEdge) | TMR_CTRL_PCS(ax->tmrInputSrc); ax->tmrBase->CHANNEL[ax->highCh].CTRL = TMR_CTRL_CM(kQTMR_CascadeCount) | TMR_CTRL_PCS(ax->cascadePcs); APP_QTMR_Disable_Low_OFLAG_Output(ax); QTMR_DisableInterrupts(ax->tmrBase, ax->lowCh, 0xFFU); QTMR_DisableInterrupts(ax->tmrBase, ax->highCh, 0xFFU); QTMR_ClearStatusFlags(ax->tmrBase, ax->lowCh, 0xFFU); QTMR_ClearStatusFlags(ax->tmrBase, ax->highCh, 0xFFU); } ax->phase = kAxisIdle; ax->armed = false; ax->running = false; ax->done = true; #if HARD_PWM_STATE_GUARD_ENABLE APP_StateGuard_Reset(ax); #endif } /* 使能 QTMR 中断 */ NVIC_SetPriority(TMR1_IRQn, 2U); NVIC_SetPriority(TMR2_IRQn, 2U); NVIC_SetPriority(TMR3_IRQn, 2U); EnableIRQ(TMR1_IRQn); EnableIRQ(TMR2_IRQn); EnableIRQ(TMR3_IRQn); }static bool APP_PWM_Config_Pulse(axis_ctrl_t *axis, uint32_t highCnt400M, uint32_t lowCnt400M) { pwm_clock_prescale_t prescale; uint16_t periodTicks; uint32_t totalCnt400M = highCnt400M + lowCnt400M; if ((axis == NULL) || (totalCnt400M == 0U)) return false; if (!APP_PWM_SelectPrescaler_FromPeriodCnt400M(totalCnt400M, &prescale, &periodTicks)) return false; uint32_t highTicks32 = (uint32_t)(((uint64_t)periodTicks * (uint64_t)highCnt400M + ((uint64_t)totalCnt400M / 2ULL)) / (uint64_t)totalCnt400M); if (highTicks32 == 0U) highTicks32 = 1U; if (highTicks32 >= periodTicks) highTicks32 = (uint32_t)periodTicks - 1U; uint32_t riseTicks32 = 0U; uint32_t fallTicks32 = highTicks32; #if HARD_PWM_LOW_START_PHASE_ENABLE uint32_t lowTicks32 = (uint32_t)periodTicks - highTicks32; if (lowTicks32 >= (2U * HARD_PWM_LOW_START_PHASE_MIN_TICKS)) { uint32_t desiredLeadCnt400M = highCnt400M; uint32_t minLeadCnt400M = (uint32_t)HARD_PWM_LOW_START_PHASE_MIN_US * 400U; if (desiredLeadCnt400M < minLeadCnt400M) desiredLeadCnt400M = minLeadCnt400M; uint32_t desiredLeadTicks32 = (uint32_t)(((uint64_t)periodTicks * (uint64_t)desiredLeadCnt400M + ((uint64_t)totalCnt400M / 2ULL)) / (uint64_t)totalCnt400M); if (desiredLeadTicks32 < HARD_PWM_LOW_START_PHASE_MIN_TICKS) desiredLeadTicks32 = HARD_PWM_LOW_START_PHASE_MIN_TICKS; uint32_t maxRiseByHalfTicks32 = lowTicks32 / 2U; uint32_t postGuardTicks32 = (uint32_t)(((uint64_t)periodTicks * (uint64_t)(HARD_PWM_VAL3_POST_LOW_GUARD_US * 400U) + ((uint64_t)totalCnt400M / 2ULL)) / (uint64_t)totalCnt400M); if (postGuardTicks32 < HARD_PWM_VAL3_POST_LOW_GUARD_MIN_TICKS) postGuardTicks32 = HARD_PWM_VAL3_POST_LOW_GUARD_MIN_TICKS; uint32_t maxRiseByPostGuardTicks32 = (lowTicks32 > postGuardTicks32) ? (lowTicks32 - postGuardTicks32) : 0U; uint32_t selectedRiseTicks32; if (maxRiseByHalfTicks32 >= desiredLeadTicks32) { selectedRiseTicks32 = desiredLeadTicks32; if (selectedRiseTicks32 > maxRiseByHalfTicks32) selectedRiseTicks32 = maxRiseByHalfTicks32; } else if (maxRiseByPostGuardTicks32 >= desiredLeadTicks32) { selectedRiseTicks32 = desiredLeadTicks32; if (selectedRiseTicks32 > maxRiseByPostGuardTicks32) selectedRiseTicks32 = maxRiseByPostGuardTicks32; } else { selectedRiseTicks32 = maxRiseByPostGuardTicks32; } if (selectedRiseTicks32 >= HARD_PWM_LOW_START_PHASE_MIN_TICKS) { riseTicks32 = selectedRiseTicks32; fallTicks32 = riseTicks32 + highTicks32; } } #endif if (fallTicks32 >= (uint32_t)periodTicks) fallTicks32 = (uint32_t)periodTicks - 1U; uint16_t riseTicks = (uint16_t)riseTicks32; uint16_t fallTicks = (uint16_t)fallTicks32; PWM_SetPwmLdok(axis->pwmBase, APP_PwmModuleMask(axis), false); uint16_t ctrl = axis->pwmBase->SM[axis->pwmModule].CTRL; ctrl &= (uint16_t)(~PWM_CTRL_PRSC_MASK); ctrl |= PWM_CTRL_PRSC(prescale); axis->pwmBase->SM[axis->pwmModule].CTRL = ctrl; axis->pwmBase->SM[axis->pwmModule].INIT = 0U; axis->pwmBase->SM[axis->pwmModule].VAL0 = 0U; axis->pwmBase->SM[axis->pwmModule].VAL1 = (uint16_t)(periodTicks - 1U); if (axis->pwmChannel == kPWM_PwmA) { axis->pwmBase->SM[axis->pwmModule].VAL2 = riseTicks; axis->pwmBase->SM[axis->pwmModule].VAL3 = fallTicks; } else if (axis->pwmChannel == kPWM_PwmB) { axis->pwmBase->SM[axis->pwmModule].VAL4 = riseTicks; axis->pwmBase->SM[axis->pwmModule].VAL5 = fallTicks; } axis->pwmBase->SM[axis->pwmModule].TCTRL = PWM_TCTRL_OUT_TRIG_EN(axis->outTrigMask); PWM_SetPwmLdok(axis->pwmBase, APP_PwmModuleMask(axis), true); PWM_SetPwmLdok(axis->pwmBase, APP_PwmModuleMask(axis), true); axis->pwmConfigValid = true; axis->cachedHighCnt400M = highCnt400M; axis->cachedLowCnt400M = lowCnt400M; return true; } Re: RT1176 PWM startup failed Hi @liu626, Could you help me isolate the configuration and test whether the issue persists when only PWM3 is initialized? After reviewing the configuration, you shared and in order to try to replicate the behavior, I have the following questions: What is the definition of axis_ctrl_t? Are HARD_PWM_LOW_START_PHASE_ENABLE and HARD_PWM_STATE_GUARD_ENABLE enabled in your application? What do the following APP functions do? APP_PWM_Unmap_Selected_Fault APP_PWM_ClearFault_Safe APP_PWM_Disable_Output APP_QTMR_Disable_Low_OFLAG_Output APP_StateGuard_Reset APP_PWM_SelectPrescaler_FromPeriodCnt400M APP_PwmModuleMask Best Regards, Pablo Re: RT1176 PWM startup failed Thank you for your reply. The GPIO pin I'm using is GPIO_EMC_B1_29 of the rt1176."axis_ctrl_t" is the definition related to the motor shaft. * PWM output pulse -> Trigger XBAR signal -> Falling edge of pulse drives the external clock input of QTMR -> * QTMR 32-bit cascaded counter decrements by 1 -> When it reaches 0, triggers QTMR comparison interrupt -> Interrupt internally turns off PWM * At the same time, QTMR triggers the hardware Fault, directly pulling down the physical output pin of PWM. .id = AXIS_Y, .name = "Y", /* Used for serial port logging or breakpoint debugging to identify the Y-axis */ /* ================= PWM Output Resource Allocation ================= */ .pwmBase = PWM3, /* The Y-axis uses the FlexPWM3 module */ .pwmModule = kPWM_Module_0, /* Uses the sub-module 0 of PWM3 (each PWM has 4 sub-modules from 0 to 3) */ .pwmChannel = kPWM_PwmA, /* Uses the output pin of phase A of sub-module 0, corresponding to the physical pin GPIO_EMC_B1_29 */ /* ================= 32-bit QTMR cascaded count resource allocation ================= */ .tmrBase = TMR3, /* The Y-axis uses the QTMR3 peripheral (corresponding to IRQ interrupt number TMR3_IRQn) */ .lowCh = kQTMR_Channel_0, /* 16-bit low counter: uses channel 0 of TMR3 */ .highCh = kQTMR_Channel_1,/* 16-bit high counter: uses channel 1 of TMR3 */ /* 👉 .lowCh and .highCh are paired, and in the hardware level, they are automatically combined into a 32-bit counter */ /* ================= Configuration of Hardware Cascaded Clock Sources (Core Critical) ================= */ .tmrInputsrc=kQTMR_ClockCounter0InputPin, /* The clock source for Channel 0: Set to "External Pin Input 0". In the XBAR configuration, the falling edge of the pulse from PWM3 is connected to the input pin of Channel 0 of TMR3 through the XBAR. Therefore, every time a pulse is output by PWM, Channel 0 (16-bit) will perform a decrement operation once. */ .cascadePcs = 4U, /* Configuration of the clock source (PCS) for the high 16-bit channel (Channel 1). In the QTMR register of i.MX RT, the PCS value corresponds as follows: 0-3 = External pin input; 4 = Overflow/Termination event of Channel 0; 5 = Overflow/Termination event of Channel 1; 6 = Overflow/Termination event of Channel 2; 7 = Overflow/Termination event of Channel 3. Here, it is configured as 4U, meaning: Let "Channel 1 of TMR3" monitor the "Overflow event of Channel 0 of TMR3". HARD_PWM_LOW_START_PHASE_ENABLE and HARD_PWM_STATE_GUARD_ENABLE have been enabled. APP_PWM_Unmap_Selected_Fault Function: Remove the Fault pin mapping corresponding to the current axis. Call the underlying PWM_SetupFaultDisableMap function to disable the Fault. The purpose is: When the hardware Fault is not needed, prevent accidental external interference from causing the PWM to be turned off, facilitating the underlying debugging process. APP_PWM_ClearFault (original code function) Function: Clear the Fault status flag (axis->pwmBase->FSTS) of the PWM module. After triggering a hardware Fault, you must first clear this flag before the PWM can be allowed to restart. APP_PWM_Disable_Output Function: Immediately stop the PWM timer, force the pin to output a low level (PWM_SetPwmForceOutputToZero), and enable the output. Its purpose is to ensure that the pin does not output a high level due to being left floating or in the default state before the motor starts, which could cause the motor to move erratically. APP_QTMR_Disable_Low_OFLAG_Output Function: Disable the OFLAG (status flag) output of QTMR and force the OFLAG to be at a low level. In conjunction with the XBAR hardware, its role is to cut off the path from the QTMR output to the PWM Fault pin, preventing accidental triggering of Fault before startup. APP_StateGuard_Reset Function: Clears the counters and flags of the state guard (watchdog). This function is used to reset these protection variables before stopping or restarting the system if it encounters a long period of no pulse change or a deadlock when HARD_PWM_STATE_GUARD_ENABLE is enabled. APP_PWM_SelectPrescaler_FromPeriodCnt400M Function: This is a very core underlying frequency calculation function. It receives the total 400MHz count value of High + Low, and calculates how many prescalers (PRSC) and PWM periods (PERIOD) should be set in order to fit into the 16-bit PWM register. Please note: If the calculated period exceeds 65535 and the division coefficient is out of range, this function will return false, causing the motor to fail to start. APP_PwmModuleMask Function: Convert the index number of the PWM sub-module (for example, kPWM_Module_0 with the value 0) into a bit mask shifted left by N bits. Many of NXP's PWM registers (such as OUTEN, MCTRL) are controlled bit by bit. This function is responsible for generating the correct binary mask. Re: RT1176 PWM startup failed I have found the cause. It is because the internal load of the PIT interrupt in the cm4 core is too heavy, which has affected the PWM operation of the cm7 core. After I reduced the load of the PIT interrupt, the failure of PWM startup disappeared.
View full article
S32DS 3.4 ライセンスの問題 NXPチームの皆様へ S32DS 3.4の再アクティベーションを試みましたが、できず、下の画像のようなメッセージが表示されました。現在、古いコンピューターでライセンスを復元することができません。この問題を解決するお手伝いをしていただけないでしょうか?よろしくお願いいたします。 ben_chin_0-1784189249520.png Re: S32DS 3.4 License Problem こんにちは、 利用可能なライセンス数が増加しました。
View full article
KW47 extended advertising Hi, The sdk version I'm using is 26.06 . The routine is kw47loc_loc_reader_freertos . #define gAppIsPeripheral_d                   1U   It was found that the return value of calling BluetoothLEHost_StartExtAdvertising is 4(gBleFeatureNotSupported_c)  I'd like to use extended advertising. Please give me your support.   Thanks!   Re: KW47 extended advertising Hello, Hope you are doing well. What modifications have you made in the example? In order to configure Extended Advertising in an application, the first steps are to set the extended advertising parameters with Gap_SetExtAdvertisingParameters and setting the advertising data by calling Gap_SetExtAdvertisingData. For the full setup sequence and parameter details, please check this guide: Extended advertising — MCUXpresso SDK Documentation   Hope this helps! Best regards, Ana Sofia. Re: KW47 extended advertising Hi, The sdk version I'm using is 26.06. The imported routine is kw47loc_loc_reader_freertos.  Modify the macro definition of gAppIsPeripheral_d in the routine to 1, and at the same time add BleApp_Start() in the BluetoothLEHost_AppInit function;  Nothing else has been modified. It was found that the return value of calling BluetoothLEHost_StartExtAdvertising is 4(gBleFeatureNotSupported_c)  wjw2026_1-1784164794603.png wjw2026_0-1784164779249.png   Thanks! Re: KW47 extended advertising Hi @wjw2026 , Could you please confirm if you were able to follow the steps from the Extended Advertising Guide ? There are several required steps involved in the Peripheral configuration for extended advertising, verifying those settings may be helpful in troubleshooting the behavior you're observing. Best regards, Ana Sofia.
View full article
i.MX95におけるUSXGMIIマルチレート こんにちは、 i.MX95に以下のイーサネット速度をサポートできるイーサネットポートを実装できるかどうかを評価しようとしています。 10GBASE-T 5GBASE-T 2.5GBASE-T 1000BASE-T 100BASE-TX 10BASE-Te 一般的に、デザイン上に10Gbit対応のイーサネットPHYを設置し、USXGMIIまたはXFIのいずれかのインターフェースを通じてi.MX95イーサネットコントローラに接続する必要があります 私たちの理解では、USXGMIIインターフェースは理論上マルチレートインターフェースであり、1リンクで10Gbitから10bitまでのあらゆる速度を実現できます。 これに対し、XFIインターフェースは単一レートのインターフェースで、10Gbitしか対応できません。 i.MX95のリファレンスマニュアル(例:)セクション104.2、表621)i.MX95はXFIおよび「10G-USXGMII」の両方をサポートしています。最初は、私たちが望むUSXGMIIインターフェースがサポートされているように見えます。 しかし、いくつか私たちを困惑させる点があります。 1.「10G-USXGMII」という宣言は、理論上はインターフェースがUSXGMIIリンクであることを意味するかもしれませんが、実際には10Gbitモードでしか動作しません。 2. NXP評価ボードIMX95LPD5EVK-19は、Marvell AQR113C PHYを使用して10GBase-Tポートを実装しています。 a) 図1のブロック図、セクション1.1では、PHYがUSXGMIIインターフェースに接続されているように見えます: stefan_wenninge_0-1784101377785.png b) 関連するセクション2.11.3「10 Gbitイーサネットインターフェース」では、AQR113Cイーサネットトランシーバーが10Gbitから10bitまでのすべてのデータレートをサポートするとされており、真のUSXGMIIを示唆しています: stefan_wenninge_1-1784101562514.png c) この節では、イーサネットPHYを接続するインターフェースがXFIであることも記載されています。 stefan_wenninge_2-1784101765113.png 結論として、i.MX95がフルのマルチレートUSXGMIIに対応しているのか、それとも10Gbit専用バージョンのみ対応しているのか混乱しています。 NXPの評価ボードを参考にしてみましたが、そのボードの10GbEポートがUSXGMII(10Gbitから10bitまでのマルチレート対応)で接続されているのか、XFI(10Gbitのみ)で接続されているのかも分かりません。 教えていただけますか: i.MX95に10Gbitから10Gbitまでの速度をサポートする真のマルチレート10GbEポートを実装することは可能でしょうか? Re: USXGMII multi-rate on i.MX95 詳細なご回答をいただき、誠にありがとうございます。 これで私たちの側の混乱は解消されました! Re: USXGMII multi-rate on i.MX95 1. 「10G-USXGMII」の意味 「10G-USXGMII」とは、10G専用モードではなく、標準的なマルチレートUSXGMIIプロトコルを指します。「10G」は固定されたSerDesレーン速度を示し、USXGMIIは10M、100M、1G、2.5G、5G、10Gイーサネットの帯内レート適応をサポートしています。 i.MX95では、このモードはPCS_PROT_10G_SXGMII設定で表されます。 2. i.MX95 EVKで使用されたインターフェース i.MX95 EVKは、USXGMIIではなくXFI(10GBASE-R)を使用します。imx95-19x19-evk.dtsでは、enetc_port2 は次のように設定されています。 phy-mode = "10gbase-r"; したがって、搭載されているAQR113CはXFIモードで動作します。 3. 真のマルチレートUSXGMIIはサポートされていますか? はい。i.MX95 NETCハードウェアはUSXGMIIをサポートし、LinuxのENETC4ドライバはenetc4_set_port_speed()を通じて速度変更を処理します。Marvell AQR113CはUSXGMIIホストインターフェースモードもサポートしています。 4. カスタムボードに必要なものは何ですか? マルチレート動作を完全に有効にするには: デバイスツリーの設定: phy-mode = "usxgmii"; managed = "in-band-status"; AQR113Cのファームウェアを、XFIではなくUSXGMIIホストモードに設定してください。 EVKは10GbEポートにXFIを使用していますが、カスタムi.MX95設計ではUSXGMIIをAQR113C(または類似のPHY)と組み合わせて、10M/100M/1G/2.5G/5G/10Gを単一のMACからPHYリンクまでサポートできます。 よろしくお願いします。 Re: USXGMII multi-rate on i.MX95 もう一つ追加で質問します:Marv AQR113C ellのドライバはNXP Linux BSPに含まれているのか、それとも自分たちで用意しなければならない外部モジュールですか? Re: USXGMII multi-rate on i.MX95 私は元の投稿者ではありませんが、私もusxgmiiを動作させようとしています。 NXPは、usxgmiiがBSPカーネル上で動作するかどうかを検証したことがありますか?mv-cux3610 PHYで使用しようとしていますが、以下のエラーが発生します。 [ 43.063202] nxp_enetc4 0002:00:10.0 (unnamed net_device) (uninitialized): MAC returned PCS which does not support usxgmii [ 43.074224] nxp_enetc4 0002:00:10.0 (unnamed net_device) (uninitialized): failed to validate link configuration for inband [ 43.085308] nxp_enetc4 0002:00:10.0: Failed to create phylink [ 43.091726] nxp_enetc4 0002:00:10.0: probe with driver nxp_enetc4 failed with error -22 これは、NetC PCSがUSXGMIIサポートを宣伝しておらず、10Gbase-R、2500-basex、SGMIIのみが原因のようです: quentin_sai_0-1784223770904.png (これはLF-6.18.YのLinux-IMXブランチでの話です) Re: USXGMII multi-rate on i.MX95 このドライバーはNXP Linux BSPに含まれています。リンク: https://github.com/nxp-real-time-edge-sw/real-time-edge-linux/blob/linux_6.18.20/drivers/net/phy/aquantia/aquantia_main.c Re: USXGMII multi-rate on i.MX95 お返事ありがとうございます! 最後に質問です。i.MX95 EVKのenetc_port2とAQR113CをUSXGMIIモードに設定することは可能でしょうか?これにより、EVK上でUSXGMIIインターフェースのマルチレート機能をテストできるのでしょうか? Re: USXGMII multi-rate on i.MX95 EVKで単純に「DTSをusxgmiiに切り替える」のはソフトウェアレベルの試みに過ぎません。 また、USXGMIIファームウェアでAQR113Cを再プロバイニングする必要があり、EVKのXFI向けボード設計のため、マルチレート検証には信頼性が高くありません。 もし目標が真のマルチレートUSXGMII(10M/100M/1G/2.5G/5G/10G)を検証することであれば、USXGMII向けにカスタムボードを作ることを推奨します(USXGMIIホストモードファームウェアではSerDes routing + AQR113C + phy-mode = "usxgmii")。 AQR113C用のUSXGMIIプロビジョニングファームウェアを取得した後、EVKボードを使うことができますが、その制限にはご注意ください。 よろしくお願いします。
View full article
eFlexPWM input capture not capturing on S32K364 – flags set but CAPTCOMPB remains zero I'm using the eFlexPWM module (instance IP_EFLEXPWM_0) on an S32K364 microcontroller to measure the frequency and period of an external signal via input capture. I am using submodule 2 (SM[2]). My configuration is as follows: SM2_CAPTCTRLB->EDGB0 = 0x02; (capture on rising edge for capture circuit 0) SM2_CAPTCTRLB->EDGB1 = 0x02; (capture on rising edge for capture circuit 1) SM2_ARMB = 1; (arm the capture circuits) After running the code, I observe the following: In SM2_CAPTCTRLB, the counter status bits show: CB0CNT = 0x4 CB1CNT = 0x4 In SM2_STS, both flag bits are set: CFB0 = 1 CFB1 = 1 However, the captured values (SM2_CAPTCOMPB) remain 0 for both capture circuits – no data is latched. What could be causing this? Is there any additional configuration needed (e.g., clock enable, input muxing, or counter setup) that I might have missed? The flags indicate that capture events are detected, but the captured values are not updated. Any insight would be greatly appreciated. Feel free to add any additional details (like your pin muxing settings or counter mode) if needed. Good luck! Re: eFlexPWM input capture not capturing on S32K364 – flags set but CAPTCOMPB remains zero Hi First, I checked the latest S32K3 RTD 7.0.x; however, the S32 Configuration Tool does not yet support the eFlexPWM E-Capture functionality. If it is convenient, could you share your project so I can test it on the S32K396? (Unfortunately, I don’t have the S32K364; I only have the S32K396-BGA-DC1 evaluation board.) Secondly, please review section “56.3.14 Enhanced capture (E-Capture)” in S32K396RM (Rev. 4, 11/2024). Please check the registers mentioned in that section, especially those in Figure 254. E-Capture logic. You can also share screenshots of the eFlexPWM_0 registers with me.  56.3.14.1.1 E-Capture logic S32K396RM (Rev. 4 11 2024).png Besides the bits you mentioned in SM2_CAPTCTRLB [EDGB0],[EDGB1],[ARMB], how did you configure the other bits in SM2_CAPTCTRLB?   Since you observed that SM2_CAPTCTRLB[CB0CNT] = 0x4 and [CB1CNT] = 0x4, have you checked the corresponding register values of SM2_CVAL4, SM2_CVAL4CYC, SM2_CVAL5, and SM2_CVAL5CYC?   In addition, if you want to read the value of SM2_CAPTCOMPB[EDGCNTB], please first enable SM2_CAPTCTRLB[EDGCNTB_EN] and SM2_CAPTCOMPB[EDGCMPB]. I’m not sure why you set SM2_CAPTCOMPB[EDGCMPB] to 0, as this seems to prevent the comparator in Figure 254. E-Capture logic from functioning correctly. Best Regards, Robin Re: eFlexPWM input capture not capturing on S32K364 – flags set but CAPTCOMPB remains zero It appears that the period of submodule2 is too short. Please read "56.3.18.3 Running a submodule at a lower frequency than submodule 0" and try selecting a lower frequency clock source for submodule2, such as AUX_CLK or EXT_CLK. Re: eFlexPWM input capture not capturing on S32K364 – flags set but CAPTCOMPB remains zero Hi@Robin_Shen , I have successfully implemented external frequency measurement by properly configuring the MCTRL and CAPTCTRLB registers. However, testing shows the minimum measurable frequency I can achieve is 5 kHz, while my requirement is to support frequencies as low as 1 Hz. I have attempted adjusting the Prescaler and PrescalerAlt configurations, yet no improvement was observed. Could you please share some suggestions and troubleshooting approaches? Thank you very much for your support.
View full article
RF Power Amplifier Design - MRF13750H Hello! I am designing an 805 MHz RF power amplifier using the MRF13750H, and my design is based on the 915 MHz reference circuit found in the datasheet. However, I only have access to Usimmics for simulating the matching networks; I do not have access to the software NXP uses to open their design files. Therefore, to design the matching networks, I am requesting the complete schematic for the MRF13750H 915 MHz reference circuit from NXP, including the microstrip line dimensions, as this information is not provided in the datasheet. If possible, I would also like to request the large-signal model impedances at 805 MHz; otherwise, I will base my design on the values ​​provided for 915 MHz. The reference circuit at 915Mhz and the datasheet is attached below. On the other hand, if anyone knows a different method for designing the matching networks at 805 MHz, I would appreciate the input.
View full article
我们能否在 i.mx9 中使用已配置的证书或密钥来设置 HTTPS 连接或 TLS 连接? i.MX93 上配置的证书和私钥可以直接用于建立 HTTPS/TLS 连接吗?如果可以,那么访问和使用这些凭据进行客户端/服务器身份验证和 mTLS 实现的推荐方法是什么? 配置完成后,安全对象 blob 会出现在 /etc/ele/ 中,那么在实际的 HTTPS/TLS 连接中使用这些已配置的凭据的推荐工作流程是什么? Re: can we use provisioned cert or key for setting up in the https connection or tls connection in i 嗨, @Manuel_Salas 谢谢你的回复。 关于 mbedTLS/opaque-key 指南——我们这边已经解决了私钥的问题。 剩下的问题具体是关于证书,该证书通过 EL2GO 配置,并与私钥一起存储在 /etc/ele/ 中。由于证书是公共数据,我们需要将其提取为纯 DER 格式,以便交给 mbedtls_x509_crt_parse_der() 进行 TLS 握手——与密钥不同,它不需要保持不透明。 支持的 SMW/PSA 调用是什么,才能检索已配置证书对象的明文 DER 字节? 具体来说:它是通过 psa_ps_get() / psa_its_get()(PSA 保护存储/内部可信存储)使用对象 ID 作为 UID 公开,还是通过不同的 SMW API 公开?我们在已安装的 SMW 头文件中看到了 protected_storage.h 和 internal_trusted_storage.h,但在基于它进行构建之前,我们想确认这是否是证书对象的预期路径。 Re: can we use provisioned cert or key for setting up in the https connection or tls connection in i 你好@NEXUSNERD 希望你一切都好。 在 i.MX93 上,配置流程的设计使得私钥始终受到ELE的保护。 因此,存储在 /etc/ele/ 中的 blob 是安全的对象表示,允许 ELE 重新加载或引用已配置的密钥材料,它们不应被视为普通的 TLS 密钥文件。 您可以查看imx-secure-enclave (Mbed-TLS)。 顺祝商祺! 萨拉斯。
View full article
LED 的 IO 扩展 我目前正在设计用于定制测量设备的开关矩阵板。 为了路由信号,我计划使用光中继器,准确地说是 G3VM-61DR1。 所以我需要控制超过 250 个!以某种方式使用 LED(1.5-1.8V 6-8mA)。 同时开启的设备数量将少于25台。 供电电压为3.3V或更低,温度应在40°C左右。 我们只需要打开或关闭它们,不需要调光或PWM调光。 我不想使用LED驱动器,因为它可能会引入噪声。 我无法使用传统的矩阵式电路,因为无法预知哪些开关会同时处于开启状态。 因此,唯一的选择是为每个继电器/LED 提供一个独立的输出,您的 IO 扩展器看起来很有希望实现这一点,例如PCAL6524 。 由于通道数量较多,我希望尽可能减少每个通道的元器件数量,因此我有几个问题: 我能否依赖 Agile IO 设备的 7.5mA 电流设置,而省略 LED 串联电阻? 如果可以的话,可能会有哪些副作用? 由于这些设备最初配置为输入,因此当它们用于控制 LED 时,某些设备会经历高电流(例如,PCA9535A数据手册第 14/15 页)。对于这么多通道来说,为每个通道使用上拉电阻的传统解决方法并不理想。这是否也会影响 Agile IO 设备? 能否通过给 LED 提供 3.3V 电压,给扩展器提供 1.65V 电压来解决这个问题? 先感谢您 奥托 Re: IO Expansion for LEDs PCAL6524 非常适合驱动大量的光继电器和 LED。然而,敏捷 I/O 驱动能力并不是为了取代所需的串联限流电阻器。为了降低上电时 I/O 仍处于输入状态时出现意外电流的风险,可以考虑使用 VDD(P) 较低的 3.3 V LED 电源,或者实现全局 LED 电源开关等方案。然而,每个 LED 通道都应该始终保留单独的限流电阻。
View full article
FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages On i.MXRT1176 we are using FLEXCAN with EDMA. (SDK 26.03) We have a callback defined for DMA transfer complete. This is our flow: 1. Call `FLEXCAN_TransferReceiveFifoEDMA()` to start the transfer. 2. On DMA transfer completion, user-defined callback is called. 3. Data is copied from DMA buffers, and `FLEXCAN_TransferReceiveFifoEDMA()` is called to continue receiving messages. 4. Repeat Steps 2-4 We noticed that when we transmit messages from another node in a burst with just the bare minimum Inter-Frame Space, we see an increase in number of ACK errors - the iMX is unable to ACK the messages.  Going through the flow, it appears that every time there is a DMA transfer complete callback, DMA is disabled on FLEXCAN. It is re-enabled again when `FLEXCAN_TransferReceiveFifoEDMA()` is called.  This is done by calling `FLEXCAN_EnableRxFifoDMA()`. The enabling/disabling DMA updates the DMA bit in FLEXCAN's MCR register, and it can only be done in Freeze mode. As we are receiving messages in a burst, it is possible that a transmission is actively in progress when FLEXCAN is put it freeze mode. And it is unable to ACK the incoming message.   We confirmed that removing that call to `FLEXCAN_EnableRxFifoDMA()` removes all ACK errors, though now we are dropping some messages. Also, we tried spacing out the messages, and that also got rid of the ACK errors. Can you please confirm if this is indeed an issue with the implementation, or if we should be rearchitecting it in a different way? Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages Hi @r-uv , Thank you for the detailed analysis. Your observation is consistent with the SDK  implementation. FLEXCAN_TransferReceiveFifoEDMA() is a finite-length transactional API. After each DMA completion, the driver disables the Rx FIFO DMA request, and the next call enables it again. Because changing MCR[DMA] requires Freeze mode, the next frame in minimum-IFS traffic may arrive before FlexCAN returns to Normal mode, resulting in a missed ACK. This also explains why removing the repeated DMA enable/disable operation eliminates the ACK errors but still causes dropped frames: the Freeze-related ACK gap is removed, but the eDMA transfer is not continuously rearmed. For continuous burst traffic, we recommend keeping the Rx FIFO DMA request enabled and using hardware-chained ping-pong/scatter-gather TCDs so that the next buffer is activated automatically. This requires a continuous DMA receive path rather than repeatedly restarting FLEXCAN_TransferReceiveFifoEDMA(). Best regards, Gavin Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages Thanks for the response. Are there any plans of adding this support in the SDK? A continuous DMA based implementation instead of just the current transactional API implementation? 
View full article
求找适用于 PCF8563TS/5,118 的电容 我正在使用 PCF8563TS/5,118 IC,想正确连接 OSCI 引脚上的外部电容。 我正在使用 50k ESR、12.5pF 32.568KHz 的晶体,尽可能短的走线,原理图与数据手册中的应用图完全相同。 我查阅了数据手册和 UM10301,尝试进行计算,以了解该设备。我发现很难找到一种清晰的方法来计算外部电容的值,因为数据表在同一主题的不同页面上提到了并联和串联,即 OSCI 和 OSCO。 我看到外部 OSCI 和 OSCO 引脚并联了一个内部 25pF 电容。数据手册中的表 30 表明 CL 是并联计算的,但有一个注释显示,CL 是串联电容的计算方法。 我找不到能让设备正常工作的外接电容。没有收到 I2C 响应。我尝试了 25pF、22.5pF、20pF、25pF、10pF、8.2pF、6pF。所有 0603 C0G/NP0 帽。 我通过完全不放置电容器,成功地让它在另一块板上工作了。经过计算,这根本说不通。 我想请您举例说明一下如何计算这些输入值(12.5pF 50k ESR 晶体),因为我无论通过计算还是暴力破解都无法使其正常工作。 Re: Help finding capacitor for PCF8563TS/5,118 是的,那是内置电容的数值,我在自己的帖子中也提到过。我已阅读过该文件。 如果你能把你想表达的意思写下来,那会更有帮助。感谢您抽出时间。 Re: Help finding capacitor for PCF8563TS/5,118 db16122_0-1784461035005.png UM10301 PCF85x3、PCF85x63、PCA8565、PCF2123 和 PCA21125 用户手册 Re: Help finding capacitor for PCF8563TS/5,118 亲爱的戴维: db16122 正确地指出了UM10301 中的表 3。如果您的目标负载电容为 12.5pF,则需要在 OSCI 引脚上连接一个 25pF 的中间值的微调电容。 JozefKozon_0-1784524368704.png JozefKozon_1-1784524409356.png 这个 25pF 值可以通过表 30 下方的公式计算得出。在PCF8563 数据手册中。 JozefKozon_2-1784524493868.png 其中 CL 为目标负载电容,在本例中为 12.5pF。 Cosco 是已知的内部电容,25pF。 JozefKozon_3-1784524560452.png 根据公式,可以推导出 Ctrim 值: CL=Ctrim*Cosco/(Ctrim+Cosco) CL*Ctrim+CL*Cosco=Ctrim*Cosco CL*Cosco=Ctrim*Cosco-CL*Ctrim CL*Cosco=Ctrim*(Cosco-CL) CL*Cosco/(Cosco-CL)=Ctrim 边际贡献 = CL * Cosco / (Cosco - CL) = 12.5 * 25 / (25 - 12.5) = 312.5 / 12.5 Ctrim=25pF 由于内部 Cosco 电容还有余量,因此需要可变微调电容。Cosco 值可能在 15pF 到 35pF 之间波动。 JozefKozon_4-1784525019076.png 最诚挚的问候, 约瑟夫
View full article
无法更新 i.MX95 FlexSPI 启动映像的 APP 容器软件版本 各位专家好, 我正在使用 i.MX95 平台,并启用ROLLBACK_INDEX_IN_CONTAINER 的回滚保护功能。 我在local.conf文件中引入了以下变量: export ROLLBACK_INDEX_IN_CONTAINER = "1" 该值会在整个构建过程中传递,构建日志证实mkimage_imx8被调用时使用了“1”。 构建eMMC 启动映像时,解析生成的镜像显示容器软件版本已正确更新。  if [ 1 ]; then \ ./../mkimage_imx8 -soc IMX9 -cntr_version 2 -sw_version 1 -c \ -ap bl31.bin a55 0x8A200000 \ -ap u-boot-hash.bin a55 0x90200000 \ -ap tee.bin a55 0x8C000000 \ -out u-boot-atf-container.img; \   然而,在构建FlexSPI 启动镜像( imx-boot-imx95-19x19-verdin-fspi.bin-flash_a55_flexspi )时,解析该镜像仍然报告默认的软件版本。 ./mkimage_imx8 -soc IMX9 -parse imx-boot-imx95-19x19-verdin-fspi.bin-flash_a55_flexspi SOC: IMX9 Input container binary to be parsed: imx-boot-imx95-19x19-verdin-fspi.bin-flash_a55_flexspi ********************************* * * * APP CONTAINER 1 * * * ********************************* Length: 0X320 (800) Tag: 0X87 Version: 0X2 Flags: 0X10 Num images: 6 Fuse version: 0 SW version: 0X0 Sig blk offset: 0X310 我在 iMX95/soc.mak 中注意到一个有趣的地方,因为在构建 flash_a55_flexspi 时没有包含 sw_version。 flash_a55_flexspi: $(MKIMG) $(AHAB_IMG) $(MCU_IMG) $(SPL_A55_IMG) $(OEI_IMG_M33) fcb.bin u-boot-atf-container.img ./$(MKIMG) -soc IMX9 -cntr_version $(CTNR_VERSION) $(XSPI_FAST_HASH) -dev flexspi -append $(AHAB_IMG) -c $(OEI_OPT_M33) -msel $(MSEL) \ -m33 $(MCU_IMG) 0 $(MCU_TCM_ADDR) \ -ap $(SPL_A55_IMG) a55 $(SPL_LOAD_ADDR_M33_VIEW) $(V2X_DUMMY) -fcb fcb.bin $(FCB_LOAD_ADDR) -out flash.bin $(call append_container,u-boot-atf-container.img,1) $(call append_fcb) 我的问题是: ROLLBACK_INDEX_IN_CONTAINER是否预期会更新 FlexSPI 启动映像的软件版本? FlexSPI 镜像是否遵循不同的容器生成流程,需要单独配置回滚索引/软件版本? 这是 i.MX95 imx-mkimage版本流程中已知的限制或问题吗? 如果有人已成功在 i.MX95 上为 FlexSPI 启动映像启用ROLLBACK_INDEX_IN_CONTAINER ,能否分享一下预期流程或所需的任何其他配置? 提前感谢! 顺祝商祺! 阿伦·库马尔 Re: Unable to update APP container software version for i.MX95 FlexSPI boot image 你好@arun16598 FlexSPI 镜像不是 AHAB 格式的另一种变体,而是采用了一种组合过程,即先生成引导容器,然后附加 U-Boot/ATF 容器。您的-sw_version 1已在u-boot-atf-container.img上设置;但是,包含 SM/M33、OEI、SPL 和 FCB 的 APP 容器( flash_a55_flexspi首先创建)没有传递-sw_version选项,因此该容器仍然显示SW 版本:0。ROLLBACK_INDEX_IN_CONTAINER用于生成辅助 U-Boot/ATF APP 容器,但它没有传递给flash_a55_flexspi创建的主 APP 容器。如果第一个 FlexSPI APP 容器需要相同的软件版本,则还必须将-sw_version $(ROLLBACK_INDEX_IN_CONTAINER)添加到flash_a55_flexspi中的 mkimage_imx8 调用中。 如果目标是真正实现 AHAB 防回滚强制执行,则需要验证和配置的关键设置是fuse_version和-fuse_version ,而不仅仅是sw_version 。S PSDK 的 i.MX95 防回滚示例明确指出,OEM 防回滚使用 AHAB 容器 YAML 中指定的fuse_version ,然后通过 ELE 的OEM_FW_FUSE提交过程提交该版本。 此致, 志明
View full article
AUTOSAR マカルMPC5744P こんにちは、MPC5744P用のAUTOSAR MCALアプリケーションを無料で作成できるコンパイラオプションはありますか? Re: AUTOSAR MCAL MPC5744P こんにちは、 レガシーのAUTOSAR MCAL for MPC5744Pパッケージ(MPC574xP MCAL 4.x)では、公式に検証されたツールチェーンは通常以下の通りです: Wind River Diab Compiler(最も一般的な資格) グリーンヒルズコンパイラ(GHS) 実際には、AUTOSAR MCALには公式にサポートされているフリーコンパイラMPC5744P提供されていません。 MPC5744Pエコシステムは一般的な組み込み開発のためにS32 Design Studio for Power Architectureをサポートする一方で、MCALパッケージ自体は主にDiabとGHSで開発・検証されました。 DEVKIT-MPC5744P情報にはGCC(S32DS経由)、GHS、Cosmic、その他のMPC5744P開発ツールチェーンが掲載されていますが、それがAUTOSAR MCALリリースがGCCに適格であることを意味しません。 検証済みコンパイラのリストは常にMCALパッケージに付属するリリースノートに記載されています。 よろしくお願いします、 ピーター
View full article
FLEXCAN EDMA - 接收 CAN 消息突发时出现 ACK 错误 在 i.MXRT1176 上,我们使用 FLEXCAN 和 EDMA。(SDK 26.03) 我们定义了 DMA 传输完成的回调函数。 这是我们的流程: 1.调用 ` FLEXCAN_TransferReceiveFifoEDMA()` 开始传输。 2. DMA 传输完成后,调用用户定义的回调函数。 3. 从 DMA 缓冲区复制数据,并调用 `FLEXCAN_TransferReceiveFifoEDMA()` 继续接收消息。 4. 重复步骤 2-4 我们注意到,当我们从另一个节点以突发方式发送消息,且帧间间隔仅为最小值时,ACK 错误的数量会增加——iMX 无法确认消息。 从流程来看,每次 DMA 传输完成回调时,FLEXCAN 上的 DMA 都会被禁用。当调用 `FLEXCAN_TransferReceiveFifoEDMA()` 时,DMA 功能会重新启用。这可以通过调用 ` FLEXCAN_EnableRxFifoDMA()` 来实现。启用/禁用 DMA 会更新 FLEXCAN 的 MCR 寄存器中的 DMA 位,并且只能在冻结模式下进行。由于我们以突发方式接收消息,因此当 FLEXCAN 进入冻结模式时,可能正在进行传输,导致它无法确认接收到的消息。   我们确认,移除对 `FLEXCAN_EnableRxFifoDMA()` 的调用可以消除所有 ACK 错误,但同时也会丢弃一些消息。此外,我们还尝试拉开消息之间的间隔,这样也消除了 ACK 错误。请问这是否确实是实现方面的问题,或者我们是否应该采用不同的架构方式? Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages 嗨@r-uv , 感谢您提供的详细分析。您的观察结果与SDK的实现一致。 FLEXCAN_TransferReceiveFifoEDMA() 是一个有限长度的事务 API。每次 DMA 操作完成后,驱动程序会禁用 Rx FIFO DMA 请求,下一次调用时会再次启用该请求。由于更改 MCR[DMA] 需要冻结模式,最小 IFS 流量中的下一帧可能在 FlexCAN 恢复正常模式之前到达,从而导致 ACK 丢失。 这也解释了为什么移除重复的 DMA 启用/禁用操作可以消除 ACK 错误,但仍然会导致丢帧:与冻结相关的 ACK 间隙被消除,但 eDMA 传输没有持续重新开始。 对于连续突发流量,我们建议保持 Rx FIFO DMA 请求启用,并使用硬件链式乒乓/分散聚集 TCD,以便自动激活下一个缓冲区。这需要连续的 DMA 接收路径,而不是反复重新启动 FLEXCAN_TransferReceiveFifoEDMA()。 此致, 加文 Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages 谢谢你的回复。SDK 是否有计划添加此功能的支持?是采用基于连续DMA的实现方式,还是仅仅采用当前的事务性API实现方式?
View full article
LED用IO拡張機能 現在、カスタム測定機器用のスイッチマトリックスボードで設計しています。 信号のルーティングには、光リレー、具体的にはG3VM-61DR1を使用する予定です。 だから>250をコントロールしなきゃいけないんだ!LED(1.5~1.8V、6~8mA)何らかの方法で。 同時にオンにできるのは25個未満のみです 供給電圧は3.3V以下、温度は40℃前後である必要があります。 オンオフするだけでよく、調光やPWM制御は不要です。 LEDドライバはノイズが出るかもしれないので使いたくありません どのスイッチが同時にオンになるか分からないため、従来のマトリックス配置は使えません ですので、唯一の選択肢は各リレー/LEDごとに独立した出力を持つことです。例えば、IOエクスパンダーはその用途で有望に見えます。 PCAL6524。 チャネル数が多いため、チャネルごとのコンポーネント数をできるだけ減らしたいので、いくつか質問があります。 Agile IOデバイスの7.5mA電流設定を頼りにして、LED直列抵抗を省いてもいいのでしょうか? これが問題ない場合、考えられる副作用は何ですか? デバイスは入力として構成されて開始されるため、LED の制御に使用される場合、高電流が発生する場合があります (例:PCA9535Aデータシート14/15ページ)。各チャネルにプルアップを付けるという古典的な解決策は、多くのチャネルにはあまり良くありません。これはAgile IOデバイスにも影響しますか? LEDには3.3V、エキスパンダーには1.65Vを供給することで、この問題を回避できますか? よろしくお願いします オットー Re: IO Expansion for LEDs PCAL6524は、多数の光リレーやLEDを駆動するのに最適です。ただし、Agile I/Oの駆動能力は、必要な直列電流制限抵抗器を置き換えることを意図したものではありません。I/Oがまだ入力状態にある状態で電源を入れる際の意図しない電流のリスクを軽減するため、3.3V LED電源にVDD(P)を低く設定したり、グローバルLED電源スイッチの実装などが検討されることがあります。それでも、各LEDチャネルごとに個別の電流制限抵抗は常に保持すべきです。
View full article
S32K328 HSE-B:推荐的采用 Mem_43_INFLS 进行 A/B 交换的架构(无需 Vector FOTA) 您好,NXP团队, 我们目前正处于为运行在 S32K328 上的现有应用程序添加 OTA A/B 交换支持的设计和实施阶段。 这是初步实现,我们是在现有软件的基础上扩展 OTA 功能,而不是集成完整的 FOTA 框架。 当前环境 MCU:S32K328(8 MB P-Flash) AUTOSAR 堆栈:矢量 MICROSAR RTD:S32K3_RTD_6_0_0_QLP04_D2508_ASR_REL_4_7_REV_0000_20250822 二进制传输接口:UART 镜像激活服务:HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK HSE A/B 切换可通过 RTD 配置实现 OTA 二进制文件通过 UART 由定制的 OTA CDD 接收。 我们目前的 Vector 配置仅包含用于 NvM/Fee (D-Flash) 的 MemAccM。没有用于对应用程序 P-Flash 进行编程的 MemAccM 配置,我们也没有使用 Vector OTA/FOTA。 因此,我们正在考虑使用 OTA CDD 中的 Mem_43_INFLS 直接擦除和编程非活动应用程序闪存。 我们希望就以下几点获得指导。 1. 推荐方法 在不使用 Vector 的 OTA/FOTA 软件包的情况下,Mem_43_INFLS 是否是 A/B 交换设置中管理 OTA 映像编程的推荐底层驱动程序? 或者,MemAccM 是否应该扩展到涵盖 P-Flash 编程,即使是针对自定义 OTA 实现? 2. 非活动闪存块寻址 启用 HSE A/B 切换后: 非活动应用程序 P-Flash 块是否始终通过内存布局中定义的固定物理地址进行访问? HSE 是否为被动模块提供了任何逻辑映射或抽象? 3. 激活的前提条件 成功执行 HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK 的必要前提条件是什么? 例如: 图像头格式 元数据要求 对齐约束 身份验证/签名要求 闪光状态或属性 4. Flash 控制器并发性 S32K328 上的 C40 闪存控制器是否支持 D-Flash(费用/NvM)和 P-Flash(非活动块)之间的并发操作? 如果不是,那么推荐的同步策略是什么? 应用层调度 RTD司机仲裁 MemAccM 使用情况 5. 推荐架构 以下架构是否符合恩智浦半导体(NXP)的建议? UART ↓ 自定义OTA CDD ↓ Mem_43_INFLS(擦除/写入非活动 P-Flash) ↓ 图像验证 ↓ HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK ↓ 系统重置 ↓ HSE/BAF激活被动阻断 我们特别想了解这种轻量级方法是否合适,是否符合 HSE 要求。 如果您有任何关于带有 HSE A/B 交换的自定义 OTA 的应用笔记、RTD 示例或参考实现,我们将非常感谢您的指导。 感谢您的支持。 此致, 文卡特什·KV #s32k328 Re: S32K328 HSE-B: Recommended Architecture for A/B Swap using Mem_43_INFLS (without Vector FOTA) 嗨@venkatesh-kv 1.自定义 OTA 实现可以直接使用 Mem_43_INFLS 来擦除和编程被动分区。 MemAccM 是否应该扩展是一个架构决策,主要取决于应用程序是否需要通用的闪存访问和仲裁层。 2. 被动应用程序映像通常使用其物理 P-Flash 地址范围进行编程。HSE 没有为被动块提供专用的逻辑寻址抽象。应用程序/引导加载程序负责将新映像写入非活动分区,之后可以使用 HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK 在下次 RESET 时激活该分区。 3. 如果使用安全启动,则应相应地更新签名(取决于安全启动模式和其他设置),以便在下次重置后能够成功验证和执行新应用程序。 旧版本的 HSE 固件需要超级用户权限才能执行服务 HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK。在固件版本 0.2.55.0 及更高版本中,此功能已降级为普通用户权限。 4. 一次只能运行一个闪存操作。闪存访问仲裁的实现由应用程序架构决定。 一般来说,建议避免多个软件组件同时进行闪存操作,并确保闪存访问正确同步,以防止 OTA 编程活动与系统中的任何其他闪存用户发生冲突。 Fee/NvM 和 Mem_43_INFLS 之间没有同步支持。 5. 是的,流程正确。事实上,唯一的要求是,在交换分区之前,被动分区中必须存在有效的应用程序,并且签名(或一般的安全启动配置)应相应地进行更新。 我们有适用于 S32K344 的基本 OTA 演示“SW32K3_OTADEMO_0.8.0_D2203” - 它展示了如何将新应用程序写入被动块,然后请求 AB SWAP(这是 HSE 固件的一个功能)。本演示中使用的是 RTD 1.0.0 版本。 接下来更高级的演示是“S32K396 OTA Demo version 0.4.0”,它展示了如何通过以太网更新固件。这个版本使用的是 RTD 3.0.0。P07。 这两个演示程序都可以在 S32K3 参考软件中找到: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D 点击链接,然后搜索“汽车软件 - S32K3 - OTA 演示”。 这些是我们仅有的版本,它只是参考软件,如果需要,用户需要将其迁移到其他衍生版本或更新的 RTD 软件包。 我们提供以下OTA培训: https://www.nxp.com/design/design-center/training/TIP-CONNECTS2021-AUT428 https://www.nxp.com/design/design-center/training/TIP-NXP-AUT-T3955A 这两点都可以在S32K3页面的“培训”部分找到: https://www.nxp.com/products/S32K3 您还可以查看“S32K3XX HSE 和 OTA 高级培训 [TR744101]”,该培训可从“文档”->“安全文件”下载: https://www.nxp.com/products/S32K3 问候, 卢卡斯
View full article
RT1176 PWM启动失败 我使用PWM+故障+QTimer来实现电机脉冲控制,但PWM3子模块0的PWM_A通道偶尔无法启动,在第一个高电平之后就一直保持高电平,后续脉冲不再出现。检查后发现,PWM的“运行”位没有正确设置。即使后来在程序中添加了重复启动操作,这种异常情况仍然发生。 liu626_0-1782287927569.png Re: RT1176 PWM startup failed 你好@liu626 , 你用的是定制板还是EVK板?如果你使用的是 EVK,你对它进行过任何修改吗? 能否分享一下您使用的PWM3配置? 您是使用示例作为参考吗?如果是,是哪一个? 如果尝试使用仅包含 PWM3 的项目来重现该问题,问题是否仍然存在? 这种情况是否只发生在 PWM3 子模块 0 PWM_A 通道上?其他PWM模块或子模块是否也出现过这种情况? 是否还有其他任务或中断会操作 PWM3 寄存器,从而影响或覆盖运行位? 此致, 巴勃罗 Re: RT1176 PWM startup failed 您好,我使用的是定制电路板。我没有举任何例子。这是在项目正式开发过程中发现的问题。我配置了六个PWM通道用于脉冲控制。只有这个通道出现了问题,其他子模块都没有出现此类问题。我检查后发现,只有这个通道使用了 PWM3 模块。未检测到其他干扰因素。以下是我的配置。 静态 axis_ctrl_t g_axes[AXIS_NUM] = { { 。ID= AXIS_X1,.name= "X1", .pwmBase= PWM1,.pwmModule= kPWM_Module_0,.pwmChannel= kPWM_PwmA, .tmrBase= TMR3,.lowCh= kQTMR_Channel_2,.highCh= kQTMR_Channel_3, .tmrInputsrc=kQTMR_ClockCounter2InputPin,.cascadePcs= 6U, 故障编号= 0U,.hwExactSupported= true,.outTrigMask= kPWM_ValueRegisterMask_3, }, { 。ID= AXIS_X2,.name= "X2", .pwmBase= PWM2,.pwmModule= kPWM_Module_0,.pwmChannel= kPWM_PwmA, .tmrBase= TMR2,.lowCh= kQTMR_Channel_0, .highCh= kQTMR_Channel_1, .tmrInputsrc=kQTMR_ClockCounter0InputPin,.cascadePcs= 4U, 故障编号= 0U,.hwExactSupported= true,.outTrigMask= kPWM_ValueRegisterMask_3, }, { 。ID= AXIS_Y,.name= "Y", .pwmBase= PWM3,.pwmModule= kPWM_Module_0,.pwmChannel= kPWM_PwmA, .tmrBase= TMR3,.lowCh= kQTMR_Channel_0, .highCh= kQTMR_Channel_1, .tmrInputsrc=kQTMR_ClockCounter0InputPin,.cascadePcs= 4U, 故障编号= 0U,.hwExactSupported= true,.outTrigMask= kPWM_ValueRegisterMask_3, }, { 。ID= AXIS_Z,.name= "Z", .pwmBase= PWM4,.pwmModule= kPWM_Module_0,.pwmChannel= kPWM_PwmA, .tmrBase= TMR1,.lowCh= kQTMR_Channel_0, .highCh= kQTMR_Channel_1, .tmrInputsrc=kQTMR_ClockCounter0InputPin,.cascadePcs= 4U, 故障编号= 0U,.hwExactSupported= true,.outTrigMask= kPWM_ValueRegisterMask_3, }, { 。ID= AXIS_EX1,.name= "EX1", .pwmBase= PWM1,.pwmModule= kPWM_Module_1,.pwmChannel= kPWM_PwmA, .tmrBase= TMR1,.lowCh= kQTMR_Channel_2,.highCh= kQTMR_Channel_3, .tmrInputsrc=kQTMR_ClockCounter2InputPin,.cascadePcs= 6U, 故障编号= 1U,.hwExactSupported= true,.outTrigMask= kPWM_ValueRegisterMask_3, }, { 。ID= AXIS_EX2,.name= "EX2", .pwmBase= PWM2,.pwmModule= kPWM_Module_1,.pwmChannel= kPWM_PwmA, .tmrBase= TMR2,.lowCh= kQTMR_Channel_2,.highCh= kQTMR_Channel_3, .tmrInputsrc=kQTMR_ClockCounter2InputPin,.cascadePcs= 6U, 故障编号= 1U,.hwExactSupported= true,.outTrigMask= kPWM_ValueRegisterMask_3, }, };static void APP_Init_PWM_QTMR(void) { pwm_config_t pwmConfig; pwm_fault_param_t faultConfig; qtmr_config_t qtmrConfig; PWM_GetDefaultConfig(&pwmConfig); pwmConfig.pairOperation= kPWM_Independent; pwmConfig.reloadLogic = kPWM_ReloadImmediate; PWM_FaultDefaultConfig(&faultConfig); faultConfig.faultLevel = true; faultConfig.enableCombinationPath= false; faultConfig.faultClearingMode= kPWM_手动安全; faultConfig.recoverMode = kPWM_NoRecovery; QTMR_GetDefaultConfig(&qtmrConfig); CLOCK_EnableClock(kCLOCK_Qtimer1); CLOCK_EnableClock(kCLOCK_Qtimer2); CLOCK_EnableClock(kCLOCK_Qtimer3); PWM_StopTimer(PWM1, 0x0FU); PWM_StopTimer(PWM2, 0x0FU); PWM_StopTimer(PWM3, 0x0FU); PWM_StopTimer(PWM4, 0x0FU); pwm_fault_input_filter_param_t faultFilter; 故障过滤器.故障过滤器周期= 255U; faultFilter.faultFilterCount= 7U; faultFilter.faultGlitchStretch= false; /* 记录每个PWM实例上已配置的故障通道,避免重复设置 */ uint16_t pwm1FaultDone = 0U, pwm2FaultDone = 0U, pwm3FaultDone = 0U, pwm4FaultDone = 0U; for (uint8_t i = 0U; i < AXIS_NUM; i++) { axis_ctrl_t *ax = &g_axes[i]; PWM_Init(ax->pwmBase, ax->pwmModule, &pwmConfig); PWM_SetupFaults(ax->pwmBase, (pwm_fault_input_t)ax->faultNum, &faultConfig); /* 故障提示(每个 PWM 实例的每个故障通道只设置一次) */ { uint16_t *faultDone; 如果 (ax->pwmBase == PWM1) faultDone = &pwm1FaultDone; 否则如果 (ax->pwmBase == PWM2) faultDone = &pwm2FaultDone; 否则如果 (ax->pwmBase == PWM3) faultDone = &pwm3FaultDone; 否则 faultDone = &pwm4FaultDone; uint16_t faultBit = (uint16_t)(1U << ax->faultNum); 如果 ((*faultDone & faultBit) == 0U) { PWM_SetupFaultInputFilterExt(ax->pwmBase, (pwm_fault_channels_t)ax->faultNum, &faultFilter); *faultDone |= faultBit; } } /* 故障时输出低电平 */ ax->pwmBase->SM[ax->pwmModule].OCTRL &= ~(PWM_OCTRL_PWMAFS_MASK | PWM_OCTRL_PWMBFS_MASK); APP_PWM_Unmap_Selected_Fault(ax); APP_PWM_ClearFault_Safe(ax); ax->pwmBase->SM[ax->pwmModule].INIT = 0U; ax->pwmBase->SM[ax->pwmModule].VAL0 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL1 = 1U; ax->pwmBase->SM[ax->pwmModule].VAL2 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL3 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL4 = 0U; ax->pwmBase->SM[ax->pwmModule].VAL5 = 0U; ax->pwmBase->SM[ax->pwmModule].TCTRL = PWM_TCTRL_OUT_TRIG_EN(ax->outTrigMask); APP_PWM_Disable_Output(ax); 如果 (ax->hwExactSupported) { qtmrConfig.primarySource= ax->tmrInputSrc; QTMR_Init(ax->tmrBase, ax->lowCh, &qtmrConfig); QTMR_Init(ax->tmrBase, ax->highCh, &qtmrConfig); ax->tmrBase->CHANNEL[ax->lowCh].CTRL = TMR_CTRL_CM(kQTMR_PriSrcRiseEdge) | TMR_CTRL_PCS(ax->tmrInputSrc); ax->tmrBase->CHANNEL[ax->highCh].CTRL = TMR_CTRL_CM(kQTMR_CascadeCount) | TMR_CTRL_PCS(ax->cascadePcs); APP_QTMR_Disable_Low_OFLAG_Output(ax); QTMR_DisableInterrupts(ax->tmrBase, ax->lowCh, 0xFFU); QTMR_DisableInterrupts(ax->tmrBase, ax->highCh, 0xFFU); QTMR_ClearStatusFlags(ax->tmrBase, ax->lowCh, 0xFFU); QTMR_ClearStatusFlags(ax->tmrBase, ax->highCh, 0xFFU); } ax->phase = kAxisIdle; ax->armed = false; ax->running = false; ax->done = true; #if HARD_PWM_STATE_GUARD_ENABLE APP_StateGuard_Reset(ax); #endif } /* 使能 QTMR 中断 */ NVIC_SetPriority(TMR1_IRQn, 2U); NVIC_SetPriority(TMR2_IRQn, 2U); NVIC_SetPriority(TMR3_IRQn, 2U); 启用IRQ(TMR1_IRQn); 启用IRQ(TMR2_IRQn); 启用IRQ(TMR3_IRQn); }static bool APP_PWM_Config_Pulse(axis_ctrl_t *axis, uint32_t highCnt400M, uint32_t lowCnt400M) { pwm_clock_prescale_t 预分频; uint16_t periodTicks; uint32_t totalCnt400M = highCnt400M + lowCnt400M; 如果 ((axis == NULL) || (totalCnt400M == 0U)) 返回 false; 如果 (!APP_PWM_SelectPrescaler_FromPeriodCnt400M(totalCnt400M, &prescale, &periodTicks)) 返回 false; uint32_t highTicks32 = (uint32_t)(((uint64_t)periodTicks * (uint64_t)highCnt400M + ((uint64_t)totalCnt400M / 2ULL)) / (uint64_t)totalCnt400M); 如果 (highTicks32 == 0U) highTicks32 = 1U; 如果 (highTicks32 >= periodTicks) highTicks32 = (uint32_t)periodTicks - 1U; uint32_t riseTicks32 = 0U; uint32_t fallTicks32 = highTicks32; #if HARD_PWM_LOW_START_PHASE_ENABLE uint32_t lowTicks32 = (uint32_t)periodTicks - highTicks32; 如果 (lowTicks32 >= (2U * HARD_PWM_LOW_START_PHASE_MIN_TICKS)) { uint32_t desiredLeadCnt400M = highCnt400M; uint32_t minLeadCnt400M = (uint32_t)HARD_PWM_LOW_START_PHASE_MIN_US * 400U; 如果 (desiredLeadCnt400M < minLeadCnt400M) desiredLeadCnt400M = minLeadCnt400M; uint32_t desiredLeadTicks32 = (uint32_t)(((uint64_t)periodTicks * (uint64_t)desiredLeadCnt400M + ((uint64_t)totalCnt400M / 2ULL)) / (uint64_t)totalCnt400M); 如果 (desiredLeadTicks32 < HARD_PWM_LOW_START_PHASE_MIN_TICKS) desiredLeadTicks32 = HARD_PWM_LOW_START_PHASE_MIN_TICKS; uint32_t maxRiseByHalfTicks32 = lowTicks32 / 2U; uint32_t postGuardTicks32 = (uint32_t)(((uint64_t)periodTicks * (uint64_t)(HARD_PWM_VAL3_POST_LOW_GUARD_US * 400U) + ((uint64_t)totalCnt400M / 2ULL)) / (uint64_t)totalCnt400M); 如果 (postGuardTicks32 < HARD_PWM_VAL3_POST_LOW_GUARD_MIN_TICKS) postGuardTicks32 = HARD_PWM_VAL3_POST_LOW_GUARD_MIN_TICKS; uint32_t maxRiseByPostGuardTicks32 = (lowTicks32 > postGuardTicks32) ? (lowTicks32 - postGuardTicks32):0U; uint32_t selectedRiseTicks32; 如果 (maxRiseByHalfTicks32 >= desiredLeadTicks32) { selectedRiseTicks32 = desiredLeadTicks32; 如果 (selectedRiseTicks32 > maxRiseByHalfTicks32) selectedRiseTicks32 = maxRiseByHalfTicks32; } 否则如果(maxRiseByPostGuardTicks32 >= desiredLeadTicks32) { selectedRiseTicks32 = desiredLeadTicks32; 如果 (selectedRiseTicks32 > maxRiseByPostGuardTicks32) selectedRiseTicks32 = maxRiseByPostGuardTicks32; } 别的 { selectedRiseTicks32 = maxRiseByPostGuardTicks32; } 如果 (selectedRiseTicks32 >= HARD_PWM_LOW_START_PHASE_MIN_TICKS) { riseTicks32 = selectedRiseTicks32; fallTicks32 = riseTicks32 + highTicks32; } } #endif 如果 (fallTicks32 >= (uint32_t)periodTicks) fallTicks32 = (uint32_t)periodTicks - 1U; uint16_t riseTicks = (uint16_t)riseTicks32; uint16_t fallTicks = (uint16_t)fallTicks32; PWM_SetPwmLdok(axis->pwmBase, APP_PwmModuleMask(axis), false); uint16_t ctrl = axis->pwmBase->SM[axis->pwmModule].CTRL; ctrl &= (uint16_t)(~PWM_CTRL_PRSC_MASK); ctrl |= PWM_CTRL_PRSC(预分频); axis->pwmBase->SM[axis->pwmModule].CTRL = ctrl; axis->pwmBase->SM[axis->pwmModule].INIT = 0U; axis->pwmBase->SM[axis->pwmModule].VAL0 = 0U; axis->pwmBase->SM[axis->pwmModule].VAL1 = (uint16_t)(periodTicks - 1U); 如果 (axis->pwmChannel == kPWM_PwmA) { axis->pwmBase->SM[axis->pwmModule].VAL2 = riseTicks; axis->pwmBase->SM[axis->pwmModule].VAL3 = fallTicks; } 否则如果 (axis->pwmChannel == kPWM_PwmB) { axis->pwmBase->SM[axis->pwmModule]。VAL4 = riseTicks; axis->pwmBase->SM[axis->pwmModule].VAL5 = fallTicks; } axis->pwmBase->SM[axis->pwmModule].TCTRL = PWM_TCTRL_OUT_TRIG_EN(axis->outTrigMask); PWM_SetPwmLdok(axis->pwmBase, APP_PwmModuleMask(axis), true); PWM_SetPwmLdok(axis->pwmBase, APP_PwmModuleMask(axis), true); axis->pwmConfigValid = true; axis->cachedHighCnt400M = highCnt400M; axis->cachedLowCnt400M = lowCnt400M; 返回 true; } Re: RT1176 PWM startup failed 你好@liu626 , 您能否帮我找出配置问题,并测试一下仅初始化 PWM3 时问题是否仍然存在? 在查看了您分享的配置后,为了尝试重现该行为,我有以下问题: axis_ctrl_t 的定义是什么? 您的应用程序中是否启用了 HARD_PWM_LOW_START_PHASE_ENABLE 和 HARD_PWM_STATE_GUARD_ENABLE? 以下APP功能是做什么用的? APP_PWM_Unmap_Selected_Fault APP_PWM_ClearFault_Safe APP_PWM_禁用输出 APP_QTMR_Disable_Low_OFLAG_Output APP_StateGuard_Reset APP_PWM_SelectPrescaler_FromPeriodCnt400M APP_PwmModuleMask 此致, 巴勃罗 Re: RT1176 PWM startup failed 感谢你的回复。我使用的 GPIO 引脚是 rt1176 的 GPIO_EMC_B1_29。“axis_ctrl_t”是与电机轴相关的定义。 * PWM 输出脉冲 -> 触发 XBAR 信号 -> 脉冲下降沿驱动 QTMR 的外部时钟输入 -> * QTMR 32 位级联计数器递减 1 -> 当计数器达到 0 时,触发 QTMR 比较中断 -> 中断内部关闭 PWM * 同时,QTMR 触发硬件故障,直接拉低 PWM 的物理输出引脚。。ID= AXIS_Y, 。姓名= "Y", /* 用于串口日志记录或断点调试,以识别 Y 轴 */ /* ================= PWM 输出资源分配 ================= */ .pwmBase= PWM3, /* Y轴使用FlexPWM3模块 */ .pwm模块= kPWM_Module_0, /* 使用 PWM3 的子模块 0(每个 PWM 有 4 个子模块,编号从 0 到 3) */ .pwm通道= kPWM_PwmA, /* 使用子模块 0 的 A 相输出引脚,对应于物理引脚 GPIO_EMC_B1_29 */ /* ================= 32 位 QTMR 级联计数资源分配 ================= */ .tmrBase= TMR3, /* Y轴使用QTMR3外设(对应于IRQ中断号TMR3_IRQn) */ 低= kQTMR_Channel_0, /* 16 位低计数器:使用 TMR3 的通道 0 */ .highCh= kQTMR_Channel_1,/* 16 位高位计数器:使用 TMR3 的通道 1 */ /* 👉 .lowCh 和 .highCh它们成对出现,在硬件层面上,它们会自动组合成一个 32 位计数器。 /* ================= 硬件级联时钟源配置(核心关键) ================= */ .tmrInputsrc=kQTMR_ClockCounter0InputPin, /* 通道 0 的时钟源:设置为“外部引脚输入 0”。 在 XBAR 配置中,PWM3 脉冲的下降沿通过 XBAR 连接到 TMR3 通道 0 的输入引脚。 因此,每次 PWM 输出脉冲时,通道 0(16 位)将执行一次减量操作。*/ .cascadePcs = 4U, /* 高 16 位通道(通道 1)的时钟源 (PCS) 配置。 在 i.MX RT 的 QTMR 寄存器中,PCS 值对应如下: 0-3 = 外部引脚输入; 4 = 通道 0 的溢出/终止事件; 5 = 通道 1 的溢出/终止事件; 6 = 通道 2 的溢出/终止事件; 7 = 通道 3 的溢出/终止事件。 这里配置为 4U,意思是:让“TMR3 的通道 1”监测“TMR3 的通道 0 的溢出事件”。 已启用 HARD_PWM_LOW_START_PHASE_ENABLE 和 HARD_PWM_STATE_GUARD_ENABLE。APP_PWM_Unmap_Selected_Fault 功能:移除与当前轴对应的故障引脚映射。调用底层 PWM_SetupFaultDisableMap 函数来禁用故障。目的是为了:在不需要硬件故障的情况下,防止意外的外部干扰导致 PWM 关闭,从而方便底层调试过程。 APP_PWM_ClearFault(原始代码函数) 功能:清除 PWM 模块的故障状态标志(axis->pwmBase->FSTS)。触发硬件故障后,必须先清除此标志,然后才能允许 PWM 重新启动。 APP_PWM_禁用输出 功能:立即停止 PWM 定时器,强制引脚输出低电平(PWM_SetPwmForceOutputToZero),并启用输出。它的目的是确保在电机启动之前,引脚不会因为浮空或处于默认状态而输出高电平,这可能会导致电机运动不规则。 APP_QTMR_Disable_Low_OFLAG_Output 功能:禁用 QTMR 的 OFLAG(状态标志)输出,并强制 OFLAG 处于低电平。它与 XBAR 硬件配合使用,其作用是切断 QTMR 输出到 PWM 故障引脚的路径,防止在启动前意外触发故障。 APP_StateGuard_Reset 功能:清除国家卫队(看门狗)的计数器和旗帜。如果启用 HARD_PWM_STATE_GUARD_ENABLE 时系统遇到长时间无脉冲变化或死锁,则此功能用于在停止或重新启动系统之前重置这些保护变量。 APP_PWM_SelectPrescaler_FromPeriodCnt400M 功能:这是一个非常核心的底层频率计算函数。它接收高电平 + 低电平的总 400MHz 计数值,并计算应设置多少个预分频器 (PRSC) 和 PWM 周期 (PERIOD) 才能放入 16 位 PWM 寄存器中。请注意:如果计算出的周期超过 65535 且除法系数超出范围,则此函数将返回 false,导致电机无法启动。 APP_PwmModuleMask 功能:将 PWM 子模块的索引号(例如,值为 0 的 kPWM_Module_0)转换为左移 N 位的位掩码。NXP 的许多 PWM 寄存器(例如 OUTEN、MCTRL)都是逐位控制的。该函数负责生成正确的二进制掩码。 Re: RT1176 PWM startup failed 我找到了原因。这是因为 cm4 内核中 PIT 中断的内部负载过重,影响了 cm7 内核的 PWM 操作。降低 PIT 中断的负载后,PWM 启动失败的问题就消失了。
View full article
PCF8563TS/5,118用のコンデンサを探すお手伝いをします 私はPCF8563TS/5118 ICを使用しており、OSCIピンの外部コンデンサを正しく接続しようとしています。 私は50k ESR、12.5pF、32.568KHzの結晶、可能な限り短いトレース、データシートのアプリケーション図と同じ回路図を使っています。 デバイスを理解するために、データシートとUM10301の両方を参照して計算を試みました。外部コンデンサの値を明確に計算する方法を見つけるのが難しかったです。なぜなら、データシートには同じトピックの別々のページ、OSCIとOSCOで並列と直列が記載されているからです。 外部のOSCIピンとOSCOピンに並列に25pFの内部コンデンサが接続されているのがわかります。データシートの表30では、CLは並列接続の場合に計算されると記載されていますが、代わりに直列接続の場合の計算方法を示す注記があります。 デバイスを動かす外部コンデンサが見つかりません。I2Cからの応答がありません。25pF、22.5pF、20pF、25pF、10pF、8.2pF、6pFを試しました。0603 C0G/NP0 キャップすべて。 別の基板では、コンデンサを全く取り付けないことで動作させることができました。計算してみると、それは全く意味をなさない。 これらの入力値(12.5pF、50k ESR水晶発振器)の計算方法の例を教えていただけないでしょうか。計算しても、値を総当たりで試しても、うまく動作させることができませんでした。 Re: Help finding capacitor for PCF8563TS/5,118 はい、それは内蔵コンデンサの値で、私自身の投稿でも触れました。私はそのファイルを読みました。 あなたが伝えたいことを実際に書いてくれた方が、はるかに役に立つでしょう。時間を割いていただきありがとうございました。 Re: Help finding capacitor for PCF8563TS/5,118 db16122_0-1784461035005.png UM10301 PCF85x3、PCF85x63、PCA8565、PCF2123、PCA21125のユーザーマニュアル Re: Help finding capacitor for PCF8563TS/5,118 親愛なるデイビッド、 db16122さんが正しく表3を案内してくれました。UM10301で。目標負荷静電容量が12.5pFなら、OSCIピンに25pF中間値のトリムコンデンサを接続する必要があります。 JozefKozon_0-1784524368704.png JozefKozon_1-1784524409356.png この25pF値は表30の下記式から計算できます。PCF8563のデータシートに記載されています。 JozefKozon_2-1784524493868.png ここでCLは目標負荷静電容量、あなたの場合は12.5pFです。 コスコは既知の内部静電容量、25pFです。 JozefKozon_3-1784524560452.png この式から、Ctrimは次のように導くことができます: CL = Ctrim * Cosco / (Ctrim + Cosco) CL*Ctrim+CL*Cosco=Ctrim*Cosco CL*Cosco=Ctrim*Cosco-CL*Ctrim CL*Cosco=Ctrim*(Cosco-CL) CL*Cosco/(Cosco-CL)=Ctrim Ctrim = CL * Cosco / (Cosco - CL) = 12.5 * 25 / (25 - 12.5) = 312.5 / 12.5 Ctrim=25pF 可変トリムコンデンサが必要なのは、内部のCoscoコンデンサに余裕があるためです。Coscoは15pFから35pFの範囲で変動する場合があります。 JozefKozon_4-1784525019076.png 敬具、 ヨゼフ
View full article
can we use provisioned cert or key for setting up in the https connection or tls connection in i.mx9 Can the provisioned certificate and private key on the i.MX93 be used directly to establish HTTPS/TLS connections? If yes, what is the recommended method for accessing and utilizing these credentials for client/server authentication and mTLS implementations? once provisioning is complete and the secure object blobs are present in /etc/ele/, what is the recommended workflow for using those provisioned credentials in a real HTTPS/TLS connection? Re: can we use provisioned cert or key for setting up in the https connection or tls connection in i Hi ,@Manuel_Salas  Thanks for your reply. Following up on the mbedTLS/opaque-key guidance — that's resolved on our side for the private key. Remaining question is specifically about the certificate, provisioned via EL2GO and stored in /etc/ele/ alongside the private key . Since a certificate is public data, we need to extract it as plain DER to hand to mbedtls_x509_crt_parse_der() for the TLS handshake — unlike the key, it doesn't need to stay opaque. What is the supported SMW/PSA call to retrieve the plaintext DER bytes for a provisioned certificate object? Specifically: is it exposed via psa_ps_get() / psa_its_get() (PSA Protected Storage / Internal Trusted Storage) using the object ID as the UID, or through a different SMW API? We see protected_storage.h and internal_trusted_storage.h in the installed SMW headers but want to confirm this is the intended path for certificate objects before building against it. Re: can we use provisioned cert or key for setting up in the https connection or tls connection in i Hello @NEXUSNERD  Hope you are doing very well. On the i.MX93, the provisioning flow is designed so that the private key remains protected by the ELE. So, the blobs stored in /etc/ele/ are secure object representations that allow ELE to reload or reference the provisioned key material, and they are not intended to be treated as ordinary TLS key files. You can take a look to the imx-secure-enclave (Mbed-TLS). Best regards, Salas.
View full article
オンラインプロビジョニング ボードのオンラインプロビジョニングは無事完了しました。あとは、edge2lockのプロビジョニング後に作成された証明書やキーを抽出するか、場合によっては読み取る必要があるのですが、それは可能でしょうか? Frdm i.mx93 を使用しています Re: Online Provisioning こんにちは、 pkcs11-toolを使っても構いません。こちらのドキュメントをご覧ください。 https://github.com/nxp-imx/imx-smw/blob/release/version_5.x/Documentations/user_guide/pkcs11/pkcs11_tool_user_guide.md また、SMWのユーザーマニュアルもご覧になることをお勧めします: https://github.com/nxp-imx/imx-smw/blob/release/version_5.x/Documentations/user_manual/SMW_UserManual_UM12513.pdf よろしくお願いいたします。 アルド。 Re: Online Provisioning こんにちは、アルドさん。 お返事ありがとうございます。 FRDM i.MX93でオンラインプロビジョニングに成功した後、SMW PKCS#11プロバイダーでpkcs11-toolを使おうとしましたが、プロビジョニング済みの証明書やキーが見えたり読み取ったりできません。 もう少し詳しく教えていただけますか: プロビジョニングされた証明書と秘密鍵はPKCS#11インターフェースを通じてアクセス可能でしょうか? そうでない場合、それらはELEに安全に保存され、エクスポートされることなくPSA Crypto/SMW APIを通じてのみ使用されることを意図しているのでしょうか? 私の目標は、プロビジョニングされた認証情報を使用して相互TLS接続を確立することです。 ありがとう。
View full article