Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Getting Started with USB Audio on i.MX boards Introduction.  USB is a highly efficient interface for transporting audio and voice data, offering sufficient bandwidth for applications from voice telephony to high-quality audio playback and recording. To ensure compatibility between devices, the USB Audio Class specification defines standardized mechanisms for audio transport and control, allowing audio peripherals to operate with generic drivers and minimizing platform software requirements.    For i.MX processors, this article describes how an i.MX board can function as a standard USB audio device, enabling audio data to be streamed through the USB port to a host computer. This capability is important for applications such as USB microphones, speakers, audio gateways, and voice-processing systems.   As a result, developers can efficiently implement real time audio transfer between i.MX boards and host systems using standard USB audio drivers without requiring additional proprietary interfaces.   Required equipment. i.MX95 FRDM board (this is the selected board for this post, it works for others). Debug USB-C cable. Data USB-C cable. USB-C power supply. Ethernet cable. Speakers or headphones with 3.5mm input plug. Personal computer. To start, we need to flash our Linux BSP into the board. You can build it by yourself or use the pre-built BSP to facilitate the process. This post was tested with Linux 6.18.20_2.0.0, if you have issues to flash the board, please refer to this article: Flashing Linux BSP using UUU This is how my hardware setup looks: Media.jpg USB gadget setup. The following script configures the board to work as an USB audio gadget in Linux. This setup allows the board to be detected as a standard audio device, enabling audio streaming over the USB connection without requiring a custom USB protocol on the host side. The script creates the USB gadget configuration, assigns the required USB descriptors, with predefined audio parameters such as 16 kHz sample rate, 32-bit sample size, and single-channel capture/playback support. This example is useful for applications such as voice capture, audio processing, USB microphones, or embedded audio demos. #!/bin/sh # USB gadget ConfigFS paths CONFIGFS=/sys/kernel/config/usb_gadget GADGET=$CONFIGFS/g1 CONFIG=$GADGET/configs/c.1 FUNCTIONS=$GADGET/functions # USB device descriptors and audio configuration VID="0x1fc9" PID="0x0330" SERIALNUMBER="0123456789" MANUFACTURER="NXP Semiconductors" PRODUCT="i.MX USB Audio Gadget" SAMPLE_RATE=16000 SAMPLE_SIZE=4 # 32-bit audio samples echo "Setting up USB gadget with the following parameters:" echo " Vendor ID: $VID" echo " Product ID: $PID" echo " Serial Number: $SERIALNUMBER" echo " Manufacturer: $MANUFACTURER" echo " Product: $PRODUCT" echo " Sample Rate: $SAMPLE_RATE Hz" function add_uac2_function() { # Create a USB Audio Class function instance mkdir $FUNCTIONS/uac2.$1 echo "$PRODUCT $1" > $FUNCTIONS/uac2.$1/function_name # c_* parameters configure USB Capture # p_* parameters configure USB Playback # Audio sample rate configuration echo $SAMPLE_RATE > $FUNCTIONS/uac2.$1/c_srate echo $SAMPLE_RATE > $FUNCTIONS/uac2.$1/p_srate # Audio sample size in bytes echo $SAMPLE_SIZE > $FUNCTIONS/uac2.$1/c_ssize echo $SAMPLE_SIZE > $FUNCTIONS/uac2.$1/p_ssize echo $2 > $FUNCTIONS/uac2.$1/c_chmask echo $3 > $FUNCTIONS/uac2.$1/p_chmask # Enable mute and volume controls visible to the USB host echo 0x1 > $FUNCTIONS/uac2.$1/c_mute_present echo 0x1 > $FUNCTIONS/uac2.$1/c_volume_present echo 0x1 > $FUNCTIONS/uac2.$1/p_mute_present echo 0x1 > $FUNCTIONS/uac2.$1/p_volume_present # Add the UAC2 function to the active USB configuration ln -s $FUNCTIONS/uac2.$1 $CONFIG } function create_config() { # Create the USB gadget device mkdir $GADGET # Set USB Vendor ID and Product ID echo $VID > $GADGET/idVendor echo $PID > $GADGET/idProduct # Standard USB string descriptors mkdir $GADGET/strings/0x409 echo $SERIALNUMBER > $GADGET/strings/0x409/serialnumber echo $MANUFACTURER > $GADGET/strings/0x409/manufacturer echo $PRODUCT > $GADGET/strings/0x409/product # Create USB configuration description mkdir -p $CONFIG/strings/0x409 echo $1 > $CONFIG/strings/0x409/configuration } # Create a UAC2 audio gadget with mono capture and mono playback create_config "UAC2" add_uac2_function "Active" 0x1 0x1 echo "Done" Clean USB gadget. If you need to free up the USB port, it is necessary to run the following script. #!/bin/sh # USB gadget ConfigFS paths CONFIGFS=/sys/kernel/config/usb_gadget GADGET=$CONFIGFS/g1 CONFIG=$GADGET/configs/c.1 FUNCTIONS=$GADGET/functions # Verify that the gadget exists before attempting cleanup if [ ! -d "$GADGET" ]; then echo "Gadget does not exist" exit 0 fi # Disconnects the gadget from the host before removal. echo "" > $GADGET/UDC 2>/dev/null # Remove UAC2 function links from the configuration rm -f $CONFIG/uac2.* 2>/dev/null # Remove UAC2 function instances rmdir $FUNCTIONS/uac2.* 2>/dev/null # Remove configuration strings and configuration directory rmdir $CONFIG/strings/0x409 2>/dev/null rmdir $CONFIG/strings 2>/dev/null rmdir $CONFIG 2>/dev/null # Remove gadget string descriptors rmdir $GADGET/strings/0x409 2>/dev/null rmdir $GADGET/strings 2>/dev/null # Remove the gadget itself rmdir $GADGET 2>/dev/null echo "Cleanup completed" Testing. Both scripts can be created into the board using nano or a similar text editor through the console but is easier to do it in your host machine and send it for example using SCP. After you created both scripts you can send them with the next command: scp @ : Once you connected the Ethernet cable in any of the available RJ45 connectors in your board, you can get the IP address with the next command: ifconfig Now, in your host machine, you can go to the path where are your USB scripts and send them: scp cleanup_usb_gadget.sh root@ :~/ scp setup_usb_gadget.sh root@ :~/ After transfer the scripts to the board, you need to change file permissions to execute the scripts with chmod and run USB gadget setup script to configure the board as a USB audio interface. chmod u+x *_usb_gadget.sh JorgeCas_0-1782324986101.png Once this script have been executed you can see the USB port in ALSA as a sink/source device: JorgeCas_2-1782325559529.png Then, you need to connect the USB port to a host computer and will be recognized as an USB interface: JorgeCas_4-1782325847685.png You can validate that the device is working according to the configuration defined in setup script: Screenshot 2026-07-29 104314.png I will use Audacity to test audio transfer from on board microphones, in Edit -> Preferences -> Audio settings select i.MX Active as recording device: JorgeCas_5-1782326183462.png Note: Use the same sample rate of setup_usb_gadget.sh configuration to avoid errors with the DAW. In the board, I will start the recording by running the following GStreamer pipeline, which captures audio from the onboard microphones and streams it through the USB port: gst-launch-1.0 alsasrc device=hw:micfilaudio,0 ! queue ! audioconvert ! audio/x-raw,channels=1,rate=16000,format=F32LE ! audioconvert ! alsasink device=hw:UAC2Gadget,0 After this configuration, add an audio track and now, is possible to get the audio and record it directly in the DAW: JorgeCas_0-1782327009216.png If you want to play audio from host PC trough the i.MX board, you need to run the next command before start the audio playback in host. Make sure that the audio card selected is not busy: gst-launch-1.0 -v alsasrc device=hw:UAC2Gadget,0 ! audio/x-raw,format=S32LE,rate=16000,channels=1 ! audioconvert ! audioresample ! audio/x-raw,format=S16LE,rate=48000,channels=2 ! audioconvert ! alsasink device=plughw:mqsaudio,0 In this case, I selected the MQS output in 3.5mm output jack, you can connect the speakers or headphones with this connector. After run the clean USB gadget script, the USB audio device is not longer detected in host PC and the board output is the next: JorgeCas_3-1782325608663.png References. USB Implementers Forum. (1998, March 18). Universal Serial Bus device class definition for audio devices (Release 1.0) [PDF]. USB-IF. https://www.usb.org/sites/default/files/audio10.pdf   
查看全文
i.MX93 AHAB セキュアブート、RSA-PSS署名、およびHSMモード こんにちは、 i.MX93-evkプラットフォームでのRSA-PSS署名認証に関してCSTで遭遇した問題を報告したいと思います。これはバグだと思います。以下に、私がこの発見に至るまでの手順を説明します。 現在、i.MX93-EVKプラットフォーム上でセキュアブート手順を実装しており、標準で文書化されたCST v4.0.1を使って動作させることに成功しました。 次に、CST の外で OpenSSL を直接使用して、さまざまなバイナリに署名したいと考えました (注: これは PKCS#11 の設定ではなく、OpenSSL CLI/API で独自の RSA キーを使用しているだけです)。私が実現したかったことをまさに説明している以下の手順書を見つけました: AHABデバイスでのコード署名のためのHSMモードの使用.pdf これは、コード署名ツール(CST)が提供するahab_pki_treeツールを使用して生成されたキーと、以下のパラメータでうまく機能します。 既存のCAキーを使用する:n キータイプ: rsa-pss 鍵長:4096ビット ダイジェストアルゴリズム: sha384 しかし、私がCST以外でバイナリに署名したい理由は、すでに他の様々な成果物の署名に使用しているRSA鍵を持っているからです。このキーを使用してさまざまなバイナリファイルに署名し、リンク先のプロセスで説明されているように署名済みハッシュを再統合しようとすると、次のエラーが発生します(CST v4.0.1)。 [ERROR] CST: The signature file spl_data.sig is not valid 全てが正しいことを再確認した後、OpenSSLを使用して署名を検証するテストも以下のように行いました。 $ openssl dgst -sha384 -verify pubkey.pem -signature spl_data.sig -sigopt rsa_padding_mode:pss -sigopt rsa_pss_saltlen:digest spl_data.bin Verified OK 予想と実際: OpenSSLが署名が有効なPSS署名であることを確認したので、CSTも再統合時にそれを受け入れると予想していました。しかし、CSTはそれを無効として拒否します。 CSTのソースコードを詳しく調べ始めたところ、OpenSSLによる検証は成功しているにもかかわらず、署名が無効であると誤って報告されていた理由が分かりました。 CSTが署名を確認する際、以下の処理を行います。 OpenSSL API呼び出しを使用して、公開鍵から「公開鍵アルゴリズム」フィールドを取得します。 このフィールドに基づいて、別の OpenSSL API 呼び出しを使用して、基本的に「指定された署名ファイルは、使用されている公開鍵アルゴリズムに対応していますか?」と問い合わせます。 NXPのドキュメントで「RSA-PSS」キーと呼ばれているものを生成・使用する場合、「公開鍵アルゴリズム」フィールドは rsassaPssと等しく、上記のチェックは正しく動作します。 しかし、汎用RSA鍵を使用する場合、「公開鍵アルゴリズム」フィールドはrsaEncryptionとなり、CSTはこれをPKCS#1 v1.5と誤って解釈しますが、実際にはPKCS#1 v2.1(PSS)形式で署名することも可能です。 私は、自分の署名がPSS署名であることをCSTのソースコードにハードコーディングすることで、この誤った仮定を検証しました。その結果、CSTによって署名が正常に検証され、最終バイナリに再挿入されることができました。その後、閉じた状態のデバイスでは期待どおりに動作しました。 必要であれば、特に関連するOpenSSLの各種関数呼び出しに関して、さらに詳しい情報を提供いたします。 これがCSTの既知の制限なのか、それとも汎用RSAキーで署名を生成・使用している点に何か見落としているのか確認してもらえますか? 余談ですが、HSDKも試しました。これはNXPがAHABベースのプラットフォーム向けに推奨している新しいツールのようですが、署名したいバイナリをエクスポートして手動で署名し、CSTの手順に似た方法で再挿入する方法が見つかりませんでした。これは実現可能かどうかご存知ですか? よろしくお願いいたします。 Re: i.MX93 AHAB Secure boot, RSA-PSS signature and HSM mode こんにちは、 実際、あなたが使っている文書は正しいです。これは、まだCSTを利用しているお客様に推奨されるアプローチです。AHABおよび特に新しいi.MX9ファミリーのお客様には、セキュリティのイネーブルメントのためにSPSDKへの移行を推奨しています。 SO、あなたが踏んだ手順やツールの変更点をCAN共有してください。必要ならSO内部チームと確認・共有CAN。 また、SPSDKについては、以下も参考にしてください。 https://docs.nxp.com/bundle/AN14785/page/topics/signing_with_offline_hsm.html お役に立てば幸いです。 よろしくお願いいたします。 アルド。
查看全文
MPC8308CVMAGDA 例外 0055255 谁能解释一下上述零件编号的例外情况。我们需要 MPC8308CVMAGDA,但收到的零件标有 SPC8308CVMAFDA ,AF 零件编号结尾表示 333Mhz,但所需零件编号表示 400Mhz。该设备的右上角还有一个我之前没见过的 “M” 标记,这是否是例外情况的一部分?部件的功能是否相同? 我附上了设备照片和收到的标签。 Re: MPC8308CVMAGDA EXCEPTION 0055255 您可以询问供应商是否有 COC 证书。只有拥有COC证书的供应商才是真正的原始供应商。 Re: MPC8308CVMAGDA EXCEPTION 0055255 你买了假货立即归还。 这是一个骗局。 我可以把正确的图片发给你。我们的 PCB 工厂会拍照。 1.png Re: MPC8308CVMAGDA EXCEPTION 0055255 您好, 我们的情况也一样。你的案子进展如何?NXP 是否确认MPC8308CVMAGDA 和S PC8308CVMA F DA 是相同的? 谢谢!
查看全文
MPC8308CVMAGDA EXCEPTION 0055255 Does anyone have an explanation for the exception on the part number above. We require MPC8308CVMAGDA, however the parts received are marked with SPC8308CVMAFDA, AF part number ending indicates 333Mhz but the required part number denotes 400Mhz. The device also has an addition 'M' marking in the top right corner which i haven't see previously, has this been added as part of the exception? Will the part have the same functionality?  I have attached a photo of the device and the label received.  Re: MPC8308CVMAGDA EXCEPTION 0055255 You can ask the supplier if they have COC certificate. Only the supplier with COC certificate is the real original supplier. Re: MPC8308CVMAGDA EXCEPTION 0055255 You bought a fake product. Return it immediately. This is a scam. I can send you the correct images. Our PCB factory takes photos. 1.png Re: MPC8308CVMAGDA EXCEPTION 0055255 hi, We have the same scenario. How did you move forward in your case?. Did NXP confirm that MPC8308CVMAGDA and SPC8308CVMAFDA are identical? Thank you.
查看全文
MPC8308CVMAGDA例外0055255 上記の部品番号の例外について説明できる人はいますか。MPC8308CVMAGDA が必要ですが、受け取った部品にはS PC8308CVMA F DA とマークされており、AF 部品番号の末尾は 333Mhz を示していますが、必要な部品番号は 400Mhz を示しています。デバイスの右上隅には、以前は見たことのない「M」マークも追加されていますが、これは例外の一部として追加されたのでしょうか?その部品は同じ機能を持ちますか? 受け取ったデバイスとラベリングの写真を添付しました。 Re: MPC8308CVMAGDA EXCEPTION 0055255 サプライヤーに COC 証明書があるかCAN尋ねることができます。COC 証明書を持つサプライヤーだけが真の正規サプライヤーです。 Re: MPC8308CVMAGDA EXCEPTION 0055255 偽造品を購入しました。すぐに返却してください。 これは詐欺です。 正しい画像をCANお送りします。当社のPCB工場では写真を撮ります。 1.png Re: MPC8308CVMAGDA EXCEPTION 0055255 こんにちは、 私たちも同じ状況です。あなたはCASEをどのように進めましたか?NXPは、MPC8308CVMAGDAとS PC8308CVMA F DAが同一であることを確認しましたか? よろしくお願いします。
查看全文
i.MX93 AHAB Secure boot, RSA-PSS signature and HSM mode Hello, I'd like to report an issue I encountered with CST regarding RSA-PSS signature verification on an i.MX93-evk platform, which I believe is a bug. Below, I describe the steps that led me to this discovery. I'm currently implementing the secure boot procedure on an i.MX93-EVK platform and successfully got it working with the standard, documented procedure using CST v4.0.1. I then wanted to sign the various binaries outside of CST, using OpenSSL directly (note: this is not a PKCS#11 setup, I'm just using my own RSA key with the OpenSSL CLI/API). I came across the following procedure, which describes exactly what I wanted to achieve: Using HSM mode for code signing in AHAB devices.pdf This works well with keys generated using the ahab_pki_tree tool provided by the Code Signing Tool (CST), with the following parameters: use an existing CA key: n key type: rsa-pss key length: 4096-bit digest algorithm: sha384 However, the reason I want to sign binaries outside of CST is that I already have an RSA key that is used for signing various other artifacts. When I use this key to sign the various bin files and then try to reintegrate the signed hashes as described in the linked procedure, I get the following error (CST v4.0.1): [ERROR] CST: The signature file spl_data.sig is not valid After double-checking that everything was correct, I also tested verifying my signature using OpenSSL as follows: $ openssl dgst -sha384 -verify pubkey.pem -signature spl_data.sig -sigopt rsa_padding_mode:pss -sigopt rsa_pss_saltlen:digest spl_data.bin Verified OK Expected vs actual: since OpenSSL confirms the signature is a valid PSS signature, I expected CST to accept it during reintegration as well. Instead, CST rejects it as invalid. I started digging into the CST source code and found why it was incorrectly reporting the signature as invalid, even though it was successfully verified by OpenSSL. When CST checks the signature, it does the following: Using OpenSSL API calls, it retrieves the "Public Key Algorithm" field from the public key. Based on this field, it uses another OpenSSL API call to essentially ask: "Does the given signature file correspond to the public key algorithm used?" When generating/using what the NXP documentation calls "RSA-PSS" keys, the "Public Key Algorithm" field is equal to rsassaPss and the checks above work correctly. However, when using a generic RSA key, the "Public Key Algorithm" field is equal to rsaEncryption, and CST wrongly assumes this means the signature format is PKCS#1 v1.5, even though it's entirely possible to sign using the PKCS#1 v2.1 (PSS) format. I confirmed this incorrect assumption by hardcoding into the CST source code that my signature was a PSS one, and I was then able to get my signature successfully verified and reinserted by CST into the final binary. It then worked as expected on my closed device. I'm happy to provide more details if needed, especially regarding the various OpenSSL function calls involved. Could you confirm whether this is a known limitation of CST, or if I might be missing something in how I'm generating/using the signature with a generic RSA key? As a side question, I also tried using SPSDK, which seems to be the new tool NXP is promoting for AHAB-based platforms, but I couldn't find a way to export the binaries to be signed, sign them manually, and then reinsert them, similar to the CST procedure. Do you know if this is feasible? Thanks in advance. Re: i.MX93 AHAB Secure boot, RSA-PSS signature and HSM mode Hello, Actually the document that you are using is correct, is the aproach we suggest for customers that are still using CST. For AHAB, and specially new i.MX9 familly we suggest customers to move to the SPSDK as this is the tool we are using for enablement on security. Even so you can share the steps you have followed and the changes you made to the tool, so I can review and share with internal team if needed. Also, for the SPSDK you may have a look to the following: https://docs.nxp.com/bundle/AN14785/page/topics/signing_with_offline_hsm.html Hope this helps, Best regards/Saludos, Aldo.
查看全文
i.MX93 AHAB 安全启动、RSA-PSS 签名和 HSM 模式 你好, 我想报告我在 i.MX93-evk 平台上使用 CST 进行 RSA-PSS 签名验证时遇到的问题,我认为这是一个 bug。下面我将描述我得出这一发现的步骤。 我目前正在 i.MX93-EVK 平台上实施安全启动程序,并已使用 CST v4.0.1 按照标准、有记录的程序成功使其工作。 然后,我想在 CST 之外对各种二进制文件进行签名,直接使用 OpenSSL(注意:这不是 PKCS#11 设置,我只是使用我自己的 RSA 密钥和 OpenSSL CLI/API)。我找到了以下步骤,它恰好描述了我想要实现的目标:在 AHAB 设备中使用 HSM 模式进行代码签名.pdf 这对于使用代码签名工具 (CST) 提供的ahab_pki_tree工具生成的密钥效果很好,参数如下: 使用现有 CA 密钥:否 密钥类型:rsa-pss 密钥长度:4096 位 摘要算法:sha384 但是,我想要在 CST 之外对二进制文件进行签名的原因是,我已经有一个 RSA 密钥,该密钥用于对各种其他工件进行签名。当我使用此密钥对各种 bin 文件进行签名,然后尝试按照链接中的步骤重新集成签名哈希值时,出现以下错误(CST v4.0.1): [ERROR] CST: The signature file spl_data.sig is not valid 在仔细检查确认一切无误后,我还使用 OpenSSL 测试了签名验证,步骤如下: $ openssl dgst -sha384 -verify pubkey.pem -signature spl_data.sig -sigopt rsa_padding_mode:pss -sigopt rsa_pss_saltlen:digest spl_data.bin Verified OK 预期与实际情况:由于 OpenSSL 确认该签名是有效的 PSS 签名,我预期 CST 在重新集成期间也会接受它。CST 却将其判定为无效并拒绝接受。 我开始深入研究 CST 源代码,并发现了它错误地将签名报告为无效的原因,即使 OpenSSL 已成功验证了该签名。 CST 检查签名时,会执行以下操作: 它使用 OpenSSL API 调用,从公钥中检索“公钥算法”字段。 根据该字段,它使用另一个 OpenSSL API 调用来询问:“给定的签名文件是否与所使用的公钥算法相符?” 当生成/使用 NXP 文档中称为“RSA-PSS”的密钥时,“公钥算法”字段等于rsassaPss ,并且上述检查工作正常。 然而,当使用通用 RSA 密钥时,“公钥算法”字段等于rsaEncryption ,CST 错误地认为这意味着签名格式为 PKCS#1 v1.5,即使完全可以使用 PKCS#1 v2.1 (PSS) 格式进行签名。 我通过在 CST 源代码中硬编码我的签名是 PSS 签名来证实了这个错误的假设,然后我成功地让 CST 验证了我的签名并将其重新插入到最终的二进制文件中。然后它在我的封闭设备上运行正常。 如有需要,我很乐意提供更多细节,特别是关于所涉及的各种 OpenSSL 函数调用。 能否确认这是否是 CST 的已知限制,或者我在使用通用 RSA 密钥生成/使用签名时是否遗漏了某些内容? 另外,我还尝试使用 SPSDK,这似乎是 NXP 为基于 AHAB 的平台推广的新工具,但我找不到导出要签名的二进制文件、手动签名,然后再重新插入的方法,类似于 CST 过程。你知道这是否可行吗? 先行致谢。 Re: i.MX93 AHAB Secure boot, RSA-PSS signature and HSM mode 你好, 实际上,您正在使用的文档是正确的,这是我们建议仍然使用 CST 的客户采用的方法。对于 AHAB,特别是新的 i.MX9 系列,我们建议客户迁移到 SPSDK,因为这是我们用于启用网络安全的工具。 即便如此,您仍然可以分享您遵循的步骤以及您对工具所做的更改,以便我进行审核,并在需要时与内部团队分享。 另外,关于SPSDK,您可以参考以下内容: https://docs.nxp.com/bundle/AN14785/page/topics/signing_with_offline_hsm.html 希望这能帮到你。 此致敬礼/Saludos, 阿尔多。
查看全文
ARA240(.dvm)用のカスタムONNX/TFLiteモデルをコンパイルする方法は?(搬送波はi.MX95 FRDMを使用しています) 私はi.MX95 FRDMのARA240 M.2アクセラレータを評価しています。 ランタイムは正常に動作しています。 ARA240はPCIe経由で検出されます。 nnapp は提供された .dvm を正常に実行しますモデル. ランタイムSDKs(rt-sdk-ara240)とPython DVAPIバインディングがインストールされています。 しかし、自分でMobileNetモデルを展開したいのですが、モデルを.dvmにコンパイルするためのツールチェーンが見つかりません形式。 私の質問は以下のとおりです。 カスタムONNX/TFLiteモデルを.dvmにコンパイルする際のサポートワークフローは何ですか?ARA240用ですか? Ara2コンバータ(またはdvconvert/dvnc)は公開されているのか、それともRuntime SDKsとは別に配布されているのか? NXPがサポートするカスタムCNNモデルを展開する方法はありますか(例:MobileNet) を ARA240 に移植する際に、私が見落としている点はありますか? どんなガイダンスやドキュメントでも大変ありがたいです。 よろしくお願いします! Re: How to compile custom ONNX/TFLite models for ARA240 (.dvm) ?(carrier being used i.MX95 FRDM) CNNモデルには、公式ウェブサイトからダウンロードできるAra2ランタイムパッケージが役立つかもしれません Ara240のランタイム環境を提供します。Ara240モジュール上で事前コンパイルされたCNNおよびGenAIモデルをダウンロードし実行するためのスクリプトを提供します。ご質問への回答は、下記のAIによる回答をご参照ください。お役に立てれば幸いです。 =========================================================================== まず、重要な背景説明から始めましょう。 ARA240(旧名:キナラ・アラ2).dvm= Kinara DNN 仮想マシンのバイナリモデル、このDNPU用の独自のコンパイルされたグラフ形式。 rt-sdk-ara2 (target runtime + DVAPI) ≠ コンパイラツールチェーン. i.MX95には推論ランタイムのみがインストールされています。オフラインモデルコンパイラは別のソフトウェアです。 1. サポートされているワークフロー: ONNX / TFLite → .dvm 公式なエンドツーエンドの流れ: PyTorch/TensorFlow → ONNX / TFLite → Ara2オフラインコンパイラ(dvconvert / dvnc、Ara2コンバーター) → 量子化(MobileNetのようなCNNではint8推奨) → 最適化された.dvmバイナリ → .dvm を i.MX95 FRDM にデプロイする → PCIe経由でARA240にDVAPI / nnapp / libaraclientをロードして実行する 重要な制約:コンパイルはi.MX95ターゲットボード上で実行できません。 コンパイラはホスト側のLinux x86_64ツールチェーンで、外部のPC/ワークステーション上で実行されます。 2. dvconvert / Ara2 Converterは公開されているのでしょうか? いいえ。コンバーターは一般にダウンロードできません。 NXP GitHubでホストされているrt-sdk-ara2 Debianパッケージには、ターゲットランタイム、DVAPI Pythonバインディング、事前構築済みのデモ.dvmのみが含まれていますモデル.コンパイラバイナリは含まれていません。 Ara2コンパイラスイート(dvconvert、dvnc)はNXPの制限付きソフトウェアアクセスのもとで別途配布されています。 このツールチェーンはキナラに起源を持ち、NXPがキナラを買収した後は、NXPの営業/CAS(お客様アプリケーションサポート)を通じてアクセス管理が行われました。 3. NXPが公式にサポートするカスタムCNN(MobileNet)の導入方法はありますか? はい、ただしAra SDKコンパイラへのアクセスを正式に申請する必要があります: コンバータを入手するための公式なルート お近くのNXP FAE / NXP CASサポートチケットにお問い合わせください: ハードウェア: FRDM i.MX95 + ARA240 M.2 DNPU リクエスト:カスタムONNX/TFLite CNNコンパイルを.dvmにするためのAra SDKオフラインモデルコンパイラ(dvconvert)へのアクセス 制限付きAraツールについてはNXPのソフトウェアライセンス契約に署名する必要があります。 NXPは当初、更新されたeIQ Toolkit(2026年中頃予定)と並行してより広範なリリースを計画していました。現在はサポートされている評価お客様向けにゲートされています。 ツールアクセスを待つ間の回避策と代替案 カスタム.dvmは生成できませんdvconvertを使用せずにローカルで実行します。ARA240.dvm用のオープンソースのサードパーティ製コンバーターは存在しません。 オプションA:早期アクセス評価の一環としてNXPのエンジニアリングサポートにモデルコンパイルを依頼する。 オプションB:一時的にワークロードを分散:未コンパイルのONNXをi.MX95オンボードeIQ Neutron上で実行し、Araコンパイラへのアクセスを待つ間に実行します(これはARA240へのオフロードなし)。 注意:i.MX95の内蔵Neutron NPU(.neutronモデル)と外部のARA240 DNPU(.dvm)を混同しないでください。彼らは完全に互換性のないバイナリフォーマットを使っています。 4. 避けるべき主な落とし穴 rt-sdk-ara2内にはPaddle2ONNX / ONNXコンバーターユーティリティはありません。 事前に構築されたデモ用.dvmファイルSDKに付属して配布されたファイルは、変換ロジックを抽出するためにリバースエンジニアリングすることはできません。 現在、ARA240用のウェブベースのモデルコンバーターは利用できません。 MobileNet v1/v2は、ツールチェーンを入手すればdvconvertによって完全にサポートされるアーキテクチャです。ONNXがクリーンアップされていることを確認してください(未使用のノードを削除し、入力形状を固定し、標準演算のみを使用する)。 NXPサポートチケットに直接送る提案文言 FRDM i.MX95上でARA240 M.2モジュールを評価しています。PCIe列挙、サンプル.dvmを提供実行、rt-sdk-ara2、DVAPIは機能します。カスタムMobileNet ONNXモデルを.dvmにコンパイルするには、Ara2オフラインコンパイラ(dvconvert/dvnc)へのアクセスが必要ですバイナリ。ホスト側のAra SDKモデル変換ツールチェーンを取得する手順を共有してください。
查看全文
How to compile custom ONNX/TFLite models for ARA240 (.dvm) ?(carrier being used i.MX95 FRDM) I'm evaluating the ARA240 M.2 accelerator on the i.MX95 FRDM. The runtime is working correctly: ARA240 is detected over PCIe. nnapp successfully runs the provided .dvm models. The Runtime SDK (rt-sdk-ara240) and Python DVAPI bindings are installed. However, I would like to deploy my own MobileNet model, and I'm unable to find the toolchain required to compile models into the .dvm format. My questions are: What is the supported workflow to compile a custom ONNX/TFLite model into .dvm for ARA240? Is the Ara2 Converter (or dvconvert/dvnc) publicly available, or is it distributed separately from the Runtime SDK? Is there an NXP-supported way to deploy custom CNN models (e.g. MobileNet) onto ARA240, that I am missing? Any guidance or documentation would be greatly appreciated. Thanks! Re: How to compile custom ONNX/TFLite models for ARA240 (.dvm) ?(carrier being used i.MX95 FRDM) For CNN model,Ara2 Runtime Package could be helpful which can downloaded from the official website Provides a runtime environment for Ara240.Provides scripts to download and run pre-compiled CNN and GenAI models on Ara240 modules. For your question, please refer to the AI generated answer as below, hope it helps  =========================================================================== First, critical background: ARA240 (formerly Kinara Ara-2) .dvm = Kinara DNN Virtual Machine binary model, proprietary compiled graph format for this DNPU. rt-sdk-ara2 (target runtime + DVAPI) ≠ compiler toolchain. You have only the inference runtime installed on i.MX95; the offline model compiler is separate software. 1. Supported workflow: ONNX / TFLite → .dvm Official end-to-end flow: PyTorch/TensorFlow → ONNX / TFLite → Ara2 Offline Compiler (dvconvert / dvnc, Ara2 Converter) → Quantization (int8 preferred for CNN like MobileNet) → Optimized .dvm binary → Deploy .dvm to i.MX95 FRDM → Load & run via DVAPI / nnapp / libaraclient over PCIe to ARA240 Important constraint: Compilation cannot run on the i.MX95 target board. The compiler is a host-side Linux x86_64 toolchain, executed on an external PC/workstation. 2. Is dvconvert / Ara2 Converter public? NO. The converter is NOT publicly downloadable. The rt-sdk-ara2 Debian packages hosted on NXP GitHub only contain target runtime, DVAPI Python bindings, prebuilt demo .dvm models. No compiler binaries included. The Ara2 compiler suite (dvconvert, dvnc) is distributed separately under NXP restricted software access. This toolchain originated from Kinara; after NXP acquired Kinara, access is managed via NXP sales / CAS (Customer Application Support). 3. Is there an official NXP-supported path to deploy custom CNN (MobileNet)? Yes, but you need to formally request access to the Ara SDK compiler: Official route to obtain the converter Contact your local NXP FAE / NXP CAS support ticket referencing: Hardware: FRDM i.MX95 + ARA240 M.2 DNPU Request: Access to Ara SDK offline model compiler (dvconvert) for custom ONNX/TFLite CNN compilation to .dvm You will need to sign NXP’s software license agreement for restricted Ara tooling. NXP originally planned wider release alongside updated eIQ Toolkit (previously scheduled mid-2026); at present, it remains gated to supported evaluation customers. Workarounds & alternatives while waiting for tool access You cannot generate custom .dvm locally without dvconvert. There is no open-source third-party converter for ARA240 .dvm. Option A: Ask NXP engineering support to perform model compilation as part of your early access evaluation. Option B: Split workload temporarily: run uncompiled ONNX via CPU/Neutron NPU on i.MX95 onboard eIQ Neutron while waiting for Ara compiler access (this does not offload to ARA240). Note: Do not confuse i.MX95’s built-in Neutron NPU (.neutron model) with external ARA240 DNPU (.dvm). They use completely incompatible binary formats. 4. Key pitfalls to avoid There is no Paddle2ONNX / ONNX converter utility inside rt-sdk-ara2. Prebuilt demo .dvm files distributed with the SDK cannot be reverse-engineered to extract conversion logic. No web-based model converter available for ARA240 today. MobileNet v1/v2 are fully supported architectures by dvconvert once you receive the toolchain; ensure ONNX is cleaned (remove unused nodes, fixed input shape, standard ops only). Suggested wording you can directly send to NXP support ticket We are evaluating ARA240 M.2 module on FRDM i.MX95. PCIe enumeration, provided sample .dvm execution, rt-sdk-ara2 and DVAPI are functional. We require access to the Ara2 offline compiler (dvconvert/dvnc) to compile custom MobileNet ONNX models into .dvm binaries. Please share procedure to obtain the host-side Ara SDK model conversion toolchain.
查看全文
如何为 ARA240 (.dvm) 编译自定义 ONNX/TFLite 模型?(载板型号为 i.MX95 FRDM) 我正在评估 i.MX95 FRDM 上的 ARA240 M.2 加速器。 运行时运行正常: 通过 PCIe 检测到 ARA240。 nnapp 成功运行提供的 .dvm 文件模型。 已安装运行时 SDK (rt-sdk-ara240) 和 Python DVAPI 绑定。 但是,我想部署我自己的 MobileNet 模型,却找不到将模型编译成 .dvm 文件所需的工具链。格式。 我的问题是: 将自定义 ONNX/TFLite 模型编译成 .dvm 文件的受支持工作流程是什么?适用于 ARA240? Ara2 变流器(或 dvconvert/dvnc)是公开提供的,还是与运行时 SDK 分开分发的? NXP 是否支持部署自定义 CNN 模型(例如)MobileNet) 到 ARA240,我漏掉了什么吗? 任何指导或文件都将不胜感激。 谢谢您! Re: How to compile custom ONNX/TFLite models for ARA240 (.dvm) ?(carrier being used i.MX95 FRDM) 对于 CNN 模型,Ara2 运行时代码包,软件包可能很有帮助,可以从官方网站下载。 为 Ara240 提供运行时环境。提供脚本以下载并在 Ara240 模块上运行预编译的 CNN 和 GenAI 模型。关于您的问题,请参考下方人工智能生成的答案,希望对您有所帮助。 =========================================================================== 首先,需要一些关键背景信息: ARA240(原名 Kinara Ara-2).dvm= Kinara DNN 虚拟机二进制模型,此 DNPU 的专有编译图格式。 rt-sdk-ara2(目标运行时 + DVAPI)≠ 编译器工具链。 i.MX95 上只安装了推理运行时;离线模型编译器是单独的软件。 1. 支持的工作流程:ONNX / TFLite → .dvm 官方端到端流程: PyTorch/TensorFlow → ONNX / TFLite → Ara2 离线编译器(dvconvert / dvnc,Ara2 变流器) → 量化(对于像 MobileNet 这样的 CNN,首选 int8) → 优化后的 .dvm二进制 → 将 .dvm 文件部署到 i.MX95 FRDM → 通过 PCIe 经由 DVAPI / nnapp / libaraclient 加载并运行至 ARA240 重要限制:编译无法在 i.MX95 目标板上运行。 该编译器是主机端 Linux x86_64 工具链,在外部 PC/工作站上执行。 2. dvconvert / Ara2 变流器 是公开的吗? 不。该变流器不可公开下载。 NXP GitHub 上托管的 rt-sdk-ara2 Debian 软件包仅包含目标运行时、DVAPI Python 绑定和预构建的演示 .dvm 文件。模型。不包含编译器二进制文件。 Ara2 编译器套件(dvconvert、dvnc)根据 NXP 限制软件访问权限单独分发。 该工具链源自 Kinara;NXP 收购 Kinara 后,访问权限由 NXP 销售/CAS(客户应用支持)管理。 3. NXP 是否有官方支持的途径来部署自定义 CNN(MobileNet)? 是的,但您需要正式申请访问 Ara SDK 编译器: 获取变流器的官方途径 请联系您当地的 NXP FAE / NXP CAS 支持团队,并参考,引用: 硬件:FRDM i.MX95 + ARA240 M.2 DNPU 请求:提供 Ara SDK 离线模型编译器 (dvconvert) 的访问权限,以便将自定义 ONNX/TFLite CNN 文件编译为 .dvm 文件。 您需要签署 NXP 的受限 Ara 工具软件许可协议。 NXP 最初计划与更新后的 eIQ Toolkit(原计划于 2026 年年中发布)一同进行更广泛的版本;目前,它仍然只对受支持的评估客户开放。 等待工具访问期间的变通方法和替代方案 您无法生成自定义 .dvm 文件。本地不使用 dvconvert。目前没有适用于 ARA240 .dvm 的开源第三方变流器。 方案 A:请 NXP 工程支持部门执行模型编译,作为您早期访问评估的一部分。 选项 B:暂时拆分工作负载:在等待 Ara 编译器访问期间,通过 i.MX95 板载 eIQ Neutron 上的 CPU/Neutron NPU 运行未编译的 ONNX(这不会卸载到 ARA240)。 注意:不要将 i.MX95 内置的 Neutron NPU(.neutron 型号)与外部 ARA240 DNPU(.dvm)混淆。它们使用完全不兼容的二进制格式。 4. 需要避免的关键陷阱 rt-sdk-ara2 中没有 Paddle2ONNX / ONNX 变流器实用程序。 预构建演示 .dvmSDK 中分发的文件无法通过逆向工程提取转换逻辑。 目前还没有适用于 ARA240 的基于网络的模型变流器。 一旦您收到工具链,dvconvert 将完全支持 MobileNet v1/v2 架构;确保 ONNX 已清理(删除未使用的节点、固定输入形状、仅使用标准操作)。 您可以直接将以下措辞发送给恩智浦技术支持工单。 我们正在对 FRDM i.MX95 上的 ARA240 M.2 模块进行评估。PCIe 枚举,提供示例 .dvm执行方面,rt-sdk-ara2 和 DVAPI 功能正常。我们需要访问 Ara2 离线编译器 (dvconvert/dvnc) 来将自定义 MobileNet ONNX 模型编译成 .dvm 文件。二进制.请分享获取主机端 Ara SDK 模型转换工具链的步骤。
查看全文
Create a new model and configure it for NXP Hardware 1 Table of Contents • Introduction • Prerequisites • Creating a New Simulink Model • Configure the Model for NXP Hardware • Add Simulink Blocks • Build the Model • Flash and Run on Hardware • References • Conclusion 2 Introduction Developing embedded applications for NXP microcontrollers—especially platforms like the S32K series—involves using tools such as MATLAB/Simulink (MBDT – Model-Based Design Toolbox), S32 Design Studio (S32DS), and EB tresos. This article walks through the key steps involved in creating a new model and configuring it properly for NXP hardware, focusing on a practical workflow used in automotive and embedded systems projects. 3 Prerequisites Before starting, ensure the following tools are installed and correctly configured: MATLAB & Simulink NXP MBDT S32 Design Studio / EB tresos NXP RTD drivers USB / JTAG debugger (e.g., PEMicro) Target hardware (e.g., S32K344, S32K358) In addition to having the required tools installed, it is important to ensure that all components are properly integrated and compatible with each other. This includes matching the MATLAB/Simulink version with the supported release of the NXP MBDT, as well as aligning the RTD package with the selected microcontroller and AUTOSAR version. Environment variables, compiler paths, and licensing (for MATLAB, Simulink, and EB tresos) should also be verified prior to starting development. From a hardware perspective, make sure that the evaluation board or target ECU is correctly powered and that the debug interface (such as PEMicro) is functioning. Installing the appropriate USB drivers and checking connection through debug tools can prevent communication issues later in the workflow. Finally, it is recommended to validate the toolchain setup by running a simple example, such as a GPIO toggle or LED blink application, either directly in S32DS or through an existing Simulink example provided by MBDT. This step helps confirm that code generation, compilation, flashing, and execution on the target hardware are all working correctly before moving on to a more complex development. 4 Creating a New Simulink Model Step 1: Launch Simulink Open MATLAB Type simulink in the command window Select Blank Model Sebastian13_0-1784719500241.png Step 2: Save the Model Save with a clear naming convention, e.g. s32k344_led_blink.mdl 5 Configure the Model for NXP Hardware Step 3: Open Model Configuration Parameters Navigate to Model Settings ( Ctrl + E ) → Hardware Implementation Step 4: Select Hardware Board Set Hardware board to the appropriate NXP target For example, NXP S32Kxx Step 5: Select a Configuration Template Set Configuration Project Template to the appropriate NXP target For example, S32K344-Q172 S32 Config Tool If the board is not visible, ensure MBDT is properly installed. Sebastian13_1-1784719557125.png 6 Add Simulink Blocks Using the Library Browser, configure hardware peripherals. Sebastian13_3-1784719625876.png Step 6: Configure GPIO for LED Add a Dio block Configure: Function: Dio_FlipChannel Channel: e.g. DioLed0 Step 7: Add Level Variable Add Data Store Memory and Data Store Write blocks Connect the Dio block to the Data Store Write This will blink an LED because the Dio_FlipChannel function toggles the logical state of the selected GPIO pin every time it is executed. By connecting it to a Data Store Write, you are effectively allowing the system to store or propagate the updated state within the model. The blinking frequency is directly controlled by the task rate of your model, which makes it easy to adjust the LED behavior simply by changing the sample time, without modifying the core logic. In the Library Browser you will find numerous example projects that may be helpful (for example, s32k3xx_dio_s32ct ). Sebastian13_4-1784719654387.png 7 Build the Model Step 8: Generate Code Click Build Model ( Ctrl + B ) Sebastian13_5-1784719707916.png When you press the build button, Simulink automatically translates your model into C code and prepares it for execution on the target microcontroller. The generated files can be found in the project folder, where you can explore how each block was converted into embedded code. After generation, the toolchain creates an executable file and attempts to deploy it directly to the target board. 8 Flash and Run on Hardware Step 9: Connect Target Board Connect via debugger (USB / JTAG) Step 10: Deploy From Simulink (External Mode or Build & Deploy) Or manually via S32 Design Studio 9 References Quick Start Guide for S32K3X4EVB Board Model-Based Design Toolbox (MBDT) – How To 10 Conclusion Creating a new model and configuring it for NXP hardware involves: Setting up the Simulink model Configuring hardware-specific parameters Adding peripheral blocks Generating and deploying embedded code This workflow enables rapid prototyping and production-ready embedded development, especially in automotive systems leveraging AUTOSAR and NXP platforms. Developing embedded applications for NXP microcontrollers—especially platforms like the S32K series—often involves using tools such as MATLAB/Simulink (MBDT – Model-Based Design Toolbox), S32 Design Studio (S32DS), and AUTOSAR tools like EB tresos. This article walks through the key steps involved in creating a new model and configuring it properly for NXP hardware, focusing on a practical workflow used in automotive and embedded systems projects.
查看全文
Functional Safety in Motor Control with AMMCLib and ASCLib When developing motor control for automotive and industrial systems, functional safety is a core requirement to ensure a motor does not produce unintended torque or speed. However, implementing complex algorithms like Field-Oriented Control (FOC) as a functionally safe component introduces severe architectural complexity, significantly increases development effort, and degrades overall performance. To solve this, NXP utilizes a safety decomposition approach that divides the application into a non-safety-related part (QM) and a safety-related part (ASIL). For this approach, NXP plans to provide the Automotive Safety Checker Library (ASCLib), which delivers ready-to-use safety checkers for the safety part. This enables high safety compliance without requiring a redesign of the QM motor control (MC) part. The Perfect Match: AMMCLib (QM) + ASCLib (ASIL) Many applications use highly optimized NXP's Automotive Math and Motor Control Library (AMMCLib) for the motor control part. While AMMCLib delivers exceptional performance, it is a Quality Management (QM) level library. Compliance with safety standards (such as ISO 26262) required teams to build custom safety mechanisms around the QM-level AMMCLib, consuming significant time and effort. NXP's ASCLib solves this by providing standardized, production-ready safety checkers. This eliminates proprietary safety software development and significantly reduces time-to-certification. Untitled Diagram (1).png How AMMCLib and ASCLib Fit Together The block diagram below illustrates a standard FOC system using this concept. The blue motor control blocks represents the QM-level AMMCLib functions, while the green blocks represent the ASCLib checkers that monitor key points to ensure safety. This architecture is based on the IEEE Low Complexity Safety Concept for FOC PMSM. source-NXPcommunity5.drawio.png This reference architecture shows that integrating ASCLib requires no changes to the existing QM motor control architecture. Full data-type compatibility allows ASCLib checkers to map directly to AMMCLib signals, ensuring seamless interconnection. The architecture assumes that Freedom from Interference (FFI) between the safety-related and QM software components is ensured. While standard FOC is a common use case, ASCLib is not limited to it. Thanks to its modular, independent blocks, the library supports alternative topologies and advanced techniques - including sensorless FOC and single-shunt current measurement. Inside ASCLib: A Layered Safety Architecture The ASCLib features a highly structured, layered software model organized hierarchically into Layers and Packages: pavelsvadbik_0-1784127185062.png The Service Layer (Top Layer) Exposes high-level functionalities directly to the safety application through two independent packages: High-Level Checkers (HLC): Wide range of application-level safety checkers tailored for various motor control systems. Fault Manager (FMG): Sophisticated fault-handling component managing error synchronization, configuration, and application notifications. The Core Layer (Foundational Layer) Provides the low-level building blocks utilized by the Service Layer. It consists of two essential packages: Low-Level Checkers (LLC): Delivers fundamental mathematical and verification functions. Fault-Debouncing (FDB): Provides generic fault debouncing algorithms. Tip.pngDeveloper Tip: The entire library is fully modular, isolated, and independent. If your application requires a unique checker, you can easily build your own custom checkers using the existing low-level blocks inside the LLC and FDB packages. Furthermore, the Fault Management (FMG) package is entirely optional—you are not forced to use it and can implement your own application-level error handling instead.   Not Just For Automotive Don't let the name fool you. While ASCLib has "Automotive" in its title and natively supports ISO 26262 workflows, its safety principles are universal. ASCLib applies perfectly to industrial systems complying with IEC 61508. To fit seamlessly into your existing development workflow, ASCLib features a dual-delivery option: Pure C Source Files: For direct integration into any bare-metal or RTOS-based embedded project. BAM (Bit Accurate Models): Ready-to-use blocks for Model-Based Design (MBD), allowing you to drag, drop, and simulate your safety architecture directly in MATLAB®/Simulink®. Key Benefits for Developers AMMCLib Remains QM: Keep using your existing, highly optimized AMMCLib code for core motor control. Model-Based development: Accelerate your design cycle by building and simulating your entire safety part using dedicated ASCLib BAM directly in MATLAB®/Simulink® before generating target C code. Accelerated Certification: Pre-designed safety checkers and integrated fault management significantly simplify your safety compliance and auditing processes. Get Started and Share Your Thoughts ASCLib is designed to be completely MCU-independent, giving you the flexibility to deploy it across various NXP hardware platforms. To accelerate your development, it is planned to be fully verified and ready to integrate with NXP’s automotive and industrial MCUs. By separating control from safety, you get the best of both worlds: maximum motor performance and uncompromising safety. Working on an upcoming ISO 26262 or IEC 61508 motor control project? Let’s discuss in the comments how the AMMCLib + ASCLib approach can simplify your design. We would also highly appreciate it if you could take a moment to fill out our quick survey below to share your insights with us! This project has received national funding from the MEYS and the funding from European Union’s Horizon Europe research and innovation framework programme under grant agreement No. 101112274. The ISOLDE project, nr. 101112274 is supported by the Chips Joint Undertaking and its members Austria, Czechia, France, Germany, Italy, Romania, Spain, Sweden, Switzerland. Building functionally safe motor control systems doesn’t have to mean sacrificing performance or redesigning your architecture. Discover how NXP combines AMMCLib and ASCLib to separate safety from motor control, reduce development effort, and accelerate certification—without compromising efficiency. Motor Control
查看全文
FS26 LDO Off Issue Hello I am using the FS26 and S32K358. I am using the FS26's VLDO2 as the power supply for the MCU and the FS26's VLDO1 as the power supply for the CAN transceiver. When the MCU is left in a state of CAN communication, the FS26's VLDO turns OFF, cutting off the MCU's power. (This occurs randomly, approximately every 1 to 8 hours.) The VLDO is restored only after the FS26's power supply is cut off and then restored. This issue occurs on all boards, not just a single one, and does not occur when CAN communication is not in progress. The status when the issue occurs is as follows: Vpre 6V O VDIG 1.6V O VBOS 5V O VLDO2 X VLDO1 X VCORE X DFS is disabled via OTP. I would like to know the current state of the FS26 and what causes this to happen. Re: FS26 LDO Off Issue Hello kjy106906  Good day! Is the watchdog enabled? What are the values of: FS_STATES FS_GRL_FLAGS FS_OVUV_REG_STATUS M_REG_FLG M_STATUS immediately after failure? Have you checked if FS26 is not displaying any UV or OV flags? Also could you share your M_STATUS? I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck. Re: FS26 LDO Off Issue @RafaR  Thank you for the reply. Unfortunately, the MCU is receiving power from the SBC, but communication is not possible because the VLDO is OFF. You must cut off and resupplied the board power for the MCU to function. The watchdog window is infinite. Re: FS26 LDO Off Issue Hello kjy106906 Good day! Looks as if the FS26 analog front end is still powered, but the internal power-tree supplying the system has been disabled. One possible explanation is that a fault has been detected on one of the monitored regulators (VCORE, VLDO1, VLDO2), and the configured reaction disables the regulator outputs. FS26 documentation indicates that regulators can remain disabled after a fault depending on the configured fault-reaction settings. I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck. Re: FS26 LDO Off Issue db16122_0-1785211448726.png Please refer to PMIC initiailization process for debug. AN13431 NXP PMIC solution for TI TMS570 series MCU should be helpful Re: FS26 LDO Off Issue Thank you @RafaR  This is an important issue, so I would appreciate your response. I would like to check exactly what state FS26 is in and why it failed. When the issue occurred, I read the registers using an external tool. FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORCMD:0x1c]W:0x001d; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MIRRORDATA:0x1d]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [ID_VOTP:0x1D]R:0x00 FS26 [FS_WDW_DURATION:0x0b]W:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]W:0x2f74; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_DEVICEID:0x00]R:0x65d8; CRC[MOSI:0x00; MISO:0x00] FS26 [M_PROGID:0x01]R:0x0105; CRC[MOSI:0x00; MISO:0x00] FS26 [M_STATUS:0x02]R:0x5020; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_FLG:0x03]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_MSK:0x04]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_FLG:0x05]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_MSK:0x06]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_FLG:0x07]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_VSUP_MSK:0x08]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_FLG:0x09]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_MSK:0x0a]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_FLG:0x0b]R:0x0005; CRC[MOSI:0x00; MISO:0x00] FS26 [M_COM_MSK:0x0c]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_SYS_CFG:0x0d]R:0x0001; CRC[MOSI:0x00; MISO:0x00] FS26 [M_TSD_CFG:0x0e]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CFG:0x0f]R:0x0002; CRC[MOSI:0x00; MISO:0x00] FS26 [M_WIO_CFG:0x10]R:0x0202; CRC[MOSI:0x00; MISO:0x00] FS26 [M_REG_CTRL1:0x11]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_AMUX_CTRL:0x13]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG1:0x14]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG2:0x15]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CFG3:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_LDT_CTRL:0x17]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY0:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [M_MEMORY1:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_GRL_FLAGS:0x00]R:0x5000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WDW_DURATION:0x0b]R:0xd08b; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_NOT_WDW_DURATION:0x0c]R:0x2144; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_WD_TOKEN:0x0e]R:0x5ab2; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_ABIST_ON_DEMAND:0x0f]R:0x0040; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_OVUV_REG_STATUS:0x10]R:0x1544; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_1:0x12]R:0xf000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_SAFE_IOS_2:0x13]R:0x035f; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY1:0x14]R:0x03c3; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_DIAG_SAFETY2:0x15]R:0x0010; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_INTB_MASK:0x16]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_STATES:0x17]R:0x0009; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LP_REQ:0x18]R:0x0000; CRC[MOSI:0x00; MISO:0x00] FS26 [FS_LDT_LPSEL:0x19]R:0x0000; CRC[MOSI:0x00; MISO:0x00] I am attaching the waveform when an issue occurs. kjy106906_0-1785205262839.png Blue VSUP / Red VBOS / Green RSTB / Yellow VDIG kjy106906_1-1785205354126.png Blue VSUP / Red VPre / Green Vcore / Yellow RSTB
查看全文
T1024 QorIQ Bare-Metal BSP for CodeWarrior PA10.5 We need official QorIQ T10xx bare-metal BSP package matching CodeWarrior Power Architecture v10.5. Required content: 1. Complete bare-metal startup BSP for T1024 2. RCW, reset, L1/L2 cache, DDR, interrupt, PCIe low-level driver source 3. CodeWarrior PA10.5 stationary project templates 4. Reference bare-metal demo project for T10xx RDB board Background: We are developing bare-metal firmware on T1024 using CodeWarrior PA10.5, LSDK 2.0 Linux SDK only provides U-Boot & Linux source, missing official CodeWarrior bare-metal BSP. Please provide the official BSP archive or download link. Thanks. Re: T1024 QorIQ Bare-Metal BSP for CodeWarrior PA10.5 We don't have Bare-Metal BSP for T1024 platform. You could require NetComm software for other platform to have reference. https://www.nxp.com.cn/products/processors-and-microcontrollers/power-architecture/qoriq-communication-processors/p-series/netcomm-software-resources:NetComm_Software
查看全文
GUI Guider 2.0におけるSpangroupウィジェットの利用可能性とFUTUREロードマップに関する問い合わせ こんにちは、NXPコミュニティの皆さん、 現在、プロジェクト開発においてGUI Guider 2.0を使用しています。 バージョン2.0への移行中に、以前のGUI Guider 1.xで利用可能だったSpangroupウィジェットが削除されていることに気づきました。基盤となるLVGLライブラリは依然としてSpangroupをサポートしているため、最新リリースでこの欠落がなぜか気になりました。 このウィジェットはUIデザインに非常に役立ちました。ぜひ教えていただけませんか: 今後のGUI Guiderのリリースで、Spangroupウィジェットを再導入する予定はありますか? もしSOなら、次のリリーススケジュールの大まかなスケジュールやロードマップを共有してもらえますか? この件に関して何かご意見やご助言をいただければ大変ありがたいです。 サポートありがとうございます! よろしくお願いいたします。 Re: Inquiry regarding Spangroup widget availability in GUI Guider 2.0 and future roadmap こんにちは、 @mastergbc さん、 既にGUI Guider開発チームに評価を依頼しており、進展があれば随時ご報告いたします。 その間、実用的な回避策としては、主要なUI設計とコード生成にはGUI Guider 2.0を使用し、必要なLVGLネイティブspangroup実装を手動で生成プロジェクトに追加することです。 GUI Guiderウィジェットパレットに直接公開されていないLVGL機能については、カスタムコードで統合できます。 お役に立てば幸いです。 BR セレステ Re: Inquiry regarding Spangroup widget availability in GUI Guider 2.0 and future roadmap 最新情報のご提供ありがとうございます。 私たちのユースケースについて少し説明すると、プロジェクトでは Spangroup ウィジェットを使って異なるフォントスタイルや言語をシームレスに混ぜ、特に英語と韓国語のフォントを1つのテキストブロック内で混同しています。 現在、Spangroupを使用して構築されたUIオブジェクトは約12個あります。このウィジェットは、先行する子要素のテキストや長さが変更された場合、後続の子要素のテキストが自動的に再配置され、整列を維持しながらスムーズに折り返されるため、非常に重要な役割を果たしています。 GUI GuiderでSpangroupウィジェットを再実装する長期的な計画がない場合、このマルチフォント/マルチスタイルのテキスト巻き取り動作を実現するための推奨の代替案や回避策をご提案いただけますか? ご協力いただき、改めて感謝申し上げます。 よろしくお願いいたします。 Re: Inquiry regarding Spangroup widget availability in GUI Guider 2.0 and future roadmap こんにちは、 @mastergbc さん、 投稿ありがとうございます。 現在、 SpanGroupウィジェット はGUI Guider 2.0で利用可能ではなく、近い将来に追加する計画もありません。 しかし、お客様の要望をよりよく理解し、要望を評価したいと考えています。SpanGroup Widgetで達成しようとしている機能について、もう少し詳しく教えていただけますか?例えば、具体的なユースケース、期待される動作、使用頻度、そしてこの機能がプロジェクトにとってどれほど重要かなどです。この情報は、リクエストを評価し、必要に応じてGui-Guiderチームに転送するのに役立ちます。 さらに、現在どの製品を使っているのか(MCUかMPUモデルか)教えていただけますか?これにより、あなたのアプリケーション状況をよりよく理解できます。 良い1日を。 BR セレステ
查看全文
Support Period for Yocto Linux BSP Hello, Could you please provide information regarding the following? We are planning to use the Yocto Linux BSP provided by NXP for a board based on the i.MX 8M Plus. Could you please answer the following questions regarding the BSP? 1. How long are updates provided after a BSP is released? 2. When a new Yocto LTS release becomes available, how long does it typically take for the BSP to be updated to incorporate the new Yocto LTS version? 3. We understand that security updates are available through "BSP Lifecycle Maintenance: Keeping Your Linux® BSP Secure." Could you please let us know: - the maximum support period available, and - the approximate cost of this service? Thank you for your support. We look forward to your response. Best regards,
查看全文
MCUXpresso IDE v25.6.136升级内置的config tools之后不能启动调试,为什么 我正在使用MCUXpresso IDE v25.6.136开发FRDM-IMXRT1186,从官网下载最新的IDE安装之后,安装最新的SDK(26.06),导入一个frdmimxrt1186_rled_blinky_cm7示例工程之后点击mex无法打开,于是我升级了配置工具,这时mex文件可以打开了,但是点击调试无法连接到开发板,如图所示,怎么办? (已经尝试升级linkserver版本,没用) breeze_i_0-1785204475278.png #FRDM-IMXRT1186 #MIMXRT1180 MCUXpresso-IDE  LINKERSERVER  回复: MCUXpresso IDE v25.6.136升级内置的config tools之后不能启动调试,为什么 感谢来信。 请您在 MCUXpresso IDE 的 Preferences → MCUXpresso IDE → Debug Options → LinkServer Options 中确认当前 IDE 实际使用的 LinkServer 路径。 请进入该路径对应的 LinkServer 安装目录,执行下面命令,确认该 LinkServer 是否可以识别板载调试器:linkserver probes 请注意,建议在该目录下执行命令,而不是直接在任意命令行窗口执行,以避免调用到系统 PATH 中其他版本的 LinkServer。 如果您单独安装了其他版本的 LinkServer,也可以尝试勾选 Custom path ,并指定到对应的 LinkServer 安装目录,避免 IDE 仍然调用旧版本或异常路径下的 LinkServer。 回复: MCUXpresso IDE v25.6.136升级内置的config tools之后不能启动调试,为什么 都试过了,还是不行 Re: MCUXpresso IDE v25.6.136升级内置的config tools之后不能启动调试,为什么 Hi @breeze_i , 感谢您关注 NXP RT 系列产品并使用 NXP 社区。 关于您的问题我建议您检查下面几点: 1:首先检查防火墙或杀毒软件是否拦截 IDE / LinkServer / redlinkserv 的 localhost 通信; 2:不要在原 workspace 上继续试,新建一个空的 workspace,然后重新导入demo; 3:在 IDE 中执行 Clean Up Debug ,然后关闭 IDE,拔掉开发板/调试器,重新连接后再尝试 Debug。 mayliu1_0-1785219755566.png 请先按以上步骤排查。 Best  Regards May
查看全文
asoc-simple-card: parse error after upgrading to kernel 6.18.x Hi, here is my working DT for Kernel 6.6.52: / { codec: max98357a@0{ compatible = "maxim,max98357a"; #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&sdmode_en>; sdmode-gpios = <&gpio4 28 GPIO_ACTIVE_HIGH>; status = "okay"; }; sound { compatible = "simple-audio-card"; simple-audio-card,name = "SAI3 MAX98357A"; simple-audio-card,format = "i2s"; simple-audio-card,widgets = "Speaker","Speakers"; simple-audio-card,routing = "Speakers","Speaker"; simple-audio-card,bitclock-master = <&cpu_dai>; simple-audio-card,frame-master = <&cpu_dai>; cpu_dai: simple-audio-card,cpu { sound-dai = <&sai3>; clocks = <&clk IMX8MP_CLK_SAI3>; clock-names = "mclk"; //system-clock-frequency = <&clk IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>; dai-tdm-slot-num = <2>; dai-tdm-slot-width = <32>; }; codec_dai: simple-audio-card,codec { sound-dai = <&codec>; //clocks = <&clk IMX8MP_CLK_SAI3>; }; }; }; &sai3{ pinctrl-names = "default"; pinctrl-0 = <&pinctrl_sai3>; #sound-dai-cells = <0>; clocks = <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_IPG>, <&clk IMX8MP_CLK_DUMMY>, <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>, <&clk IMX8MP_CLK_DUMMY>, <&clk IMX8MP_CLK_DUMMY>, <&clk IMX8MP_AUDIO_PLL1_OUT>, <&clk IMX8MP_AUDIO_PLL2_OUT>; clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3", "pll8k", "pll11k"; assigned-clocks = <&clk IMX8MP_CLK_SAI3>, <&clk IMX8MP_AUDIO_PLL1>, <&clk IMX8MP_AUDIO_PLL2>; assigned-clock-parents = <&clk IMX8MP_AUDIO_PLL2_OUT>, <&clk IMX8MP_AUDIO_PLL1_OUT>; // Try common MCLK rates that divide well to 48 kHz multiples // Option A: 24.576 MHz (very common for MAX98357A + 48 kHz) assigned-clock-rates = <24576000>, // PLL2 for 48 kHz <22579200>; // PLL1 for 44.1 kHz // Option B (if 44.1 kHz needed later): use PLL1 + 22579200 //assigned-clock-rates = <22579200>; fsl,sai-asynchronous; fsl,sai-mclk-direction-output; status = "okay"; }; After moving to kernel 6.18.20 SAI3 is not probing and I got no sound-card. The boot log shows: platform sound: deferred probe pending: asoc-simple-card: parse error What changes in the DT syntax from kernel 6.6.52 to 6.18.x? I didn't find anything relevant. How can I investigate the parse error? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux Yocto Project Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x Hello, Could you please share your dmesg log? Best regards. Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x Hi Jorge, dmesg log and running device tree (./dtc -I fs -O dts /proc/device-tree > /tmp/running.dts) attached. Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x Hi, I have moved one step forward. After enabling the kernel configuration option CONFIG_IMX_AIPSTZ=y, the sound card device is now available. Because  sai3 node is a sub node of aips5 I also had to enable aips5 in my devicetree: &aips5 { status = "okay"; }; Now I got the following error messages: [ 13.081746] fsl-sai 30c30000.sai: ASoC error (-110): at snd_soc_dai_hw_params() on sai-tx-rx [ 13.090223] sai-tx-rx-HiFi: ASoC error (-110): at __soc_pcm_hw_params() on sai-tx-rx-HiFi speaker-test -c 2 -r 48000 -t sine 2>&1 | head -20 [ 31.368187] fsl-sai 30c30000.sai: ASoC error (-110): at snd_soc_dai_hw_params() on sai-tx-rx [ 31.376682] sai-tx-rx-HiFi: ASoC error (-110): at __soc_pcm_hw_params() on sai-tx-rx-HiFi Unable to set hw params for playback: Connection timed out speaker-test 1.2.11 Playback device is default Stream parameters are 48000Hz, S16_LE, 2 channels Sine wave rate is 440.0000Hz Rate set to 48000Hz (requested 48000Hz) Buffer size range from 24 to 131072 Period size range from 12 to 16383 Periods = 4 Setting of hwparams failed: Connection timed out Re: asoc-simple-card: parse error after upgrading to kernel 6.18.x I got it, sound is working. My kernel configs: CONFIG_SND_IMX_SOC=m CONFIG_SND_IMX_SOC=m CONFIG_SND_SOC_FSL_SAI=m CONFIG_SND_SOC_FSL_UTILS=m CONFIG_IMX_AIPSTZ=y The devicetree part: /{ codec: max98357a@0{ compatible = "maxim,max98357a"; #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&sdmode_en>; sdmode-gpios = <&gpio4 28 GPIO_ACTIVE_HIGH>; status = "okay"; }; sound { compatible = "simple-audio-card"; status = "okay"; simple-audio-card,name = "SAI3 MAX98357A"; simple-audio-card,format = "i2s"; simple-audio-card,widgets = "Speaker", "Speaker Ext"; simple-audio-card,routing = "Speaker Ext", "Speaker"; simple-audio-card,bitclock-master = <&cpu_dai>; simple-audio-card,frame-master = <&cpu_dai>; cpu_dai: simple-audio-card,cpu { sound-dai = <&sai3>; clocks = <&clk IMX8MP_CLK_SAI3>; clock-names = "mclk"; //system-clock-frequency = <&clk IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>; dai-tdm-slot-num = <2>; dai-tdm-slot-width = <32>; }; codec_dai: simple-audio-card,codec { sound-dai = <&codec>; }; }; }; &sdma2 { status = "okay"; fsl,sdma-ram-script-name = "imx/sdma/sdma-imx7d.bin"; }; &aips5 { status = "okay"; }; &audio_blk_ctrl { status = "okay"; assigned-clocks = <&clk IMX8MP_AUDIO_PLL1>, <&clk IMX8MP_AUDIO_PLL2>; assigned-clock-rates = <393216000>, <361267200>; }; &sai3{ pinctrl-names = "default"; pinctrl-0 = <&pinctrl_sai3>; #sound-dai-cells = <0>; assigned-clocks = <&clk IMX8MP_CLK_SAI3>; assigned-clock-parents = <&clk IMX8MP_AUDIO_PLL1_OUT>; assigned-clock-rates = <12288000>; clocks = <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_IPG>, <&clk IMX8MP_CLK_DUMMY>, <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>, <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK2>, <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK3>; clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3"; dmas = <&sdma2 4 2 0>, <&sdma2 5 2 0>; dma-names = "rx", "tx"; fsl,sai-asynchronous; fsl,sai-mclk-direction-output; status = "okay"; }; The devicetree base is imx8mp.dtsi
查看全文
i.MX8QMマルチディスプレイセットアップでのAAOS 15ユーザースイッチクラッシュ こんにちは、チームの皆さん、 私たちは Android オートモーティブ OS 15(AAOS 15) を i.MX8QuadMax ボード 上で マルチ ディスプレイ 構成( メイン ディスプレイ + 乗客 ディスプレイ)で動かしています。 ユーザー 切り替え 時に デフォルトの Car Launcher に 問題 が発生しています: システムは 正常に 起動し 、 ランチャー は メインディスプレイ と 助手席側 ディスプレイの 両方 に 表示され ます 。 現在の ユーザー から 新規ユーザー や ゲスト ユーザーに 切り替え ると 、 メイン ディスプレイ と 乗客 用ディスプレイ の両方 が クラッシュ し、 使用不能 になります 。 The issue is consistently reproducible after ユーザー switching. 私たちは 以下のこと を 知り たい のです 。 i.MX8QM マルチ ディスプレイ システム での AAOS 15 での ユーザー スイッチ ングに関する 既知 の問題 はありますか? Are there any additional configurations required for passenger display handling during user スイッチ? この 問題 を さらに 分析する ために、 どのような ログ や デバッグ 情報 を 収集 す べきでしょうか ? 何かご提案やアドバイスがあれば、ぜひお聞かせください。 ありがとうございます。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup こんにちは、 @AldoG さん。 ご説明ありがとうございます。   弊社で は、 NXP BSPを搭載したNXP i.MX8QM MEK ボード を 使用 し ています 。この 問題 は Android オートモーティブに関連しているため、 AAOS関連 の適切な サポート チャネル や フォーラム を 教え ていただければ 幸いです 質問はありますか? ありがとうございます。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup こんにちは、 NXP MEKボードを使用していますか? もしそうなら、NXP BSPを使っていますか? なお、当サイトはAndroid オートモーティブをサポートしていませんが、BSPリリースで問題が発生した場合は支援が可能です。 よろしくお願いいたします。 アルド。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup こんにちは、 @AldoG さん。 ご 回答 ありがとうござい ます 。完全 な ログキャット、 再現 手順、 および マルチディスプレイを実現するために行った変更点 を添付し まし た 。 再現手順: センター ディスプレイ と 助手席 ディスプレイ を有効にした 状態で、 i.MX8QM 上で AAOS 15 を起動します 。 Open ユーザー Settings on the passenger display. 乗客ディスプレイで 新しいユーザー/ゲストユーザーにスイッチすることもできます。 ユーザー 切り替え 時、 com.android.car.carlauncher は 以下の動作で クラッシュします:   android.view.WindowManager$InvalidDisplayException: ウィンドウを追加できない場合――指定された表示が見つからない ログを見る限り、CarLauncher はユーザー切り替え 後に 使 えな くなった ディスプレイや 無効 な 表示 マッピングで再開しようとしているようです 。 CAN you please advise: これは i.MX8QM の AAOS 15 マルチ ユーザー/マルチディスプレイ シナリオ で 既知 の問題 な のでしょうか? ユーザー 切り替え 時に ディスプレイ を 割り当て る のは どの コンポーネント(OccupantZone、 CarUserService、 TaskDisplayArea、 または WindowManager)ですか? 二次 ディスプレイ での ランチャー 起動 に関する MUMD(マルチユーザー マルチディスプレイ) サポート に関する 既知 の 要件 や パッチ はありますか? Is there any recommended debug information we should collect to identify why the display becomes invalid after the user スイッチ?
查看全文
S32G274 觉醒异常 您好,NXP团队: 项目背景: 我们有两个 S32G274 芯片放置在同一块板上,分别称为芯片 1 和芯片 2。芯片 2 是芯片 1 的备份——也就是说,当芯片 1 发生故障时,芯片 2 将接管其功能。 问题描述: 两个 S32G 芯片均按照指令进入睡眠状态:MCU 进入待机状态,PMIC 进入待机状态。它们可以通过 CAN 或 KL15 唤醒。在一次测试中,我们发现芯片 1 正常唤醒并正常工作,但芯片 2 无法正常工作。 通过测量 PMIC 电压,我们发现 PMIC 输出 3.3V、1.8V、1.1V 和 5V,因此 PMIC 供电电压正常。但是,芯片 2 的串口没有输出,这意味着它还没有进入 A 核心。当时我们怀疑它卡在了引导加载程序阶段。 然后我们测量了芯片温度:芯片 1 为 50°C,而芯片 2 为 40°C。为了确定芯片 2 卡在哪里,我们通过切断主电源并重新接通电源来恢复芯片 2,并进行了以下测试: 停止芯片2 while(1) 加载 A 核时出现循环——芯片温度为 45°C。 停止芯片2 while(1) 时钟初始化前的循环——芯片温度为 42°C。 通过不断短接复位引脚,使芯片 2 始终处于复位状态——芯片温度为 40°C,与故障期间观察到的温度相符。 问题概述: 我们怀疑芯片 2 的唤醒功能运行异常,导致芯片 2 一直处于复位状态。然而,确切的根本原因仍不清楚。 请您协助我们分析可能的原因,并就如何进一步调试此问题提供建议? 期待你的答复。 此致敬礼,陈寅 Re: S32G274 Wake-up abnormality 嗨,乔伊, 感谢您的及时回复。以下是我们针对您问题的解答: 问题 1:Chip2 无法唤醒的问题是概率非常低的问题。我们已经运行了近一年,只遇到过这一个案例,因此很难重现。 问题 2:芯片 1 和芯片 2 都是通过 CAN 消息唤醒的。Chip1 和 Chip2 的代码逻辑是一致的,可能的区别仅在于主要逻辑执行和故障转移处理部分。 问题 3:备用输入流程如下: M 核通过 IPCF 通知 A 核。 A核心执行关机程序。 A 核心向 PMIC 发送命令,使其进入待机状态。 M核心进入待机模式。 如果您需要任何其他信息或日志以供进一步分析,请告知我们。 期待你的答复。 此致 Re: S32G274 Wake-up abnormality 你好,Jerry_cao 请问您能否提供更多信息? 1.Chip 2 无法唤醒的现象只出现在你的作品中。可以重现吗? 2. 芯片 1 和芯片 2 是否通过 KL15 同时觉醒? 3. 你们的待机和唤醒流程是什么?M核心和A核心都参与其中吗?M 核心是否先关闭 A 核心,然后 M 核心进入待机状态? BR 乔伊 Re: S32G274 Wake-up abnormality 你好, Jerry_cao 感谢您的回复和详细信息。 1.关于 Chip2 无法唤醒的情况,M 核心是否已唤醒,A 核心是否有任何日志?是否获得了任何关于芯片的有用信息? 2.故障是否在芯片的正常工作范围内? 3. 只有这一块电路板存在这个问题吗?其他主板也有这个问题吗?温度测试可能不足以分析问题所在。它建议您尝试实施自动化测试方法,看看是否可以再次重现该问题。 BR 乔伊 Re: S32G274 Wake-up abnormality 嗨,乔伊, 感谢您一直以来的支持。 经过进一步调查,我们找到了根本原因:问题与外部看门狗(GPT 驱动程序)的喂食操作有关。 目前的研究结果: 如果在代码的开头就禁用外部看门狗,则待机状态和唤醒状态都能正常工作,没有任何问题。 如果仅在进入待机状态之前禁用外部看门狗(而它在主逻辑期间正常运行),则问题仍然会重现。 这表明看门狗喂食操作干扰了待机进入时间。我们目前的假设是,发送到 PMIC 以进入待机状态的命令可能会受到看门狗馈电操作的干扰,从而导致时序违例,阻止设备正确进入待机状态。 问题: 请问您能否帮忙分析一下看门狗喂食操作(GPT 驱动程序)是否会影响 PMIC 待机进入命令的时序? PMIC 待机进入命令是否有特定的顺序或时序要求需要遵循? S32G 平台上的看门狗外设和 PMIC 待机进入序列之间是否存在已知的时序限制? 期待你的答复。 此致 Re: S32G274 Wake-up abnormality 你好,Jerry_cao 您的意思是,您怀疑 Chip2 SoC 已进入待机模式,但 PMIC 未能正确进入待机模式,因此导致无法唤醒吗? 我会帮您查看待机命令和看门狗是否存在时间或顺序限制,如有任何进展,我会回复您。 另外,您还可以参考 AN12880 查看相关信息。 https://www.nxp.com.cn/webapp/Download?colCode=AN12880&lang_cd=zh BR 乔伊
查看全文