Developing embedded applications for NXP microcontrollers—especially platforms like the S32K series—involves using tools such as MATLAB/Simulink (MBDT – Model-Based Design Toolbox), S32 Design Studio (S32DS), and EB tresos. This article walks through the key steps involved in creating a new model and configuring it properly for NXP hardware, focusing on a practical workflow used in automotive and embedded systems projects.
Before starting, ensure the following tools are installed and correctly configured:
In addition to having the required tools installed, it is important to ensure that all components are properly integrated and compatible with each other. This includes matching the MATLAB/Simulink version with the supported release of the NXP MBDT, as well as aligning the RTD package with the selected microcontroller and AUTOSAR version. Environment variables, compiler paths, and licensing (for MATLAB, Simulink, and EB tresos) should also be verified prior to starting development.
From a hardware perspective, make sure that the evaluation board or target ECU is correctly powered and that the debug interface (such as PEMicro) is functioning. Installing the appropriate USB drivers and checking connection through debug tools can prevent communication issues later in the workflow.
Finally, it is recommended to validate the toolchain setup by running a simple example, such as a GPIO toggle or LED blink application, either directly in S32DS or through an existing Simulink example provided by MBDT. This step helps confirm that code generation, compilation, flashing, and execution on the target hardware are all working correctly before moving on to a more complex development.
Step 1: Launch Simulink
simulink in the command windowStep 2: Save the Model
s32k344_led_blink.mdlStep 3: Open Model Configuration Parameters
Ctrl + E) → Hardware ImplementationStep 4: Select Hardware Board
Step 5: Select a Configuration Template
If the board is not visible, ensure MBDT is properly installed.
Using the Library Browser, configure hardware peripherals.
Step 6: Configure GPIO for LED
Dio_FlipChannelDioLed0Step 7: Add Level Variable
This will blink an LED because the Dio_FlipChannel function toggles the logical state of the selected GPIO pin every time it is executed. By connecting it to a Data Store Write, you are effectively allowing the system to store or propagate the updated state within the model. The blinking frequency is directly controlled by the task rate of your model, which makes it easy to adjust the LED behavior simply by changing the sample time, without modifying the core logic.
In the Library Browser you will find numerous example projects that may be helpful (for example, s32k3xx_dio_s32ct).
Step 8: Generate Code
Click Build Model (Ctrl + B)
Sebastian13_5-1784719707916.png
When you press the build button, Simulink automatically translates your model into C code and prepares it for execution on the target microcontroller. The generated files can be found in the project folder, where you can explore how each block was converted into embedded code. After generation, the toolchain creates an executable file and attempts to deploy it directly to the target board.
Step 9: Connect Target Board
Step 10: Deploy
Creating a new model and configuring it for NXP hardware involves:
This workflow enables rapid prototyping and production-ready embedded development, especially in automotive systems leveraging AUTOSAR and NXP platforms.
Developing embedded applications for NXP microcontrollers—especially platforms like the S32K series—often involves using tools such as MATLAB/Simulink (MBDT – Model-Based Design Toolbox), S32 Design Studio (S32DS), and AUTOSAR tools like EB tresos. This article walks through the key steps involved in creating a new model and configuring it properly for NXP hardware, focusing on a practical workflow used in automotive and embedded systems projects.