imx8qxp H265 sample video play I am trying to play the h265 video file and it is not playing. IMX8QXP - Scarthgap - L 6.6.52 Can you please check and provide the right command or packages/lib to play h265 video sample files, gst-launch-1.0 -v filesrc location=/root/sample.h265 ! h265parse ! v4l2h265dec ! imxvideoconvert_g2d ! fpsdisplaysink video-sink=waylandsink text-overlay=false sync=false & i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus Re: imx8qxp H265 sample video play Hi, Please find the update, root@imx8qxpc0mek:~# root@imx8qxpc0mek:~# gst-launch-1.0 -v filesrc location=/navigation/aa_video_dump.h265 ! h265parse ! v4l2h265dec ! imxvideoconvert_g2d ! fpsdisplaysink video-sink=waylandsink text-overlay=false sync=false Setting pipeline to PAUSED ... ====== V4L2DEC: 1.24.7 build on Oct 23 2024 09:43:13. ====== Pipeline is PREROLLING ... /GstPipeline:pipeline0/GstFPSDisplaySink:fpsdisplaysink0/GstWaylandSink:waylandsink0: sync = false Redistribute latency... /GstPipeline:pipeline0/GstH265Parse:h265parse0.GstPad:src: caps = video/x-h265, width=(int)1280, height=(int)720, framerate=(fraction)30/1, chroma-format=(string)4:2:0, bit-depth-luma=(uint)8, bit-depth-chroma=(uint)8, parsed=(boolean)true, stream-format=(string)byte-stream, alignment=(string)au, pixel-aspect-ratio=(fraction)1/1, profile=(string)main, tier=(string)high, level=(string)4 /GstPipeline:pipeline0/v4l2h265dec:v4l2h265dec0.GstPad:sink: caps = video/x-h265, width=(int)1280, height=(int)720, framerate=(fraction)30/1, chroma-format=(string)4:2:0, bit-depth-luma=(uint)8, bit-depth-chroma=(uint)8, parsed=(boolean)true, stream-format=(string)byte-stream, alignment=(string)au, pixel-aspect-ratio=(fraction)1/1, profile=(string)main, tier=(string)high, level=(string)4 /GstPipeline:pipeline0/v4l2h265dec:v4l2h265dec0.GstPad:src: caps = video/x-raw, format=(string)NV12_8L128, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)bt709, framerate=(fraction)30/1 /GstPipeline:pipeline0/imxvideoconvert_g2d:imxvideoconvert_g2d0.GstPad:src: caps = video/x-raw, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction)30/1, format=(string)YUY2 /GstPipeline:pipeline0/GstFPSDisplaySink:fpsdisplaysink0.GstGhostPad:sink.GstProxyPad:proxypad0: caps = video/x-raw, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction)30/1, format=(string)YUY2 /GstPipeline:pipeline0/GstFPSDisplaySink:fpsdisplaysink0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction)30/1, format=(string)YUY2 /GstPipeline:pipeline0/GstFPSDisplaySink:fpsdisplaysink0.GstGhostPad:sink: caps = video/x-raw, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction)30/1, format=(string)YUY2 /GstPipeline:pipeline0/imxvideoconvert_g2d:imxvideoconvert_g2d0.GstPad:sink: caps = video/x-raw, format=(string)NV12_8L128, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)bt709, framerate=(fraction)30/1 Redistribute latency... root@imx8qxpc0mek:~# gst-inspect-1.0 | grep -i h265 codectimestamper: h265timestamper: H.265 timestamper rtp: rtph265depay: RTP H265 depayloader rtp: rtph265pay: RTP H265 payloader typefindfunctions: video/x-h265: h265, x265, 265 video4linux2: v4l2h265dec: V4L2 H265 Decoder videoparsersbad: h265parse: H.265 parser root@imx8qxpc0mek:~# root@imx8qxpc0mek:~# root@imx8qxpc0mek:~# gst-inspect-1.0 | grep -i v4l2 video4linux2: v4l2deviceprovider (GstDeviceProviderFactory) video4linux2: v4l2h263dec: V4L2 H263 Decoder video4linux2: v4l2h264dec: V4L2 H264 Decoder video4linux2: v4l2h264enc: V4L2 H.264 Encoder video4linux2: v4l2h265dec: V4L2 H265 Decoder video4linux2: v4l2mpeg2dec: V4L2 MPEG2 Decoder video4linux2: v4l2mpeg4dec: V4L2 MPEG4 Decoder video4linux2: v4l2radio: Radio (video4linux2) Tuner video4linux2: v4l2sink: Video (video4linux2) Sink video4linux2: v4l2spkdec: V4L2 SPK Decoder video4linux2: v4l2src: Video (video4linux2) Source video4linux2: v4l2vc1dec: V4L2 VC1 Decoder video4linux2: v4l2vp8dec: V4L2 VP8 Decoder video4linux2: v4l2xviddec: V4L2 XVID Decoder root@imx8qxpc0mek:~# root@imx8qxpc0mek:~# Re: imx8qxp H265 sample video play Hello,
Since you are using Scarthgap (6.6.52), the issues could be:
v4l2h265dec not present in the image. The H.265 file is not a raw elementary stream. VPU firmware/driver not loaded. The BSP uses a different decoder element than the one specified in the pipeline.
Please provide the output of:
Shell gst-inspect-1.0 | grep -i h265 gst-inspect-1.0 | grep -i v4l2 ``
and the exact error message from gst-launch-1.0 to try to identify if one of these four cases is occurring. Re: imx8qxp H265 sample video play Hello,
The log shows that H.265 decoding and GStreamer negotiation are working:
h265parse detected a valid 1280×720 H.265 Main stream. v4l2h265dec produced decoded NV12_8L128 frames. imxvideoconvert_g2d converted them to YUY2. waylandsink accepted the caps.
This is not a missing H.265 package issue.
Try the following command and allow it to run without & so errors and pipeline state remain visible in the terminal:
gst-launch-1.0 -v filesrc location=/root/sample.h265 ! h265parse ! \ v4l2h265dec ! imxvideoconvert_g2d ! waylandsink sync=false Re: imx8qxp H265 sample video play Hi, Thank you for update. I executed following command but not working root@imx8qxpc0mek:~# gst-launch-1.0 -v filesrc location=/root/sample.h265 ! h265parse ! v4l2h265dec ! imxvideoconvert_g2d ! waylandsink sync=false Setting pipeline to PAUSED ... ====== V4L2DEC: 1.24.7 build on Oct 23 2024 09:43:13. ====== Pipeline is PREROLLING ... Redistribute latency... /GstPipeline:pipeline0/GstH265Parse:h265parse0.GstPad:src: caps = video/x-h265, width=(int)1280, height=(int)720, framerate=(fraction)30/1, chroma-format=(string)4:2:0, bit-depth-luma=(uint)8, bit-depth-chroma=(uint)8, parsed=(boolean)true, stream-format=(string)byte-stream, alignment=(string)au, pixel-aspect-ratio=(fraction)1/1, profile=(string)main, tier=(string)high, level=(string)4 /GstPipeline:pipeline0/v4l2h265dec:v4l2h265dec0.GstPad:sink: caps = video/x-h265, width=(int)1280, height=(int)720, framerate=(fraction)30/1, chroma-format=(string)4:2:0, bit-depth-luma=(uint)8, bit-depth-chroma=(uint)8, parsed=(boolean)true, stream-format=(string)byte-stream, alignment=(string)au, pixel-aspect-ratio=(fraction)1/1, profile=(string)main, tier=(string)high, level=(string)4 /GstPipeline:pipeline0/v4l2h265dec:v4l2h265dec0.GstPad:src: caps = video/x-raw, format=(string)NV12_8L128, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)bt709, framerate=(fraction)30/1 /GstPipeline:pipeline0/imxvideoconvert_g2d:imxvideoconvert_g2d0.GstPad:src: caps = video/x-raw, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction)30/1, format=(string)YUY2 /GstPipeline:pipeline0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction)30/1, format=(string)YUY2 /GstPipeline:pipeline0/imxvideoconvert_g2d:imxvideoconvert_g2d0.GstPad:sink: caps = video/x-raw, format=(string)NV12_8L128, width=(int)1280, height=(int)720, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flipped/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)bt709, framerate=(fraction)30/1 Redistribute latency... As well as one more command is working fine but, video playing is very slow. root@imx8qxpc0mek:~# gst-launch-1.0 filesrc location=/root/sample.h265 ! h265parse ! avdec_h265 max-threads=4 ! videoconvert ! video/x-raw,format=I420 ! waylandsink sync=false Setting pipeline to PAUSED ... Pipeline is PREROLLING ... Redistribute latency... Redistribute latency... Pipeline is PREROLLED ... Setting pipeline to PLAYING ... Redistribute latency... New clock: GstSystemClock 0:00:00.0 / 99:99:99. 0:00:00.0 / 99:99:99. 0:00:00.0 / 99:99:99. 0:00:00.0 / 99:99:99. 0:00:00.0 / 99:99:99. Can you please check and provide your feedback/ fix for slowness in video playing Thanks & regards, VKS Re: imx8qxp H265 sample video play Hello,
Could you try with the latest BSP?
The H.265 decoder package is not missing, the software decoder (avdec_h265) works but is slow because decoding is being done on the Cortex-A35 CPUs, your configuration bypasses the hardware H.265 decoder, that's why you have poor performance. Re: imx8qxp H265 sample video play Thank You @Oswalag for the update. Is there any other kernel or package configuration required to be added to the build to use the H.265 decoder in proper way? Thanks & regards, VKS
查看全文