Hello NXP Community,
Note: i did the card NDEF format with an App and access bytes are showing 7F078840
Hello @Saqib1
Hope you are doing well.
Please consider that PN7150 is Not Recommended for New Designs; we recommend using PN7160 instead. Additionally, MIFARE Classic is also Not Recommended for New Designs; MIFARE DESFire Light can be considered.
Before sending the write command make sure the authentication with Key A (FFFFFFFFFFFFh) on block 1Fh (Sector 7 trailer) is performed successfully.
Now, after authentication on block 1Fh, please verify that the write command is being sent following the procedure described in the MIFARE Classic EV1 1K datasheet, section 12.3. The WRITE operation consists of two parts that must be sent sequentially:
Part 1: Send the command byte and block address, including CRC: A0 + XX +CRC where XX is the block address (e.g., 1Fh for the Sector 7 Trailer). The card must respond with ACK before proceeding.
Part 2: Only after receiving the ACK, send the 16 bytes of data including CRC: [16 bytes payload] + CRC. The card will respond with a final ACK to confirm the write was accepted.
Regards,
Eduardo.