BMS SDK dereferences NULL_PTR Hi, in the Phy 665a driver within BMS SDK, pxReqLowConfig is dereferenced, even if it is NULL_PTR (RequestQueueLow sideband not used for gateway device 0 configuration). Call stack: Level,Function,Stack Frame,Source,PC,Return Address,Stack Used
0," ","32 @ 0x2040DF00","exceptions.c:101:10",0x0060E874,"[0x2040DF18]: 0x0066D3E0",248
0,"Prv_Phy_665a_SpiPackMessageBatchInactiveSync","24 @ 0x2040DF20","CDD_Phy_665a_MsghSpi.c:2379:104",0x0066D3DE,"[0x2040DF34]: 0x0066D60A",216
0,"Prv_Phy_665a_SpiPackMessageBatch","24 @ 0x2040DF38","CDD_Phy_665a_MsghSpi.c:2551:18",0x0066D606,"[0x2040DF4C]: 0x0066DA8A",192
0,"Prv_Phy_665a_IO_SendMessageSpi","24 @ 0x2040DF50","CDD_Phy_665a_MsghSpi.c:3231:26",0x0066DA86,"[0x2040DF64]: 0x00666D34",168
0,"Phy_665a_IO_SendMessage","40 @ 0x2040DF68","CDD_Phy_665a.c:2037:30",0x00666D30,"[0x2040DF8C]: 0x0066E7FC",144
0,"Bms_TD_Send","24 @ 0x2040DF90","CDD_Bms_common.c:353:22",0x0066E7F8,"[0x2040DFA4]: 0x005D54E6",104 Version Information: * Project : BMS GEN2 SDK AUTOSAR 4.7
* Platform : CORTEXM
* Peripheral :
* Dependencies :
*
* Autosar Version : 4.7.0
* Autosar Revision : ASR_REL_4_7_REV_0000
* Autosar Conf.Variant :
* SW Version : 0.9.1
* Build Version : S32K3_BMS_GEN2_SDK_0_9_1_D2601_ASR_REL_4_7_REV_0000_20260120 S32 SDK for S32K1 Re: BMS SDK dereferences NULL_PTR Hello PhilippH
Could you please provide more details on the part numbers you are using? I’d like to check the drivers, and it would also be helpful if you could share the file.
I will be waiting for your response
Have a great day and best of luck.
查看全文