2416850_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2416850_en-US

2416850_en-US

Where are Bluetooth Channel Sounding Examples for the KW47-EVK board

Where are Bluetooth Channel Sounding Examples for the KW47-EVK board with the daughter card (KW47-001-M10)? 

I've looked in the repos at https://github.com/nxp-mcuxpresso/ but cannot find any specific examples for the KW47-EVK board. I've also found a Channel Sounding example for the FRDM-MCXW72 FRDM-MCXW72: Hands-On 8: Channel Sounding FRDM to Phone. 

I also used the NXP AI help, but it came up with links that did not exist.

I have the Eclipse based MCUXpresso installed along with the SDKs for the KW47-EVK board with the daughter card (KW47-001-M10).

Thanks in advance! --Paul



Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board

Hello,


Hope you are doing well. Thanks for reaching out. To access the Channel Sounding examples for the KW47-EVK, the recommended approach is to use the MCUXpresso for VS Code extension along with the MCUXpresso SDK GitHub repository, rather than browsing the repos manually.

Here are the steps:

  • Install the MCUXpresso for VS Code extension Download and install it from the VS Code Marketplace or from the NXP page: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...
  • Import the SDK from the repository In VS Code, open the MCUXpresso Quickstart Panel, click "Import example from Repository", and select the KW47-EVK board. The extension will pull the SDK directly from the GitHub repository.
  • Use SDK version 26.06.00 (LTS) We recommend using SDK version 26.06.00, which is the current LTS release and includes the latest BLE stack updates for the KW47, including Channel Sounding support.
 

Ricardo_Zamora_1-1790704324680.png


Specifically, I would recommend checking this documentation: Running the Bluetooth Low Energy Localization Scenario — MCUXpresso SDK Documentation



Hope this helps!


Best Regards,

Ricardo

Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board

Thanks Ricardo! That worked and I was able to import the mcxw72evk_loc_reader_bm using the Visual Studio Code Extension.

Tags (1)
No ratings
Version history
Last update:
59m ago
Updated by: