Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
如何升级AT&T的问题? 遇到始终无法解决的 AT&T 问题?请联系 AT&T 升级支持团队。 Re: How to escalate a problem with AT&T? 你好,苏哈尼, 感谢您的联系,但看起来您的帖子可能发错社区了。本论坛致力于讨论恩智浦半导体 (NXP) 的 MPC5xxx 微控制器及相关技术话题。 如需AT&T支持或升级问题,我建议您直接联系他们: AT&T 商业支持: https://www.att.com/support/ AT&T 升级投诉热线:可通过您的账户门户或致电 AT&T 客户服务中心获取。 我方将结案。希望你的问题能尽快解决! 此致, 彼得
記事全体を表示
S32K5 supports various peripheral parameters I'd like to know which peripherals the S32K5 supports, and how many ports each peripheral has. Re: S32K5支持的各项外设参数 Hello @TAlice, All of the currently available information is provided in the K5's product page: S32K5 Auto General-Purpose MCUs | NXP Semiconductors. When S32K5 is publicly launched, specific peripheral information will be available. If you require further details, please contact your NXP distributor or assigned sales. Best regards, Julián
記事全体を表示
LX2080A Linux 开发支持 – Yocto 和 Buildroot 你好, 我正在使用 NXP LX2080A 平台,并希望开发一个嵌入式 Linux 系统。 我想了解恩智浦为LX2080A提供的Linux开发支持。 Yocto是否获得官方支持?如果可以,我可以在哪里找到 NXP Yocto 电路板支持包。/层? Buildroot 是否正式支持 LX2080A? NXP是否有推荐的用于Linux开发的BSP/SDK? 请分享相关文档、源代码库或指南。 谢谢! Re: LX2080A Linux Development Support – Yocto and Buildroot 请参阅https://www.nxp.com/webapp/Download?colCode=LX2160ARDBGSG ,第 11 页。 通过将 SW3[1:3] 从 111 改为 110,该板将作为 LX2080A 平台启动。 任何所需的 RCW、ATF 或其他软件修改将取决于您的具体硬件设计,并且可能与参考 LX2160ARDB 实现有所不同。 谢谢。 Re: LX2080A Linux Development Support – Yocto and Buildroot 你好, 谢谢你提供的信息。 我想澄清一下关于LX2080A的一点。 如果我们使用 LX2160A-RDB 软件和参考配置在 LX2080A 上启用 Linux,是否需要对 RCW(重置配置字)或 ATF(TF-A)配置进行任何更改以支持 LX2080A? 具体来说,LX2160A-RDB 使用的 RCW 和 ATF 配置是否可以用于 LX2080A,还是需要对 LX2080A 进行修改? 谢谢。 Re: LX2080A Linux Development Support – Yocto and Buildroot LX2080A 属于 LX2 系列,而 LX2 系列普遍支持 Linux 软件。LX2160A-RDB 通常用作软件启用的参考硬件平台。 对于 Linux 开发,支持 Layerscape Yocto BSP (LDP Yocto)。源代码和图层可从以下网址获取: https://github.com/nxp-qoriq/yocto-sdk/tree/walnascar 请参考:UG10374 和 UG10381。 NXP 的官方 Linux 支持基于 Layerscape LDP / Yocto 版本。我们没有为 LX2080A 提供专用的 Buildroot 电路板支持包 版本。 Layerscape LDP 页面提供以下最新软件版本、文档和支持的设备信息: https://www.nxp.com/design/design-center/software/embedded-software/cross-platform-embedded/layerscape-linux-distribution-poc:LAYERSCAPE-SDK 谢谢!
記事全体を表示
How to escalate a problem with AT&T? Facing an AT&T problem that keeps going unresolved? AT&T Escalation Support Team
記事全体を表示
i.NX RT 1060 PMIC_ON_REQ behavior Hello, I am designing a custom board using the MIMXRT1062CVJ5B. The power supplies are connected as shown in the attached figure. Could you please help clarify the following points regarding this configuration? (1) Does PMIC_ON_REQ go high immediately after VDD_SNVS_IN is applied, or is there any delay before it is asserted? (2) When POR_B is driven low, what is the state of PMIC_ON_REQ? Does it remain high or transition low? (3) When VDD_SNVS_IN power is removed, does PMIC_ON_REQ go low? Is the output voltage level guaranteed in this condition? (4) Does VDD_SNVS_IN have an undervoltage lockout (UVLO) function? If so, at what voltage threshold does it become active? (5) In the case shown as "Waveform - A", where only VCC_3V3 is turned off (0 V) while VDD_SNVS_IN remains powered, is this operating condition supported? In this scenario, POR_B transitions from high to low and then from low to high. Can the i.MX RT1062 boot correctly and operate normally after this sequence? Thank you for your support. i.MXRT 106x Re: i.NX RT 1060 PMIC_ON_REQ behavior Hi, PMIC_ON_REQ is associated with VDD_SNVS_IN and is a push-pull output. There is no specific reference in the documentation indicating a delay before it is asserted. You could test this on an EVK. For example, on the EVKC, you can measure PMIC_ON_REQ through R282 and VDD_SNVS_IN through J30. The documentation does not guarantee a logic-low or logic-high output state for PMIC_ON_REQ when POR_B is driven low or when VDD_SNVS_IN power is removed. You can refer to Section 21.3.3, Power Mode Transitions, of the i.MX RT1060 Processor Reference Manual for different scenarios and how PMIC_ON_REQ behaves in each case. There is no UVLO specification explicitly documented for VDD_SNVS_IN for the i.MX RT1060. The SNVS digital low-voltage detector described in the reference manual includes a mechanism to detect interruptions of the SNVS_LP power supply that could cause the LP control, status, and secure counter values to change. Regarding question 5, would these scenarios occur during power-up, power-down, or while the application code is running? Best Regards, Pablo
記事全体を表示
LX2080A Linux開発サポート – YoctoおよびBuildroot こんにちは、 私はNXPのLX2080Aプラットフォームを使っており、組み込みLinuxシステムを開発したいと考えています。 NXPが提供しているLinux開発サポートについて知りたいLX2080A。 Yoctoは公式にサポートされていますか?もしそうなら、NXP Yocto BSPやレイヤーはどこで手に入りますか? BuildrootはLX2080Aで正式にサポートされていますか? Linux開発におすすめのNXPのBSP/SDKはありますか? 関連するドキュメント、ソースリポジトリ、またはガイドを共有してください。 よろしくお願いします。 Re: LX2080A Linux Development Support – Yocto and Buildroot https://www.nxp.com/webapp/Download?colCode=LX2160ARDBGSGの11ページを参照してください。 SW3[1:3]を111から110に変更することで、ボードはLX2080Aプラットフォームとして起動します。 必要なRCW、ATF、その他のソフトウェア変更は、あなたのハードウェア設計によって異なり、リファレンスLX2160ARDB実装とは異なる場合があります。 ありがとうございます。 Re: LX2080A Linux Development Support – Yocto and Buildroot こんにちは、 情報ありがとうございます。 LX2080Aに関して、一点だけ明確にしておきたいと思います。 LX2080A上でLX2160A-RDBソフトウェアとLinuxイネーブルメントのリファレンス構成を使用する場合、LX2080AをサポートするためにRCW(リセット設定ワード)やATF(TF-A)の設定に変更が必要ですか? 具体的には、LX2160A-RDBに使われているRCWとATFの設定をLX2080Aにも使えるのか、それともLX2080A向けに変更する必要があるのか? ありがとうございます。 Re: LX2080A Linux Development Support – Yocto and Buildroot このLX2080AはLX2ファミリに属し、LinuxソフトウェアのサポートはLX2ファミリ全体で共通しています。LX2160A-RDBは通常、ソフトウェア実現のためのリファレンスハードウェアプラットフォームとして使用されます。 Linux開発にはLayerscape Yocto BSP(LDP Yocto)がサポートされています。ソースコードとレイヤーは、 https://github.com/nxp-qoriq/yocto-sdk/tree/walnascarから入手できます。 UG10374およびUG10381を参照してください。 NXPの公式LinuxイネーブルメントはLayerscapeのLDP / Yoctoリリースに基づいています。LX2080A専用のBuildroot BSPリリースは提供しておりません。 Layerscape LDPページには、最新のソフトウェアリリース、ドキュメント、サポートデバイス情報が以下に掲載されています。 https://www.nxp.com/design/design-center/software/embedded-software/cross-platform-embedded/layerscape-linux-distribution-poc:LAYERSCAPE-SDK よろしくお願いします。
記事全体を表示
如何升级AT&T的问题? 遇到始终无法解决的AT&T问题?请联系AT&T升级支持团队。
記事全体を表示
i.NX RT 1060 PMIC_ON_REQ 行为 你好, 我正在使用 MIMXRT1062CVJ5B 设计一个定制电路板。电源连接方式如图所示。 关于此配置,您能否帮忙澄清以下几点? (1)施加 VDD_SNVS_IN 后,PMIC_ON_REQ 是否立即变为高电平,还是在钳位之前会有延迟? (2)当 POR_B 被拉低时,PMIC_ON_REQ 的状态是什么?价格会保持高位还是转低? (3)当 VDD_SNVS_IN 电源被移除时,PMIC_ON_REQ 是否变为低电平?在这种情况下,输出电压等级能得到保证吗? (4)VDD_SNVS_IN 是否具有欠压锁定(UVLO)功能?如果是这样,它在多大的电压阈值下会激活? (5)在“波形 - A”所示的情况下,只有 VCC_3V3 关闭(0 V),而 VDD_SNVS_IN 保持供电,这种工作条件是否受支持? 在这种情况下,POR_B 从高到低,然后再从低到高转变。按照上述步骤操作后,i.MX RT1062 能否正常启动并正常运行? 感谢您的支持。 i.MX RT106x Re: i.NX RT 1060 PMIC_ON_REQ behavior 您好, PMIC_ON_REQ 与 VDD_SNVS_IN 相关联,并且是推挽输出。文档中没有明确说明在钳位之前会有延迟。你可以在EVK上测试一下。例如,在 EVKC 上,您可以通过 R282 测量 PMIC_ON_REQ,通过 J30 测量 VDD_SNVS_IN。 文档并未保证当 POR_B 被拉低或 VDD_SNVS_IN 电源被移除时,PMIC_ON_REQ 的输出状态为逻辑低或逻辑高。 您可以参考第 21.3.3 节,i.MX RT1060 处理器参考手册中的电源模式转换部分介绍了不同场景下的 PMIC_ON_REQ 行为,以及 PMIC_ON_REQ 在每种情况下的行为。 i.MX RT1060 的 VDD_SNVS_IN 没有明确记录的 UVLO 规范。参考手册中描述的 SNVS 数字低电压检测器包含一个机制,用于检测 SNVS_LP 电源中断,这可能会导致 LP 控制、状态和安全计数器值发生变化。 关于问题 5,这些情况会在开机、关机还是应用程序代码运行时发生? 此致, 巴勃罗
記事全体を表示
AT&Tで問題をエスカレートさせるにはどうすればよいですか? 解決されていない AT&T の問題に直面していますか? AT&T エスカレーションサポートチーム
記事全体を表示
i.NX RT 1060 PMIC_ON_REQの動作 こんにちは、 私はMIMXRT1062CVJ5Bを使用してカスタム基板を設計しています。電源は添付の図に示されているように接続されています。 この構成に関する以下の点について、教えていただけますか? (1)PMIC_ON_REQはVDD_SNVS_INが適用された直後にハイになりますか、それともアサートされるまでに遅延がありますか? (2)POR_Bがローに駆動されたとき、PMIC_ON_REQの状態はどうなりますか?高止まりするのか、それとも低迷に転じるのか? (3)VDD_SNVS_IN電源が切断されたとき、PMIC_ON_REQはローになりますか?この条件下で出力電圧レベルは保証されますか? (4)VDD_SNVS_INには低電圧ロックアウト(UVLO)機能がありますか?もしそうなら、どの電圧閾値で活性化しますか? (5) 「波形 - A」として示されている場合、VCC_3V3だけがオフ(0 V)でVDD_SNVS_INが電源を保持している場合、この動作条件はサポートされていますか? このシナリオでは、POR_Bは高から低へ、そして低から高へと変化します。この手順の後、i.MX RT1062は正常に起動し正常に動作しますか? 再開まで今しばらくお待ちください。 i.MXRT 106x Re: i.NX RT 1060 PMIC_ON_REQ behavior こんにちは、 PMIC_ON_REQはVDD_SNVS_INに関連付けられており、プッシュプル出力です。ドキュメントには、主張されるまでの遅延を示す具体的な言及はありません。EVKで試してみるのもいいでしょう。例えばEVKCでは、R282までの量PMIC_ON_REQ、J30までのVDD_SNVS_INを測定できます。 ドキュメントは、POR_Bが低電圧で駆動されたり電源が切断されたりしたときにPMIC_ON_REQの論理ロー(論理低)または論理高(logic-high)出力状態VDD_SNVS_IN保証していません。 セクション21.3.3を参照できます。i.MX RT1060プロセッサリファレンスマニュアルの電源モード移行、さまざまなシナリオとPMIC_ON_REQの挙動について。 i.MX RT1060のUVLO仕様はVDD_SNVS_INとして明示的に文書化されていません。リファレンスマニュアルに記載されているSNVSデジタル低電圧検波器には、SNVS_LP電源の遮断を検出し、LP制御、状態、セカンプカウンター値が変化する可能性のある機構が含まれています。 質問5についてですが、これらのシナリオは電源投入中、電源オフ中、それともアプリケーションコードが実行中で起こるのでしょうか? よろしくお願いします、 パブロ
記事全体を表示
PCF2123TS-1,118の外観バリエーションに関するお問い合わせ NXPチーム様:PCF2123TS-1,118チップ2リールの入荷検査中に、2種類の異なる外観タイプを発見しました。タイプ1:表面が光沢があり、ピン1のインジケータが小さく、側面のテクスチャは光沢があり、わずかに湾曲しています。タイプ2:表面が粗く、ピン1のインジケータが大きく、側面のテクスチャは粗く、直線的です。これらの違いは正常な状態でしょうか?ご回答をお待ちしております。よろしくお願いいたします。劉
記事全体を表示
KW47-EVKボードのBluetoothチャンネルサウンディング例はどこにありますか? daughterカード(KW47-001-M10)を搭載したKW47-EVKボードのBluetoothチャンネルサウンディング例はどこにありますか? https://github.com/nxp-mcuxpresso/ のリポジトリを調べましたが、KW47-EVKボードの具体的な例は見つかりませんでした。また、FRDM-MCXW72FRDM-MCXW72のチャネルサウンディングの例も見つけました:実践形式 8: チャネルサウンディング FRDMから電話への対応。   NXP AIのヘルプも利用してみましたが、存在しないリンクが表示されました。 私はEclipseベースのMCUXpressoと、d8terカード(KW47-001-M10)のKW47-EVKボード用SDKをインストールしています。 前もって感謝します!--ポール Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board こんにちは、 あなたの調子が良いといいのですが。ご連絡ありがとうございます。KW47-EVKのチャンネルサウンディング例にアクセスするには、手動でリポジトリを閲覧するのではなく、MCUXpresso for VS Code拡張機能とMCUXpresso SDKのGitHubリポジトリを併用することが推奨されます。 手順は以下の通りです。 MCUXpressoのVS Code拡張機能をダウンロードしてVS CodeマーケットプレイスまたはNXPページからインストールしてください: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code:MCUXPRESSO-VSC リポジトリからSDKをインポートしてください VS Codeで、MCUXpressoクイックスタートパネルを開き、「リポジトリからサンプルをインポート」をクリックし、KW47-EVKボードを選択します。拡張機能はGitHubリポジトリからSDKを直接取得します。 SDKバージョン26.06.00(LTS)の使用を推奨します。これは現在のLTSリリースで、KW47向けの最新のBLEスタックアップデート(チャネルサウンディングサポートを含む)を含んでいます。   具体的には、以下のドキュメントを確認することをお勧めします: Bluetooth Low Energy Localization Scenarioの実行 — MCUXpresso SDK ドキュメント お役に立てば幸いです! よろしくお願いいたします。 リカルド Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board リカルドさん、ありがとう!うまくいき、Visual Studio Code拡張機能を使用してmcxw72evk_loc_reader_bmをインポートすることができました。
記事全体を表示
如果我使用的是树莓派 Pico 2W,如何在 Arduino IDE 中查看 Serial.prints 的输出? 我花了很多时间试图弄明白这件事,但最终一无所获。我尝试运行一个简单的代码,让内置 LED 闪烁,同时在 Serial.print 中打印“hello”。LED 指示灯闪烁,但 pico 没有在串口监视器中输出任何内容。我发现 pico 在上传后会断开连接,然后重新连接,但连接的是不同的端口。我猜我的板是从 COM 5/4 重新连接到 COM 11,但是如果我尝试进入“工具”->“端口”->“COM 11”,LED 指示灯停止闪烁,IDE 显示错误信息,我的笔记本电脑发出类似板断开连接又重新连接的声音。我能做些什么吗?我考虑过从 Arduino IDE 切换到 VS Code,但是没有关于如何在 Windows 上进行切换的教程,而 GPT 也没有教会我太多东西。 Kinetis W系列MCU
記事全体を表示
How can I see the Serial.prints in Arduino IDE if I am using a raspberry pi pico 2w? I spent a lot of hours trying to figure this out and I didn't manage to do anything. I tried to run a simple code that makes the built in LED blink while also writing "hello" at Serial.print. The LED blinks, but the pico does't print anything in the serial monitor. I found out the pico disconnects after the upload and then reconnects again, but on a different port. I guess mine reconnects from com 5/4 to com 11 but if I try to go to Tools -> Port -> COM 11 the LED stops blinking, the IDE shows me an error message and my laptop makes the sound as if the board was disconnected and connected again. Is there something I can do about this? I took into consideration switching from arduino ide to vs code, but there are no tutorials on how to do that for windows and GPT didn't teach me much. Kinetis W Series MCUs
記事全体を表示
KW47-EVK板的蓝牙通道发声示例在哪里? KW47-EVK 板及其子卡 (KW47-001-M10)的蓝牙通道发声示例在哪里? 我在https://github.com/nxp-mcuxpresso/ 的仓库中查找过,但找不到任何针对 KW47-EVK 开发板的具体示例。我还找到了FRDM-MCXW72的通道探测示例:FRDM-MCXW72:动手实践 8:FRDM 到电话的通道探测。 我还使用了 NXP AI 的帮助功能,但它给出的链接并不存在。 我已经安装了基于 Eclipse 的 MCUXpresso,以及适用于 KW47-EVK 板和子卡 (KW47-001-M10) 的 SDK。 提前致谢!——保罗 Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board 你好, 希望你一切都好。感谢您的联系。要访问 KW47-EVK 的通道探测示例,建议使用 MCUXpresso for VS Code 扩展以及 MCUXpresso SDK GitHub 存储库,而不是手动浏览存储库。 步骤如下: 安装适用于 VS Code 的 MCUXpresso 扩展。您可以从 VS Code 应用商店或 NXP 页面下载并安装: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code :MCUXPRESSO-VSC 从存储库导入 SDK 在 VS Code 中,打开 MCUXpresso 快速入门面板,点击“从存储库导入示例”,然后选择 KW47-EVK 板。该扩展程序将直接从 GitHub 存储库拉取 SDK。 使用 SDK 版本 26.06.00 (LTS) 我们建议使用 SDK 版本 26.06.00,这是当前的 LTS 版本,包含 KW47 的最新 BLE 协议栈更新,包括通道探测支持。   具体来说,我建议您查看以下文档:运行低功耗蓝牙定位场景 — MCUXpresso SDK 文档 希望这能帮到你! 顺祝商祺! 里卡多 Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board 谢谢你,里卡多!这样就成功了,我可以使用 Visual Studio Code 扩展导入 mcxw72evk_loc_reader_bm。
記事全体を表示
BMS SDK dereferences NULL_PTR Hi, in the Phy 665a driver within BMS SDK, pxReqLowConfig is dereferenced, even if it is NULL_PTR (RequestQueueLow sideband not used for gateway device 0 configuration). Call stack: Level,Function,Stack Frame,Source,PC,Return Address,Stack Used 0," ","32 @ 0x2040DF00","exceptions.c:101:10",0x0060E874,"[0x2040DF18]: 0x0066D3E0",248 0,"Prv_Phy_665a_SpiPackMessageBatchInactiveSync","24 @ 0x2040DF20","CDD_Phy_665a_MsghSpi.c:2379:104",0x0066D3DE,"[0x2040DF34]: 0x0066D60A",216 0,"Prv_Phy_665a_SpiPackMessageBatch","24 @ 0x2040DF38","CDD_Phy_665a_MsghSpi.c:2551:18",0x0066D606,"[0x2040DF4C]: 0x0066DA8A",192 0,"Prv_Phy_665a_IO_SendMessageSpi","24 @ 0x2040DF50","CDD_Phy_665a_MsghSpi.c:3231:26",0x0066DA86,"[0x2040DF64]: 0x00666D34",168 0,"Phy_665a_IO_SendMessage","40 @ 0x2040DF68","CDD_Phy_665a.c:2037:30",0x00666D30,"[0x2040DF8C]: 0x0066E7FC",144 0,"Bms_TD_Send","24 @ 0x2040DF90","CDD_Bms_common.c:353:22",0x0066E7F8,"[0x2040DFA4]: 0x005D54E6",104 Version Information: * Project : BMS GEN2 SDK AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : * Dependencies : * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : 0.9.1 * Build Version : S32K3_BMS_GEN2_SDK_0_9_1_D2601_ASR_REL_4_7_REV_0000_20260120 S32 SDK for S32K1 Re: BMS SDK dereferences NULL_PTR Hello PhilippH Could you please provide more details on the part numbers you are using? I’d like to check the drivers, and it would also be helpful if you could share the file. I will be waiting for your response Have a great day and best of luck.
記事全体を表示
电池管理系统 SDK 取消引用 NULL_PTR 您好, 在 电池管理系统 SDK 中的 Phy 665a 驱动程序中,即使 pxReqLowConfig 为 NULL_PTR( RequestQueueLow 边带未用于网关设备 0 配置),也会取消引用它。 调用堆栈: Level,Function,Stack Frame,Source,PC,Return Address,Stack Used 0," ","32 @ 0x2040DF00","exceptions.c:101:10",0x0060E874,"[0x2040DF18]: 0x0066D3E0",248 0,"Prv_Phy_665a_SpiPackMessageBatchInactiveSync","24 @ 0x2040DF20","CDD_Phy_665a_MsghSpi.c:2379:104",0x0066D3DE,"[0x2040DF34]: 0x0066D60A",216 0,"Prv_Phy_665a_SpiPackMessageBatch","24 @ 0x2040DF38","CDD_Phy_665a_MsghSpi.c:2551:18",0x0066D606,"[0x2040DF4C]: 0x0066DA8A",192 0,"Prv_Phy_665a_IO_SendMessageSpi","24 @ 0x2040DF50","CDD_Phy_665a_MsghSpi.c:3231:26",0x0066DA86,"[0x2040DF64]: 0x00666D34",168 0,"Phy_665a_IO_SendMessage","40 @ 0x2040DF68","CDD_Phy_665a.c:2037:30",0x00666D30,"[0x2040DF8C]: 0x0066E7FC",144 0,"Bms_TD_Send","24 @ 0x2040DF90","CDD_Bms_common.c:353:22",0x0066E7F8,"[0x2040DFA4]: 0x005D54E6",104 版本信息: * Project : BMS GEN2 SDK AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : * Dependencies : * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : 0.9.1 * Build Version : S32K3_BMS_GEN2_SDK_0_9_1_D2601_ASR_REL_4_7_REV_0000_20260120 S32K1系列的S32SDK Re: BMS SDK dereferences NULL_PTR 你好 PhilippH 请问您能否提供更多关于您所使用零件编号的详细信息?我想检查一下驱动程序,如果您能分享一下文件就更好了。 我会等你的回复。 祝你今天过得愉快,一切顺利。
記事全体を表示
Raspberry Pi Pico 2Wを使っている場合、Arduino IDEでSerial.printsを見るにはどうすればいいですか? 何時間もかけて解決しようと試みましたが、結局何もできませんでした。内蔵LEDを点滅させながら、Serial.printに「hello」と書き込む簡単なコードを実行してみました。LEDは点滅するが、ピコはシリアルモニターに何も出力しない。アップロード後にピコが切断され、その後別のポートで再接続されることが分かりました。私のはcom 5/4からcom 11に再接続されるようですが、Tools -> Port -> COM11に行こうとするとLEDが点滅し、IDEにエラーメッセージが表示され、ノートPCは基板が外されて再接続されたかのような音を出します。これについて何かできることはありますか?Arduino IDEからVS Codeに切り替えることも考えましたが、Windows用のチュートリアルがなく、GPTもあまり教えてくれませんでした。 Kinetis Wシリーズ・マイクロコントローラ
記事全体を表示
Inquiry on PCF2123TS-1,118 Appearance Variation Dear NXP team: During incoming inspection of two reels of PCF2123TS-1,118 chips, we discovered two different appearance types: Type 1: Glossy surface, smaller pin 1 indicator; glossy and slightly curved side texture. Type 2: Rough surface, larger pin 1 indicator; rough and straight side texture. Are these differences normal? We look forward to your reply. Thank you! Sincerely, Ms. Liu
記事全体を表示
Where are Bluetooth Channel Sounding Examples for the KW47-EVK board Where are Bluetooth Channel Sounding Examples for the KW47-EVK board with the daughter card (KW47-001-M10)?  I've looked in the repos at https://github.com/nxp-mcuxpresso/ but cannot find any specific examples for the KW47-EVK board. I've also found a Channel Sounding example for the FRDM-MCXW72 FRDM-MCXW72: Hands-On 8: Channel Sounding FRDM to Phone.  I also used the NXP AI help, but it came up with links that did not exist. I have the Eclipse based MCUXpresso installed along with the SDKs for the KW47-EVK board with the daughter card (KW47-001-M10). Thanks in advance! --Paul Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board Hello, Hope you are doing well. Thanks for reaching out. To access the Channel Sounding examples for the KW47-EVK, the recommended approach is to use the MCUXpresso for VS Code extension along with the MCUXpresso SDK GitHub repository, rather than browsing the repos manually. Here are the steps: Install the MCUXpresso for VS Code extension Download and install it from the VS Code Marketplace or from the NXP page: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code:MCUXPRESSO-VSC Import the SDK from the repository In VS Code, open the MCUXpresso Quickstart Panel, click "Import example from Repository", and select the KW47-EVK board. The extension will pull the SDK directly from the GitHub repository. Use SDK version 26.06.00 (LTS) We recommend using SDK version 26.06.00, which is the current LTS release and includes the latest BLE stack updates for the KW47, including Channel Sounding support.   Specifically, I would recommend checking this documentation: Running the Bluetooth Low Energy Localization Scenario — MCUXpresso SDK Documentation Hope this helps! Best Regards, Ricardo Re: Where are Bluetooth Channel Sounding Examples for the KW47-EVK board Thanks Ricardo! That worked and I was able to import the mcxw72evk_loc_reader_bm using the Visual Studio Code Extension.
記事全体を表示