Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
MPC8313RDB board Kernel Source Hi I am trying to compile a USB driver for MPC8313 Reference Design Board.  I do not have the source code to compile the drivers on Linux. They say they have to be extracted from an .iso file (which is non existent). Is there a way to develop the driver without using the Kernel source files (some GCC switches for OS Linux & powerpc as target)? Or can somebody help me find/locate Kernel source files. If at all the kernel source is present on the CD then under what filename is this hiding? Kernel Version: 2.6.20 thanks in advance, Ak Evaluation Board Re: MPC8313RDB board Kernel Source Thanks abartky,          The steps mentioned made the process of extracting kernel files easy from the iso package and your instructions were really helpful. Thanks again, Ak Re: MPC8313RDB board Kernel Source ak79, The kernel files are in a package file, so you will not find them directly on the CD you get with the board. To get to the Kernel source files, you have to do an install of the LTIB environment and then request the kernel files to be extracted and built. When it comes to installing the LTIB environment it can be done fromt the CD or by dowloading the latest .iso file from the Freescale site. I would recommend doing the download as you will get the latest source code that way (if you really want to load from the CD, the instructions are just about the same except you need to mount the CD directly with execute privileges and run the install script from it) To find the latest BSP for the MPC8313, if you login to the Freescale site and do a keyword search at the Freescale for MPC8313 and BSP you get a link to it: https://www.freescale.com/webapp/Download?colCode=CWF-MPC8313E-RDB&location=null&fsrch=1 Fill out the form and download the file. Download that file, put it into a working directory, as root mount the .iso file CD image as an executable directory, and then as your normal Linux login, run install (example): alan@raptor:~$ ls *.iso MPC8313E_RDB_K26_20070831-LTIB.iso alan@raptor:~$ su Password: raptor:/home/alan# ls -ld cdmount drwxrwxrwx 2 alan alan 4096 2007-05-29 11:51 cdmount raptor:/home/alan# mount -o loop MPC8313E_RDB_K26_20070831-LTIB.iso cdmount raptor:/home/alan# exit exit alan@raptor:~$ alan@raptor:~$ cdmount/install Once you've done that, you need to change directory to the one you installed it in and run ltib for the first time (example) alan@raptor:~$ cd ltib-mpc8313erdb-20070824/ alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib Assuming that you've gottent the install and initial build completed, you can now ask for the Linux kernel sources to be extracted and built by; alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib --configure On the first menu that pops up, select the following two options, then exit [*] Configure the kernel [*] Leave the sources after building When the kernel config menu comes up, you can just select exit. The kernel sources will then be extracted and built, if you do this with the current version the main Linux kernel source can be found at: alan@raptor:~/ltib-mpc8313erdb-20070824$ cd rpm/BUILD/linux-2.6.20/ alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20$ alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20$ ls arch CREDITS drivers init kernel Makefile net scripts System.map vmlinux.bin.gz block crypto fs ipc lib mm README security usr COPYING Documentation include Kbuild MAINTAINERS Module.symvers REPORTING-BUGS sound vmlinux The usb drivers are under the drivers directory. alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20/drivers/usb$ ls atm class gadget image Kconfig misc net README storage built-in.o core host input Makefile mon otg serial usb-skeleton.c Hope this helps Best regards, abartky
View full article
TSM TOOL Pro 免费登录 100% 可用 2027 TSM Tool是一款基于Windows的多品牌服务软件,供移动设备维修技术人员用于设备维护。 下载 TSM 工具 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .   StarCore DSP
View full article
MPC5554 - PWM eTPU Function I want to create an interrupt for each rising edge of the PWM signal using PWM eTPU function. I have read many eTPU Application Notes and the eTPU Reference Manual, but I can't find the solution. How can I do that? What register do I need to configure or what API do I need to use?  Please guide me the solution and what document it is mentioned.   Thanks,       Re: MPC5554 - PWM eTPU Function Hi find the etpu examples in code warrior ide and  download the  bytecraft copmiler in the site given http://www.bytecraft.com/depot/depot.php.     Write micro code in byte craft compiler then it generares .h file, include the same in the main project.     Initialisation for the channels and channel paramater base address everything is given in that example..follow the same.   if { } else if { } else { }   these are entry point....   if {   contains chnnel and function initilisation..like either i/p or o/p,which tcr to be used etc.. } else if { contians incrementing period value foe the next match     } else {this is also as same as above.. }     so better to understand example given..     regards, venki Re: MPC5554 - PWM eTPU Function Thank power pc for all useful information in your posts. It's the first time I programs for eTPU. I don't have any book about programming for eTPU. I have just read eTPU_RM and Application Notes about eTPU functions and try to understand by my way. Please explain for me more about micro code entry point and m0 and m1 in your code. I see m0 and m1 is the last value and current value of the PWM signal, but how to read it from eTPU channel. According to you, what document or book are useful for me to have enough knowledge to program eTPU?   Thanks and regards,     Re: MPC5554 - PWM eTPU Function And you can also generate squre wave with linearly  increasing with time.. it is so simple just you have to increase period and it's  duty cycle periodically...if you are writing micro code on your own it is so simple insted of using  freescale code API.   regards, venki
View full article
SamFw Tool 6.2 Download Latest Version 2027 SamFW FRP Tool is a Windows utility associated with Samsung Android device servicing and troubleshooting. Download SamFW Tool . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .   StarCore DSPs
View full article
BossV による BFT Tool v1.9 全てのAndroidデバイス向け 最新[2028] BossV による BFT Tool v1.9 全てのAndroidデバイス向け 最新[2028] ダウンロードリンク . . . . . . .. . . . . . . . . . . . . . . . . . . . . . . . . .. #bft @bft
View full article
TFT MTKモジュールツールダウンロード MediaTek FRP 2027 TFT MTKモジュールツールは、MediaTek搭載のAndroidスマートフォンおよびタブレット向けに開発されたWindowsベースのモバイルサービスツールです。 ダウンロードツール . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . StarCore DSP
View full article
Power and Energy Efficiency Measurement of the MCXN947 eIQ Neutron NPU 1. Background For edge AI applications, developers typically focus on two key metrics: AI inference performance (Inference Time) Power consumption For inference performance, NXP provides the dm-mcxn947-npu-vs-tensorflm-benchmark , which compares TensorFlow Lite Micro running on the CPU with the eIQ Neutron NPU. The benchmark demonstrates the significant inference performance improvement that can be achieved by using the NPU. When it comes to power consumption, however, MCU developers often have another question: Does enabling the NPU necessarily increase power consumption? A similar analysis is provided in NXP application note AN14700 for the i.MX RT700. Although the NPU introduces a higher instantaneous current during inference, it significantly reduces inference time. As a result, the total energy consumed per inference can actually be much lower. In this article, we use the MCXN947 to perform a similar experiment. Several TensorFlow Lite Micro (TFLM) models from the MCUXpresso SDK are measured to evaluate the impact of the eIQ Neutron NPU on overall energy consumption.  2. Theoretical Analysis Current consumption is often used as a direct indicator of power consumption: Current (mA) However, for AI inference workloads, a more meaningful metric is: Energy per Inference In other words, how much energy is required to complete a single inference? The basic relationships are: Power = Voltage × Current   Energy = Power × Time   Therefore: Energy = Voltage × Current × Inference Time This means that even if the operating current increases, the total energy consumption can still decrease significantly if the inference time is reduced enough.  3. Experiment NXP provides several TFLM-based eIQ examples for the MCXN947 in the MCUXpresso SDK. For this experiment, the tflm_cifar10 demo is used as the baseline.  3.1 Test Environment Hardware FRDM-MCXN947 USB cable connected to J17 Joulescope current analyzer The current is measured at J24 on the FRDM-MCXN947 board.  Software MCUXpresso IDE eIQ Toolkit tflm_cifar10 demo from MCUXpresso SDK v26.3  3.2 Code Modifications a. Create CPU and NPU Models Following the model conversion procedure described in Sections 7.2 and 7.3 of AN14700, use the eIQ Toolkit to generate two models:   cifar10_quant.h   cifar10_npu.h   After conversion: The CPU model runs on the Cortex-M33. The NPU model is accelerated by the eIQ Neutron NPU. The two versions can be selected by modifying line 27 in model.cpp.  b. Reduce the Overall Active Power Consumption To reduce the system's active power consumption, the project can be modified based on the MCX N Power Manager AppCodeHub  example. Call lower_active_power() from low_power.cpp in main.cpp: void lower_active_power() { APP_SetVBATConfiguration(); APP_SetSPCConfiguration(); APP_SetCMCConfiguration(); /* Disable unused clocks */ CLOCK_DisableClock(kCLOCK_Rom); CLOCK_DisableClock(kCLOCK_PkcRam); CLOCK_DisableClock(kCLOCK_Gdet); CLOCK_DisableClock(kCLOCK_Pkc); CLOCK_DisableClock(kCLOCK_Css); }   This disables unused clocks and helps reduce the baseline active current.  c. Disable the NPU Clock for the CPU Baseline Test To obtain a clean CPU-only baseline, the NPU clock should also be disabled when the NPU is not being used. Define a USES_NPU macro for each model. In cifar10_quant.h: #define USES_NPU 0   In cifar10_npu.h: #define USES_NPU 1 Then modify MODEL_RunInference() so that the NPU clock is enabled only when NPU inference is performed: status_t MODEL_RunInference(void) { //If model uses NPU then turn on the NPU clock before inferencing #if (USES_NPU==1) SYSCON->AHBCLKCTRLSET[3] |= (1UL << SYSCON_AHBCLKCTRL3_NPU_SHIFT); //Turn NPU clock on to do inference using NPU #endif if (s_interpreter->Invoke() != kTfLiteOk) { PRINTF("Invoke failed!\r\n"); return kStatus_Fail; } SYSCON->AHBCLKCTRLCLR[3] |= (1UL << SYSCON_AHBCLKCTRL3_NPU_SHIFT); //Turn off NPU clock return kStatus_Success; } d. Make the Current Waveform Easier to Measure To make the different execution phases easier to distinguish in Joulescope, add the following macros to demo_config.h: #define NUM_INFERENCES 8 #define USE_DELAY 1     NUM_INFERENCES controls the number of inference iterations, while USE_DELAY adds delays between operations so that the corresponding sections can be identified more clearly in the Joulescope waveform.  e. Turn Off the NPU Clock Outside Inference To ensure that the measured current difference mainly reflects the AI inference itself, disable the NPU clock outside the actual inference period: SYSCON->AHBCLKCTRLCLR[3] |= (1UL << SYSCON_AHBCLKCTRL3_NPU_SHIFT); 3.3 Obtaining the Measurement Results a. Inference Time After running the application, the inference time can be obtained directly from the serial console output. The measured CIFAR-10 results are: CIFAR-10 CPU (150 MHz): 185.13 ms   CIFAR-10 NPU: 5.54 ms This already shows a significant reduction in execution time when the Neutron NPU is used.  b. Current Measurement Connect the Joulescope to the J24 measurement point on the FRDM-MCXN947.   Open Waveform and Multimeter from the Widgets menu in Joulescope UI to monitor and measure the current. Before taking power measurements, make sure to perform a power reset. Otherwise, the measured current may be higher than expected.  c. Calculate Energy per Inference The energy consumed for each inference can be calculated as:   Energy per Inference = Voltage × Current × Inference Time   3.4 Test Results The table below summarizes the measurements for two SDK example models. The supply voltage is assumed to be 3.3 V.   3.5 Analysis The results reveal an interesting point. Taking CIFAR-10 as an example, if we look only at current consumption, the NPU appears to consume slightly more current: CPU: 9.4 mA NPU: 10.0 mA   However, the inference time decreases dramatically: CPU: 185.13 ms NPU: 5.54 ms   As a result, the energy required for one inference decreases from 5742.7 µJ to 182.8 µJ, corresponding to a 31.4× reduction in energy consumption per inference. The same trend can be observed with the KWS model, where the NPU reduces the energy per inference by 13.7×. This behavior is consistent with the observations reported for the i.MX RT700 in AN14700.  4. Conclusion Most edge AI systems operate in an event-driven manner. The device remains in a low-power state most of the time and wakes up only when a specific event occurs to perform an AI inference. Typical examples include: Keyword spotting Environmental anomaly detection Visual detection Predictive maintenance For this type of application, looking only at the average current during inference does not provide a complete picture of the system's energy efficiency. A more meaningful metric is Energy per Inference, because it represents the total amount of energy required to complete one AI inference operation and directly affects how many inference tasks a battery-powered device can perform over its operating lifetime. The measurements in this experiment show that although the MCXN947 eIQ Neutron NPU introduces a slightly higher instantaneous operating current, it significantly reduces model execution time. As a result, the total energy consumed per inference is greatly reduced. For the CIFAR-10 and KWS models tested here, the NPU achieved more than an order-of-magnitude improvement in energy efficiency, with energy reductions of 31.4× and 13.7×, respectively. For long-running, battery-powered edge AI applications, this improvement in energy efficiency can be even more valuable than the inference performance improvement itself.  MCXN NPU|ML
View full article
SamFw Tool 6.2 最新版本下载 2027 SamFW FRP Tool 是一款与三星安卓设备维修和故障排除相关的 Windows 实用程序。 下载 SamFW 工具 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .   StarCore DSP
View full article
Ultra Unlock Tool Download Activated Version 2027 When a mobile phone gets stuck with FRP, ID, or KG locks, or faces flashing and software issues, repairing it becomes difficult for technicians. Ultra Unlock Tool v4.4.3 is a mobile servicing utility designed to handle different unlocking and repair tasks on supported devices. It offers features such as FRP, ID, and KG unlocking, code reading, firmware flashing, bootloader unlocking, certificate reading and writing, and CSC switching. This tool also supports Qualcomm, MediaTek, HiSilicon, and Unisoc chipsets across multiple mobile brands. Download Tool . . . . . .. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . PMIC for i.MX
View full article
TFT MTK模块工具下载 MediaTek FRP 2027 TFT MTK 模块工具是一款基于 Windows 的移动设备维修工具,专为搭载联发科芯片的安卓智能手机和平板电脑而开发。 下载工具 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . StarCore DSP
View full article
BossV 出品的 BFT 工具 v1.9,适用于所有安卓设备,最新版 [2028] BossV 出品的 BFT 工具 v1.9,适用于所有安卓设备,最新版 [2028] 下载链接 . . . . . . .. . . . . . . . . . . . . . . . . . . . . . . . . .. #bft @bft
View full article
三星 KG 锁 2027 版 KG Killer Tool 下载 KG Killer Tool 是一款基于 Windows 的移动设备维修工具,专为处理 KG Lock、MDM 限制和 Android 网络安全问题的移动设备维修技术人员而设计。 下载 KG Killer Tool . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . i.MX 的 PMIC
View full article
下载 Android Multi tool v1.3.5.8 最新安装包 {2027} 下载 Android Multi tool v1.3.5.8 最新安装包 {2027} . . 下载安装程序。 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .. . . . . . . . . .. . . ANDROID-AUTO @android
View full article
MPC5554 - PWM eTPU 功能 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我想使用 PWM eTPU 函数为 PWM 信号的每个上升沿创建一个中断。我阅读了许多 eTPU 应用笔记和 eTPU 参考手册,但仍然找不到解决方案。 我该怎么做?我需要配置哪个寄存器或者使用哪个API? 请指导我找到解决方案,并说明相关文档。   谢谢!       Re: MPC5554 - PWM eTPU Function <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好,请在 Code Warrior IDE 中查找 etpu 示例,并从以下网站下载 Bytecraft 编译器:http://www.bytecraft.com/depot/depot.php 。     在 字节craft 编译器中编写微代码,然后它会生成 .h 文件。文件,将其包含在主项目中。     通道初始化、通道参数基地址等所有信息都在示例中给出,请照做。   中频 { } 否则如果 { } else { }   这些是切入点……   中频 {   包含通道和函数初始化,例如输入或输出、要使用的 TCR 等。 } 否则如果 { 包含下一场比赛的递增周期值     } else {这与上面相同.. }     这样更容易理解给出的例子。     此致, 文基 Re: MPC5554 - PWM eTPU Function <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 感谢power pc在帖子中提供的所有有用信息。 这是我第一次为eTPU编程。我没有关于eTPU编程的书籍。我刚刚阅读了 eTPU_RM 和有关 eTPU 功能的应用笔记,并尝试用我自己的方式理解。 请您详细解释一下代码中的微代码入口点以及 m0 和 m1 的含义。我看到 m0 和 m1 分别是 PWM 信号的最后一个值和当前值,但是如何从 eTPU 通道读取它们呢? 您认为我应该阅读哪些文档或书籍才能获得足够的知识来编写 eTPU 程序?   感谢并致意     Re: MPC5554 - PWM eTPU Function <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你也可以生成随时间线性增加的方波。 这很简单,你只需要定期增加周期和占空比……如果你自己编写微代码,这比使用飞思卡尔代码 API 简单得多。   此致, 文基
View full article
Downlaod Android Multi tool v1.3.5.8 最新セットアップ {2027} Downlaod Android Multi tool v1.3.5.8 最新セットアップ {2027} . . セットアップをダウンロードしてください。 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .. . . . . . . . . .. . . ANDROID-車載 @android
View full article
KITPFPGMEVMEプログラマ回路図 プログラマーのKITPFPGMEVMEを使って、PMIC MMPF0100をアプリケーションボード上で直接プログラムする予定です。 プログラマー用のインターフェースをデザインするための情報が少し必要です: プログラマからのPWRON出力はオープンドレインですか?それともプッシュプル式? MMPF0100 PWRONピンにもMPUからPMIC_ON_REQピンにコネクテッドしなければならないことを考えると、どうやってインターフェースすればいいですか? プログラマーのガーバーファイルを見つけましたが、回路図はどこで見つけられますか? サポートにあらかじめ感謝いたします。 PF0100 | PF0200 Re: KITPFPGMEVME Programmer Schematic Diagram こんにちは、ミエルコ 1:PWRONが外部にプルアップする必要がある最小システム接続数が確認できます。 2: このプログラマーについての詳細は、以下にリンク先のユーザーマニュアルをご覧ください。 KITPFPGMEVME Rev B プログラマ - ユーザーガイド
View full article
MPC8313RDB 板内核源代码 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好 我正在尝试为 MPC8313 参考设计板编译 USB 驱动程序。我没有在Linux上编译驱动程序的源代码。他们说必须从 .iso 文件中提取出来。文件(不存在)。有没有办法在不使用内核源代码的情况下开发驱动程序(针对 Linux 操作系统和 powerpc 目标平台使用一些 GCC 开关)?或者有人能帮我找到内核源文件吗? 如果内核源代码确实存在于光盘上,那么它隐藏在哪个文件名下? 内核版本:2.6.20 提前致谢, 阿克 评估板 Re: MPC8313RDB board Kernel Source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 谢谢 abartky, 文中提到的步骤使得从 ISO 软件包中提取内核文件的过程变得简单,您的说明真的很有帮助。 再次感谢, 阿克 Re: MPC8313RDB board Kernel Source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ak79, 内核文件位于一个软件包文件中,因此您不会在随开发板附带的 CD 上直接找到它们。 要获取内核源文件,您必须先安装 LTIB 环境,然后请求提取和构建内核文件。 安装 LTIB 环境时,可以通过光盘安装,也可以下载最新的 .iso 文件进行安装。文件来自飞思卡尔网站。我建议下载,这样可以获得最新的源代码(如果你真的想从光盘加载,说明基本相同,只是你需要以执行权限直接挂载光盘,然后从光盘运行安装脚本)。 要查找 MPC8313 的最新电路板支持包,请登录 Freescale 网站,并在 Freescale 网站上搜索“MPC8313”和“电路板支持包”,即可获得相关链接: https://www.freescale.com/webapp/Download?colCode=CWF-MPC8313E-RDB&location=null&fsrch=1 填写表格并下载文件。 下载该文件,将其放入工作目录,然后以 root 用户身份挂载 .iso 文件。将 CD 镜像文件保存为可执行目录,然后以常规 Linux 登录身份运行 install(示例): alan@raptor:~$ ls *.iso MPC8313E_RDB_K26_20070831-LTIB.iso alan@raptor:~$ su 密码: raptor:/home/alan# ls -ld cdmount drwxrwxrwx 2 艾伦 艾伦 4096 2007-05-29 11:51 cdmount raptor:/home/alan# mount -o loop MPC8313E_RDB_K26_20070831-LTIB.iso cdmount raptor:/home/alan# 退出 exit alan@raptor:~$ alan@raptor:~$ cdmount/install 完成上述操作后,您需要切换到安装目录并首次运行 ltib(示例)。 alan@raptor:~$ cd ltib-mpc8313erdb-20070824/ alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib 假设您已经完成了安装和初始构建,现在您可以请求提取和构建 Linux 内核源代码; alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib--配置 在弹出的第一个菜单中,选择以下两个选项,然后退出。 [*] 配置内核 [*] 构建完成后保留源代码 当内核配置菜单出现时,您可以选择退出。 然后,内核源代码将被提取并构建。如果您使用当前版本执行此操作,则可以在以下位置找到主要的 Linux 内核源代码: alan@raptor:~/ltib-mpc8313erdb-20070824$ cd rpm/BUILD/linux-2.6.20/ alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/版本/linux-2.6.20$ alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/版本/linux-2.6.20$ls 架构 CREDITS 驱动程序 初始化内核 Makefile 网络脚本 System.map vmlinux.bin.gz 块加密文件系统 IPC 库 mm 自述文件 网络安全 用户 复制文档包括 Kbuild 维护者 Module.symvers 报告错误 sound vmlinux USB驱动程序位于drivers目录下。 alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20/drivers/usb$ls ATM 类小工具图像 Kconfig 其他网络 README 存储 内置.o核心主机输入 Makefile mon otg 串口 usb-skeleton.c 希望这能帮到你 顺祝商祺! 阿巴特基
View full article
MPC8313RDBボードのカーネルソース <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは リファレンス・デザインボード用のUSBドライバ MPC8313コンパイルしようとしています。Linuxでドライバをコンパイルするためのソースコードがありません。.isoファイルから抽出する必要があるとのことです。(存在しない)ファイル。カーネルソースファイル(OS、Linux、Powerpc向けのGCCスイッチなど)を使わずにドライバを開発する方法はありますか?あるいは、どなたかカーネルのソースファイルを探す手助けをしていただけませんか? もしカーネルソースがCD上に存在するとしたら、それはどのようなファイル名で隠されているのでしょうか? カーネルバージョン: 2.6.20 前もって感謝します、 AK 評価ボード Re: MPC8313RDB board Kernel Source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ありがとう、abartkyさん。    挙げられた手順のおかげで、isoパッケージからカーネルファイルを抽出する作業が簡単になりましたし、あなたの説明もとても参考になりました。 再度、感謝します、 AK Re: MPC8313RDB board Kernel Source <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ak79、 カーネルファイルはパッケージファイルに入っているので、ボード付属のCDには直接載っていません。 カーネルのソースファイルを入手するには、LTIB環境をインストールしてから、カーネルファイルの抽出とビルドを要求する必要があります。 LTIB環境のインストールは、CDから行うか、最新.isoをダウロードして行うことができますフリースケール社のサイトからファイルをダウンロードしてください。最新のソースコードを入手できるので、ダウンロードすることをお勧めします(どうしてもCDからインストールしたい場合は、手順はほぼ同じですが、CDを直接実行権限でマウントし、そこからインストールスクリプトを実行する必要があります)。 MPC8313の最新BSPを探すには、Freescaleのサイトにログインし、FreescaleのMPC8313とBSPでキーワード検索を行うと、そのリンクが表示されます。 https://www.freescale.com/webapp/Download?colCode=CWF-MPC8313E-RDB&location=null&fsrch=1 フォームに記入してファイルをダウンロードしてください。 そのファイルをダウンロードし、作業ディレクトリに配置し、root権限で.isoファイルをマウントします。ファイル CD イメージを実行ファイルディレクトリとして保存し、通常の Linux ログインとしてインストールを実行します(例): alan@raptor:~$ ls *.iso MPC8313E_RDB_K26_20070831-LTIB.iso alan@raptor:~$ su パスワード: Raptor:/home/alan# ls -ld cdmount drwxrwxrwx 2 アラン アラン 4096 2007-05-29 11:51 cdmount Raptor:/ホーム/alan# Mount -O Loop MPC8313E_RDB_K26_20070831-LTIB.iso CDMOUNT ラプター:/ホーム/アラン# 退出 終了 alan@raptor:~$ alan@raptor:~$ cdmount/install それが完了したら、インストールしたディレクトリに移動して、ltib を初めて実行する必要があります (例) alan@raptor:~$ cd ltib-mpc8313erdb-20070824/ alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib インストールと初期ビルドが完了したと仮定すると、Linuxカーネルソースの解凍とビルドを次の方法で依頼できます; alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib--設定 最初に表示されるメニューで、次の2つのオプションを選択し、終了してください。 [*] カーネルを設定する [*]ビルディング後にソースを残す カーネル設定メニューが表示されたら、そのまま終了を選ぶだけです。 その後、カーネルソースが抽出されてビルドされます。現在のバージョンでこれを行う場合、メインのLinuxカーネルソースは以下の場所で確認できます: alan@raptor:~/ltib-mpc8313erdb-20070824$ cd rpm/BUILD/linux-2.6.20/ alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20$ alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20$ls arch CREDITS ドライバ init kernel Makefile net scripts System.map vmlinux.bin.gz ブロック crypto fs ipc lib mm README セキュリティ USR コピー ドキュメントには Kbuild MAINTAINERS Module.symvers REPORTING-BUGS sound vmlinux が含まれます USBドライバはドライバディレクトリの下にあります。 alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20/ドライバ/usb$ls ATMクラスガジェットイメージKconfigその他ネットワークREADMEストレージ 組み込み済み。コアホスト入力Makefile mon otg シリアル usb-skeleton.c お役に立てれば幸いです よろしくお願いいたします。 アバートキー
View full article
SamFwツール6.2 最新バージョン2027をダウンロード SamFW FRP Toolは、Samsung Androidデバイスのメンテナンスおよびトラブルシューティングに関連するWindowsのユーティリティです。 SamFWツールをダウンロード . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .   StarCore DSP
View full article
TFT MTK Module Tool Download MediaTek FRP 2027 TFT MTK Module Tool is a Windows-based mobile servicing tool developed for MediaTek-powered Android smartphones and tablets. Download Tool . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . StarCore DSPs
View full article