DMA Error with imx93 and eqos in RMII I'm trying to make ethernet working with a LAN8742A PHY, connected to eqos, in RMII mode. I've taken the imx93-11x11-frdm.dts as base reference, and made the following changes : &iomuxc {
pinctrl_eqos: eqosgrp {
fsl,pins = <
MX93_PAD_ENET1_MDC__ENET_QOS_MDC 0x57e /* OK */
MX93_PAD_ENET1_MDIO__ENET_QOS_MDIO 0x57e /* OK */
MX93_PAD_ENET1_RD0__ENET_QOS_RGMII_RD0 0x57e /* OK */
MX93_PAD_ENET1_RD1__ENET_QOS_RGMII_RD1 0x57e /* OK */
/* MX93_PAD_ENET1_RD2__ENET_QOS_RGMII_RD2 0x57e
MX93_PAD_ENET1_RD3__ENET_QOS_RGMII_RD3 0x57e */
MX93_PAD_ENET1_RXC__ENET_QOS_RX_ER 0x51e /* OK */
/* MX93_PAD_ENET1_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK 0x51e */
MX93_PAD_ENET1_RX_CTL__ENET_QOS_RGMII_RX_CTL 0x57e /* OK */
MX93_PAD_ENET1_TD0__ENET_QOS_RGMII_TD0 0x57e /* OK */
MX93_PAD_ENET1_TD1__ENET_QOS_RGMII_TD1 0x57e /* OK */
/* refclock for Eth phy */
MX93_PAD_ENET1_TD2__CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK 0x57e /* OK */
/* MX93_PAD_ENET1_TD2__ENET_QOS_RGMII_TD2 0x57e
MX93_PAD_ENET1_TD3__ENET_QOS_RGMII_TD3 0x57e */
/* MX93_PAD_ENET1_TXC__CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK 0x5fe */
MX93_PAD_ENET1_TX_CTL__ENET_QOS_RGMII_TX_CTL 0x0000051e /* OK */
/* MX93_PAD_ENET1_TX_CTL__ENET_QOS_RGMII_TX_CTL 0x57e */
>;
}; &eqos {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eqos>;
phy-mode = "rmii";
phy-handle = <ðphy1>;
status = "okay";
/delete-property/ assigned-clocks;
/delete-property/ assigned-clock-rates;
assigned-clocks = <&clk IMX93_CLK_ENET_TIMER2>,
<&clk IMX93_CLK_ENET>;
assigned-clock-rates = <100000000>, <50000000>;
mdio {
compatible = "snps,dwmac-mdio";
#address-cells = <1>;
#size-cells = <0>;
clock-frequency = <5000000>;
ethphy1: ethernet-phy@0 {
reg = <0>;
eee-broken-1000tx;
post-power-on-delay-ms = <100>;
reset-gpios = <&pcal6524 19 GPIO_ACTIVE_LOW>;
reset-assert-us = <15000>;
reset-deassert-us = <100000>;
};
};
}; Result in uboot is : u-boot=> bootp
EQOS_DMA_MODE_SWR stuckFAILED: -110
u-boot=>
Result in linux is : [ 11.484536] imx-dwmac 428a0000.ethernet: Failed to reset the dma
[ 11.490536] imx-dwmac 428a0000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 11.499228] imx-dwmac 428a0000.ethernet eth0: __stmmac_open: Hw setup failed I don't understand what i am doing wrong, what i misconifgured, or why the dma does not initialize properly. It's pretty obvious that i'm missing something (a dma error looks like an internal error from the chip, so even if there was an error with the pinmux i don't thihnk i would get this, and i double checked the pinmux). Things i have checked : - clock is correctly sent to the PHY - communication with the PHY on mdio works Any hints on this would be greatly appreciated, Best regards, Julien Re: DMA Error with imx93 and eqos in RMII Reset is set correctly in uboot. I can see the PHY live (the leds work), and communicate with it, but i still get the DMA error. I tried manually disabling and reenabling the PHY via the reset pin in u-boot, but this didn't change anything. Here is the complete log from dmesg : [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]
[ 0.000000] Linux version 6.6.36 (
[email protected]@UC155-BE2) (aarch64-sprinte450sp-linux-gnu-gcc.br_real (Buildroot 2026.05-2-gf0cfb0f3cf-dirty) 14.3.0, GNU ld (GNU Binutils) 2.45.1) #4 SMP PREEMPT Thu Jul 23 17:04:50 CEST 2026
[ 0.000000] KASLR disabled due to lack of seed
[ 0.000000] Machine model: Sprinte 450SP board
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000b0000000..0x00000000bfffffff (262144 KiB) map reusable linux,cma
[ 0.000000] earlycon: lpuart32 at MMIO32 0x0000000044380000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xafdcf6c0-0xafdd1fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.4
[ 0.000000] percpu: Embedded 22 pages/cpu s50600 r8192 d31320 u90112
[ 0.000000] pcpu-alloc: s50600 r8192 d31320 u90112 alloc=22*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Virtualization Host Extensions
[ 0.000000] CPU features: detected: Qualcomm erratum 1009, or ARM erratum 1286807, 2441009
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258048
[ 0.000000] Policy zone: DMA
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 2.
[ 0.000000] software IO TLB: mapped [mem 0x00000000aac00000-0x00000000aec00000] (64MB)
[ 0.000000] Memory: 666980K/1048576K available (20608K kernel code, 1638K rwdata, 7744K rodata, 1984K init, 643K bss, 119452K reserved, 262144K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000048040000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
[ 0.000000] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
[ 0.008305] Console: colour dummy device 80x25
[ 0.012529] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
[ 0.022711] pid_max: default: 32768 minimum: 301
[ 0.027347] LSM: initializing lsm=capability,integrity
[ 0.032485] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.039785] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.048237] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 0.054656] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.061512] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.069127] rcu: Hierarchical SRCU implementation.
[ 0.073752] rcu: Max phase no-delay instances is 1000.
[ 0.079653] EFI services will not be available.
[ 0.084098] smp: Bringing up secondary CPUs ...
[ 0.088812] Detected VIPT I-cache on CPU1
[ 0.088870] GICv3: CPU1: found redistributor 100 region 0:0x0000000048060000
[ 0.088904] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]
[ 0.089007] smp: Brought up 1 node, 2 CPUs
[ 0.110357] SMP: Total of 2 processors activated.
[ 0.115028] CPU features: detected: 32-bit EL0 Support
[ 0.120154] CPU features: detected: 32-bit EL1 Support
[ 0.125257] CPU features: detected: Data cache clean to the PoU not required for I/D coherence
[ 0.133840] CPU features: detected: Common not Private translations
[ 0.140073] CPU features: detected: CRC32 instructions
[ 0.145196] CPU features: detected: RCpc load-acquire (LDAPR)
[ 0.150906] CPU features: detected: LSE atomic instructions
[ 0.156453] CPU features: detected: Privileged Access Never
[ 0.161998] CPU features: detected: RAS Extension Support
[ 0.167374] CPU features: detected: Speculative Store Bypassing Safe (SSBS)
[ 0.174355] CPU: All CPU(s) started at EL2
[ 0.178380] alternatives: applying system-wide alternatives
[ 0.187922] devtmpfs: initialized
[ 0.194925] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.204430] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.216607] pinctrl core: initialized pinctrl subsystem
[ 0.223019] DMI not present or invalid.
[ 0.227066] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.233367] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[ 0.240250] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.247941] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.255804] audit: initializing netlink subsys (disabled)
[ 0.261291] audit: type=2000 audit(0.172:1): state=initialized audit_enabled=0 res=1
[ 0.261671] thermal_sys: Registered thermal governor 'step_wise'
[ 0.268851] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.274855] cpuidle: using governor menu
[ 0.285411] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.292025] ASID allocator initialised with 65536 entries
[ 0.297950] Serial: AMBA PL011 UART driver
[ 0.301832] imx mu driver is registered.
[ 0.305685] imx rpmsg driver is registered.
[ 0.314130] imx93-pinctrl 443c0000.pinctrl: initialized IMX pinctrl driver
[ 0.326962] Modules: 24576 pages in range for non-PLT usage
[ 0.326973] Modules: 516096 pages in range for PLT usage
[ 0.333009] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.344824] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.351063] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.357821] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.364062] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.370821] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.377062] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.383821] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.391518] ACPI: Interpreter disabled.
[ 0.395792] iommu: Default domain type: Translated
[ 0.400360] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.406743] SCSI subsystem initialized
[ 0.410355] libata version 3.00 loaded.
[ 0.410523] usbcore: registered new interface driver usbfs
[ 0.415761] usbcore: registered new interface driver hub
[ 0.421054] usbcore: registered new device driver usb
[ 0.426646] mc: Linux media interface: v0.10
[ 0.430689] videodev: Linux video capture interface: v2.00
[ 0.436154] pps_core: LinuxPPS API ver. 1 registered
[ 0.441049] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti
[ 0.450155] PTP clock support registered
[ 0.454144] EDAC MC: Ver: 3.0.0
[ 0.457601] scmi_core: SCMI protocol bus registered
[ 0.462617] FPGA manager framework
[ 0.465811] Advanced Linux Sound Architecture Driver Initialized.
[ 0.472369] Bluetooth: Core ver 2.22
[ 0.475701] NET: Registered PF_BLUETOOTH protocol family
[ 0.480981] Bluetooth: HCI device and connection manager initialized
[ 0.487298] Bluetooth: HCI socket layer initialized
[ 0.492148] Bluetooth: L2CAP socket layer initialized
[ 0.497182] Bluetooth: SCO socket layer initialized
[ 0.502337] vgaarb: loaded
[ 0.505250] clocksource: Switched to clocksource arch_sys_counter
[ 0.511308] VFS: Disk quotas dquot_6.6.0
[ 0.515015] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.521961] pnp: PnP ACPI: disabled
[ 0.530265] NET: Registered PF_INET protocol family
[ 0.535027] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.542962] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.551110] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.558774] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.566509] TCP bind hash table entries: 8192 (order: 6, 262144 bytes, linear)
[ 0.573930] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.580120] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.586625] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.593729] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.599609] RPC: Registered named UNIX socket transport module.
[ 0.605277] RPC: Registered udp transport module.
[ 0.609945] RPC: Registered tcp transport module.
[ 0.614624] RPC: Registered tcp-with-tls transport module.
[ 0.620084] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.627260] PCI: CLS 0 bytes, default 64
[ 0.631165] kvm [1]: IPA Size Limit: 40 bits
[ 0.635194] kvm [1]: GICv3: no GICV resource entry
[ 0.639942] kvm [1]: disabling GICv2 emulation
[ 0.644371] kvm [1]: GIC system register CPU interface enabled
[ 0.650191] kvm [1]: vgic interrupt IRQ9
[ 0.654088] kvm [1]: VHE mode initialized successfully
[ 0.660051] Initialise system trusted keyrings
[ 0.664421] workingset: timestamp_bits=42 max_order=18 bucket_order=0
[ 0.670898] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.676710] NFS: Registering the id_resolver key type
[ 0.681531] Key type id_resolver registered
[ 0.685658] Key type id_legacy registered
[ 0.689659] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.696326] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.703831] 9p: Installing v9fs 9p2000 file system support
[ 0.734526] Key type asymmetric registered
[ 0.738370] Asymmetric key parser 'x509' registered
[ 0.743258] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.750590] io scheduler mq-deadline registered
[ 0.755095] io scheduler kyber registered
[ 0.759113] io scheduler bfq registered
[ 0.766447] EINJ: ACPI disabled.
[ 0.773498] Bus freq driver module loaded
[ 0.782271] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.790543] 44380000.serial: ttyLP0 at MMIO 0x44380010 (irq = 17, base_baud = 1500000) is a FSL_LPUART
[ 0.799853] printk: console [ttyLP0] enabled
[ 0.808289] printk: bootconsole [lpuart32] disabled
[ 0.827377] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 0.835386] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 0.844862] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with 4ae30000.lcd-controller
[ 0.858799] loop: module loaded
[ 0.863014] megasas: 07.725.01.00-rc1
[ 0.870948] tun: Universal TUN/TAP device driver, 1.6
[ 0.876567] thunder_xcv, ver 1.0
[ 0.879836] thunder_bgx, ver 1.0
[ 0.883080] nicpf, ver 1.0
[ 0.886825] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 0.894055] hns3: Copyright (c) 2017 Huawei Corporation.
[ 0.899390] hclge is initializing
[ 0.902728] e1000: Intel(R) PRO/1000 Network Driver
[ 0.907598] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 0.913354] e1000e: Intel(R) PRO/1000 Network Driver
[ 0.918310] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 0.924238] igb: Intel(R) Gigabit Ethernet Network Driver
[ 0.929635] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 0.935216] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.941476] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.947488] sky2: driver version 1.30
[ 0.951466] usbcore: registered new device driver r8152-cfgselector
[ 0.957746] usbcore: registered new interface driver r8152
[ 0.963616] VFIO - User Level meta-driver version: 0.3
[ 0.970278] usbcore: registered new interface driver uas
[ 0.975636] usbcore: registered new interface driver usb-storage
[ 0.981731] usbcore: registered new interface driver usbserial_generic
[ 0.988270] usbserial: USB Serial support registered for generic
[ 0.994286] usbcore: registered new interface driver ftdi_sio
[ 1.000031] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.007339] usbcore: registered new interface driver usb_serial_simple
[ 1.013862] usbserial: USB Serial support registered for carelink
[ 1.019959] usbserial: USB Serial support registered for flashloader
[ 1.026317] usbserial: USB Serial support registered for funsoft
[ 1.032327] usbserial: USB Serial support registered for google
[ 1.038251] usbserial: USB Serial support registered for hp4x
[ 1.043996] usbserial: USB Serial support registered for kaufmann
[ 1.050089] usbserial: USB Serial support registered for libtransistor
[ 1.056614] usbserial: USB Serial support registered for moto_modem
[ 1.062880] usbserial: USB Serial support registered for motorola_tetra
[ 1.069494] usbserial: USB Serial support registered for nokia
[ 1.075326] usbserial: USB Serial support registered for novatel_gps
[ 1.081686] usbserial: USB Serial support registered for siemens_mpi
[ 1.088040] usbserial: USB Serial support registered for suunto
[ 1.093963] usbserial: USB Serial support registered for vivopay
[ 1.099966] usbserial: USB Serial support registered for zio
[ 1.105629] usbcore: registered new interface driver usb_ehset_test
[ 1.114691] input: 44440000.bbnsm:pwrkey as /devices/platform/soc@0/44000000.bus/44440000.bbnsm/44440000.bbnsm:pwrkey/input/input0
[ 1.126836] i2c_dev: i2c /dev entries driver
[ 1.133908] imx7ulp-wdt 42490000.watchdog: imx93 wdt probe
[ 1.165969] Bluetooth: HCI UART driver ver 2.3
[ 1.170432] Bluetooth: HCI UART protocol H4 registered
[ 1.175564] Bluetooth: HCI UART protocol BCSP registered
[ 1.180885] Bluetooth: HCI UART protocol LL registered
[ 1.186018] Bluetooth: HCI UART protocol ATH3K registered
[ 1.191417] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.197782] Bluetooth: HCI UART protocol Broadcom registered
[ 1.203454] Bluetooth: HCI UART protocol QCA registered
[ 1.209726] sdhci: Secure Digital Host Controller Interface driver
[ 1.215922] sdhci: Copyright(c) Pierre Ossman
[ 1.220572] Synopsys Designware Multimedia Card Interface Driver
[ 1.226885] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.233614] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.240850] fsl-se-fw se-fw2: failed to init reserved memory region -19
[ 1.247608] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.254330] usbcore: registered new interface driver usbhid
[ 1.259901] usbhid: USB HID core driver
[ 1.270337] mmc0: SDHCI controller on 42850000.mmc [42850000.mmc] using ADMA
[ 1.302222] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available
[ 1.312041] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.319751] optee: probing for conduit method.
[ 1.324215] optee: api uid mismatch
[ 1.325699] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[ 1.327700] optee: probe of firmware:optee failed with error -22
[ 1.334598] mmcblk0: mmc0:0001 eMMC 58.2 GiB
[ 1.342512] NET: Registered PF_LLC protocol family
[ 1.345923] mmcblk0: p1
[ 1.349519] u32 classifier
[ 1.352252] mmcblk0boot0: mmc0:0001 eMMC 4.00 MiB
[ 1.354567] input device check on
[ 1.360666] mmcblk0boot1: mmc0:0001 eMMC 4.00 MiB
[ 1.363094] Actions configured
[ 1.363485] NET: Registered PF_INET6 protocol family
[ 1.368956] mmcblk0rpmb: mmc0:0001 eMMC 4.00 MiB, chardev (234:0)
[ 1.372113] Segment Routing with IPv6
[ 1.386309] In-situ OAM (IOAM) with IPv6
[ 1.390278] NET: Registered PF_PACKET protocol family
[ 1.395349] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 1.408425] Bluetooth: RFCOMM TTY layer initialized
[ 1.413310] Bluetooth: RFCOMM socket layer initialized
[ 1.418455] Bluetooth: RFCOMM ver 1.11
[ 1.422203] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.427502] Bluetooth: BNEP filters: protocol multicast
[ 1.432721] Bluetooth: BNEP socket layer initialized
[ 1.437676] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.443589] Bluetooth: HIDP socket layer initialized
[ 1.448783] 8021q: 802.1Q VLAN Support v1.8
[ 1.452998] lib80211: common routines for IEEE802.11 drivers
[ 1.458652] lib80211_crypt: registered algorithm 'NULL'
[ 1.458656] lib80211_crypt: registered algorithm 'WEP'
[ 1.458659] lib80211_crypt: registered algorithm 'CCMP'
[ 1.458663] lib80211_crypt: registered algorithm 'TKIP'
[ 1.458693] 9pnet: Installing 9P2000 support
[ 1.463084] Key type dns_resolver registered
[ 1.467497] NET: Registered PF_VSOCK protocol family
[ 1.486367] registered taskstats version 1
[ 1.490717] Loading compiled-in X.509 certificates
[ 1.512663] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[ 1.521013] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[ 1.539006] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with ldb-phy
[ 1.550623] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 1.558672] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 1.569462] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found
[ 1.575451] imx-dwmac 428a0000.ethernet: tx clock enable start
[ 1.581464] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[ 1.588255] imx-dwmac 428a0000.ethernet: DWMAC4/5
[ 1.593038] imx-dwmac 428a0000.ethernet: DMA HW capability register supported
[ 1.600159] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported
[ 1.607283] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported
[ 1.613973] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported
[ 1.620110] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.627757] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[ 1.634536] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.641316] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 1.648876] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width
[ 1.657380] imx-dwmac 428a0000.ethernet: tx clock disable start
[ 1.663414] imx-dwmac 428a0000.ethernet: err_drv_probe
[ 1.668557] imx-dwmac 428a0000.ethernet: err_dwmac_init
[ 1.677361] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 1.682306] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 1.709253] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 1.715211] hub 1-0:1.0: USB hub found
[ 1.718981] hub 1-0:1.0: 1 port detected
[ 1.726882] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 1.731789] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[ 1.753257] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 1.759191] hub 2-0:1.0: USB hub found
[ 1.762965] hub 2-0:1.0: 1 port detected
[ 1.770674] rtc rtc0: Power loss detected, invalid time
[ 1.776048] rtc-pcf85063 0-0051: registered as rtc0
[ 1.781185] rtc rtc0: Power loss detected, invalid time
[ 1.786407] rtc-pcf85063 0-0051: hctosys: unable to read the hardware clock
[ 1.793553] pca953x 0-0020: supply vcc not found, using dummy regulator
[ 1.800254] pca953x 0-0020: using no AI
[ 1.804716] i2c i2c-0: LPI2C adapter registered
[ 1.810507] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 1.817269] pca953x 1-0022: using AI
[ 1.822077] at24 1-0050: supply vcc not found, using dummy regulator
[ 1.828917] at24 1-0050: 1024 byte 24c08 EEPROM, writable, 16 bytes/write
[ 1.835795] i2c i2c-1: LPI2C adapter registered
[ 1.841329] i2c i2c-2: LPI2C adapter registered
[ 1.846907] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 1.854932] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 1.865632] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found
[ 1.871579] imx-dwmac 428a0000.ethernet: tx clock enable start
[ 1.877611] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[ 1.884419] imx-dwmac 428a0000.ethernet: DWMAC4/5
[ 1.889206] imx-dwmac 428a0000.ethernet: DMA HW capability register supported
[ 1.896327] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported
[ 1.903449] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported
[ 1.910153] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported
[ 1.916235] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.923878] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[ 1.930655] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.937446] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 1.945009] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width
[ 2.091986] imx-dwmac 428a0000.ethernet: tx clock disable start
[ 2.092418] sdhci-esdhc-imx 42860000.mmc: Got CD GPIO
[ 2.099328] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.111052] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 2.122102] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.130156] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 2.134093] mmc1: SDHCI controller on 42860000.mmc [42860000.mmc] using ADMA
[ 2.139573] nxp-pca9450 1-0025: pca9451a probed.
[ 2.152583] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.160637] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 2.171559] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.180575] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.186741] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 2.194068] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.197312] clk: Disabling unused clocks
[ 2.202716] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.214819] ALSA device list:
[ 2.217793] No soundcards found.
[ 2.221596] Waiting for root device /dev/mmcblk1p2...
[ 2.287788] mmc1: host does not support reading read-only switch, assuming write-enable
[ 2.298005] mmc1: new high speed SD card at address 0001
[ 2.303890] mmcblk1: mmc1:0001 00000 1.81 GiB
[ 2.311020] mmcblk1: p1 p2
[ 2.315100] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.323111] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 2.339143] exFAT-fs (mmcblk1p2): invalid boot record signature
[ 2.345082] exFAT-fs (mmcblk1p2): failed to read boot sector
[ 2.350777] exFAT-fs (mmcblk1p2): failed to recognize exfat type
[ 2.358002] erofs: (device mmcblk1p2): mounted with root inode @ nid 36.
[ 2.364768] VFS: Mounted root (erofs filesystem) readonly on device 179:98.
[ 2.371789] devtmpfs: mounted
[ 2.375967] Freeing unused kernel memory: 1984K
[ 2.380690] Run /sbin/init as init process
[ 2.384782] with arguments:
[ 2.384785] /sbin/init
[ 2.384787] with environment:
[ 2.384790] HOME=/
[ 2.384792] TERM=linux
[ 4.633259] random: crng init done
[ 12.406378] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 12.414399] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 12.424617] platform imx-lcdifv3-crtc.0: deferred probe pending And when ip link set eth0 up (there are a few non-standard traces that i added to the driver to try to debug this dma issue) : # ip link set eth0 up
[ 236.851517] imx-dwmac 428a0000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 236.859339] imx-dwmac 428a0000.ethernet: tx clock enable start
[ 236.974901] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 236.982933] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[ 237.081392] imx-dwmac 428a0000.ethernet eth0: PHY [stmmac-1:00] driver [Generic PHY] (irq=POLL)
[ 237.090112] Checking DMA clocks before reset...
[ 237.094643] DMA_HW_CAPABILITY = 0x0
[ 237.098124] RESET START: DMA_BUS_MODE = 0x1
[ 237.102301] AFTER WRITE: DMA_BUS_MODE = 0x1
[ 238.107432] POLL RESULT: ret=-110, DMA_BUS_MODE = 0x1
[ 238.112492] imx-dwmac 428a0000.ethernet: Failed to reset the dma
[ 238.118519] imx-dwmac 428a0000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 238.127210] imx-dwmac 428a0000.ethernet eth0: __stmmac_open: Hw setup failed
[ 238.194819] imx-dwmac 428a0000.ethernet: tx clock disable start
ip: SIOCSIFFLAGS: Connection timed out Thanks for your help, Best regards, Julien Re: DMA Error with imx93 and eqos in RMII Hello,
Please confirm that reset is asserted correctly in the PHY.
When the PHY is not provided with the clock for a brief period and the clock is enabled back, a reset must be provided to the PHY to latch all the configuration straps, recover into the normal working mode.
Please share your entire dmesg.
Best regards. Re: DMA Error with imx93 and eqos in RMII Hello,
Thank you for the information.
Since registers can be accessed, the MAC is not completely held in reset.
Could you please share the schematic connections to confirm how REF_CLK is provided?
Also, please share your clock summary in cat /sys/kernel/debug/clk/clk_summary
Best regards. Re: DMA Error with imx93 and eqos in RMII I don't want to share the full schematics on a public forum. Can i send them privately ? REF_CLK is provided via ENET1_TD2 (pin U12 of imx93). In device tree, this is this line : MX93_PAD_ENET1_TD2__CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK 0x57e We have checked with an oscilloscope that the clock is correct under u-boot, but we encounter a similar dma error (with less details). Under linux, something is stopping the clock (my guess is that the dma error triggers a release of the clock, which is then stopped by linux kernel as unused). Here's the content of clk_summary : enable prepare protect duty hardware connection
clock count count count rate accuracy phase cycle enable consumer id
---------------------------------------------------------------------------------------------------------------------------------------------
pcf85063-clkout 0 0 0 0 0 0 50000 Y deviceless no_connection_id
sys_pll_pfd2 1 1 0 625000000 0 0 50000 Y deviceless no_connection_id
wakeup_axi_root 2 2 0 312500000 0 0 50000 Y 42860000.mmc ahb
42850000.mmc ahb
deviceless no_connection_id
enet_qos 0 0 0 312500000 0 0 50000 N 428a0000.ethernet mem
428a0000.ethernet pclk
428a0000.ethernet stmmaceth
deviceless no_connection_id
enet1 0 0 0 312500000 0 0 50000 N 42890000.ethernet ahb
42890000.ethernet ipg
deviceless no_connection_id
edma2 1 1 0 312500000 0 0 50000 Y 42000000.dma-controller edma
deviceless no_connection_id
sys_pll_pfd2_div2 0 0 0 312500000 0 0 50000 Y deviceless no_connection_id
sys_pll_pfd1 3 3 0 800000000 0 0 50000 Y deviceless no_connection_id
media_axi_root 1 1 0 400000000 0 0 50000 Y 4ae30000.lcd-controller disp-axi
4ac10000.system-controller axi
deviceless no_connection_id
nic_media 1 1 0 400000000 0 0 50000 Y 4ac10000.system-controller nic
power-domain@44462400 no_connection_id
deviceless no_connection_id
nic_axi_root 1 1 0 400000000 0 0 50000 Y deviceless no_connection_id
ccm_cko4_root 0 0 0 266666667 0 0 50000 N deviceless no_connection_id
ccm_cko3_root 0 0 0 266666667 0 0 50000 N deviceless no_connection_id
ccm_cko2_root 0 0 0 266666667 0 0 50000 N deviceless no_connection_id
ccm_cko1_root 0 0 0 266666667 0 0 50000 N deviceless no_connection_id
usdhc3_root 0 0 0 200000000 0 0 50000 N deviceless no_connection_id
usdhc3 0 0 0 200000000 0 0 50000 N deviceless no_connection_id
usdhc2_root 0 0 0 400000000 0 0 50000 N deviceless no_connection_id
usdhc2 0 0 0 400000000 0 0 50000 N 42860000.mmc per
deviceless no_connection_id
usdhc1_root 0 0 0 400000000 0 0 50000 N deviceless no_connection_id
usdhc1 0 0 0 400000000 0 0 50000 N 42850000.mmc per
deviceless no_connection_id
flexspi1_root 0 0 0 200000000 0 0 50000 N deviceless no_connection_id
flexspi1 0 0 0 200000000 0 0 50000 N deviceless no_connection_id
sys_pll_pfd1_div2 6 6 0 400000000 0 0 50000 Y deviceless no_connection_id
enet_ref_phy_root 0 0 0 50000000 0 0 50000 N 42890000.ethernet enet_out
deviceless no_connection_id
enet_timer1_root 0 0 0 100000000 0 0 50000 N 42890000.ethernet ptp
deviceless no_connection_id
enet_timer2_root 0 0 0 100000000 0 0 50000 N 428a0000.ethernet ptp_ref
deviceless no_connection_id
media_apb_root 1 2 0 133333334 0 0 50000 Y ldb-phy apb
system-controller@4ac10000 no_connection_id
4ac10000.system-controller apb
power-domain@44462400 no_connection_id
deviceless no_connection_id
isi 0 0 0 133333334 0 0 50000 N 4ac10000.system-controller isi
deviceless no_connection_id
pxp 0 0 0 133333334 0 0 50000 N 4ac10000.system-controller pxp
deviceless no_connection_id
lcdif 0 0 0 133333334 0 0 50000 N 4ae30000.lcd-controller disp-apb
4ac10000.system-controller lcdif
deviceless no_connection_id
mipi_dsi 0 0 0 133333334 0 0 50000 N 4ac10000.system-controller dsi
deviceless no_connection_id
mipi_csi 0 0 0 133333334 0 0 50000 N 4ac10000.system-controller csi
deviceless no_connection_id
hsio_root 1 1 0 133333334 0 0 50000 Y deviceless no_connection_id
usb_controller 0 0 0 133333334 0 0 50000 N 4c200000.usb no_connection_id
4c100000.usb no_connection_id
deviceless no_connection_id
lpspi4_root 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
lpspi4 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
lpspi3_root 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
lpspi3 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
lpspi2_root 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
lpspi2 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
lpspi1_root 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
lpspi1 0 0 0 50000000 0 0 50000 N deviceless no_connection_id
swo_trace_root 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
bus_aon_root 1 1 0 133333334 0 0 50000 Y i2c@44350000 no_connection_id
i2c@44340000 no_connection_id
deviceless no_connection_id
tstmr1 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
pdm_ipg_clk 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
sai1_ipg_clk 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
tpm1 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
lpit1 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
mu1_b 0 0 0 133333334 0 0 50000 N 44230000.mailbox no_connection_id
deviceless no_connection_id
mu1_a 0 0 0 133333334 0 0 50000 Y deviceless no_connection_id
sema1 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
bus_wakeup_root 4 4 0 133333334 0 0 50000 Y 42860000.mmc ipg
i2c@42530000 no_connection_id
42850000.mmc ipg
deviceless no_connection_id
tstmr2 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
sai3_ipg_clk 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
sai2_ipg_clk 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
tpm3 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
lpit2 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
gpio4 2 2 0 133333334 0 0 50000 Y 43830000.gpio gpio
43830000.gpio port
deviceless no_connection_id
gpio3 2 2 0 133333334 0 0 50000 Y 43820000.gpio gpio
43820000.gpio port
deviceless no_connection_id
gpio2 2 2 0 133333334 0 0 50000 Y 43810000.gpio gpio
43810000.gpio port
deviceless no_connection_id
mu2_b 0 0 0 133333334 0 0 50000 N 42440000.mailbox no_connection_id
deviceless no_connection_id
mu2_a 0 0 0 133333334 0 0 50000 Y deviceless no_connection_id
sema2 0 0 0 133333334 0 0 50000 N deviceless no_connection_id
m33_root 4 4 0 200000000 0 0 50000 Y deviceless no_connection_id
gpio1 2 2 0 200000000 0 0 50000 Y 47400000.gpio gpio
47400000.gpio port
deviceless no_connection_id
edma1 1 1 0 200000000 0 0 50000 Y 44000000.dma-controller edma
deviceless no_connection_id
cm33 1 1 0 200000000 0 0 50000 Y deviceless no_connection_id
a55_mtr_bus_root 1 1 0 133333334 0 0 50000 Y deviceless no_connection_id
sys_pll_pfd0 2 2 0 1000000000 0 0 50000 Y deviceless no_connection_id
a55_alt_root 1 1 0 500000000 0 0 50000 Y deviceless no_connection_id
a55_alt 0 0 0 500000000 0 0 50000 N deviceless no_connection_id
a55_periph_root 1 1 0 333333334 0 0 50000 Y deviceless no_connection_id
sys_pll_pfd0_div2 0 0 0 500000000 0 0 50000 Y deviceless no_connection_id
usb_phy_root 0 0 0 50000000 0 0 50000 N usbphynop2 main_clk
usbphynop1 main_clk
deviceless no_connection_id
enet_ref_root 0 0 0 250000000 0 0 50000 N 42890000.ethernet enet_clk_ref
deviceless no_connection_id
enet_root 0 0 0 50000000 0 0 50000 N 428a0000.ethernet tx
deviceless no_connection_id
dummy 0 0 0 0 0 0 50000 Y deviceless no_connection_id
clk_ext1 0 0 0 133000000 0 0 50000 Y clock-controller@44450000 clk_ext1
deviceless no_connection_id
osc_24m 6 6 3 24000000 0 0 50000 Y clock-controller@44450000 osc_24m
timer@44290000 per
deviceless no_connection_id
pmro 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tmc 1 1 0 24000000 0 0 50000 Y 44482000.tmu no_connection_id
deviceless no_connection_id
sys_cnt 1 1 0 24000000 0 0 50000 Y deviceless no_connection_id
hsio_trout_24m 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
wdog5 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
wdog4 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
wdog3 1 1 0 24000000 0 0 50000 Y 42490000.watchdog no_connection_id
deviceless no_connection_id
wdog2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
wdog1 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
pal_came_scan_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
i3c2_slow_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
i3c1_slow_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
spdif_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
spdif 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
audio_xcvr_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
aud_xcvr 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
mqs2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
mqs1_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tstmr2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tstmr1_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
pdm_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
pdm 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
adc_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
adc1 0 0 0 24000000 0 0 50000 N 44530000.adc ipg
deviceless no_connection_id
mipi_phy_cfg_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
mipi_test_byte_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
cam_pix_root 0 0 0 24000000 0 0 50000 N 4ac10000.system-controller cam
deviceless no_connection_id
ml_root 0 0 0 24000000 0 0 50000 N power-domain@44461800 no_connection_id
deviceless no_connection_id
ml_apb_root 0 0 0 24000000 0 0 50000 N power-domain@44461800 no_connection_id
deviceless no_connection_id
hsio_acscan_480m_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
hsio_acscan_80m_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
hsio_usb_test_60m_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
usb_test_60m 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
sai3_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
mqs2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
sai3 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
sai2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
sai2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
sai1_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
mqs1 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
sai1 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
i3c2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
i3c2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
i3c1_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
i3c1 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi8_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi8 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi7_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi7 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi6_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi6 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi5_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpspi5 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c8_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c8 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c7_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c7 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c6_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c6 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c5_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c5 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c4_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c4 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpi2c3_root 0 0 1 24000000 0 0 50000 N deviceless no_connection_id
lpi2c3 0 0 1 24000000 0 0 50000 N i2c@42530000 no_connection_id
deviceless no_connection_id
lpi2c2_root 0 0 1 24000000 0 0 50000 N deviceless no_connection_id
lpi2c2 0 0 1 24000000 0 0 50000 N i2c@44350000 no_connection_id
deviceless no_connection_id
lpi2c1_root 0 0 1 24000000 0 0 50000 N deviceless no_connection_id
lpi2c1 0 0 1 24000000 0 0 50000 N i2c@44340000 no_connection_id
deviceless no_connection_id
lpuart8_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart8 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart7_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart7 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart6_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart6 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart5_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart5 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart4_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart4 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart3_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart3 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lpuart1_root 1 1 0 24000000 0 0 50000 Y deviceless no_connection_id
lpuart1 1 1 0 24000000 0 0 50000 Y 44380000.serial ipg
deviceless no_connection_id
can2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
can2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
can1_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
can1 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm6_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm6 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm5_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm5 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm4_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm4 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
tpm2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lptmr2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lptmr2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lptmr1_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
lptmr1 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
flexio2_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
flexio2 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
flexio1_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
flexio1 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
m33_systick_root 0 0 0 24000000 0 0 50000 N deviceless no_connection_id
video_pll 0 0 0 1039500000 0 0 50000 Y deviceless no_connection_id
media_disp_pix_root 0 0 0 148500000 0 0 50000 N 4ae30000.lcd-controller pix
4ac10000.system-controller disp
deviceless no_connection_id
media_ldb_root 0 0 0 1039500000 0 0 50000 N deviceless no_connection_id
lvds 0 0 0 1039500000 0 0 50000 N deviceless no_connection_id
audio_pll 0 0 0 393216000 0 0 50000 Y deviceless no_connection_id
arm_pll 1 1 0 1700000000 0 0 50000 Y deviceless no_connection_id
a55_sel 1 1 0 1700000000 0 0 50000 Y deviceless no_connection_id
a55_core 1 1 0 1700000000 0 0 50000 Y deviceless no_connection_id
osc_32k 1 1 0 32768 0 0 50000 Y clock-controller@44450000 osc_32k
deviceless no_connection_id
hsio_32k 2 2 0 32768 0 0 50000 Y 4c200000.usb usb_wakeup_clk
4c100000.usb usb_wakeup_clk
deviceless no_connection_id
# Re: DMA Error with imx93 and eqos in RMII Please see the other message for my answer about the ref_clk and the schematics, it looks like i mistakenly used the wrong reply button. I also tried the following : https://community.nxp.com/t5/i-MX-Processors/i-MX93-EQoS-RMII-mode-with-internal-50MHz-reference-clock/m-p/1947843 which looks a lot like the same issue, but could not get it to work as well. Thanks for your support, Re: DMA Error with imx93 and eqos in RMII I could finally get it to work, using the patch in the link, and the following settings : &eqos {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eqos>;
phy-mode = "rmii";
phy-handle = <ðphy1>;
status = "okay";
assigned-clock-parents = <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>,
<&clk IMX93_CLK_SYS_PLL_PFD0_DIV2>;
assigned-clock-rates = <100000000>, <50000000>;
enet_clk_sel = <&wakeupmix_gpr 0x2C>;
clk_csr = <5>;
// snps,rmii_refclk_ext;
mdio {
compatible = "snps,dwmac-mdio";
#address-cells = <1>;
#size-cells = <0>;
clock-frequency = <5000000>;
ethphy1: ethernet-phy@0 {
reg = <0>;
eee-broken-1000tx;
reset-gpios = <&pcal6524 19 GPIO_ACTIVE_LOW>;
reset-assert-us = <15000>;
reset-deassert-us = <100000>;
smsc,disable-energy-detect;
};
};
}; Could you explain me what the patch in https://community.nxp.com/t5/i-MX-Processors/i-MX93-EQoS-RMII-mode-with-internal-50MHz-reference-clock/m-p/1947843 does, why it is needed? Also, shouldn't these changes be upstreamed, as they look like a regular use case for the soc, nothing exceptional? Re: DMA Error with imx93 and eqos in RMII Hello,
Is good to know that is now working.
The patch modifies the driver dwmac-imx/EQoS to configure ENET_QOS when RMII is using an external clock.
This change is needed because EQoS needs a constant clock during DMA reset.
Best regards.