2398401_zh-CN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2398401_zh-CN

2398401_zh-CN

RMII 中 imx93 和 eqos 出现 DMA 错误

我正在尝试让以太网与连接到 eqos 的 LAN8742A PHY 配合使用,采用 RMII 模式。

我以 imx93-11x11-frdm.dts 为基础,并进行了以下更改:

&iomuxc {
        pinctrl_eqos: eqosgrp {
                fsl,pins = <
                        MX93_PAD_ENET1_MDC__ENET_QOS_MDC                        0x57e /* OK */
                        MX93_PAD_ENET1_MDIO__ENET_QOS_MDIO                      0x57e /* OK */
                        MX93_PAD_ENET1_RD0__ENET_QOS_RGMII_RD0                  0x57e /* OK */
                        MX93_PAD_ENET1_RD1__ENET_QOS_RGMII_RD1                  0x57e /* OK */
 /*                     MX93_PAD_ENET1_RD2__ENET_QOS_RGMII_RD2                  0x57e
                        MX93_PAD_ENET1_RD3__ENET_QOS_RGMII_RD3                  0x57e */
                        MX93_PAD_ENET1_RXC__ENET_QOS_RX_ER                      0x51e /* OK */
/*                      MX93_PAD_ENET1_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK  0x51e  */
                        MX93_PAD_ENET1_RX_CTL__ENET_QOS_RGMII_RX_CTL            0x57e /* OK */
                        MX93_PAD_ENET1_TD0__ENET_QOS_RGMII_TD0                  0x57e /* OK */
                        MX93_PAD_ENET1_TD1__ENET_QOS_RGMII_TD1                  0x57e /* OK */
/* refclock for Eth phy */
                        MX93_PAD_ENET1_TD2__CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK 0x57e /* OK */
/*                      MX93_PAD_ENET1_TD2__ENET_QOS_RGMII_TD2                  0x57e
                        MX93_PAD_ENET1_TD3__ENET_QOS_RGMII_TD3                  0x57e */
/*                      MX93_PAD_ENET1_TXC__CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK  0x5fe */
                        MX93_PAD_ENET1_TX_CTL__ENET_QOS_RGMII_TX_CTL            0x0000051e /* OK */
/*                      MX93_PAD_ENET1_TX_CTL__ENET_QOS_RGMII_TX_CTL            0x57e */
                >;
        };

&eqos {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_eqos>;
        phy-mode = "rmii";
        phy-handle = <&ethphy1>;
        status = "okay";

        /delete-property/ assigned-clocks;
        /delete-property/ assigned-clock-rates;
        assigned-clocks = <&clk IMX93_CLK_ENET_TIMER2>,
                <&clk IMX93_CLK_ENET>;
        assigned-clock-rates = <100000000>, <50000000>;


        mdio {
                compatible = "snps,dwmac-mdio";
                #address-cells = <1>;
                #size-cells = <0>;
                clock-frequency = <5000000>;

                ethphy1: ethernet-phy@0 {
                        reg = <0>;
                        eee-broken-1000tx;
                        post-power-on-delay-ms = <100>;
                        reset-gpios = <&pcal6524 19 GPIO_ACTIVE_LOW>;
                        reset-assert-us = <15000>;
                        reset-deassert-us = <100000>;
                };
        };
};

U-Boot 中的结果是:

u-boot=> bootp
EQOS_DMA_MODE_SWR stuckFAILED: -110
u-boot=> 

Linux 系统中的结果为:

[   11.484536] imx-dwmac 428a0000.ethernet: Failed to reset the dma
[   11.490536] imx-dwmac 428a0000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[   11.499228] imx-dwmac 428a0000.ethernet eth0: __stmmac_open: Hw setup failed

我不明白我哪里做错了,哪里配置错误了,或者为什么DMA无法正确初始化。很明显我漏掉了一些东西(DMA 错误看起来像是芯片内部的错误,所以即使引脚复用出现错误,我认为也不会出现这种情况,而且我已经仔细检查过引脚复用了)。

我检查过的项目:

时钟信号已正确发送至PHY。
与mdio上的PHY通信正常


任何提示都将不胜感激。

顺祝商祺!

朱利安

Re: DMA Error with imx93 and eqos in RMII

uboot 中的 RESET 设置正确。我可以看到 PHY 芯片工作正常(LED 灯亮着),并且可以与它通信,但我仍然会收到 DMA 错误。

我尝试通过 u-boot 中的复位引脚手动禁用和重新启用 PHY,但这并没有任何改变。

以下是 dmesg 的完整日志:

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]
[    0.000000] Linux version 6.6.36 ([email protected]@UC155-BE2) (aarch64-sprinte450sp-linux-gnu-gcc.br_real (Buildroot 2026.05-2-gf0cfb0f3cf-dirty) 14.3.0, GNU ld (GNU Binutils) 2.45.1) #4 SMP PREEMPT Thu Jul 23 17:04:50 CEST 2026
[    0.000000] KASLR disabled due to lack of seed
[    0.000000] Machine model: Sprinte 450SP board
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 256 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000b0000000..0x00000000bfffffff (262144 KiB) map reusable linux,cma
[    0.000000] earlycon: lpuart32 at MMIO32 0x0000000044380000 (options '')
[    0.000000] printk: bootconsole [lpuart32] enabled
[    0.000000] NUMA: No NUMA configuration found
[    0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000] NUMA: NODE_DATA [mem 0xafdcf6c0-0xafdd1fff]
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.4
[    0.000000] percpu: Embedded 22 pages/cpu s50600 r8192 d31320 u90112
[    0.000000] pcpu-alloc: s50600 r8192 d31320 u90112 alloc=22*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1 
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: Virtualization Host Extensions
[    0.000000] CPU features: detected: Qualcomm erratum 1009, or ARM erratum 1286807, 2441009
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw
[    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.000000] Fallback order for Node 0: 0 
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 258048
[    0.000000] Policy zone: DMA
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 2.
[    0.000000] software IO TLB: mapped [mem 0x00000000aac00000-0x00000000aec00000] (64MB)
[    0.000000] Memory: 666980K/1048576K available (20608K kernel code, 1638K rwdata, 7744K rodata, 1984K init, 643K bss, 119452K reserved, 262144K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] 	Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000048040000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
[    0.000000] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
[    0.008305] Console: colour dummy device 80x25
[    0.012529] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
[    0.022711] pid_max: default: 32768 minimum: 301
[    0.027347] LSM: initializing lsm=capability,integrity
[    0.032485] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.039785] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.048237] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    0.054656] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[    0.061512] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[    0.069127] rcu: Hierarchical SRCU implementation.
[    0.073752] rcu: 	Max phase no-delay instances is 1000.
[    0.079653] EFI services will not be available.
[    0.084098] smp: Bringing up secondary CPUs ...
[    0.088812] Detected VIPT I-cache on CPU1
[    0.088870] GICv3: CPU1: found redistributor 100 region 0:0x0000000048060000
[    0.088904] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]
[    0.089007] smp: Brought up 1 node, 2 CPUs
[    0.110357] SMP: Total of 2 processors activated.
[    0.115028] CPU features: detected: 32-bit EL0 Support
[    0.120154] CPU features: detected: 32-bit EL1 Support
[    0.125257] CPU features: detected: Data cache clean to the PoU not required for I/D coherence
[    0.133840] CPU features: detected: Common not Private translations
[    0.140073] CPU features: detected: CRC32 instructions
[    0.145196] CPU features: detected: RCpc load-acquire (LDAPR)
[    0.150906] CPU features: detected: LSE atomic instructions
[    0.156453] CPU features: detected: Privileged Access Never
[    0.161998] CPU features: detected: RAS Extension Support
[    0.167374] CPU features: detected: Speculative Store Bypassing Safe (SSBS)
[    0.174355] CPU: All CPU(s) started at EL2
[    0.178380] alternatives: applying system-wide alternatives
[    0.187922] devtmpfs: initialized
[    0.194925] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.204430] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.216607] pinctrl core: initialized pinctrl subsystem
[    0.223019] DMI not present or invalid.
[    0.227066] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.233367] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[    0.240250] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.247941] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.255804] audit: initializing netlink subsys (disabled)
[    0.261291] audit: type=2000 audit(0.172:1): state=initialized audit_enabled=0 res=1
[    0.261671] thermal_sys: Registered thermal governor 'step_wise'
[    0.268851] thermal_sys: Registered thermal governor 'power_allocator'
[    0.274855] cpuidle: using governor menu
[    0.285411] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.292025] ASID allocator initialised with 65536 entries
[    0.297950] Serial: AMBA PL011 UART driver
[    0.301832] imx mu driver is registered.
[    0.305685] imx rpmsg driver is registered.
[    0.314130] imx93-pinctrl 443c0000.pinctrl: initialized IMX pinctrl driver
[    0.326962] Modules: 24576 pages in range for non-PLT usage
[    0.326973] Modules: 516096 pages in range for PLT usage
[    0.333009] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.344824] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.351063] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.357821] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.364062] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.370821] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.377062] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.383821] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.391518] ACPI: Interpreter disabled.
[    0.395792] iommu: Default domain type: Translated
[    0.400360] iommu: DMA domain TLB invalidation policy: strict mode
[    0.406743] SCSI subsystem initialized
[    0.410355] libata version 3.00 loaded.
[    0.410523] usbcore: registered new interface driver usbfs
[    0.415761] usbcore: registered new interface driver hub
[    0.421054] usbcore: registered new device driver usb
[    0.426646] mc: Linux media interface: v0.10
[    0.430689] videodev: Linux video capture interface: v2.00
[    0.436154] pps_core: LinuxPPS API ver. 1 registered
[    0.441049] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti 
[    0.450155] PTP clock support registered
[    0.454144] EDAC MC: Ver: 3.0.0
[    0.457601] scmi_core: SCMI protocol bus registered
[    0.462617] FPGA manager framework
[    0.465811] Advanced Linux Sound Architecture Driver Initialized.
[    0.472369] Bluetooth: Core ver 2.22
[    0.475701] NET: Registered PF_BLUETOOTH protocol family
[    0.480981] Bluetooth: HCI device and connection manager initialized
[    0.487298] Bluetooth: HCI socket layer initialized
[    0.492148] Bluetooth: L2CAP socket layer initialized
[    0.497182] Bluetooth: SCO socket layer initialized
[    0.502337] vgaarb: loaded
[    0.505250] clocksource: Switched to clocksource arch_sys_counter
[    0.511308] VFS: Disk quotas dquot_6.6.0
[    0.515015] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.521961] pnp: PnP ACPI: disabled
[    0.530265] NET: Registered PF_INET protocol family
[    0.535027] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.542962] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[    0.551110] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.558774] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.566509] TCP bind hash table entries: 8192 (order: 6, 262144 bytes, linear)
[    0.573930] TCP: Hash tables configured (established 8192 bind 8192)
[    0.580120] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.586625] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.593729] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.599609] RPC: Registered named UNIX socket transport module.
[    0.605277] RPC: Registered udp transport module.
[    0.609945] RPC: Registered tcp transport module.
[    0.614624] RPC: Registered tcp-with-tls transport module.
[    0.620084] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.627260] PCI: CLS 0 bytes, default 64
[    0.631165] kvm [1]: IPA Size Limit: 40 bits
[    0.635194] kvm [1]: GICv3: no GICV resource entry
[    0.639942] kvm [1]: disabling GICv2 emulation
[    0.644371] kvm [1]: GIC system register CPU interface enabled
[    0.650191] kvm [1]: vgic interrupt IRQ9
[    0.654088] kvm [1]: VHE mode initialized successfully
[    0.660051] Initialise system trusted keyrings
[    0.664421] workingset: timestamp_bits=42 max_order=18 bucket_order=0
[    0.670898] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.676710] NFS: Registering the id_resolver key type
[    0.681531] Key type id_resolver registered
[    0.685658] Key type id_legacy registered
[    0.689659] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.696326] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.703831] 9p: Installing v9fs 9p2000 file system support
[    0.734526] Key type asymmetric registered
[    0.738370] Asymmetric key parser 'x509' registered
[    0.743258] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[    0.750590] io scheduler mq-deadline registered
[    0.755095] io scheduler kyber registered
[    0.759113] io scheduler bfq registered
[    0.766447] EINJ: ACPI disabled.
[    0.773498] Bus freq driver module loaded
[    0.782271] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.790543] 44380000.serial: ttyLP0 at MMIO 0x44380010 (irq = 17, base_baud = 1500000) is a FSL_LPUART
[    0.799853] printk: console [ttyLP0] enabled
[    0.808289] printk: bootconsole [lpuart32] disabled
[    0.827377] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    0.835386] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[    0.844862] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with 4ae30000.lcd-controller
[    0.858799] loop: module loaded
[    0.863014] megasas: 07.725.01.00-rc1
[    0.870948] tun: Universal TUN/TAP device driver, 1.6
[    0.876567] thunder_xcv, ver 1.0
[    0.879836] thunder_bgx, ver 1.0
[    0.883080] nicpf, ver 1.0
[    0.886825] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[    0.894055] hns3: Copyright (c) 2017 Huawei Corporation.
[    0.899390] hclge is initializing
[    0.902728] e1000: Intel(R) PRO/1000 Network Driver
[    0.907598] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    0.913354] e1000e: Intel(R) PRO/1000 Network Driver
[    0.918310] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    0.924238] igb: Intel(R) Gigabit Ethernet Network Driver
[    0.929635] igb: Copyright (c) 2007-2014 Intel Corporation.
[    0.935216] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.941476] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.947488] sky2: driver version 1.30
[    0.951466] usbcore: registered new device driver r8152-cfgselector
[    0.957746] usbcore: registered new interface driver r8152
[    0.963616] VFIO - User Level meta-driver version: 0.3
[    0.970278] usbcore: registered new interface driver uas
[    0.975636] usbcore: registered new interface driver usb-storage
[    0.981731] usbcore: registered new interface driver usbserial_generic
[    0.988270] usbserial: USB Serial support registered for generic
[    0.994286] usbcore: registered new interface driver ftdi_sio
[    1.000031] usbserial: USB Serial support registered for FTDI USB Serial Device
[    1.007339] usbcore: registered new interface driver usb_serial_simple
[    1.013862] usbserial: USB Serial support registered for carelink
[    1.019959] usbserial: USB Serial support registered for flashloader
[    1.026317] usbserial: USB Serial support registered for funsoft
[    1.032327] usbserial: USB Serial support registered for google
[    1.038251] usbserial: USB Serial support registered for hp4x
[    1.043996] usbserial: USB Serial support registered for kaufmann
[    1.050089] usbserial: USB Serial support registered for libtransistor
[    1.056614] usbserial: USB Serial support registered for moto_modem
[    1.062880] usbserial: USB Serial support registered for motorola_tetra
[    1.069494] usbserial: USB Serial support registered for nokia
[    1.075326] usbserial: USB Serial support registered for novatel_gps
[    1.081686] usbserial: USB Serial support registered for siemens_mpi
[    1.088040] usbserial: USB Serial support registered for suunto
[    1.093963] usbserial: USB Serial support registered for vivopay
[    1.099966] usbserial: USB Serial support registered for zio
[    1.105629] usbcore: registered new interface driver usb_ehset_test
[    1.114691] input: 44440000.bbnsm:pwrkey as /devices/platform/soc@0/44000000.bus/44440000.bbnsm/44440000.bbnsm:pwrkey/input/input0
[    1.126836] i2c_dev: i2c /dev entries driver
[    1.133908] imx7ulp-wdt 42490000.watchdog: imx93 wdt probe
[    1.165969] Bluetooth: HCI UART driver ver 2.3
[    1.170432] Bluetooth: HCI UART protocol H4 registered
[    1.175564] Bluetooth: HCI UART protocol BCSP registered
[    1.180885] Bluetooth: HCI UART protocol LL registered
[    1.186018] Bluetooth: HCI UART protocol ATH3K registered
[    1.191417] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    1.197782] Bluetooth: HCI UART protocol Broadcom registered
[    1.203454] Bluetooth: HCI UART protocol QCA registered
[    1.209726] sdhci: Secure Digital Host Controller Interface driver
[    1.215922] sdhci: Copyright(c) Pierre Ossman
[    1.220572] Synopsys Designware Multimedia Card Interface Driver
[    1.226885] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.233614] ledtrig-cpu: registered to indicate activity on CPUs
[    1.240850] fsl-se-fw se-fw2: failed to init reserved memory region -19
[    1.247608] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    1.254330] usbcore: registered new interface driver usbhid
[    1.259901] usbhid: USB HID core driver
[    1.270337] mmc0: SDHCI controller on 42850000.mmc [42850000.mmc] using ADMA
[    1.302222] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available
[    1.312041]  cs_system_cfg: CoreSight Configuration manager initialised
[    1.319751] optee: probing for conduit method.
[    1.324215] optee: api uid mismatch
[    1.325699] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[    1.327700] optee: probe of firmware:optee failed with error -22
[    1.334598] mmcblk0: mmc0:0001 eMMC   58.2 GiB
[    1.342512] NET: Registered PF_LLC protocol family
[    1.345923]  mmcblk0: p1
[    1.349519] u32 classifier
[    1.352252] mmcblk0boot0: mmc0:0001 eMMC   4.00 MiB
[    1.354567]     input device check on
[    1.360666] mmcblk0boot1: mmc0:0001 eMMC   4.00 MiB
[    1.363094]     Actions configured
[    1.363485] NET: Registered PF_INET6 protocol family
[    1.368956] mmcblk0rpmb: mmc0:0001 eMMC   4.00 MiB, chardev (234:0)
[    1.372113] Segment Routing with IPv6
[    1.386309] In-situ OAM (IOAM) with IPv6
[    1.390278] NET: Registered PF_PACKET protocol family
[    1.395349] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    1.408425] Bluetooth: RFCOMM TTY layer initialized
[    1.413310] Bluetooth: RFCOMM socket layer initialized
[    1.418455] Bluetooth: RFCOMM ver 1.11
[    1.422203] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    1.427502] Bluetooth: BNEP filters: protocol multicast
[    1.432721] Bluetooth: BNEP socket layer initialized
[    1.437676] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    1.443589] Bluetooth: HIDP socket layer initialized
[    1.448783] 8021q: 802.1Q VLAN Support v1.8
[    1.452998] lib80211: common routines for IEEE802.11 drivers
[    1.458652] lib80211_crypt: registered algorithm 'NULL'
[    1.458656] lib80211_crypt: registered algorithm 'WEP'
[    1.458659] lib80211_crypt: registered algorithm 'CCMP'
[    1.458663] lib80211_crypt: registered algorithm 'TKIP'
[    1.458693] 9pnet: Installing 9P2000 support
[    1.463084] Key type dns_resolver registered
[    1.467497] NET: Registered PF_VSOCK protocol family
[    1.486367] registered taskstats version 1
[    1.490717] Loading compiled-in X.509 certificates
[    1.512663] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[    1.521013] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[    1.539006] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with ldb-phy
[    1.550623] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    1.558672] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[    1.569462] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found
[    1.575451] imx-dwmac 428a0000.ethernet: tx clock enable start
[    1.581464] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[    1.588255] imx-dwmac 428a0000.ethernet: 	DWMAC4/5
[    1.593038] imx-dwmac 428a0000.ethernet: DMA HW capability register supported
[    1.600159] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported
[    1.607283] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported
[    1.613973] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported
[    1.620110] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[    1.627757] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[    1.634536] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)
[    1.641316] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[    1.648876] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width
[    1.657380] imx-dwmac 428a0000.ethernet: tx clock disable start
[    1.663414] imx-dwmac 428a0000.ethernet: err_drv_probe
[    1.668557] imx-dwmac 428a0000.ethernet: err_dwmac_init
[    1.677361] ci_hdrc ci_hdrc.0: EHCI Host Controller
[    1.682306] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[    1.709253] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[    1.715211] hub 1-0:1.0: USB hub found
[    1.718981] hub 1-0:1.0: 1 port detected
[    1.726882] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    1.731789] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[    1.753257] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    1.759191] hub 2-0:1.0: USB hub found
[    1.762965] hub 2-0:1.0: 1 port detected
[    1.770674] rtc rtc0: Power loss detected, invalid time
[    1.776048] rtc-pcf85063 0-0051: registered as rtc0
[    1.781185] rtc rtc0: Power loss detected, invalid time
[    1.786407] rtc-pcf85063 0-0051: hctosys: unable to read the hardware clock
[    1.793553] pca953x 0-0020: supply vcc not found, using dummy regulator
[    1.800254] pca953x 0-0020: using no AI
[    1.804716] i2c i2c-0: LPI2C adapter registered
[    1.810507] pca953x 1-0022: supply vcc not found, using dummy regulator
[    1.817269] pca953x 1-0022: using AI
[    1.822077] at24 1-0050: supply vcc not found, using dummy regulator
[    1.828917] at24 1-0050: 1024 byte 24c08 EEPROM, writable, 16 bytes/write
[    1.835795] i2c i2c-1: LPI2C adapter registered
[    1.841329] i2c i2c-2: LPI2C adapter registered
[    1.846907] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    1.854932] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[    1.865632] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found
[    1.871579] imx-dwmac 428a0000.ethernet: tx clock enable start
[    1.877611] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[    1.884419] imx-dwmac 428a0000.ethernet: 	DWMAC4/5
[    1.889206] imx-dwmac 428a0000.ethernet: DMA HW capability register supported
[    1.896327] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported
[    1.903449] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported
[    1.910153] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported
[    1.916235] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[    1.923878] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[    1.930655] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)
[    1.937446] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[    1.945009] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width
[    2.091986] imx-dwmac 428a0000.ethernet: tx clock disable start
[    2.092418] sdhci-esdhc-imx 42860000.mmc: Got CD GPIO
[    2.099328] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    2.111052] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[    2.122102] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    2.130156] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[    2.134093] mmc1: SDHCI controller on 42860000.mmc [42860000.mmc] using ADMA
[    2.139573] nxp-pca9450 1-0025: pca9451a probed.
[    2.152583] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    2.160637] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[    2.171559] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    2.180575] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    2.186741] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[    2.194068] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    2.197312] clk: Disabling unused clocks
[    2.202716] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[    2.214819] ALSA device list:
[    2.217793]   No soundcards found.
[    2.221596] Waiting for root device /dev/mmcblk1p2...
[    2.287788] mmc1: host does not support reading read-only switch, assuming write-enable
[    2.298005] mmc1: new high speed SD card at address 0001
[    2.303890] mmcblk1: mmc1:0001 00000 1.81 GiB
[    2.311020]  mmcblk1: p1 p2
[    2.315100] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    2.323111] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[    2.339143] exFAT-fs (mmcblk1p2): invalid boot record signature
[    2.345082] exFAT-fs (mmcblk1p2): failed to read boot sector
[    2.350777] exFAT-fs (mmcblk1p2): failed to recognize exfat type
[    2.358002] erofs: (device mmcblk1p2): mounted with root inode @ nid 36.
[    2.364768] VFS: Mounted root (erofs filesystem) readonly on device 179:98.
[    2.371789] devtmpfs: mounted
[    2.375967] Freeing unused kernel memory: 1984K
[    2.380690] Run /sbin/init as init process
[    2.384782]   with arguments:
[    2.384785]     /sbin/init
[    2.384787]   with environment:
[    2.384790]     HOME=/
[    2.384792]     TERM=linux
[    4.633259] random: crng init done
[   12.406378] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[   12.414399] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[   12.424617] platform imx-lcdifv3-crtc.0: deferred probe pending

当 ip link 设置 eth0 时(我向驱动程序添加了一些非标准跟踪,以尝试调试此 DMA 问题):

# ip link set eth0 up
[  236.851517] imx-dwmac 428a0000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[  236.859339] imx-dwmac 428a0000.ethernet: tx clock enable start
[  236.974901] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[  236.982933] imx93-ldb ldb-display-controller: No data-mapping in DT, will use negotiated bus format.
[  237.081392] imx-dwmac 428a0000.ethernet eth0: PHY [stmmac-1:00] driver [Generic PHY] (irq=POLL)
[  237.090112] Checking DMA clocks before reset...
[  237.094643] DMA_HW_CAPABILITY = 0x0
[  237.098124] RESET START: DMA_BUS_MODE = 0x1
[  237.102301] AFTER WRITE: DMA_BUS_MODE = 0x1
[  238.107432] POLL RESULT: ret=-110, DMA_BUS_MODE = 0x1
[  238.112492] imx-dwmac 428a0000.ethernet: Failed to reset the dma
[  238.118519] imx-dwmac 428a0000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[  238.127210] imx-dwmac 428a0000.ethernet eth0: __stmmac_open: Hw setup failed
[  238.194819] imx-dwmac 428a0000.ethernet: tx clock disable start
ip: SIOCSIFFLAGS: Connection timed out

感谢您的帮助!

顺祝商祺!

朱利安

Re: DMA Error with imx93 and eqos in RMII

你好,

请确认PHY中的复位信号是否正确生效。

当 PHY 在短时间内没有获得时钟信号,并且时钟信号恢复后,必须对 PHY 进行 RESET,以锁存所有配置带,恢复到正常工作模式。

请分享您的完整 dmesg 日志。

顺祝商祺!

Re: DMA Error with imx93 and eqos in RMII

你好,

谢谢你提供的信息。

由于可以访问寄存器,MAC 不会完全保持 RESET 状态。

能否提供原理图连接图,以便确认 REF_CLK 的提供方式?

另外,请在 `cat /sys/kernel/debug/clk/clk_summary` 文件中分享您的时钟摘要信息。

顺祝商祺!

Re: DMA Error with imx93 and eqos in RMII

关于ref_clk和原理图的回复,请查看另一条消息,我好像不小心按错了回复按钮。

我还尝试了以下方法: https://community.nxp.com/t5/i-MX-Processors/i-MX93-EQoS-RMII-mode-with-internal-50MHz-reference-clo... ,这看起来很像同一个问题,但也没能成功解决。

感谢您的支持!

Re: DMA Error with imx93 and eqos in RMII

我不想在公共论坛上分享完整的原理图。我可以私下发送吗?

REF_CLK 通过 ENET1_TD2(imx93 的 U12 引脚)提供。在设备树中,就是这一行:

 MX93_PAD_ENET1_TD2__CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK 0x57e

我们已经用示波器检查过,在 u-启动 下时钟是正确的,但是我们遇到了类似的 DMA 错误(细节较少)。

在 Linux 系统下,某些东西停止了时钟(我猜测是 DMA 错误触发信号,使时钟的版本随后被 Linux 内核停止,因为它未使用)。

以下是 clk_summary 的内容:

                                 enable  prepare  protect                                duty  hardware                            connection
   clock                          count    count    count        rate   accuracy phase  cycle    enable   consumer                         id
---------------------------------------------------------------------------------------------------------------------------------------------
 pcf85063-clkout                     0       0        0        0           0          0     50000      Y   deviceless                      no_connection_id         
 sys_pll_pfd2                        1       1        0        625000000   0          0     50000      Y   deviceless                      no_connection_id         
    wakeup_axi_root                  2       2        0        312500000   0          0     50000      Y      42860000.mmc                    ahb                      
                                                                                                              42850000.mmc                    ahb                      
                                                                                                              deviceless                      no_connection_id         
       enet_qos                      0       0        0        312500000   0          0     50000      N         428a0000.ethernet               mem                      
                                                                                                                 428a0000.ethernet               pclk                     
                                                                                                                 428a0000.ethernet               stmmaceth                
                                                                                                                 deviceless                      no_connection_id         
       enet1                         0       0        0        312500000   0          0     50000      N         42890000.ethernet               ahb                      
                                                                                                                 42890000.ethernet               ipg                      
                                                                                                                 deviceless                      no_connection_id         
       edma2                         1       1        0        312500000   0          0     50000      Y         42000000.dma-controller         edma                     
                                                                                                                 deviceless                      no_connection_id         
    sys_pll_pfd2_div2                0       0        0        312500000   0          0     50000      Y      deviceless                      no_connection_id         
 sys_pll_pfd1                        3       3        0        800000000   0          0     50000      Y   deviceless                      no_connection_id         
    media_axi_root                   1       1        0        400000000   0          0     50000      Y      4ae30000.lcd-controller         disp-axi                 
                                                                                                              4ac10000.system-controller      axi                      
                                                                                                              deviceless                      no_connection_id         
       nic_media                     1       1        0        400000000   0          0     50000      Y         4ac10000.system-controller      nic                      
                                                                                                                 power-domain@44462400           no_connection_id         
                                                                                                                 deviceless                      no_connection_id         
    nic_axi_root                     1       1        0        400000000   0          0     50000      Y      deviceless                      no_connection_id         
    ccm_cko4_root                    0       0        0        266666667   0          0     50000      N      deviceless                      no_connection_id         
    ccm_cko3_root                    0       0        0        266666667   0          0     50000      N      deviceless                      no_connection_id         
    ccm_cko2_root                    0       0        0        266666667   0          0     50000      N      deviceless                      no_connection_id         
    ccm_cko1_root                    0       0        0        266666667   0          0     50000      N      deviceless                      no_connection_id         
    usdhc3_root                      0       0        0        200000000   0          0     50000      N      deviceless                      no_connection_id         
       usdhc3                        0       0        0        200000000   0          0     50000      N         deviceless                      no_connection_id         
    usdhc2_root                      0       0        0        400000000   0          0     50000      N      deviceless                      no_connection_id         
       usdhc2                        0       0        0        400000000   0          0     50000      N         42860000.mmc                    per                      
                                                                                                                 deviceless                      no_connection_id         
    usdhc1_root                      0       0        0        400000000   0          0     50000      N      deviceless                      no_connection_id         
       usdhc1                        0       0        0        400000000   0          0     50000      N         42850000.mmc                    per                      
                                                                                                                 deviceless                      no_connection_id         
    flexspi1_root                    0       0        0        200000000   0          0     50000      N      deviceless                      no_connection_id         
       flexspi1                      0       0        0        200000000   0          0     50000      N         deviceless                      no_connection_id         
    sys_pll_pfd1_div2                6       6        0        400000000   0          0     50000      Y      deviceless                      no_connection_id         
       enet_ref_phy_root             0       0        0        50000000    0          0     50000      N         42890000.ethernet               enet_out                 
                                                                                                                 deviceless                      no_connection_id         
       enet_timer1_root              0       0        0        100000000   0          0     50000      N         42890000.ethernet               ptp                      
                                                                                                                 deviceless                      no_connection_id         
       enet_timer2_root              0       0        0        100000000   0          0     50000      N         428a0000.ethernet               ptp_ref                  
                                                                                                                 deviceless                      no_connection_id         
       media_apb_root                1       2        0        133333334   0          0     50000      Y         ldb-phy                         apb                      
                                                                                                                 system-controller@4ac10000      no_connection_id         
                                                                                                                 4ac10000.system-controller      apb                      
                                                                                                                 power-domain@44462400           no_connection_id         
                                                                                                                 deviceless                      no_connection_id         
          isi                        0       0        0        133333334   0          0     50000      N            4ac10000.system-controller      isi                      
                                                                                                                    deviceless                      no_connection_id         
          pxp                        0       0        0        133333334   0          0     50000      N            4ac10000.system-controller      pxp                      
                                                                                                                    deviceless                      no_connection_id         
          lcdif                      0       0        0        133333334   0          0     50000      N            4ae30000.lcd-controller         disp-apb                 
                                                                                                                    4ac10000.system-controller      lcdif                    
                                                                                                                    deviceless                      no_connection_id         
          mipi_dsi                   0       0        0        133333334   0          0     50000      N            4ac10000.system-controller      dsi                      
                                                                                                                    deviceless                      no_connection_id         
          mipi_csi                   0       0        0        133333334   0          0     50000      N            4ac10000.system-controller      csi                      
                                                                                                                    deviceless                      no_connection_id         
       hsio_root                     1       1        0        133333334   0          0     50000      Y         deviceless                      no_connection_id         
          usb_controller             0       0        0        133333334   0          0     50000      N            4c200000.usb                    no_connection_id         
                                                                                                                    4c100000.usb                    no_connection_id         
                                                                                                                    deviceless                      no_connection_id         
       lpspi4_root                   0       0        0        50000000    0          0     50000      N         deviceless                      no_connection_id         
          lpspi4                     0       0        0        50000000    0          0     50000      N            deviceless                      no_connection_id         
       lpspi3_root                   0       0        0        50000000    0          0     50000      N         deviceless                      no_connection_id         
          lpspi3                     0       0        0        50000000    0          0     50000      N            deviceless                      no_connection_id         
       lpspi2_root                   0       0        0        50000000    0          0     50000      N         deviceless                      no_connection_id         
          lpspi2                     0       0        0        50000000    0          0     50000      N            deviceless                      no_connection_id         
       lpspi1_root                   0       0        0        50000000    0          0     50000      N         deviceless                      no_connection_id         
          lpspi1                     0       0        0        50000000    0          0     50000      N            deviceless                      no_connection_id         
       swo_trace_root                0       0        0        133333334   0          0     50000      N         deviceless                      no_connection_id         
       bus_aon_root                  1       1        0        133333334   0          0     50000      Y         i2c@44350000                    no_connection_id         
                                                                                                                 i2c@44340000                    no_connection_id         
                                                                                                                 deviceless                      no_connection_id         
          tstmr1                     0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          pdm_ipg_clk                0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          sai1_ipg_clk               0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          tpm1                       0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          lpit1                      0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          mu1_b                      0       0        0        133333334   0          0     50000      N            44230000.mailbox                no_connection_id         
                                                                                                                    deviceless                      no_connection_id         
          mu1_a                      0       0        0        133333334   0          0     50000      Y            deviceless                      no_connection_id         
          sema1                      0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
       bus_wakeup_root               4       4        0        133333334   0          0     50000      Y         42860000.mmc                    ipg                      
                                                                                                                 i2c@42530000                    no_connection_id         
                                                                                                                 42850000.mmc                    ipg                      
                                                                                                                 deviceless                      no_connection_id         
          tstmr2                     0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          sai3_ipg_clk               0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          sai2_ipg_clk               0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          tpm3                       0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          lpit2                      0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
          gpio4                      2       2        0        133333334   0          0     50000      Y            43830000.gpio                   gpio                     
                                                                                                                    43830000.gpio                   port                     
                                                                                                                    deviceless                      no_connection_id         
          gpio3                      2       2        0        133333334   0          0     50000      Y            43820000.gpio                   gpio                     
                                                                                                                    43820000.gpio                   port                     
                                                                                                                    deviceless                      no_connection_id         
          gpio2                      2       2        0        133333334   0          0     50000      Y            43810000.gpio                   gpio                     
                                                                                                                    43810000.gpio                   port                     
                                                                                                                    deviceless                      no_connection_id         
          mu2_b                      0       0        0        133333334   0          0     50000      N            42440000.mailbox                no_connection_id         
                                                                                                                    deviceless                      no_connection_id         
          mu2_a                      0       0        0        133333334   0          0     50000      Y            deviceless                      no_connection_id         
          sema2                      0       0        0        133333334   0          0     50000      N            deviceless                      no_connection_id         
       m33_root                      4       4        0        200000000   0          0     50000      Y         deviceless                      no_connection_id         
          gpio1                      2       2        0        200000000   0          0     50000      Y            47400000.gpio                   gpio                     
                                                                                                                    47400000.gpio                   port                     
                                                                                                                    deviceless                      no_connection_id         
          edma1                      1       1        0        200000000   0          0     50000      Y            44000000.dma-controller         edma                     
                                                                                                                    deviceless                      no_connection_id         
          cm33                       1       1        0        200000000   0          0     50000      Y            deviceless                      no_connection_id         
       a55_mtr_bus_root              1       1        0        133333334   0          0     50000      Y         deviceless                      no_connection_id         
 sys_pll_pfd0                        2       2        0        1000000000  0          0     50000      Y   deviceless                      no_connection_id         
    a55_alt_root                     1       1        0        500000000   0          0     50000      Y      deviceless                      no_connection_id         
       a55_alt                       0       0        0        500000000   0          0     50000      N         deviceless                      no_connection_id         
    a55_periph_root                  1       1        0        333333334   0          0     50000      Y      deviceless                      no_connection_id         
    sys_pll_pfd0_div2                0       0        0        500000000   0          0     50000      Y      deviceless                      no_connection_id         
       usb_phy_root                  0       0        0        50000000    0          0     50000      N         usbphynop2                      main_clk                 
                                                                                                                 usbphynop1                      main_clk                 
                                                                                                                 deviceless                      no_connection_id         
       enet_ref_root                 0       0        0        250000000   0          0     50000      N         42890000.ethernet               enet_clk_ref             
                                                                                                                 deviceless                      no_connection_id         
       enet_root                     0       0        0        50000000    0          0     50000      N         428a0000.ethernet               tx                       
                                                                                                                 deviceless                      no_connection_id         
 dummy                               0       0        0        0           0          0     50000      Y   deviceless                      no_connection_id         
 clk_ext1                            0       0        0        133000000   0          0     50000      Y   clock-controller@44450000       clk_ext1                 
                                                                                                           deviceless                      no_connection_id         
 osc_24m                             6       6        3        24000000    0          0     50000      Y   clock-controller@44450000       osc_24m                  
                                                                                                           timer@44290000                  per                      
                                                                                                           deviceless                      no_connection_id         
    pmro                             0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    tmc                              1       1        0        24000000    0          0     50000      Y      44482000.tmu                    no_connection_id         
                                                                                                              deviceless                      no_connection_id         
    sys_cnt                          1       1        0        24000000    0          0     50000      Y      deviceless                      no_connection_id         
    hsio_trout_24m                   0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    wdog5                            0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    wdog4                            0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    wdog3                            1       1        0        24000000    0          0     50000      Y      42490000.watchdog               no_connection_id         
                                                                                                              deviceless                      no_connection_id         
    wdog2                            0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    wdog1                            0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    pal_came_scan_root               0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    i3c2_slow_root                   0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    i3c1_slow_root                   0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    spdif_root                       0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       spdif                         0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    audio_xcvr_root                  0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       aud_xcvr                      0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    mqs2_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    mqs1_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    tstmr2_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    tstmr1_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    pdm_root                         0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       pdm                           0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    adc_root                         0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       adc1                          0       0        0        24000000    0          0     50000      N         44530000.adc                    ipg                      
                                                                                                                 deviceless                      no_connection_id         
    mipi_phy_cfg_root                0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    mipi_test_byte_root              0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    cam_pix_root                     0       0        0        24000000    0          0     50000      N      4ac10000.system-controller      cam                      
                                                                                                              deviceless                      no_connection_id         
    ml_root                          0       0        0        24000000    0          0     50000      N      power-domain@44461800           no_connection_id         
                                                                                                              deviceless                      no_connection_id         
    ml_apb_root                      0       0        0        24000000    0          0     50000      N      power-domain@44461800           no_connection_id         
                                                                                                              deviceless                      no_connection_id         
    hsio_acscan_480m_root            0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    hsio_acscan_80m_root             0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    hsio_usb_test_60m_root           0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       usb_test_60m                  0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    sai3_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       mqs2                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
       sai3                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    sai2_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       sai2                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    sai1_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       mqs1                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
       sai1                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    i3c2_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       i3c2                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    i3c1_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       i3c1                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpspi8_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpspi8                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpspi7_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpspi7                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpspi6_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpspi6                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpspi5_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpspi5                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpi2c8_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c8                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpi2c7_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c7                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpi2c6_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c6                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpi2c5_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c5                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpi2c4_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c4                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpi2c3_root                      0       0        1        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c3                        0       0        1        24000000    0          0     50000      N         i2c@42530000                    no_connection_id         
                                                                                                                 deviceless                      no_connection_id         
    lpi2c2_root                      0       0        1        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c2                        0       0        1        24000000    0          0     50000      N         i2c@44350000                    no_connection_id         
                                                                                                                 deviceless                      no_connection_id         
    lpi2c1_root                      0       0        1        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpi2c1                        0       0        1        24000000    0          0     50000      N         i2c@44340000                    no_connection_id         
                                                                                                                 deviceless                      no_connection_id         
    lpuart8_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpuart8                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpuart7_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpuart7                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpuart6_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpuart6                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpuart5_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpuart5                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpuart4_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpuart4                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpuart3_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpuart3                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpuart2_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lpuart2                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lpuart1_root                     1       1        0        24000000    0          0     50000      Y      deviceless                      no_connection_id         
       lpuart1                       1       1        0        24000000    0          0     50000      Y         44380000.serial                 ipg                      
                                                                                                                 deviceless                      no_connection_id         
    can2_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       can2                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    can1_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       can1                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    tpm6_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       tpm6                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    tpm5_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       tpm5                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    tpm4_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       tpm4                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    tpm2_root                        0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       tpm2                          0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lptmr2_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lptmr2                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    lptmr1_root                      0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       lptmr1                        0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    flexio2_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       flexio2                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    flexio1_root                     0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
       flexio1                       0       0        0        24000000    0          0     50000      N         deviceless                      no_connection_id         
    m33_systick_root                 0       0        0        24000000    0          0     50000      N      deviceless                      no_connection_id         
    video_pll                        0       0        0        1039500000  0          0     50000      Y      deviceless                      no_connection_id         
       media_disp_pix_root           0       0        0        148500000   0          0     50000      N         4ae30000.lcd-controller         pix                      
                                                                                                                 4ac10000.system-controller      disp                     
                                                                                                                 deviceless                      no_connection_id         
       media_ldb_root                0       0        0        1039500000  0          0     50000      N         deviceless                      no_connection_id         
          lvds                       0       0        0        1039500000  0          0     50000      N            deviceless                      no_connection_id         
    audio_pll                        0       0        0        393216000   0          0     50000      Y      deviceless                      no_connection_id         
    arm_pll                          1       1        0        1700000000  0          0     50000      Y      deviceless                      no_connection_id         
       a55_sel                       1       1        0        1700000000  0          0     50000      Y         deviceless                      no_connection_id         
          a55_core                   1       1        0        1700000000  0          0     50000      Y            deviceless                      no_connection_id         
 osc_32k                             1       1        0        32768       0          0     50000      Y   clock-controller@44450000       osc_32k                  
                                                                                                           deviceless                      no_connection_id         
    hsio_32k                         2       2        0        32768       0          0     50000      Y      4c200000.usb                    usb_wakeup_clk           
                                                                                                              4c100000.usb                    usb_wakeup_clk           
                                                                                                              deviceless                      no_connection_id         
# 

Re: DMA Error with imx93 and eqos in RMII

我终于成功运行了,使用了链接中的补丁和以下设置:


&eqos {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_eqos>;
        phy-mode = "rmii";
        phy-handle = <&ethphy1>;
        status = "okay";

        assigned-clock-parents = <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>,
                         <&clk IMX93_CLK_SYS_PLL_PFD0_DIV2>;
        assigned-clock-rates = <100000000>, <50000000>;
        enet_clk_sel = <&wakeupmix_gpr 0x2C>;

        clk_csr = <5>;
//      snps,rmii_refclk_ext;

        mdio {
                compatible = "snps,dwmac-mdio";
                #address-cells = <1>;
                #size-cells = <0>;
                clock-frequency = <5000000>;

                ethphy1: ethernet-phy@0 {
                        reg = <0>;
                        eee-broken-1000tx;
                        reset-gpios = <&pcal6524 19 GPIO_ACTIVE_LOW>;
                        reset-assert-us = <15000>;
                        reset-deassert-us = <100000>;
                        smsc,disable-energy-detect;
                };
        };
};

能否解释一下https://community.nxp.com/t5/i-MX-Processors/i-MX93-EQoS-RMII-mode-with-internal-50MHz-reference-clo...中的补丁是什么?确实需要吗?为什么需要?

另外,这些更改难道不应该提交到上游吗?因为它们看起来像是 SoC 的常规用例,没什么特别的。

Re: DMA Error with imx93 and eqos in RMII

你好,

很高兴知道现在一切正常。

该补丁修改了驱动程序 dwmac-imx/EQoS,以便在 RMII 使用外部时钟时配置 ENET_QOS。

之所以需要进行此项更改,是因为 EQoS 在 DMA RESET 期间需要恒定的时钟。

顺祝商祺!

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎08-01-2026 03:30 AM
更新者: