Clarification on MBIST Availability and Usage in i.MX RT1170 Hello Team, We are currently using the i.MX RT1176 in a space application and would appreciate some clarification regarding the Memory Built-In Self-Test (MBIST) functionality referenced in the Cortex-M7 subsystem. While reviewing the Reference Manual, we noticed a single mention of "MBIST access" in the TCM_MASTER encoding table (shown below). However, we could not find any further documentation describing MBIST registers, control interfaces, configuration procedures, or software APIs. Based on the limited information available, our current understanding is that the MBIST functionality may not be exposed to user applications. We would appreciate confirmation on the following points: Is the MBIST functionality available to customer software on the i.MX RT1170 family? If so, is there any documented software interface, register set, or programming guide that describes how it can be invoked and monitored? If not, is the MBIST implementation intended solely for internal manufacturing, test, or diagnostic purposes? If MBIST is accessible, which memory regions are supported? ITCM DTCM OCRAM FlexRAM banks Any other internal SRAM blocks Are there any application notes, safety manuals, or additional documentation available that describe MBIST support and limitations for the i.MX RT1170 devices? The reference that led to this question is the TCM_MASTER field definition, which lists an encoding corresponding to "MBIST access", but no further details could be found in the Reference Manual. Thank you for your assistance. We look forward to your clarification. Best regards, Ruthvik R Re: Clarification on MBIST Availability and Usage in i.MX RT1170 Hi @Gavin_Jia , Thanks for the quick reply and clarification, Thanks and regards, Ruthvik Re: Clarification on MBIST Availability and Usage in i.MX RT1170 Hi @ruthvik_1 ,
Thank you for your questions!
For RT1170, we have not identified a documented, supported MBIST control interface, register configuration procedure, or SDK API for customer software. Therefore, we cannot currently provide a supported method for invoking MBIST.
“MBIST access” in TCM_MASTER identifies the source of an access request. It is not an MBIST control interface and does not establish that application software can initiate MBIST.
For comparison, AN14969 documents software-controlled BIST on S32K3xx using STCU2 and the SPD driver, including configuration, execution, and result checking. However, this document and its procedures do not apply to RT1170.
Best regards, Gavin
View full article