Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
PN7160A and linux_libnfc-nci on Raspberry Pi 5 2026 64-bit Trixie Hello, I am trying to bring up a PN7160A for a work project and cannot manage to get any attempt of linux_libnfc-nci to work. The patch is obsolete, lgpiod had a overhaul going to version 2. Also have to use flag sudo make install CFLAGS="-Wno-error=implicit-function-declaration" " otherwise I get "demoapp/main.c: In function ‘onMessageReceived’: demoapp/main.c:451:5: error: implicit declaration of function ‘PrintNDEFContent’ [-Wimplicit-function-declaration] 451 | PrintNDEFContent(NULL, NULL, message, length);" I found an old post in 2025 for a PN7150 but when I try to compile I get strange errors such as 'uint8_t' not declared in scope, use . I have the newest Raspberry Pi OS, Trixie Debian 13.6. Looking for some help, thank you. Re: PN7160A and linux_libnfc-nci on Raspberry Pi 5 2026 64-bit Trixie Hello @paulwitulski  Please apply the patch as attachment.
記事全体を表示
GUIGuider 1.10.1 到 2.0.0 的迁移 我们的 GUIGuider 项目是用 1.10.1 版本构建的,我很有兴趣迁移到新的 2.0.0 版本来体验新功能。我发现旧的 GUIGuider 项目文件无法在新版本中加载,我认为这是因为 2.0.0 项目使用了新的 JSON 结构。 有没有简单的方法可以将项目迁移到新版本的 GUIGuider,还是必须手动转换?
記事全体を表示
FETMX6ULL-C: Random CTP I2C communication errors when LCD and CTP are connected simultaneously, CTP Hardware platform: FETMX6ULL-C core board.   Capacitive Touch Panel (CTP) GT911 works stably without any I2C errors when only the CTP is connected.   After connecting both LCD display and CTP at the same time, random I2C communication exceptions occur on CTP, which leads to touch function failure occasionally. We suspect that electromagnetic interference introduced by the LCD circuit causes unstable I2C signal of the touch panel.   Related kernel dmesg logs are attached for analysis.   Our software environment: Linux 4.1.15 BSP.   CTP communicates via I2C bus. We have checked hardware wiring and power supply, but the issue still exists.   Looking forward to your technical suggestions.
記事全体を表示
Raspberry Pi 5 2026 64ビット Trixie 上の PN7160A と linux_libnfc-nci こんにちは、 仕事のプロジェクトでPN7160Aを出そうとしているのですが、linux_libnfc-NCIの試みが全くうまくいきません。このパッチは古くなっています。lgpiodはバージョン2にアップデートされ、大幅に改良されました。 また、フラグ sudo make install CFLAGS="-Wno-error=implicit-function-declaration" を使用する必要があります そうでなければ私は "demoapp/main.c:関数「onMessageReceived」内: demoapp/main.c:451:5:エラー: 関数 'PrintNDEFContent' の暗黙的な宣言 [-Wimplicit-function-declaration] 451 | PrintNDEFContent(NULL, NULL, message, length);" PN7150 に関する 2025 年の古い投稿を見つけましたが、コンパイルしようとすると、「'uint8_t' がスコープ内で宣言されていません。 を使用してください」などの奇妙なエラーが発生します。私は最新のRaspberry Pi OS、Trixie Debian 13.6を使用しています。 助けていただきたいのですが、よろしくお願いします。 Re: PN7160A and linux_libnfc-nci on Raspberry Pi 5 2026 64-bit Trixie こんにちは、 @paulwitulski さん。 添付ファイルとしてパッチを適用してください。
記事全体を表示
Accessing SEMA42 unit on main platform domain from two different cortex M7 in S32K5 I am trying to access SEMA42_1 unit on main platform from two different cortex M7 cores (M7_0 and M7_1) in S32K5. The system hangs up. I cannot share the inhouse workspace here.  The errata ERR053433 states: SEMA42: Simultaneous access to SEMA42_0 and PBRIDGE_2 by more than one application core causes the system to hang. Unfortunately the workaround of using SEMA42_1 does not fix the system hang issue. Can you configure and verify two cortex M-7 cores on S32K56x and have them access gate0 of the SEMA42_1 unit on your Design studio and enable the optimization -Os. The system hang issue goes away by using any ONE of the following, Disable optimisations -O0 Disable Instruction cache Use SRAM of another domain on the SoC e.g. CPE Stepping in via debugger Re: Accessing SEMA42 unit on main platform domain from two different cortex M7 in S32K5 Hello @seasonedbit, As you may know, S32K5 is currently in a preproduction phase; Enablement (documentation, software, and boards) are available for approved customers only, and thus is not supported by our global online support team yet. Could you please contact your FAE or assigned NXP contact who provided the device in the first place? They will be able to provide further support. Thank you for your understanding. Best regards, Julián
記事全体を表示
TagWriter can not read the PN7160 tag I am running the RWandCE example (LPC55S69+PN7160). When I use the TagWriter app on an Android phone to read the tag, it fails with no response. The log shows that it activated the poll mode. However, TagInfo can read it, but it shows a "communication interrupt" popup, and the result on the phone may be incorrect. Is this because both poll and listen are enabled in the discovery loop? But my requirement is that both poll and listen must be enabled simultaneously. And I have also closed all emulation cards on my android phone. BillyHu_0-1783415582716.png Please help me, thank you. LPC55xx Re: TagWriter can not read the PN7160 tag Hello @BillyHu Hope you are doing well. Please try updating PN7160 FW to the latest version available .You can refer to PN7160 - FW Update via MCUXpresso for more information on this. Regards, Eduardo. Re: TagWriter can not read the PN7160 tag Hi Eduardo, My firmware version is already 12.50.11. Poll and listen work perfectly fine when used individually, but when both are enabled in discoveryTechnologies, I cannot read the card emulation of the PN7160 using the tagwriter. Have you encountered this issue on your side? Thanks, Re: TagWriter can not read the PN7160 tag Dear Eduardo, Do you have any suggestions? Is this phenomenon normal for the PN7160? Thanks,
記事全体を表示
在 S32K5 中,从两个不同的 Cortex M7 访问主平台域上的 SEMA42 单元 我正在尝试从 S32K5 中的两个不同的 cortex M7 内核(M7_0 和 M7_1)访问主平台上的 SEMA42_1 单元。系统崩溃了。我无法在此分享内部工作空间。 勘误表 ERR053433 指出:SEMA42:多个应用程序核心同时访问 SEMA42_0 和 PBRIDGE_2会导致系统挂起。 遗憾的是,使用 SEMA42_1 的变通方法并不能解决系统崩溃问题。 您能否在 S32K56x 上配置和验证两个 cortex M-7 内核,并让它们访问 Design studio 中的SEMA42_1单元的 gate0,并启用优化-Os。 使用以下任一方法均可解决系统卡顿问题: 禁用优化 -O0 禁用指令缓存 使用SoC上另一个功能域的SRAM,例如CPE 通过调试器单步执行 Re: Accessing SEMA42 unit on main platform domain from two different cortex M7 in S32K5 你好@seasonedbit , 如您所知,S32K5 目前处于预生产阶段;启用(文档、软件和板)仅提供给已批准的客户,因此我们的全球在线支持团队尚未提供支持。 请您联系当初提供该设备的现场应用工程师 (FAE) 或指定的恩智浦联系人。他们将能够提供进一步的支持。 感谢您的理解。 此致, 朱利安
記事全体を表示
Looking for GUI Guider v1.9.0 installer I'm currently working on a project that was originally created with GUI Guider v1.9.0. For compatibility reasons, I need to get the exact v1.9.0 installer, but the official NXP website now only offers newer versions. Does anyone still have the Gui-Guider-Setup-1.9.0 file handy, or know where I can download this specific older version? Also, if I open a v1.9.0 project directly with a newer version (e.g., v1.10.0), will it cause any compatibility issues? Any help or pointers would be greatly appreciated. Thanks! Re: Looking for GUI Guider v1.9.0 installer Hello @李先森 , Thanks for your post. The GUI Guider v1.9.0 installer was not provided any more. However, GUI Guider can upgrade projects created by the last major version and related minor version. Therefore, you can directly use GUI Guider v1.10.x and import project created by GUI Guider v1.9.x. Hope it helps. BR Celeste ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
PNEV7642FAMA pack Keil MDK project from SDK_2_12_1_PNEV7642FAMA requires PackID NXP.PN7642_DFP.15.0.0, but it is missing from :·https://mcuxpresso.nxp.com/cmsis_pack/repo/NXP.pidx· and direct pack URL returns 404. Please provide NXP.PN7642_DFP.15.0.0.pack or enable access. Re: PNEV7642FAMA pack Hello @Sinrow  PackID NXP.PN7642_DFP.15.0.0 is security file, you need to sign NDA with NXP and then request this file.
記事全体を表示
IMX95 { 15 x 15 }はLPDDR4/4X 16 GB RAMをサポートしていますか? こんにちは、NXPチームの皆さん、 IMX95{ 15 x 15 }について一般的な情報が欲しいです。MIMX9556CVTXN"は16GBのRAMをサポートします{ LPDDR4/4X } "MT53E4G32D8GS-046 WT:C ?" 16GB RAMをIMX 95に接続するための回路図の参照が見つかりませんでした { 15x 15} 16GB RAMのIMX95 { 19 x 19 }の回路図しか見つけられませんでした。 もし対応しているなら、16GB RAM{ LPDDR4/4x }とimx95{ 15 x 15 }の接続について教えていただけませんか? そしてBSPファイルはどうですか?16GBのRAMに対してDTSファイルが存在するのか、それとも手動で生成する必要があるのか。 Yocto Project Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Asadeds さん。 NXPサポートまでご連絡いただきありがとうございます。 当社の メモリ互換性ガイドによると、メモリ部品番号MT53E4G32D8GS-046はi.MX95と完全に互換性があり、このプラットフォーム上で徹底的に検証・テストされています。 したがって、このデバイスは推奨される構成および 設計ガイドラインに従い、i.MX95と併用可能です。 よろしくお願いします、 アレハンドロ・ガルシア Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Asadeds さん。 MT53E4G32D8GSはサポートされているメモリデバイスであり、i.MX95との社内検証済みです。しかし、このデバイスは特別なバイトモード構成を使用しており、設定ツールとソフトウェアスタックの両方で追加のサポートが必要です。 現時点では内部サポートはありますが、現在のConfig Toolsの公開リリースには、この特定のメモリデバイスを設定するための必要なオプションはまだ含まれていません。このメモリのサポートはFUTUREツールリリースで予定されています。 よろしくお願いします、 チャビラ Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは @Chavira  迅速な返信ありがとうございます。 DDRの設定を試みると「Imx 26.06のConfig tool」アプリケーションが表示され、対応可能な LPDDR4/4xは最大8GBまでしかなく、対応するパッケージは LPDDR5 を選択します 最大16GBです。 参考のためにスクリーンショットを添付しました。もし何か見落としている点があれば教えてください。 Asadeds_0-1784697908014.png Asadeds_1-1784698046354.png これについて助けていただけませんか?それと、プロジェクトにLPDDR4/4xを使いたいと思っています。部品番号は「MT53E4G32D8GS-046 WT:C」です。 Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Chavira さん。 迅速なご返信ありがとうございます。 まだ混乱しているので、質問を簡単にしたいと思います。 今のところ、特定のRAMベンダーと部品番号は無視しましょう。 config Toolsが i.MX95 の 15× 15または 19×19 パッケージで 16GB LPDDR4/LPDDR4X メモリ をサポートしているか確認していただけます か? もし答えがノーなら、どうやって16GBのサポートを得るのでしょうか?社内サポートが利用可能だとおっしゃっていましたので、そのサポートにアクセスする手続きについて説明していただけると助かります。 現在、PCB設計を最終調整中で、RAMの選択肢のせいでプロジェクトは保留中です。これが前進を妨げる唯一の残された問題なので、できるだけ早く明確な答えが必要です。 ご回答をいただければ幸いです。 よろしくお願いします。 Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Asadeds さん。 社内チームと協議した結果、以下のとおり最新情報をお伝えいたします。 NXPは通常、四半期ごとに新しいバージョンのConfig Toolsをリリースするため、次のリリースはバージョン26.09が予定されています。 i.MX95自体はこの16GBメモリデバイスをサポートしていますが、現在の公開版DDR設定ツールはまだこの特定のメモリの設定をサポートしていません。良いニュースは、すでにツールの内部バージョンでサポートが存在しているものの、まだ公開リリースには組み込まれていないことです。 内部ツールへのアクセスが可能かどうかは確信が持てません。ただし、会社のメールアドレスを使って当 サイト からサポートケースを開くことをお勧めします。これにより、適切なチームがあなたの要望を確認し、追加のサポートや早期サポートの選択肢があるかどうかを判断できます。 ご不便をおかけし申し訳ありません。今後の公開リリースにこのサポートが統合されるまでのご理解に感謝いたします。 よろしくお願いします、 チャビラ
記事全体を表示
imx93 lpddr4x の JSL4BAG16 設定が不安定です こんにちは、専門家の皆様: JSL4BAG16 の lpddr4x 設定に関して問題があります。設定後、「機能」テストはパスしますが、「最適化->CA 最適化の Vref」で失敗することがあります。常に失敗するわけではなく、時々失敗します。 「vTSA -> CA eye」のテストを実行すると、合格と表示されますが、同時に「エラーログ」も表示されます。 「Vref DQ config」と「Vref CA config」の調整方法について質問があります。JSL4BAG16のVref値は「EVKで使用されているミクロン値」と異なりますが、範囲0または範囲1を設定する必要がありますか? 私の知る限り、Vref DQは「アイダイアグラム」テストの結果に基づいて設定されますが、「読み取りダイアグラム」と「書き込みダイアグラム」のどちらを使用すればよいのでしょうか? JSL4BAGのデータシートと、「CA eye」テストログおよびmexファイルを添付しました。     よろしくお願いします。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは、 LPDDR4Xは、 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-93-Memory-Compatibility-Guide/ta-p/1725656の一部です。 Vref DQ チューニングには、JSL4BAG16 のレンジ 1 (デフォルト) を使用し、読み取りではなく書き込みアイ ダイアグラムを使用してください。   Micron/EVKの設定を再利用しないでください。必ずJSL4BAG16に合わせてVrefを再調整してください。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは、オズワラグさん。 ご返信ありがとうございます。私は「i.MX config tool」でテストに合格し、「最適化」テスト結果でDQとCAの「Vref」を使用しました。 しかし、まだ2つの問題があります。 1.あるボードでは「CA Charts」が表示されず、「CA Eye」テストには誤差がありますが、合格と表示されます 2.lpddr4x_timing.cを更新した後すべての合格ボードで「i.MX config tool」によって生成されたものをシステムで「memtest」を実行すると、「Stuck Address」で失敗します。常にではありませんが、時々発生します。 よろしくお願いします。 Re: imx93 lpddr4x config for JSL4BAG16 unstable 私のFRDM-IMX93ボードにも同じチップが搭載されていますが、市販のイメージファイルでは正常に起動しません。どうすれば解決できますか? Re: imx93 lpddr4x config for JSL4BAG16 unstable いいえ、していません。弊社では、flex-installerが提供する市販のイメージファイルを使用して、市販のfrdm-imx93ボードを使用しています。 入門マニュアルには「i.Mx設定ツール」についての記載はありません。 手順はどうなりますか?マニュアルはありますか?また、使い始めるにあたって、どのような手順で部品を交換する必要がありますか? これはまた、すべてのFRDM-IMX93ボードに対して1つの標準イメージを使うことはできず、各ボードを確認するか、搭載DDRによって2〜3つのイメージバージョンを持つ必要があるということですか? ご注意ください。私たちは(共有の)お客様に対して既製の動作を期待しています。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは、SynchronicITさん。 「i.MX config tool」を使用してDDRテストに合格しましたか?まずそれを通過させてから、lpddr4x_timging.c を使用する必要があります。「i.MX設定ツール」によって生成されました。 Re: imx93 lpddr4x config for JSL4BAG16 unstable こんにちは: NXP公式の「FRDM i.MX 93開発ボード」と公式リリースを使っているようですね。大丈夫でしょう。「DDRテスト」を行う必要はありません。私は「FRDMボード」を持っていません。NXPのボードの使い方に関するドキュメントを参照できるかもしれません。
記事全体を表示
在 i.MX8 QuadMax 上使用 AAOS 15 启用多用户功能,并设置多显示器 各位同事好, 我们 在 i.MX8 QuadMax 平台 上使用 Android Automotive OS( AAOS) 15 。 我们目前的硬件配置包括三个显示器: 主中央显示屏(驾驶员/中央显示屏) 乘客显示屏 仪表盘显示 我们 希望 在 该 平台 上 启用 和 验证 Android 多用户 功能 , 包括 支持 用户 切换、 访客 用户 和 用户特定的 应用 程序/设置 。 请问 您 能否 就 以下 问题 提供 指导 : 在 i.MX8QM 上 启用 AAOS 15 的 多 用户 支持 需要 哪些 配置 ? NXP 方面 是否 需要 对 电路板支持包 进行 任何 特定的 更改 ? 必须 启用 哪些 框架 覆盖层、 功能 标志 或 系统 属性 ? 任何指导或建议都将不胜感激。   谢谢! Re: Enabling Multi-User Functionality in AAOS 15 on i.MX8 QuadMax with Multi-Display Setup 嗨@harshi03 请参阅官方 Android Automotive 文档: Android Automotive 多用户支持 前台和后台用户系统处理 对于多个显示器上的并发用户,请参考 Android Automotive 多显示器和乘员区域架构: Android Automotive 15 功能 多显示器通信 API 此致, 志明
記事全体を表示
IMX95 { 15 x 15 } 是否支持 LPDDR4/4X 16 GB 内存 NXP团队您好, 我想了解一些关于 IMX95{ 15 x 15 } " MIMX9556CVTXN" 是否支持 16 GB RAM { LPDDR4/4X } "MT53E4G32D8GS-046 WT:C ?" 的一般信息。 我找不到将 16 GB RAM 连接到 IMX 95 { 15x 15} 的原理图参考资料。 我只找到了配备 16 GB RAM {LPDDR5} 的 imx95 { 19 x 19 } 的原理图。 请问能否帮我解决一下 16GB RAM{ LPDDR4/4x } 与 imx95{ 15 x 15 } 的连接问题(如果支持的话)? 电路板支持包 文件呢?16 GB 内存的 DTS 文件是否存在,还是需要手动生成? Yocto Project Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM 嗨@Asadeds , 感谢您联系恩智浦技术支持。 根据我们的内存兼容性指南,内存部件号 MT53E4G32D8GS-046 与 i.MX95 完全兼容,并且已在该平台上进行了彻底的验证和测试。 因此,按照推荐的配置和设计指南,该设备可以与 i.MX95 一起使用。 此致, 亚历杭德罗·加西亚 Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM 嗨@Chavira 感谢您的快速回复。 当我尝试配置 DDR 时,我看到“imx 26.06 配置工具”应用程序仅支持最大 8GB 的 LPDDR4/4x ,而当我选择任何软件包的LPDDR5时,它却支持最大 16GB。 我附上了截图供您参考,如果我遗漏了什么,请告诉我。 Asadeds_0-1784697908014.png Asadeds_1-1784698046354.png 请问您能帮我解决这个问题吗?另外,我的项目需要使用LPDDR4/4x内存,型号是“MT53E4G32D8GS-046 WT:C”。 Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM 嗨@Asadeds , MT53E4G32D8GS 是一款受支持的存储设备,已通过 i.MX95 的内部验证。但是,该设备使用特殊的字节模式配置,这需要在配置工具和软件堆栈中提供额外的支持。 目前,虽然内部支持可用,但当前公开发布的 Config Tools 版本尚未包含配置此特定内存设备所需的选项。计划在未来的工具版本中加入对该内存的支持。 此致, 查维拉 Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM 嗨@Chavira , 感谢您的快速回复。 我仍然有些困惑,所以我想简化一下这个问题。 目前,我们暂且忽略具体的内存供应商和部件号。 请问配置工具是否支持i.MX95的16GB LPDDR4/LPDDR4X内存,无论是15×15还是19×19封装? 如果答案是否定的,那么我们如何才能获得16GB内存的支持?您提到公司内部有技术支持,所以如果您能解释一下如何获得这种支持,我将不胜感激。 我们目前正在敲定PCB设计,项目暂停仅仅是因为内存条的选择问题。这是唯一阻碍我们继续前进的因素,所以我们需要尽快得到明确的答复。 希望您能尽快澄清。 谢谢! Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM 嗨@Asadeds , 与内部团队讨论后,我谨提供以下最新进展。 NXP 通常每季度发布一个新版本的 Config Tools,因此下一个预计版本是 26.09。 虽然 i.MX95 本身支持这款 16 GB 内存设备,但当前公开版本的 DDR 配置工具尚不支持配置此特定内存。好消息是,该工具的内部版本已经支持此功能,但尚未将其纳入公开版本中。 我不确定是否有可能提供对内部工具的访问权限。不过,我建议您使用公司邮箱地址通过我们的网站提交支持请求。这将使相关团队能够审核您的请求,并确定是否有任何额外的帮助或提前支持方案。 由此给您带来的不便,我们深表歉意,并感谢您的耐心等待,我们将把这项支持整合到未来的公开版本中。 此致, 查维拉
記事全体を表示
FRDM-IMX95-1 は fsl-se-fw se-fw2: 応答失敗 = 0x29 で停止しています EdgeLock Enclave(ELE)/System マネージャのファームウェアが起動時に初期化に失敗します:   [ 0.182931] fsl-se-fw se-fw2: コマンドID[23]、応答失敗 = 0x29 [ 0.182942] fsl-se-fw se-fw2: ele fw の初期化に失敗しました。 ELEの初期化に失敗したためです。 MaliのGPU(4d900000.gpu)パワードメインはオフのままで、LinuxがGPUをプロブングするとARM64 SError割り込みカーネルパニックを引き起こします。 GPUノードを無効にすると起動は進めますが、 USDHCストレージ(mmc0およびmmc1 )が初期化に失敗しエラー-5が発生し、Linuxがrootファイルシステム(/dev/mmcblk*p2)をマウントできません。 「システムの再インストール」を実行しても、この問題は解決しません。管理者の方が 、FRDM-IMX95-1ユニットのプライマリブートローダー/ELEファームウェアを再フラッシュしてもらえますか? クラウド・ラボ オンラインラボ 仮想テスト Re: FRDM-IMX95-1 is stuck with fsl-se-fw se-fw2: Response Failure = 0x29 こんにちは、 テスト用のソフトウェア/ハードウェアのセットアップについて、もう少し教えていただけますか? カスタム画像を使用している場合は、変更内容を共有してください。 また、基板のファームウェアを再書き込みしてみてください。 よろしくお願いいたします。
記事全体を表示
寻找 GUI Guider v1.9.0 安装程序 我目前正在开发一个项目,该项目最初是用 GUI Guider v1.9.0 创建的。出于兼容性考虑,我需要获取 v1.9.0 的安装程序,但 NXP 官方网站现在只提供更新的版本。 请问有人手头还有 Gui-Guider-Setup-1.9.0 文件吗?或者知道哪里可以下载这个旧版本?另外,如果我用新版本(例如 v1.10.0)直接打开 v1.9.0 的项目,会不会出现兼容性问题? 任何帮助或建议都将不胜感激。谢谢! Re: Looking for GUI Guider v1.9.0 installer 你好@李先森, 感谢您的帖子。GUI Guider v1.9.0 安装程序已不再提供。 但是,GUI Guider 可以升级由上一个主要版本和相关的次要版本创建的项目。因此,您可以直接使用 GUI Guider v1.10.x 并导入由 GUI Guider v1.9.x 创建的项目。 希望对您有所帮助。 BR 塞莱斯特 ----------------------------------------------------------------------------------------------------------------------- 注:如果此帖解答了您的问题,请点击“接受为解决方案”按钮。谢谢你! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
S32K3 Unlock Secure Debug with Trace32 Hello S32K3 Team, I am currently experiencing an issue with secure debug unlock. The debugger I am using is Trace32 and autosar os using.... The Life Cycle (LC) has been switched to OEM, and secure debug is configured in password mode (not challenge–response). The configured TEST password is: 0xFFEEDDCCBBAA99887766554433221100 Before switching the LC, I confirmed that the HASH value matched correctly. I have tried the following two methods to unlock secure debug: Using the Trace32 command: SYStem.Option KEYCODE %Byte 0xFF 0xEE 0xDD 0xCC 0xBB 0xAA 0x99 0x88 0x77 0x66 0x55 0x44 0x33 0x22 0x11 0x00 Using the S32_JTAG_WRITE.cmm script However, both methods failed to unlock secure debug. I would appreciate your guidance on what I should check next or any potential causes I might be overlooking. I have attached my script for reference. Best regards, NewbieNerd_0-1768555507583.png #HSE #secureDebug Re: S32K3 Unlock Secure Debug with Trace32 I have recently test it. See attached scripts debug_authorization.cmm shows how to enter the password and then it calls other scripts. I am sending you attachment directly. Re: S32K3 Unlock Secure Debug with Trace32 Hello, I am experiencing the same issue in the same environment. Could you please share the file with me as well? I would really appreciate your help. Thank you! Re: S32K3 Unlock Secure Debug with Trace32 Dear NewbieNerd, I am facing the same issue in a similar environment. If you were able to resolve it, could you please share the solution and explain what changed compared to the previous setup? Your experience would be greatly appreciated and would be very helpful for troubleshooting this issue on my side. Thank you for your time and support. Re: S32K3 Unlock Secure Debug with Trace32 Please create new ticket and I will send it to you. Thanks for understanding. https://www.nxp.com/support/support:SUPPORTHOME Re: S32K3 Unlock Secure Debug with Trace32 Thank you for your response. I have already created a support ticket (Case#00994181), which is currently being handled by another support engineer. If possible, would you be able to take a look at the ticket or provide additional support? Thank you again for your support.
記事全体を表示
S32K3 使用 Trace32 解除锁定安全调试 你好,S32K3 团队、 我目前遇到了安全调试解锁的问题。 我使用的调试器是 Trace32 和 autosar os,使用.... ,生命周期(LC)已切换到 OEM,安全调试配置为密码模式(不是挑战-响应)。 配置的 TEST 密码为 0xFFEEDDCCBBAA99887766554433221100 在切换 LC 之前,我确认了 HASH 值是否正确匹配。 我尝试了以下两种方法来解锁安全调试: 使用 Trace32 命令 SYStem.Option KEYCODE%字节 0xFF 0xEE 0xDD 0xCC 0xBB 0xAA 0x99 0x88 0x77 0x66 0x55 0x44 0x33 0x22 0x11 0x00 使用 S32_JTAG_WRITE.cmm 脚本 然而,这两种方法都无法解锁安全调试。 如果您能指导我下一步应该检查什么,或者我可能忽略的任何潜在原因,我将不胜感激。 我附上了我的脚本以供参考。 顺祝商祺! NewbieNerd_0-1768555507583.png #HSE #安全调试 Re: S32K3 Unlock Secure Debug with Trace32 我最近进行了测试。见所附脚本 debug_authorization.cmm 演示如何输入密码,然后调用其他脚本。 我直接向您发送附件。 Re: S32K3 Unlock Secure Debug with Trace32 你好, 我在相同的环境下也遇到了同样的问题。 您能否也把文件分享给我?非常感谢您的帮助。 谢谢! Re: S32K3 Unlock Secure Debug with Trace32 请创建新工单,我会发送给您。谢谢您的理解。 https://www.nxp.com/support/support:SUPPORTHOME Re: S32K3 Unlock Secure Debug with Trace32 亲爱的新手书呆子, 我在类似的环境下也遇到了同样的问题。 如果您能够解决这个问题,能否分享一下解决方案,并解释一下与之前的设置相比有哪些变化? 您的经验将不胜感激,对解决我这边遇到的问题非常有帮助。 感谢您的时间和支持。 Re: S32K3 Unlock Secure Debug with Trace32 感谢您的反馈, 我已经创建了一个支持工单(工单号:00994181 ) ,目前由另一位支持工程师处理。如果可以的话,您能否查看一下该工单或提供更多支持? 再次感谢您的支持。
記事全体を表示
Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM Hi NXP Team,  I want some general Information about the IMX95{ 15 x 15 } "MIMX9556CVTXN" will support 16 GB of RAM { LPDDR4/4X } "MT53E4G32D8GS-046 WT:C ?" I could not able to find the reference of the schematic to connect the 16 GB RAM to IMX 95 { 15x 15}  ,  I only found the schematic of  imx95 { 19 x 19 } with the 16 GB RAM {LPDDR5}.  can you please help me out with connection of 16GB RAM{ LPDDR4/4x } with imx95{ 15 x 15 } if Supported. and What about the BSP file? , is DTS file present for the 16 GB of ram or need to generated manually.  Yocto Project Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM Hi @Asadeds, Thank you for contacting NXP Support. According to our Memory Compatibility Guide, the memory part number MT53E4G32D8GS-046 is fully compatible with the i.MX95 and has been thoroughly validated and tested on this platform. Therefore, this device can be used with the i.MX95 following the recommended configuration and design guidelines. Best regards, Alejandro Garcia Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM Hi @Asadeds, The MT53E4G32D8GS is a supported memory device and has been validated internally with the i.MX95. However, this device uses a special byte mode configuration, which requires additional support in both the configuration tools and software stack. At the moment, although internal support is available, the current public release of Config Tools does not yet include the required options to configure this specific memory device. Support for this memory is planned for a future tool release. Best Regards, Chavira Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM Hi @Chavira  Thanks for the quick Reply,  As I see the Application " Config tool for imx  26.06" when I try to configure the DDR , then there is Only supportable LPDDR4/4x upto 8GB, while i select the LPDDR5 for any packages it Support upto 16GB. As i attached  the screenshot for reference , If i m missing something please let me know. Asadeds_0-1784697908014.png Asadeds_1-1784698046354.png can you please help me Out this , and as well as , i want to use LPDDR4/4x for my project the part number is this one "MT53E4G32D8GS-046 WT:C" Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM Hi @Chavira , Thank you for your quick reply. I am still confused, so I'd like to simplify the question. For now, let's ignore the specific RAM vendor and part number. Could you please confirm whether the Config Tools support 16GB LPDDR4/LPDDR4X memory for the i.MX95, for either the 15×15 or 19×19 package? If the answer is no, then how are we expected to obtain support for 16GB? You mentioned that internal support is available, so I would appreciate it if you could explain the process for accessing that support. We are currently finalizing our PCB design, and our project is on hold solely because of the RAM selection. This is the only remaining item preventing us from moving forward, so we need a clear answer as soon as possible. I would appreciate your prompt clarification. Thank you. Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM Hi @Asadeds, After discussing this with the internal team, I would like to provide the following update. NXP typically releases a new version of Config Tools once per quarter, so the next expected release is version 26.09. Although the i.MX95 itself supports this 16 GB memory device, the current public version of the DDR configuration tool does not yet support configuring this specific memory. The good news is that support already exists in an internal version of the tool, but it has not yet been incorporated into the public release. I am not certain whether it will be possible to provide access to the internal tool. However, I recommend opening a support case through our website using your company email address. This will allow the appropriate teams to review your request and determine whether any additional assistance or early support options are available. We apologize for the inconvenience and appreciate your patience while this support is integrated into a future public release. Best regards, Chavira
記事全体を表示
NXP牵引/轴向电机参考固件 你好, 我正在进行一个牵引/轴向控制电机项目,我想了解恩智浦半导体(NXP)用于轴向电机开发的参考软件,这将对我们正在进行的项目的研究和开发非常有帮助。 因此,我请求您提供此问题的解决方案,同时,NXP 提供的牵引/轴向电机参考软件将为我们的研发工作提供可靠的参考。 谢谢 帕万 Re: NXP reference firmware for traction/axial motors 你好, NXP 不提供专门用于轴向磁通电机的专用软件。在大多数情况下,轴向磁通永磁同步电机可以使用与传统径向磁通永磁同步电机相同的永磁同步电机FOC参考软件进行控制。主要的改进在于电机参数化(Rs、Ld、Lq、极对数、磁链等),而控制算法基本保持不变。 典型的切入点是: S32K344 / S32K396 电机控制参考设计 永磁同步电机磁场定向控制(FOC)示例 AMMCLIB 电机控制库 基于模型的设计工具箱示例(如果使用 MATLAB/Simulink) 顺祝商祺! Peter
記事全体を表示
NXP reference firmware for traction/axial motors Hello, I am working on a Traction/Axial control motor project and I wanted to know about the reference software for the Axial motor based development from NXP,so it will be very helpful for the reasearch and development of our ongoing project. So I am requesting to provide me the solution for this and also the reference software for Traction/Axial motor from NXP will be a solid reference for our R and D. Thank you Pavan Re: NXP reference firmware for traction/axial motors Hello, NXP does not provide dedicated software specifically for axial-flux motors. In most cases, axial-flux PMSM motors can be controlled using the same PMSM FOC reference software as conventional radial-flux PMSM motors. The main adaptation is the motor parameterization (Rs, Ld, Lq, pole-pair count, flux linkage, etc.), while the control algorithm remains essentially the same. Typical starting points are: S32K344 / S32K396 motor-control reference designs PMSM Field-Oriented Control (FOC) examples AMMCLIB motor-control library Model-Based Design Toolbox examples (if MATLAB/Simulink is used) Best regards, Peter
記事全体を表示