Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
S32DS arm V1.3 activation code failed Hello, the software activation code of my S32DS Arm V1.3 has expired. Could you help me extend the time.   My original activation code was:FF3F-27C7-FFAB-837F Re: S32DS arm V1.3 activation code failed Hello, It is extended now. Best regards, Peter 回复: S32DS arm V1.3 activation code failed My activation ID (0D3F-EFEF-B771-DA51) is new, and both online and offline activation failed when I tried to activate the same version of the software. The failure screen is in the attachment below. I hope you can help me solve this. Thank you.
記事全体を表示
MIFARE DESFire EV3 / EV3C 4-byte NUID configuration MIFARE DESFire EV3 / EV3C all can config 4-byte NUID,But when use RFIDDiscover set configuration,it shows set 4 bit NUID(only for MIFARE DESFire EV3 C),How can we set 4-byte NUID for DESFire EV3 by RFIDDiscover? DSC Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration Hello, Thank you for your interest in our products. I have to clarify that MIFARE DESFire EV3 is a different IC than MIFARE DESFire EV3C.  Re: MIFARE DESFire EV3C configuration Dear Fabian, we have a large real estate industrial portfolio worldwide (>700!) So we try to use EV3 [C]. because lots of our office, warehouse and production are on Mifare Cassic. While in Germany, Norway and China we have all cardreaders etc. on DESFire. problem: we don´t know how to code the card in Siemens Siportsoftware. We need to keep our existing Classic key, and will have a DESFire key, created new. How is this done? We have a very few testcards, so don´t want to crash them. There is no manual from Siemens side, but an existing function (german: Ausweis codieren (Mifare Classi and DESFire) I would like to send you a picture, but don´t know how. Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration Yes, I know, I am looking for any information how to code EV3[C] cards in Siport/Sipass software, which are the most used solution worldwide. Keep the exsting Classic key and add a DESFire red key. Even inside Siemens AG there is very little knowledge about this. Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration Hello sir, I sent you a private message. MIFARE DESFire EV3 C help is needed read message to user Barton. Need support in DESFire Ev3 C. and coding in Siport or Sipass from Siemens AG as our coding and access control software. Need help, otherwise we would not buy this and stay with outdated Classic.  Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration Dear Fabian, from NXP support. We want to equipe our 130.000 employees with EV3 C. We have worldwide RE portfolio 700location with all kind of cardreaders. We have some testcards, and never been able to code with red key. Classic key is in the system and should be continued. DESFire key should be basaed on this. We need help in card coding. We have Siport and Sipass software for coding. 
記事全体を表示
GUIGuider 1.10.1 から 2.0.0 への移行 私たちはGUIGuiderプロジェクトをバージョン1.10.1で構築してきましたが、新しいバージョン2.0.0に移行して新機能を試してみたいと思っています。古いGUIGuiderプロジェクトファイルが新しいバージョンでは読み込めないことが分かりました。おそらくそれはプロジェクトが使う新しいJSON構造の2.0.0のせいだと思います。 GUIGuiderの新しいバージョンにプロジェクトを簡単に移行する方法はありますか?それとも手動で変換する必要がありますか?
記事全体を表示
S32K5の2つの異なるコルテックスM7からメインプラットフォームドメインのSEMA42ユニットにアクセスする S32K5の2つの異なるCortex M7コア(M7_0とM7_1)からメインプラットフォームのSEMA42_1ユニットにアクセスしようとしています。システムがフリーズします。ここで社内作業スペースを共有することはできません。 訂正ERR053433には次のように記載されています:SEMA42:複数のアプリケーションコアによるSEMA42_0およびPBRIDGE_2への同時アクセスによりシステムがハングします。 残念ながら、SEMA42_1を使用するという回避策では、システムハングアップの問題は解決しません。 S32K56xで2つのCortex M-7コアを設定・検証し、Design StudioのSEMA42_1ユニットのgate0にアクセスして最適化-OSを有効にしてもらえますか? システムのフリーズ問題は、以下のいずれか1つを使用することで解消されます。 最適化を無効にする -O0 命令キャッシュを無効にする SoC上の別のドメインのSRAMを使用する例CPE デバッガー経由でステップインする Re: Accessing SEMA42 unit on main platform domain from two different cortex M7 in S32K5 こんにちは、 @seasonedbit さん。 ご存知かもしれませんが、S32K5は現在プリプロダクション段階にあります。イネーブルメント(ドキュメント、ソフトウェア、ボード)は承認されたお客様のみが利用可能であり、そのため当社のグローバルオンラインサポートチームからはまだサポートされていません。 最初にこの装置を提供したFAEやNXPの担当者に連絡していただけますか?彼らはさらなる支援を提供できるでしょう。 ご理解いただきありがとうございます。 よろしくお願いします、 ジュリアン
記事全体を表示
S32K314でDMAを使用したUARTが正しく動作しません こんにちは、 現在、DMAと連携するようにLPUART0チャネルの設定を試みています。UARTチャネルは1Mbpsのビットレートで動作している必要があります。 現在のUARTとDMAの設定は以下のようになっています。 CosminSbera_0-1784803400829.png CosminSbera_1-1784803453733.png CosminSbera_2-1784803479911.png CosminSbera_3-1784803495720.png CosminSbera_4-1784803522819.png CosminSbera_5-1784803539872.png MCUではクロックが有効化され、バッファはキャッシュできない領域内に宣言され、DMAのISR優先度はLPUARTよりも小さいです。 私たちの問題は、RXバッファ内のデータを見ることができない、あるいはデータが不完全であることです。 私たちのワークフローはこうです(LINコミュニケーションに似ています) 😞 受信バッファを準備 -> AsyncReceive スレーブにヘッダーを送信する -> AsyncSend 次のサイクルでスレーブからデータが受信されるまで待機します(私の関数は1msのタスクで実行されます)。 AsyncSendの実行後にブレークポイントを設けると、RXバッファ内のスレーブからのすべてのデータ送信が確認できます。 そのまま実行させても、何も表示されないか、不完全な結果しか得られない。 私の推測では、DMA割り込みは後から発生する。 私たちの設定のどこが問題なのか、あるいは次に何をチェックすればいいのか、いくつかヒントを教えてもらえますか? ご回答をお待ちしています。 コスミン Re: Uart using DMA is not working correct on S32K314 こんにちは、@ CosminSbera 1. DMA要求オプションを有効にするのを忘れないでください。 Senlent_0-1784861937675.png 2. 「プラットフォーム」コンポーネントでLPUART0_IRQn割り込みを有効にするのを忘れないでください。 「プラットフォーム」->」LPUART0_IRQn--LPUART_UART_IP_0_IRQHandler」
記事全体を表示
i.MX93プロセッサ向けパラレルプログラミングシステム 私はIMX93プロセッサを使っていて、2台のボードを同時にプログラムする必要があります。しかし、それを試すと、ボードの1つでHID(W)エラーが発生し、他のボードのフラッシュは正常に完了します。 uu.exe -m 1:10 -b uuu-xxxxxx.flash uu.exe -m 1:7 -b uuu-xxxxxx.flash パス(1:10,1:7)を指定しても同じエラーが発生します。 案内してください。 Re: Parallel Programming System for i.MX93 Processors こんにちは、 次のコマンドを実行してみてください。 uuu -d -m 1:7 -m 1:10 uuu-xxxxxx.flash 何が手に入るの? uuu -lsusb 列挙されたポート番号に従って、正しいポート番号を使用していることを確認してください。 よろしくお願いいたします。
記事全体を表示
S32K314 上使用 DMA 的 UART 功能无法正常工作 你好, 我们目前正在尝试配置 LPUART0 通道以使其与 DMA 配合使用。UART 通道需要以 1Mbps 的比特率工作。 我们目前的 UART 和 DMA 配置如下所示。 CosminSbera_0-1784803400829.png CosminSbera_1-1784803453733.png CosminSbera_2-1784803479911.png CosminSbera_3-1784803495720.png CosminSbera_4-1784803522819.png CosminSbera_5-1784803539872.png MCU 中时钟已启用,缓冲区在不可缓存区域内声明,DMA ISR 的优先级低于 LPUART。 我们的问题是,我们无法看到 RX 缓冲区中的数据,或者数据不完整。 我们的工作流程如下(类似于LIN通信)。 😞 准备接收缓冲区 -> 异步接收 将头部信息发送到从设备 -> AsyncSend 等待下一个周期从从设备接收到数据(我的函数运行时间为 1 毫秒)。 如果我在 AsyncSend 执行后设置断点,我可以看到从设备发送的所有数据都在 RX 缓冲区中。 如果我让它运行,要么什么都没有,要么运行不完整。 我的假设是 DMA 中断稍后发生。 您能否提供一些关于配置中哪里出了问题的线索,或者我接下来应该检查哪些方面? 谢谢! 科斯明 Re: Uart using DMA is not working correct on S32K314 嗨@CosminSbera 1.不要忘记启用DMA请求选项。 Senlent_0-1784861937675.png 2.不要忘记在“平台”组件中启用 LPUART0_IRQn 中断。 “平台”->“LPUART0_IRQn --LPUART_UART_IP_0_IRQHandler“
記事全体を表示
MIFARE DESFire EV3 / EV3C 4 バイト NUID 構成 MIFARE DESFire EV3 / EV3C はすべて 4 バイトの NUID を設定CANますが、RFIDDiscover 設定を使用すると、4 ビットの NUID が設定されていることが表示されます (MIFARE DESFire EV3 C のみ)。RFIDDiscover を使用して DESFire EV3 に 4 バイトの NUID を設定するにはどうすればよいでしょうか。 DSC Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration こんにちは、 弊社製品にご興味をお持ちいただきありがとうございます。 MIFARE DESFire EV3 は、MIFARE DESFire EV3C とは異なる IC であることを明確にする必要があります。 Re: MIFARE DESFire EV3C configuration ファビアン様、弊社は世界中に大規模なインダストリアル不動産ポートフォリオ(700以上!)を保有しております。そこで、EV3 [C] を使ってみることにしました。なぜなら、当社のオフィス、倉庫、生産拠点の多くはMifare Classicを使用しているからです。ドイツ、ノルウェー、中国では、すべてのカードリーダーなどがDESFireに対応しています。問題点:シーメンスSiportソフトウェアでカードをどのようにコーディングすればよいかわかりません。既存のClassicキーは保持し、新たにDESFireキーを作成する必要があります。これはどのように行うのですか?テストカードの数が非常に少ないので、クラッシュさせたくありません。シーメンス側からのマニュアルはありませんが、既存の機能 (ドイツ語: Ausweis codieren (Mifare Classi および DESFire)) があります。写真を送りたいのですが、方法がわかりません。 Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration はい、わかっています。私は、世界で最も広く使用されているソリューションであるSiport/SipassソフトウェアでEV3[C]カードをコーディングする方法に関する情報を探しています。既存のクラシックキーはそのままにして、DESFireの赤いキーを追加します。シーメンスAG社内ですら、この件についてはほとんど知られていない。 MIFARE DESFire EV3 C help is needed ユーザーバートンへのメッセージを読み上げてください。DESFire Ev3 C.のサポートと、Siemens AGのコーディングおよびアクセス制御ソフトウェアとしてSiportまたはSipassでのコーディングが必要です。助けが必要です。そうでなければ、これを買わずに旧式のClassicを使い続けるでしょう。 Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration 親愛なるファビアン、NXPサポートより。私たちは13万人のNXP社員向けにEV3 Cを装備したいと考えています。当社は世界中のRE Portfolio 700locationとあらゆる種類のカードリーダーをご用意しています。テストカードはいくつか持っていますが、赤いキーを使ってコーディングできたことは一度もありません。従来のキーはシステムに登録されており、引き続き使用する必要があります。DESFireキーはこれに基づいて作成されるべきです。カードのコーディングについて助けが必要です。コーディングにはSiportとSipassのソフトウェアがあります。 Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration お世話になります。 プライベートメッセージを送りました。
記事全体を表示
FETMX6ULL-C:LCDとCTPが同時に接続された際のランダムなCTP I2C通信エラー、CTP ハードウェアプラットフォーム:FETMX6ULL-Cコアボード。   CTP接続時はI2Cエラーなしで安定的に動作します。   LCDディスプレイとCTPを同時に接続すると、CTP上でランダムにI2C通信例外が発生し、タッチ機能が時折動作しなくなる。 LCD回路によって発生する電磁干渉が、タッチパネルのI2C信号の不安定化を引き起こしているのではないかと疑っています。   関連するカーネルのdmesgログを分析のために添付します。   当社のソフトウェア環境:Linux 4.1.15BSP。   CTPはI2Cバスを介して通信します。ハードウェアの配線と電源を確認しましたが、問題は依然として解決していません。   技術的なご提案をお待ちしております。
記事全体を表示
MIFARE DesFire EV3/EV3C 4 字节 NUID 配置 MIFARE DesFire EV3/EV3C 都可以配置 4 字节 NUID,但是当使用 RFIDDiscover 设置配置时,它会显示设置的 4 位 NUID(仅适用于 MIFARE DesFire EV3 C),我们怎样才能为 RFIDiscover 的 DesFire EV3 设置 4 字节 NUID? DSC Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration 你好 感谢您对我们的产品感兴趣。 我必须澄清,MIFARE DESFire EV3 与 MIFARE DESFire EV3C 是不同的 IC。 Re: MIFARE DESFire EV3C configuration 亲爱的 Fabian,我们在全球拥有庞大的工业房地产投资组合 (>700!)因此,我们尝试使用 EV3 [C]。因为我们的许多办公室、仓库和生产都使用 Mifare Cassic。而在德国、挪威和中国,我们的所有读卡器等都使用 DESFire。问题: 我们不知道如何在西门子 Siportsoftware 中为卡编码。我们需要保留现有的 Classic 密钥,并创建一个新的 DESFire 密钥。如何做到这一点?我们只有很少的测试卡,所以不想让它们崩溃。西门子方面没有提供手册,但有一个现有功能(德语: Ausweis codieren (Mifare Classi 和 DESFire) 我想给您发一张图片,但不知道如何发送。 Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration 是的,我知道,我在寻找如何在 Siport/Sipass 软件中对 EV3[C] 卡进行编码的任何信息,Siport/Sipass 是全球最常用的解决方案。保留经典钥匙,增加 DESFire 红色钥匙。即使在西门子股份公司内部,对此也知之甚少。 MIFARE DESFire EV3 C help is needed 阅读发送给用户 Barton 的消息。我们需要西门子股份公司提供的 DESFire Ev3 C 方面的支持,以及使用 Siport 或 Sipass 进行编码,因为我们使用的是这些编码和访问控制软件。我们需要帮助,否则我们不会购买这款产品,而是会继续使用过时的经典款。 Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration 您好,先生, 我给你发了私信。 Re: MIFARE DESFire EV3 / EV3C 4-byte NUID configuration 尊敬的 Fabian,我是 NXP 支持团队的成员。我们希望为我们的 13 万名员工配备 EV3 C。我们在全球 700 个地点拥有各种类型的读卡器。我们有一些测试卡,但一直无法使用红钥匙进行编码。经典密钥已存在于系统中,应该继续使用。DESFire密钥应该以此为基础。我们需要卡片编码方面的帮助。我们有Siport和Sipass这两款编程软件。
記事全体を表示
Unresolved: The programmer cannot burn TEA2016 and TEA2017. Our customer received two batches of I2C programmers for programming TEA2016 and TEA2017. The older programmers worked without issues, but the newly delivered programmers mostly encountered problems during programming, making it impossible to program. The customer's description is below: Please refer to the documentation. Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017 Hello 風火 Good day! There is no record of any complaints about the new programmer. Please provide the I²C waveforms captured during a successful programming cycle (old programmer) and a failing cycle (new programmer) It would also be very helpful if you could share the part number or distinguishing number between these two products. If I'm not mistaken, you're using RDK01DB1563, right? Have a great day and best of luck. Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017   The waveforms of the old and new boxes testing the same product are shown below. Please help analyze why the new box cannot be tested. _0-1784508231440.png _1-1784508244694.png The new box test FAIL waveform is as follows: _2-1784508277742.png _3-1784508289288.png _4-1784508300765.png _5-1784508337980.png _6-1784508346130.png Thank you! Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017 I've provided the waveform in this post; could you please analyze it for me? Thank you!
記事全体を表示
尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017 我们的客户有两个批次的I2C烧录器,用于烧录TEA2016和TEA2017.其中旧的烧录器使用没有问题,新交付的烧录器大多数情况下烧录出现问题,导致无法烧录。以下为客户描述:請參考文檔 Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017 风火你好 再会! 没有关于这位新程序员的任何投诉记录。 请提供在成功编程周期(旧编程器)和失败编程周期(新编程器)中捕获的 I²C 波形。 如果您能提供这两个产品的零件编号或区分编号,那就非常有帮助了。如果我没记错的话,你用的是 RDK01DB1563,对吧? 祝你今天过得愉快,一切顺利。 Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017   新舊盒子測試同一臺產品的波形如下,請幫忙分析為什麼新的盒子測試不了 _0-1784508231440.png _1-1784508244694.png 新的盒子測試FAIL波形如下: _2-1784508277742.png _3-1784508289288.png _4-1784508300765.png _5-1784508337980.png _6-1784508346130.png 謝謝! Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017 我在這個帖子上提供波型,請幫忙分析一下,謝謝!
記事全体を表示
Uart using DMA is not working correct on S32K314 Hello,  We are currently trying to configure LPUART0 channel to work with DMA. The uart channel need to be working at a bitrate of 1Mbps. Our current configuration for UART and DMA looks like this.  CosminSbera_0-1784803400829.png CosminSbera_1-1784803453733.png CosminSbera_2-1784803479911.png CosminSbera_3-1784803495720.png CosminSbera_4-1784803522819.png CosminSbera_5-1784803539872.png The clock is enable in MCU, the buffers are declared inside a non cacheable area , the DMA ISR priority is smaller than the LPUART. Our problem is that we are not able to see the data inside the RX buffer or is incomplete.  Our workflow is like this (similar to LIN communication 😞 prepare rx buffer -> AsyncReceive send the header to the slave -> AsyncSend wait until the data from the slave is received in the next cycle (my function runs in a 1ms task) If I put a break point after AsyncSend is executed I can see all the data send from slave inside the RX buffer. If I let it run there is nothing there or is incomplete. My assumption is that the DMA interrupt comes later.  Could you give us some hints on what is wrong inside our configuration or what I could check next? Thank you! Cosmin Re: Uart using DMA is not working correct on S32K314 Hi@CosminSbera 1.Don't forget to enable DMA Request Option. Senlent_0-1784861937675.png 2.Don't forget to enable the LPUART0_IRQn interrupt in the "Platform" component. "Platform"->"LPUART0_IRQn --LPUART_UART_IP_0_IRQHandler“
記事全体を表示
TagWriterはPN7160タグを読み取ることができません 私はRWandCEのサンプルプログラム(LPC55S69+PN7160)を実行しています。AndroidスマートフォンでTagWriterアプリを使ってタグを読み取ろうとすると、応答がなく失敗します。ログには、ポーリングモードが有効になったことが示されています。しかし、TagInfoはそれを読み取ることはできますが、「通信中断」のポップアップが表示され、電話機に表示される結果が正しくない可能性があります。これは、検出ループでポーリングとリスニングの両方が有効になっているためでしょうか?しかし、私の要件は、ポーリングとリスニングの両方を同時に有効にすることです。また、Androidスマートフォン上のすべてのエミュレーションカードも無効にしました。 BillyHu_0-1783415582716.png どうか助けてください、ありがとうございます。 LPC55xx Re: TagWriter can not read the PN7160 tag こんにちは、 @BillyHu さん。 あなたの調子が良いといいのですが。 PN7160 FWを最新バージョンに更新してみてください。詳細については、 PN7160 - MCUXpressoのFWアップデート を参照してください。 よろしくお願いいたします。 エドゥアルド。 Re: TagWriter can not read the PN7160 tag こんにちは、エドゥアルドさん。 私のファームウェアのバージョンは既に12.50.11です。ポールとリッスンは個別に使うと問題なく動作しますが、discoveryTechnologiesで両方を有効にしていると、タグライターを使ってPN7160のカードエミュレーションを読み取ることができません。そちら側でも同様の問題が発生したことはありますか? ありがとうございます Re: TagWriter can not read the PN7160 tag エドゥアルド様、 何かご提案はありますか?この現象はPN7160では正常なものですか? ありがとうございます
記事全体を表示
i.MX93处理器并行编程系统 我正在使用imx93处理器,需要同时对两块板子进行编程。但是每当我尝试这样做时,其中一个板子会出现HID(W)错误,而其他板子的刷写则成功完成。 uu.exe -m 1:10 -b uuu-xxxxxx.flash uu.exe -m 1:7 -b uuu-xxxxxx.flash 即使我指定路径(1:10,1:7),也会出现同样的错误。 请指导。 Re: Parallel Programming System for i.MX93 Processors 你好, 请尝试运行以下命令: uuu -d -m 1:7 -m 1:10 uuu-xxxxxx.flash 你能得到什么? uuu -lsusb 请确保您使用的端口与枚举结果一致。 顺祝商祺!
記事全体を表示
FETMX6ULL-C:LCD 和 CTP 同时连接时出现随机 CTP I2C 通信错误,CTP 硬件平台:FETMX6ULL-C 核心板。   当仅连接电容式触摸面板 (CTP) GT911 时,该面板能够稳定工作,不会出现任何 I2C 错误。   同时连接液晶显示屏和CTP后,CTP上会出现随机的I2C通信异常,导致触摸功能偶尔失效。 我们怀疑液晶显示电路引入的电磁干扰导致触摸面板的 I2C 信号不稳定。   已附上相关的内核 dmesg 日志以供分析。   我们的软件环境:Linux 4.1.15电路板支持包。.   CTP通过I2C总线进行通信。我们已经检查了硬件线路和电源,但问题仍然存在。   期待您的技术建议。
記事全体を表示
GUIGuider 1.10.1 to 2.0.0 migration We have build our GUIGuider projects in version 1.10.1 and I am interested in migrating to the new 2.0.0 version to check out the new features. I found out the old GUIGuider project file could not be loaded in the new version, and I think it is because of the new JSON structure 2.0.0 projects use. Is there an easy way to migrate the projects to the newer version of GUIGuider or do we have to manually convert it? Re: GUIGuider 1.10.1 to 2.0.0 migration Hi @MJHammers_ICP, As you correctly mention, due to the redesigned architecture and new project structure of GUI Guider v2.0.0, this new version of GUI Guider is not fully backward compatible with GUI Guider v1.x. The recommended path would be to recreate the project in GUI Guider v2.0 rather than attempting a file-level conversion. You can find the recommended migration workflow to help you with this task in the following link: Tutorials — GUI Guider Documentation BR, Edwin.
記事全体を表示
未解決: プログラマーは TEA2016 および TEA2017 を書き込むことができません。 お客様はTEA2016およびTEA2017のプログラミング用に、2つのバッチのI2Cプログラマを受け取りました。以前のプログラマは問題なく動作しましたが、新しく納品されたプログラマはプログラミング中にほとんどの場合問題が発生し、プログラミングが不可能でした。お客様からの説明は以下のとおりです。ドキュメントを参照してください。 Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017 こんにちは風火 良い一日! 新しいプログラマーに関する苦情の記録は一切ありません。 プログラミングが成功したサイクル(旧プログラマー使用時)と失敗したサイクル(新プログラマー使用時)で取得したI²C波形を提供してください。 また、これら2つの製品の部品番号や識別番号も教えていただけるととても助かります。私の記憶が正しければ、あなたはRDK01DB1563を使用していますよね? 良い一日をお過ごしください。幸運を祈ります。 Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017   下記は、同じ製品をテストした旧型および新型ボックスの波形です。新型ボックスがテストできない理由を分析するお手伝いをお願いします。 _0-1784508231440.png _1-1784508244694.png 新しいボックステストのFAIL波形は以下のとおりです。 _2-1784508277742.png _3-1784508289288.png _4-1784508300765.png _5-1784508337980.png _6-1784508346130.png ありがとう! Re: 尚未解決: 燒錄器不能燒錄 TEA2016和 TEA2017 この投稿に波形を添付しましたので、分析していただけないでしょうか?よろしくお願いいたします!
記事全体を表示
TagWriter can not read the PN7160 tag I am running the RWandCE example(LPC55S69+PN7160). When I use the TagWriter app on an Android phone to read the tag, it fails with no response. The log shows that it activated the poll mode. However, TagInfo can read it, but it shows a "communication interrupt" popup, and the result on the phone may be incorrect. Is this because both poll and listen are enabled in the discovery loop? But my requirement is that both poll and listen must be enabled simultaneously. And  I have also closed all emulation cards on my android phone. BillyHu_0-1783415582716.png Please help me, thanks. LPC55xx Re: TagWriter can not read the PN7160 tag 你好@BillyHu 希望你一切都好。 请尝试将PN7160固件更新到最新版本。您可以参考“PN7160 - 通过MCUXpresso进行固件更新”了解更多信息。 问候, 爱德华多。 Re: TagWriter can not read the PN7160 tag 你好,爱德华多, 我的固件版本已经是 12.50.11 了。单独使用轮询和监听功能时,两者都能正常工作,但当在 discoveryTechnologies 中同时启用这两个功能时,我无法使用 tagwriter 读取 PN7160 的卡模拟信息。您那边遇到过这个问题吗? 谢谢! Re: TagWriter can not read the PN7160 tag 亲爱的爱德华多: 您有什么建议吗?PN7160出现这种现象正常吗? 谢谢!
記事全体を表示
Parallel Programming System for i.MX93 Processors I am using a imx93 processor i need to program two boards at a time. But whenever i try that on of the boards get an HID(W) error and others flashing gets completed successfully. uu.exe -m 1:10 -b uuu-xxxxxx.flash uu.exe -m 1:7 -b uuu-xxxxxx.flash Even when i specify the path(1:10,1:7) i get the same error. Please guide. Re: Parallel Programming System for i.MX93 Processors Hello, Please try to run the next command: uuu -d -m 1:7 -m 1:10 uuu-xxxxxx.flash What do yo get with: uuu -lsusb Please make sure that you are using the correct port according to the enumeration. Best regards.
記事全体を表示