2398088_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2398088_en-US

2398088_en-US

NXP reference firmware for traction/axial motors

Hello,

I am working on a Traction/Axial control motor project and I wanted to know about the reference software for the Axial motor based development from NXP,so it will be very helpful for the reasearch and development of our ongoing project.

So I am requesting to provide me the solution for this and also the reference software for Traction/Axial motor from NXP will be a solid reference for our R and D.

Thank you
Pavan

Re: NXP reference firmware for traction/axial motors

Hello,

NXP does not provide dedicated software specifically for axial-flux motors. In most cases, axial-flux PMSM motors can be controlled using the same PMSM FOC reference software as conventional radial-flux PMSM motors. The main adaptation is the motor parameterization (Rs, Ld, Lq, pole-pair count, flux linkage, etc.), while the control algorithm remains essentially the same.

Typical starting points are:

  • S32K344 / S32K396 motor-control reference designs
  • PMSM Field-Oriented Control (FOC) examples
  • AMMCLIB motor-control library
  • Model-Based Design Toolbox examples (if MATLAB/Simulink is used)

Best regards,

Peter

Tags (1)
No ratings
Version history
Last update:
‎07-24-2026 02:30 AM
Updated by: