i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
A discussion of random hangs and other issues using Windows Embedded Compact on Freescale i.MX6 application processor and how they were solved. This white paper is about the investigation and shares some of our discoveries. All information in this document applies to Windows Embedded Compact 7 and 2013 as well as all variants of the i.MX6.    
記事全体を表示
NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator. The aggregator portion of the i.MX Power Profiling System sits between the "smart" current sensor boards and the host computer. It provides power and signal connections to each connected sensor board. The communication is done over I2C, where three I2C bus extenders (PCA9518) effectively provide a dedicated bus to each I2C device, to better allow for cabling.  More information will follow... A photo, layout images and schematic attached below.   MBED source for the FRDM-KL25Z is available here: 30848-KL25Z-AGGREGATOR    Smart Sensor Connections At each smart sensor header JP0-JP13, these are the connections provided: 5V: powers the 3.3V regulator on each sensor board 12V: all the gates of all the switching FETs are pulled pulled up to 12V GND: ground connection SCL/TX0: I2C clock line  SDA/RX0: I2C data line  SWD_CLK:  global line for triggering smart sensors to make measurements RESET_B:  global line for resetting all smart sensor boards SWD_IO_n: individual select line for each smart sensor I2C Bus Connection Three I2C bus extenders (PCA9518) provide buffered connections between the FRDM board and all the connected smart sensors. The bus extenders were added to allow for longer cables between the aggregator and the smart sensor boards. Each bus extender has five ports and along with connections that allow extending the bus to more bus extenders. Gate Supply The aggregator contains a boost regulator that boost the 5V input from the FRDM board to 12V. The boosted voltage is fed to each of the smart sensor headers. It's used by the smart sensor board to pull up the gates of the switching FETs above any of the rails under test by at least 4.5V in order to benefit from a lower Rds(on). Caution must be exercised with some older FRDM boards since the 5V from the USB connection passes through diodes with a maximum current of 200mA.  The boost regulator and the load presented by the smart sensor boards may exceed the diode's limit and damage it. (Yes, it's happened... two older FRDM-KL25Z boards were used during development. One of them failed with the diode shorted (~0.05 Ohms), so everything kept working. The other failed with a  short of ~45 Ohms, so it kind of worked but not really...) Application Code for Aggregator  To date, application code has only been developed for the FRDM-KL25Z board. The latest application code resides at: https://os.mbed.com/users/r14793/code/30848-KL25Z-AGGREGATOR/, with the latest binary attached below. SWD Programming of Smart Sensors  Connectors J5 and JP15 are provided as an adapter for programming the smart sensor boards via SWD. JP15 provides power to the smart sensor board, since they have no direct 3.3V input for the KL05Z. An SWD programmer (or suitably modified FRDM-KL05Z board) connects to J5. Both connections use 10-pin 0.05"-spaced ribbon cables. Additionally, when a smart sensor is connected to JP15, J6 provides access to the UART pins of the smart sensor (the I2C pins on the smart sensor also mux out the UART of the KL05Z). No hardware changes are necessary at all; changing the code running on the smart sensor is all that's required. In fact, during the initial prototyping of the smart sensors, the serial UART connection was used instead of I2C. Modify Aggregator To Use SWD Dongle To Program Smart Sensor:  Add a wire as shown on the bottom side of the aggregator board as shown below. This ties 3.3V on the aggregator to the debug header, enabling the voltage level translators on the dongle to communicate with the KL05Z on the smart sensor board.  
記事全体を表示
Q: What is i.Mx6 ECSPI max frequency? https://community.freescale.com/message/338305 But in the RM we clearly state 60 MHz is the default config while Boot from SPI. I cannot measure it because I have no board where I can boot from SPI Nor. Also if I look at clocking, PLL  is 480MHz divided by 8 is fixed thus we get 60 MHz. Next divider can be either 1, thus ECSPI_CLK_ROOT  = 60MHz or 2, thus ECSPI_CLK_ROOT = 30 MHz. A: From i.MX6 Datasheet (IMX6DQCEC, Rev. 2.3, 07/2013), Table 52 (ECSPI Master Mode Timing Parameters) : ECSPIx_SCLK Cycle Time–Read • Slow group                                        55 ns • Fast group                                        40 ns         ECSPIx_SCLK Cycle Time–Write          15 ns So, only for writing we can get ~60 MHz.
記事全体を表示
The Linux L4.14.98_1.0.0_GA; and SDK2.5 for 8QM/8QXP Post GA, SDK2.5.1 for 7ULP GA3 release are now available. Linux on IMX_SW web page, Overview -> BSP Updates and Releases -> Linux L4.14.98_2.0.0 SDK on https://mcuxpresso.nxp.com Files available: Linux:  # Name Description 1 imx-yocto-L4.14.98_2.0.0_ga.zip L4.14.98_2.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 L4.14.98_2.0.0_ga_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6Solox Linux Binary Demo Files 3 L4.14.98_2.0.0_ga_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 L4.14.98_2.0.0_ga_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 L4.14.98_2.0.0_ga_images_MX7DSABRESD.zip i.MX 7Dual SABRESD Linux Binary Demo Files  6 L4.14.98_2.0.0_ga_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  7 L4.14.98_2.0.0_ga_images_MX8MMEVK.zip i.MX 8MMini EVK Linux Binary Demo Files  8 L4.14.98_2.0.0_ga_images_MX8MQEVK.zip i.MX 8MQuad EVK Linux Binary Demo files 9 L4.14.98_2.0.0_ga_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 L4.14.98_2.0.0_ga_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.tar.gz System Controller Firmware (SCFW) porting kit of L4.14.98_2.0.0 12 imx-aacpcodec-4.4.5.tar.gz Linux AAC Plus Codec v4.4.5 13 VivanteVTK-v6.2.4.p4.1.7.8.tgz Vivante Tool Kit v6.2.4.p4.1.7.8   SDK: On https://mcuxpresso.nxp.com/, click the Select Development Board, EVK-MCIMX7ULP//MEK-MIMX8QM/MEK-MIMX-8QX to customize the SDK based on your configuration then download the SDK package.  Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD and SABRE-AI Boards MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board What’s New/Features: Please consult the Release Notes.   Known issues For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-sumo ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-sumo#
記事全体を表示
These instructions used ltib-imx27ads-20071219. First, get u-boot v2.0: git clone http://git.denx.de/u-boot-v2.git u-boot-v2 Enter the U-Boot directory: cd u-boot-v2 Export the proper compilation paths and environment variables: export ARCH=arm export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" export CROSS_COMPILE=arm-none-linux-gnueabi- Configure it for the i.MX27ADS board: make mx27ads_defconfig You may want to enable the FEC driver: make menuconfig And go to Drivers -> Network drivers and select Yes on i.MX FEC Ethernet driver Exit the config menu (don't forget to save the configuration) and just make it: make Or if you prefer the verbose mode make V=1 After a quick build, you should get a uboot.bin on your current directory. I used the ADS Toolkit to program the NOR flash.
記事全体を表示
I followed the Yocto Training up until Task #4 - Deploy and test.... and I got stuck here. I am not able to download the .sdcard image to my SD card. Do I need to format it first? It is brand new. Since the sudo dd if=core-image-base-imx6solosabresd.sdcard of=/dev/sdb1 bs=1M did not work for me, I was not able to boot from the SD on my board. The board switches are set to boot from SD4. Is imx6solosabresd the correct MACHINE to use for the solox? I tried setting MACHINE=imx6sxsabersd in the local.conf file but I got an error message (Task #2). This is why I want to try the MFGTool. I have set the board to boot from SD3 so it can go into "download mode". When I go through the MFGTool, it says No Device Connected although HID-compliant vendor-defined device shows up. This document was generated from the following discussion: 
記事全体を表示
The attached patches slow-down the DDR's clock (from 528000000Hz to 396000000Hz) on i.MX6Q Sabre SDB-P boards. These were tested on Android JB4.2.2_1.0.0 and Linux L3.0.35_4.1.0. To verify patches were correctly applied, one the serial console one should see the following TWO bold lines Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ] Boot Device: MMC I2C:   ready DRAM:   1 GB MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3 *** Warning - bad CRC or MMC, using default environment mx6q pll1: 792MHz mx6q pll2: 528MHz mx6q pll3: 480MHz mx6q pll8: 50MHz ipg clock     : 49500000Hz ipg per clock : 49500000Hz uart clock    : 80000000Hz cspi clock    : 60000000Hz ahb clock     : 99000000Hz axi clock   : 198000000Hz emi_slow clock: 99000000Hz ddr clock     : 396000000Hz usdhc1 clock  : 198000000Hz usdhc2 clock  : 198000000Hz usdhc3 clock  : 198000000Hz usdhc4 clock  : 198000000Hz nfc clock     : 24000000Hz In:    serial Out:   serial Err:   serial Found PFUZE100! deviceid=10,revid=10 Net:   got MAC address from IIM: 00:04:9f:02:67:46 FEC0 [PRIME] Hit any key to stop autoboot:  0 kernel   @ 10808000 (4709060) ramdisk  @ 11800000 (183100) kernel cmdline:     use boot.img command line:     console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale Starting kernel ... Uncompressing Linux... done, booting the kernel. . . . sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms Set periph_clk's parent to pll2_pfd_400! arm_max_freq=1.2GHz . . .
記事全体を表示
Hi All, The i.MX6 Android R13.4.1.04 patch release is now available onwww.freescale.com ·         Files available # Name Description 1 IMX6_R13.4.1.04_ANDROID_PATCH This patch release is based on the i.MX 6 Android R13.4.1   release. The purpose of this patch release is correct the PFD workflow in   U-Boot, fix the miscalibration issue for the thermal sensor and corrects   ramp-up time of the internal LDOs
記事全体を表示
Voltage overshoot (>1.8V) is found on VDD_ARM_SSOC_IN when the EVK board is powered down by POWER BUTTON long pressed after the Linux kernal loaded. It would not happen if only U-boot is run. It happens also when the system recovers from idle. The overshoot is out of i.MX6UL maximum rating.
記事全体を表示
You can boot from SPI NOR Flash using the following procedure:      1 - Download ATK Release 1.7. The version ATK 1.7 can be downloaded here. 2 - Unzip file iMX_AdvancedToolKit_R170.zip into "C:\Program Files\freescale\AdvancedToolKit-STD\image\".      3 - Open the file "C:\Program Files\freescale\AdvancedToolKit-STD\config\ADSToolkit.cfg" and add the following lines: [MX25_TO11] MMC/SD::image\mx25_mmc.bin:0x(unknown) NAND::image\mx25_nand.bin:0x(unknown) SPI::image\mx25_spi.bin:0x(unknown) [MX31]   4 - Set the SPI Boot Config on MX25PDK:   SW22: no influence SW21[1-8]: 11110010 BT_MEM_CTL[0:1] = 11 (Expansion) BT_MEM_TYPE[0:1] = 11 (Serial ROM via SPI) BT_PAGE_SIZE[0:1] = no influence BT_BUS_WIDTH[0:1] = 10 (3-Address SPI (24-bit) Note: BT_BUS_WIDTH[0]=1, BT_BUS_WIDTH[1]=0 On Debug Board the red switches: (SW5-SW10) = 000011 (0=off) Boot Config Switches (SW21, SW22) on Personality Board have no influence.   5 - Connect USB or Serial cable between Host PC and PDK and execute ATK   6 - Select USB/UART serial boot on MX25PDK and power on the board   7 - Configure ATK as following: Device = i.MX25_TO1.1 device memory initial = DDR2 Communication channel: COMn (select the COM port on your PC) or Communication channel: USB If you choose COM (serial UART connection) you MUST disconnect USB cable from OTG connector on i.MX25 PDK.   8 - Configure ATK "Flash Tool" as following: Tick "Program" Tick "Read Back Check" Flash Model = SPI Address = 0x0 Image = mx25_3stack_redboot_TO1_1.bin (same file as for NAND boot). Same should be applicable to U-boot.   Note: SPI NOR Boot requires internal boot mode. On Debug Card all red switches must be off (SW5-SW10) = 000000 (0=off). Note: if booting from SPI NOR, Redboot needs approx 2 seconds before it shows messages on the console.
記事全体を表示
This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX28 L2.6.35_1.1.0_130130. It has been tested to build GNOME profile and with FSL Standard MM codec. A) Basic Requirement: Set up the Linux Host PC using ubuntu-13.10-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 $ sudo apt-get install libc6-dev-i386 $ sudo apt-get install u-boot-tools $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd $ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so   /usr/lib/librt.so C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L2.6.35_1.1.0_130130_source.tar.gz $ ./L2.6.35_1.1.0_130130_source/install After that, you will find ~/ltib directory created D) Apply the patch to make L2.6.35_1.1.0_130130 could be installed and compiled on Ubuntu 13.10 64bit OS $ cd ~/ltib $ git apply 0001_make_L2.6.35_1.1.0_130130_compile_on_ubuntu_13.10_64bit_OS.patch What the patch is doing: a) The patch modifies the following files: dist/lfs-5.1/base_libs/base_libs.spec dist/lfs-5.1/elftosb/elftosb.spec dist/lfs-5.1/lkc/lkc.spec dist/lfs-5.1/mux_server/mux_server.spec dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory: pkgs/elftosb-2.6.35.3-1385779630.patch pkgs/elftosb-2.6.35.3-1385779630.patch.md5 pkgs/lkc-1.4-lib.patch pkgs/lkc-1.4-lib.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L2.6.35_1.1.0_130130_docs/doc/mx28/Setting_Up_LTIB_Host_on_Ubuntu_9_04.pdf https://community.freescale.com/docs/DOC-93394 https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 scrollkeeper is for the gnome-desktop compilation elftosb compilation issue fixed by added -lm to LIBS in the elftosb-2.6.35.3-1.1.0/makefile.rules NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
記事全体を表示
Dear,   We want to start application program from bootloader, we have below questions: We we use I.MX6UL bootrom start BootLoader, we need use mkimage.sh, compile and generator bin file, then we convert to executable file. If we need use Bootloader run application program,whether application image also need convert by mkimage.sh?  The file which convert by mkimage.sh is compressed file. we do not know its format, how about its start address, how to realize the the address jump, do you have example? Thanks.  
記事全体を表示
The document includes the following contents: (1)document how to port ov5646 to android jb4.2.2 (2) ov5645 driver for Linux 3.0.35 (3) ov5645 schematic based on i.MX6Q/DL (4)ov5645 for android camera HAL   [Note:]      P5V29A-0JG is a camera module based on OV5645, and PAO532-0JG is based on OV5640, both manufactured by NINGBO SUNNY OPOTECH CO.LTD (China), If customer wants to use them on i.MX6 platform, can send me email to ask for datasheets of P5V29A & PAO532 , or discuss corresponding questions on porting.   Email: [email protected]
記事全体を表示
Add kcontrol API for Headphone Jack and Spk for WM8962, from this kcontrol, you can use amixer to change freely between Headphone and Spk. The names of the mixers 1: HP Function 2: SPK Function amixer controls: numid=62,iface=MIXER,name='HP Function' numid=63,iface=MIXER,name='SPK Function' 1: How to enable HeadPhone using this Kcontrol: amixer cget numid=62 numid=62,iface=MIXER,name='HP Function'    ; type=ENUMERATED,access=rw------,values=1,items=2    ; Item #0 'off'    ; Item #1 'on'    : values=0 amixer cset numid=62 1 //enable HP numid=62,iface=MIXER,name='HP Function'    ; type=ENUMERATED,access=rw------,values=1,items=2    ; Item #0 'off'    ; Item #1 'on'    : values=1 2: How to enable Speaker using this Kcontrol: amixer cget numid=63 numid=63,iface=MIXER,name='SPK Function'    ; type=ENUMERATED,access=rw------,values=1,items=2    ; Item #0 'off'    ; Item #1 'on'    : values=0 amixer cset numid=63 1 //SPK enable numid=63,iface=MIXER,name='SPK Function'    ; type=ENUMERATED,access=rw------,values=1,items=2    ; Item #0 'off'    ; Item #1 'on'    : values=1
記事全体を表示
       There are 8 UART ports on i.mx6ul and one uniform Linux driver for these UARTs. Form UART1~UART6, there is no special operation or attention to use them. But for UART7/UART8, there is a special rule to enable them.       According to i.mx6ul RM, we can see UART7/8 RTS pins are muxed with ENET TX_CLK pins. When SION bit of ENET_TX_CLK is set, we need switch to other MUX mode as input signal for UARTx_RTS. Otherwise, UARTx_RTS will be interrupted by loopback ENET clock signal. So we should set IOMUXC_UART7_RTS_B_SELECT_INPUT and IOMUXC_UART8_RTS_B_SELECT_INPUT registers to 0x2/03 to avoid ENET clock's conflict no matter whether we enable UART7/8 RTS/CTS function or not. Let's summarize the different scenarios to enable UART7/8 as follows: 1. ENET driver is disabled and UART7/8 is enabled. There is no special operation to do, just use UART7/8 like other UARTs 2. ENET and UART7/8 are both enabled. There are two use models, RTS/CTS enabled or disabled.     2a. If we enable RTS/CTS feature and configure RTS/CTS pins in the device tree, of course, we should avoid the conflict between UART CTS/RTS pins and ENET TX_CLK pins. There is no special operation to do becuase your RTS/CTS device tree would automatically set  IOMUXC_UART7_RTS_B_SELECT_INPUT/ IOMUXC_UART8_RTS_B_SELECT_INPUT register to correct value.     2b. If we don't enable RTS/CTS feature and no RTS/CTS pin configuration in devcie tree, we should manually add code to set  IOMUXC_UART7_RTS_B_SELECT_INPUT/  IOMUXC_UART8_RTS_B_SELECT_INPUT register because the default value is 0x0(ENETx_TX_CLK_ALT1) Here is an example to show how to use UART7 on EVK board in scenario 2b. 1. modify imx6ul-14x14-evk.dts to enable UART7     a. remove all  LCD settings to disable lcdif because we configure UART7 TX/RX pin pad to LCD data line     b. add UART7 related settings                &uart7 {                     pinctrl-names = "default";                     pinctrl-0 = <&pinctrl_uart7>;                    status = "okay";                 };               &iomuxc {                   pinctrl-names = "default";                   pinctrl-0 = <&pinctrl_hog_1>;                   ....                           pinctrl_uart7: uart7grp {                           fsl,pins = <                                       MX6UL_PAD_LCD_DATA16__UART7_DCE_TX 0x1b0b1                                       MX6UL_PAD_LCD_DATA17__UART7_DCE_RX 0x1b0b1                           >;                  }; 2. add code to set IOMUXC_UART7_RTS_B_SELECT_INPUT register in arch/arm/mach-imx/mach-imx6ul.c          static void __init imx6ul_init_machine(void)          {               struct device *parent;               void __iomem *iomux;               struct device_node *np;               ...........               imx6ul_pm_init();               np = of_find_compatible_node(NULL,NULL,"fsl,imx6ul-iomuxc");               iomux = of_iomap(np, 0);               writel_relaxed(0x2,iomux+0x650);            } 3. build zImage and imx6ul-14x14-evk.dtb 4. Test in linux console      root@imx6ulevk: ls /dev/ttymxc*                      //you can see ttymxc6 is in the list     root@imx6ulevk: echo hello > /dev/ttymxc6         root@imx6ulevk:
記事全体を表示
Background Configure Trace32 Attach to SCFW with Lauterbach Snooping Perf Examples Example 1 : Snoop a function call (or a variable) Example 2: MonitorFrame Per Second Example 3: Monitor Frame Per Second and rendering size Background None of my automotive have trace pins on their board. Trace is consequently not possible. Anyway you can do "Snooping" with your Lauterbach JTAG probe. Snooping just send data as fast as possible. In the following example I will Snoop the i.MX8X' SCFW, notice I do not have the sources (except board.c) but I have the elf file (thus I have debug info with functions names for instance). Notice Snooping is available on all MCU/MPU with JTAG.   In my case I used it for the first time in 2015 on Vybrid, our first heterogeneous dual core (Cortex-A5 & Cortex-M4) with no XRDC... My customer has sent the final product with a JTAG connector and flashed SW product to me. I had a laconic comment: "software is done all around the world in UK, India and the US, when we flash all the software the Vybrid Reset for some version, we don't have the sources for this specific software we have flashed in this product. Good Luck". In this case snooping on both core at the same time was the only solution for me... At the end I have discovered (thanks to the last PC addresses before the crash) the cortex-A5 was deconfiguring a pin of the QSPI flash interface on which the M4 was eXecuting In Place (XiP). Configure Trace32 When your Trace32 is open, CPU>>System Settings... menu and configure the JtagClock as fast as possible (here 40MHz) to have fast data streaming: go in Trace>>Configuration menu Select "SNOOPer" Select to stream the Pointer Counter thus select the mode "PC" Pass to State to "Arm" You can increase also the SIZE of the buffer Launch your code: Attach to SCFW with Lauterbach In Trace32, CPU>>System Settings, chose IMX8QXP-SCU: And then do an "Attach": Then yu should see your SCU core running: Snooping And break your code, your "used" field " should be filled: Open Trace>>List>>Default Click on "Chart" On the trace list you can see the sampling rate: around 48µs in our case. It means you may (almost) not see functions lasting less than 48µs (depends when it is sampled), or you'll see it sometimes. But for performance analysis it can be useful to see which function is too slow (rather then instrument the code), but as I mentioned in my case function has to last more than 48µs! Perf You can also get Performance analysis. But keep in mind if your function is faster than 48µs in my case, the result will not be accurate! Go in Perf>>Perf Configuration (it can also be done un real time with Perf>>Perf List Dynamic)... and select "Snoop": Then put the State in "Arm" and click on "List" to open the "List Window" Launch your code and stop it. In the "List" window you'll see all the function ranked according to their usage occurrence (my SCFW is almost always in sleep!) Examples Example 1 : Snoop a function call (or a variable) With Snooping you cannot trace a function calls. To do that I add a global variable in the function. You'll have a little overhead due to that. I will use an i.MXRT1170 with the SDK 2.6.1. I have built the Tiger example (vglite). April 4th 2020: i.MXRT1170 is not public, meaning not officially supported by Lauterbach. Please follow the instruction in my SharePoint folder (if the link disappears, it may signify i.MXRT1170 is supported) to add support of the i.MXRT1170. https://nxp1-my.sharepoint.com/:f:/g/personal/vincent_aubineau_nxp_com/Ej8ID8mXaNZPnVgTWgYgqHQBzR0XcE0K4sl1WusR3UMBnw?e=…  I want to know the framerate. To do that I have to monitor the redraw() calls. What I do, is I put the "n" variable as global. Trace>>Configuration ... Chose "memory" and "changes" (to log only when the variable is changing): Then then click on select... and "i" Search for "n" variable and select it: Launch your software and then do a break. Click on "List": You have the list of your function call (as you can see it is not always the same), in the "ti. call" you have the duration between 2 call (keep in mind the function must not be called at high frequency: If you click on "draw", you can display the variable values (click on  to scale it): Example 2: Monitor Frame Per Second I can also monitor the fps if I pass "time" variable global: And you can have a reprensentation of you fps (notive I have unchecked "Changes" to have an easy to intrepret curve Example 3: Monitor Frame Per Second and rendering size Results often depends of several variables. If you display 2 variables on 1 display window, if the 2 variable does not have the same range, it is not easy to observe. The best solution I have found in this case is to have 2 "Draw" Windows. Add the 2 variables in the "SElect" field ("time" and "ScaleCount", beware, it is case sensitive). Launch your code, and stop it after a while. Then right click on the "time" and "ScaleCount" variable in your code to display 2 "Draw" window: Thus you have 2 "Draw" windows, and you see FPS depends on rendering size... logical!  
記事全体を表示
Video Tips for video in host side Testing Image Sensor and Display Testing on i.MX31 PDK Gstreamer in the iMX board The i.MX family has a big set of plugins that enable a lot of formats. It has some hardware acceleration, but each board has some peculiarities. I.MX27ADS Board I.MX51EVK Board I.MX53QSB Board How to create an application to play Audio+Video using gstreamer TV Out - Configuring I.MX27ADS TV Out AlphaBlending AlphaBlending is used to exibhit two images on display, one of these is transparent image. Normally you use a solid background image and a transparent (alpha) image on foreground. i.MX31PDK AlphaBlending DirectFB i.MX31PDK DirectFB How to get a screenshot from framebuffer display? i.MX31PDK Screenshot Theora Creating a Theora Encoder Example
記事全体を表示
The imx_bootlets package in LTIB contains the code that will be the first code loaded and executed by ROM when booting a build of the Linux BSP. It is responsible for initializing some of the low level peripherals such as the integrated power supply and the DRAM controller as well as a few other initialization tasks. The default configuration of the bootlet code for the latest i.MX233 and i.MX28x release (SDK 10.05 and SDK 10.12 respectively) support a hardware configuration that has both a LiIon battery configuration (as shown in the reference schematics for these platforms as shown on freescale.com). For other configurations though such as a VDD5V connection only or a DCDC_BATT/Battery connection only, some additional changes are recommended.
記事全体を表示
This page describes how to determine the NAND timing parameters for use in the NAND driver. This is independent of any OS that may be used. Analyzing NAND Datasheets  We use a spreadsheet to capture and analyze NAND features. That spreadsheet is [attached to this wiki page|Adding support for a new NAND with i.MX28– Nand Analysis^nand_analysis_template.xls]. We analyze a NAND as described below. We must have the NAND datasheet to do the analysis. Copy the *analysis spreadsheet* to a new filename with the exact part number(s) of the NAND(s) being analyzed. Fill in sheet 1 ("Cover Page") of the analysis spreadsheet. Work on sheet 3 next: Fundamental Features. Other tables. If the NAND is one of a family listed together in a data sheet, then analyze the whole family with one spreadsheet. You can use the "Similar to" rows for the additional members of the family. Add more rows if needed. Most NANDs have an asyncrhronous interface, so there is not a simple clock frequency involved. Instead, there are various setup times, hold times, and output delays that imply limits on the I/O rate to/from the NAND. The spreadsheet compares the NAND's timing specifications to see if sums of the setup, hold, and output times are shorter than the minimim read-cycle or write-cycle times. The spreadsheet is specifically intended for use with the Nand controller in STMP378x/i.MX233/i.mx28 chips, so the spreadsheet performs the timing calculations with the goal of deriving the timing parameters *TSU*, *TDS*, and *TDH* for those CPUs. If the TDS and/or TDH quantities {color:#ff0000}turn red{color} after all the timings have been computed, then the computed TDS and/or TDH are too short for the specified cycle-time of the NAND. In that case:           You will have to increase one or both of them in the software. Write a note somewhere in the analysis spreadsheet about the values that you choose, but don't mess up the automatic computations. Record how the flash denotes factory-marked bad-blocks. (Some use the first page of a block, some use the last page,, etc.) Compare it to this [current superset of bad-block marking methods [http://wiki.freescale.net/display/PSGSW/Storage+Media%2C+Flash+Bad+Block+Marks] used to detect any flash factory bad block. Example Analysis Examples of NAND datasheets and analyses can be found on the [Hynix NAND Page | http://wiki.freescale.net/display/PSGSW/Hynix+NAND+Flash+Documents].
記事全体を表示