i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Platform: Demo images, i.MX8MPlus EVK   Some customer need test ffs gadget function on i.MX8MPlus EVK. Here is demo for ffs test, please connect EVK and Ubuntu PC before test.   Test script: #!/bin/sh # Setup the device (configfs) modprobe libcomposite mkdir -p config mount none config -t configfs cd config/usb_gadget/ mkdir g1 cd g1 echo 0x1fc9 >idVendor echo 0x0146 >idProduct mkdir strings/0x409 echo 12345 >strings/0x409/serialnumber echo "Signal 11" >strings/0x409/manufacturer echo "Test" >strings/0x409/product mkdir configs/c.1 mkdir configs/c.1/strings/0x409 echo "Config1" >configs/c.1/strings/0x409/configuration # Setup functionfs mkdir functions/ffs.usb0 ln -s functions/ffs.usb0 configs/c.1 cd ../../../ mkdir -p ffs mount usb0 ffs -t functionfs cd ffs ffs-test 64 & # from the Linux kernel, with mods! sleep 3 cd .. # Enable the USB device echo 38100000.usb > config/usb_gadget/g1/UDC   EVK log root@imx8mpevk:~# ./test2.sh [ 17.859597] file system registered ffs-test: dbg: ep0: writing descriptors (in v2 format) ffs-test: dbg: ep0: writing strings ffs-test: dbg: ep1: starting ffs-test: dbg: ep2: starting ffs-test: dbg: ep1: starts ffs-test: dbg: ep0: starts ffs-test: dbg: ep2: starts Event BIND Event ENABLE Ubuntu PC log: lzm@lzm-GL552VW:~$ lsusb -D /dev/bus/usb/001/008 Device: ID 1fc9:0146 NXP Semiconductors Test Device Descriptor: bLength 18 bDescriptorType 1 bcdUSB 2.10 bDeviceClass 0 bDeviceSubClass 0 bDeviceProtocol 0 bMaxPacketSize0 64 idVendor 0x1fc9 NXP Semiconductors idProduct 0x0146 bcdDevice 6.01 iManufacturer 1 Signal 11 iProduct 2 Test iSerial 3 12345 bNumConfigurations 1 Configuration Descriptor: bLength 9 bDescriptorType 2 wTotalLength 0x0020 bNumInterfaces 1 bConfigurationValue 1 iConfiguration 4 Config1 bmAttributes 0x80 (Bus Powered) MaxPower 2mA Interface Descriptor: bLength 9 bDescriptorType 4 bInterfaceNumber 0 bAlternateSetting 0 bNumEndpoints 2 bInterfaceClass 255 Vendor Specific Class bInterfaceSubClass 0 bInterfaceProtocol 0 iInterface 5 Source/Sink Endpoint Descriptor: bLength 7 bDescriptorType 5 bEndpointAddress 0x81 EP 1 IN bmAttributes 2 Transfer Type Bulk Synch Type None Usage Type Data wMaxPacketSize 0x0200 1x 512 bytes bInterval 0 Endpoint Descriptor: bLength 7 bDescriptorType 5 bEndpointAddress 0x01 EP 1 OUT bmAttributes 2 Transfer Type Bulk Synch Type None Usage Type Data wMaxPacketSize 0x0200 1x 512 bytes bInterval 1 Binary Object Store Descriptor: bLength 5 bDescriptorType 15 wTotalLength 0x0016 bNumDeviceCaps 2 USB 2.0 Extension Device Capability: bLength 7 bDescriptorType 16 bDevCapabilityType 2 bmAttributes 0x0000010e BESL Link Power Management (LPM) Supported BESL value 256 us SuperSpeed USB Device Capability: bLength 10 bDescriptorType 16 bDevCapabilityType 3 bmAttributes 0x00 wSpeedsSupported 0x000f Device can operate at Low Speed (1Mbps) Device can operate at Full Speed (12Mbps) Device can operate at High Speed (480Mbps) Device can operate at SuperSpeed (5Gbps) bFunctionalitySupport 1 Lowest fully-functional device speed is Full Speed (12Mbps) bU1DevExitLat 0 micro seconds bU2DevExitLat 0 micro seconds Device Status: 0x0001 Self Powered  
查看全文
Traditional non-matter devices cannot directly join the matter network. But Matter Bridge solves the problem. Matter bridge can join a Matter network as a Matter device and nonmatter devices need to be mapped to Matter network as a dynamic endpoint. In this way, other Matter devices can communicate with non-matter devices through dynamic endpoints. The Guide is a Matter Zigbee Bridge implement based on i.MX93 + K32W0.     Feature List • Matter over Ethernet • Matter over Wi-Fi • Register and Remove Zigbee Deivces • Connect Zigbee devices into Matter ecosystem seamlessly • Zigbee Devices o OnOff cluster o Temperature Sensor Cluster • Matter Actions o Start Zigbee Network o Zigbee Network Permit Join o Factory Reset • No limitation if migrating to other i.MX MPU like i.MX6ULL, i.MX8MP • OTBR and Zigbee bridge can be integrated into one single device
查看全文
Usually, device tree source files are not a signal pure dts file. It could include dtsi, dts or C code heads .h files. Need C compiler finish the pre-compile to a pure dts file first. It is integrated inside the like Linux build system(Makefile, etc.). This document shows the original way to compile device tree. This document will show compile device tree under windows.    
查看全文
test ov5640 with 480p, raw10 via ISP on imx8mp
查看全文
  Platform & BSP :i.MX8MPlus, L6.1.36   The attachments enable the i.MX8MPlus pci function in uboot. lspci in Linux root@imx8mpevk:~# lspci -nn 00:00.0 PCI bridge [0604]: Synopsys, Inc. DWC_usb3 / PCIe bridge [16c3:abcd] (rev 01) 01:00.0 Ethernet controller [0200]: Marvell Technology Group Ltd. Device [1b4b:2b42] (rev 11) pci test results in uboot:  u-boot=> pci BusDevFun VendorId DeviceId Device Class Sub-Class _____________________________________________________________ 00.00.00 0x16c3 0xabcd Bridge device 0x04 u-boot=> pci bar 00.00.00 ID Base Size Width Type ---------------------------------------------------------- 0 0x0000000018000000 0x0000000000100000 32 MEM u-boot=> pci regions 00 Buses 00-01 # Bus start Phys start Size Flags 0 0x0000000000000000 0x000000001ff80000 0x0000000000010000 io 1 0x0000000018000000 0x0000000018000000 0x0000000007f00000 mem 2 0x0000000040000000 0x0000000040000000 0x0000000016000000 mem sysmem 3 0x0000000058000000 0x0000000058000000 0x00000000a8000000 mem sysmem 4 0x0000000100000000 0x0000000100000000 0x00000000c0000000 mem sysmem u-boot=> pci header 00.00.00 vendor ID = 0x16c3 device ID = 0xabcd command register ID = 0x0007 status register = 0x0010 revision ID = 0x01 class code = 0x06 (Bridge device) sub class code = 0x04 programming interface = 0x00 cache line = 0x08 latency time = 0x00 header type = 0x01 BIST = 0x00 base address 0 = 0x18000000 base address 1 = 0x00000000 primary bus number = 0x00 secondary bus number = 0x01 subordinate bus number = 0x01 secondary latency timer = 0x00 IO base = 0x10 IO limit = 0x00 secondary status = 0x0000 memory base = 0x1820 memory limit = 0x1810 prefetch memory base = 0xfff0 prefetch memory limit = 0x0000 prefetch memory base upper = 0x00000000 prefetch memory limit upper = 0x00000000 IO base upper 16 bits = 0x0000 IO limit upper 16 bits = 0x0000 expansion ROM base address = 0x18100000 interrupt line = 0xff interrupt pin = 0x01 bridge control = 0x0000
查看全文
The configuration of DDR is very important. NXP provides a tool for configuring DDR for users of i.MX series products. Here are the details steps for it. Hope can do help for someone. 1\ The DDR part startup and initialization sequence of MX8MM:   The MX 8M series DDR tools include: DDR Register Programming Aid --->Configurate custom DDR initialization MSCALE DDR Tool(DDR Stress Test Tool) --->Test DDR initialization And DDR interface ---> Generate custom DDR initialization code for the u-boot SPL DDR RPA(RPA) is an Excel spreadsheet tool used to develop DDR initialization for specific DDR configurations (DDR device type, density, etc.) of users. RPA generates DDR initialization (in a separate Excel worksheet tab). Detailed explanations and introductions will be provided here. DDR stress testing tool is a software tool based Windows that initializes PHY and generates DDRC configuration Uboot source code to verify whether DDR initialization can be used for u-boot and OS startup. DDR stress testing script, this format is specifically used for DDR stress detection. First, copy the content from this worksheet tab, and then paste it into a text file, naming the document with the ". ds" file extension. Select this file when performing DDR stress testing. 2\i.MX8M series DDR tool work flow           Above is the DDR Tool flow for the i.MX8MM: DDR RPA Tool: Configure DDR parameters to generate DDR Stress Test script ". ds". DDR Sress Test Tool: Test DDR initialization and DDR interface, generate DDR initialization code for the u-boot SPL DDR driver. For the newest DDR RPA version as below:   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443 In the above link, you can download the corresponding DDR configuration tools for i.MX8MM using different DDRs.   3\How to use this script to configure DDR parameters (1)Obtain the required DRAM data sheet from the DRAM supplier firstly. The DDR parameter configuration content will be completed in the "Register Configuration" worksheet tab.   (2)"Register Configuration",Update the device information table to include DRAM information and system usage. DDR RPA tool:  Register Configuration---->Device Information table   It should be filled out based on the datasheet and relevant hardware circuit design of the selected DDR chip. Specific users can refer to the manual for selecting DDR chips and their own hardware design. Take the i.MX 8M Mini LPDDR4 EVK board as example, it selects the Micron MT53D512M32D2DS-053 WT:D, we can go the Micron website to download the DDR’s datasheet and we can see bellow:   Density per channel (Gb)= Device density (Per Channel Per CS)=8Gb Number of ROW Addresses=R[15:0]=16 Number of Channels=2 (2 Channels i.MX8MM DDR is 32bit) Number of COLUMN Addresses=C[9:0]=10 Total DRAM density(Gb) Automatic calculation:Density per channel (Gb) * Number of Channels * Number of Chip Selects used  =8Gb * 2 * 1=16Gb=2GB Bus Width=M32=32bit: i.MX8MM DDR support 32bit Cycle Freq (MHz)=1500MHZ: The DDR controller clock of the i.MX8MM is set to 1500MHZ. The information filled in is shown in the table below:   (3)Browse through various shaded cells in the spreadsheet to update using data from the DRAM table (pay special attention to the "Legend" table to determine the meaning of different shaded cells; in many cases, these cells may not need to be updated). On the parameter filling page, we can also see the following table, with different colors indicating the need to modify and maintain the original parameters and the affected parameter information. On the register configuration tab, basically only the orange part of the color represents the bit segments that usually need to be updated, and the rest do not need to be modified or configured.   (4)Go to the BoardDataBusConfig tab, fill in the i.MX8MM data bus mapping to the memory device correctly. DDR RPA tool: BoardDataBusConfig ---->Configurate data bus bit   Users should pay special attention to ensuring that this worksheet is configured correctly, otherwise the LPDDR4 system may not function properly. The memory controller of i.MX8MM allows for BYTE internal swapping. For layout convenience, BYTE internal swapping is usually performed, so the BoardDataBusConfig column needs to be configured according to the actual schematic design. We can see the tab in the BoardDataBusConfig, user fill the i.MX8MM data bit connection to associated LPDDR4, the filling in of data bits here should be consistent with the order of our hardware design wiring, which means that if there are swapped data bits, the corresponding relationship must be filled in. Take the LPDDR4 connection to the i.MX8MM as example, the highest 8 bits on the channel B of the LPDDR4   connect to the side of DRAM_DQ00~DRAM_DQ07 of CPU, and the lowest 8 bits on the channel B of the LPDDR4 DRAM_DQ08~DRAM_DQ15 of CPU side,the lowest 8 bits on the channel A of the LPDDR4 connect to the DRAM_DQ16~DRAM_DQ23 of CPU side,the highest 8 bits on the channel A of the LPDDR4 connect to the DRAM_DQ24~DRAM_DQ31 of the CPU side. The i.MX8MM memory controller allows for BYTE internal swapping. For layout convenience, BYTE internal swapping is usually performed, and this needs to be filled in according to the actual wiring in the data bus.       (5)Generate the “.ds” file DDR RPA tool: DDR stress test file ----> “.ds”   Copy the content of the DDR stress test file into a text file and name it a. ds file. For subsequent DDR stress testing purposes.   4\Do the DDR Stress test and Generate the DDR Code The following is the workflow of the DDR tool for the MX8MM series:   Preparation Board: i.MX 8M Mini LPDDR4 EVK Software download: mscale_ddr_tool_v3.31_setup.exe(Install it) PC:Window10 PC file .ds file Hardware requirements for the board: (Please note that these interfaces are necessary when using our stress testing tools) Serial download mode USB OTG port Debug UART port 4.1 Hardware connection   SW1101set 1010xxxxxx go to Serial Download mode, connect the USB-OTG and UART to PC, USB OTG is used for serial download of binary files: UART is used to communicate with users. Note: It is recommended to connect the USB OTG directly to the host PC, rather than through the USB Hub. When power on the board,we can see HID-compliant vendor-defined device and USB Input Device:   UART port are COM3 and COM4:   4.2 Open MSCALEDDR_Tool. exe in administrator mode for DDR parameter calibration and pressure testing:   Select serial port Select Search in Debug UART and you can read that the other two serial ports COM3 and COM4 have been tried. Click on the Connect button. It should be noted that we have two serial ports, one for the A core and the other for the M core. Here, COM4 must be selected to load the script normally. COM4 is used for the A core. Select Target Select the MX8M-mini,speed of CPU chosse1200MHZ, DDR LPDDR4 size 2GB. Select .ds file, Load DDR Script: Copy the generate mx8mm_micron_lpddr4_2gb_2d_1500m_200m_50m_32bit_1cs_RPAv22.ds to the path of the DDR TOOL, then press the Download button. After the download is successful, there will be a print message indicating the successful download and the startup information of the board. We can see the CPU parameters and DDR configuration.   Pres Calibration: This step mainly involves executing the DDR initialization and calibration process. If there is a failure, it is necessary to analyze the DDR problem based on the printed information. If there is no problem, the following interface will appear.   (5) If there are no problems after calibration, perform a pressure test. Only perform this operation when the calibration is passed. Run the test on all frequency set points. If the DDR pressure test passes, you can see that the test has passed successfully. If there is an error, you should search for the problem with the DDR based on the error message.   (6) Generate u-boot timing After the stress test is successfully completed, clicking the Gen Code button will generate a file lpddr4_timing. c, and then the lpddr4_timing. C file can be copied to the u boot directory.     5\ Modifying and configuring DDR frequencies that are not supported by default         The above test is for the frequency point 1500MHZ that is supported by default in our tool. RPA provides default DRAM PLL settings (DRAM frequency) based on the default settings supported in u-boot. If the customer is not using the default supported frequency, in addition to updating the new frequency in RPA, the new DRAM PLL settings should also be manually updated in the u boot SPL. (1) Firstly, in the RPA script, "Clock Cycle Freq (MHz)" is set to the frequency we need (2) Then search for 'memory set 0x30360054' in the RPA DDR stress test file worksheet tab, with a default setting of 1500MHZ.   We can see the DRAM PLL register and bit settings:   For special frequencies, we have a calculation formula here: DDR_freq = [(24MHz x pll_main_div)/(pll_pre_div x 2^pll_post_div)] x 2 1500 = [(24 x 250) / (8 x 2^1)] x 2 Bellow are some special examples of the required configurations for various frequencies:     Finishing configuration, create a. ds test DDR script in the RPA script to specify the frequency of this configuration. (3)After creating a DDR script for the DDR stress testing tool, run the calibration and perform the DDR pressure test. Generating the lpddr4_timing.c, modify the required DDR rate parameters Manually. (4)Modify the DRAM PLL,DRAM_freq = DRAM_PLL x 2 in SPL,u-boot SPL DDR driver can will not automatically change DRAM PLL based on generated code. Therefore, users will need to manually modify the dram_pll_init  for the required DDR PLL parameter.
查看全文
Note: This guide is specifically for use with Segger software. For steps to use with the MCUXpresso extension for VSCode please refer to How to Use Segger J-Link Plus with i.MX 8M Process... - NXP Community This guide aims to be a technical reference to start using the SEGGER J-Link Plus debug probe on the i.MX 8M Family processors. The board used for this guide specifically is the i.MX 8M Nano EVK, but it also applies to all processors of the i.MX 8M Family. Here we will describe the process using the following structure: Hardware requirements Software requirements How to find, build, and download the i.MX SDK Host setup Build an example application Target setup Run an example application Hardware requirements Evaluation Kit for the i.MX8M Nano Applications Processor (i.MX 8M Nano Evaluation Kit | NXP Semiconductors) Quick Start Guide for i.MX8M Nano (I.MX 8M Nano EVK Quick Start Guide (nxp.com)) J-Link Plus JTAG/SWD debug probe with USB interface (SEGGER J-Link PLUS) Features Download speed up to 1MB/s Unlimited breakpoints in flash memory Supports direct download into RAM and flash memory Supported NXP Devices Supported Devices - Search results "nxp" (segger.com) 9 Pin Cortex-M Adapter (9-Pin Cortex-M Adapter (segger.com)) Description Adapts from the 20-pin 0.1'' JTAG connector to a 9-pin 0.05'' Samtec FTSH connector as defined by Arm. Software requirements Windows 10 OS (host) J-Link Software and Documentation Pack for Windows (https://www.segger.com/products/debug-probes/j-link/models/j-link-plus/) i.MX 8M Nano SDK (Welcome | MCUXpresso SDK Builder (nxp.com)) MinGW CMake GNU ARM Embedded Toolchain Terminal Emulator for serial port connection (Tera Term, PuTTY, etc.)   How to find, build, and download the i.MX 8M Nano SDK Enter Welcome | MCUXpresso SDK Builder (nxp.com) Click on "Select Development Board"  Select EVK-MIMX8MN (MIMX8MN6xxxJZ) from Boards -> i.MX -> EVK-MIMX8MN Click on the Build MCUXpresso SDK button Click on Download SDK, you'll be redirected to the MCUXpresso SDK Dashboard Look for the i.MX 8M Nano SDK and click on Download SDK Click on Download SDK archive and documentation, accept the Software Terms and Conditions and the .zip file for the SDK will be downloaded.   Host Setup J-Link Software and Documentation Pack for Windows Download J-Link Software and Documentation Pack for Windows (https://www.segger.com/products/debug-probes/j-link/models/j-link-plus/) Execute .exe file downloaded and then click on "Next" Follow the installation wizard with default parameters and click on "Finish".   MinGW Download the MinGW installer from MinGW - Minimalist GNU for Windows - Browse /Installer at SourceForge.net. Follow the installer instructions leaving all options in their default values. Click on Continue when the installer finishes. A MinGW Installation Manager window will pop up, select mingw32-base and msys-base from basic setup. Click on the Installation menu and select Apply Changes. On the next window, click on Apply and wait for the package to finish downloading. Add the appropriate item to the Windows operating system path environment variable. It can be found under Control Panel->System and Security->System->Advanced System Settings in the Environment Variables... section. The path is: \bin. Assuming the default installation path, "C:\MinGW". If the path is not set correctly, the toolchain does not work. Note: If you have C:\MinGW\msys\x.x\bin in your PATH variable (as required by KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.   CMake Download CMake Windows x64 Installer from  Download CMake. Scroll down to find the latest release for the installer: Run the installer and follow the instructions. Make sure to check the Add CMake to system PATH for all users option during the installation process. Restart your PC to apply changes. GNU ARM Embedded Toolchain Download the GNU ARM Embedded Toolchain installer from Downloads | GNU Arm Embedded Toolchain Downloads – Arm Developer, scroll down to find the latest release for the installer: Follow the installer instructions and check the Add to PATH option at the end of the process. Add a new system environment variable named ARMGCC_DIR with the GNU ARM embedded Toolchain installation path as its value ARMGCC_DIR=ARMGCC_DIR=C:\Program Files (x86)\GNU Arm Embedded Toolchain\10 2021.10​   Build and example application Press the Windows Key and search for GCC Command Prompt and run it. Change the directory to the example application project directory (inside the armgcc folder), for example: C:\Users/<user>\Documents\8MNANO\boards\evkmimx8mn\demo_apps\hello_world\armgcc Type build_debug.bat on the command line or double click the build_debug.bat file (inside the armgcc folder of the application project) through Windows Explorer Wait for the building process to end and make sure no error messages are shown. Target Setup Connect the debug cable (USB-UART) to the board and the other end to your PC. Connect the power cable to the second USB-C port and to a wall socket. Don't turn on the board yet. Connect the JLink Plus to your PC with the USB cable. Connect the JLink Plus to the JTAG of the i.MX 8M Nano EVK board In this part we will need to identify pin number 1 from the 9 Pin Cortex-M adapter and from the i.MX 8M Nano EVK board. For the first one identify pin 7 identifiable by a "Non-connect pin". For the i.MX 8M Nano, you can identify easily with a number 1 in one corner of the connectors.    The whole setup should look similar to this: Run an example application Open a terminal application (TeraTerm, PuTTY, etc.) on your host PC and set it to the serial debug port with the lowest numbered port with the following settings: Speed: 115200 Data: 8-bit Parity: none Stop bits: 1 bit Flow Control: none Start SEGGER J-Link GDB Server. On section “Target Device” select MIMX8MN6_M7 and click “OK”. You will see the following window. Open a new instance of GCC Command Prompt. Change to the directory with the example previously compiled. Here is the path to folder that contains the files: <install_dir>/boards/<boad_name>/<example_type>/<application_name>/armgcc/debug​ Run the command: arm-none-eabi-gdb.exe <application_name>.elf.​ Example: At this point you are in the GDB Command Prompt, run the following commands: target remote localhost:2331 monitor reset monitor halt load monitor go The application will be now running and you can see the “hello world” on your terminal (PuTTY,Tera Term, etc.).  
查看全文
One of the most popular use cases for embedded systems are projects destinated to show information and interact with users. These views are called GUI or Graphic User Interface which are designed to be intuitive, attractive, consistent, and clear. There are many tools that we can use to achieve great GUIs, mostly implemented for platforms such as Web, Android, and iOS. Here, we will need to introduce the concept of framework, basically, it is a set of tools and rules that provides a minimal structure to start with your development. Frameworks usually comes with configuration files, code snippets, files and folders organization helping us to save time and effort. Also, it is important to review the concept of SDK or Software Development Kit which is a set of tools that allows to build software for specific platforms. Usually supplies debugging tools, documentation, libraries, API’s, emulators, and sample code. Flutter is an open-source UI software development kit by Google that help us to create applications with great GUIs on different platforms from a single codebase. Depends on the reference, you can find Flutter defined as a framework or SDK and both are correct, however, an SDK could be a best definition thanks to Flutter supplies a wide and complete package to create an application in which framework is also included. This article is aimed at those that are in a prototyping stage looking for a different tool to develop projects. Also, this article pretends to be a theoretical introduction explaining the most important concepts. However, is a good practice to learn more about reviewing the official documentation from Flutter. (Flutter documentation | Flutter) Here is the structure used throughout this article: What is Flutter? Flutter details Platforms Programming language Official documentation Flutter for embedded systems What is Flutter? Flutter was officially released by Google in December 2018 with a main aim, to give developers a tool to create applications natively compiled for mobile (Android, iOS), web and desktop (Windows, Linux) from a single codebase. It means that as a developer, Flutter will create a structure with minimal code, configuration files, build files for each operating system, manifests, etc. in which we will add our custom code and finally build this code for our preferred OS. For example, we can create an application to review fruit and vegetable information and compile for Android and iOS with the same code. A basic Flutter development process based on my experience looks like the following diagram: Flutter has the following key features: Cross-platform development. Flutter allows the developer to create applications for different platforms using a single codebase. It means that you will not need to recreate the application for each platform you want to support.   Hot-reload. This feature allows the developer to see changes in real time without restarting the whole application, this results in time savings for your project.   High Performance Flutter apps achieve high performance due to the app code is compiled to native ARM code. With this tool no interpreters are involved.   UI Widgets Flutter supplies a set of widgets (UI components such as boxes, inputs text, buttons, etc.) predefined by UI systems guidelines Material on Android and Cupertino for iOS. Source: Material 3 Design Kit | Figma Community Source: Design - Apple Developer   Great community support. This feature could be subjective but, it is useful when we are developing our project find solutions to known issues or report new ones. Because of Flutter is an open source and is widely implemented in the industry this tool owns a big community, with events, forums, and documentation. Flutter Details Supported Platforms With Flutter you can create applications for: Android iOS Linux Debian Linux Ubuntu macOS web Chrome, Firefox, Safari, Edge Windows Supported deployment platforms | Flutter Programming Language Flutter use Dart, a programming language is an open-source language supported by Google optimized to use on the creation of user interfaces. Dart key features: Statically typed. This feature helps catching errors making the code robust ensuring that the variable’s value always match with the declared variable’s type. Null safety. All variables on Dart are non-nullable which means that every variable must have a non-null value avoiding errors at execution time. This feature also, make the code robust and secure. Async/Await. Dart is client-optimized which means that this language was specially created to ensure the best performance as a client application. Async/Await is a feature part of this optimization making easier to manage network requests and other asynchronous operations. Object oriented. Dart is an object-oriented language with classes and mixin. This is especially useful to use on Flutter with the usage of widgets. Compiler support of Just-In-Time (JIT) and Ahead-of-Time (AOT) JIT provides the support that enables the Hot Reload Flutter feature that I mentioned before. It is a complex mechanism, but Dart “detects” changes in your code and execute only these changes avoiding recompiling all the code. AOT compiler produces efficient ARM code improving start up time and performance. Official documentation Flutter has a rich community and documentation that goes from UI guidelines to an Architectural Overview. You can find the official documentation at the following links: Flutter Official Documentation: Flutter documentation | Flutter Flutter Community: Community (flutter.dev) Dart Official Documentation: Dart documentation | Dart Flutter for embedded systems So far, we know all the excellent features and platforms that Flutter can support. But, what about the embedded systems? On the official documentation we can find that Flutter may be used for embedded systems but in fact there is no an official supported platform. This SDK has been supported by their community, specially there is one repository on GitHub supported by Sony that provides documentation and Yocto recipes to support Flutter on embedded Linux. To understand the reason to differentiate between Flutter for Linux Desktop with official support and to create a specific Flutter support for embedded Linux is important to describe the basics of Flutter architecture. Based on the Flutter documentation the system is designed using layers that can be illustrated as follows:   Source: Flutter architectural overview | Flutter We can see as a top level “Framework” which is a high-level layer that includes widgets, tools and libraries that are in contact with developers. Below “Framework,” the layer “Engine” is responsible of drawing the widgets specified in the previous layer and provides the connection between high-level and low-level code. This layer is mostly written in C++ for this reason Flutter can achieve high performance running applications. Specifically for graphics rendering Flutter implements Impeller for iOS and Skia for the rest of platforms. The bottom layer is “Embedder” which is specific for each target and operating system this layer allows Flutter application to run as a native app providing the access to interact with different services managed by the operating systems such as input, rendering surfaces and accessibility. This layer for Linux Desktop uses GTK/GDK and X11 as backend that is highly dependent of unnecessary libraries and expensive for embedded systems which have constrained resources for computation and memory. The work around founded by Sony’s Flutter for Embedded Linux repository is to change this backend using a widely implemented backend for embedded systems Wayland. The following image illustrates the difference between Flutter for Linux Desktop and Flutter for Embedded Linux.   Source: What's the difference between Linux desktop and Embedded Linux · sony/flutter-embedded-linux Wiki · GitHub   Source: What's the difference between Linux desktop and Embedded Linux · sony/flutter-embedded-linux Wiki · GitHub Here is the link to the mentioned repository: GitHub - sony/flutter-elinux: Flutter tools for embedded Linux (eLinux) Finally, I would like to encourage you to read the official Flutter documentation and consider this tool as a great option compared to widely used tools on embedded devices such as Qt or Chromium. Also, please have a look to a great article written by Payam Zahedi delving into the implementation of Flutter for Embedded Linux measuring performance and giving conclusions about the usage of Flutter in embedded systems. (Flutter on Embedded Devices. Learn how to run Flutter on embedded… | by Payam Zahedi | Snapp Embedded | Medium).    
查看全文
On behalf of Gopise Yuan. This is an update for the DRM framebuffer capture tool I used to share with the team. Some enhancement added. Might be useful for debugging some display related issues.   Some special notes: Behavior of DRM subsystem is different between L4.x and L5.x. For L4.x, you can capture the RGB buffer without any problem. But, there’s no API for YUV (multi-plane) buffer. To capture YUV, need to apply “kernel_0001-drm-Add-getfb2-ioctl_L4.14.98.patch”. For L5.x, mapping/capturing the internal buffer is not allowed by default due to security reason. A simple change in “0001-drm-enable-mapping-of-internal-object-for-debugging_L5.x.patch” can disable this guard. Capture raw data only. RGB and YUV (packed/planar, 420/422) supported. Support de-tile on “Amphion tile” (VPU, NV12 only) and “Super tile” (Vivante GPU). Please use “-t” to enable this. Other tile might not be supported. This is a static linked binary. You can run it on any ARM64 based Linux/Android system in theory (prerequisites in item #1). If you need source code, come to me.   To get more details on how to use it, use “-?” option: DRM screen capture DRM based screen capture program Usage:     ./drmfbcap [OP] [ARG] [OP] OPeration (optional):     -v Show version.     -? Show help information.     -i Show information about target DRM device only (no capture).     -t Perform de-tile for tile format.     -d DRM device to open. [ARG] should contain the path to the device node. Default: '/dev/dri/card0'     -o Output folder. [ARG] should contain the path to the output folder. Default: '.'     -p Specific plane # to capture. [ARG] should contain the plane number. If no '-p' specified, capture all planes   Example:     ./drmfbcap   Capture all planes on default DRM device.     ./drmfbcap -d /dev/dri/controlD64   Capture all planes on '/dev/dri/controlD64' device.     ./drmfbcap -p 44 -t -o /sdcard   Capture plane 44, do de-tile after capture and then output to /sdcard/.   Raw buffer capture will be done for each enabled/target plane and one file for each. Captured file will be saved to './' if not specified. --- By Gopise, 2022/08   Updated_2023_10_16: continuous capture (repeat mode) support with this link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/DRM-screen-capture-tool/ta-p/1725363
查看全文
this article write down the steps when help customer bring dual camera under single mipi csi with NXP switch NX3DV642, just for a reference, connect OV5640 + os08a20 with mipi csi0 via ISP, as default, mipi csi0 just has one port with one camera, this document improve how to enable os08a20 with second port under mipi csi0, refer to the document and patch as attachment, for how to enable ov5640 with ISP, pls refer to my another document
查看全文
What is a device tree? The device tree is a data structure that is passed to the Linux kernel to describe the physical devices in a system. Before device trees came into use, the bootloader (for example, U-Boot) had to tell the kernel what machine type it was booting. Moreover, it had to pass other information such as memory size and location, kernel command line, etc. Sometimes, the device tree is confused with the Linux Kernel configuration, but the device tree specifies what devices are available and how they are accessed, not whether the hardware is used. The device tree is a structure composed of nodes and properties: Nodes: The node name is a label used to identify the node. Properties: A node may contain multiple properties arranged with a name and a value. Phandle: Property in one node that contains a pointer to another node. Aliases: The aliases node is an index of other nodes. A device tree is defined in a human-readable device tree syntax text file such as .dts or .dtsi. The machine has one or several .dts files that correspond to different hardware configurations. With these .dts files we can compile them into a device tree binary (.dtb) blobs that can either be attached to the kernel binary (for legacy compatibility) or, as is more commonly done, passed to the kernel by a bootloader like U-Boot. What is Devshell? The Devshell is a terminal shell that runs in the same context as the BitBake task engine. It is possible to run Devshell directly or it may spawn automatically. The advantage of this tool is that is automatically included when you configure and build a platform project so, you can start using it by installing the packages and following the setup of i.MX Yocto Project User's Guide on section 3 “Host Setup”. Steps: Now, let’s see how to compile your device tree files of i.MX devices using Devshell. On host machine. Modify or make your device tree on the next path: - 64 bits. ~/imx-yocto-bsp/<build directory>/tmp/work-shared/<machine>/kernel-source/arch/arm64/boot/dts/freescale - 32 bits. ~/imx-yocto-bsp/<build directory>/tmp/work-shared/<machine>/kernel-source/arch/arm/boot/dts To compile, it is needed to prepare the environment as is mentioned on i.MX Yocto Project User's Guide on section 5.1 “Build Configurations”. $ cd ~/imx-yocto-bsp $ DISTRO=fsl-imx-xwayland MACHINE=<machine> source imx-setup-release.sh -b <build directory> $ bitbake -c devshell virtual/kernel (it will open a new window) On Devshell window. $ make dtbs (after finished, close the Devshell window) On host machine. $ bitbake -c compile -f virtual/kernel $ bitbake -c deploy -f virtual/kernel This process will compile all the device tree files linked to the machine declared on setup environment and your device tree files will be deployed on the next path: ~/imx-yocto-bsp/<build directory>/tmp/deploy/images/<machine> I hope this article will be helpful. Best regards. Jorge.
查看全文
SoC: i.MX8MP LDP: Ubuntu22.04 and Ubuntu 20.04 Yocto: 6.1.22 mickledore   This doc includes two parts: 1)How to enable qt5 in LDP 2)How to enable qt5 in Yocto Linux 6.1.22     How to use qt5 in LDP(Linux Distribution Poc): The gcc and glibc is diffrent from Yocto Linux and Linux Distribution Poc. To cross compile the file between Linux and Ubuntu, we need to care about that.   To full enable the GPU usage of QT lib, please use "-gles" libs by apt-get command. Qt source code is not suggested, for it has not been tested. Building Qt5, for example: sudo apt-get update sudo apt-get -y install libqt5gui5-gles sudo apt-get -y install libqt5quick5-gles sudo apt-get -y install qtbase5-gles-dev   opengles test case glmark: sudo apt-get -y install glmark2-es2-wayland How to find the missing lib for apt-get: sudo apt-get install apt-file apt-file search xx   open wifi if needed NXP internal internet has limitation: sudo modprobe moal mod_para=nxp/wifi_mod_para.conf   and add "nameserver 8.8.8.8" in vi /etc/resolv.conf. You can also try:  echo "nameserver 8.8.8.8" | sudo tee /etc/resolv.conf > /dev/null   some times system time is not automatically update, and that cause apt-get update fail User and choose manually configure it by: sudo date -s "2023-08-31 14:00:00"   For Chinese support for ubuntu, please use: sudo apt-get install ttf-wqy-microhei ttf-wqy-zenhei xfonts-wqy   possible env path you need to export: XDG_RUNTIME_DIR="/run/user/1000" export QT_QPA_PLATFORM=wayland   User can choose root login by command like: user@imx8mpevk:~$ sudo passwd New password: Retype new password:   please use qmake to build qt project: 1)qmake -o Makefile HelloWorld.pro 2)make   some other qt libs: sudo apt-get install -y qtwayland5 sudo apt-get install -y qml-module-qtquick-controls sudo apt-get install -y qml-module-qtquick-controls2 sudo apt-get install -y qml-module-qtcharts sudo apt-get install -y libqt5multimedia5 sudo apt-get install -y libqt5serialport5 sudo apt-get install -y libqt5script5 sudo apt-get install -y qml-module-qt-labs-settings sudo apt-get install -y qml-module-qt-labs-platform sudo apt-get install -y qml-module-qtmultimedia sudo apt-get install -y libqt5webengine5 sudo apt-get install -y qml-module-qtwebengine sudo apt-get install -y qml-module-qtquick-dialogs     How to enable qt5 in Yocto 6.1.22: 1.download meta-qt5 git clone https://github.com/meta-qt5/meta-qt5.git git checkout origin/mickledore   copy Yocto version 5.10.72_2.2.0 sources\meta-imx\meta-sdk\dynamic-layers\qt5-layer to the same path of Yocto 6.1.22   2.apply two patches qt5-1.patch: modify the path from qt6 to qt5 qt5-2.patch: modify the qt5 related in meta-imx, including: 1)Yocto grammer update,from "_" to ":";  2)NXP grammer,from mx8 to mx8-nxp-sdk;  3)remove gstreamer1.0-plugins-good-qt, for qt5 has been natively added into gst-plugin-good-1.22(which is not in 1.18)   3.after input command like "DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build-xwayland", comment the "meta-nxp-demo-experience"   # i.MX Yocto Project Release layers BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-bsp" BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-sdk" BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-ml" BBLAYERS += "${BSPDIR}/sources/meta-imx/meta-v2x" #BBLAYERS += "${BSPDIR}/sources/meta-nxp-demo-experience"      
查看全文
Customer is asking high-capacity external storage(for example >64GB) support on i.MX BSP, ext4 is ok for HC storage, but it can’t be supported by Windows. Pls find NFTS and exFAT support status on Linux BSP below: Updated test result on L5.4.70.2.3.0 and L6.1.22: L5.4.70.2.3.0 1.You can enable ntfs support in kernel config as below,  ntfs can be mounted normally, but you can only modify existing file content in disk, you can’t create/delete/rename file on disk. > File systems > DOS/FAT/NT Filesystems   Log: root@imx8mpevk:~# mount -t ntfs /dev/sda1 /mnt/fat/ [  662.732869] ntfs: volume version 3.1. root@imx8mpevk:~# cp ntfs-3g /mnt/fat/ cp: cannot create regular file '/mnt/fat/ntfs-3g': Permission denied root@imx8mpevk:~# ls /mnt/fat/ 111.png  Image_org  System Volume Information  gpuinfo.sh root@imx8mpevk:~# vi /mnt/fat/gpuinfo.sh root@imx8mpevk:~# umount /mnt/fat/ root@imx8mpevk:~# ntfs file system can be accessed via ntfs-3g in user space as below //build: wget https://tuxera.com/opensource/ntfs-3g_ntfsprogs-2017.3.23.tgz tar zxvf ntfs-3g_ntfsprogs-2017.3.23.tgz cd ntfs-3g_ntfsprogs-2017.3.23/ source ../../sdk/environment-setup-aarch64-poky-linux   ./configure --host=aarch64-linux --build=aarch64-poky-linux --disable-shared --enable-static   make   ls /src/ntfs-3g   //put it into rootfs cp ntfs-3g /bin   //test log: root@imx8mpevk:/# [ 1058.724471] usb 1-1: USB disconnect, device number 4 [ 1062.058613] usb 1-1: new high-speed USB device number 5 using xhci-hcd [ 1062.214029] usb-storage 1-1:1.0: USB Mass Storage device detected [ 1062.220986] scsi host0: usb-storage 1-1:1.0 [ 1063.235871] scsi 0:0:0:0: Direct-Access     VendorCo ProductCode      2.00 PQ: 0 ANSI: 4 [ 1063.246185] sd 0:0:0:0: [sda] 15728640 512-byte logical blocks: (8.05 GB/7.50 GiB) [ 1063.254023] sd 0:0:0:0: [sda] Write Protect is off [ 1063.259164] sd 0:0:0:0: [sda] No Caching mode page found [ 1063.264540] sd 0:0:0:0: [sda] Assuming drive cache: write through [ 1063.296946]  sda: sda1 [ 1063.300860] sd 0:0:0:0: [sda] Attached SCSI removable disk   root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh root@imx8mpevk:/# cp /unit_tests/memtool /mnt/fat/ root@imx8mpevk:/# umount /mnt/fat/ root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh  memtool root@imx8mpevk:/#   3.exFAT is not supported on this BSP..   L6.1.22(you can check it on L5.15 and above, should be the same) You can enable ntfs support in kernel config as below, full features can be supported. > File systems > DOS/FAT/EXFAT/NT Filesystems   Pls use ‘-t ntfs3’ during mounting, otherwise it will be mounted as ‘read-only’ Log: root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information' root@imx8ulpevk:~# root@imx8ulpevk:~# cp gpuinfo.sh /mnt/fat/ root@imx8ulpevk:~# umount /mnt/fat/ root@imx8ulpevk:~# root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information'   gpuinfo.sh root@imx8ulpevk:~#   exFAT has been supported in L6.1.22. > File systems > DOS/FAT/EXFAT/NT Filesystems   /dev/sda1 on /run/media/sda1 type exfat (rw,relatime,fmask=0022,dmask=0022,iocharset=utf8,errors=remount-ro) root@imx8ulpevk:~# ls /run/media/sda1 'Certificate of Completion.pdf'             carlife.MP4 Image_org                                  example.tflite L5.4.70_2.3.0                              mx8mp_vpu.txt NXP-5G.mp4                                 sd.mp4 'System Volume Information'                 vela.ini android_p9.0.0_2.1.0-auto-ga_image_8qmek root@imx8ulpevk:~# ls Image_org  gpuinfo.sh root@imx8ulpevk:~# cp gpuinfo.sh /run/media/sda1/ root@imx8ulpevk:~# umount /run/media/sda1 root@imx8ulpevk:~#
查看全文
Platform i.MX8MPlus EVK, Android 13 Background Customer find we have enabled all configs about pstore and ramoops, but they can't get ramoops log in /sys/fs/pstore node on Android 13. Solution The default reboot will reset all hardware including the DDR control, so this will result in the loss of the log stored in RAM. We have include such codes in ATF, the default code will use imx_wdog_restart(true) to reset all hardware. void __dead2 imx_system_reset(void) { #ifdef IMX_WDOG_B_RESET imx_wdog_restart(true); #else imx_wdog_restart(false); #endif }   To avoid DDR reset, we should comment  IMX_WDOG_B_RESET in vendor/nxp-opensource/arm-trusted-firmware/plat/imx/imx8m/imx8mp/include/platform_def.h   Result evk_8mp:/sys/fs/pstore # ls console-ramoops-0 dmesg-ramoops-0 pmsg-ramoops-0  
查看全文
In the i.MX 8M Plus LPDDR4 EVK board there are two Type-C port design. For the port0 is used to power supply no usb function, for the port1 used for USB function but without PD function. But in customer’s design, customer only use one USB design on their board, how to make the one USB work with the PD and USB function, we need to make the hardware design and software modify. This article only give method to realized it and have tested and realized the port1 PD function. 1 Introduction of the USB interface on i.MX8MP         There are two USB 3.0 TypeC controllers with integrated PHY interface on the i.MX8MP: Backward compatibility with USB 2.0 Spread spectrum clock support   The USB on the i.MX8MP supports USB3.0 and is compatible with USB2.0 downward. We can see that the upper layer is the universal layer for USB 2.0 and USB 3.0 operations. This is a common interface, buffer management block, list processor, used to schedule and control the status register (CSR) function: USB 2.0 physical layer and MAC layer USB 3.0 physical layer, link layer and MAC layer   Features of USB 3.0: USB compliant version 3.0 (xHCI compatible) Supports operation as a stand-alone USB host controller USB dual role operation, configurable as host or device Ultra high speed (5Gbit/s), high speed (480Mbit/s), full speed (12Mbit/s) and low speed (1.5Mbit/s) operation. Support independent single port USB operation Support for four programmable bidirectional USB endpoints Support system memory interface with 40 bit addressing capability   2 Design of USB on Development Board         The i.MX 8M Plus processor includes two USB 2.0/3.0 controllers and two integrated USB PHYs. USB supports both running as an independent USB host controller and dual role USB operation, and can be configured as a host or device. Therefore, the design of these two functions is implemented on the development board of i.MX8MP.   We can see that on the development board, one USB1 is used for the USB Type-C port and the other USB2 is used for the USB 3.0 host port. USB Type-C port 0 (J5) is only used for power supply. It does not support USB data transfer. It is the only power port, so the system must always be powered.   On the CPU side of the schematic diagram, we can also see that USB1 is the port for USB Type-C, and USB2 is the host for USB3.0.    USB1 is designed as USB Type-C:   USB2 USB3.0 Host design:   Power design of the USB Type-C port:   3 Only one USB interface is used in the design (compatible with both USB PD function and USB dual roles function)         Two USB Type-C ports are used on our development board. One is used to power the board separately, and the other is used as the function of USB Type-C. However, due to the limited design cost and chip layout and space on the board, some customers will use a USB interface to realize the dual role function of power supply and USB. How to achieve this? USB Device(Download mode):     USB Host mode(power+device Need the hub support PD function):     The specific implementation and design are as follows: 3.1 Hardware realize PTN5110 To realize the USB Type-C support power supply function, PTN5110 (USB PD TCPC PHY IC) chip is required to realize Type-C data logic and power control and management. The selection of PTN5110 is critical and important.   PTN5110 is a single port USB PD (power supply) PHY IC that conforms to TCPC. It integrates Type-C configuration channel (CC) interface and USB PD physical layer functions into Type-C port manager (TCPM) that handles PD policy management. It complies with USB PD, Type-C and TCPC specifications.   The IC is mainly aimed at applications in system platforms (such as laptops, desktops, Chromebooks, tablets, flip notebooks, etc.). Other application cases may be feasible, depending on the application architecture, such as docking stations, displays, accessories, cable adapters, smartphones, etc.   It can support various Type-C applications: Sink, Source, Sink with accessory support or DRP. It executes Type-C CC simulation part (i.e. Rd/Rp/Ra detection, Rd/Rp indication) and PD Tx/Rx PHY and protocol state machine. PTN5110 supports TCPM in the system implementation of the following PD roles.   PTN5110 integrates VCONN load switch, programmable current limit, reverse leakage current blocking and over temperature protection (OTP). It is equipped with two enable control outputs to control the load switch/FET in the VBUS pull and/or sink path. It can also perform VBUS voltage monitoring/measurement, VBUS forced discharge and discharge discharge.   PTN5110 provides the main IO related functions for the main processor/TCPM, so that Type-C/PD interfaces can be easily controlled and managed through the TCPC interface.   PTN5110 supports a wide range of power input voltages, providing platform integrators with great flexibility. PTN5110 can run on VBUS to support specific system use cases that require no power operation.https://www.nxp.com/products/interfaces/usb-interfaces/usb-type-c/usb-pd-phy-and-cc-logic/usb-pd-tcpc-phy-ic:PTN5110   The design only use the USB1:   Here, it is required to weld R53 or R54. You can refer to this design completely. 2 Software modify Modify the BPS of the software: Take the newest released Linux 5.15.32_2.0.0​ as example: In the u-boot /board/freescale/imx8mp_evk/imx8mp_evk.c     It can be seen that the PD function of the port is turned off, so if you want to use USB1 for power supply, remove the following commands and turn on the PD function of USB1. “-   .disable_pd = true,” Use the above action to enable Port1 PD function. Kernel section modify: Kernel section modify towards to PTN5110. Type-C Configure channel (CC) interface: root/drivers/usb/typec/tcpm/tcpci.c @@ -524,6 +524,7 @@ static int tcpci_vbus_force_discharge(struct tcpc_dev *tcpc, bool enable)  static int tcpci_set_vbus(struct tcpc_dev *tcpc, bool source, bool sink)  {        struct tcpci *tcpci = tcpc_to_tcpci(tcpc); +      unsigned int reg;        int ret;          if (tcpci->data->set_vbus) { @@ -533,16 +534,20 @@ static int tcpci_set_vbus(struct tcpc_dev *tcpc, bool source, bool sink)                         return ret < 0 ? ret : 0;        }   +      ret = regmap_read(tcpci->regmap, TCPC_POWER_STATUS, &reg); +      if (ret < 0) +              return ret; +        /* Disable both source and sink first before enabling anything */   -       if (!source) { +      if (!source && (reg & TCPC_POWER_STATUS_SOURCING_VBUS)) {                 ret = regmap_write(tcpci->regmap, TCPC_COMMAND,                                     TCPC_CMD_DISABLE_SRC_VBUS);                 if (ret < 0)                         return ret;        }   -       if (!sink) { +      if (!sink && (reg & TCPC_POWER_STATUS_SINKING_VBUS)) {                 ret = regmap_write(tcpci->regmap, TCPC_COMMAND,                                     TCPC_CMD_DISABLE_SINK_VBUS);                 if (ret < 0)   Type-C port manager managed by PD (TCPM): root/drivers/usb/typec/tcpm /tcpm.c @@ -340,6 +340,7 @@ struct tcpm_port {         */        bool vbus_vsafe0v;   +      bool vbus_keep;        bool vbus_never_low;        bool vbus_source;        bool vbus_charge; @@ -3662,7 +3663,8 @@ static void tcpm_reset_port(struct tcpm_port *port)        port->rx_msgid = -1;          port->tcpc->set_pd_rx(port->tcpc, false); -       tcpm_init_vbus(port);     /* also disables charging */ +      if (!port->vbus_keep) +              tcpm_init_vbus(port);  /* also disables charging */        tcpm_init_vconn(port);        tcpm_set_current_limit(port, 0, 0);        tcpm_set_polarity(port, TYPEC_POLARITY_CC1); @@ -5834,6 +5836,9 @@ static void tcpm_init(struct tcpm_port *port)          port->tcpc->init(port->tcpc);   +      port->vbus_present = port->tcpc->get_vbus(port->tcpc); +      if (port->vbus_present) +              port->vbus_keep = true;        tcpm_reset_port(port);          /* @@ -5872,7 +5877,10 @@ static void tcpm_init(struct tcpm_port *port)         * Some adapters need a clean slate at startup, and won't recover         * otherwise. So do not try to be fancy and force a clean disconnect.         */ -       tcpm_set_state(port, PORT_RESET, 0); +      if (!port->vbus_keep) +              tcpm_set_state(port, PORT_RESET, 0); + +      port->vbus_keep = false;  }    static int tcpm_port_type_set(struct typec_port *p, enum typec_port_type type) Note: The software just needs to modify these two parts. You also need to mention to the proper the I2C port use, if not proper the driver of the PTN5110 can not driver. 4 Test         In our i. MX8MP EVK development board show that R53 and R54 in the USB1 part of our development board are in DNP status, so VBUS_ IN is disconnected and no power comes in. Here, connect R53 or R54 with solder, so that VBUS_ IN, the power comes in again. After the power is connected. The board can be powered through USB1. 4.1 Download images to the emmc on the Board: Power from the USB1, set the boot mode to serial download mode, then go to download images finished. 4.2 Boot up the board from the EMMC Change the boot mode to boot up from EMMC,the board boot up, the log file is as following show:   It will stop at the TCPC for the section of PTN5110 driver. By default, the PD function of port1 in the u-boot is turned off, so if you want to use USB1 for power supply, remove the following commands and turn on the PD function of USB1. “-   .disable_pd = true,” After the PD function is turned on, the board can be started normally, but the whole part running to the kernel will be powered down, so the kernel part of PTN5110 still needs to be modified. After the patch modification of the above kernel part, the board can run normally.         I also did the same experiment on the i.MX8MM EVK development board. The same phenomenon occurs when the kernel starts. Therefore, similar modifications to the above i. MX8MP can work normally. Summary: In one word i.MX8MP and i.MX8M series can realize the role of using a USB for power supply and USB Dual. The hardware design refers to our development board, and we must use the logic chip PTN5110. For software, refer to the above code modification.  
查看全文
Hello everyone! In this quick example its focused on how to customize uboot code to generate an uboot image with a silent console so its speed up the flash and boot time, this may provide helpful for customers who have a bigger images or just want to have a silent console. Note: this should not be enabled if the image is still being under test, since this will disable all communication with the debug terminal and there won't be boot messages. Requirements: I.MX 8M Nano DDR4 EVK i.MX 8M Nano EVK Prebuilt image (6.1.1-1.0.0) UUU tool First clone the code from the uboot repository: $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.1.1-1.0.0 $ cd uboot-imx After we get the code, then proceed to enable the silent console in the uboot defconfig: $ nano configs/imx8mn_ddr4_evk_defconfig CONFIG_SILENT_CONSOLE=y CONFIG_SILENT_U_BOOT_ONLY=y For this to actually work we need to create the silent environmental variable and give it a value different from "0": $ nano include/configs/imx8mn_evk.h "silent=1\0"      \ As specified in our Linux porting guide: Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set Target-Machine to the machine you are building for. See Section "Build configurations" in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG) Set up the host terminal window toolchain environment: $ source/opt/fsl-imx-xwayland/6.1.1/environment-setup-aarch64-poky-linux $ export ARCH=arm64 Build uboot binary: $ make distclean $ make imx8mn_ddr4_evk_defconfig $ make Build ARM Trusted Firmware (ATF) $ cd .. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.1.1-1.0.0 $ cd imx-atf/ $ make PLAT=imx8mn bl31 In case you get the error aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' $ unset LDFLAGS Download the DDR training & HDMI binaries $ cd .. $ mkdir firmware-imx $ cd firmware-imx $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.19.bin $ chmod a+x firmware-imx-8.19.bin $ ./firmware-imx-8.19.bin Accept EULA and the firmware will be deployed. Download imx-mkimage and build the boot image $ cd .. $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.1.1-1.0.0 $ cd imx-mkimage $ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ $ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ $ cp ../uboot-imx/arch/arm/dts/imx8mn-ddr4-evk.dtb iMX8M/ $ cp ../imx-atf/build/imx8mn/release/bl31.bin iMX8M/ $ cp ../firmware-imx/firmware-imx-8.19/firmware/ddr/synopsys/ddr4_* iMX8M/ $ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot $ make SOC=iMX8MN flash_ddr4_evk After this we can download our uboot image to our board, we can either use the uboot image for boot or for flashing purpose only. We can compare the time it takes using UUU with a standard pre-built image uuu -V -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-full-imx8mnevk.wic It takes 485.5 seconds using normal uboot with debug console enabled. uuu -V -b emmc_all flash.bin imx-image-full-imx8mnevk.wic It takes 477.5 seconds using silent uboot console. Even if the speed is not greatly improved (~8 seconds), in larger files it could help to speed up flashing, even if wants to have the console silent is a good option. Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
查看全文
1.Test environment Board: i.MX8MPlus, RM67199 BSP: uboot 2022.04, linux-6.1.1-1.0.1 2.Modification of uboot  In uboot, you need comment the video_link_shut_down and dm_remove_devices_flags in announce_and_cleanup function. #if defined(CONFIG_VIDEO_LINK) //video_link_shut_down(); #endif board_quiesce_devices(); printf("\nStarting kernel ...%s\n\n", fake ? "(fake run for tracing)" : ""); /* * Call remove function of all devices with a removal flag set. * This may be useful for last-stage operations, like cancelling * of DMA operation or releasing device internal buffers. */ // #ifndef CONFIG_POWER_DOMAIN // dm_remove_devices_flags(DM_REMOVE_ACTIVE_ALL | DM_REMOVE_NON_VITAL); // /* Remove all active vital devices next */ // dm_remove_devices_flags(DM_REMOVE_ACTIVE_ALL); // #endif cleanup_before_linux(); }  After doing this, the uboot logo will not be cleaned before Linux PM framework. 3.Modification of Linux You need add  CONFIG_LOGO=n into defconfig file to disable kernel logo.  3.1 Disable the power down of mediamix and mipi-dphy in gpcv2.c Please add below code into the beginning of  imx_pgc_power_down function if ((strcmp(genpd->name, "mipi-phy1") == 0) || (strcmp(genpd->name, "mediamix") == 0)) { return 0; }  3.2 Only reset lcdif in the last call of drm framework Please modify imx_lcdifv3_runtime_resume function like this. The imx_lcdifv3_runtime_resume function will be called two times, thus the lcdif will be reset two times.We can let it only reset last time,which before the rootfs mount. bool rst = false; ////////////////////////////// static int imx_lcdifv3_runtime_resume(struct device *dev) { int ret = 0; struct lcdifv3_soc *lcdifv3 = dev_get_drvdata(dev); if (unlikely(!atomic_read(&lcdifv3->rpm_suspended))) { dev_warn(lcdifv3->dev, "Unbalanced %s!\n", __func__); return 0; } if (!atomic_dec_and_test(&lcdifv3->rpm_suspended)) return 0; /* set LCDIF QoS and cache */ if (of_device_is_compatible(dev->of_node, "fsl,imx93-lcdif")) regmap_write(lcdifv3->gpr, 0xc, 0x3712); request_bus_freq(BUS_FREQ_HIGH); ret = lcdifv3_enable_clocks(lcdifv3); if (ret) { release_bus_freq(BUS_FREQ_HIGH); return ret; } ////////////////////////////// if (rst) { /* clear sw_reset */ writel(CTRL_SW_RESET, lcdifv3->base + LCDIFV3_CTRL_CLR); rst = false; } rst = true; ////////////////////////////// /* enable plane FIFO panic */ lcdifv3_enable_plane_panic(lcdifv3); return ret; } 4.Conclusion The uboot logo will be cleaned at log "imx-drm 1.0.0 20120507 for display-subsystem on minor 1". The boot time of  systemd service on evk is very long. For weston.service, it needs 3 seconds. From log here we test, the pcie and ethernet probe after drm system also cost about 1 second. If you want to reduce the boot time of other modules, you can try to reduce the system service and disable pcie/ethernet drivers if you don't need them. [ 2.505616] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1 [ 2.620324] imx6q-pcie 33800000.pcie: iATU unroll: enabled [ 2.620335] imx6q-pcie 33800000.pcie: iATU regions: 4 ob, 4 ib, align 64K, limit 16G [ 2.720689] imx6q-pcie 33800000.pcie: PCIe Gen.1 x1 link up [ 2.820996] imx6q-pcie 33800000.pcie: PCIe Gen.2 x1 link up [ 2.821003] imx6q-pcie 33800000.pcie: Link up, Gen2 [ 2.821010] imx6q-pcie 33800000.pcie: PCIe Gen.2 x1 link up [ 2.821112] imx6q-pcie 33800000.pcie: PCI host bridge to bus 0000:00 [ 2.821119] pci_bus 0000:00: root bus resource [bus 00-ff] [ 2.821126] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 2.821133] pci_bus 0000:00: root bus resource [mem 0x18000000-0x1fefffff] [ 2.821161] pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400 [ 2.821176] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff] [ 2.821187] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref] [ 2.821232] pci 0000:00:00.0: supports D1 [ 2.821237] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold [ 2.824664] pci 0000:01:00.0: [1b4b:2b42] type 00 class 0x020000 [ 2.824725] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x000fffff 64bit pref] [ 2.824761] pci 0000:01:00.0: reg 0x18: [mem 0x00000000-0x000fffff 64bit pref] [ 2.825066] pci 0000:01:00.0: supports D1 D2 [ 2.825072] pci 0000:01:00.0: PME# supported from D0 D1 D3hot D3cold [ 2.835499] pci 0000:00:00.0: BAR 0: assigned [mem 0x18000000-0x180fffff] [ 2.835511] pci 0000:00:00.0: BAR 15: assigned [mem 0x18100000-0x182fffff pref] [ 2.835519] pci 0000:00:00.0: BAR 6: assigned [mem 0x18300000-0x1830ffff pref] [ 2.835530] pci 0000:01:00.0: BAR 0: assigned [mem 0x18100000-0x181fffff 64bit pref] [ 2.835561] pci 0000:01:00.0: BAR 2: assigned [mem 0x18200000-0x182fffff 64bit pref] [ 2.835590] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 2.835598] pci 0000:00:00.0: bridge window [mem 0x18100000-0x182fffff pref] [ 2.835899] pcieport 0000:00:00.0: PME: Signaling with IRQ 218 [ 2.897767] Console: switching to colour frame buffer device 135x120 [ 3.098361] imx-drm display-subsystem: [drm] fb0: imx-drmdrmfb frame buffer device [ 3.111239] pps pps0: new PPS source ptp0 [ 3.316650] fec 30be0000.ethernet eth0: registered PHC device 0 [ 3.323645] imx-dwmac 30bf0000.ethernet: IRQ eth_lpi not found [ 3.329593] imx-dwmac 30bf0000.ethernet: force_sf_dma_mode is ignored if force_thresh_dma_mode is set. [ 3.340074] imx-dwmac 30bf0000.ethernet: User ID: 0x10, Synopsys ID: 0x51 [ 3.346883] imx-dwmac 30bf0000.ethernet: DWMAC4/5 [ 3.351684] imx-dwmac 30bf0000.ethernet: DMA HW capability register supported [ 3.358825] imx-dwmac 30bf0000.ethernet: RX Checksum Offload Engine supported [ 3.365966] imx-dwmac 30bf0000.ethernet: Wake-Up On Lan supported [ 3.372113] imx-dwmac 30bf0000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 3.379778] imx-dwmac 30bf0000.ethernet: Enabled L3L4 Flow TC (entries=8) [ 3.386573] imx-dwmac 30bf0000.ethernet: Enabled RFS Flow TC (entries=10) [ 3.393373] imx-dwmac 30bf0000.ethernet: Enabling HW TC (entries=256, max_off=256) [ 3.400950] imx-dwmac 30bf0000.ethernet: Using 34 bits DMA width [ 3.608045] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.613580] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1 [ 3.621621] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220fe6d hci version 0x110 quirks 0x0000002001010010 [ 3.631059] xhci-hcd xhci-hcd.1.auto: irq 226, io mem 0x38200000 [ 3.637197] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 3.642698] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2 [ 3.650365] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed [ 3.657695] hub 1-0:1.0: USB hub found [ 3.661473] hub 1-0:1.0: 1 port detected [ 3.665669] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 3.674445] hub 2-0:1.0: USB hub found [ 3.678220] hub 2-0:1.0: 1 port detected [ 3.683428] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 7 mkt segment 2 supported-hw 0x80 0x4 [ 3.693184] Hot alarm is canceled. GPU3D clock will return to 64/64 [ 3.702683] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO [ 3.703346] mxc-mipi-csi2-sam 32e40000.csi: supply mipi-phy not found, using dummy regulator [ 3.716645] : mipi_csis_imx8mp_phy_reset, No remote pad found! [ 3.722602] mxc-mipi-csi2-sam 32e40000.csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 500000000 [ 3.739353] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA [ 3.752018] isi-m2m 32e00000.isi:m2m_device: Register m2m success for ISI.0 [ 3.759172] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 3.768303] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 3.787598] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 3.795171] ALSA device list: [ 3.796227] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db [ 3.799186] No soundcards found. [ 3.819630] EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Quota mode: none. [ 3.828212] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 3.834944] devtmpfs: mounted
查看全文
  Introduction   Prior to 6.1.22_2.0.0 BSP release, Bluetooth interface are based on the tty line discipline framework, so we need to use hciattach tool to enable it in the user space. From 6.1.22_2.0.0 BSP, the nxp bluetooth driver no longer needs the help of the userspace hciattach tool, and the tty port bound by bluetooth also won't be exported to the user space, so you cannot find the corresponding tty device anymore. So, you won't see the (/dev/ttymxcX), for the Bluetooth interface. All jobs has been done in the new NXP Bluetooth driver. New Method   The new NXP Bluetooth UART Driver is based on a server driver for the NXP BT serial protocol, which can enable the built-in Bluetooth device inside an NXP BT chip. This driver has a Power Save feature that will put the chip into a sleep state whenever there is no activity for 2000ms and will be woken up when any activity is to be initiated over UART.  Device Tree support The new BT framework requires adding a "bluetooth" sub node with a device compatibility string to the attached UART node in the dts file &uart1 { bluetooth { compatibility = "nxp,88w8987-bt"; fw-init-baudrate = <3000000>; #Optional. Default is considered 115200 if this parameter not defined. }; };   Note: The parameter ‘compatibility = “nxp,88w8987-bt”’ will use for 88W8987, IW416, 88Q9098, IW612 chipsets and need to change for 88W8997 with parameter ‘compatibility = “nxp,88w8997-bt”’.   Note: ’fw-init-baudrate’ parameter depends on the module vendor. The Murata and Azuere wifi modules support in BSP release uses the default value -- 115200. We strongly recommend looking at the module vendor-specific baud rate parameter. Note: For the old 88Q9098 Murata 1XL module that uses the 3Mbps by default, please add the fw-init-baudrate = <3000000> property in dts files to make it work. Enable Guide   Use wifi interface to load combo (wifi & bt) firmware and enable BT Need to load wifi driver first, then load the BT driver, otherwise, BT driver suspend/resume test will fail. This is a HW limitation, since NXP wifi and BT module use the same power control pin(W_DISABLE1#), if we don't load the wifi driver, SDIO bus will power down the wifi chip during suspend resume, which may cause the BT chip also been powered down and cannot work after resume back. So we need to load the wifi driver to make sure SDIO bus won't power down the BT chip to make sure BT functions can work during suspend resume. modprobe moal mod_para=nxp/wifi_mod_para.conf modprobe btnxpuart or insmod mlan.ko insmod moal.ko mod_para=nxp/wifi_mod_para.conf insmod btnxpuart   Unload UART Driver modprobe moal Make sure run hciconfig hci0 up or hciconfig hci0 reset or bluetootctl power on before unload btnxpuart driver. If we don't open hci0 interface, the driver cannot send change to 115200 baud rate command to BT chip, which causes the host and BT chip baud rate mismatch, the host still uses 115200bps talk to the BT chip which now use 3Mbps, it cannot work anymore. So we need to make sure open the hci0 interface before unload btnxpuart driver.   mod_para=nxp/wifi_mod_para.conf modprobe btnxpuart sleep 3 hciconfig hci0 up #Note: Need to up hci interface before unload the BT module hcitool -i hci0 cmd 3F 23 02 00 00 modprobe -r btnxpuart modprobe -r moal sleep 3​ For better reference: Please find the I.MX 8MQ Linux getting started user guide, UM11483, Chapter "7.1 Bring-up using NXP Bluetooth UART driver"  Bluetooth Deep Sleep Feature App Note AN13920, Chapter 6 Load NXP UART driver module NOTE: Please do not run the power save feature for Murata IW612 2EL Module Regards, Mario
查看全文
In the i.MX8MP support 3 SDIO interface, and in the reference board i.MX 8M Plus LPDDR4 EVK design default use the eMMC connect to the USDHC3 to boot up from emmc,use the SD card connect to the USDHC2 port. When the U-Boot starts, it will detect the starting slot and automatically set mmcdev and mmcroot, for the USDHC3 in the default Linux set is mmc dev 2. But some customer need to change to the mmc dev 0, make the mmc0 work, see the following introduction.   1 For the EMMC         MMC (multiMedia card) is a communication protocol that supports two modes, SPI and MMC. EMMC is a chip that supports MMC protocol. Both eMMC and SD card package the flash controller and NAND Flash together, but their interfaces are different. eMMC is generally BGA packaged and soldered on PCB.   EMMC includes 11 signals, namely CLK, CMD, DATA0-7 and Data Strobe. The specific signals are as follows: CLK: It is used to output clock signal from the host side, synchronize data transmission and drive device operation. Each cycle can be transmitted on the rising or falling edge, or both CMD: The signal is mainly used by the host to send a command to the eMMC and the eMMC to send a response to the host. DAT0-7: DAT0-7 signal is mainly used for data transmission between Host and eMMC. After the eMMC is powered on or soft reset, only DAT0 can transmit data. After initialization, DAT0-3 or DAT0-7 can be configured for data transmission, that is, the data bus can be configured as 4 bits or 8 bits. Data Strobe: The clock signal is sent to the host by eMMC with the same frequency as the CLK signal. It is used for synchronization of data reception at the host side. The Data Strobe signal can only be configured and enabled in the HS400 mode. After being enabled, the stability of data transmission can be improved and the bus tuning process can be omitted. 2 For the EMMC design on the i.MX8MP LPDDR4 EVK 2.1 The i.MX8MP The i.MX8MP there is 3 SDIO interface,and the i.MX8MP has 3 USDHC ports:USDHC1, USDHC2 and USDHC3.   At i MX8MP supports SD/MMC/eSD/eMMC/SDXC, and starts and boots using the USDHC port based on setting of the BOOT_MODE[3:0] pins.       In the reference design, eMMC is connected to USDHC3, and SD card is connected to USDHC2. USDHC3 is used as the eMMC boot device by default on the development board. We can see the detailed definitions of the three USDHC interfaces in the reference manual. Among them, USDHC1 and USDHC3 are 8 bits and support 8-bit data, while USDHC2 only supports 4-bit data.   2.2 Hardware and software design   The hardware design is as shown above. The eMMC is connected to the SD3 interface, and the software is configured in this way by default. 2.3 The port number of the default BSP In the i.MX 8M Plus LPDDR4 EVK development board design, the eMMC is connected to the USDHC3 as the default boot device When the U-Boot starts, it will detect the starting slot, and automatically set mmcdev and mmcroot. For USDHC3, the default is mmc dev 2.   The device structure of SD/MMC cards is similar. MMC should be the predecessor of SD, but the design of MMC at that time was half that of SD. Therefore, the SD/MMC driver is universal, and the device node of Linux continues the name of MMC.   Meaning of blk: blk is a block device, and the number after ⾯ is the serial number of the device   Meaning of p: p indicates partition, and p1 is the first partition   We can see the correspondence between the USDHC interface and the mmc under Linux. The kernel MMC module now uses a fixed mmcblk index for the uSDHC slot. The default BSP is "mmc2=&usdhc3":   In the design of the MX 8M Plus LPDDR4 EVK development board, by default, the eMMC is connected to the USDHC3, SD3 is used, and mmcblk2 is used in the SD3 slot. When setting the kernel parameters in the u-boot, you can see that: ### select mmc dev 2 (USDHC3) on the i.MX 8M Mini EVK, i.MX 8M Nano EVK, and i.MX 8M Plus EVK: U-Boot > mmc dev 2 0 For the emmc the related port is :mmcblk2 By default, the flash target is MMC: 2 after the Demo images burning of the development board is started.   3 mmc0 work as emmc device and boot up We need to modify the device, u-boot, kernel related part for the mmc0 work on the android BSP, 3.1 Software modify 2.2.1 u-boot: Dts section root/arch/arm/dts/imx8mp-evk.dts: memory@40000000 {                  device_type = "memory";                  reg = <0x0 0x40000000 0 0xc0000000>,                        <0x1 0x00000000 0 0xc0000000>;         }; aliases { /* SD/MMC: eMMC/SD slot numbering fix */        mmc0 = &usdhc3; /*Modify the usdhc3 and mmc0, default is mmc2*/        mmc1 = &usdhc2; /* usdhc2 and mmc0 do not change*/        mmc2 = &usdhc1; /*Modify the usdhc1 to mmc2, make the usdhc1 work*/         }; reg_can1_stby: regulator-can1-stby {…..} Board secton: root/board/freescale/imx8mp_evk/imx8mp_evk.c int board_init(void) {         struct arm_smccc_res res; } int board_mmc_get_env_dev(int devno) {        if(devno == 0)         return devno + 2;           else if (devno == 2)         return devno - 2;           else         return devno; }   int mmc_map_to_kernel_blk(int devno) {         return devno; } int board_late_init(void) {         board_late_mmc_env_init(); } SPL: root/common/spl/spl_mmc.c int spl_mmc_load_image(struct spl_image_info *spl_image,                         struct spl_boot_device *bootdev) {…..} Default settings:     2.2.2 kernel section: In the kernel section need to change all the related mmcblk2 to mmcblk0.                   2.2.3 device section modify: Change all the related mmcblk2 to mmcblk0. Change the uuu_imx_android_flash.bat /android_build/device/nxp/common/tools/fastboot_imx_flashall.bat if not [%soc_name:imx8mp=%] == [%soc_name%] (  set vid=0x1fc9& set pid=00x0146& set chip=MX8MP  set uboot_env_start=0x2000& set uboot_env_len=0x8  - set emmc_num=2& set sd_num=1 + set emmc_num=0& set sd_num=1  set board=evk  goto :device_info_end   All the modify see the Patch in the attachment.
查看全文
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there.  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
查看全文