技术日 - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

讨论

排序依据:
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks.
查看全文
This class provides an introduction to the model-based design tools for vision and RADAR. The lecture will provide an overview of each of the tools along with a demonstration.
查看全文
This class provides an introduction on the S32 Design Studio for Vision IDE with the new S32 Debugger and S32 Debug Probe. The lecture will provide an overview of the S32 Design Studio for Vision IDE with S32 Debugger and S32 Debug Probe along with a demonstration. Also, there will be a preview of the S32 Configuration Tool coming in the next generation S32 Design Studio.
查看全文
Tired of failing EMC certification over and over again? Join the crowd. Shrinking IC geometries and resulting increase in switching speeds make designing compliant printed circuit boards more challenging than ever. We need a new design methodology to change this unacceptable status quo, one based on electromagnetic field physics. This training module presents a basic introduction to EM fields and provides guidelines for building successful, cost-effective printed circuit boards. This presentation includes example designs and test results.
查看全文
Full power helm! A new way to design your power system, focused on the “Plumbing”! A simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC. Examples with results will be discussed.
查看全文
In this class, you will learn to use NXP’s FreeMASTER debug tool to aid in system development and debug. Although it is has many uses in various applications, we will demonstrate the features and use of FreeMASTER to simplify the development process with a motor control example based on our MagniV MC9S12ZVMRM microcontroller. Participants will see how useful and easy it is to use and configure so that system variables can be adjusted on the fly or watch system parameters real time.
查看全文
Combustion and motor control is moving to more computation-intensive techniques.  Hear about how the S32 Automotive platform will support this trend with Arm® NEON and math acceleration.
查看全文
Explores the fast-growing Automotive Gateway market, identifying key use cases and requirements, and how gateways will evolve over the next decade.
查看全文
How to conduct early development for next-generation Vehicle Dynamics and Safety (VDS) S32P2/S2 devices with the GreenBox development tool.
查看全文
Overview of the extended resource domain controller of the S32x devices.
查看全文
Achieving the lowest MCU power during sleep presents challenges to HW and SW designers from switching off clocks and power to modules. Low-power use cases and concepts for NXP's Mode Entry module are presented along with implications to hardware design, software design and debugging.
查看全文
The session is intended for engineers either getting started or are interested in seeing how to use AUTOSAR MCAL to generate and implement code. “Hello world” level examples are presented using the Tresos configuration tool to generate AUTOSAR defined structures. These structions are combined with NXP written drivers and user code to build an application.
查看全文
Overview of the S32x next-generation safety architecture spanning ASIL B to ASIL D. What’s new and how we better enable the customer with a full set of safety collateral including MCU HW, SW and SBC HW.
查看全文
Hands-on getting started with MagniV. Participants will work with bare metal application code and Processor Expert, working with an S12ZVC development kit and CodeWarrior IDE. Short presentations followed by hands-on labs. Learn coding secrets for fast application startup!
查看全文
Hands-on getting started with S32K. Participants will work with bare metal application code, working with an S32K144 development kit and S32 Design Studio. Short presentations followed by hands-on labs. Learn coding secrets for S32K and Arm® Cortex-M!
查看全文
A hands-on session to show how to prepare and program device for CSEc security operations. Session also covers both bare metal and SDK approach to program CSEc module. The NVM part will cover the enablement/configuration of the different types of memory and tools that NXP provides for calculating the endurance.
查看全文
Presentation of the high-performance packet processing solutions being developed on i.MX processors and expected performance gains compared to a standard software stack.
查看全文
Introduction to the new i.MX 8 and 8X automotive applications processor product families and associated target applications, development tools, and software ecosystem.
查看全文
Start using UUU and the Pins Tool for i.MX family. First, overview of the new firmware download tool called Univeral Update Utility. Then learn about exciting updates to the Pins Tool for streamlining hardware development.
查看全文
Introduction to i.MX RT products and automotive qualified variants for multimedia applications requiring real time processing and low bill of materials.
查看全文