テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Understand the value, benefits and features  of Arm's latest Cortex-M33 core through a LPC5500-based product training and hand-on session.
記事全体を表示
Join this session to understand all the security features integrated in the recently launched LPC5500 MCU Family and learn how to implement these features to design a low-power system with robust security using the MCUXpresso Software & Tools.
記事全体を表示
Hands-on class diving into advanced debugging and trace features featured in MCUXpresso IDE.
記事全体を表示
Join this session to understand all the security features integrated in the recently launched LPC5500 MCU Family and learn how to implement these features to design a low-power system with robust security using the MCUXpresso Software & Tools.
記事全体を表示
Do you need a robust MCU for high reliability and safety applications? Join this class to learn about the S32K MCU platform which offers auto grade, CAN-FD, lower power, hardware and software scalability and a minimum 15 year longevity.
記事全体を表示
S32V234 vision product family introduction.
記事全体を表示
SE050: The New Generation of NXP’s Plug & Trust Solutions to Secure Your IoT Services
記事全体を表示
Solutions Around the Core – Interfaces and Power Solutions
記事全体を表示
Introducing Murata Wi-Fi IBT Connectivity Modules for NXP i.MX & RT Platform.
記事全体を表示
Hands-on workshop, NTAG I2C Plus Brings NFC Connectivity into Consumer Electronics for Tiny Devices
記事全体を表示
Hands-on workshop introducing LCP55xx. Lab materials.
記事全体を表示
Hands-on workshop introducing LCP55xx.
記事全体を表示
Evolving IoT Needs of Brands Protect and Enhance Product Experiences through Advances in NFC Technology
記事全体を表示
Introducing the new KE1xZ 5V robust MCUs with Touch and CAN. This class will provide an overview of the new KE1xZ MCUs and give details on the highlighted features of TSI and CAN. A touch demo presentation will also help the attendees understand the TSI measurement and innovate new touch applications.
記事全体を表示
NXP security solutions and use cases. The fast, easy way to deploy secure IoT connections.
記事全体を表示
LPC5500 MCU series, industrial and IoT edge applications based on Arm® Cortex®-M33 microcontrollers.
記事全体を表示
This presentation will first highlights some basic training techniques, such as data augmentation, but the primary focus will be on various ways to deploy neural network frameworks and classical machine learning algorithms, and most importantly, utilizing a variety of open source tools and techniques. We will show how these techniques fit in with some real use cases such as object recognition and anomaly detection. The hands-on session portion of the class will allow attendees to take a trained neural network model and deploy it on a i.MX 8M. Attendees will utilize the Linux development environment and implement an end-to-end use case.
記事全体を表示
Learn how to create a secure / non-secure application and debug on a secure Cortex-M33 NXP device.
記事全体を表示
The rise of NFC is ongoing. Now that traditional markets such as mobile payment and contactless access are well-established, we see NFC creating new markets on its own and providing technological advancements that fuel a new wave of innovation. This session looks into new use cases for NFC. It will also be the first time NXP presents its next technological evolution for NFC.
記事全体を表示
OpenIL is an open source software distribution for industrial and automation market.  OpenIL provides industrial-grade real time, security and network determinism. OpenIL is an ideal Linux distribution for PLC, HMI, industrial control and robotics. In this session, an overview of OpenIL is conducted including Xenomai, baremetal solution, TEE, TSN, Industrial network with OPCUA and EtherCAT and how they run on Layerscape.
記事全体を表示