テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
記事全体を表示
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
記事全体を表示
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
記事全体を表示
Learn how to solve your I2C system challenges by deploying I3C. Our experts will provide a comprehensive introduction into the new MIPI I3C interface and its advantages compared to the well-known, I2C interface. This session gives an overview of how to develop I3C-based systems as well as provide a view of NXP’s MIPI I3C slave RTL, which is the first verified, freely available RTL source code available for download.
記事全体を表示
Near-field-communication (NFC) is the better, safer way to protect brands while ensuring ease of use for accessories and consumables. With NFC, the device itself can verify the authenticity and can configure operating modes or change settings based on the type of accessory or consumable. With a standard NFC phone, a user can check the originality or trigger a reorder through a simple tap. In this presentation we will show which options exist on NFC tag and reader side, and how to implement a solution in a practical example.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
記事全体を表示
Business Line Smart Antenna Solution delivers a broad range of RF products for many different applications ranging from mobile phones to wireless infrastructure. All these applications require high performance RF products to deliver reliable, high data rate connections. This training will show how our RF products can be successfully used in IoT applications to improve the RF connection: range extension by using LNAs in the receive chain or by adding a PA at the transmit side. Our wide product portfolio ensures that  the different needs of IoT (frequency range, power consumption and performance gain) can be met.
記事全体を表示
This session will highlight the features and design advantages of the QN9080 BLE SoC portfolio for small form factor products with rich feature sets that can operate for multiple years on small coin cell batteries.
記事全体を表示
This session will introduce the Sensor Toolbox, the complete ecosystem for product development with the NXP sensors. The key focal points would be introducing the IoT Sensing SDK (ISSDK) application development framework, Freedom Sensor Toolbox-Community Edition (STB-CE) and a wide range of the new sensor boards. The highlight of the training would be showcasing multiple STB-CE out of box sensor demonstrations and the steps to get started with IoT Sensing SDK (ISSDK) sensor application development.
記事全体を表示
Extending the scalable range of the i.MX product line, the i.MX 8 series establishes an unmatched range of cost-performance scaling with pin-compatible options and the highest level of software reuse. Built with a high-level integration to support graphics, video, image processing, vision, audio and voice functions, the i.MX 8 series transforms your everyday interactions. Preview the next generation i.MX 8 series applications processors for Automotive, Consumer and Industrial applications.
記事全体を表示
Discover NXP’s Layerscape multicore 64-bit ARM®-based solutions and learn how this scalable family leverages line-rate networking and production grade software to accelerate your time-to-market in industrial, networking and consumer applications.
記事全体を表示
Technical deep dive on product architecture and software offering. Learn how to build an automotive application using the S32 SDK drivers, stacks and FreeRTOS. Integration with S32 Design Studio IDE, tips and tricks.
記事全体を表示
When choosing the NFC device for a new design, the system architect must consider many parameters. Usually a strong focus is put on hardware specific aspects like the environment, possible antenna size, performance and interface. To avoid unpleasant surprises during software implementation phase, software has to be taken into account as well from the beginning. Different NFC IC categories (NFC Frontends, NFC Controller, Connected Tag) have different strengths, depending on the software environment. The way how highly integrated operating systems like Linux are structured brings both new challenges and advantages. This session examines the considerations necessary when designing in NFC in different operating systems or "bare metal" systems. It also discusses the advantages and disadvantages of the different device categories in dependence of the designated environment.
記事全体を表示
Building on its 10+ year of industry-leading innovation, an exciting future is in store for the LPC portfolio. Join this session to learn more about the renewed LPC roadmap and take a closer look into the power advantages offered with by the latest family introduced – the LPC546xx MCU family.
記事全体を表示
Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and accurate media compatibility. This class will step through some of key the leading applications in the Medical and Industrial markets that have found usage of motion and pressure sensors as well as some up and coming applications. 
記事全体を表示
Introduction to the standard - with emphasis on how to apply it, cross BL.
記事全体を表示
Learn about NXP's S32V family for vision processing, with a special focus product architectures and software (enablement and application level). You will also see real application use case examples using APEXCV Libraries and EVB.
記事全体を表示
Enabling Design, Technologies & Solutions All You Need to Know About DDR4  Boost Your Productivity with CodeWarrior® Development Tools for ARM®v8 Architecture  Hands-On Workshop: General Purpose MCU S32K Deep Dive and S32 SDK  Hands-On Workshop: Kinetis Motor Suite  Hands-On Workshop: MCUXpresso Software and Tools  Hands-On Workshop: MCUXpresso Software and Tools_Lab Guide.pdf  Innovation Made Easy With LPC MCUs: A Roadmap Overview and Deeper Dive Into LPC546xx MCU Family Power Advantages  Introduction to the Next-Generation USB Type-C Connector and NXP’s End-to-End Solution  NFC Integration in Real-Time and Non-Real-Time Operating Systems - Which NFC Product Fits the Best?  NXP’s Next-Generation Layerscape Linux® SDK  NXP’s Sensor Toolbox Ecosystem Overview of the I3C Interface, Successor of the Well-Known I2C Interface  Secure Connected & Automated Vehicles IEC61508 Functional Safety Overview  S32V MPU for Vision, Surround and Fusion Processing  Secure Mobile, Healthcare & Wearables Designing with the New Ultra-Low-Power BLE System on Chip  Smart Buildings & Consumer Goods Google™ Home and NXP®: Android Things, Google Assistant and Chromecast™ Built-in  i.MX 8 Applications Processors Family Overview: i.MX 8, i.MX 8X, i.MX 8M  Low-Power i.MX Applications Processors Overview  Secure Authentication for Anti-Counterfeit Applications  Sensor Products for Medical and Industrial Markets  Voice Control Solutions: Creating Amazon® Alexa® Devices with i.MX  Smart Machinery & Industrial Automation NFC in Industrial and Healthcare—More Use Cases than You Can Imagine  The Next Wave of Industrial Networking with Time Sensitive Networking (TSN)  Smart Networks & Computing Overview of Layerscape 64-bit ARM® Family  San Jose & Westford: Leverage NXP Security and Trust Features for Your System 
記事全体を表示
The i.MX 8M was designed with consumer and industrial customers in mind. The i.MX 8M series of processors are the first in a completely new paradigm of processors designed targeting market leading performance for audio, video and voice. The i.MX 8M starts with a system solution in mind and drives optimized solutions (best in class performance, optimized system cost, built with Google/Amazon/Msft ecosystems in mind) for many different customers from HMI, audio, video, voice, IOT, digital signage, printers, machine vision, etc. Best in class 4K video with HDR, best in class audio interfaces, low-power and optimized for lower cost. Come see what this new family of processors is all about and learn where we are headed.
記事全体を表示
This class will introduce Android Things, the new version of Android designed for the IoT market. The when, what and how of Android Things will be explained and how NXP has worked with Google™ to enable certified boards based on NXP silicon. A live demo of Android Things will be shown sampling and analyzing data real time via the cloud. Finally the relationship between Android Things, Google Voice Assistant and Chromecast will be explained and what NXP parts are most appropriate for optimal performance.
記事全体を表示