テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Discover NXP’s Layerscape multicore 64-bit ARM®-based solutions and learn how this scalable family leverages line-rate networking and production grade software to accelerate your time-to-market in industrial, networking and consumer applications.
記事全体を表示
This training will take a user from “out of box” to a functioning IoT system including edge devices, gateway/border router, smart phone app and cloud connectivity, then run the system through its paces to highlight a subset of common IoT capabilities. The training will leverage the NXP Modular IoT Framework using a currently shipping, fully documented, Integrated Development Experience for the exercises. Southbound connectivity between gateway and the edge devices will be Thread and ZigBee®. Device commissioning will be via NFC and BLE. Northbound connectivity from gateway to cloud will be Wi-Fi. Cloud support will be via a major cloud provider. Note: Users will be able to use their own Android or iPhone with a recent OS version.
記事全体を表示
When choosing the NFC device for a new design, the system architect must consider many parameters. Usually a strong focus is put on hardware specific aspects like the environment, possible antenna size, performance and interface. To avoid unpleasant surprises during software implementation phase, software has to be taken into account as well from the beginning. Different NFC IC categories (NFC Frontends, NFC Controller, Connected Tag) have different strengths, depending on the software environment. The way how highly integrated operating systems like Linux are structured brings both new challenges and advantages. This session examines the considerations necessary when designing in NFC in different operating systems or "bare metal" systems. It also discusses the advantages and disadvantages of the different device categories in dependence of the designated environment.
記事全体を表示
The rise of NFC is ongoing. Now that traditional markets such as mobile payment and contactless access are well-established, we see NFC creating new markets on its own and providing technological advancements that fuel a new wave of innovation. This session looks into new use cases for NFC. It will also be the first time NXP presents its next technological evolution for NFC.
記事全体を表示
Automotive Advanced Analog Solutions  Emerging Trends & Innovation NXP Microcontroller Update Smart Machinery & Industrial Automation Hands-On Workshop: Secure Connection to Google Cloud IoT Core  Smart Networks & Computing Layerscape - Edge Computing  Smarter World Solutions & Multimode Connectivity Are You Ready for the Next i.MX Product Launch?  Hands-On Workshop: i.MX RT Cross-Over Processors  NXP Secure, Interface and Power Solutions  See What's Next on NFC Technology 
記事全体を表示
Learn how to create a custom SDK for your specific hardware board featuring MCUXpresso SDK and config tools.
記事全体を表示
Using our product demonstration and reference design, this class will teach you how to build your own cloud connected end node with our latest power-efficient LPC54018 flashless MCU. We will use Amazon Web Services (AWS).
記事全体を表示
This class will provide an overview of the i.MX RT series, key peripheral, including a hands-on tutorial using the i.MX RT EVK.
記事全体を表示
Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. To protect firmware execution given today’s threat landscape, there must be a policy to only allow execution of authenticated firmware. The methods used to enforce this policy rely on MCU security technology to create a protected boot flow. The boot firmware can contain public key cryptography to authenticate application code. In addition to these components integrated in the end device, there are tools and steps that must be taken in the manufacturing environment using manufacturing hardware for code signing and host programs for provisioning. Join this session to explore the design and implementation of a secure boot with i.MX RT.
記事全体を表示
Introduction to the new i.MX 8 and 8X automotive applications processor product families and associated target applications, development tools, and software ecosystem.
記事全体を表示
Introduction to Kinetis KW and Thread.
記事全体を表示
Learn about NXP i.MX next-generation solutions (i.MX 7ULP, i.MX 8).
記事全体を表示
This session will introduce the PMSM motor parameter measurement, tuning tools, FreeMASTER and motor control library as well as the configuration of a new PMSM. Get hands-on experience running the PMSM step-by-step and do some PMSM FOC tasks for testing.
記事全体を表示
Whether you are looking for an easy and cost-efficient parametrization solution or want to use a smartphone for ad-hoc diagnosis of a device, Near-field-communication (NFC) makes this possible now. Or you might want to communicate with a fully sealed, battery-less device? Learn in this session about many new use cases, in which NFC simplifies handling, saves cost or enables features which were not possible before in industrial or healthcare applications. There are more possibilities than you would have imagined!
記事全体を表示
This session will feature the LPC54114 MCU, the latest release of the LPC54000 low-power series, to demonstrate how to take advantage of dual-core architecture in always-on applications. Optimize product design for extended battery life and bring them to market quickly with this hands-on session. Topics will range from system architecture, software design and debugging, to power optimization, sound detection, and voice triggering.
記事全体を表示
This hands-on session will show users how to get to market faster by leveraging MCUXpresso SDK examples within their end product designs. Attendees will get hands-on with key SDK demo applications and driver examples.
記事全体を表示
Solutions from NXP provide the right hardware, modular software, certifications, partners and documentation to accelerate time-to-market for our customers. Join this class to experience a deep dive on what is delivered from the newly launched SLN-POS-RDR Card Reader Solution.
記事全体を表示