テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Design, Software & Services EUF-DES-T2474 - Interface Solutions  Insight & Innovation EUF-INS-T2477 - Sensor Update  Secure Connected & Automated Vehicles Advanced Analog Products for Automotive and Industrial Markets  EUF-AUT-T2475 - Analog Products  Secure Mobile, Healthcare & Wearables EUF-MHW-T2470 - Wireless Solutions  Smart Home & Buildings EUF-HMB-T2472 - Are You Ready for the Next Generation of NFC?  Smart Networks EUF-NET-T2471 - Layerscape Update 
記事全体を表示
In automotive sub-system applications, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems or the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, high-speed switches, voltage level translators and GPIO expanders are often used to bridge between the interconnects on the board. In this session, we will explore the application of these interface devices from NXP and discuss their applications in automotive sub-systems.
記事全体を表示
This class provides an introduction to the model-based design tools for vision and RADAR. The lecture will provide an overview of each of the tools along with a demonstration.
記事全体を表示
This training will take a user from “out of box” to a functioning IoT system including edge devices, gateway/border router, smart phone app and cloud connectivity, then run the system through its paces to highlight a subset of common IoT capabilities. The training will leverage the NXP Modular IoT Framework using a currently shipping, fully documented, Integrated Development Experience for the exercises. Southbound connectivity between gateway and the edge devices will be Thread and ZigBee®. Device commissioning will be via NFC and BLE. Northbound connectivity from gateway to cloud will be Wi-Fi. Cloud support will be via a major cloud provider. Note: Users will be able to use their own Android or iPhone with a recent OS version.
記事全体を表示
DDR4 (and beyond) dramatically increased the complexity of DDR configuration - even after simulation. More importantly, knowing the right parameters for DDR can make or break the performance of your product. Learn how to configure, optimize and validate DDR functionality directly on your board. Understand the tools and techniquest to obtain the data eye margins, reduce the time for DDR board bring-up and functional validation from weeks to hours.
記事全体を表示
Learn more about the main Wireless protocols and the NXP value proposition for each of them.
記事全体を表示
Overview of the i.MX RT family, where to find the related tools, getting started, and where to go for support.
記事全体を表示
At NXP, our broad portfolio of analog, interface and NFC solutions means that we are able to offer complete solutions around the core. With a range of options that attach to any core, our product expertise in areas such as NFC, power management, networking and interfaces is deep-rooted.
記事全体を表示
Experience design freedom through our advanced analog technologies, motor and load drivers, power management, in-vehicle networking, etc.
記事全体を表示
Evolution of Automotive car architecture with more hybridization and ADAS power computing require evolution of power management to fit with application and environment changes. During this session you will have an overview of automotive market dynamics and a deep dive of latest safety power management solutions to support applications up to ASIL D (FS66, FS84, FS85).
記事全体を表示
This hands-on session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs based on the ARM® Cortex®-M core. Using either Kinetis or LPC development hardware, attendees will build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application.
記事全体を表示
Design, Software & Services APF-DES-T2229 - Kinetis New Products, KE+, Security with K8x & KL8x  Smart Machinery & Industrial Automation APF-SMI-T2225 - Motion Sensors for Industry and Medical
記事全体を表示
Presented by Cao Nan, Nanjing Normal University Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
記事全体を表示
EUF-MHW-T1748 - This session will give an overview of the wearables for the IoT.
記事全体を表示
Sense everything you need on a connected world with NXP sensors.
記事全体を表示
With its broad portfolio, NXP is uniquely positioned to propose a full system allowing a scalability from NCAP to L4/L5 autonomous driving. To address such scalability, NXP has faced some challenging decisions about the system partitioning, performance, safety decomposition, AI Acceleration and Programming language. All these challenges will be addressed during the session.
記事全体を表示
Near-field-communication (NFC) is the better, safer way to protect brands while ensuring ease of use for accessories and consumables. With NFC, the device itself can verify the authenticity and can configure operating modes or change settings based on the type of accessory or consumable. With a standard NFC phone, a user can check the originality or trigger a reorder through a simple tap. In this presentation we will show which options exist on NFC tag and reader side, and how to implement a solution in a practical example.
記事全体を表示
Lab material from "Hands-On Workshop: Optimizing and Tuning FreeRTOS Applications with MCUXpresso Software and Tools".
記事全体を表示