テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
AWS Shadow - Labs 1-2
記事全体を表示
Hands-on getting started with S32K. Participants will work with bare metal application code, working with an S32K144 development kit and S32 Design Studio. Short presentations followed by hands-on labs. Learn coding secrets for S32K and Arm® Cortex-M!
記事全体を表示
An Overview on QorIQ Trust Features for Securing Embedded Systems ARM® v8 Virtualization for Layerscape Multicore Communications Processors Logical Abstraction and Resource Management with Layerscape Management Complex Low-Power Wireless Connectivity Solutions for Home Automation NFC Everywhere - The new NFC use cases for your customers Powerful QorIQ Multicore Processors for the New Virtualized Network RF Power Solutions for Industry-Avionics-Military-Cooking-Cellular Markets (L Gauthier) Scalable Multicore QorIQ Layerscape Processors Scalable Multicore QorIQ Layerscape Processors Based on 64-bit Software Environment for Enterprise, Home and Industrial Applications (H Cohen) Solutions for the Wearable Market QorIQ Layerscape LS2085/88 Multicore Communications Processors For the Future of Networking QorIQ LS2 Series: AIOP, WRIOP, DPAA2 - High-Performance Datapath and Network Peripheral Interfaces VORTIQA INTELLIGENT VIRTUALIZATION ACCELERATION SOFTWARE (IVAS)
記事全体を表示
This session will introduce the Sensor Toolbox, the complete ecosystem for product development with the NXP sensors. The key focal points would be introducing the IoT Sensing SDK (ISSDK) application development framework, Freedom Sensor Toolbox-Community Edition (STB-CE) and a wide range of the new sensor boards. The highlight of the training would be showcasing multiple STB-CE out of box sensor demonstrations and the steps to get started with IoT Sensing SDK (ISSDK) sensor application development.
記事全体を表示
Design, Software & Services APF-DES-T2233 - Kinetis KW MCU and Thread  APF-DES-T2229 - Kinetis New Products, KE+, Security with K8x & KL8x  Secure Connected & Automated Vehicles APF-AUT-T2295 - Hands-On Workshop: How to Tune a New PMSM Step-by-Step  Secure Mobile, Healthcare & Wearables APF-MHW-T2232 - LPC541xx for Wearable  Smart Machinery & Industrial Automation APF-SMI-T2225 - Motion Sensors for Industry and Medical
記事全体を表示
Industrial OEMs have been hampered by the large array of networking protocols that they need to support in their devices. The new IEEE Time Sensitive Networking (TSN) standard offers to consolidate multiple proprietary protocols with a common IEEE based standard. Come learn what you can achieve with TSN.
記事全体を表示
The MQX Application Builder is the most recent addition to the MCUXpresso Config Tools. In this session you will use this powerful tool to rapidly create a sophisticated IoT application without requiring detailed knowledge of the protocols used, or how to configure them. By the end of the session you will have created an application that serves up customized web pages, uses the REST and MQTT protocols to remotely access key application parameters, interfaces with a cloud server, synchronize with a time server, remotely control your application with Lua Scripting Language, and more. Learn the power of using the MQX platform over other operating system such as FreeRTOS.
記事全体を表示
Products today need to support a wide array of wireless technologies. This session will address the challenges of supporting multiple IoT protocols (BLE® and 802.15.4) on a single device while coexisting with Wi-Fi from another device, all in the same product.
記事全体を表示
Across almost every market, brand owners face increasing threats from counterfeits of their own products. Counterfeit electronic accessories, often built with inferior quality, not only impact a company's revenue stream but can also result in product reliability and safety issues along with damage to company brands. Learn how the A1006 Secure Authenticator from NXP provides a robust security solution to prevent counterfeits, hacks and attacks to keep your systems secure. With low-power consumption, small footprint, and flexible interfaces, the A1006 offers superior security that is easy to integrate into a range of electronic devices that are common targets of electronic counterfeiters.
記事全体を表示
EUF-NET-T1746 - DPAA2 is composed of new component with various advance features. This presentation is a deep dive into the following DPAA2 components WRIOP, AIOP, SW DPAA object. The viability of the QorIQ LS2085/88 architecture is shown through a "life of a packet" overview.
記事全体を表示
Introduction to Ethernet capable processors for automotive.
記事全体を表示
EUF-NET-T1753 - Shaping a New Era in NFC. With the introduction of its new portfolio of NFC controllers, front ends and connected NFC tag solutions, NXP enables a new era in the evolution of NFC bringing intuitive proximity technology everywhere. Enabling new applications within access, payment, industrial, consumer, smart home and IoT.
記事全体を表示
Show the importance of OTA updates and the requirements for a total system solution for FOTA.
記事全体を表示
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project to get started working on NXP reference boards.
記事全体を表示
This class will provide an overview of NXP's broad and scalable MCU portfolio and give details on which product families are available for different markets and use cases. It will also give an overview of the unified tools, software and solutions that enable the portfolio as well as a demo presentation across the MCU portfolio.
記事全体を表示
Do you plan to secure your data transmission keeping high data throughput, low power and CPU load? Layerscape family is your best choice.
記事全体を表示
No other company has the breadth and diversity of embedded solutions for addressing the challenge of IoT security. From secure element ICs to advanced multimedia and networking microprocessors, NXP delivers the technology needed for securing the entire Lifecycle of the end or edge node. In addition, with Edgescale Cloud services software, devices can be maintained from deployment until decomissioning. Join this class for an overview of NXP's security solution.
記事全体を表示
Hands-on workshop introducing LCP55xx.
記事全体を表示