技术日 - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

讨论

排序依据:
Learn more about NFC's co-inventor product proposal and use cases.
查看全文
Discover NXP’s Layerscape multicore 64-bit ARM®-based solutions and learn how this scalable family leverages line-rate networking and production grade software to accelerate your time-to-market in industrial, networking and consumer applications.
查看全文
Enabling Design, Technologies & Solutions Hands-On Workshop: MCUXpresso Software and Tools  Hands-On Workshop: MCUXpresso Software and Tools_Lab Guide.pdf  Hands-On Workshop: Using MCUXpresso SDK  Introduction to the Next-Generation USB Type-C Connector and NXP’s End-to-End Solution  Irvine: Boost Your Productivity with CodeWarrior® Development Tools for ARM®v8 Architecture  Irvine: LPC800 MCUs Technical Overview: NXP®’s Fastest Growing Portfolio for the Broad, 8-bit Alternative Market  Irvine: Overview of the I3C Interface, Successor of the Well-Known I2C Interface  NXP’s Next-Generation Layerscape Linux® SDK  Payment, Banking & Retail Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 1  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 2  Secure Connected & Automated Vehicles i.MX 8 and 8X Applications Processor Overview  Introduction to Wireless Charging Solutions  Smart Buildings & Consumer Goods Google™ Home and NXP®: Android Things, Google Assistant and Chromecast™ Built-in  Identification and Authentication of Consumables and Accessories via NFC  i.MX 8M Processor Overview and the Road Ahead  Irvine: Modular IoT Framework  Irvine: NFC in Consumer Electronics and Home Appliances  Low-Power i.MX Applications Processors Overview  Secure Authentication for Anti-Counterfeit Applications  Voice Control Solutions: Creating Amazon® Alexa® Devices with i.MX  Smart Networks & Computing How Far Can You Go with NXP's Flexible Layerscape Portfolio?  Learn from Our Experience! Hints, Tips and Tricks to Speed your QorIQ® LS1012A, LS1043A and LS1046A Design Cycle using NXP Support  NXP RF Solutions for IoT to Deliver Reliable, High-Performance Wireless Connections What Can You Build with a 1W 64-bit ARM®v8 SoC? 
查看全文
When choosing the NFC device for a new design, the system architect must consider many parameters. Usually a strong focus is put on hardware specific aspects like the environment, possible antenna size, performance and interface. To avoid unpleasant surprises during software implementation phase, software has to be taken into account as well from the beginning. Different NFC IC categories (NFC Frontends, NFC Controller, Connected Tag) have different strengths, depending on the software environment. The way how highly integrated operating systems like Linux are structured brings both new challenges and advantages. This session examines the considerations necessary when designing in NFC in different operating systems or "bare metal" systems. It also discusses the advantages and disadvantages of the different device categories in dependence of the designated environment.
查看全文
This class will teach you how to spin a BLDC, PMSM or ACIM motor with KMS. You do not need prior motor control experience. You will use the KMS GUI to do motor tuning and MCUXpresso IDE to develop a stand-alone motor control project. Bring your own motor and we will test it with KMS. With your registration please indicate the voltage and max current of your motor.
查看全文
The rise of NFC is ongoing. Now that traditional markets such as mobile payment and contactless access are well-established, we see NFC creating new markets on its own and providing technological advancements that fuel a new wave of innovation. This session looks into new use cases for NFC. It will also be the first time NXP presents its next technological evolution for NFC.
查看全文
Automotive Advanced Analog Solutions  Emerging Trends & Innovation NXP Microcontroller Update Smart Machinery & Industrial Automation Hands-On Workshop: Secure Connection to Google Cloud IoT Core  Smart Networks & Computing Layerscape - Edge Computing  Smarter World Solutions & Multimode Connectivity Are You Ready for the Next i.MX Product Launch?  Hands-On Workshop: i.MX RT Cross-Over Processors  NXP Secure, Interface and Power Solutions  See What's Next on NFC Technology 
查看全文
Learn how to create a custom SDK for your specific hardware board featuring MCUXpresso SDK and config tools.
查看全文
Using our product demonstration and reference design, this class will teach you how to build your own cloud connected end node with our latest power-efficient LPC54018 flashless MCU. We will use Amazon Web Services (AWS).
查看全文
This class will provide an overview of the i.MX RT series, key peripheral, including a hands-on tutorial using the i.MX RT EVK.
查看全文
Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. To protect firmware execution given today’s threat landscape, there must be a policy to only allow execution of authenticated firmware. The methods used to enforce this policy rely on MCU security technology to create a protected boot flow. The boot firmware can contain public key cryptography to authenticate application code. In addition to these components integrated in the end device, there are tools and steps that must be taken in the manufacturing environment using manufacturing hardware for code signing and host programs for provisioning. Join this session to explore the design and implementation of a secure boot with i.MX RT.
查看全文
Introduction to the new i.MX 8 and 8X automotive applications processor product families and associated target applications, development tools, and software ecosystem.
查看全文
Introduction to Kinetis KW and Thread.
查看全文
Learn about NXP i.MX next-generation solutions (i.MX 7ULP, i.MX 8).
查看全文
This session will introduce the PMSM motor parameter measurement, tuning tools, FreeMASTER and motor control library as well as the configuration of a new PMSM. Get hands-on experience running the PMSM step-by-step and do some PMSM FOC tasks for testing.
查看全文
Whether you are looking for an easy and cost-efficient parametrization solution or want to use a smartphone for ad-hoc diagnosis of a device, Near-field-communication (NFC) makes this possible now. Or you might want to communicate with a fully sealed, battery-less device? Learn in this session about many new use cases, in which NFC simplifies handling, saves cost or enables features which were not possible before in industrial or healthcare applications. There are more possibilities than you would have imagined!
查看全文
This session shows how to optimize FreeRTOS™ applications using the MCUXpresso SDK and IDE, including tools as Segger SystemView and Percepio Tracealizer. The  session covers optimizing the RTOS with configuration settings, inspecting stack and run-time using NXP Kernel Awareness, streaming real time data using Segger RTT and SystemView and up to analyzing and optimizing system performance with RTOS and application trace.
查看全文