テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Understand the value, benefits and features  of Arm's latest Cortex-M33 core through a LPC5500-based product training and hand-on session.
記事全体を表示
EUF-NET-T1742 - This session provides an overview on the security technologies NXP offers to secure a system through two complementary technologies: 1) the Trust Architecture already present in QorIQ P- and T-series including Secure Boot and 2) the TrustZone® technology introduced in the ARM®-based QorIQ LS series processors. We will outline the motivations for offering these technologies in embedded processors and show how they can be complementary for making a final system “Trustable” in the sense it does what its users and suppliers expect it to do.
記事全体を表示
Learn about capabilities, contents of the kit and how to engage with third party supply kit, AutonomouStuff. Understand the target applications and the value proposition. Target Audience: Customers who are looking for rapid prototyping environment with a path to embedded automotive silicon for Level 2/3 autonomous driving systems.
記事全体を表示
Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. To protect firmware execution given today’s threat landscape, there must be a policy to only allow execution of authenticated firmware. The methods used to enforce this policy rely on MCU security technology to create a protected boot flow. The boot firmware can contain public key cryptography to authenticate application code. In addition to these components integrated in the end device, there are tools and steps that must be taken in the manufacturing environment using manufacturing hardware for code signing and host programs for provisioning. Join this session to explore the design and implementation of a secure boot by making use of the Arm mbed TLS open source software and protect against firmware attacks.
記事全体を表示
A complete family of versatile amplifier modules enabling rapid deployment of base station to address the ultra-low latency/high data rate needs of 5G Wireless Infrastructure equipment.
記事全体を表示
Full power helm! A new way to design your power system, focused on the “Plumbing”! A simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC. Examples with results will be discussed.
記事全体を表示
QorIQ platforms provide a rich set of features for embedding security and trust into networking, storage and industrial systems. Learn how you can leverage these features via several tools, APIs and drivers provided by NXP. Additionally, learn about our complete turn-key solutions for IoT and security appliances, and get to know our software services team, which can customize a solution for your specific use-case.
記事全体を表示
Anywhere you see a need for secure communications, you should think of Layerscape as a potential solution. Learn about NXP's Layerscape solutions portfolio and roadmap addressing industrial, gateways, automotive and all types of IoT applications. Learn about the latest developments and get a comprehensive view of Layerscape solutions. Catch a glimpse of the SOC and software roadmap that's under development.
記事全体を表示
EUF-NET-T1756 - This session will go over the RF solutions for the industrial and military market.
記事全体を表示
Secure Connected & Automated Vehicles ETAS: AUTOSAR Toolchain Overview General Overview of the i.MX 8 Family  Getting Ethernet on the Road  Green Hills Software: Trusted Software Foundation for Safe and Secure Automotive Systems on i.MX 8 and S32  i.MX 8QM/QX Security Capabilities  Lauterbach: Debug & Trace for New NXP i.MX 8 and S32 Automotive Processors  Leveraging i.MX 8 Hardware for Automotive Functional Safety Case Study of SafeAssure Display and Rear View Camera 
記事全体を表示
Learn from our experiences with thousands of Layerscape customers. We'll share tips and tricks we have learned through designing the NXP LS1012A, LS1043A and LS1046A products, as well as through assisting early adopters. These products are suited for cost and power conscious applications where high core performance and high integration is required. We will also review various tools services and support offered by NXP.
記事全体を表示
Overview of a platform solution that addresses the proliferation of Ethernet networks and enables new applications that will transform vehicles.
記事全体を表示
Combustion and motor control is moving to more computation-intensive techniques.  Hear about how the S32 Automotive platform will support this trend with Arm® NEON and math acceleration.
記事全体を表示
Want to know more about USB Type-C or Secure Authentication? Don't miss this slot.
記事全体を表示
This sessions give the participants a quick overview of what NFC is, what products are a part of portfolio and how can they be used in different use cases across several verticals. It also guides the participants through a quick overview of the development kits and SW resources available that come in handy for prototyping. In short, this is the best crash-course you can have to get started with NFC.
記事全体を表示
We will walk you through the key features of the LPC800 and LPC1100 product series and how these low-power, low-cost MCUs bring numerous advantages over your 8-bit architecture. In this session, we will discuss bridge from 8-bit to 32-bit applications using the LPC800 and LPC1100. Customers can expect 8-bit simplicity, real-time performance, and better code density with easy-to-use tools while maintaining lower power at a much lower cost. NXP delivers all the key ingredients that embedded engineers need for successful USB application development.
記事全体を表示
S32V234 vision product family introduction.
記事全体を表示
EUF-NET-T1743 - The QorIQ LS2085/88 are versatile Layerscape 2 devices. The GPP layer contains eight A57/A72 ARM® cores. The APP layer contains AIOP, PME, DCE and SEC engines. The WRPP layer contains WRIOP, SATA and PCIe engines. This presentation will give an overview of the various component and target use case for the QorIQ LS2085/88 processors.
記事全体を表示