テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Overview of NXP Kinetis new products, KE+, security with K8x & KL8x.  
記事全体を表示
The Kinetis KE1x family is the next generation MCU solution in the Kinetis E series. Designed with more memory, enhanced features and new IPs, this family extends the NXP 5 V portfolio to cover higher performance applications and use cases. Together with the Kinetis KE0x family for entry level MCUs, the Kinetis E family becomes an ideal solution for markets needing 5 V, robustness, and more flash size, providing platform solutions for low-end to high-end applications. Join this session to learn how the strong EMC performance across the Kinetis E family makes it suitable for main control and HMI (touch) in home appliances, industrial, and other applications needed in harsh electrical noise environments.  
記事全体を表示
MCU Alexa Voice, software and tools installation. Learn how to debug and develop code on the MCU all throughout to cloud enablement.
記事全体を表示
This class provides an introduction on the S32 Design Studio for Vision IDE with the new S32 Debugger and S32 Debug Probe. The lecture will provide an overview of the S32 Design Studio for Vision IDE with S32 Debugger and S32 Debug Probe along with a demonstration. Also, there will be a preview of the S32 Configuration Tool coming in the next generation S32 Design Studio.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
記事全体を表示
The i.MX 8M was designed with consumer and industrial customers in mind. The i.MX 8M series of processors are the first in a completely new paradigm of processors designed targeting market leading performance for audio, video and voice. The i.MX 8M starts with a system solution in mind and drives optimized solutions (best in class performance, optimized system cost, built with Google/Amazon/Msft ecosystems in mind) for many different customers from HMI, audio, video, voice, IOT, digital signage, printers, machine vision, etc. Best in class 4K video with HDR, best in class audio interfaces, low-power and optimized for lower cost. Come see what this new family of processors is all about and learn where we are headed.
記事全体を表示
EUF-HMB-T1750  - Wireless connectivity represents a fundamental aspect of the home automation applications we will see in a near future, local wireless connected nodes are the building block of a domestic network. During this session the presenter will introduce NXP Semiconductors relevant technology for the simple node up to the gateway towards the external world. The session will also have a focus on the security aspects that are becoming more and more important in the everything connected scenario.
記事全体を表示
Design, Software & Services APF-DES-T2274 - Kinetis KW and Thread  Insight & Innovation APF-INS-T2270 - Kinetis New Products, KE+, Security with K8x & KL8x  Secure Mobile, Healthcare & Wearables APF-MHW-T2232 - LPC541xx for Wearable
記事全体を表示
In electronic systems, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems or the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators and GPIO expanders are often used to bridge between the interconnects on the board. In this session, we will explore the application of these interface devices from NXP and discuss their applications in various customer systems.
記事全体を表示
The PF81 and PF82 PMIC family is designed for high-performance processing applications such as infotainment, telematics, clusters, vehicle networking, ADAS, vision and sensor fusion. It is ideal for i.MX 8, i.MX 8X, S32V, and Networking processors in Automotive, Industrial, and Consumer applications. In this session we will offer a detailed overview of the family, its features and advantages of scalability and functional safety
記事全体を表示
Security is fast becoming a hot topic in the automotive world, as a foundational element in building connected, and increasingly autonomous vehicles. From secure boot support to higher level functionality enabling leaner & cheaper SW upgrades and protecting OEM IP, you will find out in this session what will the i.MX 8 QM/QX offer as basis to build your secure solutions around it.
記事全体を表示
Amazon Alexa has changed voice control forever. Come learn about our i.MX based solutions for Amazon Alexa. Learn about our reference platforms, what are the key factors to consider when designing a voice control solution and see how easily you can add Alexa into your next-generation devices.
記事全体を表示
The session will discuss IoT and Thread/BLE solutions.
記事全体を表示
This session will examine the Freescale technologies best suited for use in-home portable medical applications. Specific examples will be referenced during the session. Based on Kinetis. Presented by: David Niewolny Presented at: FTF 2014 Session ID: FTF-HCR-F0214
記事全体を表示
This class will introduce Android Things, the new version of Android designed for the IoT market. The when, what and how of Android Things will be explained and how NXP has worked with Google™ to enable certified boards based on NXP silicon. A live demo of Android Things will be shown sampling and analyzing data real time via the cloud. Finally the relationship between Android Things, Google Voice Assistant and Chromecast will be explained and what NXP parts are most appropriate for optimal performance.
記事全体を表示