テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Learn how to create a custom SDK for your specific hardware board featuring MCUXpresso SDK and config tools.
記事全体を表示
Join this session to get a glimpse of where you will see i.MX 8/8X in the near future and why graphics, ML, AI, video, image processing, vision, connectivity, audio and voice functions make the i.MX 8 series ideal for Automotive and Industrial applications. Learn about the i.MX 8/8X families that are comprised of common subsystems establishing an unmatched range of performance scaling with pin-compatible options and the highest level of software reuse. In addition, learn more about the upcoming i.MX 8DualMax product line to help customers meet additional cost performance scaling across the i.MX 8 family.
記事全体を表示
This presentation will first highlights some basic training techniques, such as data augmentation, but the primary focus will be on various ways to deploy neural network frameworks and classical machine learning algorithms, and most importantly, utilizing a variety of open source tools and techniques. We will show how these techniques fit in with some real use cases such as object recognition and anomaly detection. The hands-on session portion of the class will allow attendees to take a trained neural network model and deploy it on a i.MX 8M. Attendees will utilize the Linux development environment and implement an end-to-end use case.
記事全体を表示
Join this session to understand all the security features integrated in the recently launched LPC5500 MCU Family and learn how to implement these features to design a low-power system with robust security.
記事全体を表示
Learn how to create a custom SDK for your specific hardware board featuring MCUXpresso SDK and config tools.
記事全体を表示
Partnering with Cypress and Murata, NXP now offers a full range of state of the art Wi-Fi and combo Wi-Fi/BLE solutions for every i.MX product. From low-power 802.11n for battery applications based on i.MX RT up to 802.11ac 2x2 for high performance audio/video streaming and automotive applications based on i.MX 8 and i.MX 8M. Drivers for Linux and FreeRTOS supported in Linux SDK and MCUXpresso SDK.
記事全体を表示
Introduction to A100x secure authenticator, authentication protocols, what to look for in security IC, and potential use cases.
記事全体を表示
In this session you will learn how to use Machine Learning fundamentals using Layerscape family of processors. The class will cover: Machine Learning fundamentals; Networks used for training and different models; Sample Object recognition training and Inference use case; Ease of use to use with LS platform for Machine Learning.
記事全体を表示
Learn how to use the LS1028A to quickly create industrial networks with TSN for deterministic, redundant communications.
記事全体を表示
2019 is forecasted to be the year that voice will move beyond smart speakers to all segments of the IoT/industrial market. In this class we will give an overview of different architectures and solutions that can be implemented based on NXP processors.
記事全体を表示
Extend your logistics track and trace with condition insights. NTAG SmartSensor enables sensing and logging with NFC readout. NTAG SmartSensor enables your IOT application for smart logistics, smart healthcare, drug delivery and smart packaging.
記事全体を表示
Completing a production-ready smart charging or resonant converter design can be tricky, tedious, and even challenging for many engineers. 1. Purpose of this training is to discuss design of smart charging: Introduce smart power design tools to address design challenges in order to improve conversion. 2. Resonant converters: Highlight key elements a designer needs to understand in order to effectively design a resonant converter. An online based resonant converter design tool is introduced to further help resonant converter design.
記事全体を表示
Graphics on the i.MX RT lab material. The i.MX RT series supports product designs that include advanced multimedia for GUI and enhanced human machine interface (HMI) experience. Its features include advanced 2D graphics acceleration engine, LCD display controllers, camera sensor interfaces, and audio interfaces for high-performance, multi-channel audio streaming. Join this session to learn how to develop graphics on i.MX RT. The attendees in this class will leave with an i.MX RT1060 board on behalf of Digi-Key.
記事全体を表示
Creating Graphics on the i.MX RT1060 lab material. The i.MX RT series supports product designs that include advanced multimedia for GUI and enhanced human machine interface (HMI) experience. Its features include advanced 2D graphics acceleration engine, LCD display controllers, camera sensor interfaces, and audio interfaces for high-performance, multi-channel audio streaming. Join this session to learn how to develop graphics on i.MX RT. The attendees in this class will leave with an i.MX RT1060 board on behalf of Digi-Key.  
記事全体を表示
If you find yourself in need of using a low cost co-processor to act as a communications hub, why not consider a GPIO expander?  With the features in our latest GPIO expanders, this device can almost mimic a low cost MCU while being more cost-effective and reducing the complexity of your system. Come learn about the features and benefits, and actually see the GPIO expander in action on a simple PCB you’ll experiment with in this class.
記事全体を表示
When choosing the NFC device for a new design, the system architect must consider many parameters. Usually a strong focus is put on hardware specific aspects and software aspects are often grossly underestimated. To avoid unpleasant surprises during software implementation phase, software has to be taken into account as well from the beginning. Different NFC IC categories (NFC Frontends, NFC Controller, Connected Tag) have different strengths, depending on the software environment. The way how highly integrated operating systems like Linux are structured brings both new challenges and advantages. This session examines the considerations necessary when designing in NFC in different operating systems or "bare metal" systems. It also discusses the advantages and disadvantages of the different device categories in dependence of the designated environment.
記事全体を表示
Security is critical to the growing market for IoT-enabled devices: There were already more than 5 billion connected devices in the world last year, and use is expected to grow to 12 billion by 2020. To support this rapid expansion, prominent internet players, including Alibaba, AWS, Google, IBM and Microsoft are establishing their own cloud services and industrial suppliers are moving quickly to broaden their private cloud offerings. At NXP, we believe strong security doesn't have to be hard to work with. Our "Plug & Trust" approach simplifies the implementation of strong security mechanisms in today's IoT devices. NXP's latest A71CH provides just this level of Plug & Trust IoT Security and delivers proven, chip-to-cloud security right out of the box, enabling every customer to secure IoT devices and safely connect to IoT clouds and services without writing security codes or exposing keys.
記事全体を表示
Learn how to create an IoT proof-of-concept in real time without writing any C code. Skeptical? Rapid IoT combines processing, connectivity, sensing and security with an easy to use web IDE. The presentation and live demo walks you through creating a simple IoT solution including embedded, mobile and cloud applications. The demo lab will focus on use cases such as anomaly detection and vertical applications.
記事全体を表示
Join Rob Diebold and Mark Melone from NuCurrent to learn about the technical landscape of wireless charging along with practical guidance on how to move it from concept into production. This session will provide an overview of wireless charging technologies with an emphasis on charging solutions that utilize Qi and NFC Direct Charging. Several demonstrations that combine NXP and NuCurrent technologies will be provided along with a Q&A session with subject matter experts.
記事全体を表示
Join this session to get a glimpse of where you will see i.MX 8/8X in the near future and why graphics, ML, AI, video, image processing, vision, connectivity, audio and voice functions make the i.MX 8 series ideal for Automotive and Industrial applications. Learn about the i.MX 8/8X families that are comprised of common subsystems establishing an unmatched range of performance scaling with pin-compatible options and the highest level of software reuse. In addition, learn more about the upcoming i.MX 8DualMax product line to help customers meet additional cost performance scaling across the i.MX 8 family.
記事全体を表示