テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
2019 is forecasted to be the year that voice will move beyond smart speakers to all segments of the IoT/industrial market. In this class we will give an overview of different architectures and solutions that can be implemented based on NXP processors.
記事全体を表示
With its broad portfolio, NXP is uniquely positioned to propose a full system allowing a scalability from NCAP to L4/L5 autonomous driving. To address such scalability, NXP has faced some challenging decisions about the system partitioning, performance, safety decomposition, AI Acceleration and Programming language. All these challenges will be addressed during the session.
記事全体を表示
NXP recently announced its first Azure Sphere-certified crossover applications processor chip, the i.MX 8ULP-CS SoloLite with Azure Sphere, and plans to build additional Azure Sphere-certified chips as part of the NXP i.MX 9 series. Join this tech talk to learn about Azure Sphere and what it means to have a highly secured solution from the hardware to the cloud. We’ll discuss the specific challenges of building and securing connected devices and what sets the i.MX 8ULP-CS apart. We’ll dig into the four components of Azure Sphere, all of which are included with the i.MX 8ULP-CS: Microsoft Pluton on NXP EdgeLock™ secure enclave for a secured hardware root of trust, the secured Azure Sphere OS, the cloud-based Azure Sphere Security Service, and the ongoing OS updates and security improvements supported by Microsoft experts for the lifetime of the device. Presenters: Sudhanva Huruli, Program Manager, Azure Sphere Naama Bak, Business Development and IoT Security, NXP Semiconductors
記事全体を表示
S32K11x, S32K14x product and solution, migration to future S32K products.
記事全体を表示
Join this session for an introduction of Alango’s voice enhancement software used to create high-performance speakerphones and headphones based on NXP’s i.MX RT MCUs. You’ll learn about Extended Voice Communication Package (eVCP), a universal package adaptable to different speakerphone designs (form-factors) that provides high-grade noise reduction and seamless duplexity. In addition, you’ll learn about VoiceDefender, a four microphone voice acquisition and processing package that provides clear voice transmission for on/over ear headphones. Presenters: Robert Schrager, Director of Sales and Marketing, Alango Brendon Slade, MCU Ecosystem Director, NXP
記事全体を表示
S32V234 vision product family introduction.
記事全体を表示
The i.MX RT10xx MCU family leverages high performance, extensive memory options, and security features aimed at protecting your IP. IP protection is a key concern for companies developing products based on embedded devices and these concerns may seem particularly troubling when working with external memories and board level programming facilities. This webinar explores how to utilize key security features during the production process to alleviate these concerns when developing with the i.MX RT10xx MCUs. The session will showcase the Cyclone production programmers available from PEmicro, the development workflow enabling the creation of an encrypted stand-alone programming (eSAP) image with the Secure Boot Utility, and establishing a secure connection to the device for provision and programming. Presenters: Clark Jarvis, Ecosystem Product Marketer, NXP Kevin Perreault, President, PEmicro
記事全体を表示
The biggest challenge in embedded GUI development is managing changes in design (iterations) that nearly all projects encounter. Historically, changes at the design level resulted in teams needing to hunt for and replace all changed assets manually within the project. This would result in development delays, changes being missed, coded behavior being lost, and ultimately, poor UX. Join this session to learn how customers from medical to automotive have leveraged Storyboard’s Rapid Design Import and Iteration Technology to streamline design changes and develop embedded GUI applications that provided outstanding user experiences while getting to market on a tight deadline. Presenters: Garry Clarkson, FAE, Crank Software Shelby Unger, MCU Ecosystem Product Marketer, NXP
記事全体を表示
If you find yourself in need of using a low cost co-processor to act as a communications hub, why not consider a GPIO expander?  With the features in our latest GPIO expanders, this device can almost mimic a low cost MCU while being more cost-effective and reducing the complexity of your system. Come learn about the features and benefits, and actually see the GPIO expander in action on a simple PCB you’ll experiment with in this class.
記事全体を表示
Controller area network (CAN) is used to create robust and flexible networks in applications such as industrial automation, motor control, and many others. To take full advantage of CAN, a higher-level protocol like CANopen FD is needed. Join this session to learn how EmSA’s CANopen FD stacks in the MCUXpresso SDK can be combined with other middleware components to create custom applications. We will discuss the steps taken to create an application where acceleration data from an LPC55S16 EVK is transferred to and visualized on an i.MX RT1064 EVK. Presenters: Olaf Pfeiffer, President, EmSA Shelby Unger, MCU Ecosystem Product Marketer, NXP
記事全体を表示
Presented by LIANG PING Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
記事全体を表示
Presented by Cao Nan, Nanjing Normal University Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
記事全体を表示
Ensuring that valuable IP is protected throughout the product lifecycle can help bring peace of mind and prevent loss of business revenue. This webinar will provide an overview of the security features available on the LPC5500 MCU series from NXP and how they can be leveraged as part of the manufacturing process. EPS Global, a worldwide provider of IC programming and secure provisioning services, will discuss the value these security features bring to IP protection and outline the manufacturing flows available for the LPC5500 MCU series to deliver end-to-end security throughout the product’s lifecycle, from design, and throughout the manufacturing supply chain. Presenters:  Clark Jarvis, Ecosystem Product Marketer, NXP Brian Colgan, Field Applciation Engineer, EPS Global
記事全体を表示
Presented by Taki Chow, Advantech Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
記事全体を表示
In this session attendees will learn how to use the FreeMASTER tool to debug and develop a real time control loop - balancing an inverted pendulum using the new i.MX RT1176 crossover MCU on Embedded Artists' i.MX RT1176 MCU-based Developer's Kit. Presenters: Anders Rosvall, Technical Director, Embedded Artists Brendon Slade, MCU Ecosystem Director, NXP
記事全体を表示