S32K知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K Knowledge Base

标签

讨论

排序依据:
To accelerate S32K demand creation and support urgent evaluation requriement in Great China, we build one batch boards locally. These boards will only be given out to our potential opportunities for free. The boards are made by China local partner and verified by AE and FAE team. if you have any question on this kind of board, please go to China Auto CAS or Auto MCU marketing for support. 1. Board overview   2. Pinout 3. Test point 4. Block diagram 3. The main difference between NXP official S32K EVB and this FRDM-S32K144 board are OpenSDA firmware and CAN PHY The original OpenSDA firmware in this board is from MBED which is not supported by S32DS, thus we need to change to PEmicro OpenSDA firmware, and then we can use S32DS for development.   Unplug the USB cable (if attached). Press and hold the Reset button. Plug in a USB cable from a USB Host to the OpenSDA USB port. Release the RESET/Bootloader button. A removable drive will be visible in the host file system with a volume label of BOOTLOADER. Drag/drop or copy/paste attached firmware “DEBUG-FRDM-K64F_Pemicro_v108a_for_OpenSDA_v2.0.bin” into the removable drive. Unplug the USB cable and plug it in again. The OpenSDA application should now be running. The CAN physical is different. This board used standalone CAN PHY but not CAN SBC. Please refer SCH file for debug.   Original Attachment has been moved to: dmeo2.rar
查看全文
******************************************************************************************************************************************** Detailed Description: This example shows use of RTC in VLPS mode. The MCU is put into the VLPS mode (Sleep-On-Exit). RTC alarm interrupt brings it to VLPR every 3s and toggles BLUE LED (PTD0). Since it works in the Sleep-On-Exit mode, after the ISR, the MCU goes to VLPS again without calling the WFI instruction. When BTN0 (S32K144 EVB) is pressed, the power mode switch from VLPS to VLPR and other way round. Interrupt is triggered on rising edge (PTC12), filtered by digital filter (clocked from LPO). In VLPR, RTC seconds interrupt is enabled as well and toggles RED LED (PTD15) in the ISR. RTC_CLKOUT (1Hz) and CLKOUT (bus_clk) can be monitored at PTD13 and PTD14 respectively. CLKOUT is not available in VLPS. The MCU needs to be power-cycled and run stand-alone. -------------------------------------------------------------------------------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100 MCU: S32K 0N57U Debugger: S32DS_ARM_2.2, OpenSDA Target: internal_FLASH ********************************************************************************************************************************************
查看全文
[RTD400 LLD]K344 Center Aligned PWM Trigger ADC BCTU 1. Abstract     Not long ago, a customer's actual project needed to implement the high-level center point of the center-aligned PWM on the S32K3XX to trigger the ADC BCTU multi-channel sampling. This function requires the use of EMIOS, ADC, and BCTU. At the beginning, the customer was always unable to achieve the trigger at the center point of the PWM, and the trigger position was wrong. Later, After we give the explanation and analysis of the principles of the K3 related modules to the customer, as well as the guidance of the actual code configuration test, and the customer also achieved the required function. For the convenience of testing, PIT and UART printf functions are also added here. So here is a summary of the specific situation of this function, so that other customers who encounter similar functional requirements in the future can have a reference and can quickly build it. The requirements are as shown in the figure below. In the up-down counting mode, the center-aligned PWM is output, and the trigger sampling of the ADC BTCU LIST is realized at the center point of the high level. This article will implement 1KHZ center-aligned PWM, 50% duty cycle, and high-level center point to achieve ADC BTCU LIST sampling on the official S32K344-EVB board, based on the RTD400 LLD version.   kerryzhou_12-1737802508258.png Fig 1 2. Center-aligned PWM center point trigger ADC principle       Regarding the principle, there is no suspense about ADC. You can directly refer to the previous article on ADC software and hardware triggering: [RTD400 LLD]K344 ADC SW+HW trigger This is the structure shown in Figure 2. After configuring ADC, BCTU and select the triggered EMIOS channel. When the relevant flag of EMIOS is generated, BCTU will be triggered. After the watermark is reached, a notification will be generated to store all LIST ADC channel values ​​in the buffer, and then the ADC value can be printed out for easy viewing according to the situation.  kerryzhou_13-1737802525461.png   Fig 2 In the current working condition, the logic that needs to be concerned about is mainly: how to generate center-aligned PWM, how to generate a flag at the high-level center point, and use this flag to trigger BTCU sampling. 2.1 How to generate center-aligned PWM      First, let’s take a look at the channel status of EMIOS and the channel status that supports center-aligned PWM. kerryzhou_14-1737802545570.png  Fig 3 The center-aligned PWM mode is: OPWMCB As shown in Figure 1, we can see that the counter count mode in this mode is up and down. Let's take a look at the channel types that support OPWMCB. We can see that there is only type G.  kerryzhou_15-1737802657145.png  Fig 4 So, what are the channels supported by Type G? See the figure below: kerryzhou_16-1737802660362.png  Fig 5 The mystery is solved. Only CH1-CH7 of eMIOS supports center-aligned PWM. Well, then a new question arises. Can this mode directly generate a trigger signal at the center point of the PWM high level to trigger the ADC BCTU sampling? Answer: No! The reason can be seen from Figure 1. In this PWM mode, there are two trigger flags generated when the up and down count comparison is completed. Therefore, if this mode channel is used to directly trigger ADC sampling, two triggers will be generated in one cycle, and both are on the edge of PWM. Since OPWMCB cannot directly generate a trigger at the center point of PWM, how to achieve it? In addition, open a dedicated channel, and the clock source is the same as OPWMCB, but that channel only counts to generate trigger flags and does not output any waveform. 2.2 How to generate PWM center point trigger flag   Key information: OPWMCB simultaneous clock source, only counting mode, or up and down MCB mode, only one channel is satisfied: ADC CH0, counter bus type also needs to be selected as counter_bus_B      kerryzhou_17-1737802664429.png  Fig 6 Let's take a look at the trigger flag of MCB: kerryzhou_18-1737802668518.png  Fig 7 As you can see, it is perfect. The trigger mark is at the top of the upward and downward counting, which is exactly the center point of the high level of the same source PWM. So, here, the specific channel arrangement has been determined in principle, two channels: EMIOS0_CH0 MCB mode pure counting and triggering the generation of flags to trigger ADC sampling; EMIOS0_CH1-CH7 is OPWMCB mode, simply outputting center-aligned PWM. 3. Software configuration and implementation       The software uses the S32K3 RTD400 version, and other versions have similar configurations! 3.1 Demo CT  module configuration First, you need to prepare a K344 demo, and then configure the pins, clocks, and peripheral modules. The following will explain the configurations. The modules used are: 2 GPIOs, ADC, BCTU, EMIOS clock, EMIOS PWM, LPUART for printing logs, PIT for timed printing, Trgmux is configured but not used in this article, so I won't talk about it!      3.1.1 Pin configuation       The pins used are as follows: kerryzhou_19-1737802674350.png  Fig 8 The two GPIOs are used to toggle in BCTU trigger notification and BCTU watermark notification respectively, to test the waveform positioning. ADC1_s10 pin is used for ADC1, but this article mainly uses BCTU to combine ADC0. ADC0 does not add specific external pins, but uses internal signals. LPUART is used for printing, and EMIOS0_CH1 is used to generate center-aligned PWM waveforms. 3.1.2 Clock configuration      The clocks that need to be paid attention to here are: ADC clock, EMIOS clock, UART clock, and PIT clock. kerryzhou_20-1737802679200.png  Fig 9 These clocks will be used later when configuring specific timing periods and baud rates. 3.1.3 Peripheral configuration       The peripherals used mainly include the following modules: kerryzhou_21-1737802684346.png  Fig 10 (1)Adc_Sar_Ip The configuration of the ADC0 module uses the one shot mode, that is, one conversion is generated after one trigger. In this way, the timer EMIOS channel can be used to generate trigger conditions to trigger a conversion. Pre-sampling is enabled to prevent the residual charge of the sampled value of the previous channel from affecting the result of the current channel and causing deviation of the ADC value. The trigger mode uses BCTU. For the configuration of Adc prescaler value and calibration prescale, the frequency division requirements in RM need to be met. The final configuration is as follows: kerryzhou_22-1737802689462.png  Fig 11  kerryzhou_23-1737802693578.png   Fig 12 (2)Bctu_Ip The configuration of Bctu_Ip needs to select the right EMIOS channel to use. From the above principle, we can know that EMIOS0_CH0 is used, and then LIST mode is adopted. For ADC0, three internal channels are currently added to the LIST: BANDGAP, VREFL, VREFH. The specific configuration is as follows: kerryzhou_24-1737802696994.png  Fig 13  kerryzhou_25-1737802702313.png  Fig 14 (3)Emios_Mcl_Ip Here we need to consider the PWM cycle that needs to be generated. The goal is to generate a 1Khz center-aligned PWM, so the EMIOS mode is the MCB up-down counting mode. The clock cycle formula for MCB is: (2 x AS1) – 2. So for the EMIOS0 clock source of 160Mhz, what is the corresponding 1KHZ counter? First do 160 divide to get 1Mhz, and then calculate according to (2 x AS1) – 2: (2 x AS1) – 2 = 1Mhz/1KHZ=>AS1=1000/2 +1= 501. The configuration is as follows: kerryzhou_26-1737802711894.png  Fig 15 (3)Emios_Pwm The previous principle analysis shows that the PWM uses the OPWMCB center-aligned mode PWM, the clock comes from the counter bus B of EMIOS CH0, then the period is 1khz, and the duty cycle is 50%. The specific configuration is as follows: kerryzhou_27-1737802722172.png  Fig 16 (4)Lpuart_Uart Configure UART6 clock baud rate to 115200.  kerryzhou_28-1737802726379.png  Fig 17 (5)Pit  kerryzhou_29-1737802729584.png  Fig 18 (6)IntCtrl_Ip The interrupt configuration is as follows, and it can actually be configured via code. kerryzhou_30-1737802734820.png  Fig 19 3.2 Main code situation After the configuration is completed, the output of the center PWM and the sampling of the ADC BCTU can be realized by calling the following code in main. #include "Clock_Ip.h" #include "IntCtrl_Ip.h" #include "Adc_Sar_Ip.h" #include "Bctu_Ip.h" #include "Siul2_Port_Ip.h" #include "Pit_Ip.h" #include "Siul2_Dio_Ip.h" #include "Trgmux_Ip.h" #include "Lpuart_Uart_Ip.h" #include "Lpuart_Uart_Ip_Irq.h" #include "string.h" #include "stdio.h" #include "retarget.h" #include "Emios_Mcl_Ip.h" #include "Emios_Pwm_Ip.h" /* PIT instance used - 0 */ #define PIT_INST_0 0U /* PIT Channel used - 0 */ #define CH_0 0U /* PIT time-out period - equivalent to 1s */ #define PIT_PERIOD 40000000 static volatile uint8 toggleLed = 0U; #ifdef ADC_3V3_VREF_SELECTED #define ADC_BANDGAP 5980U /* Vbandgap ~ 1.2V on 14 bits resolution, 3.3V VrefH */ #else #define ADC_BANDGAP 3932U /* Vbandgap ~ 1.2V on 14 bits resolution, 5V VrefH */ #endif #define ADC_SAR_USED_CH 48U /* Internal Bandgap Channel */ #define BCTU_USED_SINGLE_TRIG_IDX 0U #define BCTU_USED_FIFO_IDX 0U #define BCTU_FIFO_WATERMARK 3U #define ADC_TOLERANCE(x,y) (((x > y) ? (x - y) : (y - x)) > 200U) /* Check that the data is within tolerated range */ #define LED_Q172_PIN 13u #define LED_Q172_PORT PTA_H_HALF #define GPIO_PTA2_PIN 2u #define GPIO_PTA2_PORT PTA_L_HALF #define EMIOS_INST0 0U volatile int exit_code = 0; volatile boolean notif_triggered = FALSE; volatile boolean notif_triggered1 = FALSE; volatile uint16 data; volatile uint16 data1; volatile uint16 data_bctu[3]; #define UART_LPUART_INTERNAL_CHANNEL 6 #define WELCOME_MSG_1 "Hello, This message is sent via Uart!\r\n" volatile Lpuart_Uart_Ip_StatusType lpuartStatus = LPUART_UART_IP_STATUS_ERROR; uint32 remainingBytes; uint32 T_timeout = 0xFFFFFF; uint8* pBuffer; extern void Adc_Sar_0_Isr(void); extern void Bctu_0_Isr(void); extern void Adc_Sar_1_Isr(void); void AdcEndOfChainNotif(void) { notif_triggered = TRUE; data = Adc_Sar_Ip_GetConvData(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_USED_CH); /* Checks the measured ADC data conversion */ } void AdcEndOfChainNotif1(void) { notif_triggered1 = TRUE; data1 = Adc_Sar_Ip_GetConvData(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, 34); /* Checks the measured ADC data conversion */ } void Pit0ch0Notification(void) { toggleLed = 1U; } void BctuWatermarkNotif(void) { uint8 idx; Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 1U); notif_triggered = TRUE; for (idx = 0u; idx < BCTU_FIFO_WATERMARK; idx++) { data_bctu[idx] = Bctu_Ip_GetFifoData(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_USED_FIFO_IDX); } Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); } void BcutTriggerNotif() { Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 1U); Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 0U); } void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } int main(void) { StatusType status; uint8 Index; Clock_Ip_StatusType clockStatus; /* Initialize and configure drivers */ clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); while (clockStatus != CLOCK_IP_SUCCESS) { clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); } Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); #if 1 Bctu_Ip_Init(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &BctuHwUnit_0_BOARD_INITPERIPHERALS); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_0_BOARD_InitPeripherals); while (status != E_OK); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_1_BOARD_InitPeripherals); while (status != E_OK); /* set PIT 0 interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(PIT0_IRQn); /* Install and enable interrupt handlers */ IntCtrl_Ip_InstallHandler(ADC0_IRQn, Adc_Sar_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(BCTU_IRQn, Bctu_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(ADC1_IRQn, Adc_Sar_1_Isr, NULL_PTR); IntCtrl_Ip_EnableIrq(ADC0_IRQn); IntCtrl_Ip_EnableIrq(BCTU_IRQn); IntCtrl_Ip_EnableIrq(ADC1_IRQn); // IntCtrl_Ip_EnableIrq(EMIOS0_5_IRQn); /* Call Calibration function multiple times, to mitigate instability of board source */ for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); /* Start a SW triggered normal conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_NORMAL); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; /* Start a SW triggered injected conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_INJECTED); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; #endif /* Initialize PIT instance 0 - Channel 0 */ Pit_Ip_Init(PIT_INST_0, &PIT_0_InitConfig_PB_BOARD_InitPeripherals); /* Initialize channel 0 */ Pit_Ip_InitChannel(PIT_INST_0, PIT_0_CH_0); /* Enable channel interrupt PIT_0 - CH_0 */ Pit_Ip_EnableChannelInterrupt(PIT_INST_0, CH_0); /* Start channel CH_0 */ Pit_Ip_StartChannel(PIT_INST_0, CH_0, PIT_PERIOD); // Trgmux_Ip_Init(&Trgmux_Ip_xTrgmuxInitPB);// Lpuart_Uart_Ip_Init(UART_LPUART_INTERNAL_CHANNEL, &Lpuart_Uart_Ip_xHwConfigPB_6_BOARD_INITPERIPHERALS); Emios_Mcl_Ip_Init(EMIOS_INST0, &Emios_Mcl_Ip_0_Config_BOARD_INITPERIPHERALS); Emios_Pwm_Ip_InitChannel(EMIOS_PWM_IP_BOARD_INITPERIPHERALS_I0_CH1_CFG, &Emios_Pwm_Ip_BOARD_InitPeripherals_I0_Ch1); printf("S32K344 PIT TRIGMUX ADC demo RTD400.\r\n"); /* Uart_AsyncSend transmit data */ lpuartStatus = Lpuart_Uart_Ip_AsyncSend(UART_LPUART_INTERNAL_CHANNEL, (const uint8 *) WELCOME_MSG_1, strlen(WELCOME_MSG_1)); /* Check for no on-going transmission */ do { lpuartStatus = Lpuart_Uart_Ip_GetTransmitStatus(UART_LPUART_INTERNAL_CHANNEL, &remainingBytes); } while (LPUART_UART_IP_STATUS_BUSY == lpuartStatus && 0 < T_timeout--); Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); while(1) { #if 1 if( toggleLed == 1) { toggleLed = 0; printf("ADC0_bandgap ch48 data_bctu = %d .\r\n", data_bctu[0]); printf("ADC0_vrefl ch54 data_bctu = %d .\r\n", data_bctu[1]); printf("ADC0_vrefh ch55 data_bctu = %d .\r\n", data_bctu[2]); } #endif } return exit_code; } 3.3 Test result    The test results include two parts: the printed results show the ADC sampling value, and the relationship between the PWM output and the BCTU trigger position. The printed results are as follows, and you can see that the values ​​of the three different ADC channels are correct: kerryzhou_31-1737802747820.png  Fig 20 PWM wave test result is: Ch1:PTB13 PWM Ch2:PTA29 BCTU trigger notification Ch3: PTA2 BCTU watermark notification kerryzhou_33-1737802767062.png   Fig 21 From the figure, we can see that the first BCTU trigger is at the center point of the PWM high level, and the BCTU watermark notification is used to store data after the ADC sampling is triggered three times. Here is another waveform to view the PWM cycle: kerryzhou_34-1737802770654.png  Fig 22 It can be seen that the PWM period is 1Khz, the duty cycle is 50%, and the first trigger of BCTU is at the center of the PWM high pulse. 4. Summary and trip description Through the above configuration, the RTD400 LLD method was finally used on the S32K344-EVB to implement a 1Khz, 50% duty cycle center-aligned PWM, and the high pulse center position triggered the ADC BCTU LIST acquisition. The trip encountered were my own configuration problems. At the beginning, I mistakenly thought that the watermark configuration value was consistent with the number of LIST channels. In fact, the watermark trigger is triggered only when the watermark value is exceeded. Therefore, if it is a 3-channel LIST, the watermark needs to be configured as 2, not 3. If it is 3, the test waveform is as follows: kerryzhou_35-1737802774543.png Fig 23 As you can see, the watermark notification is actually generated after it is triggered 4 times. Therefore, remember to match the FIFO number of the watermark. Attachment: 1. S32K344_centerPWM1k_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip Center PWM triggered BCTU LIST   2.S32K344_CPWM1k_TRIGMUX_BCTUHWLIST_EMIOSch4_ADC_printf_RTD400.zip PWM emios0_ch4 falling edge trigger the BCTU, for the comment situation.   3. Another method of center trigger: MCB_Counter up. Emios0_CH0 as the counter bus EMIOS0_CH1 as the PWM output EMIOS0_CH2 as the center trigger, but no PWM output, OPWMB S32K344_NCPWM1k1_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip
查看全文
This page supports the NXP Tech Days training session AUT-T4978 for "Hands-On Workshop: The Safety Peripheral Driver in the S32K3 - The Next Level to Achieve Safety". The full installation pre-requisites are attached below, as well as the required S32DS demo application project.
查看全文
Hi Everyone, Here I'd like to share three S32K1xx SDK FlexCAN PD and PAL component sample projects to demonstrate its basic and advanced features: 1. S32K144_CAN_PAL_SamplePrj_Basic_TxRx_ID_FiltersConfig_SDKRTM3P0 34.png Functions implementation key points and tips: This sample project is made to demonstrate the following S32K1xx FlexCAN features with SDK FlexCAN PAL driver: 1. Configure to receiver the following exact 16 standard ID CAN message with RxFIFO 8x ID filter table with format type-B(2x 16-bit ID) Standard ID: 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x111, 0x222, 0x333, 0x444, 0x555, 0x666, 0x777, 0x788 The RxFIFO is configured to use CPU interrupt for CAN message receive, and CAN_PAL cannot support DMA for RxFIFO directly. Note: A. FlexCAN of S32K1xx dose not support to receive CAN-FD message frame with RxFIFO, so no CAN-FD support in this demo project. B. All the filter table elements must be configured to contain only standard or extend ID, if it contains both standard and extend ID, the IDE-bit mask will be ignored.  C. After RxFIFO enabled, MB0~MB5 is used as the RX FIFO, at least MB6~MB7 are used as the ID filter table(to store the acceptance ID), the actual available MB number is determined by RxFIFO ID filter table size, details please refer to section--55.4.6 Rx FIFO structure of S32K1xx RM Rev.12.1  2. Configure two extra individual MBs to receive: RX_MB1: 16 standard ID CAN 2.0 message with the lower 4LSB masked(mask=0x7F0, acceptance ID = 0x123): 0x120 ~ 0x12F and  RX_MB2: 4 standard ID CAN 2.0 message with the ID8 and ID9 masked(mask=0x4FF, acceptance ID = 0x256): 0x056, 0x156, 0x256 and 0x356 Both the RxFIFO and individual MBs RX use non-blocking receive method/API with MB TX/RX complete ISR callback installed to set a new circle buffer for next message frame receive 3. Configure one individual MB to blocking transmit a standard CAN 2.0 message with ID = 0x100 periodically(period = 5ms), and also send back the received CAN messages(if it's available) to the CAN bus as a response. 4. Provide the FlexCAN bus-off manual recovery configuration API and interrupt ISR callback codes for reference, changing the macro CAN_BUSOFF_RECOVERY_MANUAL(in include/Config.h) to select the bus off recovery method(enable the macro definition: manual recovery, comment the macro definition: automatic recovery); Note: In this sample project, the macro CAN_BUSOFF_RECOVERY_MANUA is commented by default, so manual recovery codes does not work. To make the bus-off recovery callback work, user should replace the flexcan PD driver codes and S32K144_feature.h with S32K1xx RTM 4.0.0(which can be downloaded from nxp.com with registered account login and then installed stand-alone or installed via S32DS v3.3 IDE update). This is not done this sample project!!!  5. There 3 on-board RGB LED are used to indicate the FlexCAN working status: red RGB LED will be toggled after RXFIFO received a CAN message; blue RGB LED will be toggled after individual MB received a CAN message; green RGB LED will be turn ON after enter bus-off and turn OFF after exist bus-off(recover successfully). To run this sample project, the following HW and SW require: SW: S32DS for ARM v2.2 IDE with S32K1xx SDK RTM 3.0.3 installation HW: S32K144EVB-Q100 Rev.C with a DC-12V adapter for its power supply by J16 and a USB-to-CAN adapter(such as PEAK CAN) to connect PC with J13 of the EVB 2.S32K144_CAN_PAL_CANFD_ClassicCAN_Mix_TxRx_Wakeup_SDKRTM3P0 39.png Functions implementation key points and tips: This sample project is made to demonstrate the following S32K1xx FlexCAN features with SDK FlexCAN PAL driver: 1. Configure to enable CAN-FD with 500 Kbit/s arbitration phase bitrate and 2Mbit/s data phase bitrate, so it can support both classic CAN 2.0 A/B and CAn-FD message frame transfer. Note: A. The RxFIFO is disabled to work with CAN-FD message frame. B. After CAN-FD enabled, CAN-FD message frame data length can support up to 64 Bytes, so the actual available MB number is determined by the max frame data length need to support, details please refer to section--55.4.5 FlexCAN message buffer memory map of S32K1xx RM Rev.12.1  C. In order to support bitrate bigger than 1Mbit/s for CAN-FD data phase with bitrate switch enabed, PE clock source of CAN_PAL should be configured to use peripheral clock(80MHz generated from SPLL) instead of 8MHz oscillator clock; 2. Configure 3 individual MBs to receive: RX_MB0: 16 extend ID CAN 2.0/FD message with the lower 4LSB masked(mask=0x1FFFFFF0, acceptance ID = 0xfff021): 0xfff020 ~ 0xfff02F RX_MB1: 16 standard ID CAN 2.0/FD message with the lower 4LSB masked(mask=0x7F0, acceptance ID = 0x123): 0x120 ~ 0x12F RX_MB2: 4 standard ID CAN 2.0/FD message with the ID8 and ID9 masked(mask=0x4FF, acceptance ID = 0x256): 0x056, 0x156, 0x256 and 0x356 Both the RxFIFO and individual MBs RX use non-blocking receive method/API with MB TX/RX complete ISR callback installed to set a new circle buffer for next message frame receive 3. Configure 3 individual MBs to transmit: TX_MB0: send back any CAN(2.0/FD) messages received from RX_MB0; TX_MB1: send back any CAN(2.0/FD) messages received from RX_MB1; TX_MB2: send back any CAN(2.0/FD) messages received from RX_MB2; 4. Configure one individual MB(TX_MB3) to blocking transmit a standard CAN FD message with ID = 0x100 periodically(period = 5ms) and length = 64 bytes, and also send back the received CAN messages(if it's available) to the CAN bus as a response. 5. Provide the FlexCAN bus-off manual recovery configuration API and interrupt ISR callback codes for reference, changing the macro CAN_BUSOFF_RECOVERY_MANUAL(in include/Config.h) to select the bus off recovery method(enable the macro definition: manual recovery, comment the macro definition: automatic recovery); Note: In this sample project, the macro CAN_BUSOFF_RECOVERY_MANUA is commented by default, so manual recovery codes does not work. To make the bus-off recovery callback work, user should replace the flexcan PD driver codes and S32K144_feature.h with S32K1xx RTM 4.0.0(which can be downloaded from nxp.com with registered account login and then installed stand-alone or installed via S32DS v3.3 IDE update). This is not done this sample project!!!  6. Provided the sample codes of how to configure FlexCAN as the VLPS low-power mode wakeup source, RXD of FlexCAN0 is configured as GPIO IRQ interrupt with falling edge trigger before entering VLPS mode, and after wakeup, re-configure it back to RXD function. Note: A. S32K1xx FlexCAN is unable to work as the VLPS wakeup source B. After wakeup, it's necessary to call SDK clock_manager's API--CLOCK_SYS_UpdateConfiguration() to reconfigure the system clock, or it will use 8MHz SIRC, 48 MHZ FIRC and SPLL are disabled after wakeup. c. By default, after receive ID = 0x123(it can be configured via macro LP_REQUEST_ID in /include/Config.h ) standard CAN(CAN 2.0 or CAN-FD), the MCU will go to VLPS mode 7. There 3 on-board RGB LED are used to indicate the FlexCAN working status: blue RGB LED will be toggled after individual MB received a CAN message; green RGB LED will be turn ON after enter bus-off and turn OFF after exist bus-off(recover successfully). To run this sample project, the following HW and SW require: SW: S32DS for ARM v2.2 IDE with S32K1xx SDK RTM 3.0.3 installation HW: S32K144EVB-Q100 Rev.C with a DC-12V adapter for its power supply by J16 and a USB-to-CAN adapter(such as PEAK CAN) to connect PC with J13 of the EVB 3.S32K144_FlexCAN_PD_SamplePrj_RxFIFO_DMA_Receive_SDKRTM3P0 36.png Functions implementation key points and tips: This sample project is made to demonstrate the following S32K1xx FlexCAN features with SDK FlexCAN PD driver: 1. Configure to receiver the following exact 16 standard ID CAN message with RxFIFO 8x ID filter table with format type-B(2x 16-bit ID) Standard ID: 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x111, 0x222, 0x333, 0x444, 0x555, 0x666, 0x777, 0x788 The RxFIFO is also configured to use eDMA channel 0 for CAN message receive, user can easily change to use CPU interrupt for RxFIFO in processor expert flexcan component configuration if required. Note: A. FlexCAN of S32K1xx dose not support to receive CAN-FD message frame with RxFIFO, so no CAN-FD support in this demo project. B. all the filter table elements must be configured to contain only standard or extend ID, if it contains both standard and extend ID, the IDE-bit mask will be ignored.  C. After RxFIFO enabled, MB0~MB5 is used as the RX FIFO, at least MB6~MB7 are used as the ID filter table(to store the acceptance ID), the actual available MB number is determined by RxFIFO ID filter table size, details please refer to section--55.4.6 Rx FIFO structure of S32K1xx RM Rev.12.1  2. Configure one extra individual MB(MB8) to receive 16 standard ID CAN 2.0 message with the lower 4LSB masked(mask=0x7F0, acceptance ID = 0x123): 0x120 ~ 0x12F; Both RxFIFO and individual MB RX use non-blocking receive method/API with MB TX/RX complete ISR callback installed to set a new circle buffer for next message frame receive 3. Configure one individual MB(MB9) to blocking transmit a standard CAN 2.0 message with ID = 0x100 periodically(period = 5ms), and also send back the received CAN messages(if it's available) to the CAN bus as a response. 4. Provide the FlexCAN bus-off manual recovery configuration API and interrupt ISR callback codes for reference, changing the macro CAN_BUSOFF_RECOVERY_MANUAL(in include/Config.h) to select the bus off recovery method(enable the macro definition: manual recovery, comment the macro definition: automatic recovery); Note: In this sample project, the macro CAN_BUSOFF_RECOVERY_MANUA is enabled by default, and manual recovery codes works. To make the bus-off recovery callback work, user should replace the flexcan PD driver codes and S32K144_feature.h with S32K1xx RTM 4.0.0(which can be downloaded from nxp.com with registered account login and then installed stand-alone or installed via S32DS v3.3 IDE update). This is already done this sample project!!!  5. There 3 on-board RGB LED are used to indicate the FlexCAN working status: red RGB LED will be toggled after RXFIFO received any CAN message; blue RGB LED will be toggled after individual MB received any CAN message; green RGB LED will be turn ON after enter bus-off and turn OFF after exist bus-off(recover successfully). To run this sample project, the following HW and SW require: SW: S32DS for ARM v2.2 IDE with S32K1xx SDK RTM 3.0.3 installation HW: S32K144EVB-Q100 Rev.C with a DC-12V adapter for its power supply by J16 and a USB-to-CAN adapter(such as PEAK CAN) to connect PC with J13 of the EVB Attached are the sample project for your reference, and details can also be fiound with the detailed comments in source codes. Hope it can help you, and any comments/questions are welcomed, and you can just ask in this thread and I will try to anwser them. Best regard, Enwei Hu(胡恩伟).  
查看全文
Dear all, I'd like to share some useful tips about S32DS for ARM v2018.R1 IDE and S32K1xx development  in Chinese as below: 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》; 《S32K SDK使用详解之S32 SDK软件编程思想详解》; 《S32K SDK使用详解之S32 SDK软件架构详解》; 《 S32K1xx系列MCU使用Tips--功能介绍及软件开发和硬件设计FAQ》; 《 S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决》; 《S32DS使用Tips--S32DS for Power V1.2 链接文件和启动过程详解》; 《S32K1xx系列MCU使用Tips之SDK软件架构和使用详解》; 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》; 《S32DS IDE使用Tips--应用工程调试常见问题(FAQ)答疑》; 《 S32DS 使用Tips之S32DS for Power不同版本之间的GNU工具链差异与外设寄存器位域访问问题总结》; 《 S32DS使用Tips之S32DS for Power v1.1应用工程升级到v1.2重新编译运行程序跑飞问题解决》; 《S32DS 使用tips--S32DS for ARM v1.3工程到S32DS for ARM V2.0迁移升级方法和注意事项》; 《  S32DS 使用 tips--工程属性配置(编译选项和C编译器、汇编器及链接器设置)》; 《 S32DS使用Tips--如何编译生成和调用静态库》; 《S32DS使用Tips--如何通过创建新的编译目标(Build Target)在同一个S32DS工程中同时编译静态库和应用程序》; 《 S32DS使用Tips--如何配置和使能Attach功能定位软件程序bug和完成bootloader与应用程序工程的联合调试》; 《 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定)》; 《 S32DS 使用 tips--使用Flash from file下载S19或elf文件》; 《S32DS for ARM v2018.R1安装IAR Eclipse插件调用IAR工具链开发S32K系列MCU应用程序详解》 For more contents, please follow below link: “汽车电子expert成长之路”微信公众号最新最全原创技术分享文章列表 ; Hope this can help you and have a nice day~! Best regard, Enwei Hu(胡恩伟)
查看全文
Hi all, Recently, we completed S32K Sound Mixer reference code and demo, and glad to share this demo at here.   Some key feature of this demo:  - Demo HW based on S32K344/S32K148 + audio codec SGTL5000 + QSPI flash MX25L6433.  - Demo SW based on S32K3 RTD RTM 2.0.0 and S32K1 RTD RTM 1.0.0.  - Demo provided 2 kinds of sound mixing algorithm realization code, and corresponding audio materials and codec SGTL5000 driver.  - Demo showed how to programming QSPI flash and its AHB accessing via audio storage and playing process.  - Demo used mono audio as source for processing, and output stereo audio (I2S format) via SAI HW FIFO combine (Line_Mux) function with nearly no extra cost.   HMI/Cluster apps need multiple audio sources (usually warning sounds) be played simultaneously, which brings sound mixing ability requirement. However, S32K1/3 lack of this HW/SW feature support. With the demand from local key customer, and considering potential customer requirements, we planned to enable a SW sound mixer with scheduled peripherals, to enhance the S32K family audio mixing ability. It shall be easy of using/porting on S32K1/3, and use QSPI flash (AHB mode read) to store the music. Attachment the Sound Mixer package includes 2 sound mixing examples based on S32K344 EVB and S32K148 T-Box RDB, and some slides to introduce this implementation and quick start guide.    Thanks and welcome any comment from you. Best Regards, Shuailin Li
查看全文
******************************************************************************** * Detailed Description: * * This example shows how to use the back-to-back mode of the PDB to trigger * sequence of ADC channels conversion. 4 PDB channel 0 pre-triggers/triggers are * generated upon single PDB SW trigger. The first trigger is started by the PDB, * no delay is used. Next 3 triggers start after corresponding acknowledgment is * received from ADC0. * * Converted data is used to change color of the EVB led based on Trimmer position. * * ------------------------------------------------------------------------------ * Test HW:         FRDM-S32K144 * MCU:             PS32K144HFVLL 0N77P * Fsys:            default * Debugger:        S32DS * Target:          internal_FLASH * ********************************************************************************
查看全文
**************************************************************************************** Detailed Description: This is a rather simple example that shows LPI2C0 in Master mode. MPL3115A2 sensor is used as a slave device. I2C bus at PTA2 SDA, PTA3 SCL (2-pin open drain mode), external pull-up resistors on BRKTSTBC-P3115 board. BRKTSTBC-P3115 supplied from P3V3 (J3.7). Baud rate 400kHz, source SIRCDIV2 8MHz. The master reads periodically MPL3115A2 status register (every 200ms) and temperature / altitude data once they are ready. ------------------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100, BRKTSTBC-P3115 MCU: S32K144 0N57U IDE: S32DSR1, OpenSDA Target: internal_FLASH ****************************************************************************************
查看全文
The purpose of this demo application is to show you the usage of the FlexCAN module configured to use Flexible Data Rate using the S32 SDK API. - In the first part, the application will setup the board clocks, pins and other system functions such as SBC if the board uses this module as a CAN transceiver. - Then it will configure the FlexCAN module features such as FD, Bitrate and Message buffers - The application will wait for frames to be received on the configured message buffer or for an event raised by pressing one of the two buttons which will trigger a frame send to the recipient. - Pressing SW3 button of board 1 shall trigger a CAN transfer that results in toggling the RED led on board 2. - Pressing SW2 button of board 1 shall trigger a CAN transfer that results in toggling the GREEN led on board 2. - This demo application requires two boards, one configured as master and the other one configured as slave (see MASTER/SLAVE defines in application code) or single board connected with CAN tool. - Both the event and error callbacks are installed, callback_test variable indicates event entering bit0 .. RX complete bit1 .. TX complete bit2 .. ERR INT flag set bit3 .. BOFF INT flag set - to enter bus off simply short CANH with GND and send message using either SW1 or SW2, FlexCAN enters bus off (error event) and blue LED is ON. Also TX MB is aborted. Remove short connection and send message again normally, blue LED is off.   ------------------------------------------------------------------------------ * Test HW: S32K144EVB-Q100 * MCU: FS32K1441 0N57U * Compiler: S32DS.ARM.2.2 * SDK release: S32SDK_S32K1xx_RTM_3.0.3 * Debugger: Lauterbach, OpenSDA * Target: internal_FLASH  
查看全文
******************************************************************************** Detailed Description: This example shows SRAM ECC injection. By default, a double-bit ECC error is injected on read access of a location in SRAM_U region. This can be changed with the SRAM_U and DOUBLE_BIT macros. The errors can be detected by both the ERM and MCM modules and the corresponding interrupts can be called. Although only ERM is needed, for demonstration purposes, the MCM interrupt is enabled as well with a lower priority than the ERM interrupts. The ERM interrupts that are called first disable the injection mechanism so that subsequent errors can not be detected during a stack read access. The default S32 Design Studio start_up file copies the vector table to the SRAM_L region. To be able to inject ECC errors in this SRAM region and call the interrupts, the copying is disabled by __flash_vector_table__ symbol  declared in the start_up.h file and defined in the S32K144_64_flash linker file. -------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100 MCU: S32K144 0N57U Debugger: S32DSR1 Target: internal_FLASH ********************************************************************************
查看全文
******************************************************************************* * * The purpose of this demo application is to present a usage of the ADC_SAR and * BCTU IP Driver for the S32K3xx MCU. * * The example uses the PIT0 trigger to trigger BCTU conversion list. Five standard * ADC channels are selected to be converted. * Converted result from BCTU data register are moved by DMA into result array. * This result array should be placed into no cacheable area if data cache is enabled. * * ADC channel S10 is connected to board's potentiometer, and converted value is * used to dim board's LED. * * * ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K344 * Compiler: S32DS3.4 * SDK release: RTD 1.0.0 * Debugger: Lauterbach * Target: internal_FLASH ********************************************************************************
查看全文
NXP S32K1xx serial MCU is widely used in automotive body control and many general-purpose automotive applications, while to target some applications with special requirements such as requiring more peripherals instance than the portfolio can offer (e.g. 6x CAN-FD, 6x LIN or 4 I2C) like mid-end BCM or DCU, an on-board dual/multi MCU sync solution is proposed as an alternate solution to extend the S32K1xx MCU peripherals/memory resource and CPU process capability. The eRPC (Embedded Remote Procedure Call) is a Remote Procedure Call (RPC) system created by NXP(https://github.com/EmbeddedRPC/erpc/). An RPC is a mechanism used to invoke a software routine on a remote system using a sample local function call. eRPC software architecture Figure 1. eRPC software architecture In this project, we ported the eRPC protocol to S32K1xx platform, tested and figured out its performance. An out-of-box software package with detailed user guide (this document) is provided to simplify and accelerate users’ assessment of eRPC on S32K1xx. Two S32K144EVB boards are connected to demonstrate the usage of the eRPC protocol. One works as the client, another as the server. The client board starts an eRPC request and the server board responds to the request and executes the service. eRPC task workflow on S32K144-EVB.png Figure 2. eRPC task workflow on S32K144-EVB There are three types of MCU extensions are demonstrated in the project: MCU IO extension: Set LED; MCU peripheral extension: CAN and LIN message forwarding, LED luminance regulator; CPU process capability extension: Matrix multiply and addition math operation. Please find the attached sample projects and user guide for more details. Table of Contents in User Guide.png Figure 3. Table of Contents in User Guide •Note: Even though we did a lot of tests for the solution with the sample projects on S32K144-EVB, it’s still customer’s responsibility to ensure the total quality by themselves when it’s integrated in a real application project, all the sample codes and user guide documentation are just reference for customer. If you have any questions about this solution, please post here and we can have an open discussion. Best Regard, Enwei Hu(胡恩伟) GPIS System Apps Engineer.  
查看全文
[S32K3 Tools Part] How to use VScode to compile EB MCAL project       For EB configured MCAL code, it is usually based on RTD and then compiled using the command line. When I first started learning, I always opened the relevant files directly to modify them, and then used the window cmd method to type commands. This method is very clumsy. Therefore, this article will show how to use VScode to open and compile a RTD4.0.0 S32K344 MCAL project. Of course, for MCAL EB projects, before compiling, you need to use the EB tool to open the configuration file of the corresponding project, and then close it after the project is generated. 1 VScode tool and configuration VScode download link: https://code.visualstudio.com/Download After downloading, install it. Here are some installation plug-ins I often use:   1.png Fig 1 2.png Fig 2 You can search in extensions and install it directly. 2. Use VScode to compile the RTD MCAL project This article takes RTD4.0.0, SW32K3_S32M27x_RTD_R21-11_4.0.0 as an example, and the platform is the official S32K344-EVB board. The code takes Dio_TS_T40D34M40I0R0 project as an example. In order not to affect the original routine, Dio_TS_T40D34M40I0R0 is copied and saved as Dio_TS_T40D34M40I0R0_vscode 2.1 Use EB tresos generate the configuration Open EB tools, import the project in path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject 3.png Fig 3 Double-click someId, then right-click. If you do not need to make custom configurations, just click generate project. Wait for the generation to complete without errors and close the EB IDE. 4.png Fig 4 2.2 VScode  open project    First open VScode and select the project path in open Folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344 5.png Fig 5 After opening, you can see that all the files in the path have been put in: 6.png Fig 6 You can save the workspace so you don't need to open the folder every time. File->Save workspace as, save to the path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344   2.3 Modify mk file The project mk file needs to be modified to specify gcc, tresos paths, etc. Modify points:project_parameters.mk GCC_DIR = C:/NXP/S32DS.3.5_RTD400/S32DS/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_4.0.0/eclipse/plugins 7.png Fig 7 Modify points: check_build_params.mk Delete ifeq ("$(wildcard $(T32_DIR)/bin/windows/t32marm.exe)","") $(error Invalid path set to Trace32. \ The provided path: from project_parameters.mk T32_DIR=$(T32_DIR) is invalid!) Endif 8.png Fig 8 Then save all files:File->save all 2.4 Compile the file Terminal->New Terminal Enter the following command: >make generate >make build 9.png Fig 9 10.png Fig 10 As you can see, after make build, an elf file has been generated in the out folder. This elf file can be directly downloaded using two methods: (1) S32DS empty project link to elf to download (2) Lauderbach directly download elf file   2.5 debug the generated elf file Since the S32K344-EVB has an onboard opensda tool, we directly use the S32DS empty project to link to the generated main.elf file to download and debug. Create a new S32DS project, and the interface is PE Multilink, then directly change the elf file to main.elf in the debug configuration, and then put the previously generated elf file into the folder of the new S32DS project:  \Debug_FLASH 11.png Fig 11 Then, enter debug mode, the results are as follows: 12.png Fig 12 As you can see, the chip has entered debug mode and can run successfully. Running at full speed, you can see the onboard red light flashing, so at this point, VSCode has compiled the MCAL code and run successfully.  
查看全文
******************************************************************************** * Detailed Description: * * This example shows how to init DMA for simple memory to memory copy. * Eight 16-bit values are copied upon SW start. * * ------------------------------------------------------------------------------ * Test HW:         FRDM-S32K144 * MCU:             PS32K144HFVLL 0N77P * Fsys:            default * Debugger:        S32DS * Target:          internal_FLASH * ******************************************************************************** Original Attachment has been moved to: Example-S32K144-DMA-RAM2RAM-test-v1_0-S32DS.zip
查看全文
************************************************************************************************ Detailed Description: WDOG tested in SystemInit() function (system_S32K116.c) after POR. For debugging purposes: - WDOG counter reference clock is pre-scaled to slow the test (CS_PRES = 1). - During CNT_LOW test, BLUE LED (PTE8) ON. - During CNT_HIGH test, RED LED (PTD16) ON. - Once both tests have passed, GREEN LED (PTD15) ON. If either of the test fails, WDOG will stay in its default configuration and rest the MCU. ---------------------------------------------------------------------------------------------------------------- Test HW: S32K116EVB-Q048 REV.B MCU: S32K116 0N96V Debugger: S32DSR1, OpenSDA Target: internal_FLASH ************************************************************************************************
查看全文
Welcome to the S32K Microcontrollers forum. Get expert advice from the NXP developer community. Our support team also monitors these forums to provide answers and take your feedback.   Anyone can read the discussions, but only registered NXP Community members can post questions and comments. Before you ask a question, please search the community to find if someone has already offered a solution. If you don’t see a solution, then ask the community your question. S32K Web page S32K Reference manual S32K Data sheet S32K Application notes and other documents S32K Evaluation Board S32 Design Studio IDE https://community.nxp.com/docs/DOC-334170 
查看全文
******************************************************************************** Detailed Description: This example shows the use of SRAM retention after SW reset. The SW reset is triggered by pressing the SW3 button on the S32K144 EVB The reset is delayed in RCM module: 514 LPO cycles. In the RCM interrupt, SRAMU_RETEN and SRAML_RETEN are cleared allowing to retain SRAM data during the reset. After software reset, SRAMU_RETEN and SRAML_RETEN are set to1 to allow accesses to SRAM.  During software initialization in the startup_S32K144.S, ECC RAM initialization is skipped.  After that, we can check the written data before reset are still placed in the SRAM.  ------------------------------------------------------------------------------ Test HW: S32K144EVB-Q100 MCU: S32K 0N57U Debugger: S32DSR1 ********************************************************************************
查看全文
******************************************************************************* The purpose of this demo application is to use pad keeping for  PINS and enter the standby mode & before entering the standby mode update variables in Standby RAM memory with pin state. Once wake up from the standby mode update the pins values from the STANDBY RAM variables.  S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** =============== How this DEMO works ========== Before entring standby :-- Before entering standby mode, i make BLUE LED high SW6 on board pressed to enter the standby mode. Wakeup from Standby :-- SW5 on board pressed to wakeup from standby After wakeup from Stand by:-- I glow Green LED Unglow the BLUE LED Wait for SW6 on board to be pressed to enter the standby mode. ===============  Stand by RAM location =============== As noted, the Standby SRAM is allocated at the first 32 KB of the SRAM Memory. https://www.mouser.com/pdfDocs/S32K3MemoriesGuide.pdf =============== Pins used for PAD keeping =============== PTA30, PTA31, PTD14 Dinesh_Guleria_1-1706609081807.png   Dinesh_Guleria_2-1706609164083.png   =============== Switches used =============== Dinesh_Guleria_0-1706609013348.png   Enter Standby mode, by pressing SW6 on Board EXIT Standby mode, by pressing SW5 on Board =============== Wakeup source, SW5 PTB26 =============== Dinesh_Guleria_3-1706609222511.png =============== WKPU[41]  ---> WKPU_CH_45=============== Because First 4 WKPU are timers, so 41 + 4 = 45 Dinesh_Guleria_0-1706610068634.png   =============== Linker file changed =============== Added Standby RAM memory & sections for standby RAM memory. Changes can be seen by comparing the original linker file  Dinesh_Guleria_4-1706609365318.png   Dinesh_Guleria_5-1706609374981.png Dinesh_Guleria_6-1706609386872.png   Dinesh_Guleria_7-1706609395948.png =============== Startup file changed , startup_cm7.s =============== Added call to Initialise the Standby RAM Changes can be seen by comparing the original startup_cm7.s file Dinesh_Guleria_8-1706609506315.png     ======================= How to verify if Standby RAM is working =============== 1> Declare two variables in file Wkup.c :-- __attribute__ ((section (".standby_ram_data"))) volatile int test_0_value ; __attribute__ ((section (".standby_ram_data"))) volatile int test_1_value ; Dinesh_Guleria_0-1706795824611.png   2> function set_pin_value() will be called before entering the standby mode. Initialise the values to these two variables inside function set_pin_value() in file Wkup.c. Dinesh_Guleria_1-1706795851364.png   3> Now burn the code inside the MCU using the PE micro debugger.     Once code is burned do not run the code & disconnect the debugger. 4> Power OFF and power ON the S32K312 board. Now code is waiting to enter standby mode. Press switch SW6 MCU will enter standby mode & Blue LED glowing. Press switch SW5 MCU will wakeup from the standby mode. Code will Now code is waiting to enter standby mode 5> Now open your debugger configuration, and attach to running target. Dinesh_Guleria_2-1706795891040.png   6> Once connected click on the ELF file & press pause button. Dinesh_Guleria_3-1706795905290.png   7> In Debug window you can see the value of variables test_0_value & test_1_value same as initialised before entering the standby mode. Dinesh_Guleria_4-1706795934951.png   Dinesh_Guleria_0-1706799345237.png   Dinesh_Guleria_1-1706799364449.png  
查看全文
       This routine implements all four different mask setting methods.Users can refer to these routines to implement some application scenarios.Please note that this routine is for reference only.When posting this routine, I only did some limited tests, and I don't make sure that there are no problems. If you find it, please leave a message and I will revise it in time.       When the program was flashed into the S32K142EVB, the Blue Led will toggles every 500ms, this Led shows that the program is running on well condictions. If a message was received by S32K142EVB from external CAN bus, the Green Led will toggle,at the same time, the S32K142EVB will sent a message to CAN Bus which have the same data with the message received,and the ID is 0x02.At the last,the Red Led will toggle when a CAN error is occurd.   1.FlexCAN Mask Setting Overview          S32K1XX FlexCAN support  Frame mask function ,as you can see the FlexCAN mask can be set to Global Mask or Individual Mask,and user can choose to use FIFO or MB to receive message,but only MB can be used for sending messages.and one more thing you should be care is that the FIFO can not be used for CAN FD,this is because the FIFO data filed only support 8 bit datafiled. Senlent_0-1662637755060.png           If you use MB14 or MB15, have to set the mask of these tow MBs separately,and you can take a look at the two functions in the below. ->FLEXCAN_DRV_SetRxMb14Mask();  ->FLEXCAN_DRV_SetRxMb15Mask();   2.Hardware Needs. 1.S32k142EVB,(or own made board which can support CAN communications.) 2.CAN TOOL's which used for send or receive messages from CAN Bus on your computer.   If you don't have such tools ,you can use another board which can replace the CAN tools to send or receive CAN messages. 3.S32K142EVB should be powered by external 12V DC, and don't forget to connect the J107 to 1-2.   3.Software Needs. 1.This demo build on S32 Design Studio for ARM V2.2  2.The SDK version is SDK_S32K1XX_15   4.FlexCAN_RX_MB_Mask_Setting 4.1.Set the Mask Type to Global Mask Type.      In this case, we can only receive the messages which ID from 0x300~0x37F and 0x400~0x47F.      If you try to sent the messages with other ID's, the S32K142EVB will not have any reponse!  4.2.Set the Mask Type to Individual Mask Type.      In this routine,we can only receive frames with IDs in the range of 0x400~0x47F. 5.FlexCAN_RX_FIFO_Mask_Setting 5.1.Set the Mask Type to Global Mask Type.      In this routine,we can only receive frames with IDs in the range of 0x10~0x17, 0x20~0x27,0x30~0x37,0x40~0x47, 0x50~0x57,0x60~0x67,0x70~0x77,0x80~0x87. 5.2.Set the Mask Type to Individual Mask Type.      In this routine, we can only receive frames with IDs in the range of 0x10~0x17,0x20~0x27,0x30~0x37,0x40~0x47, 0x50~0x57,0x60~0x67,0x70~0x77,0x80~0x87.   End       If you need to use CAN FD, please note that FIFO cannot be used. Regarding FIFO, it has three filtering formats, you can refer to the following chapters in the data sheet for details. S32K-RM Rev 13. Chapter:55.4.2.15 Rx FIFO Global Mask register (RXFGMASK) Chapter:55.4.6 Rx FIFO structure          
查看全文