S32K知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K Knowledge Base

标签

讨论

排序依据:
The script performs secure‑recovery and mass‑erase initialization of locked S32K142 MCUs by keeping the device in system reset (PTA5 RESET_B held low) from the moment of power‑on. Before running the script, connect PTA5 (RESET_B) to VSS, power‑cycle the MCU, and start the script. The script first reads the MDM‑AP Status register to determine the MCU’s security and flash‑ready state, then prompts the user to initiate a mass‑erase operation through the MDM‑AP Control register. After the mass erase completes, the user is instructed to release RESET_B (remove PTA5 from VSS), after which the debugger re‑attaches and displays the flash configuration area at address 0x400. Finally, the script prompts whether the MCU should be reprogrammed from an ELF file, and if confirmed, programs flash, loads the project, and executes it.
查看全文
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K344 to enable pinging the lwIP stack * from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * EVB: * - All jumpers in default positions * * Configuration: * - Updated pin configuration * - Updated clock configuration * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Added DIO * * main.c * - Updated only the header * device.c * - No changes * test.c * - Commented out the code that shuts down the TCP/IP stack after * its predefined timeout * - Added LED task * * ----------------------------------------------------------------------------- * Test HW: S32K344MINI-EVB SCH-94921 REV B, 700-94921 REV B * MCU: S32K344 * Debugger: On Board * Target: internal_FLASH * EVB connection: EMAC <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
查看全文
******************************************************************************************************* * Detailed Description: These demos showcase how to use eMIOS in Input Capture mode with DMA, utilizing both low-level drivers (Ip) and high-level drivers (MCAL). They demonstrate how timestamp data from captured input signals is stored and how a GPIO toggle provides a simple visual confirmation that the interrupt is being triggered as expected. * Connections:  ******************************************************************************************************* * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Debugger: S32DS 3.6.2, OpenSDA * Target: internal_FLASH ******************************************************************************************************* * Important information:  eMIOS Pwm: Configures EMIOS 0 Channel 1 as OPWMB (Output Pulse Width Modulation Buffered). This channel generates a waveform that will be captured by Channel 9 eMIOS Icu with DMA: Configures EMIOS 0 Channel 9 in ICU_MODE_TIMESTAMP using SAIC (Single Action Input Capture) mode. This channel captures the timestamps of the waveform generated by Channel 1. After a predefined number of captures, a DMA interrupt is triggered. ******************************************************************************************************* Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
查看全文
S32K344 + MC33664 + MC33774 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33664-MC33774-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2028783 S32K344 + MC33665 + MC33774 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33665-MC33774-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2127108 S32K344 + MC33664 + MC33775 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33664-MC33775-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2127049 S32K344 + MC33665 + MC33775 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33665-MC33775-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2127140 S32K144 : RTD-1.0.1 porting for : BCC_S32K144_FreeMASTER :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K144-RTD-1-0-1-porting-for-BCC-S32K144-FreeMASTER/ta-p/2130167
查看全文
[RTD400 LLD]K344 Center Aligned PWM Trigger ADC BCTU 1. Abstract     Not long ago, a customer's actual project needed to implement the high-level center point of the center-aligned PWM on the S32K3XX to trigger the ADC BCTU multi-channel sampling. This function requires the use of EMIOS, ADC, and BCTU. At the beginning, the customer was always unable to achieve the trigger at the center point of the PWM, and the trigger position was wrong. Later, After we give the explanation and analysis of the principles of the K3 related modules to the customer, as well as the guidance of the actual code configuration test, and the customer also achieved the required function. For the convenience of testing, PIT and UART printf functions are also added here. So here is a summary of the specific situation of this function, so that other customers who encounter similar functional requirements in the future can have a reference and can quickly build it. The requirements are as shown in the figure below. In the up-down counting mode, the center-aligned PWM is output, and the trigger sampling of the ADC BTCU LIST is realized at the center point of the high level. This article will implement 1KHZ center-aligned PWM, 50% duty cycle, and high-level center point to achieve ADC BTCU LIST sampling on the official S32K344-EVB board, based on the RTD400 LLD version.   Fig 1 2. Center-aligned PWM center point trigger ADC principle       Regarding the principle, there is no suspense about ADC. You can directly refer to the previous article on ADC software and hardware triggering: [RTD400 LLD]K344 ADC SW+HW trigger This is the structure shown in Figure 2. After configuring ADC, BCTU and select the triggered EMIOS channel. When the relevant flag of EMIOS is generated, BCTU will be triggered. After the watermark is reached, a notification will be generated to store all LIST ADC channel values ​​in the buffer, and then the ADC value can be printed out for easy viewing according to the situation.    Fig 2 In the current working condition, the logic that needs to be concerned about is mainly: how to generate center-aligned PWM, how to generate a flag at the high-level center point, and use this flag to trigger BTCU sampling. 2.1 How to generate center-aligned PWM      First, let’s take a look at the channel status of EMIOS and the channel status that supports center-aligned PWM.  Fig 3 The center-aligned PWM mode is: OPWMCB As shown in Figure 1, we can see that the counter count mode in this mode is up and down. Let's take a look at the channel types that support OPWMCB. We can see that there is only type G.   Fig 4 So, what are the channels supported by Type G? See the figure below:  Fig 5 The mystery is solved. Only CH1-CH7 of eMIOS supports center-aligned PWM. Well, then a new question arises. Can this mode directly generate a trigger signal at the center point of the PWM high level to trigger the ADC BCTU sampling? Answer: No! The reason can be seen from Figure 1. In this PWM mode, there are two trigger flags generated when the up and down count comparison is completed. Therefore, if this mode channel is used to directly trigger ADC sampling, two triggers will be generated in one cycle, and both are on the edge of PWM. Since OPWMCB cannot directly generate a trigger at the center point of PWM, how to achieve it? In addition, open a dedicated channel, and the clock source is the same as OPWMCB, but that channel only counts to generate trigger flags and does not output any waveform. 2.2 How to generate PWM center point trigger flag   Key information: OPWMCB simultaneous clock source, only counting mode, or up and down MCB mode, only one channel is satisfied: ADC CH0, counter bus type also needs to be selected as counter_bus_B       Fig 6 Let's take a look at the trigger flag of MCB:  Fig 7 As you can see, it is perfect. The trigger mark is at the top of the upward and downward counting, which is exactly the center point of the high level of the same source PWM. So, here, the specific channel arrangement has been determined in principle, two channels: EMIOS0_CH0 MCB mode pure counting and triggering the generation of flags to trigger ADC sampling; EMIOS0_CH1-CH7 is OPWMCB mode, simply outputting center-aligned PWM. 3. Software configuration and implementation       The software uses the S32K3 RTD400 version, and other versions have similar configurations! 3.1 Demo CT  module configuration First, you need to prepare a K344 demo, and then configure the pins, clocks, and peripheral modules. The following will explain the configurations. The modules used are: 2 GPIOs, ADC, BCTU, EMIOS clock, EMIOS PWM, LPUART for printing logs, PIT for timed printing, Trgmux is configured but not used in this article, so I won't talk about it!      3.1.1 Pin configuation       The pins used are as follows:  Fig 8 The two GPIOs are used to toggle in BCTU trigger notification and BCTU watermark notification respectively, to test the waveform positioning. ADC1_s10 pin is used for ADC1, but this article mainly uses BCTU to combine ADC0. ADC0 does not add specific external pins, but uses internal signals. LPUART is used for printing, and EMIOS0_CH1 is used to generate center-aligned PWM waveforms. 3.1.2 Clock configuration      The clocks that need to be paid attention to here are: ADC clock, EMIOS clock, UART clock, and PIT clock.  Fig 9 These clocks will be used later when configuring specific timing periods and baud rates. 3.1.3 Peripheral configuration       The peripherals used mainly include the following modules:  Fig 10 (1)Adc_Sar_Ip The configuration of the ADC0 module uses the one shot mode, that is, one conversion is generated after one trigger. In this way, the timer EMIOS channel can be used to generate trigger conditions to trigger a conversion. Pre-sampling is enabled to prevent the residual charge of the sampled value of the previous channel from affecting the result of the current channel and causing deviation of the ADC value. The trigger mode uses BCTU. For the configuration of Adc prescaler value and calibration prescale, the frequency division requirements in RM need to be met. The final configuration is as follows:  Fig 11    Fig 12 (2)Bctu_Ip The configuration of Bctu_Ip needs to select the right EMIOS channel to use. From the above principle, we can know that EMIOS0_CH0 is used, and then LIST mode is adopted. For ADC0, three internal channels are currently added to the LIST: BANDGAP, VREFL, VREFH. The specific configuration is as follows:  Fig 13   Fig 14 (3)Emios_Mcl_Ip Here we need to consider the PWM cycle that needs to be generated. The goal is to generate a 1Khz center-aligned PWM, so the EMIOS mode is the MCB up-down counting mode. The clock cycle formula for MCB is: (2 x AS1) – 2. So for the EMIOS0 clock source of 160Mhz, what is the corresponding 1KHZ counter? First do 160 divide to get 1Mhz, and then calculate according to (2 x AS1) – 2: (2 x AS1) – 2 = 1Mhz/1KHZ=>AS1=1000/2 +1= 501. The configuration is as follows:  Fig 15 (3)Emios_Pwm The previous principle analysis shows that the PWM uses the OPWMCB center-aligned mode PWM, the clock comes from the counter bus B of EMIOS CH0, then the period is 1khz, and the duty cycle is 50%. The specific configuration is as follows:  Fig 16 (4)Lpuart_Uart Configure UART6 clock baud rate to 115200.   Fig 17 (5)Pit   Fig 18 (6)IntCtrl_Ip The interrupt configuration is as follows, and it can actually be configured via code.  Fig 19 3.2 Main code situation After the configuration is completed, the output of the center PWM and the sampling of the ADC BCTU can be realized by calling the following code in main. #include "Clock_Ip.h" #include "IntCtrl_Ip.h" #include "Adc_Sar_Ip.h" #include "Bctu_Ip.h" #include "Siul2_Port_Ip.h" #include "Pit_Ip.h" #include "Siul2_Dio_Ip.h" #include "Trgmux_Ip.h" #include "Lpuart_Uart_Ip.h" #include "Lpuart_Uart_Ip_Irq.h" #include "string.h" #include "stdio.h" #include "retarget.h" #include "Emios_Mcl_Ip.h" #include "Emios_Pwm_Ip.h" /* PIT instance used - 0 */ #define PIT_INST_0 0U /* PIT Channel used - 0 */ #define CH_0 0U /* PIT time-out period - equivalent to 1s */ #define PIT_PERIOD 40000000 static volatile uint8 toggleLed = 0U; #ifdef ADC_3V3_VREF_SELECTED #define ADC_BANDGAP 5980U /* Vbandgap ~ 1.2V on 14 bits resolution, 3.3V VrefH */ #else #define ADC_BANDGAP 3932U /* Vbandgap ~ 1.2V on 14 bits resolution, 5V VrefH */ #endif #define ADC_SAR_USED_CH 48U /* Internal Bandgap Channel */ #define BCTU_USED_SINGLE_TRIG_IDX 0U #define BCTU_USED_FIFO_IDX 0U #define BCTU_FIFO_WATERMARK 3U #define ADC_TOLERANCE(x,y) (((x > y) ? (x - y) : (y - x)) > 200U) /* Check that the data is within tolerated range */ #define LED_Q172_PIN 13u #define LED_Q172_PORT PTA_H_HALF #define GPIO_PTA2_PIN 2u #define GPIO_PTA2_PORT PTA_L_HALF #define EMIOS_INST0 0U volatile int exit_code = 0; volatile boolean notif_triggered = FALSE; volatile boolean notif_triggered1 = FALSE; volatile uint16 data; volatile uint16 data1; volatile uint16 data_bctu[3]; #define UART_LPUART_INTERNAL_CHANNEL 6 #define WELCOME_MSG_1 "Hello, This message is sent via Uart!\r\n" volatile Lpuart_Uart_Ip_StatusType lpuartStatus = LPUART_UART_IP_STATUS_ERROR; uint32 remainingBytes; uint32 T_timeout = 0xFFFFFF; uint8* pBuffer; extern void Adc_Sar_0_Isr(void); extern void Bctu_0_Isr(void); extern void Adc_Sar_1_Isr(void); void AdcEndOfChainNotif(void) { notif_triggered = TRUE; data = Adc_Sar_Ip_GetConvData(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_USED_CH); /* Checks the measured ADC data conversion */ } void AdcEndOfChainNotif1(void) { notif_triggered1 = TRUE; data1 = Adc_Sar_Ip_GetConvData(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, 34); /* Checks the measured ADC data conversion */ } void Pit0ch0Notification(void) { toggleLed = 1U; } void BctuWatermarkNotif(void) { uint8 idx; Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 1U); notif_triggered = TRUE; for (idx = 0u; idx < BCTU_FIFO_WATERMARK; idx++) { data_bctu[idx] = Bctu_Ip_GetFifoData(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_USED_FIFO_IDX); } Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); } void BcutTriggerNotif() { Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 1U); Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 0U); } void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } int main(void) { StatusType status; uint8 Index; Clock_Ip_StatusType clockStatus; /* Initialize and configure drivers */ clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); while (clockStatus != CLOCK_IP_SUCCESS) { clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); } Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); #if 1 Bctu_Ip_Init(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &BctuHwUnit_0_BOARD_INITPERIPHERALS); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_0_BOARD_InitPeripherals); while (status != E_OK); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_1_BOARD_InitPeripherals); while (status != E_OK); /* set PIT 0 interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(PIT0_IRQn); /* Install and enable interrupt handlers */ IntCtrl_Ip_InstallHandler(ADC0_IRQn, Adc_Sar_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(BCTU_IRQn, Bctu_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(ADC1_IRQn, Adc_Sar_1_Isr, NULL_PTR); IntCtrl_Ip_EnableIrq(ADC0_IRQn); IntCtrl_Ip_EnableIrq(BCTU_IRQn); IntCtrl_Ip_EnableIrq(ADC1_IRQn); // IntCtrl_Ip_EnableIrq(EMIOS0_5_IRQn); /* Call Calibration function multiple times, to mitigate instability of board source */ for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); /* Start a SW triggered normal conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_NORMAL); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; /* Start a SW triggered injected conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_INJECTED); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; #endif /* Initialize PIT instance 0 - Channel 0 */ Pit_Ip_Init(PIT_INST_0, &PIT_0_InitConfig_PB_BOARD_InitPeripherals); /* Initialize channel 0 */ Pit_Ip_InitChannel(PIT_INST_0, PIT_0_CH_0); /* Enable channel interrupt PIT_0 - CH_0 */ Pit_Ip_EnableChannelInterrupt(PIT_INST_0, CH_0); /* Start channel CH_0 */ Pit_Ip_StartChannel(PIT_INST_0, CH_0, PIT_PERIOD); // Trgmux_Ip_Init(&Trgmux_Ip_xTrgmuxInitPB);// Lpuart_Uart_Ip_Init(UART_LPUART_INTERNAL_CHANNEL, &Lpuart_Uart_Ip_xHwConfigPB_6_BOARD_INITPERIPHERALS); Emios_Mcl_Ip_Init(EMIOS_INST0, &Emios_Mcl_Ip_0_Config_BOARD_INITPERIPHERALS); Emios_Pwm_Ip_InitChannel(EMIOS_PWM_IP_BOARD_INITPERIPHERALS_I0_CH1_CFG, &Emios_Pwm_Ip_BOARD_InitPeripherals_I0_Ch1); printf("S32K344 PIT TRIGMUX ADC demo RTD400.\r\n"); /* Uart_AsyncSend transmit data */ lpuartStatus = Lpuart_Uart_Ip_AsyncSend(UART_LPUART_INTERNAL_CHANNEL, (const uint8 *) WELCOME_MSG_1, strlen(WELCOME_MSG_1)); /* Check for no on-going transmission */ do { lpuartStatus = Lpuart_Uart_Ip_GetTransmitStatus(UART_LPUART_INTERNAL_CHANNEL, &remainingBytes); } while (LPUART_UART_IP_STATUS_BUSY == lpuartStatus && 0 < T_timeout--); Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); while(1) { #if 1 if( toggleLed == 1) { toggleLed = 0; printf("ADC0_bandgap ch48 data_bctu = %d .\r\n", data_bctu[0]); printf("ADC0_vrefl ch54 data_bctu = %d .\r\n", data_bctu[1]); printf("ADC0_vrefh ch55 data_bctu = %d .\r\n", data_bctu[2]); } #endif } return exit_code; } 3.3 Test result    The test results include two parts: the printed results show the ADC sampling value, and the relationship between the PWM output and the BCTU trigger position. The printed results are as follows, and you can see that the values ​​of the three different ADC channels are correct:  Fig 20 PWM wave test result is: Ch1:PTB13 PWM Ch2:PTA29 BCTU trigger notification Ch3: PTA2 BCTU watermark notification   Fig 21 From the figure, we can see that the first BCTU trigger is at the center point of the PWM high level, and the BCTU watermark notification is used to store data after the ADC sampling is triggered three times. Here is another waveform to view the PWM cycle:  Fig 22 It can be seen that the PWM period is 1Khz, the duty cycle is 50%, and the first trigger of BCTU is at the center of the PWM high pulse. 4. Summary and trip description Through the above configuration, the RTD400 LLD method was finally used on the S32K344-EVB to implement a 1Khz, 50% duty cycle center-aligned PWM, and the high pulse center position triggered the ADC BCTU LIST acquisition. The trip encountered were my own configuration problems. At the beginning, I mistakenly thought that the watermark configuration value was consistent with the number of LIST channels. In fact, the watermark trigger is triggered only when the watermark value is exceeded. Therefore, if it is a 3-channel LIST, the watermark needs to be configured as 2, not 3. If it is 3, the test waveform is as follows: Fig 23 As you can see, the watermark notification is actually generated after it is triggered 4 times. Therefore, remember to match the FIFO number of the watermark. Attachment: 1. S32K344_centerPWM1k_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip Center PWM triggered BCTU LIST   2.S32K344_CPWM1k_TRIGMUX_BCTUHWLIST_EMIOSch4_ADC_printf_RTD400.zip PWM emios0_ch4 falling edge trigger the BCTU, for the comment situation.   3. Another method of center trigger: MCB_Counter up. Emios0_CH0 as the counter bus EMIOS0_CH1 as the PWM output EMIOS0_CH2 as the center trigger, but no PWM output, OPWMB S32K344_NCPWM1k1_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip
查看全文
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 2 AFE MC33774 board connected in TPL 3> Change following macro in mc33774_cfg.h file  to change the numbers of AFE connected in TPL. RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33774 AFE connected in TPL mode.         =============== MCU Pins used =========== TPL1-TX :-- TPL1TXCSB  --> PTC6/LPSPI0_PCS1 TPL1TXSCLK --> TPL12TXCLK --> PTE1/LPSPI0_SCK    TPL1TXDATA --> TPL12TXDATA --> PTE2/LPSPI0_SOUT    TPL1-RX :-- TPL1RXCSB  --> PTB17/LPSPI1_PCS3 TPL1RXCLK  --> PTB14/LPSPI1_SCK TPL1RXDATA --> PTB15/LPSPI1_SIN     ================= EVB Link ================== https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/analog-toolbox/evaluation-board-for-mc33664atl-isolated-network-high-speed-transceiver:FRDMDUALK3664EVB https://www.nxp.com/design/design-center/development-boards-and-designs/mc33774ata-evaluation-board-with-isolated-daisy-chain-communication:RD33774ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172   ================== Measurement types used in example ===== Periodic measurement is done by 33774 , this is cyclic Other Two : application , sync  need send command to start Application measurement , need send app_capture command twice , and then read the result. Synchronous measurement take out the Primary adc result(VC)and secondary result(VB) .But the VC and VB result comes from different adc. Period measurement start when you send  API "MSR_StartMeasurement" and then 774 will do period measurement automatically periodically :--   Why we need to measure Vc & Vb both :-- ASIL-D ,yes we can measurement VC channel by primary ADC and measurement VB by secondary ADC from hardware VC and VB are come from same point of battery cell. Now 2 ADC compare with each other, that lead to high safety (ASIL D). Primary & Secondary Device temperature reading :-- This API is used for it MC33774_CDD_BCC_SWC_Running_Slot4(). ============= Cell Balancing =========== Cell Balancing method used :-- MC33774 balance will switch between odd channel (1,3,5,7,... 17) and even channel (2,4,6,8,..18) by 500ms period , (250ms for odd and then switch to even 250ms and then odd 250ms...)it is because of IC design and cannot change by software.   MC33774 have lots of balance method  this example uses "timer method ". How to check Balancing is enabled :-- Following function MC33774_CDD_BCC_SWC_Running_Slot5() read the : Balance status & fault registers BAL_SWITCH_STAT0, BAL_SWITCH_STAT1 represent the balancing MOSFET current status.   Measure the voltage drop across the balancing register is the best approach. You will see the voltage drop appears every 250ms if PWM is 100%.  Please check the schematic of the 33774 EVB, find the balancing resistor on which channel balancing is enabled.     ======= How much time to wait to extract the measurements results ======= 240 us is the time of one SCAN Time between each Application measurement sequence. Min App measure time for 16 sample :-- 4.08ms = (16+1) *240 Min 1 SYNC measurement time, for 16 samples = 18 cycle ≈ 18 * (16*240us) ≈ 69 ms ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255) Disable Communication timeout in code :--   ================= Results for FIRST AFE =========================== Application Measurement : Cell voltage result :-- SYNC measurement : VC, VB same for both primary & Secondary  measure :--      
查看全文
The purpose of this demo application is to show you the usage of the FlexCAN module configured to use CAN FD and Enhance RXFIFO using the S32 RTD API. - This demo application requires two boards, or single board connected with CAN tool. - CAN FD is enabled with bitrate 500/2000 kbps - MB0 is configured to transmit either std. or ext ID - MB1 is configured to receive ext ID 0xFACE and MB2 to receive std ID 0x1 - Enhanced RXFIFO is enabled and 3 enhanced RXFIFO filter elements (filter + mask scheme) are defined ext ID 0xABCD with mask 0x1FFFFFFF std ID 0x123 with mask 0x7FF std ID 0x456 with mask 0x7FF - DMA is used to read enhanced RXFIFO, watermark is set to 5 - Callback function is used as well to handle TX and RX process in MBs and Enhanced RXFIFO after DMA complete 5 reading of RXFIFO  ------------------------------------------------------------------------------  Test HW: S32K3444EVB-Q172  MCU: PS32K344EHVPBS 1P55A  Compiler: S32DS.ARM.3.5  SDK release: S32K3_RTD_4_0_0_D2311  Debugger: Lauterbach  Target: internal_FLASH
查看全文
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Polling mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for IPWM mode .  :--       IPWM mode ,  ICU Driver User Manual :--   Result :--    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the ICU & PWM MCAL Driver for the S32K3xx MCU. This example uses the custom IRQ. The example uses:-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty       Result :--      ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文
Hi everyone, Welcome to the NXP Tech Days 2024 training session AUT-T4977: Hands - On Workshop: S32K3 Ethernet- How to Configure Hardware and Software. This session was initially planned for 15 attendees. But due to the popularity of the lecture, we have increased the number of available seats . Therefore, we will work in pairs during the Hands-On. My name is Alejandro Flores Triana (Alex) and I will be your guide during this conference. I am an Automotive Applications Engineer supporting different OEMs, Tier1s, Partners and other internal NXP teams on topics related to communication protocols (e.g. CAN, LIN, SPI, I2C, Ethernet, etc.). The idea of this session is for you to understand how to program the S32K3 Ethernet interface using NXP Real-Time Drivers (RTDs) – Autosar MCAL Layer. We will use a base project and together modify it to create a simple Ethernet application. Therefore, to be ready follow the steps below to get your environment up and running before the session. On your laptop, install the NXP Software environment described in the attached presentation: Hands - On Workshop: S32K3 Ethernet Prerequisites.   Once you have the NXP software environment installed, download the attached project: S32K344_ETH_MCAL_TechDays.exe   Run the .exe project with administrator rights. Accept the license and install in the desired folder         Open the NXP Design Studio. Click File -> Import -> Existing Projects into Workspace   Select root directory and browse the folder where you downloaded the project   Select Copy projects into workspace   Click Finish. Select the project. Click on the arrow next to the hammer. Click on Debug_FLASH. Then you are ready for the session! See you soon. Best Regards, Alejandro Flores Triana
查看全文
  1. Abstract This article also explains the S32DS+EB configuration, RTD400. The MCAL training of other modules will be based on this structure in the future. However, this article will provide a command line version of the code. If you need the command line mode, you can directly copy one under the RTD MCAL code package and use VScode to compile it. The hardware of this article is based on K312-miniEVB, and the board situation is as follows:      Fig 1 Function: In the K312 MCAL code, the UART transceiver function is implemented using DMA. Since RTD400 does not have K312 routines, there is also a process of porting from RTD400 to K312 MCAL. Of course, the previous article has explained it very clearly, and also provided the S32DS project template. This article will be based on the previous S32DS EB project template.  2. Function Implementation 2.1 K312 MINIEVB hardware configuration For the hardware configuration, since this article only uses UART, the structure is very simple, using the pins: LPUART3_TX: PTD2 LPUART3_RX: PTD3 and an external TTL-USB tool to achieve signal communication. 2.2 EB Configuration     Here we list all the modules used in EB tresos related to this article, and focus on the modules that require specific configuration. Fig 2 2.2.1 Mcl module The Dma Logic Channel interface needs to be configured. The main purpose is to configure two DMA channels for LPUART3_TX and RX. (1)dmalogicChannel_Type_0 Fig 3 (2)dmalogicChannel_Type_2 Fig 4 The callback registered here can also be called directly in the code. 2.2.2 Mcu module Mcu->McuClockSettingConfig->McuClockReferencePoint->Lpuart3_clk Fig 5 In fact, it configures the clock source frequency of LPUART to 24Mhz, which comes from AIPS_SLOW_CLK. 2.2.3 Platform module Platform->Interrupt Controller->IntCtrlConfig,Configure 3 channels: Fig 6 Here we only need to pay attention to the LPUART3 interrupt, as well as the DMA0 channel 6 and channel 7 interrupts, because these two DMA channels are configured for UART TX and RX. FlexIO is ignored, it is just a matter of whether it is deleted in the original routine. 2.2.4 Port module Port->PortContainer, add PTD2,PTD3 pins: Fig 7 Fig 8 2.2.5 Uart module There are two places to configure: (1)uart->General Fig 9 (2)uart->uartChannel Fig 10 There are 4 points to note here: Point 1: Select the clock source configured in the mcu Point 2: Configure the baud rate to 115200 Point 3: Select the asynchronous mode as DMA Point 4: Select the two DMA channels configured in the mcl, and you need to match TX and RX to the corresponding DMA channels. 2.2.6 Rm module Rm->DMA MUX Configure 2 DMA_MUX channels: Fig 11 Fig 12 2.3 main code     #include "Mcl.h" #include "Mcu.h" #include "CDD_Uart.h" #include "CDD_Rm.h" #include "Port.h" #include "Platform.h" #include "Lpuart_Uart_Ip_Irq.h" #include "Flexio_Uart_Ip_Irq.h" //#include "check_example.h" #include <string.h> #include "Port_Cfg.h" #define UART_LPUART_INTERNAL_CHANNEL 0U #define UART_FLEXIO_TX_CHANNEL 1U #define UART_FLEXIO_RX_CHANNEL 2U /* Welcome messages displayed at the console */ #define WELCOME_MSG "MCAL UART DMA Helloworld for automotive with S32K312!\r\n" /* Error message displayed at the console, in case data is received erroneously */ #define ERROR_MSG "An error occurred! The application will stop!\r\n" /* Length of the message to be received from the console */ #define MSG_LEN 50U #define UART_BUFFER_LENGTH ((uint32)10U) Std_ReturnType T_Uart_Status; //uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_START_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" __attribute__(( aligned(32) )) uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_STOP_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" uint32 g_Uart_CallbackCounter = 0U; uint32 g_DmaCh16_ErrorCallbackCounter = 0U; uint32 g_DmaCh17_ErrorCallbackCounter = 0U; //void Uart_Callback (void); void Uart_Callback(const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData); void Mcl_DmaCh16_ErrorCallback (void); void Mcl_DmaCh17_ErrorCallback (void); void Uart_Callback(const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData) { if(Event == LPUART_UART_IP_EVENT_END_TRANSFER) { __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_TX_EMPTY) { __asm volatile ("nop"); __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_RX_FULL) { __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_ERROR) { __asm volatile ("nop"); } else { __asm volatile ("nop"); } } void Mcl_DmaCh6_ErrorCallback (void) { g_DmaCh16_ErrorCallbackCounter++; } void Mcl_DmaCh7_ErrorCallback (void) { g_DmaCh17_ErrorCallbackCounter++; } boolean User_Str_Cmp(const uint8 * pBuffer1, const uint8 * pBuffer2, const uint32 length) { uint32 idx = 0; for (idx = 0; idx < length; idx++) { if(pBuffer1[idx] != pBuffer2[idx]) { return FALSE; } } return TRUE; } /** * @brief Main function of the example * @details Initializez the used drivers and uses the Icu * and Dio drivers to toggle a LED on a push button */ int main(void) { Std_ReturnType UartStatus = E_NOT_OK; uint32 RemainingBytes; uint32 Timeout = 0xFFFFFF; Uart_StatusType UartReceiveStatus = UART_STATUS_TIMEOUT; Uart_StatusType UartTransmitStatus = UART_STATUS_TIMEOUT; /* Initialize the Mcu driver */ Mcu_Init(NULL_PTR); Mcu_InitClock(McuClockSettingConfig_0); Mcu_SetMode(McuModeSettingConf_0); /* Initialize Mcl module */ Mcl_Init(NULL_PTR); /* Initialize Rm driver for using DmaMux*/ Rm_Init (NULL_PTR); /* Initialize all pins using the Port driver */ Port_Init(NULL_PTR); /* Initialize IRQs */ Platform_Init(NULL_PTR); /* Initializes an UART driver*/ Uart_Init(NULL_PTR); T_Uart_Status = Uart_AsyncSend(UART_LPUART_INTERNAL_CHANNEL, (const uint8 *)WELCOME_MSG, strlen(WELCOME_MSG)); if (E_OK == T_Uart_Status) { do { /* Get transmission status */ UartTransmitStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_SEND); } while (UART_STATUS_NO_ERROR != UartTransmitStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartTransmitStatus = UART_STATUS_TIMEOUT; } for(;;) { /* Receive data from the PC - Get 10 bytes in total */ UartStatus = Uart_AsyncReceive (UART_LPUART_INTERNAL_CHANNEL, Rx_Buffer, UART_BUFFER_LENGTH); if (E_OK == UartStatus) { do { /* Get receive status */ UartReceiveStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_RECEIVE); } while (UART_STATUS_NO_ERROR != UartReceiveStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartReceiveStatus = UART_STATUS_TIMEOUT; } UartStatus = E_NOT_OK; /* Send data to the PC - Echo back the received data */ UartStatus = Uart_AsyncSend (UART_LPUART_INTERNAL_CHANNEL, Rx_Buffer, UART_BUFFER_LENGTH); if (E_OK == UartStatus) { do { /* Get transmission status */ UartTransmitStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_SEND); } while (UART_STATUS_NO_ERROR != UartTransmitStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartTransmitStatus = UART_STATUS_TIMEOUT; } UartStatus = E_NOT_OK; } Uart_Deinit(); Mcl_DeInit(); // Exit_Example((T_Uart_Status1 == E_OK) && (T_Uart_Status2 == E_OK)); return (0U); }     It should be noted here that according to RTD C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Uart_TS_T40D34M40I0R0\doc的RTD_UART_IM.pdf, RTD_UART_UM.pdf. Fig 13 When doing DMA transfer, the buffer needs to be placed in the noncacheable area. That's why this article is:     #define UART_START_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" __attribute__(( aligned(32) )) uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_STOP_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h"     3. Test Result Use UART3, pin UART3_TX:PTD2, UART3_RX:PTD3 After the chip is reset, send first: Helloworld for automotive with S32K344! Then wait for reception. After receiving 10 bytes of data, generate uart_callback interrupt and enter LPUART_UART_IP_ENET_END_TRANSFER. You can see that the data received in RX_Buffer is consistent with the data sent. Then, the code will loop back the received data. The test situation is as follows: The figure below shows two groups of tests: PC sends: 1234567890, after MCU receives it, loop it back. PC sends: 0987654321, after MCU receives it, debug stops at the breakpoint, you can check the received buffer situation, you can see that the buffer data is correct. Fig 14 Fig 15 Attached are two code packages: (1) Uart_TS_T40D34M40I0R0_miniK312_3.zipEB MCAL command line method After unzip the code, put it in: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins, and then you can compile it directly using the command line : Fig 16 (2)Mcal_UARTDMA_S32K312_RTD400_S32DS.zip:The way to import into S32DS, of course, it already contains the EB project: Fig 17 PS: Add another code, it add the IDLE function, based on the RTD400,  Mcal_UARTDMA_IDLE_S32K312_RTD400_S32DS.zip Test result is:      
查看全文
1 Abstract After learning S32K3 PWM and have written some MCAL codes, this is the first MCAL article record starts with the combination of K344 EMIOS+ICU+TRIMUX+LCU, which can involve comprehensive configurations such as PORT, DIO, EMIOS, interrupt ICU, TRIGMUX, LCU, etc. The board platform is still based on NXP official S32K344EVB, RTD400, and the function is: use two channels of EMIOS0 and one channel of EMIOS1. After one channel of EMIOS 0 outputs PWM, it connects LCU through TRIGUMX to generate a set of complementary PWM, and the other channel can realize hardware interrupt control of PWM duty cycle through SW5 PT26 button. One channel of EMIOS1 is directly connected to the PTA29 onboard red light, and the brightness is gradually changed by changing the PWM duty cycle, and then the breathing light effect is realized by directly changing the on and off cycle. At the same time, when the PWM turns off the red light, the onboard green light is turned on through DIO, and when the PWM turns on the red light, the DIO turns off the onboard green light. Text description is always less intuitive than graphic description, so here is the picture:      Fig 1 2. Function realization This article is based on porting the MCAL code to the S32DS demo. Then, on the S32DS platform, MCAL related modules are configured through EB, and then compiled and downloaded for simulation through S32DS. Of course, if you like the command line mode, you can directly use the xmd file configured by EB, and then compile with VScode. The process is also very simple. This article will not go into details about the command line method.     2.1 Hardware and software platform Board:S32K344EVB,also can use other K3 boards. IDE:S32DS3.5 RTD: K344 RTD 400 MCAL tool: EBtresos Studio 29.0 2.2 Software control process Before talking about the specific MCAL configuration, here is the software flow chart of the functions in this article:                                                                             Fig 2 Here you can see that the default situation is the one configured through MCAL, and then the PWM frequency is also modified in the code, and the PWM duty cycle is modified by keystrokes and loop delays. 2.3 Resource Allocation Overview The hardware resources and functions used in this article are listed as follows: Fig 3 The configuration of emios related buses is as follows: Fig 4 It should be noted here that for the master bus and bus mode in MCL emios, it is necessary to select the appropriate PWM mode and counter bus in the PWM module, otherwise either the configuration will be wrong or the correct PWM waveform cannot be generated. From the official S32K3 RM, you can check the clock channel and bus type: Fig 5 For example, if EMIOS_CH23 is selected in PWM0, then this bus corresponds to bus A, and this clock can be used for all channels, so PWM0 is CH12 and can use Bus A. CH22 corresponds to bus F, and this clock can also be used for all channels, so it is no problem to select Bus F for PWM1 CH4. CH0 corresponds to bus B, and this clock corresponds to channels 0-7, so it can also be used for PWM2 is CH2. When selecting the counter bus clock source for your EMIOS channel, you must consider the channel coverage of the counter bus. In addition to the selection of the counter bus, there is also the PWM mode selection, which is easier to handle. For clock counting up, select OPWMB, and for clock counting up and down, select OPWMCB center-aligned PWM.      In actual use, the mode selection is usually determined based on one's own PWM requirements, and then based on the following RM table: Fig 6 You can find the channel types that the corresponding mode can support, and then select the corresponding channel, counter bus, etc. according to the channel type in Figure 5. With these basic knowledge, we can directly enter the EB configuration. 2.4 EB configuration    Here we list all the modules used in EB tresos related to this article, and focus on the modules that require specific configuration. Fig 7 2.4.1 Dio module The DioPort interface needs to be configured. The main purpose is to configure PTA30, onboard green light, select DioPort Id=1, Dio Channel Id=14. The rules for DioPortId and Dio Channel Id are as follows:     Channel = DioChannelId + DioPortId∗16 For S32K3X4 derivatives – Port AL=0 – Port AH=1 – Port BL=2 – Port BH=3 – Port CL=4 – Port CH=5 – Port DL=6 – Port DH=7 – Port EL=8 – Port EH=9 – Port FL=10 – Port FH=11 – Port GL=12 – Port GH=13 PTA30=>30=DioChannelId(14)+DioPortId*16 2.4.2 Icu module First, configure IcuSiul2, the goal is to enable the input interrupt of onboard SW5, PTB26. PTB26 corresponds to EIRQ[13], Then, the corresponding interrupt situation is as follows: Fig 8 Fig 9 (1) Icu->IcuSiul2->IcuSiul2Channels:13 (2) Icu->IcuChannel configuration is: Fig 10 Select IcuChannelRef as the previously configured IcuSiul2Channels, and add the interrupt notification function: User_EdgeDetect, note that this function is the name of the user interrupt processing function that needs to be added in the code.    (3)Icu->IcuHwInterruptConfigList-> ICU Peripheral ISR Name: SIUL2_0_IRQ_CH_13,IcuIsrEnable enable 2.4.3 Mcl module This module is mainly used to configure emios counting clock, trgmux, and LCU configuration. (1)Mcl->Trgmux Logic Instance->Hardware Instance: TRGMUX_IP_HW_INST_0   (2) Mcl->Trgmux Logic Group: Fig 11 The main purpose is to connect PWM1 Emios0_ch4 to LCU0_IN0 through Trigmux. (3)Mcl->LCU Configuration Here is the configuration of the LCU module. The main function is to configure the logic input and logic output. There is one input IN0 and two outputs OUT0 and OUT1. Fig 12 Fig 13 Fig 14 OUTPUT0  value is 0XAAAA=43690, OUTPUT1 value is 0X5555=21845 The purpose of this is to generate a pair of complementary PWMs from the input PWM. Fig 15 (4)Mcl->Emios Common Add two Emios, EMIOS_0 and EMIOS_1, which means two EMIOS are used. EMIOS0 is configured with two master bus channels: CH_22 and CH_0, and has different mode types, counting up and down and counting up. EMIOS1 is configured with one master bus channel: CH_23, counting up Corresponding to Figure 4. Fig 16 Fig 17 Note that the channel here is not the actual PWM output channel, but the counter bus channel of the PWM channel, which has the ability to provide clocks. 2.4.4 Mcu module   This module is the basis for the entire MCU to configure the clock. When using the default setting of the original RTD PWM demo, there is only one point that needs attention Mcu->McuClockSettingConfig_0->McuClockReferencePoint->McuClockReferencePoint_0->core clock 48MHZ. This clock is the source of the EMIOS clock. With the clock source, it is not difficult to calculate the actual PWM frequency according to the set period. For example, if a 1Khz PWM is required, you can configure period=48M/1K=48000 2.4.5 Platform module Platform->Interrupt Controller->IntCtrlConfig0, enable SIUL_1_IRQn, and add Handler as: SIUL2_EXT_IRQ_8_15_ISR Note that this SIUL2_EXT_IRQ_8_15_ISR is not written randomly, but must correspond to the one in Siul2_Icu_Ip_Irq.c, otherwise an error will be reported. Fig18 Different interrupts have different interrupt service functions. You need to find the function name defined in the code and fill it into EB. EB configuration is as follows: Fig 19 2.4.6 Port module The configuration of 8 pins is as follows: Fig 20 As you can see, there are 3 main EMIOS PWMs, one input interrupt, one output GPIO, and two output LCU complementary PWMs. 2.4.7 Pwm module Mcl configures the counter clock channel of EMIOS. The PWM channels to be output need to be configured in the Pwm module and linked to the MCU clock source and the emios counter bus source in Mcl. (1) Pwm->PwmEmios Add two groups for the corresponding EMIOS modules. For example, this article uses EMIOS0 and EMIOS1, so two need to be added: Fig 21 For PwmEmios_1, there is one channel, and the configuration is as follows: Fig 22 PwmEmiosBusRef: /Mcl/Mcl/MclConfig/EmiosCommon_1/EmiosMclMasterBus_0 Fig 23 As you can see, the busRef of PwmEmios_1 here is Emios_ch_23 in Mcl, that is, BusA. That is to say, the bus reference clock used by EMIOS1_CH12 comes from EMIOS1_CH23, that is, Bus A. There are two channels configured in PwmEmios_0, and the configuration is as follows: Fig 24 Fig 25 The bus reference clock used by EMIOS0_CH4 comes from EMIOS0_CH22, which is Bus F. Another EMIOS0 channel: Fig 26 Fig 27 The bus reference clock used by EMIOS0_CH2 comes from EMIOS0_CH0, that is, Bus B, so select Bus BCDE. At this point, we can clearly understand the relationship between the real PWM output channel and the internal MCL Emios counter bus channel. (2)Pwm->PwmEmios With the specific information of PWM configured above, we can directly configure the PWM channels. There are three channels in total: PWM0, PWM1, PWM2, which are also the flags needed in the code. Fig 28 2.5 main code   #include "Pwm.h" #include "Mcu.h" #include "Port.h" #include "Mcl.h" #include "Platform.h" #include "Dio.h" #include "Icu.h" //#include "check_example.h" #define NUM_BLINK_LED (uint32)10U #define DELAY_TIMER (uint32)5000000U #define MCL_EMIOS_1_CH_23 (uint16)279U #define MCL_EMIOS_0_CH_22 (uint16)22U Mcl_LcuSyncOutputValueType PWM_OutputList[2]; volatile uint8 UserCountIrqCH0; void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer<delay) { DelayTimer++; } DelayTimer=0; } void User_EdgeDetect(void) { /* increment IRQ counter */ UserCountIrqCH0++; if(UserCountIrqCH0 % 2 == 0) { Pwm_SetDutyCycle(PwmChannel_2, 0X6000); } else { Pwm_SetDutyCycle(PwmChannel_2, 0X2000); } } int main(void) { uint8 num_blink = 0U, i = 0; uint16 duty_cnt = 0; UserCountIrqCH0 = 0U; /* Initialize the Mcu driver */ Mcu_Init(&Mcu_Config_VS_0); /* Initialize the clock tree */ Mcu_InitClock(McuClockSettingConfig_0); /* Apply a mode configuration */ Mcu_SetMode(McuModeSettingConf_0); Platform_Init(NULL_PTR); /* Initialize all pins using the Port driver */ Port_Init(&Port_Config_VS_0); /* Initialize Mcl driver */ Mcl_Init(&Mcl_Config_VS_0); /* Initialize the Icu driver */ Icu_Init(NULL_PTR); Icu_EnableEdgeDetection(IcuChannel_0); Icu_EnableNotification(IcuChannel_0); /* Initialize Pwm driver , after that Led on*/ Pwm_Init(&Pwm_Config_VS_0); /* PTA29 duty cycle is 50% */ Pwm_SetDutyCycle(PwmChannel_0, 0X4000); // PTB16,pwm1 , emios0_ch4, use trigmux LCU output 2 Complementarity PWM Mcl_LcuSyncOutputValueType lcuEnable[2U]; lcuEnable[0].LogicOutputId = 0; lcuEnable[0].Value = 1U; lcuEnable[1].LogicOutputId = 1; lcuEnable[1].Value = 1U; Mcl_SetLcuSyncOutputEnable(lcuEnable, 2U); TestDelay(DELAY_TIMER); /* Set new period for all channels used external counter bus */ Mcl_Emios_SetCounterBusPeriod(MCL_EMIOS_1_CH_23, 4800, FALSE); // pwmchannel_0 10Khz Mcl_Emios_SetCounterBusPeriod(MCL_EMIOS_0_CH_22, 1200, FALSE);// for PwmChannel_1, 20Khz // PWM0: 10kHZ //PWM1: 20KHZ //PWM2:1KHZ // PTA29 10kHZ /* PTA29 duty cycle is 50% */ Pwm_SetDutyCycle(PwmChannel_0, 0X4000); /* Setup new duty cycle to the pin*/ Pwm_SetDutyCycle(PwmChannel_1, 0x4000); for(i=0; i <= 10; i++) { duty_cnt = i * 0x800; Pwm_SetDutyCycle(PwmChannel_0, duty_cnt); TestDelay(DELAY_TIMER); } /* Using duty cycle 0% and 100% to Blink LED */ while(1) { /* pwm1 when duty cycle is 75% */ Pwm_SetDutyCycle(PwmChannel_1, 0X6000); //Led off Pwm_SetDutyCycle(PwmChannel_0, 0X0000); //red off Dio_WriteChannel(DioConf_DioChannel_Digital_ledgreenPTA30, STD_HIGH); //green on TestDelay(DELAY_TIMER); /* pwm 1 when duty cycle is 25% */ Pwm_SetDutyCycle(PwmChannel_1, 0X2000); //Led ON Dio_WriteChannel(DioConf_DioChannel_Digital_ledgreenPTA30, STD_LOW); //Green OFF Pwm_SetDutyCycle(PwmChannel_0, 0X8000); //RED ON TestDelay(DELAY_TIMER); num_blink++; } /* De-Initialize Pwm driver */ Pwm_DeInit(); //Exit_Example(TRUE); return 0U; }   3. Test Result After power-on, the onboard red light flashes, then gradually turns bright from off, and flashes alternately with the green light. Test PWM1 PTB16: EMIOS0_CH4, the waveform is 20Khz after stabilization, and the duty cycle changes alternately between 25% and 75%. PWM2 PTB14: EMIOS0_CH2, after stabilization, the frequency is 1KHZ, and as the onboard SW5 is pressed, the duty cycle changes alternately between 25% and 75%. Test PTD3, PTD2, it can be seen that it is a pair of complementary waveforms, and the frequency is the same as PTB16, and the duty cycle change rule is also the same. It can be seen that the key interrupt, 3 main PWM, and 2 LCU PWM in this article are already working. Fig 29 Fig 30  
查看全文
[S32K3 Tools Part] How to use VScode to compile EB MCAL project       For EB configured MCAL code, it is usually based on RTD and then compiled using the command line. When I first started learning, I always opened the relevant files directly to modify them, and then used the window cmd method to type commands. This method is very clumsy. Therefore, this article will show how to use VScode to open and compile a RTD4.0.0 S32K344 MCAL project. Of course, for MCAL EB projects, before compiling, you need to use the EB tool to open the configuration file of the corresponding project, and then close it after the project is generated. 1 VScode tool and configuration VScode download link: https://code.visualstudio.com/Download After downloading, install it. Here are some installation plug-ins I often use:   Fig 1 Fig 2 You can search in extensions and install it directly. 2. Use VScode to compile the RTD MCAL project This article takes RTD4.0.0, SW32K3_S32M27x_RTD_R21-11_4.0.0 as an example, and the platform is the official S32K344-EVB board. The code takes Dio_TS_T40D34M40I0R0 project as an example. In order not to affect the original routine, Dio_TS_T40D34M40I0R0 is copied and saved as Dio_TS_T40D34M40I0R0_vscode 2.1 Use EB tresos generate the configuration Open EB tools, import the project in path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject Fig 3 Double-click someId, then right-click. If you do not need to make custom configurations, just click generate project. Wait for the generation to complete without errors and close the EB IDE. Fig 4 2.2 VScode  open project    First open VScode and select the project path in open Folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344 Fig 5 After opening, you can see that all the files in the path have been put in: Fig 6 You can save the workspace so you don't need to open the folder every time. File->Save workspace as, save to the path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344   2.3 Modify mk file The project mk file needs to be modified to specify gcc, tresos paths, etc. Modify points:project_parameters.mk GCC_DIR = C:/NXP/S32DS.3.5_RTD400/S32DS/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_4.0.0/eclipse/plugins Fig 7 Modify points: check_build_params.mk Delete ifeq ("$(wildcard $(T32_DIR)/bin/windows/t32marm.exe)","") $(error Invalid path set to Trace32. \ The provided path: from project_parameters.mk T32_DIR=$(T32_DIR) is invalid!) Endif Fig 8 Then save all files:File->save all 2.4 Compile the file Terminal->New Terminal Enter the following command: >make generate >make build Fig 9 Fig 10 As you can see, after make build, an elf file has been generated in the out folder. This elf file can be directly downloaded using two methods: (1) S32DS empty project link to elf to download (2) Lauderbach directly download elf file   2.5 debug the generated elf file Since the S32K344-EVB has an onboard opensda tool, we directly use the S32DS empty project to link to the generated main.elf file to download and debug. Create a new S32DS project, and the interface is PE Multilink, then directly change the elf file to main.elf in the debug configuration, and then put the previously generated elf file into the folder of the new S32DS project:  \Debug_FLASH Fig 11 Then, enter debug mode, the results are as follows: Fig 12 As you can see, the chip has entered debug mode and can run successfully. Running at full speed, you can see the onboard red light flashing, so at this point, VSCode has compiled the MCAL code and run successfully.  
查看全文
     In fact, this topic has been written by many people before, and it is well written. However, in actual operation, you may encounter some pitfalls, so this article will not write the article steps in detail, but will provide a real and direct operation video process. The main reference article source link is: https://www.wpgdadatong.com.cn/blog/detail/74936 The method is very useful. I have tried the existing RTD4.0.0 MCAL code and also imported it into my own configured MCAL code. The method is reliable and effective. Platform:     SW32K3_S32M27x_RTD_R21-11_4.0.0 S32DS3.5 EB tresos Studio 29.0 S32K344-EVB Attach the video directly: The main steps are as follows: STEP 1. Create a new S32DS project STEP 2. S32DS project configuration Including folder deletion, addition, filter condition addition, include files, link files, optimization conditions, macro definitions, etc. STEP 3. Create a new EB project Configure a new RTD, or copy the existing RTD configuration to avoid unnecessary problems and errors. STEP 4. Compile and download The following are some related files that need to be copied: MCAL_Plugins->Link Source Resource Filters   Fig 1 Includes   Fig 2 "${ProjDirPath}/Generate/include" "${MCAL_PLUGIN_PATH}/Adc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ae${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/BaseNXP${MCAL_MODULE_NAME_SUFFIX}/header" "${MCAL_PLUGIN_PATH}/BaseNXP${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Can_43_FLEXCAN${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CanIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CanTrcv_43_AE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Crc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CryIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Crypto_43_HSE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Csm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dem${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Det${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dio${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dpga${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EcuM${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Eth_43_GMAC${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthSwt${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthTrcv${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Fee${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Gdu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Gpt${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/I2c${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/I2s${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Icu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Lin_43_LPUART_FLEXIO${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/LinIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/LinTrcv_43_AE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mcl${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mcu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_EEP${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_EXFLS${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_INFLS${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/MemAcc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/MemIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ocotp${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ocu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Os${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/startup/include" "${MCAL_PLUGIN_PATH}/Port${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Pwm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Rm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Rte${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Sent${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Spi${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Uart${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Wdg${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/WdgIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Zipwire${MCAL_MODULE_NAME_SUFFIX}/include"   Preprocessor   Fig  3 S32K3XX S32K344 GCC USE_SW_VECTOR_MODE D_CACHE_ENABLE I_CACHE_ENABLE ENABLE_FPU   Linker   Fig  4 "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/build_files/gcc/linker_flash_s32k344.ld" optimization   Fig 5 -fno-short-enums -funsigned-char -fomit-frame-pointer -fstack-usage   main.c Comment: #include "check_example.h #Exit_Example(TRUE);   Attached code: MCAL_Dio_S32K344_S32DS363_RTD600_CP.zip: RTD MCAL copy to S32DS project MCAL_Dio_S32K312_RTD600_MCUPLL.zip: S32K312 MCU with PLL, add UART printf Others attachment all link the MCAL to RTD install path.
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3xx MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x50_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Results :-- Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20417DAA = 541162922     Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407e64 - 0x00407e38 = 44 bytes      S32K3 FLASH Memory Terminology :--    
查看全文
************************************************************************************************* * Detailed Description: * DCF record disables or enables POR_WDG depending on the POR_WDG_EN macro in main.c. * Find first available location in UTEST, by default, first available address is 0x1B000780 * * NOTE: There is a bug in this RTD version. * Change FLS_MAX_VIRTUAL_SECTOR to 272 in C40_Ip_Cfg.h * ------------------------------------------------------------------------------ * Test HW: : S32K312EVB-Q172 * MCU: : S32K312 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : 3.0.0 * Build Version : S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331 *************************************************************************************************
查看全文
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K324 SPI Transmit & Receive, using Interrupt :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-I2C-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1818631 Example S32K324 Bootloader to Application Jump DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-Bootloader-to-Application-Jump-DS3-5-RTD300/ta-p/1832649 Example S32K324 STANDBY wake up using GPIO Switch DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-STANDBY-wake-up-using-GPIO-Switch-DS3-5-RTD300/ta-p/1892849 Example S32K324 STANDBY wake up using CAN-0-RX and GPIO Switch DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-STANDBY-wake-up-using-CAN-0-RX-and-GPIO-Switch/ta-p/1911972
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the Bootloader Jump to Application.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************   Jump is decided based on the boot_header, size we use to jump to the RESET handler:--   Cortex M-7 Interrupt vector table, RESET handler is 4 byte offset from starting of vector table :--   // Reset_Handler+1  --> required in IVT, to avoid hard fault As per Arm®v7-M Architecture Reference Manual  --> DDI0403E_e_armv7m_arm.pdf         How to burn elf file of both application & bootloader code :--  
查看全文
S32K344 - FOC integrated with FreeRTOS This example demonstrates a 3-phase Permanent Magnet Synchronous Motor (PMSM) vector control (Field Oriented Control - FOC) drive with 2- shunt current sensing with and without position sensor integrated in FreeRTOS environment. This design serves as an example of motor control design using NXP S32K3 automotive family. Example was designed on S32K344 Brushless Direct Current and Permanent Magnet Synchronous Motor Control Development Kit.  C-project based examples are part of MCSPTE1AK344 Development Kit Application Software. An innovative drivers set, Real-Time Drivers (RTD),are used to configure and control the MCU. It complies with Automotive-SPICE, ISO 26262, ISO 9001 and IATF 16949. Production-ready Automotive Math and Motor Control Library set provides essential building blocks for algorithm. FreeMASTER is used as useful run-time debugging tool. Application software contains:  MCSPTE1AK344_PMSM_FOC_2Sh_ll_FreeRTOS - Low-level drivers of RTD and S32 Design Studio Configuration Tools (S32CT) are used to demonstrate non-AUTOSAR approach. Since the motor control structure of the example is similar to dual shunt example, detailed description of the example can be found in application note AN13767 and FreeRTOS related part in AN12881 .
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the LPI2C-0 as MASTER and LPI2C-1 SLave, using DMA for TX & RX for the S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文