S32K ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K Knowledge Base

ラベル

ディスカッション

ソート順:
Hi all,   Many customers complained about the K3 FlexIO I2S can not support continuous transferring because there is a gap time between 2 times of invoking SendData. This gap time will break the audio continuity and bring jitters. It is gapped by the transfer API closing and re-entry time cost.   To avoid this gap and implement a real continuous transferring, we made some changes with eDMA configurations. Finally, it works!   Besides, we also enabled eDMA half-complete interrupt to support double-buffer (ping-pong buffer) operation for user's further development.   Attachments are the example projects and corresponding introduction slides, please kindly check if you are interested in. Any problem, just let me know. Welcome your comments here.   Best Regards, Shuailin Li NXP GPIS, AE   --- Additional topic: Regarding the use of S32K3 SAI I2S to receive continuous audio data, user can use DMA continuous or S/G mode + ping-pong buffer. For details, please refer to the attached file & related codes (Use Case Share-S32K3 SAI I2S is used for audio data reception.pdf). For reference only.
記事全体を表示
*******************************************************************************************************  Detailed Description:  Configures the MCU to run system clock from XOSC.  LPUART1 is set to respond to LIN header sent from master.  Based on ID received the LPUART1 either receive frame's data and compare checksum  or publish requested data with calculated checksum. Enhanced checksum is used.  Interrupt is used for RX and TX operation and 2 versions of interrupt routine are available.  VER 1 ... during response transmission receiver disabled and transmit interrupt enabled  VER 2 ... during response transmission receiver is kept enabled  ------------------------------------------------------------------------------  Test HW: S32K116 EVB-Q048  MCU: PS32K116LAM 0N96V  Fsys: 40MHz  Debugger: Lauterbach  Target: internal_FLASH ******************************************************************************************************
記事全体を表示
****************************************************************************************************************** Detailed Description: The example code shows CMP in Round-robin mode. CMP is clocked (125kHz) and triggered (80ms) by LPTMR, operates in VLPS. Input channels are CMP0_IN1 (PTA1), CMP0_IN2 (PTC4), CMP0_IN3 (PTE8), CMP0_IN4 (PTC3). The initial state of CMP outputs is 0 (Input analog pins < DAC input (Vin1/2)) The input pins are pulled down internally for debugging purposes. CPM will wake up the MCU if an input has changed. BLUE LED flashes 1x if CMP_IN1 has changed, 2x CMP0_IN2, 3x CMP0_IN3, 4x CMP0_IN4. After that, the MCU goes back to VLPS. ------------------------------------------------------------------------------------------------------------------------------------- Test HW: S32144EVB-Q100X MCU: S32K144 (0N47T) Debugger: S32DS2.0, OpenSDA Target: internal_FLASH ******************************************************************************************************************
記事全体を表示
【RTD400 MCAL 3】 K312 MCU clock system configuration 1. Abstract This document is talking about how to configure the clock system in the MCU of the K3 chip MCAL. This topic was always disdainful to talk about when I was doing LLD before, because the clock system of K3 is too simple, with internal fast and slow clock sources, external fast and slow clock sources, a PLL multiplier, and then various core peripherals to share. K3's RM even made a few options to frame the rules. From the perspective of LLD, especially the perspective of S32DS CT configuration, it is even more concise and clear. Here is a CT picture to show it:   Fig 1     Fig 2 With such a clock system, you can generate code with just a few taps and pokes. However, LLD is too free, and MCAL often encounters problems. Therefore, I decided to spend some time to understand the entire clock system of this MCAL MCU. This article takes K312 as an example to explain. Other K3 series are similar. 2. Clock system theory and configuration 2.1 K312 clock system From the clock chapter of RM, you can see the whole system block diagram:     Fig 3 This block diagram clearly shows the situation of each part. There are four clock sources: Internal fast clock FIRC: 48MHz, +/-5% error, maximum startup time 25us Internal slow clock SIRC: 32KHz, +/-10% error, maximum startup time 3ms External fast clock FXOSC: 8-40MHz, startup stabilization time FXOSC_CTRL[EOCV] × 128 External slow clock SXOSC: 32.768KHz, startup stabilization time SXOSC_CTRL[EOCV] x 128 One PLL: input 8-40MHZ, VOC output 640M-1280Mhz, PLL_PHIn_CLK output 25-480MHz. MUX_0: Output CORE_CLK, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK MUX_1: Output system timer STM0_CLK MUX_3: Output FLEXCAN0-2 clock MUX_4: Output FLEXCAN3-5 clock MUX_5: Output CLKOUT_STANDBY MUX_6: Output CLKOUT_RUN MUX_11: Output TRACE_CLK RTC_CLK: RTC clock 2.1.1 PLL From the PLL perspective, we need to know which values ​​the frequency multiplier is related to, which can be calculated using the following formula:     Fig 4 If it is an integer, the red box in the above figure is the common method, and this article will also use the above method to configure. PLL_PHI is the clock output by the final PLL, which is provided to the MC corresponding to other MUXs for selection. 2.1.2 MUX_0 System The MUX_0 system with details can be seen from RM:     Fig 5 As you can see, the clock source of MUX_0 can be two types: PLL or internal FIRC. Then the core clock can be generated later, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK. So what is the specific frequency of the generated clock? In principle, it can meet the maximum clock corresponding to each module, but the K3 series also makes some option recommendations. For example, K312 recommends using option B mode when RUN, especially the HSE clock, which usually needs to strictly meet the option recommendation. 2.1.3 MUX_6 Clock output In order to check the corresponding clock situation in the chip, the corresponding clock can be output through the CLKOUT pin. The CLKOUT pin can correspond to the selection of multiple clock sources. The specific situation is as follows:     Fig 6 The yellow content in the figure is what K312's CLKOUT_RUN can support. After the clock is configured, the corresponding clock will be selected to test whether the output is consistent with the configuration. 2.1.4 option B Recommended Solution In this article, K312 will configure the clock of option B in EB.     Fig 7 2.2 EB configuration        First, create a new K312 EB project. For the specific creation method, please refer to the previous article: [S32K3 Tools Part] How to port RTD's existing MCAL demo to other K3 chips This article will focus on the clock configuration corresponding to the MCU module based on RTD400 MCAL. For MCU configuration, two documents need to be consulted as reference books: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Mcu_TS_T40D34M40I0R0\doc: RTD_MCU_UM.pdf and RTD_MCU_IM.pdf If you don’t know how to configure, just follow the default values ​​recommended by the document. The following figure is an overview of the MCU. The main configured modules have the following three components: General, McuClockSettingConfig, McuModeSettingConf     Fig 8 2.2.1 General configuration In addition to Figure 8, you need to turn on the internal and external fast and slow clock control and PLL control, and add the corresponding API, as well as the crystal oscillator frequency. If this is not turned on, the corresponding configuration later will not be able to be configured.     Fig 9 2.2.2 McuClockSettingConfig configuration        This is the core area of ​​MCU clock configuration, which includes clock source, PLL, and various MUX conditions. First, you need to add a clock configuration:     Fig 10 Click in and there will be detailed configuration:     Fig 11 There are 17 items in total. You can keep the default configuration for options 1 and 6. Since the board does not connect to the external slow crystal oscillator 5, it is not configured. The rest should be configured according to the actual situation. The following explains them one by one: 2.2.2.1 McuFIRC configuration    Internal fast clock, 48MHz:     Fig 12 2.2.2.2 McuSIRC configuration Internal slow clock 32Khz     Fig 13 2.2.2.3 McuFXOSC configuration External crystal oscillator 16MHZ, fill in according to the actual connection situation.     Fig 14 2.2.2.4 McuCgm0ClockMux0 configuration Mux0 configuration, here are configured core clock, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE, DCM_CLK, is to meet the optionB requirements, and the clock comes from PLL_PHI0_CLK. When actually configuring, first configure the PLL clock to output the correct PLL_PHI0_CLK, PLL_PHI1_CLK clock.     Fig 15 2.2.2.5 McuCgm0ClockMux1 configuration     Fig 16 It can be configured according to the clock source required by the actual module. 2.2.2.6 McuCgm0ClockMux3 configuration Configure the clock source of the FLEXCAN0-2 module:     Fig 17 2.2.2.7 McuCgm0ClockMux4 configuration Configure the clock source of the FLEXCAN3-5 module:     Fig 18 2.2.2.8 McuCgm0ClockMux5 configuration Configure the clock source of the CLKOUT_STANBY module:     Fig 19 2.2.2.9 McuCgm0ClockMux6 configuration Configure the clock source of the CLKOUT_RUN module     Fig 20 2.2.2.10 McuCgm0ClockMux11 configuration Configure the clock source of the TRACE_CLK module     Fig 21 2.2.2.11 McuRtcClockSelect configuration Configure the clock source of the RTC module     Fig 22 2.2.2.12 McuPLL configuration Configure the clock source of the PLL module     Fig 23 2.2.2.13 McuClockReferencePoint configuration Configure the reference clock and the clock source selection interface of the peripheral modules.     Fig 24 At this point, the clock configuration is complete. For verification, you can use the CLKOUT_RUN output to output the corresponding clock to pin PTD10 for viewing. 2.2.3 McuModeSettingConf  configuration In Mcu's McuModeSettingConf->McuPeripheral, you need to turn on the peripherals you want to use:     Fig 25 2.2.4 PORT  configuration Because the internal clock needs to be output to CLKOUT_RUN, K312's PTD10 MSCR106 is checked, so the PORT pin is added as follows:     Fig 26 3. Test Result Next, on the S32K312-EVB board, we modify the clock source of EB's CLKOUT_RUN to test whether the clock matches the configuration. Commonly used MCU-related drivers are as follows:     Fig 27 The calling sequence of system startup MCU initialization is as follows: 1). Mcu_Init() 2). Mcu_InitClock() 3). Mcu_GetPllStatus() - Till PLL is locked. 4). Mcu_DistributePllClock() 5). Mcu_SetMode() 6). Mcu_InitRamSection() - If required The corresponding main code is as follows: #include "Mcu.h" #include "Mcu_Cfg.h" #include "Port.h" #include "Dio.h" #include "Port_Cfg.h" #include "Platform.h" void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } /** * @brief Main function of the example * @details Initialize the used drivers and uses the Icu * and Dio drivers to toggle a LED on a push button */ int main(void) { uint8 count = 0U; uint8 u8TimeOut = 100U; /* Initialize the Mcu driver */ #if (MCU_PRECOMPILE_SUPPORT == STD_ON) Mcu_Init(NULL_PTR); #elif (MCU_PRECOMPILE_SUPPORT == STD_OFF) Mcu_Init(&Mcu_Config_VS_0); #endif /* (MCU_PRECOMPILE_SUPPORT == STD_ON) */ /* Initialize the clock tree and apply PLL as system clock */ Mcu_InitClock(McuClockSettingConfig_0); #if (MCU_NO_PLL == STD_OFF) while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() ) { } Mcu_DistributePllClock(); #endif /* Apply a mode configuration */ Mcu_SetMode(McuModeSettingConf_0); /* Initialize all pins using the Port driver */ Port_Init(NULL_PTR); /* Initialize Platform driver */ Platform_Init(NULL_PTR); while (count++ < 10) { Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_HIGH); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_HIGH); TestDelay(5000000); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_LOW); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_LOW); TestDelay(5000000); } // Exit_Example(TRUE); return (0U); } #ifdef __cplusplus } #endif 3.1 CLKOUT FIRC_CLK DIV2     Fig 28 It can be seen that the original 48Mhz clock of FIRC is divided by 2 and the clock waveform of 24Mhz is obtained, which is correct! 3.2 CLKOUT SIRC_CLK DIV2     Fig 29 It can be seen that the original 32Khz clock of SIRC is divided by 2 and the clock waveform of 16khz is obtained, which is correct! 3.3 CLKOUT FXOSC_CLK DIV10     Fig 30 It can be seen that the original 16Mhz clock of FXOSC is divided by 10 and the clock waveform of 1.6Mhz is obtained. 3.4 CLKOUT PLLPH0 CLK DIV10     Fig 31 It can be seen that the original 120Mhz clock of PLLPH0 is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.5 CLKOUT CORE CLK DIV10     Fig 32 It can be seen that the original 120Mhz clock of CORE is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.6 CLKOUT PLLPH1 CLK DIV4     Fig 33 It can be seen that the original 48Mhz clock of PLLPH1 is divided by 4 and the 12Mhz clock waveform is obtained. 3.7 CLKOUT HSE CLK DIV10     Fig 34 It can be seen that the original 60Mhz clock of HSE is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.8 CLKOUT AIPS_PLAT CLK DIV10     Fig 35 It can be seen that the original 60Mhz clock of AIPS_PLAT_CLK is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.9 CLKOUT AIPS_SLOW CLK DIV10     Fig 36 It can be seen that the original 30Mhz clock of AIPS_SLOW_CLK is divided by 10 and the clock waveform of 3Mhz is obtained, which is correct.  
記事全体を表示
This article is written in Chinese. It is mainly for the disty and mass market customers in local China. It is useful for the the developers who is newly in touch with S32K1, and will help them install several software of S32K1, otherwise it may waste a lot of time.     S32DS中快速搭建S32K1的开发环境 一.背景 我最近换装了新电脑,需要重新安装S32DS,发现存在很多问题。尤其是对比之前的安装过程,发现官网的很多链接已经失效,甚至有一定的迷惑性。 最新的S32K1安装包比较隐蔽,而且安装存在前后依赖,对于刚接触NXP S32系列的新手非常不友好,所以写这篇文档总结一下典型的问题和解决方法。 同时也希望提供一个check的思路和步骤,在后续新版本发布时,升级IDE的时候更方便找到合适的安装包。 二.S32DS中各个包依赖关系解析 在S32DS中,每一个系列的MCU,总共需要安装两个插件包,一个是基础依赖包,一个是SDK(也叫RTD,同一个意思)。 1.基础依赖包 这个包对应S32DS版本,比如当前的3.4.3,官网可以下载离线版,一般大小在3GB左右,会更新S32DS中的很多组件,如下图1所示:            图1 尤其需要关注图1中红框的内容,没有这个development package的话,是无法进行对应MCU的debug。 图1中安装的包,对应到S32DS中安装的内容如图2所示:            图2 2.RTD安装包(与SDK同义) 这个包对应于RTD版本,也会标识AutoSAR的版本,比如最新的2.0.0,AutoSar 4.4,如图3所示:           图3 基础依赖包与RTD安装包存在前后依赖关系,如果不安装基础依赖包直接安装RTD,在安装时会报错。另外,我们下载的RTD包,即使写明是K3,里面也会包含K1的RTD,这点需要注意。如果此时还没有装K1的development package,就会出错。 三.S32K1开发环境搭建 官网对于S32K3的软件划分为standard software和reference software,其中S32DS和基础依赖包在standard software中,可以很方便的找到。 但S32K1的官网却仅有一个reference software,页面也只能找到几个RTD(或SDK)链接:                                                                             图4 这里面所有的链接都不是我们需要的,全是RTD。问题就出在这里,K1的网页中没有K1的基础依赖包!而前面讲过,缺基础依赖包会导致RTD也无法安装。经过我研究,K1的基础依赖包隐藏的非常深,可以通过两个方法找到: 从S32K1的reference software进去,然后重新点击product list,如下图5所              图5         进入如下页面,如图6所示,这里最能看出来,针对K1的界面很不友好,需要点最底下的NXP Software.              图6 在NXP.com官网首页搜索栏直接搜S32DS,找到S32 Design Studio for S32 Platform(注意不要选成for ARM或或者for PowerPC),从S32DS的主界面进入,然后一直下拉,找到S32DS service pack 1,这个才是K1的,如图7所示:                 图7 这个链接更加隐蔽,要在40多个选项里挨个找。   经过上面两个方法,都可以进入图8所示的界面,然后再按图8所示操作:              图8   这回终于到了最终可以下载S32K1基础依赖包的地方,如图9所示。我们需要重点关注一下命名,SW32开头的,会包含所有S32的development package,包括K1,K3,G;SW32K1开头的,仅有K1,同理如果你在K3的界面中,可以看到SW32K3开头的。            图9 下载最新版本的S32K1基础依赖包,然后再安装RTD,大功告成。
記事全体を表示
******************************************************************************************** * Detailed Description: * LPIT_ch0 triggers DMA_ch0 periodically (1ms). * Every trigger starts a minor DMA loop (8 bytes) transfer to the LPSPI1 TX FIFO. * There are 8 minor loops per one major loop (64 bytes in 8ms). * LPSPI1 sends two 32bit frames every 1ms. * LPSPI1 RX data are masked, they are not stored in the RX FIFO. * ------------------------------------------------------------------------------ * Test HW: S32K144EVB-Q100 * MCU: S32K144 0N57U * Debugger: S32DS 2.2, OpenSDA * Target: internal_FLASH ********************************************************************************************
記事全体を表示
************************************************************************************************************************** * Detailed Description: * * Connect PTC24 (PWM) to PTC25 (IC) * * PWM signal generated by EMIOS_1_ch0 (in OPWFMB mode) is measured by EMIOS_1_ch_1 (IPWM mode). * * EMIOS_1 global global clock (core clock = 48MHz) prescaled in EMIOS_Mcl driver (/48) = 1MHz. * * BUS_A generated by EMIOS_1_ch_23 * Tick = 10us (1MHz global clock prescaled by 10 = 100kHz) * * PWM (OPWFMB), EMIOS_1_ch_0, PTC24 * Tick = 10us (1MHz global clock prescaled by 10 = 100kHz) * * IC (IPWM), EMIOS_1_ch_1, PTC25 * Clocked by BUS_A * Tick = 10us * * ------------------------------------------------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K344 * Debugger: S32DS 3.4, PEMicro Multilink rev.C * Target: internal_FLASH **************************************************************************************************************************
記事全体を表示
1 Abstract After learning S32K3 PWM and have written some MCAL codes, this is the first MCAL article record starts with the combination of K344 EMIOS+ICU+TRIMUX+LCU, which can involve comprehensive configurations such as PORT, DIO, EMIOS, interrupt ICU, TRIGMUX, LCU, etc. The board platform is still based on NXP official S32K344EVB, RTD400, and the function is: use two channels of EMIOS0 and one channel of EMIOS1. After one channel of EMIOS 0 outputs PWM, it connects LCU through TRIGUMX to generate a set of complementary PWM, and the other channel can realize hardware interrupt control of PWM duty cycle through SW5 PT26 button. One channel of EMIOS1 is directly connected to the PTA29 onboard red light, and the brightness is gradually changed by changing the PWM duty cycle, and then the breathing light effect is realized by directly changing the on and off cycle. At the same time, when the PWM turns off the red light, the onboard green light is turned on through DIO, and when the PWM turns on the red light, the DIO turns off the onboard green light. Text description is always less intuitive than graphic description, so here is the picture:      Fig 1 2. Function realization This article is based on porting the MCAL code to the S32DS demo. Then, on the S32DS platform, MCAL related modules are configured through EB, and then compiled and downloaded for simulation through S32DS. Of course, if you like the command line mode, you can directly use the xmd file configured by EB, and then compile with VScode. The process is also very simple. This article will not go into details about the command line method.     2.1 Hardware and software platform Board:S32K344EVB,also can use other K3 boards. IDE:S32DS3.5 RTD: K344 RTD 400 MCAL tool: EBtresos Studio 29.0 2.2 Software control process Before talking about the specific MCAL configuration, here is the software flow chart of the functions in this article:                                                                             Fig 2 Here you can see that the default situation is the one configured through MCAL, and then the PWM frequency is also modified in the code, and the PWM duty cycle is modified by keystrokes and loop delays. 2.3 Resource Allocation Overview The hardware resources and functions used in this article are listed as follows: Fig 3 The configuration of emios related buses is as follows: Fig 4 It should be noted here that for the master bus and bus mode in MCL emios, it is necessary to select the appropriate PWM mode and counter bus in the PWM module, otherwise either the configuration will be wrong or the correct PWM waveform cannot be generated. From the official S32K3 RM, you can check the clock channel and bus type: Fig 5 For example, if EMIOS_CH23 is selected in PWM0, then this bus corresponds to bus A, and this clock can be used for all channels, so PWM0 is CH12 and can use Bus A. CH22 corresponds to bus F, and this clock can also be used for all channels, so it is no problem to select Bus F for PWM1 CH4. CH0 corresponds to bus B, and this clock corresponds to channels 0-7, so it can also be used for PWM2 is CH2. When selecting the counter bus clock source for your EMIOS channel, you must consider the channel coverage of the counter bus. In addition to the selection of the counter bus, there is also the PWM mode selection, which is easier to handle. For clock counting up, select OPWMB, and for clock counting up and down, select OPWMCB center-aligned PWM.      In actual use, the mode selection is usually determined based on one's own PWM requirements, and then based on the following RM table: Fig 6 You can find the channel types that the corresponding mode can support, and then select the corresponding channel, counter bus, etc. according to the channel type in Figure 5. With these basic knowledge, we can directly enter the EB configuration. 2.4 EB configuration    Here we list all the modules used in EB tresos related to this article, and focus on the modules that require specific configuration. Fig 7 2.4.1 Dio module The DioPort interface needs to be configured. The main purpose is to configure PTA30, onboard green light, select DioPort Id=1, Dio Channel Id=14. The rules for DioPortId and Dio Channel Id are as follows:     Channel = DioChannelId + DioPortId∗16 For S32K3X4 derivatives – Port AL=0 – Port AH=1 – Port BL=2 – Port BH=3 – Port CL=4 – Port CH=5 – Port DL=6 – Port DH=7 – Port EL=8 – Port EH=9 – Port FL=10 – Port FH=11 – Port GL=12 – Port GH=13 PTA30=>30=DioChannelId(14)+DioPortId*16 2.4.2 Icu module First, configure IcuSiul2, the goal is to enable the input interrupt of onboard SW5, PTB26. PTB26 corresponds to EIRQ[13], Then, the corresponding interrupt situation is as follows: Fig 8 Fig 9 (1) Icu->IcuSiul2->IcuSiul2Channels:13 (2) Icu->IcuChannel configuration is: Fig 10 Select IcuChannelRef as the previously configured IcuSiul2Channels, and add the interrupt notification function: User_EdgeDetect, note that this function is the name of the user interrupt processing function that needs to be added in the code.    (3)Icu->IcuHwInterruptConfigList-> ICU Peripheral ISR Name: SIUL2_0_IRQ_CH_13,IcuIsrEnable enable 2.4.3 Mcl module This module is mainly used to configure emios counting clock, trgmux, and LCU configuration. (1)Mcl->Trgmux Logic Instance->Hardware Instance: TRGMUX_IP_HW_INST_0   (2) Mcl->Trgmux Logic Group: Fig 11 The main purpose is to connect PWM1 Emios0_ch4 to LCU0_IN0 through Trigmux. (3)Mcl->LCU Configuration Here is the configuration of the LCU module. The main function is to configure the logic input and logic output. There is one input IN0 and two outputs OUT0 and OUT1. Fig 12 Fig 13 Fig 14 OUTPUT0  value is 0XAAAA=43690, OUTPUT1 value is 0X5555=21845 The purpose of this is to generate a pair of complementary PWMs from the input PWM. Fig 15 (4)Mcl->Emios Common Add two Emios, EMIOS_0 and EMIOS_1, which means two EMIOS are used. EMIOS0 is configured with two master bus channels: CH_22 and CH_0, and has different mode types, counting up and down and counting up. EMIOS1 is configured with one master bus channel: CH_23, counting up Corresponding to Figure 4. Fig 16 Fig 17 Note that the channel here is not the actual PWM output channel, but the counter bus channel of the PWM channel, which has the ability to provide clocks. 2.4.4 Mcu module   This module is the basis for the entire MCU to configure the clock. When using the default setting of the original RTD PWM demo, there is only one point that needs attention Mcu->McuClockSettingConfig_0->McuClockReferencePoint->McuClockReferencePoint_0->core clock 48MHZ. This clock is the source of the EMIOS clock. With the clock source, it is not difficult to calculate the actual PWM frequency according to the set period. For example, if a 1Khz PWM is required, you can configure period=48M/1K=48000 2.4.5 Platform module Platform->Interrupt Controller->IntCtrlConfig0, enable SIUL_1_IRQn, and add Handler as: SIUL2_EXT_IRQ_8_15_ISR Note that this SIUL2_EXT_IRQ_8_15_ISR is not written randomly, but must correspond to the one in Siul2_Icu_Ip_Irq.c, otherwise an error will be reported. Fig18 Different interrupts have different interrupt service functions. You need to find the function name defined in the code and fill it into EB. EB configuration is as follows: Fig 19 2.4.6 Port module The configuration of 8 pins is as follows: Fig 20 As you can see, there are 3 main EMIOS PWMs, one input interrupt, one output GPIO, and two output LCU complementary PWMs. 2.4.7 Pwm module Mcl configures the counter clock channel of EMIOS. The PWM channels to be output need to be configured in the Pwm module and linked to the MCU clock source and the emios counter bus source in Mcl. (1) Pwm->PwmEmios Add two groups for the corresponding EMIOS modules. For example, this article uses EMIOS0 and EMIOS1, so two need to be added: Fig 21 For PwmEmios_1, there is one channel, and the configuration is as follows: Fig 22 PwmEmiosBusRef: /Mcl/Mcl/MclConfig/EmiosCommon_1/EmiosMclMasterBus_0 Fig 23 As you can see, the busRef of PwmEmios_1 here is Emios_ch_23 in Mcl, that is, BusA. That is to say, the bus reference clock used by EMIOS1_CH12 comes from EMIOS1_CH23, that is, Bus A. There are two channels configured in PwmEmios_0, and the configuration is as follows: Fig 24 Fig 25 The bus reference clock used by EMIOS0_CH4 comes from EMIOS0_CH22, which is Bus F. Another EMIOS0 channel: Fig 26 Fig 27 The bus reference clock used by EMIOS0_CH2 comes from EMIOS0_CH0, that is, Bus B, so select Bus BCDE. At this point, we can clearly understand the relationship between the real PWM output channel and the internal MCL Emios counter bus channel. (2)Pwm->PwmEmios With the specific information of PWM configured above, we can directly configure the PWM channels. There are three channels in total: PWM0, PWM1, PWM2, which are also the flags needed in the code. Fig 28 2.5 main code   #include "Pwm.h" #include "Mcu.h" #include "Port.h" #include "Mcl.h" #include "Platform.h" #include "Dio.h" #include "Icu.h" //#include "check_example.h" #define NUM_BLINK_LED (uint32)10U #define DELAY_TIMER (uint32)5000000U #define MCL_EMIOS_1_CH_23 (uint16)279U #define MCL_EMIOS_0_CH_22 (uint16)22U Mcl_LcuSyncOutputValueType PWM_OutputList[2]; volatile uint8 UserCountIrqCH0; void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer<delay) { DelayTimer++; } DelayTimer=0; } void User_EdgeDetect(void) { /* increment IRQ counter */ UserCountIrqCH0++; if(UserCountIrqCH0 % 2 == 0) { Pwm_SetDutyCycle(PwmChannel_2, 0X6000); } else { Pwm_SetDutyCycle(PwmChannel_2, 0X2000); } } int main(void) { uint8 num_blink = 0U, i = 0; uint16 duty_cnt = 0; UserCountIrqCH0 = 0U; /* Initialize the Mcu driver */ Mcu_Init(&Mcu_Config_VS_0); /* Initialize the clock tree */ Mcu_InitClock(McuClockSettingConfig_0); /* Apply a mode configuration */ Mcu_SetMode(McuModeSettingConf_0); Platform_Init(NULL_PTR); /* Initialize all pins using the Port driver */ Port_Init(&Port_Config_VS_0); /* Initialize Mcl driver */ Mcl_Init(&Mcl_Config_VS_0); /* Initialize the Icu driver */ Icu_Init(NULL_PTR); Icu_EnableEdgeDetection(IcuChannel_0); Icu_EnableNotification(IcuChannel_0); /* Initialize Pwm driver , after that Led on*/ Pwm_Init(&Pwm_Config_VS_0); /* PTA29 duty cycle is 50% */ Pwm_SetDutyCycle(PwmChannel_0, 0X4000); // PTB16,pwm1 , emios0_ch4, use trigmux LCU output 2 Complementarity PWM Mcl_LcuSyncOutputValueType lcuEnable[2U]; lcuEnable[0].LogicOutputId = 0; lcuEnable[0].Value = 1U; lcuEnable[1].LogicOutputId = 1; lcuEnable[1].Value = 1U; Mcl_SetLcuSyncOutputEnable(lcuEnable, 2U); TestDelay(DELAY_TIMER); /* Set new period for all channels used external counter bus */ Mcl_Emios_SetCounterBusPeriod(MCL_EMIOS_1_CH_23, 4800, FALSE); // pwmchannel_0 10Khz Mcl_Emios_SetCounterBusPeriod(MCL_EMIOS_0_CH_22, 1200, FALSE);// for PwmChannel_1, 20Khz // PWM0: 10kHZ //PWM1: 20KHZ //PWM2:1KHZ // PTA29 10kHZ /* PTA29 duty cycle is 50% */ Pwm_SetDutyCycle(PwmChannel_0, 0X4000); /* Setup new duty cycle to the pin*/ Pwm_SetDutyCycle(PwmChannel_1, 0x4000); for(i=0; i <= 10; i++) { duty_cnt = i * 0x800; Pwm_SetDutyCycle(PwmChannel_0, duty_cnt); TestDelay(DELAY_TIMER); } /* Using duty cycle 0% and 100% to Blink LED */ while(1) { /* pwm1 when duty cycle is 75% */ Pwm_SetDutyCycle(PwmChannel_1, 0X6000); //Led off Pwm_SetDutyCycle(PwmChannel_0, 0X0000); //red off Dio_WriteChannel(DioConf_DioChannel_Digital_ledgreenPTA30, STD_HIGH); //green on TestDelay(DELAY_TIMER); /* pwm 1 when duty cycle is 25% */ Pwm_SetDutyCycle(PwmChannel_1, 0X2000); //Led ON Dio_WriteChannel(DioConf_DioChannel_Digital_ledgreenPTA30, STD_LOW); //Green OFF Pwm_SetDutyCycle(PwmChannel_0, 0X8000); //RED ON TestDelay(DELAY_TIMER); num_blink++; } /* De-Initialize Pwm driver */ Pwm_DeInit(); //Exit_Example(TRUE); return 0U; }   3. Test Result After power-on, the onboard red light flashes, then gradually turns bright from off, and flashes alternately with the green light. Test PWM1 PTB16: EMIOS0_CH4, the waveform is 20Khz after stabilization, and the duty cycle changes alternately between 25% and 75%. PWM2 PTB14: EMIOS0_CH2, after stabilization, the frequency is 1KHZ, and as the onboard SW5 is pressed, the duty cycle changes alternately between 25% and 75%. Test PTD3, PTD2, it can be seen that it is a pair of complementary waveforms, and the frequency is the same as PTB16, and the duty cycle change rule is also the same. It can be seen that the key interrupt, 3 main PWM, and 2 LCU PWM in this article are already working. Fig 29 Fig 30  
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR and BCTU IP Driver for the S32K3xx MCU.  The example uses the PIT0 trigger to trigger BCTU conversion list to  perform  conversions on ADC1.  ADC channels  are selected to be converted on  ADC-1:  ADC1: P0, p1, p2, p3, p4, p5, p6, S10  Converted results from  BCTU_ADC_DATA_REG are moved by DMA into result array.  ADC channel S10 is connected to board's potentiometer.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Set PIT Freeze Enable :--- All channels are for ADC-1 , in BCTU list :--     "NEW DATA DMA enable mask" :-- controls These bit field in MCR register     "ADC target mask" :-- It controls "ADC_SEL " bit field in "Trigger Configuration (TRGCFG_0 - TRGCFG_71)" for single conversions you can enable only one instance so the possible values for target mask: 1 (0b001) ADC0 2 (0b010) ADC1 3 (0b100) ADC2| for list of conversions we can enable also parallel con version for example 3 (0b011) parallel conversion of ADC0 and ADC1 The trigger is configured as a list of parallel conversions ADC0, ADC1 in “Adc Target Mask”. List of ADC channels is defined in “BCTU List Items” while order is given by the “Adc Target Mask”: BctuListItems_0 is ADC0, BctuListItems_1 is ADC1 etc.      
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR and BCTU IP Driver for the S32K3xx MCU.  The example uses the PIT0 trigger to trigger BCTU conversion list to  perform parallel conversions on ADC0/ADC1. Three ADC channels  are selected to be converted on each ADC:  ADC0: S8 , P0, S8  ADC1: S10, S13, S17  Converted results from BCTU FIFO are moved by DMA into result array.  ADC channel S10 is connected to board's potentiometer, and converted value is  used to dim board's LED.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: Lauterbach * Target: internal_FLASH ********************************************************************************
記事全体を表示
[S32K3 Tools Part] How to port RTD's existing MCAL demo to other K3 chips  1. Abstract     From the release notes of NXP's RTD4.0.0, we can see that the supported chip models are very complete: Fig 1 From this point, we can know that RTD4.0.0 can cover all S32K3 series chips. But if you want a ready-made demo, such as MCAL demo, you can see it under the ready-made demo path, for example: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0\examples\EBT Just S32K344,S32K358,S32K388,S32K396,S32M276。 Therefore, if you use other S32 chips, such as K312, in actual use, although it is within the range supported by RTD, but there is no ready-made demo to use, you need to do the porting by yourself. This article will explain how to port the RTD4.0.0 K344 MCAL demo to S32K312 and configure the corresponding EB project. First, implement the execution in the command line. After success, port the working MCAL code EB project to S32DS. 2. Platform and migration steps 2.1 Platform Description This article is based on RTD4.0.0: SW32K3_S32M27x_RTD_R21-11_4.0.0 For other versions with patch or HF, the operation process is the same! Hardware platform: S32K312 mini EVB or S32K312EVB Other official EVBs, such as S32K31XEVB, or the customer's own S32K3 hardware board also have the same steps. Due to the lack of official EVB boards, this article is based on S32K312 mini EVB, combined with P&E Multilink simulator download simulation. The platform situation is as follows: Fig 2 2.2 Migration steps The reference demo can be any existing demo in RTD4.0.0. In order to simplify the process, this article takes DIO as an example: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344 2.2.1 Copy the project and configure 2.2.1.1 Copy the project In order not to affect the original RTD default demo, here we directly copy a Dio_TS_T40D34M40I0R0 and open the path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins Copy Dio_TS_T40D34M40I0R0 and save it in a folder named: Dio_TS_T40D34M40I0R0_miniK312_doc The process for other chips is similar. You only need to change the chip name and related configuration to the required chip. Open folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX Copy Dio_Example_S32K344 to Dio_Example_S32K312 Fig 3    Open path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject  Modify the EB project Dio_Example_S32K344 to Dio_Example_S32K312 Fig 4 2.2.1.2 Configure the project Enter the newly created Dio_Example_S32K312, open the path with VScode, and save the VScode workspace to this path. Modify project_parameters.mk: GCC_DIR = C:/NXP/S32DS.3.5_RTD400/S32DS/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_4.0.0/eclipse/plugins EXAMPLE_DERIVATIVE = S32K312 TRESO_PROJECT_NAME = Dio_Example_S32K312 ​ Fig 5 Fig 6 Check_build_params.mk, delete the following code: ifeq ("$(wildcard $(T32_DIR)/bin/windows/t32marm.exe)","") $(error Invalid path set to Trace32. \ The provided path: from project_parameters.mk T32_DIR=$(T32_DIR) is invalid!) endif This part is used for lauterbach trace32. If it is not deleted, an error will be reported. 2.2.2 EB project configuration The following is the configuration of the EB project. Open the EB tresos Studio 29.0 software and import the project. File->Import->General->Existing Projects into Workspace, add the EB project path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject\Dio_Example_S32K312 Note, do not click copy projects into workspace!!! Select the project Dio_Example_S32K344, right-click the mouse, and rename it to: Dio_Example_S32K312 Fig 7 Double-click someId to open the configuration module. Open the Resource module, General->ResourceSubderivative select the target chip partbumber, here select: s32k312_hdqfp172 Fig 8 After saving, you will find many errors reported as follows: Fig 9 There is no need to worry too much here, because if you analyze it carefully, you will find that it is actually because there are many modules on K344 that K312 does not have. So enter the error prompt location and delete the missing K312 module. Mcu->McuModeSettingConf->McuPeripheral If you click in, you can find that if the K312 does not have a module, there is a red cross in front of the peripheral Name. Fig 10 The direct method is to delete all the error items, a total of 41. After deleting, you can find that all the problems are gone: Fig 11 Select someId in the project, right-click, and click Generate Code. You can see that the project can be generated without any errors. Fig12 Don't take it lightly here. Although the code can be generated without error, there is still a place that needs to be modified. Here, we can firstly close the EB tresos tool, then open terminal->new terminal in VScode and enter: Fig13 We can see the error content is : mcucgm0_clockMux0/McuClockMux0Divider5, McuClockMux0Divider6, McuClkMux0Div5_En, McuClkMux0Div6_En. Open S32KRM here, and you can see that K312 actually does not have MUX_0_5,6. Fig 14 At this time, when I opened the EB tresos software again, there was indeed such an error on the interface, and there was no divider 5,6 option in mcucgmClockMux0. Fig 15 Don't worry at this time, there is a way to fix this problem. Close the EB tresos tool and open the text: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject\Dio_Example_S32K312\config\ Mcu.xdm file. Directly turn off the enablement and value configuration of divider 5 and 6 in the file. Modify the following code:Modified to:The main thing is to change the enable and frequency value of Mux0Divider5,6 hidden in the file. Reopen it and you can see that the error disappears. Right-click on the EB project someId, generate project, and the code can be generated normally without error. Here is a little trick: In order to prevent the mismatch between the previously generated code and the latest EB project, you can also change: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\generate Folder:src,include clean it,then regenerate in EB tresos when generating a project. Close the EB software and enter make generate again in the terminal of the Vscode project You can see that there are no problems at this time: Fig 16  3.Command line compilation and result testing From the above steps, the code and EB configuration migration of an existing RTD K344 project to a K312 MCAL project has been completed. Now, through VScode, command line form, generate main.elf, and then download and test. Command: make generate make build the main.elf can be found in the following folder path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\out Regarding testing, because there is a main.elf file and PE Multilink, you can create a new K312 project in S32DS. The debug interface is PE Multilink. After compiling and generating the code, copy main.elf to the Debug_FLASH folder of the new project. In the S32DS debug configuration, directly replace the C/C++ application with main.elf and download it for testing.  Fig 17 As you can see, you can enter the debug interface, and the LED light on the actual test board can flash successfully. This means that the MCAL code has been successfully ported to K312. 4. S32DS project migration and testing       In the previous document: https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-import-RTD-EB-project-into-S32DS/ta-p/1966207 Previously, the RTD MCAL EB project was transplanted to the K344 project of S32DS. Simply modify the project name, project chip model, ld file, driver file inclusion, etc., then clean the project and compile the project.      It is assumed here that you already have an RTD MCAL project imported into the S32DS project, and then modify it based on this. 4.1 S32DS Project Configuration     Because the folder was copied under the original RTD folder, there is a newly created folder in the S32DS project Mcal_Plugins->Link_Source. This folder needs to be excluded from compilation: Select Dio_TS_T40D34M40I0R0_minik312_doc, right-click Build path->remove from->Debug_FLASH.      Fig 18 Rename the project from Mcal_Dio_S32K344_RTD400 to Mcal_Dio_S32K312_RTD400. Modify the following project configuration, project->properties: (1)preprocessor S32K344->S32K312 Fig 19   (2) Sstandard S32DS C Linker->General Modify "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/build_files/gcc/linker_flash_s32k344.ld" To "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/build_files/gcc/linker_flash_s32k312.ld" After modification, click apply and close Now, change the main.c content to the content in path:  C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\src\main.c Add header file: #include "Port_Cfg.h" Comment code: // #include "check_example.h" // Exit_Example(TRUE);   4.2 EB project replacement Copy: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject\Dio_Example_S32K312\config All the .xdm file to the S32DS EB folder, replace the old file: Mcal_Dio_S32K312_RTD400\Tresos_Project\Mcal_Dio_S32K344_RTD400\config Use the EB tresos open the above project, then Generate project,after the code is generated, close the EB project, back to the S32DS side. 4.3 MCAL S32DS project testing clean project:project->clean project,  then build the project Fig 20 You can see that it can be compiled successfully, then RUN->debug configuration selects the downloaded code xxx_Debug_FLASH_PNE. Note that you need to change the Device from S32K344 to S32K312 Fig 21 After successful configuration, click debug, download the code and simulate. The results are as follows: Fig 22 As you can see, we can successfully enter debug, and the light on the board is actually blinking, which means that the RTD MCAL project demo can be successfully ported to S32K312 S32DS. Video: 1.MCAL demo porting K344 to K312 based on RTD500     2.S32DS CT MCAL demo porting K344 to K312 based on RTD500 Attachment: Dio_Example_S32K312_MCALRTD600.zip: unzip it, get Dio_Example_S32K312, put in the RTD600 folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_xxx\examples\EBT\S32K3XX Dio_TS_T40D34M60I0R0_xxx is copy from Dio_TS_T40D34M60I0R0
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the Bootloader Jump to Application.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************   Jump is decided based on the boot_header, size we use to jump to the RESET handler:--   Cortex M-7 Interrupt vector table, RESET handler is 4 byte offset from starting of vector table :--   // Reset_Handler+1  --> required in IVT, to avoid hard fault As per Arm®v7-M Architecture Reference Manual  --> DDI0403E_e_armv7m_arm.pdf         How to burn elf file of both application & bootloader code :--  
記事全体を表示
[S32K3 tool part]:How to use IAR compiler or IAR project to compile MCAL project   1.    Abstract      Through regular observation, it has been found that there are still many customers using platforms such as MCAL+IAR, including those using IAR compilers and those directly using IAR IDEs. In fact, when I was working on industrial MCUs in the past, I also particularly liked IAR IDE for its fast compilation speed, high compilation efficiency, and small code generation. However, when I came to auto MCU, I found that its popularity was not very high, and I also noticed that some customers encountered various problems when importing MCAL into IAR. Therefore, I will directly write a tool article on how to use IAR compiler or IAR IDE project to compile NXP S32K MCAL in combination with EB tresos MCAL. This article uses S32K344 combined with RTD600 to illustrate the compilation of MCAL projects using IAR compiler and the direct import of MCAL into IAR IDE projects 2. IAR Complier with S32K3 RTD MCAL project 2.1 S32K3 HW and SW SW32K3_S32M27x_RTD_R21-11_6.0.0 S32K3X4-EVB Based on Dio_TS_T40D34M60I0R0 IAR:IAR EW for Arm 9.70.1 EB tresos29.0.0 2.2 Compile MCAL project steps using IAR compiler CMD method 2.2.1 Copy one RTD MCAL new project Open path C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins Copy Dio_TS_T40D34M60I0R0 , rename it as Dio_TS_T40D34M60I0R0_IAR Fig 1 2.2.2 Complie EB tresos project Use EB tresos tool open the following EB tresos project : C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_IAR\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject Generate code: Fig 2 2.2.3 Vscode open Dio_TS_T40D34M60I0R0_IAR project Use VS code open the following path folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_IAR\examples\EBT\S32K3XX\Dio_Example_S32K344 Of course, you can also directly open this folder path using the command line, as long as you ensure that it is in the same layer path as the. mk and makefile scr Fig 3 2.2.4   Project_parameters.mk modification Mainly modify the following points: TOOLCHAIN = iar IAR_DIR = C:/IAR/ewarm-9.70.1 TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_6.0.0/eclipse/plugins The path of IAR must be consistent with the version of IAR software used to ensure that the corresponding IAR compiler can be found. Fig 4 2.2.5   Check_build_params.mk modification Add the following content to check_build_params.mk: else ifeq ($(TOOLCHAIN),iar) ifeq ("$(wildcard $(IAR_DIR)/arm/bin/iccarm.exe)","") $(error Invalid path set to the IAR compiler. \ The provided path: from project_parameters.mk IAR_DIR=$(IAR_DIR) is invalid!) Endif Fig 5 2.2.6        Makefile modification   Makefile need the following 5 points modification: (1)Compilier change ifeq (${TOOLCHAIN},iar) CC := $(IAR_DIR)/arm/bin/iccarm.exe LD := $(IAR_DIR)/arm/bin/ilinkarm.exe AS := $(IAR_DIR)/arm/bin/iasmarm.exe # Intel Hexadecimal Flash image tool GENHEX := $(IAR_DIR)/arm/bin/ielftool.exe HEX_OPTS := --ihex OUT_OPTS := -o endif Fig 6 (2) SRC_DIRS  add TOOLCHAIN SRC_DIRS += $(foreach mod,$(MCAL_MODULE_LIST),$(PLUGINS_DIR)/$(mod)_$(AR_PKG_NAME)/src) \ $(foreach mod,$(MCAL_MODULE_LIST_ADDON),$(PLUGINS_DIR_ADDON)/$(mod)_$(AR_PKG_NAME_ADDON)/src) \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src/m7 \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src/m7/$(TOOLCHAIN) Fig 7 (3) Linker file  modification ifeq ($(LOAD_TO),flash) ifeq (${TOOLCHAIN},iar) LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/${TOOLCHAIN}/linker_flash_$(DERIVATIVE_LOWER).icf else LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_flash_$(DERIVATIVE_LOWER).ld endif else ifeq (${TOOLCHAIN},iar) LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_ram_$(DERIVATIVE_LOWER).icf else LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_ram_$(DERIVATIVE_LOWER).ld endif endif Fig 8 (4) Complier options change ifeq (${TOOLCHAIN},iar) ################################################################################ # iar Compiler options ################################################################################     clib        := $(IAR_DIR)/arm/lib     CCOPT           +=  --cpu=Cortex-M7 \                         -DAUTOSAR_OS_NOT_USED \                         -DUSE_MCAL_DRIVERS \                         --fpu=FPv5-SP \                         --cpu_mode=thumb \                         --endian=little \                         -e \                         -Ohz \                         --debug \                         --no_clustering \                         --no_mem_idioms \                         --do_explicit_zero_opt_in_named_sections \                         --require_prototypes \                         --no_wrap_diagnostics \                         --diag_suppress=Pa050 \                         $(MISRA) \                         -D$(PLATFORM) \                         -D$(DERIVATIVE) \                         -DIAR \                         -DUSE_SW_VECTOR_MODE  \                         -DENABLE_FPU \                         -DD_CACHE_ENABLE \                         -DI_CACHE_ENABLE                             LDOPT           :=  --entry _start \                         --enable_stack_usage \                         --skip_dynamic_initialization \                         --no_wrap_diagnostics \                         --cpu=Cortex-M7 \                         --fpu=FPv5-SP                             ASOPT           :=  $(ASOPT) \                         --cpu Cortex-M7 \                         --cpu_mode thumb \                         -g \                         -r \                         -DMULTIPLE_CORE   endif   Fig 9 Fig  10 So how did these IAR compilation options come about? You can refer to the release note of RTD600, which contains corresponding descriptions Fig 11 (5) Elf related change ifeq (${TOOLCHAIN},iar) %.elf: %.o $(LINKER_DEF)               @echo "Linking $@"               @$(LD) $(ODIR)/*.o $(LDOPT) --config $(LINKER_DEF) --map $(ODIR)/ -o $(ODIR)/$@@               @$(GENHEX) $(HEX_OPTS) "$(ODIR)/$(ELFNAME).elf" "$(ODIR)/$(ELFNAME).hex" else %.elf: %.o $(LINKER_DEF)               @echo "Linking $@"               @$(LD) -Wl,-Map,"$(MAPFILE)" $(LDOPT) -T $(LINKER_DEF) $(ODIR)/*.o -o $(ODIR)/$@@               @$(GENHEX) $(HEX_OPTS) "$(ODIR)/$(ELFNAME).elf" $(OUT_OPTS) "$(ODIR)/$(ELFNAME).hex" endif   Fig 12 2.2.7   Build to generate elf Commander: make clean make build to generate the elf files: Fig 13 After generation, the elf can be burned onto the S32K344 EVB board for testing. The test results show that the onboard red light is flashing, indicating that the IAR compiler can work in command-line mode. 3. Import RTD MCAL to IAR IDE project This chapter explains how to create an IAR IDE project and import MCAL drivers to implement S32K3 MCAL combined with EB tresos for running. 3.1 MCAL IAR IDE project 2 methods Difference between two methods and how to import MCAL drivers: (1) Directly copy the RTD MCAL driver to the IAR IDE project directory (2) Connect the IAR IDE project driver to the original RTD driver path Fig 14 3.2 MCAL IAR IDE project import steps 3.2.1 create the new RTD MCAL IAR project folder    Create a new folder, named as:S32K344_DIO_MCAL_RTD600_IAR 3.2.2 create the sub folder for IAR project       Generate:EB tresos project code       Include:app related include file       Mcal: mcal driver copy from RTD       src: project main file       Tresos_Project:EB tresos project Fig 15 3.2.3 create EB tresos project (1) Create the EB tresos project in the followign path:  S32K344_DIO_MCAL_RTD600_IAR\Tresos_Project\Mcal_Dio_S32K344_RTD600_IAR   (2)Add modules: BaseNXP, Dem, Dio, EcuC, Mcu, Platform, Port, Resource   (3)Copy RTD xdm files in the following path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject\Dio_Example_S32K344\config to: S32K344_DIO_MCAL_RTD600_IAR\Tresos_Project\Mcal_Dio_S32K344_RTD600_IAR\config   (4)EB tresos Generate project EB tresos code will be generated to folder: S32K344_DIO_MCAL_RTD600_IAR\Generate Fig 16 3.2.4 Copy RTD related drivers to IAR project folder (1) BaseNXP: header, include, src (2)Det:  include, src (3)Dio:  include, src (4)Mcu:  include, src (5)Platform: build_files, include, src, startup (6)Port: include, src (7)Rte: include, src Copy RTD folder to IAR project is one method, if don’t want to copy the file, also can use the linker to add the RTD install path drivers directly. Fig 17 3.2.5 IAR IDE create IAR project   (1) Project->Create new project   (2) In the IAR project, add group   The related folder in project can be structured like the fig 18, which contains:   Generate: Include and src->EB tresos project generate code   Mcal:  Base, Det, Dio, Mcu, Platform, Port, Rte->Mcal driver   Src: Main.c->project main code      (3) Add RTD mcal related drivers to IAR project The RTD MCAL related driver files can be directly downloaded from the RTD installation path or copied to a folder in the IAR project, and both methods yield the same result. Fig 18 (4)IAR project platform folder added result: Fig 19 (5)main code add Main.c can copy from path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344\src to S32K344_DIO_MCAL_RTD600_IAR\src Comment:  //#include "check_example.h"  // Exit_Example(TRUE);   3.2.6 IAR project options configuration (1)General options->Target->Device->NXP S32K344 (2)C/C++ Complier->Preprocessor Addional include directories: Use IAR project folder drivers which copied from RTD install path, the directories are: $PROJ_DIR$\Generate\include $PROJ_DIR$\mcal\BaseNXP_TS_T40D34M60I0R0\header $PROJ_DIR$\mcal\BaseNXP_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Mcu_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Rte_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\startup\include $PROJ_DIR$\mcal\Det_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Dio_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Port_TS_T40D34M60I0R0\include $PROJ_DIR$\include If use the RTD install path drivers, use the following directories: $PROJ_DIR$\Generate\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\BaseNXP_TS_T40D34M60I0R0\header C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\BaseNXP_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Mcu_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Platform_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Rte_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Platform_TS_T40D34M60I0R0\startup\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Port_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Det_TS_T40D34M60I0R0\include $PROJ_DIR$\include   Defined symbols: S32K3XX S32K344 IAR USE_SW_VECTOR_MODE D_CACHE_ENABLE I_CACHE_ENABLE ENABLE_FPU   Extra options: --no_clustering --no_mem_idioms --do_explicit_zero_opt_in_named_sections --require_prototypes --no_wrap_diagnostics   Languate 1:   Check Require prototypes   Diagnostics Suppress these disgnostics: Pa050 Fig 20 (3)Linker: Two points need to be added: $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\build_files\iar\linker_flash_s32k344.icf Library->Entry symbols: _start Fig 21 (4)Debugger Setup: PE micro, run to main Extra Options: Use command line options: --drv_vector_table_base=__ENTRY_VTABLE Fig 22 3.2.7  Build IAR project Project->Rebuild All Fig 23 3.2.8  Test result Download and debug result: Fig 24 After downloading and running, the red led is blinking on the board, indicating that the IAR IDE MCAL import method project has been successfully run.  
記事全体を表示
1. Abstract The S32K344 ADC is a SAR ADC with a resolution which can up to 14 bits. It has a variety of software and hardware triggering methods, supports various external trigger sources, and introduces BCTU so that the trigger resources can be externally connected to multi-channel EMIOS and TRIGMUX, adding more ADC trigger sources. This article mainly explains the following ADC software and hardware triggering methods, and provides supporting codes.     Fig 1 It is mainly divided into 5 parts: (1) SW+ADC: software trigger, by adding timer PIT, the software trigger ADC is called regularly to complete channel sampling, and the collected value is printed out through UART printf. (2) SW+BCTU+ADC: software trigger, by adding timer PIT, the software trigger BTCU is called regularly to complete ADC channel sampling, and the collected value is printed out through UART printf. (3) PIT+TRIGMUX+ADC: hardware trigger, connect PIT to ADC through TRIGMUX, trigger ADC channel sampling through PIT hardware, and print the conversion value after the sampling conversion is completed. (4) EMIOS+BCTUHW+ADC: hardware trigger, through EMIOS timing trigger BCTU to complete the corresponding ADC single channel sampling, due to the high sampling rate, only the BCTU sampling value is printed regularly. (5) EMIOS+BCTUHWLIST+ADC: hardware trigger, through EMIOS timing trigger BCTU to complete ADC list channel sampling, due to the high sampling rate, the list channel value sampled by BCTU is printed regularly. 2. ADC SW HW Trigger 2.1 Hardware and software platform SW: RTD400 LLD,S32DS3.5 HW:S32K3X4EVB-T172 2.2 SW+ADC software trigger     In fact, the original ADC demo of RTD400 already has ADC software and BCTU software trigger. This article adds PIT timing software trigger based on this function, and prints it out through UART printf, making it more convenient to check the ADC test value through serial port printing. The block diagram structure of the software triggering ADC in this article is as follows:     Fig 2      The S32K344EVB board has a potentiometer connected to ADC1_S10, PTA11:   Fig 3 Therefore, the software trigger in this section is mainly used to collect ADC1_S10. The UART printing port uses the serial port of the onboard emulator: LPUART6_RX PTA15, LPUART6_TX PTA16, with a baud rate of 115200. For the software trigger demo in this article, the main configuration involves the following modules: (1)Pins:   Fig 4 ADC1_s10: PTA11 is the voltage of the onboard potentiometer to be tested, which is adjustable. PTA29: Connect the onboard D13 red light to test the PIT timer interrupt and enter the flashing state, used as the breathing light of the PIT. PTA16: UART6_TX, used to send the collected ADC value. (2)clocks Used to configure the system clock. You need to pay attention to the UART6 clock source of 40Mhz, the ADC1 clock source of 160Mhz, and the PIT0 clock source of 40Mhz (3)Peripherals Involved peripheral modules Siul2_Port,Siul2_Dio, Pit, Lpuart_Uart, Adc_Sar_Ip, IntCtrl_Ip. Siul2_Port: Add 4 pins ADC PTA11 MSCR 11, RED LED PTA29 MSCR 29, UART6_RX PTA15 MSCR 15, UART6_RX PTA16 MSCR 16. Siul2_Dio: Add the module mainly to allow related API functions to come in, so as to control GPIO pins. Pit: Used to generate 1S timing, the main configuration is as follows:   Fig 5                                                             Fig 6 Lpuart_Uart: Fig 7 Adc_Sar_Ip:   Fig 8                                                                         Fig 9 It should be noted here that ADC calibration prescale and Adc prescaler vale need to meet the following conditions, which can be found on S32K3RM:   Fig 10 Since the clock source of ADC1 is 160MHz, the calibration division is configured as 4 and the conversion division is configured as 2. IntCtrl_Ip:   Fig 11 The purpose is to open the interrupt of PIT and LPUART6, and register the corresponding handler. CT configuration is completed, and the code is generated. Next, move to the main function and add the following code: void AdcEndOfChainNotif1(void) { notif_triggered1 = TRUE; data1 = Adc_Sar_Ip_GetConvData(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, 34); /* Checks the measured ADC data conversion */ // while (ADC_TOLERANCE(data, ADC_BANDGAP)); } void Pit0ch0Notification(void) { toggleLed = 1U; Siul2_Dio_Ip_TogglePins(LED_Q172_PORT, (1<<LED_Q172_PIN)); } int main(void) { StatusType status; uint8 Index; Clock_Ip_StatusType clockStatus; /* Initialize and configure drivers */ clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); while (clockStatus != CLOCK_IP_SUCCESS) { clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); } Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); /* set PIT 0 interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(PIT0_IRQn); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_1_BOARD_InitPeripherals); while (status != E_OK); IntCtrl_Ip_InstallHandler(ADC1_IRQn, Adc_Sar_1_Isr, NULL_PTR); IntCtrl_Ip_EnableIrq(ADC1_IRQn); for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); /* Initialize PIT instance 0 - Channel 0 */ Pit_Ip_Init(PIT_INST_0, &PIT_0_InitConfig_PB_BOARD_InitPeripherals); /* Initialize channel 0 */ Pit_Ip_InitChannel(PIT_INST_0, PIT_0_CH_0); /* Enable channel interrupt PIT_0 - CH_0 */ Pit_Ip_EnableChannelInterrupt(PIT_INST_0, CH_0); /* Start channel CH_0 */ Pit_Ip_StartChannel(PIT_INST_0, CH_0, PIT_PERIOD); Lpuart_Uart_Ip_Init(UART_LPUART_INTERNAL_CHANNEL, &Lpuart_Uart_Ip_xHwConfigPB_6_BOARD_INITPERIPHERALS); printf("S32K344 PIT TRIGMUX ADC demo RTD400.\r\n"); while(1) { #if 1 if( toggleLed == 1) { toggleLed = 0; /* Start a SW triggered normal conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_NORMAL); /* Wait for the notification to be triggered and read the data */ while (notif_triggered1 != TRUE); notif_triggered1 = FALSE; printf("ADC1_s10 ch34 data = %d .\r\n", data1); } #endif } } The test results are printed as follows:   Fig 12 This section content supporting code: S32K344_PIT_SW_ADC_RTD400.zip   2.3 SW+BCTU+ADC Software trigger BCTU Based on SW+ADC trigger, add BCTU, and use BCTU software trigger to complete ADC sampling. The block diagram structure is as follows:   Fig 13 This section uses BCTU software to trigger ADC0 sampling. The sampling channel does not actually use external pin input, but collects the bandgap value of ADC0. The software trigger calls the software trigger function through the PIT 1S cycle, and prints the ADC sampling conversion value to UART after completion. In the CT tool, the main modification points are peripherals, adding ADC0 in adc_sar_lp, and configuring it as BCTU trigger.   Fig 14                                                        Fig 15 Here we can see that in Figure 14, the adc ctu mode is: trigger mode. Add the Bctu_Ip module and configure it as follows:   Fig 16 The corresponding selected BCTU channel is 48, which corresponds to the internal bandgap module.   Fig 17 The typical value is 1.2V, so the reference voltage is 5V, and the corresponding 14-bit ADC bandgap expected value is: (2^14)*1.2/5=3932 around. After completing the CT configuration code generation, add the following code in main.c: void AdcEndOfChainNotif(void) { notif_triggered = TRUE; data = Adc_Sar_Ip_GetConvData(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_USED_CH); } void Pit0ch0Notification(void) { toggleLed = 1U; Siul2_Dio_Ip_TogglePins(LED_Q172_PORT, (1<<LED_Q172_PIN)); } void BctuWatermarkNotif(void) { uint8 idx; notif_triggered = TRUE; for (idx = 0u; idx < BCTU_FIFO_WATERMARK; idx++) { data_bctu = Bctu_Ip_GetFifoData(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_USED_FIFO_IDX); } } int main(void) { StatusType status; uint8 Index; Clock_Ip_StatusType clockStatus; /* Initialize and configure drivers */ clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); while (clockStatus != CLOCK_IP_SUCCESS) { clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); } Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); Bctu_Ip_Init(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &BctuHwUnit_0_BOARD_INITPERIPHERALS); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_0_BOARD_InitPeripherals); while (status != E_OK); /* set PIT 0 interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(PIT0_IRQn); /* Install and enable interrupt handlers */ IntCtrl_Ip_InstallHandler(ADC0_IRQn, Adc_Sar_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(BCTU_IRQn, Bctu_0_Isr, NULL_PTR); IntCtrl_Ip_EnableIrq(ADC0_IRQn); IntCtrl_Ip_EnableIrq(BCTU_IRQn); /* Call Calibration function multiple times, to mitigate instability of board source */ for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); /* Start a SW triggered conversion on BCTU using a single trigger */ Bctu_Ip_SetGlobalTriggerEn(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, TRUE); Bctu_Ip_EnableNotifications(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_IP_NOTIF_FIFO1); /* Initialize PIT instance 0 - Channel 0 */ Pit_Ip_Init(PIT_INST_0, &PIT_0_InitConfig_PB_BOARD_InitPeripherals); /* Initialize channel 0 */ Pit_Ip_InitChannel(PIT_INST_0, PIT_0_CH_0); /* Enable channel interrupt PIT_0 - CH_0 */ Pit_Ip_EnableChannelInterrupt(PIT_INST_0, CH_0); /* Start channel CH_0 */ Pit_Ip_StartChannel(PIT_INST_0, CH_0, PIT_PERIOD); Trgmux_Ip_Init(&Trgmux_Ip_xTrgmuxInitPB);// Lpuart_Uart_Ip_Init(UART_LPUART_INTERNAL_CHANNEL, &Lpuart_Uart_Ip_xHwConfigPB_6_BOARD_INITPERIPHERALS); printf("S32K344 PIT TRIGMUX ADC demo RTD400.\r\n"); while(1) { if( toggleLed == 1) { toggleLed = 0; Bctu_Ip_SwTriggerConversion(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_USED_SINGLE_TRIG_IDX); while (notif_triggered != TRUE); notif_triggered = FALSE; printf("ADC0_bandgap ch48 data_bctu = %d .\r\n", data_bctu); } } } Test result: Fig 18 It is close to the typical expected value, indicating that it has been successfully run. Used demo code:S32K344_PIT_TRIGMUX_BCTUSW_ADC_printf_RTD400.zip   2.4 PIT+TRIGMUX+ADC hardware PIT TRIGUMX trigger This section is about hardware triggering. PIT is used in combination with TRIGMUX to directly trigger ADC1 channel 34, i.e. ADC1_S10 sampling. The trigger structure diagram is as follows:   Fig 19 Also based on the previous code, you need to add an additional module Trgmux_Ip in the CT peripherals, and the rest of the configuration remains unchanged.   Fig 20 Here, the input of Trigmux is selected as PIT0_CH0 and the output is ADC1. The code is also much simpler. Add the following code in main: Trgmux_Ip_Init(&Trgmux_Ip_xTrgmuxInitPB);// while(1) { if(notif_triggered1 == TRUE) { notif_triggered1 = FALSE; printf("ADC1_s10 ch34 data = %d .\r\n", data1); } } In While(1), we can see that there is no software-triggered call. We can directly check the ADC1 conversion completion flag and then print the data. The test results are as follows: Fig 21 It can be seen that as the external potentiometer changes, the sampled value of ADC1_S10 also changes. Used demo:S32K344_PIT_TRIGMUX_ADC_printf_RTD400.zip   2.5 EMIOS+BCTUHW+ADC hardware EMIOS BCTU trigger The block diagram structure of this section is as follows:   Fig 22 Use eMIOS0_CH0 to generate a 10Khz clock to trigger BCTU to complete the sampling of ADC0_48 channel, that is, bandgap. In the CT tool, add Emios_Mcal_Ip and configure it as follows:       Fig 23 Change the BCTU configuration to enable HW triggering. The configuration is as follows:   Fig 24 Main code related codes are as follows: Emios_Mcl_Ip_Init(EMIOS_INST0, &Emios_Mcl_Ip_0_Config_BOARD_INITPERIPHERALS); while(1) { if( toggleLed == 1) { toggleLed = 0; printf("ADC0_bandgap ch48 data_bctu = %d .\r\n", data_bctu); } } Since the sampling rate is triggered at a frequency of 10Khz, the frequency is relatively fast, so the printing here is still based on 1s. The printing results are as follows:   Fig 25 As you can see, the result is also a variable bandgap value. Used demo:S32K344_PIT_TRIGMUX_BCTUHW_EMIOS_ADC_printf_RTD400.zip   2.6 EMIOS+BCTUHW LIST+ADC hardware EMIOS BCTU trigger LIST This section is similar to the EMIOS BCTU hardware trigger above, except that the BCTU is configured in the form of LIST, which can trigger the conversion of multiple channels at once. The main modifications are in the BCTU module:   Fig 26 Add the corresponding main code as follows: #define BCTU_FIFO_WATERMARK 3U void BctuWatermarkNotif(void) { uint8 idx; notif_triggered = TRUE; for (idx = 0u; idx < BCTU_FIFO_WATERMARK; idx++) { data_bctu[idx] = Bctu_Ip_GetFifoData(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_USED_FIFO_IDX); } } while(1) { if( toggleLed == 1) { toggleLed = 0; printf("ADC0_bandgap ch48 data_bctu = %d .\r\n", data_bctu[0]); printf("ADC0_vrefl ch54 data_bctu = %d .\r\n", data_bctu[1]); printf("ADC0_vrefh ch55 data_bctu = %d .\r\n", data_bctu[2]); } } Test result is: Fig 27 It can be seen that the results are consistent with the collected bandgap, VREFL, and VREFH, indicating that the code function is running normally. Code in this section:S32K344_PIT_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip  
記事全体を表示
Hi everyone, Welcome to the NXP Tech Days 2024 training session AUT-T4977: Hands - On Workshop: S32K3 Ethernet- How to Configure Hardware and Software. This session was initially planned for 15 attendees. But due to the popularity of the lecture, we have increased the number of available seats . Therefore, we will work in pairs during the Hands-On. My name is Alejandro Flores Triana (Alex) and I will be your guide during this conference. I am an Automotive Applications Engineer supporting different OEMs, Tier1s, Partners and other internal NXP teams on topics related to communication protocols (e.g. CAN, LIN, SPI, I2C, Ethernet, etc.). The idea of this session is for you to understand how to program the S32K3 Ethernet interface using NXP Real-Time Drivers (RTDs) – Autosar MCAL Layer. We will use a base project and together modify it to create a simple Ethernet application. Therefore, to be ready follow the steps below to get your environment up and running before the session. On your laptop, install the NXP Software environment described in the attached presentation: Hands - On Workshop: S32K3 Ethernet Prerequisites.   Once you have the NXP software environment installed, download the attached project: S32K344_ETH_MCAL_TechDays.exe   Run the .exe project with administrator rights. Accept the license and install in the desired folder         Open the NXP Design Studio. Click File -> Import -> Existing Projects into Workspace   Select root directory and browse the folder where you downloaded the project   Select Copy projects into workspace   Click Finish. Select the project. Click on the arrow next to the hammer. Click on Debug_FLASH. Then you are ready for the session! See you soon. Best Regards, Alejandro Flores Triana
記事全体を表示
******************************************************************************** * Detailed Description: * Example is based on Siul2_Port_Ip_Example_S32K344 and its purpose it to show * how to integrate ITCM and DTCM memories to the project. * * Modification has been done in following files: * - main.c * - startup_cm7.s * - linker_flash_s32k344.ld * * In the main function, function is placed to ITCM memory and executed. Also * data field in placed to DCTM and accessed. * ******************************************************************************** * Test HW: S32K3X4EVB-Q172 * MCU: S32K344 * Compiler: S32DS3.4 * SDK release: PlatformSDK_S32K3_3_0_0 * Debugger: Lauterbach Trace32 ******************************************************************************** Revision History: Ver Date Author Description of Changes 0.1 Apr-04-2019 David Tosenovjan Initial version *******************************************************************************/
記事全体を表示
Due to K3 hasn't been mass-produced yet, this content is moved to S32K3 Internal forum: https://community.nxp.com/t5/S32K3-Internal-Community/S32K3-Low-power-lab/ta-p/1280219 Any question, pls contact [email protected].
記事全体を表示
********************************************************************************  Detailed Description:  Example shows how to use FlexCAN 0 Pretended networking mode to allow FlexCAN  module to wake up MCU from STOP mode.  Wake up by Timeout and wake up by Match events are enabled.  Also pin interrupt can be used to exit STOP mode.  So MCU enters STOP mode by pressing SW3 button.  MCU exits STOP mode when one of following happens:  - no CAN message comes in 8sec (CAN PN timeout event)  - message with standard ID 0x554 or 0x555 comes (CAN PN match event)  - SW2 button is pressed (PTC12 interrupt)  In run mode blue LED is dimming and the rate is different for each wakeup event  ------------------------------------------------------------------------------  Test HW: S32K144 EVB-Q100  MCU: FS32K144UAVLL 0N57U  Fsys: 160MHz  Debugger: Lauterbach, OpenSDA  Target: internal_FLASH ********************************************************************************
記事全体を表示