S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0 Update 3          What is new? S32 SDK 0.8.6 EAR (Early Access Release)  for S32K142, S32K144, S32K146, S32K148)- see attached release notes for more details Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32 Design Studio for ARM v2.0 - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2_0/com.freescale.s32arm.updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use this direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button. This will starts the update installation process.
View full article
There are 2 methods to run; GUI, and terminal window. GUI Method 1) Make sure EVB is powered and connected to PC via USB (micro to USB) 2) Launch DDR Stress Test Tool, C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\DDR_Tester.exe 3) Load Image (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\bin\s32v234_ddr_test.bin) 4) Load Init Script (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\scripts\S32V234_LDDR2_MMDC0_2Gb.inc) 5) Select COM port 6) Press Download, then wait for it to complete. (may temporarily show 'not responding') 7) In 32bit Memory Read/Write section, enter address 80000000 in ADDR field. 😎 Change SIZE to 32 WORD 9) Click Read 10) See results 11) In DDR Stress Test section, enter 533 in both Start Freq and End Freq fields 12) Click Stress Test 13) See results 14) Results can be saved (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\log) Terminal window Method (JTAG) This checks what settings are already uploaded in MMDC module 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach AND via USB cable. 2) In S32DS, create a simple project a. File->New->S32DS Application Project b. Enter name 'test' c. Select S32V234 Cortex-A53 d. Next e. Uncheck boxes for cores 2-4 f. Finish 3) Setup debug configuration a. Run->Debug Configurations… b. Select test_A53_1_PNE c. Change C/C++ Application to C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\ddr-test-uboot-jtag-s32v234.elf d. Select Debugger tab e. Click Advanced Options f. Check box for Enable initialization script g. Browse to find C:\NXP\S32DS_Vision_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.1.3.201709051622\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR.mac h. OK 4) Click Debug. You will see error message indicating the source file could not be found. This is expected. 5) Open terminal (such as PuTTY.exe) and connect a serial line using the USB port you have connected to the EVB, speed set to 115200, 8 data bits, 1 stop bit, and no parity or flow control. 6) Click Resume in S32DS Debugger. 7) In terminal window, you will see the test script has started. 😎 Select the MMDC channel (for example, enter 1 for MMDC1) 9) Select the DDR density (for example, enter 6 for 32MB) 10) Enter 'n' to decline the DDR Calibration 11) Enter 'y' to accept the DDR Stress Test 12) Enter Start and End frequencies (for example, enter 533, as was done in GUI method) 13) Enter 0 to run only once 14) See the results
View full article
There are three methods to run the configuration tool; from S32DS, from Terminal and JTAG, and from command line. S32DS Method 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach 2) Launch S32DS for Vision 3) File -> New -> S32V DDR Configuration Project 4) Enter a name for the project, for example 'DDR_Config_test'. Click Next 5) Expand 'S32V' and select 'S32V_234' 6) Click Finish to generate the project with default settings OR if you wish, to view or adjust more project settings, click Next. For this demonstration, we click Next. a. Select which DDR controller to which the settings will be applied. For this demonstration, we leave it at default (1st DDR Controller) b. There is an option to import settings from a file c. Board setting allows you to select from a list of predefined configurations, one for each of the NXP S32V234 evaluation boards i. S32V234_EVB is for LPDDR2 (SCH28899 and SCH28292(old board)) ii. X_TR_DVAL_625 is for DDR3 (SCH28662(old board)) iii. S32V234_NXP_EVB is for SCH29288 (S32V234-EVB2) iv. Custom allows for more options to be selected. See user manual for more detail d. For this demonstration, we select S32V234_EVB e. Click Finish 7) It will take a couple minutes to generate the project. You will get a prompt to pen the S32V DDR Configuration perspective. Click Yes. 😎 Now the project is generated and you can see it listed in the Project Explorer 9) Notice the Components and Component Inspector views of the S32V DDR Configuration perspective. 10) Select the component 'MMDC_0:Init_MMDC from the Components view 11) In the Component Inspector window you can see all of the configuration settings. You can modify the settings here. Changes made to some of the high-level settings may also cause changes to some of the low-level settings. There are some consistency checks that are run automatically after settings are changed which will trigger an error message in the case of an invalid configuration. a. For an example of high-level settings affecting low-level settings, try changing the 'Memory type' from LPDDR2 to DDR3. You can see the Burst Length, Column Address Width, and Row Address Width have changed. b. For an example of a consistency check on an invalid configuration, try changing the CAS Read Latency value (MDCFG0) from 8 to 12 (valid range as displayed with mouse hover tooltip shows 3-11), you will see the error appear. Change back to 8 and error is gone. 12) Open Configuration Registers view. Window -> Show View -> Other -> Processor Expert -> Configuration Registers. This shows how the settings will appear in the memory map. As you change the settings, the values will update here and the affected rows will be highlighted. Try it by changing Column Address Width in MDCTL of the Component Selector window. Likewise, you can try changing the value manually in the Configuration Registers view and see the setting in the Component Selector window update as well. *Hint: enter the name of the view in the search bar to find it quicker 13) Once all changes to the settings are complete, code can be generated. Press the 'Generate Processor Expert Code' button in the Components view. The generated .c and .h file will appear in the 'Generated_Code' folder of the Configuration project. These can be copied into your application project. OR 14) Back in the Component Inspector view, there are tabs for Import and Export settings. The Import settings tab will allow you to import existing settings files, as was also shown in the new project wizard. From the Export settings tab, you can generate a settings file for storage or sharing. The settings files for MMDC_0 and MMDC_1 for each of the supported NXP EVBs are included and can be located in 'C:\NXP\S32DS_Vision_v2.0\eclipse\ProcessorExpert\Optimization\resources\S32V\Boards' and then select the folder for the specific board. The CodeWarrior Register Text format is recommended for these files. 15) Now select the 'Validation' tab (some views, such as Configuration Registers, can be minimized for better view). Here we can execute a validation of the configuration settings we've made. Now is a good time to double check the hardware connections. 16) Select the connection method (either PEMicro or Lauterbach, depending on your setup). We will use System: S32V234; PEMICRO 17) Press 'Connect to Target' 18) Check a box for one of the scenarios. For example, select 'Read Delay Calibration' 19) Select the 'Choose Tests' tab 20) You can select tests from a list. To see the script behind the test, simply double-click on the name. For faster operation, ELF file versions are also provided. 21) Select the tests you wish to execute and press 'Start Validation'. For example select 'Write-Read-Compare-Elf', 'Walking Ones Elf', and 'Walking Zeros Elf'. 22) These tests will try different values and to determine which will work and which will not. After the test is finished, the best values are chosen and written back to the project configuration settings. To see the values change, go to the Properties tab and find 'PHY Read delay-lines Configuration' or restore the 'Configuration Registers' view and see the values changed. 23) For each test, you can see the errors which occurred in the 'Summary' tab, Test results section. There is also Updated configuration registers section which shows the register and the new value which was written to it. For more details on the errors, there is a Log tab which displays the log for each test which was run. Finally there is a Scripts tab which shows the script for each test containing the test settings. Each test box is colored to reflect the result of the test. Clicking on different ones causes the display below to change and show the results for that test. 24) The Write Delay Calibration test scenario is very similar to the Read Delay Calibration test scenario, but instead, the Write delay-lines Configuration will be updated. 25) The Operational DDR Tests run the same tests, but no value in the configuration is changed. You can set it to run for many repetitions to test for stability. Terminal window Method (JTAG) This checks what settings are already uploaded in MMDC module 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach (to load test application) AND serial communications via USB cable(for terminal access). 2) In S32DS, create a simple project a. File->New->S32DS Application Project b. Enter name 'test' c. Select S32V234 Cortex-A53 d. Next e. Uncheck boxes for cores 2-4 f. Finish 3) Setup debug configuration a. Run->Debug Configurations… b. Select test_A53_1_PNE c. Change C/C++ Application to C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\ddr-test-uboot-jtag-s32v234.elf d. Select Debugger tab e. Click Advanced Options f. Check box for Enable initialization script g. Browse to find C:\NXP\S32DS_Vision_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.1.3.201709051622\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR.mac h. OK 4) Click Debug. You will see error message indicating the source file could not be found. This is expected. 5) Open terminal (such as PuTTY.exe) and connect a serial line using the USB port you have connected to the EVB, speed set to 115200, 8 data bits, 1 stop bit, and no parity or flow control. 6) Click Resume in S32DS Debugger. 7) In terminal window, you will see the test script has started. 😎 Select the MMDC channel (for example, enter 1 for MMDC1) 9) Select the DDR density (for example, enter 6 for 32MB) 10) Enter 'y' to accept the DDR Calibration 11) Enter 'y' to accept the DDR frequency of 533MHz 12) Wait and watch while the test completes. 13) When the test completes, the results are shown. You will have to manually update your settings from the information displayed. 14) Next you will have the option to run the DDR Stress Test.
View full article
This document shows the step-by-step process to create a simple 'Blinking_LED' project. There is also a video which demonstrates the same steps. This project uses the S32K144EVB-Q100 EVB, connected to a PC through USB (OpenSDA) connection. 1. New S32DS Project OR 2. Provide a name for the project, for example 'S32K144_Blinking_LED'. The name must be entered with no space characters. 3. Expand Family S32K1xx, Select S32K144 4. Click Next 5. Click '…' button next to SDKs 6. Check box next to S32K144_SDK. 7. Click OK 8. Click Finish, wait for project generation wizard to complete 9. Notice Processor Expert views have opened. 10. Make sure the project is selected in Project Explorer view, then from the Components - S32K144_Blinking_LED view, select: Components -> pinmux:PinSettings 11. From the Routing tab, select the GPIO pin routing group and scroll the list until PTD Pin 15 and Pin 16 are visible 12. Click on the fields in the Pin/Signal Selection and Direction columns to set the following:       a. Row: Pin 15, Pin/Signal Selection: PTD15, Direction: Output       b. Row: Pin 16, Pin/Signal Selection: PTD16, Direction: Output 13. Click Save 14. Project -> Generate Processor Expert Code OR, click the button from the Components view 15. The main.c file from 'Sources' folder should be already open, if not, then in the project window click to expand the project folder then Sources, and finally double click the main.c file to open it. 16. Expand the clock_manager component in the Components Window, then locate CLOCK_DRV_Init 17. Drag and drop the CLOCK_DRV_Init function into main, after the comment 'Write your code here' 18. Now we need to supply an argument so the CLOCK_DRV_Init() function knows what clock settings to use. With clockMan1:clock_manager selected in the Components view, look at the Components Inspector and locate the name of the only clock configuration listed, 'clockMan1_InitConfig0'. 19. Enter the name of the clock configuration, with address operator, to the input arguments of CLOCK_DRV_Init(). Notice the name is shaded grey and a mouse-hover reveals the definition. 21. Expand the pin_mux:PinSettings component  in the Components Window 22. Drag and drop the PINS_DRV_Init function into main, below the clock configuration  24. Drag and drop the PINS_DRV_SetPinsDirection function into main immediately after PINS_DRV_Init 25. Drag and drop the PINS_DRV_SetPins function into main 26. Drag and drop the PINS_DRV_ClearPins function into main 27. For each of the PINS_DRV functions, there are 2 arguments, first is always PTD (which is macro defined in SDK), the second is defined as follows: PINS_DRV_SetPinsDirection: OR-ing of LEDRGB_RED and LEDRGB_GREEN = 1 << 15U | 1 << 16U PINS_DRV_SetPins: Bit shift of LEDRGB_RED = 1 << 15U PINS_DRV_ClearPins: Bit shift of LEDRGB_GREEN = 1 << 16U 28. Include an infinite loop after these functions 29. Drag and drop the PINS_DRV_TogglePins function in to main, and place it inside the 'for' loop. 30. Again, the first argument will be PTD and the second is the same as for PINS_DRV_SetPinsDirection above. 31. Within the 'for' loop, and prior to the PINS_DRV_TogglePins function, add a delay of 720000 cycles int cycles = 720000; while(cycles--); 32. Build 'Blinking_LED_S32DS'. Select the project name in 'C/C++ Projects' view and then press 'Debug_RAM'. Or you can build for Debug_FLASH, but programming RAM won't overwrite anything you already have in FLASH. 33. After the build completes, check that there are no errors. 34. Open Debug Configurations and select 'Blinking_LED_S32DS_Debug_RAM' OR 35. Check the Debugger settings and ensure that 'OpenSDA Embedded Debug - USB Port' is selected for interface. Or select the settings which are appropriate for your hardware configuration. 36. Click Debug 37. Set breakpoint on PINS_DRV_TogglePins. Double-click on the blue shaded area at left on the line of code to set breakpoint. 38. Step through initialization calls 39. To see the output register bits change, go to 'EmbSys Registers' tab and expand 'GPIO', then 'PTD' and 'PDOR'. Double-click on PDOR to enable reading of the values. 40. Click resume to advance to the breakpoint, see the LED on board change color. 41. Click resume again and see LED change to other color
View full article
Example shows how can be expanded default 512kB flash memory by 64 kB using FlexNVM as a program/data flash. In FlexNVM are stored two ASCII images and function PrintImage. FlexNVM is divided into 32kB data section and 32kB code section in the linker file. Output is printed on terminal. As a output device you can use putty or any other serial terminal. Terminal settings: 9600, 8N1 - no flow control. In debugger settings you have to Enable partitioning device with code 0F0C. This value is written into FCCOB4 and FCCOB5 registers before flashing. Putty settings: Test HW: S32K144EVB, MCU: S32K144 Debugger: OpenSDA Target: internal_FLASH (debug mode and release mode)
View full article
1. Click on the "S32 Design Studio for ARM" icon OR, from the Start menu, NXP S32 Design Studio -> S32 Design Studio for ARM -> S32 Design Studio for ARM 2. Select workspace: a. Use the default one, or b. Specify a new one Note: If you check the box "Use this as the default and do not ask again", this prompt will not appear the next time you launch S32 Design Studio for ARM. However, if later you should decide you want this to appear again, simply uncheck the box "Prompt for workspace on startup" from within the Preferences dialog window General -> Startup and Shutdown -> Workspaces. The Preferences dialog window can be opened from the Eclipse menu bar Window -> Preferences. 3. Click OK. 4. Create a new project. Go to the Eclipse menu bar and select File -> New -> New S32DS Project 5. Enter a project name. Example: FirstProject (must not contain spaces) 6. Select processor. Example: expand 'Family S32K1xx' folder, then select S32K144. 7. Click Next. 8. Select Debugger Support and Library Support. If supported, also select SDK: a. SDK for GCC b. Automotive Math and Motor Control Library Set for GCC c. FreeMASTER Serial Communication Driver 9. Click Finish 10. The new project wizard will generate the new project and then the indexer will run. It is recommended to wait until all processes complete before proceeding with any further actions.
View full article
Included in the S32DS for ARM is a set of example projects, which include one called 'hello'. This example shows a basic application which activates an LED when a button is pressed on the S32K144EVB-Q100 evaluation board. The S32K SDK is not used in this example. In this HOWTO, we will show how to load the project into the workspace, build, download to the target, and run debug. 1. Create Project a. File -> New -> New S32DS Project from Example   OR from the Dashboard b. Select S32DS Example Projects -> S32K144 -> hello 2. Examine the code a. Locate the project in C/C++ Projects view b. Expand 'hello', then 'src' c. Double-click on 'hello.c', to open the file in the editor 3. Build the project a. Click to select hello project, this is to ensure that the tool knows which project you wish to build. b. Click Build button. By default, the standard 'Debug' build configuration will be used. Projects created using either the New S32DS Project from Example, or New S32DS Project wizard are setup with 3 build configurations: Debug, Debug_RAM, and Release. The 'Debug' configuration contains settings to build the project with the lowest compiler optimization setting and to occupy the Flash memory space on the target. The 'Debug_RAM' configuration is very similar to the 'Debug' configuration with one exception. It is set to occupy the RAM memory space on the target. The 'Release' configuration will build the project with the highest optimization setting and to occupy the Flash memory space on the target. c. From the console tab, the build status output is displayed. Check here to confirm the build completed and there were no errors. 4. Setup Debug Configuration a. Click Run -> Debug Configurations… OR from the Debug button menu b. Expand the 'GDB PEMicro Interface Debugging' group. c. Select the configuration which matches the build configuration you just used to build the project. For each build configuration generated by the new project wizard, it also generates a matching debug configuration. d. Select the Debugger tab. The debug configuration was created with the 'PE Micro GDB server' option selected, but there are several hardware options for this. Select the option which matches your hardware setup. For example, for the S32K144, most likely you have the standard evaluation board, which has OpenSDA integrated. In this case, you would use the OpenSDA interface option. For other MCUs, you may have hardware which requires the USB Multilink or Cyclone. e. Click Refresh to ensure the correct port is selected. 5. Click Debug to start the debugger launch sequence. It is not necessary to click on the 'Apply' button unless setting changes are being made without intention to launch the debugger. The scripts behind the Debug button include the actions of the script behind the Apply button. 6. When the launch sequence completes, the application is executed until the start of main(), where a breakpoint was automatically set. 7. It is now possible to run or step through the code, view variables and registers. 8. Click Resume and when Button 0 is pressed, the LED will turn on as Blue, and when Button 0 is released, the LED turns off. 9. To end the debug session, click the 'Terminate' button. It is a good idea to also click on 'Remove All Terminated Launches', before starting another debug session.
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1         The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Power Architecture version 2017.R1. It is the successor of S32 Design Studio for Power v1.2. - the versioning scheme has changed. Release content (What is new?) Eclipse Neon 4.6 Framework GNU Build Tools for e200 processors (support VLE and BookE ISA, based on gcc 4.9.4 [7.October 2017], binutils 2.28 and gdb 7.8.2) - see the complete GCC release notes Libraries included: newlib, newlib-nano and Freescale EWL2 P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v1.7.2.201709281658) New Project wizard to create application and library projects for supported devices Peripherals Register and Special Purpose Registers View Fully integrated MPC5748G/MPC5746C SDK EAR v.0.8.1. For the details on the feature set of SDK please refer to SDK Release notes attached and Reference Manuals (Please note that SDK has Early Access Release status, which means that there could be some limitations and/or issues. Also note, the SDK is available for Windows host only). SDK management included: o FreeMASTER Serial Communication driver (v2.0 August 31th 2016) o Automotive Math and Motor Control Libraries(v1.1.9) Windriver Diab compiler support by new project wizard Lauterbach, iSystem, and PLS debuggers support by new project wizard (The plugins to support Diab, iSystem, Lauterbach are not included and have to be installed from the corresponding update site or installation. The current version of the GreenHills plugin is not compatible with Eclipse Neon version, so it should not be used with this release) Kernel Aware debugging for FreeRTOS, eCOS, OSEK Devices supported: S32R274 S32R372 MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5744B, MPC5745B, MPC5746B, MPC5744C, MPC5745C, MPC5746C MPC5744P, MPC5743P, MPC5742P, MPC5741P MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A, MPC5642A MPC5643L MPC5676R MPC5632M, MPC5633M, MPC5634M MPC5674F MPC5673K, MPC5674K, MPC5675K Collateral Getting Started page Bug Fixes C preprocessor tool added for C++ projects configuration The makefile generation is updated to fix and issue with building a project on the Korean version of Windows - Code page switch command cannot be executed. The Rename Project functionality is improved to cover referenced projects and launch configurations Complete S32 Design Studio for Power Architecture 2017.R1 release notes are available here Installation Notes To download the installer please visit the S32DS for Power Architecture product page: downloads section. The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the installer downloading process: Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space: https://community.nxp.com/community/s32/s32ds    
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0 Update 2          What is new? S32 SDK 0.8.5 EAR (S32K142, S32K144, S32K146, S32K148) - see attached release notes for more details   MXQ 4.2 for MAC47D54H - see attached MQX release notes for more details. Installation instructions The update is available for online (via Eclipse Updater) or offline (direct download link) installation   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository  "S32 Design Studio for ARM v2.0 - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2_0/com.freescale.s32arm.updatesite" select all available items and click "Next" button.   offline installation:  go to S32 Design Studio product page -> Downloads section or use the direct download link to download the Update archive file. Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update archive file you downloaded in the previous step: Select all available items and click "Next" button. This will starts the update installation.
View full article
Perhaps you are just using the S32DS for Power for the first time, and maybe you've seen the provided examples and want to learn a bit more about how they were created. Here are the steps to create a simple application for the MCP5748G MCU which toggles a pin causing one of the user LEDs to blink. This example includes use of the S32 SDK for Power Architecture. Please note: There are options in the steps below to cover the case of either the DEV-KIT(DEVKIT-MPC5748G) or Motherboard(X-MPC574XG-MB) with Daughtercard(X-MPC574XG-324DS) hardware EVBs. 1) Launch S32DS for Power 2) Select File -> New -> New S32DS Project 3) Enter a name for the project, such as 'BlinkingLED' 4) Locate, from the list of processors, Family MPC574xG -> MPC5748G, and select it. 5) Click Next 6) Uncheck the boxes for cores e200z4 and e200z2, leaving just e200z4 (boot) checked. This is because the application will run on the boot core and will not use either of the other two cores. 7) Click on the '…' button next to SDKs, in the column for BlinkingLED_Z4_0. 😎 Check the box next to MPC5748G_SDK_Z4_0_GCC to include support for the SDK within the new project and for the core we have selected. 9) Click OK 10) Click Finish to close the New Project wizard window and start the project generation. 11) Wait a minute or two for the project generation script to complete. 12) Go to the 'Components Library' view then locate and double-click on 'pit' component to add it to the project.  Alternatively, right-click and select Add to project. You can verify it was added by inspecting the 'Components - <project_name>' view. 13) With 'pit' selected in the 'Components - BlinkingLED_Z4_0' view, go to the 'Component Inspector' view to see the configurations for the PIT component. Locate the section for 'Configuration 0'. You may have to scroll down to see it. Change the 'Time period' setting to 500000 microsec(0.5 sec). Note that we are editing the settings for Clock configuration 'clockMan_InitConfig0', you will need the name of this configuration later. 14) Back in the 'Components' view, select 'pin_mux' component and return to the 'Component Inspector' view 15) From the 'Routing' tab, select the 'SIUL2' sub-tab and scroll down the Signals list until 'GPIO_0' (DEV-KIT) or 'GPIO_99' (Motherboard) is shown. 16) Change to the following settings: a. Pin/Signal Selection: PA[0] (DEV-KIT) / PG[3] (Motherboard) b. Direction: Output Pin PA0/PG3 is connected to user LED 2 on the evaluation board. 17) All configuration settings are now complete. Click Generate Processor Expert code button in the 'Components' view or use the menu bar Project-> Generate Processor Expert Code. 18) Wait for the code generation to complete. 19) Now, from the 'Project Explorer' view, the generated code is visible in the folder 'Generated_Code' of the project 'BlinkingLED_Z4_0'. 20) If not already open, in 'Project Explorer' open the file 'BlinkngLED_Z4_0\Sources\main.c' by double-click. This will open the file in the editor view. 21) Scroll down until the following comments are shown: /* Write your code here */ /* For example: for(;;) { } */ We need to add some code here to initialize the clocks, timers and pins. Then we will setup a timer interrupt handler to toggle the pin. 22) First we need to initialize the clocks. From the 'Components' view, expand 'clock_manager' and then drag & drop CLOCK_DRV_Init function into main() of main.c, just after the comments identified in the previous step within the text editor view. 23) Add to the function CLOCK_DRV_Init(), the parameter &clockMan1_InitConfig0 to give it the address of the user configuration structure generated by ProcessorExpert in '.../Generated_Code/clockMan1.c'. This is the clock configuration for which we edited the timer period in an earlier step. 24) Next we need to initialize the pins. Back in the 'Components' view, expand the 'pin_mux' then drag and drop the function PINS_DRV_Init after the clock initialization. 25) Again from the 'Components' view, expand 'interrupt_manager', then drag & drop INT_SYS_InstallHandler in 'main()'. This installs the PIT channel 0 interrupt handler. 26) Enter the parameters: PIT_Ch0_IRQn, &pitCh0Handler, NULL 27) In the User includes section at the start of main.c, add the implementation of the handler a. Create a function called pitCh0Handler b. In the function body: clear the interrupt flag and toggle LED   /* IRQ handler for PIT ch0 interrupt */   void pitCh0Handler(void)   { /* Clear PIT channel 0 interrupt flag */ PIT_DRV_ClearStatusFlags(INST_PIT1, 0U); /* Toggle LED (GPIO 0 connected to user LED 2) */ SIUL2->GPDO[0] ^= SIUL2_GPDO_PDO_4n_MASK; // DEV-KIT /* SIUL2->GPDO[99/4] ^=SIUL2_GPDO_PDO_4n3_MASK;*/ // Motherboard   } Note: Get PIT_DRV_ClearStatusFlags by drag & drop from the 'pit' component. 28) In 'Components' view, expand 'pit' component and then drag & drop PIT_DRV_Init, PIT_DRV_InitChannel & PID_DRV_StartChannel in main() after INT_SYS_InstallHandler(). 29) Fill in the second parameter of the last function(channel number): 0U 30) Build the code. Click the down arrow next to the 'Build' button and select Debug_RAM. Check that there are no build errors. 31) Enter the 'Debug Configurations' menu: a. From the menu bar, Run -> Debug Configurations... b. From the toolbar, down arrow next to Debug button -> Debug Configurations... 32) The Debug Configurations window appears. Select the configuration BlinkingLED_Z4_0_Debug_RAM from within the GDB PEMicro Interface Debugging group. 33) Select the 'Debugger' tab to setup the connection to the debugger hardware device. 34) Select the PEMicro Interface which corresponds to your setup: a. If using the motherboard, you will likely use the USB Multilink, which is connected to your PC via USB cable (type A on one end, type B on the other) and is connected to the motherboard via the 14-pin JTAG cable. b. If using the DEV-KIT board, you will likely choose the OpenSDA, which is integrated into the DEV-KIT board and is connected with just a USB cable (type A on one end, type micro on the other). 35) Click Debug To launch the debugging session. This will also open the Debug perspective. 36) In the Debug perspective, once the debugging session has fully launched, the code will be executed to the start of main(), where a breakpoint was automatically set for you. Press Resume button in the toolbar, Run -> Resume in the menu bar, or F8 on your keyboard to run the application. 37) You should now see the User LED2 on the board blink every 0.5 seconds. 38) To see the value of the output register bit for the output pin connected to the LED: a. Set a breakpoint on a line within pitCh0Handler() b. Go to the EmbSys Registers view, expand the SIUL2 module and scroll down to the GPDO register index which is accessed in the code. Double-click it to read the value. Expand it to see the individual bits. c. Press Resume a few times to see the register value change
View full article
This Example demonstrates an alternative way to multi-core projects. This is basically a single eclipse project that generates the single elf file for dual core MCU (MPC5777C) See the project structure below where the sources for each core are separated into a core specific source folder: Main core0 [e200z7_0] performs basic initialization (Clocks, ports..) Each core initializes the interrupt controller in order to service interrupts generated by PIT (Periodic Interrupt Timer): Core 0 (e200z7_0) services PIT channel 0 interrupts generated once per second. Core 1 (e200z7_1) services PIT channel 2 interrupts generated once per two seconds.
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v1.2, Update 3            September 21, 2017   What is new? S32 SDK EAR 0.8.1 supporting MPC5748G & MPC5748C. The new project wizard now offers the new version of S32 SDK: "New S32 Project from Example" offers additional demos and examples. The complete S32 SDK EAR 0.8.1 release notes attached below. Installation instructions This is a cumulative installer - all previous updates (except previous version of S32 SDK EAR 0.8.0) are included so you do not need to install any previous update. The update is available for online (Eclipse Updater) or offline (direct download link) installation. online installation go to menu "Help" -> "Install New Software..." dialog  select predefined NXP S32 Design Studio update repository select all available items http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite click "Next" button offline installation  go to S32 Design Studio product page -> Downloads section or use the direct download linkand download the "S32 Design Studio for Power v1.2 - Update 3" file. Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 3 archive file Select all available items and click "Next" button.
View full article
Build your project and choose Debug Configuration option  On the left side select Launch Group of your choice (Flash/RAM) and press Debug button Wait while debug session is fully started. If you left default startup configuration - all cores has active break-point at the beginning of main() function. You can chose any core for debugging just by clicking on the core's thread. Sometimes are init functions - including startup of other cores - inside main() of boot core (for S32R274 is boot core Z4). In this case you should let boot core perform init sequence first and then try debug other cores. On next picture are all cores halted.  On this picture are core 1 (Z4) and 2 (Z7_0) running - and third one is stopped. You can perform any debug operation on this core (memory/registers view, instruction step...) without effect on other cores.  On the last picture are running cores 1 (Z4) and 3 (Z7_1) and second core (Z7_0) is stopped and any debug operation can be performed on this core. 
View full article
Requirements:  SD card with installed Linux image connected to EVB (HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK ) Serial link connection between PC and EVB (HOWTO: Setup A Remote Linux Connection in S32DS for Vision ) Static IP address on PC machine Network connection between PC and EVB Use case: This settings is useful when you don't have DHCP server available or for some reason you can't connect EVB into existing network - like on this scenario:  Procedure: Setup static IP address on your PC machine - (Windows 7) click on Start -> Control Panel -> Network and Sharing center. On the left side click on "Change adapter settings" Select network interface connected to EVB ( Local area connection ) and choose "Internet protocol Version 4 (TCP/IPv4)" option and click on Properties button.   Select "Use the Following IP address" radio button and enter IP address for PC side of network connection and click on OK button.    Turn on EVB and connect to EVB via serial link using putty or any other terminal (115200 baud, 8N1). Login as the root user. Edit network interfaces configuration file by command vi /etc/network/interfaces and modify (press INS key to switch vi editor to edit mode) the file by the way as shown on next screenshot. Set IP address from range of your PC machine network settings.  Save new settings by :w command (press ESC key to switch vi editor to command mode) and exit from vi by :q command. Restart network by command /etc/init.d/networking restart  Check the IP address by command ifconfig and try ping to your PC machine.  Troubleshooting: If you can't ping to PC machine and IP address is the same as you requested - check IP address on PC side and cable connection.  If the IP address on EVB is different than you requested - check if you commented out the dhcp configuration. You may also try to reboot EVB instead of restarting network only. 
View full article
Example show one of the methods how to create and use shared memory with symbols between cores. In source code shared_mem.c are variables which can be seen by each core. This file is built once (during s32r274_shmemZ7_0 project compilation) and is linked to other core's elf file by linker into shared_mem section (see linker file for each core) starting on the very same address for each core. Hardware semaphores are used for access shared memory. Lock/Unlock functions are implemented in the shared_func.c (build once during s32r274_shmemZ7_0 project compilation too) file and the object is linked into .text section. Each core has it's own instance of shared functions. There is counter in the shared memory for each core increased each time when shared memory can be accessed by particular core.
View full article
The list of S32 Design Studio examples has been moved here: https://community.nxp.com/docs/DOC-341380  S32K144 EXAMPLE: S32K_printf_implementation - S32DS  EXAMPLE: S32k144 UART printf/scanf under FreeRTOS - S32DS  EXAMPLE: S32K SDK  - Function call on configurable period using LPIT timer.  EXAMPLE: FlexNVM used as code/data flash  EXAMPLE: S32K144 EEEPROM usage  EXAMPLE: S32K144 EEEPROM usage - No SDK  EXAMPLE: S32K144 .noinit section usage  For more examples and how to's: S32K1xx document &amp; example list
View full article
Create Project From Example S32DS for ARM: Create and Debug a New Project from Example Code in S32 DS IDE for ARM based MCUs. Learn how to create a new project in S32 Design Studio IDE and load an example code to blink an LED using the S32K144EVB and build and debug the project. Create New Project S32DS for ARM: Create and Debug a New Project in S32 DS IDE for ARM based MCUs Learn how to create a new project in S32 Design Studio IDE using Processor Expert and SDK to blink an LED using the S32K144EVB and build and debug the project.
View full article
Create From Example 1 | Create an ISP Project from Example A demonstration of how to load an example ISP image processing application project featuring RGB, YUV, and GS8 image formats, in the S32 Design Studio. 2 | Create an APEX2 Project from Example A demonstration of how to load an example ORB-based APEX2 image processing application project in the S32 Design Studio. https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS Create New Project 3 | Create a New ISP Project A demonstration of how to create a new Debayer-based ISP image processing application project in the S32 Design Studio. 4 | Create a New APEX2 Project A demonstration of how to create a new APEX2 image processing application project featuring upscaling and downscaling in the S32 Design Studio. https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS Debug 5 | ISP Debugging w/ S32 Debug Probe A demonstration of how to setup and debug an ISP application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 6 | APEX2 Debugging w/ S32 Debug Probe A demonstration of how to setup and debug an APEX2 application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 7 | APEX2 Debugging with Emulator A demonstration of how to debug an emulated-APEX2 image processing application project in the S32 Design Studio. 8 | Debug a bare-board APEX2 Project A demonstration of how to debug a bareboard APEX2 image processing application project in the S32 Design Studio with Lauterbach TRACE32. 9 | Debug a Linux A53 Project A demonstration of how to debug a Linux A53 application project in the S32 Design Studio for Vision version 2.0. The example shown also includes code for APEX, but currently GDB Remote Linux only supports debug of the A53 code. 10 | Debug a bare-board A53 Project A demonstration of how to debug a bareboard A53 image processing application project in the S32 Design Studio for Vision version 2.0 using PEMicro GDB interface. The example shown also includes code for APEX, but currently PEMicro only supports debug of the A53 code.
View full article
Getting started with APEX2 S32DS for Vision: Getting Started - APEX2 Graph Tool Tutorial  Getting started with ISP S32DS for Vision: Getting Started - ISP Graph Tool Tutorial 
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Vision v2.0          Austin, Texas, USA September 15, 2017 The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Vision  v2.0. The S32 Design Studio enablement simplifies and accelerates the deployment of ADAS vision and neural network solutions in automotive, transportation and industrial applications. Release Content Eclipse Neon 4.6 Framework GNU Tools for ARM® Embedded Processors (launchpad) build (4.9.3 20150529) ARM64: Linaro GCC 4.9-2015.05 Libraries included: newlib, newlib-nano and ewl2 (ewl and ewlnano) NXP Array Processor Unit (APU) Compiler P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) Fully integrated Vision SDK release v.1.0.0. (for the details on the feature set of SDK please refer to Reference Manuals) New Project wizard to create application, library and Visual Graph projects for supported devices Visual Graph tools to support ISP and APU/APEX2 program development Peripherals Register View DDR configuration and validation tools Lauterbach debugger support by new project wizard Kernel Aware debugging for FreeRTOS, OSEK. Devices supported: S32V234 Complete S32 Design Studio for Vision v2.0 release notes are available here. Installation To download the installer please visit the S32 Design Studio product page downloads section or click the direct here. The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. For more information about the product installation see S32DS Vision 2.0 Installation Manual.   Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
View full article