S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
This document shows the step-by-step process to create a simple blinking LED application for the S32R41 family using the S32 RTD AUTOSAR drivers. This example used for the S32R41 EVB, connected via ethernet connection through S32 Debugger. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32R41 development package and the S32R41 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. Launch S32 Design Studio for S32 Platform Procedure New S32DS Project OR Provide a name for the project, for example 'Blinking_LED_RTD_With_AUTOSAR'. The name must be entered with no space characters. Expand Family S32R41, Select S32R418AB Cortex-M7  Click Next Click '…' button next to SDKs   Check box next to PlatformSDK_SAF85_S32R41_2022_08_S32R418AB _M7_0. Click OK And also, uncheck the other core Cortex_M7_1 Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents. To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file. Select the overview tab and disable Pins tool. Make sure to overview tab windows shows settings shown as below.  Here, we are disabling pin tools and using MCAL driver from peripheral tools for using AUTOSAR drivers. Now from Overview menu, select peripheral tools and double click to open it. In the driver sections, “Siul2_Port_1 driver” is the non-AUTOSAR version driver and so it must be replaced. Right click on ‘Siul2_Port_1’ and remove it. Keep BaseNXP driver as it is. Click on the ‘+’ next to the MCAL box. Locate and then select the ‘Dem’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Dio’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Mcu’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Port’ component from the list and click OK. Now components tab should show like below : Now we required to configure the different MCAL drivers that we added. Starting with Dio configuration, open the Dio configuration. No change is required for Dem configuration. Now, open the ‘DioGeneral’ tab, and select checkmark as per shown below: Now, open the ”DioConfig” tab. In that Select  “+” sign adjacent to Dio Channel. Then Edit Name to “Digital_Output_LED_0” and Dio Channel Id to ‘4’ instead of ‘0’. From the schematic for S32R41 EVB, checking for signal line for the user LED, channel 4 is connected to user LED signal, so we use channel 4 for signal line for user LED on the chip. So, we select the signal line for Dio channel Id 4 for the LED connected on the S32R41 EVB. Now Select Port tab for Port configuration. And open the Port Configuration tab, and from that open “PortConfigSet” tab. Change the PortPin Mscr to 36 , PortPin Direction to PORT_PIN_INOUT as shown below: Now, at the bottom you will find the “UnTouchedPortPin ’’ . Click on “+’’ and add PortPins. Now add port pins 0, 1, 2, 3,4 as per below configuration Now configure MCU component. Select Mcu component in MCAL, and then open the Mcu configuration. In Mcu configuration click MCUModuleConfiguration and then select  “McuModesettingConf” from the dropdown menu as shown below. From McuModeSettingConf select McuPartitionConfiguration Now open “McuPartition0Config” tab. And under the McuCore0Configuration for “McuCoreClockEnable” select checkbox and for “McuCoreResetEnable” uncheck  the checkbox. Similarly, And under the McuCore1Configuration for “McuCoreClockEnable” select checkbox and for “McuCoreResetEnable” uncheck  the checkbox. After modification it should be as shown below: Now open the “McuPartition1Config” tab. for "McuPartitionClockEnable" select checkmark to true and for "McuPartitionResetEnable" uncheck  the checkmark   And under McuCore0Configuration for "McuCoreClockEnable"  select checkmark to true and for "McuCoreResetEnable" uncheck  the checkmark After modification it should be as shown below: Now, click on global setting icon as shown below: And, Confirm that ComponentGenerationMethod is set to “FunctionalGroups” Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar. To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective. If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added. Before anything else is done, Initialize the clock tree and apply PLL as system clock, Apply a mode configuration, Initialize all pins using the Port driver by adding – editing code before write code here comment in main function.        /* Initialize the Mcu driver */        Mcu_Init(&Mcu_Config_BOARD_InitPeripherals);        /* Initialize the clock tree and apply PLL as system clock */        Mcu_InitClock(McuClockSettingConfig_0);        /* Apply a mode configuration */        Mcu_SetMode(McuModeSettingConf_0);        /* Initialize all pins using the Port driver */        Port_Init(NULL_PTR); Now replace the logic of for loop as shown below code section, which will enable the LED blinking for 10 times: You also need to declare and initialize the loop variable: uint8 i = 0U; Then replace the code as below after write your code comment: /*Logic for blinking LED 10 times*/ while (i++ < 10) {       /* Get input level of channels */       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_0, STD_HIGH);       TestDelay(3000000);       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_0, STD_LOW);       TestDelay(3000000); } Before the 'main' function, add a delay function as follows: void TestDelay(uint32 delay); void TestDelay(uint32 delay) {     static volatile uint32 DelayTimer = 0;     while(DelayTimer<delay)     {         DelayTimer++;     }     DelayTimer=0; } Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application: Add #include "Mcu.h" #include "Port.h" #include "Dio.h" Now, in open peripheral tools again by clicking on icon as shown below. And then click on global setting icon as shown below: And, Confirm that ComponentGenerationMethod is set to “FunctionalGroups” Build 'Blinking_LED_RTD_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'. After the build completes, check that there are no errors. Open Debug Configurations and select 'Blinking_LED_RTD_with_AUTOSAR_Debug_RAM'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist. And make selection as shown in screenshot below. You need to select the ethernet connection for S32 debugger and provide its IP address Click Debug To see the LED blink, click ‘Resume' This code as it will blink the LED 10 times, you can make changes in for loop condition to blink it infinitely.
View full article
Project created by S32 Design Studio (S32DS) new project wizard typically contains the debugger configurations to load  and debug the project into the code memory (Flash/RAM). However there might be situations that require also to load a content/data (e.g. calibration values) into a special on-chip memory (such as shadow flash, data flash, utest flash...) or an external memory (QSPI). This document describes how to program multiple memory types (using different programming algorithms) just by single click on the debug button. The decription applies to PEMICRO probes (Multilink Universal, Multilink FX or OpenSDA) anyway a similar approach might be applicable for other vendor probes. The process can be splitted into two steps: 1. create a separate debugger configurations to program a specific memory modules(QSPI,  data flash,..) 2. associate the program and debug configurations into the single launch group  - this alows to execute multiple actions by invoking the single debug launch . Let's demonstrate this on MPC5744P and program code and data flash memory using S32DS for Power v2.1 (similar approach can be applied also to other architectures/versions of S32DS). •  Create a new empty project for MPC5744P. Such a project typically contains Debug/Debug_RAM debugger configuration. First we will add a dummy code  (see below) that creates a record to be stored into the data flash memory (different to code flash memory block). • The project linker file (MPC57xx_flash.ld) should have the data flash memory block and a linker section associated with data flash (.dflash) defined: MEMORY { dflash : org = 0x00800000, len = 0x1F /* not entire dflash - just for test*/ flash_rchw : org = 0x00FA0000, len = 0x4 cpu0_reset_vec : org = 0x00FA0004, len = 0x4 m_text : org = 0x1000000, len = 2048K m_data : org = 0x40000000, len = 384K local_dmem : org = 0x50800000, len = 64K } SECTIONS { .dflash : { KEEP(*(.dflash)) } > dflash … •Add a test code into main.c that results in creating a dummy data record in data flash memory (0x0800000) __attribute__((section(".dflash"))) volatile char dflash_data[]="DTEST String"; // place the string into .dflash segment int main(void) { volatile int counter = 0; volatile char test_str[10]; test_str[0] = dflash_data[0]; // use DFLASH data (to avoid deadstripping) /* Loop forever */ for(;;) { counter++; } } Now if you build the project you can see the data that belong to dflash and code flash in the .map or srec file. If you debug the project using the default debug configuration data flash (DFLASH) memory is not programmed. To program DFLASH you should create another debug configuration simply by duplicating the existing one and changing the programming algorithm to dflash one: nxp_mpc5744p_1x32x20k_dflash.pcp. Note: There are many flash programming algorithms available in PEMICRO eclipse plugin folder typically located here (version of plugin may vary): "C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\" S32DS: Duplicate Debug Configuration S32DS: Load parameters S32DS: Choose alternative programming algorithmNow the new debug configuration (MPC5744P_code_dflash_Debug_DFLASH) is able to program data flash memory. The final step is to create a launch group configuration and associate it with all the programming/debugging configurations that should be executed once debug is started. Add the debug configuration used just for programming purpose as flash type and code debug configuration as debug type. In order to avoid interference between programming of various memories select post launch action -> "Wait until terminated" Finally as soon as the debug session is established by launching the launch group created above - all the memories are programmed and you can debug the code. Note: There is an information about executed flash configurations in the debug context view. Since the programming has alredy finished the thread is terminated and could be cleared by double cross icon. Enjoy single click programming&debugging in S32 Design Studio!
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio v3.3 Vision Extension Package for S32V234 1.2.0          What is new? Integrated VSDK 1.6.0   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for S32 Platform product page -> Downloads section or use direct link to download the update archive zip file        Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step       Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
View full article
S32DS for Vision contains many example projects from which you can learn how S32DS for Vision can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS for Vision. In this document, the procedure for creating a project from one of the provided ISP examples through to execution on the EVB is detailed. 1) Launch S32DS for Vision 2) Select "New S32DS Project from example" 3) Select isp_sonyimx224_csi_dcu project    In this particular project, the ISP graph diagram is included. If you wish to view it, go to the Project Explorer panel and expand 'isp_sonyimx224_csi_dcu_graph'. Then double click on 'ISP data flow : isp_sonyimx224_csi_dcu_graph'. The ISP graph diagram will appear in the editor panel. 4) Change to C/C++ perspective, click on 'Switch to C/C++ Development' 5) Select isp_sonyimx224_csi_dcu: A53 in the Project Explorer panel 6) Build project for A53  7) Start a debug session using method as described in HOWTO Create A53 Linux Project in S32DS for Vision, beginning at step 9. 😎 Should get results similar to this:
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 2          What is new? This update adds bare-board device support for S32K118 and some minor fixes. This is a cumulative update - it includes all the content of previous Update 1 Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
View full article
This release of S32K116 Bootloader was compiled and tested with the following development tools: S32DS Rappid Bootloader  Tested on the hardware: Development Board S32K116EVB – Q048 Processor  PS32K116MLF- Q048   Supported communication: UART0 (Pin PTB0-PTB1) CAN0 (Pin PTE4-PTE5)
View full article
CAN communication is supported in the latest version of MPC5744P Bootloader .rbf file (attached below) + Supported UART1/LINFlexD_1(OpenSDA on DevKit): PD9-PD12 pins(Speed: 115200b/s) + Supported  CAN_0 (J5 on DevKit):  PB0-PB1 pins(Speed: 500Kb/s)   Tested on the dev boards:   Development Board DEVKIT-MPC5744P MPC5744P-144DC MPC5744P-257DC Processor MPC5744P-FML09 1N15P MPC5744P-FMLQ8 0N65H PPG5744P-FMMM8 0N65H  
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v1.2, Update 3            September 21, 2017   What is new? S32 SDK EAR 0.8.1 supporting MPC5748G & MPC5748C. The new project wizard now offers the new version of S32 SDK: "New S32 Project from Example" offers additional demos and examples. The complete S32 SDK EAR 0.8.1 release notes attached below. Installation instructions This is a cumulative installer - all previous updates (except previous version of S32 SDK EAR 0.8.0) are included so you do not need to install any previous update. The update is available for online (Eclipse Updater) or offline (direct download link) installation. online installation go to menu "Help" -> "Install New Software..." dialog  select predefined NXP S32 Design Studio update repository select all available items http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite click "Next" button offline installation  go to S32 Design Studio product page -> Downloads section or use the direct download linkand download the "S32 Design Studio for Power v1.2 - Update 3" file. Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 3 archive file Select all available items and click "Next" button.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 8          What is new? S32 SDK for Power Architecture 1.8.0 EAR supporting MPC5777C, MPC5775B, MPC5775E, MPC5746R, MPC5745R, MPC5743R This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7 ). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0 Update 3          What is new? S32 SDK 0.8.6 EAR (Early Access Release)  for S32K142, S32K144, S32K146, S32K148)- see attached release notes for more details Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32 Design Studio for ARM v2.0 - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2_0/com.freescale.s32arm.updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use this direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button. This will starts the update installation process.
View full article
Create From Example 1 | Create an ISP Project from Example A demonstration of how to load an example ISP image processing application project featuring RGB, YUV, and GS8 image formats, in the S32 Design Studio. 2 | Create an APEX2 Project from Example A demonstration of how to load an example ORB-based APEX2 image processing application project in the S32 Design Studio. https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS Create New Project 3 | Create a New ISP Project A demonstration of how to create a new Debayer-based ISP image processing application project in the S32 Design Studio. 4 | Create a New APEX2 Project A demonstration of how to create a new APEX2 image processing application project featuring upscaling and downscaling in the S32 Design Studio. https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS Debug 5 | ISP Debugging w/ S32 Debug Probe A demonstration of how to setup and debug an ISP application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 6 | APEX2 Debugging w/ S32 Debug Probe A demonstration of how to setup and debug an APEX2 application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 7 | APEX2 Debugging with Emulator A demonstration of how to debug an emulated-APEX2 image processing application project in the S32 Design Studio. 8 | Debug a bare-board APEX2 Project A demonstration of how to debug a bareboard APEX2 image processing application project in the S32 Design Studio with Lauterbach TRACE32. 9 | Debug a Linux A53 Project A demonstration of how to debug a Linux A53 application project in the S32 Design Studio for Vision version 2.0. The example shown also includes code for APEX, but currently GDB Remote Linux only supports debug of the A53 code. 10 | Debug a bare-board A53 Project A demonstration of how to debug a bareboard A53 image processing application project in the S32 Design Studio for Vision version 2.0 using PEMicro GDB interface. The example shown also includes code for APEX, but currently PEMicro only supports debug of the A53 code.
View full article
KEA64 RAppID Bootloader rbf file for KEA64    MPC57xx RAppID Bootloader rbf file for MPC5744P   RAppID Bootloader rbf file for MPC5746R  RAppID Bootloader rbf file for MPC5777C  RAppID Bootloader rbf file for MPC5777C - BookE (non-VLE)    S32Kxx RAppID Bootloader rbf file for S32K116 RAppID Bootloader rbf file for S32K144W  
View full article
This instruction details the steps to create an image vector table, then subsequently generate a blob image which can be written to external flash on the S32R45 EVB. For this, the 'hello_world_s32r45' example project from the S32R45 SDK installed to S32 Design Studio IDE. This instruction shows the process for QSPI, however, SD, MMC, and eMMC are also supported.   The Image Vector Table (IVT) image is a set of pointers to other images which are required by the BootROM. It typically contains the following images, though not all are required to create a valid IVT image: DCD Self-Test DCD HSE Application Bootloader   The IVT Tool enables configuration and generation of the IVT image as specified in the BootROM reference manual.   Prerequisites Before using the IVT Tool, it will be useful to have already generated the binary image from your application project, it will be an input to the IVT. It may also be necessary to include a DCD image, for example, to initialize the SRAM. For application bootloader image, follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file, selecting 'Raw binary' option. For DCD image, follow the steps in HOWTO: Use DCD Tool To Create A Device Configuration Data Image .     Procedure With desired project open in project explorer (C/C++ perspective), switch to IVT perspective. Click on 'Open IVT'. In the Boot Configuration section, check that the correct Boot Target is selected. For the demonstration here, M7_0 is the correct selection. Check the 'Interface selection' section. If your intended boot device is SD, MMC or eMMC, then change the setting from QuadSPI Serial Flash. If your intended boot device is QuadSPI AND you do not have a QuadSPI parameter file to specify, then uncheck the box for 'Configure QuadSPI parameters'. QuadSPI parameters change some flash registers' settings away from the default setting and are generally required for larger memory sizes (for ex. applications over 1 MB in size, for some supported devices). From the Image Table section, depending on your configuration, turn off all unused images. For the demonstration here, the following will be changed to Reserved: Self-Test DCD, Self-Test DCD (backup), DCD (backup), Application bootloader (backup). The following images will remain enabled: DCD, Application bootloader. In DCD section of the Image Table, click 'Browse File' and select the DCD binary file. Ignore the red shading on the Start address and Size in bytes fields for now. Now the red shading should be resolved. This is appearing because when the DCD section was enabled, it added a block to the Memory Layout map. But the other blocks in the map are unchanged resulting in overlaps. To resolve this, click on the ‘Align’ button from within the Automatic Align section.. After the Memory Map has been aligned, a confirmation message will be displayed and the red shading will disappear. In Application bootloader section, again use  'Browse File' and select the application binary. When the application boot image is loaded, the tool processes the file to check if it contains the header for the application bootloader image. If the header is not found, it means that the file is only the raw code (the bin generated by S32 Design Studio) and it will be necessary to provide the values for RAM start & entry addresses (code length is automatically calculated), as noted with the expanded view and red shading. To set the RAM start pointer and entry pointer addresses, from to the C/C++ perspective: From Project Explorer on the C/C++ perspective, open the linker file (hello_world_s32r45\Project_Settings\Linker_Files\S32R45_common_ram.ld) and locate the RAM start address and enter it in both the RAM start pointer AND RAM entry pointer fields in the IVT Tool. Since the application binary file which was loaded is just a raw binary file, it is necessary to generate the full application bootloader image. The Export Image function takes the values entered for the RAM start & entry pointers and Code length, then generates the Application bootloader header. This header is added to the raw binary file producing a new image, the full application bootloader image file. Within the Application bootloader section, click 'Export Image' and enter a meaningful name for the image file. In addition to being a necessary source component of the IVT image, this file can more easily be shared or re-used to as an input to other IVT images. After the file has been generated, you will notice that the address settings section has collapsed. This is because it has replaced the file you originally selected with the newly generated one and the tool has recognized that the file contains the required header information. Click 'Export Blob Image' to generate the blob image file. This is what will be flashed to the target. Now that the Blob Image is generated, the 'Flash Image' button could be used to program the image to the target over serial connection, use the S32 Flash Tool, or over the JTAG connection using the Flash Programmer within the S32 Debugger (QSPI only).
View full article
Condition:  I am trying FreeRTOS using S32K118 EVB and run in DEBUG mode. When I set the break point in vTaskDelay and press Resume for the first time, there is a smooth stop at the break point. The second time I press Resume, the debugger should enter the same break point again, but there is no response. Then I press Suspend and can't press Resume again, at this point I can only leave. However, I am free to run this project with no problem, what's wrong? Analysis: This is due to an access of DDR memory region which is not initialized by default project settings. Solution: To resolve it, a macro initializing the DDR memory should be selected to run at the beginning of a debug session. A user should go to Advanced Options dialog and check "Enable initialization script". Our DDR init macros can be found at the following location within S32DS3.2 layout: eclipse\plugins\com.pemicro.debug.gdbjtag.pne_4.2.8.201909091700\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR3_EVB29288.mac. Please note that the type of the macro might depend on the revision of the board and S32V23x device one is working with. I am also attaching a picture of debug configuration and Advanced Options dialog with all the settings in place.
View full article
When you use the New Project Wizard within S32 Design Studio to create a project, starting a debugging session is easy since the wizard creates the debug configuration for you. In this document, the case for NXP devices supported by the GDB PEMicro Debugging Interface is detailed.    Prerequisites The project to be debugged should be loaded to the workspace and open                 Procedure Build the project. Select the build configuration. (optional) If you already know which build configuration is desired, you can preselect it. If not, one is already selected for you by default. It will be noted with a check mark. Typical options contain choices between RAM and FLASH memory builds and for each a choice between Debug and Release. For debugging purposes the Debug option should be selected.                 Click on Build. Clicking this button will start the build using the preset build type.     Or, select the build type from the pick list. This will start the build for the build type selected, regardless of which one is marked with a check mark.       Check there are no compiler errors.                     Configure the debug configuration to start a debug session. Click ‘Run’ pulldown menu. Select 'Debug Configurations…'     Select the debug configuration associated with your current build configuration.     Select whether to rebuild code each time debug session start is requested.   Click on Debugger tab.     Verify proper interface and port.     Click Debug      
View full article
Purpose   This document holds information about how S32 Design Studio and S32Debugger probe or PE Micro Debug probe can be used to debug applications running on NXP’s S32 family processors from the operating system perspective using OSEK Kernel awareness.   Abbreviations Abbreviation Description OSEK Open Systems and their Interfaces for Automotive Electronics is a standard developed in the automotive industry to define a common architecture for embedded Real-Time Operating Systems (RTOS). NXP RTOS NXP Real Time Operating System compliant with OSEK specification  ORTI OSEK Run Time Interface.  ORTI file is generated based on NXP RTOS configuration *.ort / *.orti OSEK system builder ORTI file extension MSI Microsoft Software Installer   Background OSEK Kernel awareness within S32 Design Studio allows you to debug your application from the operating system perspective. ORTI is a specification that enables OS awareness for external debuggers (e.g NXP S32 Debugger, Lauterbach T32, PEmicro's debug probe).  Most OSEK system builders are able to extract all necessary information of the OS component into a text file, called “ORTI file”. NXP RTOS generates an *.ort file based on the user configuration. Debuggers can load this ORTI file to add support for the operating system. S32Design Studio can load such an ORTI file and adds some special views that will allow the user to inspect the configured OS objects: Tasks, Alarms, Counters, Scheduletable.   Document structure The basic workflow for setting up and managing OSEK OS Awareness projects in S32 Design Studio remains consistent across both single-core and multi-core projects, irrespective of the debug probe used. The focus will be on the universal steps that are described in single-core projects case. For OSEK OS Awareness multi-core projects and for projects utilizing PE Micro debug probes, only the specific considerations will be highlighted.                 Hardware Support OSEK OS Awareness support in S32 Design Studio is available for: S32G27x, S32G39x S32E/Z  S32K396 S32R41 SAF85xx   OS Support OSEK OS Awareness support is available only on Windows.   How to use OSEK OS Awareness with S32 Design Studio and S32Debugger probe   Single core projects   Prerequisites Note: This HOWTo Guide describes the required steps for using OSEK Run Time Interface on a single-core example project for S32R418AA Cortex-M7 in S32 Design Studio. Prerequisites might differ depending on the project hardware type.   Software environment S32 Design Studio project or example project delivered with the NXP RTOS imported in S32 Design Studio Workspace S32R41 Development Package S32R41 Real-Time Drivers Version 1.0.0 SW32R41 RTOS 4.7.0 version 0.9.0 BETA   !Note: For this example project, NXP RTOS SysGen requires Java Runtime Environment OpenJDK-JRE 11.0.11 installed on your computer. The OpenJDK-JRE can be downloaded from the following URL (please search with exact keyword "jre-11.0.11-x64 MSI" or “jdk-11.0.11-x64 MSI” for correct version): https://developers.redhat.com/products/openjdk/download Using the installer (MSI) is recommended because it creates the HKEY_LOCAL_MACHINE\SOFTWARE\JavaSoft\JDK registry entry. JAVA_HOME environment variable must be set to point to location of Java Runtime Environment. For example: JAVA_HOME=C:\Program Files\RedHat\java-11-openjdk-jre-11.0.11-1 (Please choose correct path for your machine). Error or unexpected behavior may occur if the version of Java is different than 11.0.11 when NXP RTOS SysGen is executed (steps that are described Chapter III – “Generating Configuration”). If Java version is not found in the HKEY_LOCAL_MACHINE (HKEY_LOCAL_MACHINE\SOFTWARE\JavaSoft) a warning is reported.    Hardware environment Silicon: - Chip P/S32R418AAU(K1)MUFT (rev 1.1) Board: - X-S32R41-EVB PCB 48194 RevD SCH RevD Debug Probe: S32 Debug Probe       Project setup While in Design Studio, go to File -> New -> S32DS Project From Example  and select one of the existing single core S32 Design Studio Sample applications delivered with the NXP RTOS or import your own S32 Design Studio project.   Select the desired project from the list of examples and click finish       Generating configuration Before running the example, a configuration needs to be generated. First, go to Project Explorer View in S32 Design Studio and select the current project.   Right click and select the "S32 Configuration Tool" menu then click "Open Peripherals".  Click on the "Update Code" button.   Click on Select directory under "Generate" field to select the directory which contains example project (E.g.: D:\WorkspaceS32DS\RTOS_example_S32R418AA_SC1_M7) then click on Generate Configuration.  Click "Update Code" again.   Building the project Select the project in the S32 Design Studio Workspace and click on Build. Clicking this button will start the build using the preset build type.    Debug configuration Click on Debug Configurations   Setup the Debug Probe Connection for the project. Select either USB or Ethernet, depending upon your hardware setup. If USB is selected, the COM port for the S32 Debug Probe will automatically be detected (unless not connected or more than one probe is connected). If Ethernet is selected, then enter either the hostname (fsl + last 6 digits of MAC address) or IP address. See ‘S32_Debug_Probe_User_Guide.pdf’ ({S32DS_installation_directory}/S32DS/tools/S32Debugger/Debugger/Docs/S32_Debug_Probe_User_Guid e.pdf) for more details on the setup of the S32 Debug Probe.      Loading the ORTI file and starting debug From the OS Awareness tab select “OSEK” from the OS dropdown list. Browse and select from local system or Workspace the required *.ort file Click the Debug button.     OS Details Browser view Navigate to go to Window -> Show View -> Other…  and select the OS Details Browser view     Using the OS Details Browser view, Design Studio can display information about the tasks status on the target.   Tasks tab In the “Tasks”  tab from the OS Details Browser view you can see information about the operating system (the number of tasks, current task states, system objects):   Implementation tab Switch to the “Implementation” tab to see more detailed information gathered from the .ort file:   OS – current state Tasks – priority, state and assigned stack Stacks – usage and attributes Other OS resources defined and declared through ORTI Detailed info about ORTI data object Customize data presentation (HEX format, re-arrange the table columns) Colored presentation of data: -   White fields are static Blue fields are non-static Yellow fields are fields that changed their values from the last time they were inspected/checked.   OS information: Tasks information:   Stacks information:   Multi-core projects Prerequisites Note: This HOWTo Guide describes the required steps for using OSEK Run Time Interface on a multi-core example project for S32Z270 Cortex-R52 in S32 Design Studio. Prerequisites might differ depending on the project hardware type.   Software environment: S32 Design Studio project or example project delivered with the NXP RTOS imported in S32 Design Studio Workspace S32Z2/E2 Development Package S32Z/E Real Time Drivers Version 0.9.0 S32ZE RTOS R21-11 version 0.9.0   !Note: For this multi-core example project, NXP RTOS SysGen requires Java Runtime Environment OpenJDK-JRE 1.8 installed on your computer. The OpenJDK-JRE can be downloaded from the following URL (please search with exact keyword "jdk-8u372-x86 MSI" for correct version): https://developers.redhat.com/products/openjdk/download - Using the JDK 1.8 installer (MSI) is recommended. JAVA_HOME environment variable must be set to point to location of Java Runtime Environment. For example: JAVA_HOME= C:\Program Files (x86)\Java\java-1.8.0-openjdk-1.8.0.372-1 (Please choose correct path for your machine). Error or unexpected behavior may occur if the version of Java is different than 1.8 when NXP RTOS SysGen is executed (steps that are described in Chapter III – “Generating Configuration”).   Please notice that SysGen is not stable in JRE 1.8 64 bit. Using SG with JRE 1.8 32 bit is recommended.     Hardware environment:             Boards: S32Z27X-DC PCB 50588 RevA1 SCH RevB (DC2)             Silicon chip: P32Z270ADCK0MJFT P65C ATTJ2151A (E2). (21x21, 594 BGA) Debug Probe: S32 Debug Probe               Boards: S32Z270-DC PCB 50912 RevA SCH RevA (DC1)             Silicon chip: S32Z270ADCK0MJET (17x17, 400 BGA) Debug Probe: S32 Debug Probe   Project setup Go to File -> New -> S32DS Project From Example  and select one of the existing multi-core S32 Design Studio Sample applications delivered with the NXP RTOS or import your own S32 Design Studio project.      Generating configuration The steps for generating configuration must be performed for all projects: RTOS_example_S32Z270_SC1_multi_instance_R52_0_0, RTOS_example_S32Z270_SC1_multi_instance_R52_0_1, RTOS_example_S32Z270_SC1_multi_instance_R52_0_2, RTOS_example_S32Z270_SC1_multi_instance_R52_0_3.   Building the projects Before running, you must build all projects: RTOS_example_S32Z270_SC1_multi_instance_R52_0_0, RTOS_example_S32Z270_SC1_multi_instance_R52_0_1, RTOS_example_S32Z270_SC1_multi_instance_R52_0_2, RTOS_example_S32Z270_SC1_multi_instance_R52_0_3.     Debug configuration Click on Debug Configurations. Click the initial core under S32 Debugger in Debug configurations menu.  Setup the Debug Probe Connection.    Loading the ORTI file   Loading the ORTI file must be done for all the project configurations:  RTOS_example_S32Z270_SC1_multi_instance_R52_0_0 RTOS_example_S32Z270_SC1_multi_instance_R52_0_1 RTOS_example_S32Z270_SC1_multi_instance_R52_0_2 RTOS_example_S32Z270_SC1_multi_instance_R52_0_3   Starting debug on multi core project From the Debug Configuration menu, click on Launch Group for S32 Debugger. Check all the cores that you want to debug. Click the Debug button.   OS Details Browser view Compared with single core projects, when debugging multi core projects you can switch between the debugging sessions and information from all debugged cores   Tasks tab     Implementation tab The information displayed in Implementation tab is the same as in single-core projects case, but you can switch between the debugged cores       How to use OSEK OS Awareness with S32 Design Studio and PE Micro Debug probe Prerequisites Note: This HOWTo Guide describes the required steps for using OSEK Run Time Interface on a single-core example project for S32K396 Cortex-M7 in S32 Design Studio. Prerequisites might differ depending on the project hardware type.   Software environment: S32 Design Studio project or example project delivered with the NXP RTOS imported in S32 Design Studio Workspace S32 Design Studio 3.5.6 development package with support for S32K396 devices S32K3 Real-Time Drivers Version 3.0.0 P01 SW32K396 RTOS version 0.9.0 BETA   !Note: check the note from S32 Debugger – multi-core projects and install requires Java Runtime Environment OpenJDK-JRE 1.8   Hardware environment: Board:             Mini-module: XS32K396-BGA-DC PCB 54614 RevX1 SCH RevA              Silicon: Chip P32K396EHMJBS OP40E QAD2222F  Debug Probe: PE Micro Debug Probe     Project setup Select the desired project from the list of examples delivered with PE Micro Debug probe support or import your own S32 Design Studio project and click finish For this How To Guide, RTOS_example_S32K396_SC1_M7_0_0 was used   Generating configuration     Building the projects Select the project in the S32 Design Studio Workspace and click on Build.    Debug configuration Click on Debug Configurations. Select the debug configuration associated with your current build configuration and click on the “PEmicro Debugger” tab. Verify proper interface and port and if the device is properly detected.   Loading the ORTI file and starting debug From the OS Awareness tab select “OSEK” from the OS dropdown list. Browse and select from local system or Workspace the required *.ort file Click the Debug button.   OS Details Browser view Go to Window -> Show View -> Other…  and select the OS Details Browser view   Tasks tab In the “Tasks”  tab from the OS Details Browser view you can see information about the operating system (the number of tasks, current task states, system objects):   Implementation tab  “Implementation” tab displays more detailed information gathered from the .ort file:   Revision history: Revision no. Revision date Description 01 Nov 2023 Created document about how to use OSEK OS Awareness in S32 Design Studio on single and multi core projects with PE Micro and S32 Debug probes    
View full article
After installation of S32 Flash Tool 2.1, try to start the GUI and get below error : We noticed this behavior on some PCs – either OS setup or security rules do not allow the installer to create a link to the JRE (Java 11) that is installed with Flash Tool. A quick fix is to set the path manually by adding the following lines to “S32FlashTool_2.1\GUI\ s32ft.ini”
View full article
This application demonstrate integration Processor Expert (PE) RAppID Suite for  MPC5777M initialization tool with S32 Design Studio for Power v1.1. There is a separate RAppID project and RAppID Workspace folder included in this project:       This multicore project first initializes the device (PinMux, Clocks, PIT timer). Each core toggles with one LED with different time period. Z4_0 core: LED1...GPDO[0] Z7_0 core: LED2...GPDO[1] Z7_1 core: LED3...GPDO[2]     Yo can adjust the device initialization in PE RappID (open included workspace), generate the code and finally rebuild the project in S32DS.   Note:  Do not let generate PE_Types.h file since it includes some non-vle instructions mixed with VLE ones - this cannot be built by S32DS compiler. linker command file generation needs to be disabled otherwise it generates HighTec specific keywords that S32DS GCC linker does not understand.    Test HW:       MPC5777M-512DS, MPC57xx Motherboard MCU:             PPC5777MQMVA8 0N78H Debugger:    PeMicro USB-ML-PPCNEXUS Target:           Debug (internal flash) EVB connection:  USER LED1 connected to P8.0, LED2 connected to P8.1 LED3 connected to P8.2
View full article
The following article describes how to add FreeRTOS thread aware debugging to the Eclipse Debug view using SEGGER J-Link: Show FreeRTOS Threads in Eclipse Debug View with SEGGER J-Link and NXP S32 Design Studio | MCU on Eclipse  I hope this is useful, Erich
View full article