S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
Sometimes you would like to share sources between projects and - even better - between platforms. Let's say that we are developing software with the very same functionality for S32K144 and MPC5744P. In this case, we can identify platform independent functions - generic, platform specific functions - not related to MCU itself, but related to the way some peripheral works (for example different ADC result range) - and MCU dependent functions like clock init. In attachment is a very simple SDK which can be shared with S32K144 and MPC5744P (each in different S32DS editions).  Unzip my_sdk.zip archive (for example C:\NXP folder). You can import example projects, but instead let's start from the beginning. Create a new S32DS Application project and choose MCU: You can use default project configurations and click through to finish: Right click on project name -> Properties and select SDKs -> Add Complete the Name, Version and Description fields in New SDK dialog and click on Change button next to Location field. In Change SDK Location dialog, leave Define new variable setting selected, click Browse and find the my_sdk path: Now we can select files (sources, headers...) from selected SDK, you can select all available files. If you select a folder, then all files in that folder will be selected as well. Don't forget to select header files too: If you choose Copy - the files will be copied into project folder and you can do local changes. Without this option (default) - changes will be shared between all projects depended on this particular SDK. The ability to individually select the files to be included from the SDK as well as to copy into the project folder, provides much flexibility to customize SDK usage in your projects. Click on OK, then Attach/Detach... to attach this SDK into your project:  If you like to use your SDK for newly created projects (as an option in SDK select list) - click on Make global button: Now you can see changes in your project: As well, the SDK can be viewed in SDK Explorer (Window -> Show View -> Other...), where functions and macros are available for drag and drop functionality into your code: Platform specific code is filtered by preprocessor-defined macro. So - let's define if we are working with S32K144 or MPC5744P. Right click on project name -> Properties -> C/C++ Build -> Settings -> <Standard S32DS C Compiler OR name of your compiler> -> Preprocessor: We are done - now we can use SDK functions - S32K144:  and MPC5744P (enabling interrupts is default part of empty project for MPC5744P - that's only difference):
View full article
Eclipse caches some settings within the workspace directory. After installing a new version of S32DS, some settings in old workspaces may not match the requirement of the new version. The result is often errors reported on new as well as previously existing projects located in an existing workspace which you selected when launching S32DS. The best way to resolve this is to create a new workspace and then import your projects. This will ensure the workspace is created using all the correct settings for the version you have installed.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 2          What is new? This update adds bare-board device support for S32K118 and some minor fixes. This is a cumulative update - it includes all the content of previous Update 1 Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 8          What is new? Integrated Radar SDK RTM 1.4.0 (replacing RSDK 1.3.0) (see the RSDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
View full article
There are often errors displayed after the indexer completes building its data base following the creation of a new project or the opening of a project not already in the workspace and again just before building. Some of these errors can be due to settings in the Eclipse Indexer settings. In one scenario, a project which builds clean, that is, no compiler or IDE errors, will mark code lines in a source file which includes a large header file as 'cannot resolve symbol xxxx'. In this case, the header file is larger than 17 MB. In the Eclipse Indexer settings, there are settings 'Skip files larger than' and 'Skip included files larger than'. These settings, by default, are set to 8 MB. This would be too low for the header file in this example. In order to resolve the issue, the setting should be increased to allow for the large header file to be indexed.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 4          What is new? Radar SDK RTM 1.0.0. This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
Requirements: PC machine with telnet client (for Windows you can use Putty - Download PuTTY - a free SSH and telnet client for Windows ) DHCP server running on your PC machine or network connection with DHCP server How to install DHCP server on Linux https://www.ostechnix.com/install-dhcp-server-in-ubuntu-16-04/  DHCP server for Windows - Open DHCP Server download | SourceForge.net      S32 debug probe connected to network (with DHCP server) and visible for your PC machine   separate network using static IP addresses (or direct connection between PC and S32 debug probe). The scenario is similar like on this picture:  Procedure:   Connect power to S32 debug probe with already connected ethernet cable and wait until green LED (RX/TX) starts blink.Connect to S32 debug probe by telnet client. You can use default domain name FSLXXYYZZ where XXYYZZ are last 6 digits from S32 debug probe MAC address or assigned IP address: Static IP address can be set by netparam static_ip_address ADDRESS:NETMASK command. Make sure that you are choosing IP address from range of your Embedded network. My network uses standard 192.168.1.xxx here is mt setings:  netparam static_ip_address 192.168.1.100:255.255.255.0 You also need to set boot config from DHCP to Static: netparam bootconfig static Turn OFF and ON again S32 debug probe and check the settings by telnet with static IP address - in my case 192.168.1.100: We are done. 
View full article
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the capability to access the flash programming capabilities of the S32 Debug Probe via GTA command line and the GDB. This instruction details the steps to perform flash programming of the S32G274A EVB via the JTAG interface with the S32 Debug Probe.   Note: currently only QSPI flashing is supported.   Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. In this case, the S32G2xx development package. This is important as the S32 Debugger support within it contains the device-specific Python scripts required for initialization of the cores.  DanielBarbu_0-1729750035306.png   Setup the hardware Confirm the setup of the S32G274A evaluation board.  Configure the JTAG. The S32G274A evaluation board supports both 10- and 20- pin JTAG connections. The default board configuration is set to 20-pin, change the position of the jumper J59 from 2-3(default)  to 1-2, if you are using the 10 Pin JTAG interface. Both are supported by the S32 Debugger and S32 Debug Probe. Connect the power supply cable Setup the S32 Debug Probe Connect the S32 Debug Probe to the evaluation board via JTAG cable. Refer to the S32 Debug Probe User Manual for installation instructions. Use the JTAG connection as was confirmed in the previous step. Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard. DanielBarbu_0-1727938649769.png   Procedure Launch GTA server. From command prompt or Windows File Explorer run the command:  {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe Should see a window appear like this: DanielBarbu_1-1727938699487.png   Ensure Environment Variable for Python is set. From command prompt, run the command:  set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages DanielBarbu_2-1727938783899.png   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window. DanielBarbu_3-1727939439489.png   Configure the EVB's Boot Mode switches for Serial Boot. Issue the following commands, replacing the PROBE_IP address and FLASH_NAME, as appropriate: source {S32DS Install Path}/S32DS/tools/S32Debugger/Debugger/scripts/gdb_extensions/flash/s32flash.py py _FLASH_TYPE = "qspi" py _PROBE_IP="10.81.64.66" py _JTAG_SPEED=20000 py _GDB_SERVER_PORT=45000 py _GDB_TIMEOUT=7200 py _REMOTE_TIMEOUT=30 py _RESET_DELAY=1 py _RESET_TYPE="default" py _INIT_SCRIPT="{S32DS Install Path}/S32DS/tools/S32Debugger/Debugger/scripts/s32g2xx/s32g274a_generic_bareboard.py" py _FLASH_NAME="MX25UM51245G" py _IS_LOGGING_ENABLED=False py flash()   Note: Replace the {S32DS Install Path} in the commands above with the actual path to your installation of S32 Design Studio. Now flash commands may be used. fl_blankcheck -- blank check fl_close -- close command fl_current -- current device command fl_dump -- dump command fl_erase -- erase section of memory command, will erase whole sectors starting from 'offset' through 'size' contiguously, so to erase only one sector, ensure that the 'offset' address is within the desired sector and 'size' does not extend into the following sector fl_erase_all -- erase all memory command fl_info -- info command, shows list of registered devices fl_protect -- protect section of memory command fl_unprotect -- unprotect section of memory command fl_write -- write memory command, hex or binary are supported, options to erase first and verify after write fl_write_elf -- write elf file to memory command, options to erase first, verify after, and rearrange flash base Type 'help fl_<command>' to print the help info on the specified command Type 'help support' to print a list of the fl_ commands For example, you may wish to write a binary file: fl_write -e 0x0 C:\\Users\\<userid_folder>\\workspaceS32DS\\hello_world\\Debug_RAM\\hello_world_blob.bin Happy flashing with S32DS Flash Programmer!
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0 Update 2          What is new? S32 SDK 0.8.5 EAR (S32K142, S32K144, S32K146, S32K148) - see attached release notes for more details   MXQ 4.2 for MAC47D54H - see attached MQX release notes for more details. Installation instructions The update is available for online (via Eclipse Updater) or offline (direct download link) installation   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository  "S32 Design Studio for ARM v2.0 - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2_0/com.freescale.s32arm.updatesite" select all available items and click "Next" button.   offline installation:  go to S32 Design Studio product page -> Downloads section or use the direct download link to download the Update archive file. Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update archive file you downloaded in the previous step: Select all available items and click "Next" button. This will starts the update installation.
View full article
On some versions of Windows 10, there is an issue which could impact your ability to open documents from the Getting Started page in S32 Design Studio. While we have resolved this issue in some of the newer releases, not all editions of S32 Design Studio have been updated since this issue was discovered. Also, you may required to use an older release. The problem occurs when a document linked within the Getting Started window of S32 Design Studio. The S32 Design Studio is configured to use the Windows default web browser to open the files. For some Windows 10 installations, Microsoft Edge is the default browser and it is unable to correctly open the requested file. The typical error message is as shown below: To resolve the issue, it is necessary to change the default browser within your Windows preferences. Here are some steps to do that: 1) Click on 'Settings' from the Windows Start Menu 2) Type 'browser' in the search bar, then select 'Choose a default web browser' 3) Click on the currently selected Web browser to bring up the selection menu and select 'Internet Explorer' or 'Google Chrome' 4) Relaunch S32 Design Studio and try again to open the document from the link in Getting Started page.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 3.3  S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0          What is new? S32K1xx Development Package: New Project Wizard support for S32K1xx family, including S32K14xW P&E debugger support for S32K1 family NXP GCC for ARM NXP GCC for Arm version 6.3 build 2017 (same as was used in S32DS for ARM 2.2) S32 SDK for S32K1xx RTM 4.0.0: S32 SDK RTM 4.0.0 package adding support for S32K1xx and S32K1xxW families, cumulative release containing also the changes present in S32 SDK for S32K1xx RTM 3.0.0, 3.0.1, 3.0.2 and 3.0.3 Supports S32 Design Studio for S32 Platform v3.3 with S32 Configuration tools - Pin Wizard, Clock Configuration,... Supports creating project with NXP GCC for Arm Release version 6.3.1, GreenHills Multi and IAR Compiler Examples for supported devices with P&E Debugger and Segger J-link support Migration support for projects created in S32DS for ARM v2.2 (with Processor Expert) For more details, please review the S32SDK_for_S32K1xx_RTM_4.0.0_ReleaseNotes.pdf attached to this notice. See below. Installation instructions The update is available for online (via Eclipse Updater) or offline installation   online installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button   offline installation:   go to S32 Design Studio v3.3 product download page: S32 Design Studio for S32 Platform -> Downloads, click 'Download' button next to S32DS for S32 Platform v3.3, then select 'S32DS.S32K1.3.3.0_D2006.zip' to download the update archive zip file Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates" Add a new "Add.." S32DS Software Site and browse to select the downloaded update archive .zip file you downloaded in the previous step         Select from available items and click "Install/Update" button. This will start the update installation process.
View full article
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.1 Irina_Costachescu_0-1765805851218.png   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.1 with support for: AMCU AP RAS S32K3 Family S32G Family S32R41 Family S32K1 Family S32ZE Family S32R45 Family S32M2 Family       Major Features for S32 Design Studio 3.6.1 Installer S32 Design Studio 3.6.1 is delivered with all public NPI's in a single 2.94GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.1 using Extension and Updates mechanism as depicted below. Irina_Costachescu_0-1765875101337.png   Removed Activation Code request from installer, users will no longer be prompted for an activation code to install S32DS. Installer is now requiring admin rights upfront, Run as Administrator will correctly prompt Admin by Request for confirmation. New support to Upgrade an existing installation offline directly from the installer. 361sintalrr.jpg New support for Silent installation. Irina_Costachescu_3-1765794313757.png   Updated documentation files to the latest NXP templates. New Ubuntu 24.04 support.   Platform IDE and UI Significantly improved the look & feel in Extensions and Updates and user experience while installing packages with clearer package details (version, size, category, status), filtering options, and ability to export installed configuration to plain text and html formats. Furthermore, it provides an enhanced capability to inform the user about the new available software and what is already installed on the individual environment, each module being identified by color and group it belongs to. Ext&Updates-3.6.1 1.gif   Combine MMU Viewer entries based on the memory attributes. mmu.jpg Enabled support in Memory Spaces view to access memory via DAP (Debug Access Port). memspace.jpg Improved the refresh mechanism in Watch Registers and MMU views leading to modest gains in S32 Debugger performance. Introduced Find & Copy functions in MMU view to facilitate searching for a specific address.   S32 Debugger L1 Cache read capability for ArmV8-A. l1cache2.jpg l1cache1.jpg Enable asynchronous debug and runtime memory access with GDB non-stop mode.  nonstop.jpg Extend test connection to be able to specify a Command Converter Server (CCS) IP and port with adding value for CCS remote scenarios. Improved S32 Flash Programmer speed up to 60% for write operations. Extend mem_read and mem_write commands to use DAP – Debug Access Port for access. memsomething.jpg 3 rd Party Solutions Update of 3rd Party Debug support with TASKING v9.21.312.   Major Features for NPIs S32K389 Device Bring up support enablement of this device. Supported compilers: NXP’s GCC 9.2, 10.2;   GHS 2021.1.4  Full support of following debuggers: S32Debugger and Lauterbach k389.jpg   This release is available for download on: S32 Design Studio 3.6.1 can be found on:  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6  Automotive Software Package Manager   Target Audience: S32 Design Studio 3.6.1 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.1, available on nxp.com, in Flexera catalogue S32 Design Studio for S32 Platform v.3.6, and in Automotive Software Package Manager. If you have any local admin restrictions (ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.1 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds Irina_Costachescu_5-1765799664304.png
View full article
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.2 Irina_Costachescu_0-1765791524153.png   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.2 with support for: AMCU AP RAS S32K3 Family S32G Family S32R41 Family S32K1 Family S32ZE Family S32R45 Family S32M2 Family       Major Features for S32 Design Studio 3.6.2 Installer S32 Design Studio 3.6.2 is delivered with all public NPI's in a single 3GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.2 using Extension and Updates. Irina_Costachescu_0-1765808449510.png     Platform IDE and UI   Enhanced debugging efficiency by at least 20%. It applies to the entire debug session initialization pipeline and was measured from the moment Debug is pressed until the main() is reached. Live view mechanism was introduced in Memory Spaces and Global Variables views when target is running in non-stop mode. Users can observe real-time changes to memory addresses and variables, improving visibility into the runtime behavior. A configurable refresh rate allows tunning the update frequency based on performance needs. animation-ezgif.com-optimize.gif A new entry named assigned core was added in the Task List (FreeRTOS) view, it targets SMP cases. freertos_new.png Expressions with global scope can now be added straight from the Global Variables panel, without needing to switch to a separate view. new_var_global_var.png Added option to export registers description during data export from the Watch Registers view.  export_regs.png Find & Paste functions were enabled in Memory Management Unit (MMU) view. Added support for Enable auto build in S32 Debugger configuration. Enabled support for Additional Images in S32 Debugger configuration, for cases when additional source objects are loaded in the Flash memory. Enabled Advanced Settings to set the CCS IP and Port for S32 Debugger Flash Programmer debug configurations.   3 rd Party Solutions  Update of 3rd Party Debug support: Segger J-Link v8.28 PEmicro v6.0.2 TASKING v9.21.333   Major Features for NPIs S32K3 Family Merged  S32K389 into S32K3xx development pack to be available for all customers with S32DS 3.6.2 installer file. Enabled Wind River Diab 7.0.6 and IAR 8.50.10 compilers for S32K389. Enabled PEmicro v6.0.2 and IAR 8.50.10 debuggers for S32K389. Extended IAR and Segger debugging support for S32K36x, S32K37x, S32K39x, S32K341, S32K342 and S32K322 derivatives. Enhanced S32Flash programmer over JTAG to detect the presence of the HSE FW and adapt the flash operations considering HSE FW reserved flash addresses. gdb.jpg   This release is available for download on: S32 Design Studio 3.6.2 can be found on:  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6  Automotive Software Package Manager   Target Audience: S32 Design Studio 3.6.2 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.2, available on nxp.com, in Flexera catalogue S32 Design Studio for S32 Platform v.3.6, and in Automotive Software Package Manager. If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.2 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds Irina_Costachescu_2-1765793361328.png  
View full article
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.3 Irina_Costachescu_0-1765785502644.png   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.3 with support for: AMCU AP RAS S32K3 Family S32G Family S32R41 Family S32K1 Family S32ZE Family S32R45 Family S32M2 Family       Major Features for S32 Design Studio 3.6.3 Installer S32 Design Studio 3.6.3 is delivered with all public NPI's in a single 3GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.3 using Extension and Updates.   Irina_Costachescu_0-1765875178472.png   Added optional driver installation where user can customize the debugging functionalities. add drivers.jpg   Platform IDE and UI The latest release of Platform IDE introduces several enhancements and a wide range of bug fixes to improve stability and usability: S32 Config Tools can now generate Real Time Drivers code directly from the main S32 Design Studio perspective. A new context menu option, "Update Code and Build Project", has been added next to "Build Project" in the main S32DS perspective. When selected, this option automatically launches S32CT, triggers RTD code generation, and prepares the project for building—all without requiring the user to switch views. This enhancement significantly improves usability and streamlines the workflow between S32CT and RTD inside S32DS. animation4.gif In headless mode, the SDK_PATH environment variable is automatically set, with clear error reporting if any issues occur. As a result, projects with an attached SDK (such as RTD projects) that build successfully in S32 Design Studio IDE will also build from the command line without requiring manual configuration of SDK_PATH. The S32 Debugger configuration now offers an improved user experience by automatically selecting the appropriate launch configuration based on the currently selected project, rather than defaulting to the previously used one. This enhancement reduces the configuration time and the overall debugging process for users. selection.png Based on internal customer feedback, all SoC families are now kept collapsed by default in the New Project Wizard. Users can expand only the desired SoC family, resulting in a cleaner interface and more efficient use of space. npw.png Debugger performance has been improved when stepping over with registers expanded in the Watch Registers view. Previously, background operations in this view could create the impression that the debugger was stuck. This problem has now been resolved, resulting in a smoother debugging experience.   Major Features for NPIs S32K3 Family Added S32K356 phantom with supported toolchains in the S32K3xx development package. Enabled debug functionalities for S32K356 with Lauterbach and S32Debugger(blind). Enabled semihosting functionality on Lauterbach for multicore debug scenarios. k3363.jpg S32R45 Family New version of Radar Extension Package 1.6.1 with new LAX Compiler b432 built with MSVC 2022.   This release is available for download on: S32 Design Studio 3.6.3 can be found on:  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6  Automotive Software Package Manager   Target Audience: S32 Design Studio 3.6.3 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.3, available on nxp.com , in Flexera catalogue S32 Design Studio for S32 Platform v.3.6, and in Automotive Software Package Manager. If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.3 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds Irina_Costachescu_0-1765787998205.png  
View full article
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.4 Irina_Costachescu_0-1765785502644.png   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.4 with support for: AMCU AP RAS S32K3 Family S32G Family S32R41 Family S32K1 Family S32ZE Family S32R45 Family S32M2 Family S32N Family S32R47 Family     SAF8xxx Family   Major Features for S32 Design Studio 3.6.4 Installer S32 Design Studio 3.6.4 is delivered with all public NPI's in a single 2.49GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.4 using Extension and Updates. Irina_Costachescu_1-1765783657883.png S32DS NXP compiler (GCC) delivery: Starting with S32DS 3.6.4, only GCC 11.4 will be delivered as part of the installer. The older versions of NXP compiler are still available on the web update site https://www.nxp.com/lgfiles/updates/Eclipse/S32DS_3.6 and can be added via S32DS Extensions and Updates. S32DS Modular installer: S32DS 3.6.4 comes with a new custom installation type for both new and upgrade installations allowing users to customize their installation. This change provides greater flexibility and enables a faster, lighter installation tailored to user needs. installer.pngNote: As part of the new modular setup, components are no longer bundled, and they will not be installed by other packages anymore (e.g. installing a Development package will not update S32Debugger as well), users will have to explicitly select components to be installed/updated. For example, on S32K3xx development package, users must also select the new S32 Design Studio Debugger Core to get the latest debugger updates. ext&updates.png S32DS portable installation: S32DS 3.6.4 new installations can be moved in different locations other than the original installation directory and still run without having to change any properties inside S32DS. If moving to different machines check S32DS_Installation_Guide Chapter 4.4, to install any missing drivers. S32 Flash Tool GUI has been removed from the S32 Design Studio installation: Command-line tools are still included in S32DS. Users who need the GUI can install the standalone Flash Tool application from its own separate catalog S32 Flash Tool for S32 Platform. S32DS Docker images: In the S32DS 3.6.4 Flexera product page you will see 2 Docker files, for Windows and Linux, which are samples for how to setup S32DS inside a Docker image. For Linux we provide examples with or without GUI, for Windows only command line interface is available. Docker files use the S32DS installer directly to build the image, no existing installation is needed. Check out S32DS_Installation_Guide Chapters 6 and 7 for additional details on how to setup and use this.   Platform IDE and UI The latest release of Platform IDE introduces several enhancements and a wide range of bug fixes to improve stability and usability: The New Project Wizard now displays a visual decorator next to each NPI to show whether the selected GCC version is installed. npw (1).png S32 Design Studio now detects if a project references a missing GCC version or S32 Debugger. If so, an error appears in the Problems view with a Quick Fix option. Clicking it will automatically install the missing tool with minimal user input. animation (2).gif The Memory Spaces view now also displays the address where the monitor is set, even when monitoring is disabled. Users can now connect to an already running GTA instance instead of launching a new one. This can be configured in S32 Debugger configuration by unchecking the Launch Server option.   Major Features for NPIs S32K3 Family Enabled support for S32K324 on VDK R2.0.0 and S32K388 on VDK R6.0.0. Enabled full S32Debugger support for S32K356 and S32K36x derivatives. Extended real time printf with ITM functionality on S32K31x, S32K322 and S32K341/2 using Lauterbach. Integrated PEmicro v6.0.8 with debug support for S32K356 derivative. Integrated Segger v8.58 with debug support for S32K389 derivative. Enabled GCC 11.4 compiler in NPW and in example projects. s32k3.jpg S32K1 Family Enabled new devices in NPW: S32K116V, S32K118V and S32K144N. Enabled GCC 11.4 compiler in NPW and in example projects. Enabled Segger v8.58 with debug support for S32K142W and S32K144W derivatives. s32k1.jpg S32M2, S32G2/G3, S32Z2/E2, S32R41, S32R45, S32R47, S32N5 and SAF8xxx Families S32R47, S32N5 and S32SAF8xxx development packages are now public and delivered inside S32DS installer. Radar extensions and Add-on packages are also public and can be installed/updated using Extensions and Updates. Enabled GCC 11.4 in NPW and in example projects. Various bug fixes and improvements for arm cores and accelerators.   This release is available for download on: S32 Design Studio 3.6.4 can be found on  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6 Automotive Software Package Manager   Target Audience: S32 Design Studio 3.6.4 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.4, available on nxp.com , in Flexera catalogue S32 Design Studio for S32 Platform v.3.6, and in Automotive Software Package Manager. If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.4 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds   Irina_Costachescu_0-1765784725844.png
View full article
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.5 Irina_Costachescu_0-1765531594525.png   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.5 with support for: AMCU AP RAS APN S32K3 Family S32G Family S32R41 Family S32J Family S32K1 Family S32ZE Family S32R45 Family   S32M2 Family S32N Family S32R47 Family       SAF8xxx Family     Major Features for S32 Design Studio 3.6.5 Installer S32 Design Studio 3.6.5 is delivered with all public NPI's in a single 2.63GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.5 using Extension and Updates. Irina_Costachescu_1-1765531866020.png   Installer will require admin rights only when the user chooses to install components which need elevation (Visual Studio Redistributable or debugger drivers). If a user chooses a custom installation only with S32DS IDE and its components (no drivers) the installation will finish without admin rights. Irina_Costachescu_2-1765531914107.png   Platform IDE and UI Integrated Cody, the open-source Eclipse plugin from Sourcegraph, into S32 Design Studio. This plugin is installed by default, allowing users with a valid Cody license to log in directly within S32DS and access Generative AI features. Note: Users must agree to the Sourcegraph Terms of Service before using Cody. Irina_Costachescu_2-1765456346536.gif Enabled integration with the NXP Application Code Hub, allowing users to browse available examples and import them directly from the hub page into S32 Design Studio. Note: the application examples will be published soon on the Application Code Hub URL. Irina_Costachescu_3-1765456346537.png Note: This image is taken from internal sources. The illustrated examples are currently under development and will be available soon. Extended the Quick Fix mechanism for the missing NPI and Real Time Drivers packages. Basically, an error message displays in the Problems view whenever the IDE identifies a missing package (build tool, NPI, RTD) associated with the current project. The Quick Fix automatically installs the missing package if it is available in the configured Update Sites. Note: not all scenarios are covered, there may be cases where the tool cannot determine if a package is missing. Irina_Costachescu_4-1765456345392.png A new Recent tab has been added in S32DS Extensions and Updates to display the latest installed packages, providing a clear history of user actions related to package installations. In addition, the default sorting was changed in All tab to bring greater visibility to NXP packages. Irina_Costachescu_5-1765456346540.png Added support for drag-and-drop of S32 Design Studio p2 update sites / installable packages into the S32DS Extensions & Updates window. Users can now simply drag the ZIP file into the window, and the package will be automatically inserted and selected, requiring only a click on Next to complete the installation. Irina_Costachescu_6-1765456348052.gif Significant improvements to Secure Debugging:  Added a dedicated Debug Card view that allows users to generate debug card binaries based on custom input. Implemented Challenge & Response functionality for Linux environment.  Enabled Secure Registry Key view for managing secure registry keys on Linux.  UI is aligned to the secure debugging functionality latest changes introduced by HSE2. Irina_Costachescu_0-1765808827917.png Extended the S32 Debugger OS awareness support with FreeRTOS. OS threads are now visible in S32 Design Studio and user will be able to individually debug them. Extended the command line support to display OS threads and objects. Irina_Costachescu_8-1765456347125.png Enable debug in low power mode with S32 Debugger for S32K3xx devices:  The debug session will recover after core exits low power or standby mode, allowing the user to continue application debugging. Debugging from the first instruction after low power exit is now possible by using this configuration command when starting the debug session: monitor template config :ccs:S32K3XX:SoC#0 6 1 Expanded the S32Trace debug-info parser to fully support DWARF-5, adding compatibility with projects using GCC 11.4 and newer.   Major Features for NPIs S32N Family S32Flash Programmer improvements for erase and verify write operations on S32N5. S32G2/G3, S32J100, and SAF8xxx Families S32J100 development package is now public and delivered inside S32DS installer. Enabled debugging support for S32G2 devices on VDK R10. S32Flash Programmer enhancements for erase and verify write operations. Various bug fixes and improvements for arm cores and accelerators. Irina_Costachescu_3-1765532135684.png   This release is available for download on: S32 Design Studio 3.6.5 can be found on  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6   Target Audience: S32 Design Studio 3.6.5 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.5, available on nxp.com and in Flexera catalogue S32 Design Studio for S32 Platform v.3.6. If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.5 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, drag the ZIP file into the window, and the package will be automatically inserted and selected, requiring only a click on Next to complete the installation, or click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds   Irina_Costachescu_10-1765457452129.png
View full article
      artiom_0-1732696956675.png ​S32 Design Studio Version 3.6.0   1. IDE New Features The S32Design Studio 3.6 is delivered with all public NPI's in a single 2.5GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32Design Studio 3.6.0 using Extension and Updates mechanism as depicted below. artiom_0-1732710178116.png New S32Design Studio Installer is faster and lighter (compared to S32Design Studio 3.5) Official support for Window 11 OS and Ubuntu 20.04. Windows 10 OS is tested for compatibility. New Eclipse 2023.12, CDT11.4 and Java 17  Development, Add-Ons and Extension Packages delivered with older S32Design Studio 3.5.x are compatible with version 3.6.0 RTD and Runtime Software releases made on top of S32Design Studio 3.5.x are backward compatible with S32Design Studio 3.6.0 using smart compatibility mechanism New GDB 15.1 for ARM cores New Python 3.10 for ARM cores Improved Extension and Updates mechanism to warn the user when S32Design Studio processes are in use and the installation can not be completed Improved Watch Registers view to expand all registers and export bitfields Improved Dashboard view to include more options for quick access alexcuhureanu_0-1732806078155.png Improvements on UI, update of C/C++ and Debug perspective artiom_0-1732711988589.png Improve CLI support to facilitate New Project Creation from command line. For more details please see HOWTO_S32_Design_Studio_Command_Line_Interface.pdf Enable CCS remote for all NPIs 2. S32Debugger New Features New S32Debug Probe OS version 1.1.0 update for resolving WiFi disconnect issue when the probe is connected via USB. Follow the HOWTO_Update_the_S32Debug_Probe_OS.pdf to update the probe firmware to the new version: artiom_0-1732812339611.png Expose current exception level in Debug View for ArmV8 cores: artiom_1-1732812377926.png New GDB version GDB 15.1 integrated for Arm cores with Python3 interpreter artiom_2-1732812414314.png S32K3xx/S32M2xx/S32K14x: S32K14x flash programmer support Enhanced flash programmer to support also programming the Data Flash   3. S32Configuration Tools 1.8.0 New Features Alignment to S32Design Studio: Java 17, Windows 11, Eclipse 2023.12 3.1 DDR features: Intermediate progress report of memory test execution Import log options Access to LPDDR5 DRAM beyond 32bit address space Quickboot, retention support and multicore test execution for LPDDR5  artiom_0-1732813721964.png   3.2 Scenario Tools features: UI/UX updates for all Boot tools (IVT, DCD, QSPI), allowing quicker access to main tools functions via the built-in toolbar artiom_2-1732813845402.png   3.2 GTM Tool features: External Clock for CMU Extended configuration modes and new predefined use-cases for TIM Dynamic channel management for TOM, ATOM, TIM and TBU modules Export HTML report artiom_1-1732813783630.png   4. Major features for S32Trace 3.6.0 Added support for all S32G3 Family parts and application cores artiom_0-1732793835129.png Added support for Cortex-M7 cores for all S32G2 Family parts artiom_1-1732793884019.png   5. Major features for MCU - S32K1, S32K3, S32K37/39 and S32M2 Families: S32Debugger support of S32K14x for FLASH and RAM configuration artiom_4-1732814019704.jpeg   S32Debugger support of S32K3xx for FLASH and RAM configuration with multicore support artiom_5-1732814038995.jpeg   Now, S32K37/39 Family is part of S32K3 Family distribution S32Debugger support of S32M2xx for FLASH and RAM configuration artiom_6-1732814060171.jpeg   Update of 3rd Party Debuggers support: Segger J-Link 8.10c PEmicro v5.9.2 TASKING v9.21.273   6. This release is available: S32Design Studio 3.6.0 can be found on nxp.com and on Flexera   7. The installation instructions: 1. Navigate to S32Design Studio page on nxp.com and click Download artiom_0-1732722621582.png 2. Login(if not) and Accept License Agreement. artiom_0-1732800587705.png 3. Navigate to License Key tab and copy Activation Code artiom_1-1732800713959.png 4. Launch S32Design Studio installer and when asked for Activation code, please provide the one from above step. artiom_7-1732814087873.png   ​   ​ ` artiom_12-1732609695510.jpeg
View full article
This document shows the step-by-step process for creating a simple blinking LED application for the S32Z27x family using the S32 RTD non-AUTOSAR drivers. This example used for the S32Z27x-DC EVB, which is connected via an Ethernet connection through the S32 Debugger.   Preparation  Setup the software tools  Install S32 Design Studio for S32 Platform   Install the S32Z2/E2 development package and the S32ZE RTD AUTOSAR R21-11 Version 0.9.0 P01 Both of these are required for the S32 Configuration Tools.  DanielBarbu_0-1729770950096.png   Launch S32 Design Studio for S32 Platform  Procedure    New S32DS Project  DanielBarbu_1-1729770996860.png   OR   DanielBarbu_2-1729771028823.png                  Provide a name for the project, for example 'Blinking_LED_RTD_No_AUTOSAR'. The name must be entered with no space characters.     Expand the Family ‘S32Z27x’, and Select ‘S32Z270 (Boot core_ R52_0_0)’  DanielBarbu_3-1729771054158.png     Click '…' button next to SDKs  DanielBarbu_5-1729771121264.png   Check box next to PlatformSDK_S32ZE_2022_10_S32Z270_R52_0_0_LS (or whichever latest SDK for the S32M27x is installed). Click OK   DanielBarbu_6-1729771153344.png   Click "Finish" and wait for the project generation wizard to complete. Then, expand the project within the "Project Explorer" view to show its contents.  DanielBarbu_0-1729773632866.png     To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way is to double-click on the .MEX file.  DanielBarbu_1-1729773653875.png   By default, the Pins Tool will be presented. The S32Z27x DC EVB has user D12 LED connected to the PA_01 pin on the S32Z270 device.    To configure this pin, select the "Peripheral Signals" tab to the left of the Pins Tool perspective layout. Locate and open the SIUL2_0 from the peripheral signals tab, and from the drop-down menu, select the "gpio,1 PA_01" option as shown in the following image.  We are using Siul2_0 for GPIO usage, so we are routing the gpio,1 –> PA_01 GPIO signal to this pin.  DanielBarbu_2-1729773702826.png      The Direction required! menu will appear. Select Output then OK.  DanielBarbu_3-1729773749749.png   In Routing Details view, notice a new line has been added and highlighted in yellow.  DanielBarbu_4-1729773779967.png   Add ‘LED’ to the Label and Identifier columns for the Siul2_0, gpio-1 pin.  DanielBarbu_5-1729773841359.png   Code Preview  DanielBarbu_6-1729774044873.png DanielBarbu_7-1729774152124.png   Go to Peripherals tool and add Gpio_Dio to enable LED blinking, it adjacent to the user LED on S32Z270 EVB.    Click on the Peripherals Tool icon in the Eclipse Perspective navigation bar.  DanielBarbu_8-1729774246191.png In the Components view, click on the ‘Add a new configuration component…' button in the Drivers category. This will bring up a list of all configuration components.  DanielBarbu_10-1729774311323.png   Locate and select the 'Siul2_Dio' component from the list and click OK. Don't worry about the warning message – it's only indicating that the driver isn't already part of the current project. The associated driver package will be added automatically.   Note: it may be necessary to change the selection at the top from 'Present in the toolchain project' to 'All'.  The Siul2_Dio driver provides services for reading and writing to/from DIO Channels.   DanielBarbu_11-1729774351169.png   Now, form the toolbar selection menu at the top, select and double click on the symbol as shown as below:   DanielBarbu_12-1729774374958.png   Then, from the global settings window, for ComponentGenerationMethod from the drop down menu select “FunctionalGroups” from the drop down menu as shown below:   DanielBarbu_13-1729774390991.png   The Siul2_Dio driver requires no further configuration. Click Save to store all changes to the .MEX file.     DanielBarbu_14-1729774409193.png   Now. click ‘Update Code’ from the menu bar.  Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar.   DanielBarbu_15-1729774461735.png   To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective.  DanielBarbu_16-1729774493201.png   If the 'src' folder is not already open in the project window, click the '>' symbol next to it to show its contents. Then, double-click the 'main.c' file to open it. This is where you will add the application code.  DanielBarbu_17-1729774508583.png   To control the pin, it needs to be 'initialized' using the configuration information generated from the S32 Configuration tools. To do this, add the following line to the 'main' function after the comment 'Write your code here':         /* Initialize all pins using the Port driver */       Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);      DanielBarbu_18-1729774561333.png   Now, add logic to turn the LED on and off with some delays in between to make it visible blinking. Make sure the delays are long enough to be perceptible.     Add line to initialize variable uint8 i = 0;  Add line to declare variable level: volatile uint8 level;  Change the code within the provided for loop, and add the following lines:     /*logic for blinking LED 10 times*/     for (; i<10; i++)       {           Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 1U);         level = Siul2_Dio_Ip_ReadPin(LED_PORT, LED_PIN);           TestDelay(480000);           Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 0U);         level = Siul2_Dio_Ip_ReadPin(LED_PORT, LED_PIN);           TestDelay(480000);       }   DanielBarbu_19-1729774770933.png   Before the 'main' function, add a delay function as follows:  void TestDelay (uint32 delay);   void TestDelay (uint32 delay)   {     static volatile uint32 DelayTimer = 0;    while (DelayTimer<delay)      {          DelayTimer++;      }      DelayTimer=0;   }   DanielBarbu_20-1729775004705.png   Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application:    Remove   #include "Mcal.h"  Add   #include "Siul2_Port_Ip.h"   #include "Siul2_Dio_Ip.h"       DanielBarbu_21-1729775154749.png   Build 'Blinking_LED_RTD_No_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'.  DanielBarbu_22-1729775270319.png   After the build completes, check that there are no errors.     DanielBarbu_23-1729775288288.png   Open Debug Configurations and select 'Blinking_LED_RTD_No_AUTOSAR_Debug_RAM'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist.     DanielBarbu_24-1729775320447.png   Now, you need to Select the Interface (Ethernet or USB) by which the S32 Debug Probe is connected.   DanielBarbu_26-1729775403585.png   If connected via USB and this option is selected for interface, then the COM port will be detected automatically (in the rare event where 2 or more S32 Debug Probes are connected via USB to the host PC, then it may be necessary to select which COM port is correct for the probe which is connected to the EVB)  DanielBarbu_27-1729775489556.png   If connected via Ethernet, enter the IP address of the probe. See the S32 Debug Probe User Manual for ways to determine the IP address.  DanielBarbu_28-1729775575202.png   Click apply and Debug  To see the LED blink, click ‘Resume'.   DanielBarbu_29-1729775613296.png   This code as it is will blink the LED 10 times, you can make changes in for loop condition to blink it infinitely.     
View full article
This document details the steps to program external EEPROM with the 32 reset configuration bits in support of the 'Boot from serial RCON' method detailed in the device reference manual. The Python scripts used for this task are designed and tested to work on the EVBs, where EEPROM hardware is connected via I2C.(Serial EEPROM is not implemented on all boards).   The RCON can be set by the following:    Fuses (internal to the device)  Parallel (GPIO pins/DIP Switches on EVB)  Serial (EEPROM connected via I2C)    The Serial option can be programmed using a debug probe connected via JTAG. This enables the RCON to be controlled remotely, assuming the debug probe is setup to allow remote connections.  The images shown throughout this document are of the S32G274A device implementation and are provided for illustration purposes.               Preparation    Install S32 Design Studio IDE  Use the S32DS Extensions and Updates menu to install the Development Package for the device subject to debugging. This is important as the Development Packages add the S32 Debugger support which provides access to the EEPROM programming capabilities via I2C of the S32 Debug Probe.  Connect the S32 Debug Probe to the EVB and the host PC containing S32 Design Studio installation.  Set BOOTMOD pins to boot from RCON  DanielBarbu_0-1727701984224.png   Set BOOT_CFG[8]=1 on the EVB, for serial RCON mode DanielBarbu_1-1727702012683.png   Procedure    Depending on the way the device used and how the {device name}_i2c_RCON.py is edited, user must use the old procedure on the new one. Both detailed below. To choose between the Old procedure and the new procedure, you must check in the {device_name}_i2c_RCON.py if variables like “INTERACTIVE_MODE” and “RCON_DATA” exist. The {device_name}_i2c_RCON.py can be found in: {INSTALL_DIR}…S32DS/tools/S32Debugger/Debugger/scripts/{device_name}/ {device_name_part_name}_i2c_RCON.py If the variables exist, please use the old procedure. If the variables were removed, please use the new procedure. I.  Old procedure ( If “INTERACTIVE_MODE” variable still exists)   Open cmd window to the S32 Debugger folder where the device-specific scripts are located. ../S32Debugger/Debugger/Scripts/{device_name/part_number} Set Python path so correct version is used (if not already set in env vars)   set PYTHONPATH=C:\NXP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\N XP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages   Edit the python script to adjust the value to be programmed to RCON, {device_name}_i2c_RCON.py. Note: The listed examples show only the minimum values required to configure each of the external memory types. Additional settings may be required for your specific application.   Adjust RCON_DATA for the configuration you wish to program. Do not adjust RCON_ADDR. Adjust S32DBG_IP for the IP address of your S32 Debug Probe. Adjust INTERACTIVE_MODE i. Set True, if desired to be prompted in the command window to enter RCON_DATA      ii. Set False, if desried to have script automatically enter RCON_DATA, based on the value set     within the file. Adjust _SOC_NAME as appropriate for the specific device you are using. The valid options are defined in {device_name}_context.py Enter the command to start GDB, passing in the RCON Python script:   Windows OS: ../ S32DS\tools\gdb-arm\arm32-eabi\bin/arm-none-eabi-gdb-py.exe -x {device_name}_i2c_RCON.py OR ../ S32DS\tools\gdb-arm\arm64-eabi\bin/arm-none-eabi-gdb-py.exe -x {device_name}_i2c_RCON.py Linux OS: arm-none-eabi-gdb-py -x {device_name}_i2c_RCON.py DanielBarbu_2-1727702132471.png   If everything worked properly, then the value you programmed will be displated to the screen. DanielBarbu_3-1727702173392.png   To exit GDB, enter ‘quit’. II.  New Procedure ( If “INTERACTIVE_MODE” variable was deleted)   Set Python path so correct version is used (if not already set in env vars)  set PYTHONPATH=C:\NXP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\N XP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages  Start GDB Server. (…\S32Debugger\Debugger\Server\gta\gta.exe) DanielBarbu_4-1727702233412.png   Start Command Prompt and enter the command to start GDB with python: Example:   C:\NXP\S32DS.3.5_230912_devpck\S32DS\tools\gdb-arm\arm32eabi\bin\arm-none-eabi-gdb-py.exe Linux OS: arm-none-eabi-gdb-py   DanielBarbu_5-1727702254435.png   In s32rcon.py ( C:\NXP\S32DS.3.5_230912_devpck\S32DS\tools\S32Debugger\Deb ugger\scripts\gdb_extensions\rcon\s32rcon.py😞 Edit connection parameters (Probe IP, GDB server port, JTAG speed, etc.) Edit _RCON_SCRIPT parameter with absolute path to the desired I2C RCON script for the desired board: Example: _RCON_SCRIPT = " C:/NXP/S32DS.3.5_230912_devpck/S32DS/tools/S32Debugger/Deb ugger/scripts/s32g2xx/ s32g274a_i2c_RCON.py"      c. Source s32rcon.py in GDB. Example: source C:/NXP/S32DS.3.5_230912_devpck/S32DS/tools/S32Debugger/Deb ugger/scripts/gdb_extensions/rcon/s32rcon.py     d. Run command py rcon() in GDB. OBS:  Steps a, b can be done after c directly from GDB, using GDB py commands: Examples:  py _GDB_SERVER_PORT=45000  py _RCON_SCRIPT="C:/NXP/S32DS.3.5_230912_devpck/S32DS/tools/S32Debugger/Debu gger/scripts/s32g2xx/ s32g274a_i2c_RCON.py" DanielBarbu_6-1727702279041.png   User can now use the available commands, like rcon_help, rcon_read, rcon_write to interact with the EEPROM.   User can write [command] -h for more information and mandatory parameters of the command. DanielBarbu_7-1727702298552.png DanielBarbu_8-1727702312607.png   User can write ‘quit’ to exit the S32 RCON services.
View full article
NXP devices can be secured either with password or challenge and response authentication scheme. The S32 Debugger included within the S32 Design Studio for S32 Platform IDE with the S32 Debug Probe provides the ability to debug a secured device. This document provides only the necessary commands specific to launching a debug session on secured NXP devices.. Once the device is unsecured, it will remain so until a power-on-reset or destructive reset occurs. The images shown throughout this document are of the S32R45 device implementation and are provided for illustration purposes. Preparation Setup the software tools Install S32 Design Studio for S32 Platform  Install the Development Package for the device you are debugging. This package is important as it contains the S32 Debugger support component  DanielBarbu_1-1727696287876.png          Setup the hardware Confirm the setup of the evaluation board.  i     Connect the power supply cable Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Manual for installation instructions. i      Connect the S32 Debug Probe to the evaluation board via JTAG cable.  ii     Connect the S32 Debug Probe to the host PC via USB cable OR via Ethernet cable (via LAN or directly connected and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Open existing project or create a new project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard. DanielBarbu_2-1727696416830.png DanielBarbu_3-1727696452564.png Procedure Before starting a secure debug session, first confirm that the device is indeed secure. Once one core is unlocked, all cores are unlocked and will remain so until a power-on-reset or destructive reset occurs. After confirming the device is secured, then select the procedure which applies to the lifecycle of the SoC to be debugged.    Check the state of the SoC   Open a command window from the installation directory containing the GTA server:              {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\ Execute the following command:              gta.exe -t s32dbg   This will invoke a utility that launces a new GTA server instance and then communicates with the target via the S32 Debug Probe and will request a set of properties of the SoC. These properties are available to be read regardless of security state. The GTA server will close once the information is returned. DanielBarbu_4-1727696544188.png   As is shown above, the Debug state is ‘Locked’. This means it is secured and the secure debug steps outlined within this document must be used. There is no way to determine the security enabled on the SoC, so this should be known by the user in order to select the correct authentication scheme. Proceed from here using the method (Password or Challenge & Response) which applies for your SoC security configuration.    Password   From S32DS, open the Debug Configurations menu, select the configuration for the project you wish to debug, select the ‘Debugger’ tab and scroll down until the ‘Secure debugging’ section is visible. DanielBarbu_5-1727696605436.png   Check the box for ‘Enable secure debugging’ and then select the Debugging type ‘Password’. DanielBarbu_6-1727696620555.png   Click Debug. When the debug session initialization reaches the stage where the password must be entered to unsecure the SoC, the following menu will appear. DanielBarbu_7-1727696637751.png   Enter the password. This is a 16-byte value entered as a hexadecimal without the leading ‘0x’. If you choose to check the box for ‘Store keyword in secure storage’, the value entered will be stored within the Eclipse secure storage and will remain available for the duration of the current S32DS instance. This saves the user from having to enter the password again, should the security state of the SoC becomes once again secured.   Now the debug session initialization will complete and debug activities may be executed as with any SoC which is not secured. After terminating the debug session, the GTA utility can be used again to see the new state of the SoC. DanielBarbu_8-1727696692362.png   This utility cannot be executed while the debug session is running. It launches a new instance of the GTA server, which would be blocked by the already running debug session.   Challenge & Response   For the Challenge & Response security scheme, the included Secure Keys Registry must be used. From the S32DS menu bar, select Window -> Show View -> Other -> ‘Secure Keys Registry’. DanielBarbu_9-1727696723307.png   The Secure Keys Registry will now appear in the current perspective. DanielBarbu_10-1727696744282.png   Since there is no current key stored in the Secure Keys local storage, a new key must be registered. Click on ‘Register Key’. This will bring up the Secure Keys Registry command dialog. DanielBarbu_11-1727696766695.png   Now enter the ADKP value (Application Debug Key/Password) which is correct for the SoC to be debugged.                  The Secure Keys Registry utility uses the same functionality as the command-line GTA utility shown earlier to check the state of the SoC. This will read the UID from the Soc. Click Connect to load the UID (Device Unique ID) from the SoC. The UID is associated with the ADKP when it is registered within the Secure Keys local storage for easier access in the future. DanielBarbu_12-1727696796841.png   Click OK to complete the registration of the new key.   Now the key is registered, the debug session can be setup and started. DanielBarbu_13-1727696825196.png   Open the Debug Configurations menu, select the configuration for the project you wish to debug, select the ‘Debugger’ tab and scroll down until the ‘Secure debugging’ section is visible. DanielBarbu_14-1727696870055.png   Check the box for ‘Enable secure debugging’ and then select the Debugging type ‘Challenge & Response’. DanielBarbu_15-1727696882545.png   Click Debug. Now the debug session initialization will complete and debug activities may be executed as with any SoC which is not secured. During debug session initialization, the key that was registered will be used to unsecure the SoC. After terminating the debug session, the GTA utility used earlier can be used again to see the new state of the SoC. DanielBarbu_16-1727696912101.png   This utility cannot be executed while the debug session is running. It launches a new instance of the GTA server, which would be blocked by the already running debug session.   Smart Card Authentication   When using a smart card, the user will need to authenticate with it. IDE has a mechanism to provide the user password for this purpose.  DanielBarbu_0-1729752686581.png   This mechanism is available from any S32 Debug Configuration, as well as Secure Key Registry views, and will be triggered anytime the IDE will call a command that requires authentication on the connected smart card (e.g.: registering a key, fetching the registered keys and trying to perform secure debug with challenge & response.)   Troubleshooting There are some messages displayed when things go wrong that can help to identify the cause of the issue. Due to the sensitive nature of the Secure Debug, the error indications detailed below are inherently general and are provided as a guide for interpreting them to determine the likely cause.   Debug session started when SoC is still secured There is an error message reported in the S32 Debugger Console to indicate the SoC is still secure. To see this message the GDB Server log must be enabled in Debug Configurations -> Debugger tab, GDB Server section: DanielBarbu_17-1727696931743.png   When this error is incurred, first indication is popup error message for Error code 102: DanielBarbu_18-1727696949456.png              Next, the following text will be displayed in the S32 Debugger console window: DanielBarbu_19-1727697026287.png   If needed, select this view from the menu: DanielBarbu_20-1727697090469.png   In addition, if GDB Traces log is enabled, the following error message can be found in the gdb traces console view: DanielBarbu_21-1727697109801.png   Enable the GDB Traces log in Window->Preferences, then search on GDB: DanielBarbu_22-1727697195301.png   To select the view from console: DanielBarbu_23-1727697341374.png                 Incorrect Challenge/Response Or Password If the SoC is setup for Challenge & Response security scheme, but Password security scheme is selected in Debug Configuration, or Challenge & Response is correctly selected but the wrong ADKP value is provided, below are the expected error messages. The result is same if the SoC is setup for Password and either Challenge & Response or wrong password is used.   First error message is Error code 601: DanielBarbu_24-1727697423509.png   Next, the gdb traces console displays the following error: DanielBarbu_25-1727697444445.png   There is no error displayed in the S32 Debugger console. Make sure you have selected the appropriate authentication scheme and provided the correct value for the security asset corresponding to that authentication scheme. E.g. For password - provide the correct password.   For challenge & response, have the correct debug key registered on the smart card.   Note: you may be required to power cycle the board before attempting to debug again after failing to authenticate properly.   Configuration Settings     SDAF (Secure Debug Authorization Framework) – the framework for which the Secure Keys Registry view serves as a graphical interface, is configurable in various aspects and the UI can be used to update the configuration. From the Secure Key Registry interface, click on Settings:   DanielBarbu_1-1729752824459.png The configuration parameters that can be updated with this view are the following: Working mode: This configuration parameter is used for selecting the working mode regarding the smart card connection. There are two possible values for this:   Managed: volkano.dll (SDAF component) iterates through all the PC/SC readers locally connected to the PC where volkano is running and identifies if a smart card with the volkano applet installed is present. If such a smart card is identified, volkano will connect and interact with it accordingly.  DanielBarbu_4-1729753183423.png     Client: volkano will try to connect to another instance of volkano running in server mode (be it remotely or on the same PC where S32DS is running). Note: Due to the fact that all the commands sent by volkano to the smart card will go through the network via TCP, some latency is expected.     DanielBarbu_3-1729753165665.png   Host: Specifies the hostname/IP address of the PC on which a volkano instance is running in server mode.   Port: Determines the port of the remote volkano instance (running in server mode) that the client will try to connect to. Logging_Verbosity: This config parameter controls the level of detail in the program’s log output. The available verbosity levels are: ERROR: Provides messages that indicate exceptions that have occurred during the execution and data transmission errors. This is the default value of the config parameter.       INFO: Provides informational messages that contains details about the normal execution flow.   DEBUG: Provides detailed debugging information.   
View full article