NXP Model-Based Design Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Tools Knowledge Base

Discussions

Sort by:
The content of this article is identical to the AN13902: 3-Phase Sensorless PMSM Motor Control Kit with S32K344 using MBDT Blocks
View full article
This page summarizes all Model-Based Design Toolbox videos related to HCP Product Family. Deploying Radar Applications to NXP´s S32R41 Processor Using Simulink® Link to the recording here This webinar shows how to use Radar Toolbox, Simulink ®  , and Embedded Coder ®  to generate C code for radar signal processing algorithms for range and speed estimation and deploy them to NXP ® ´s S32R41 high-performance processor for high-resolution radar. Based on MathWorks´ radar example models, we use Embedded Coder to generate optimized C code and run it in Processor-in-the-Loop (PIL) mode on the S32R41 processor. The code generation workflow will feature the use of NXP´s Model-Based Design Toolbox (MBDT), which provides an integrated development environment and toolchain for configuring and generating all the necessary software to execute complex applications on NXP MCUs and processors.
View full article
    Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.3.0 EAR   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.3.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K311, S32K312, S32K314, S32K322, S32K324, S32K341, S32K342, S32K344, S32K358 and S32K396 MCUs and part of their peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, UART, GPT). To enable BMS applications development, we have added support for MC33775A and MC33772C battery cell controllers (& MC33665PHY). In this release, we have also updated S32 Configuration Tools, RTD, AMMCLib, and MATLAB support for the latest versions. The product comes with over 115 examples, covering everything that is supported, including demos for battery cell controllers (BCC) and motor control.   Target audience: This product is part of the Automotive SW – S32K3 Standard Software Package.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=13957417   Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K311 S32K312 S32K314 S32K322 S32K324 S32K341 S32K342 S32K344 S32K358 S32K396   Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI UART GPT DIO   Support for MC33775A and MC33772C battery cell controllers & MC33665PHY The toolbox provides support for the MC33775A, MC33772C, and MC33665. The MC33775A and MC33772C are lithium-ion battery cell controller ICs designed for automotive applications which perform ADC conversions of the differential cell voltages and battery temperatures, while the MC33665 is a transceiver physical layer transformer driver, designed to interface the microcontroller with the battery cell controllers through a high-speed isolated communication network. The ready-to-run examples provided with the MBDT for S32K3 show how to communicate between the S32K344 and the MC33775A and MC33772C via the MC33665 transceiver. For the MC33775A, the examples show how to configure the battery cell controller to perform Primary and Secondary chains conversion, and read the cell voltages conversion results from the MC33775A, while for the MC33772C the examples show how to configure the Battery cell controller to read current. All the converted values are displayed to the user over the FreeMaster application.       Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the configuration for it once. After it is saved as a custom default project, it can be used for every model that is being developed.       Support for component restore to default settings The toolbox allows users to restore the configuration of a component (for models which use the EB Tresos configuration tool) to the settings corresponding to the Default Configuration Template the model uses. This allows reverting changes (if made) to the default values.   Support for AUTOSAR blockset (SW-C deployment) New RTD version supported  (v3.0.0 CD04) – only for S32K311, S32K358 and S32K396 New S32 Configuration Tools version supported (v1.6) Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tools or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.31: All functions in the Automotive Math and Motor Control Functions Library v1.1.31 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2021a R2021b R2022a R2022b   S32Design Studio Integration We provide a simple mechanism for the users to export the code generated from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project or for debugging purposes.     Board initialization: The Model-Based Design Toolbox for S32K3xx generates the component’s peripherals initialization function calls as configured in the Board Initialization window. The toolbox provides a default configuration including function calls for initializing the clocks, followed by pins and a custom order for the rest of the peripherals which have been configured in the project associated to the model.     Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode     Examples for every peripheral/function supported: We have added over 115 examples, including: Battery Management Systems examples Motor control applications (including eTPU example on S32K396) Communication (SPI, CAN, UART) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.3.0 is fully integrated with MATLAB® environment in terms of installation:         Target Audience This release (1.3.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt                
View full article
        Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for HCP – version 1.2.0 RFP       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for HCP version 1.2.0. This release supports automatic code generation from MATLAB/Simulink for S32G2xx, S32S2xx, and S32R41 MPUs. This new product adds support for new MATLAB versions R2022a and R2022b for running in Processor-in-the-Loop mode.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=13897177   Technical Support: NXP Model-Based Design Toolbox for HCP issues will be tracked through NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32G2xx derivatives: S32G274A Automatic C code generation from MATLAB® for NXP S32S2xx derivatives: S32S247TV Automatic C code generation from MATLAB® for NXP S32R4x derivatives: S32R41 Supported Evaluation Boards GoldBox Development Platform (S32G-VNP-RDB2 Reference Design Board) GreenBox II Development Platform X-S32R41-EVB Development Board Support for MATLAB versions: R2020a R2020b R2021a R2021b R2022a R2022b Tools update for S32R41: S32 Flash Tool v2.1 S32 Debugger v3.5 Simulation mode: We provide support for Software-in-Loop (SIL) and Processor-in-Loop (PIL) simulation mode with code execution profiling: Includes an Example library with 16 examples that cover: Software-in-Loop (SIL), Processor-in-Loop (PIL) GUI to help you setup the toolbox and the evaluation board :     For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32G2xx, S32S2xx, and S32R41  processors and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for HCP version 1.2.0 (RFP) is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.2.0 RFP) is intended for technology demonstration, evaluation purposes, and prototyping S32G2xx, S32S2xx, and S32R41 and Evaluation Boards.   Useful Resources Examples, Trainings and Support: https://community.nxp.com/community/mbdt    
View full article
  Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.2.0 RTM   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.2.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K312, S32K314, S32K322, S32K324, S32K341, S32K342, and S32K344 MCUs and part of their peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, UART, GPT). To enable BMS applications development, we have added support for MC33775A and MC33772C battery cell controllers (& MC33665PHY). In this release, we have also updated FreeMASTER, AMMCLib, and MATLAB support for the latest versions. The product comes with over 130 examples, covering everything that is supported, including demos for battery cell controllers (BCC) and motor control.   Target audience: This product is part of the Automotive SW – S32K3 Standard Software Package.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=13593437   Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K312 S32K314 S32K322 S32K324 S32K341 S32K342 S32K344     Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI UART GPT DIO   Support for MC33775A and MC33772C battery cell controllers & MC33665PHY The toolbox provides support for the MC33775A, MC33772C, and MC33665. The MC33775A and MC33772C are lithium-ion battery cell controller ICs designed for automotive applications which perform ADC conversions of the differential cell voltages and battery temperatures, while the MC33665 is a transceiver physical layer transformer driver, designed to interface the microcontroller with the battery cell controllers through a high-speed isolated communication network. The ready-to-run examples provided with the MBDT for S32K3 show how to communicate between the S32K344 and the MC33775A and MC33772C via the MC33665 transceiver. For the MC33775A, the examples show how to configure the battery cell controller to perform Primary and Secondary chains conversion, and read the cell voltages conversion results from the MC33775A, while for the MC33772C the examples show how to configure the Battery cell controller to read current. All the converted values are displayed to the user over the FreeMaster application.           Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the configuration for it once. After it is saved as a custom default project, it can be used for every model that is being developed.         Support for component restore to default settings The toolbox allows users to restore the configuration of a component (for models which use the EB Tresos configuration tool) to the settings corresponding to the Default Configuration Template the model uses. This allows reverting changes (if made) to the default values.   Support for AUTOSAR blockset (SW-C deployment) New RTD version supported  (v2.0.0) New S32Config Tools version supported (v1.5) Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.29: All functions in the Automotive Math and Motor Control Functions Library v1.1.29 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.     Support for MATLAB versions We added support for the following MATLAB versions: R2020a R2020b R2021a R2021b R2022a   S32Design Studio Integration We provide a simple mechanism to let users the opportunity to export the code generated from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project or for debugging purposes.          Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode     Examples for every peripheral/function supported: We have added over 130 examples, including: Battery Management Systems examples Motor control applications Communication (SPI, CAN, UART) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode   For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.2.0 is fully integrated with MATLAB® environment in terms of installation:         Target Audience This release (1.2.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt            
View full article
    Product Release Announcement EDGE PROCESSING   NXP Model-Based Design Toolbox for i.MX RT Crossover MCUs – version 1.3.0     The Edge Processing Tools Team at NXP Semiconductors is pleased to announce the release of the Model-Based Design Toolbox for i.MX RT 1xxx Series version 1.3.0. This release supports automatic code generation for peripherals and applications prototyping from MATLAB/Simulink for NXP’s i.MX RT 117x, 106x, 102x & 101x Series of crossover MCUs.   NXP Download Location https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   MATHWORKS Download Location https://www.mathworks.com/matlabcentral/fileexchange/81051-nxp-support-package-imxrt1xxx   Version 1.3.0 Release Content Automatic C code generation based on MCUXpresso SDK 2.11.0 drivers and MCUXpresso Configuration Tools 11.0 initializations from MATLAB®/Simulink® for: i.MX RT 1076: MIMXRT1176DVMAA,MIMXRT1176AVM8A,MIMXRT1176CVM8A i.MX RT 1075: MIMXRT1175DVMAA,MIMXRT1175AVM8A,MIMXRT1175CVM8A i.MX RT 1073: MIMXRT1173CVM8A i.MX RT 1072: MIMXRT1172DVMAA,MIMXRT1172AVM8A,MIMXRT1172CVM8A i.MX RT 1071: MIMXRT1171DVMAA,MIMXRT1171AVM8A,MIMXRT1171CVM8A i.MX RT 1061: MIMXRT1061CVJ5A,MIMXRT1061CVL5A,MIMXRT1061DVJ6A,MIMXRT1061DVL6A i.MX RT 1062: MIMXRT1062CVJ5A,MIMXRT1062CVL5A,MIMXRT1062DVJ6A,MIMXRT1062DVL6A i.MX RT 1064: MIMXRT1064CVJ5A,MIMXRT1064CVL5A,MIMXRT1064DVJ6A,MIMXRT1064DVL6A i.MX RT 1011: MIMXRT1011CAE4A,MIMXRT1011DAE5A i.MX RT 1024: EVKMIMXRT1024     Multiple options for configuration of MCU packages, Build Toolchain and embedded Target Connections are available via Simulink Model Configuration UI       Multiple MCU peripherals and Drivers are supported. The following subsystems highlighted in red as supported in Simulink environments in various forms: blocks, files, options                           i.MX RT 117x derivatives     i.MX RT 106x derivatives i.MX RT 101x derivatives     Basic and Advanced Simulink Block configuration modes via MCUXpresso Configuration Tools 11.0 UIs for Pins, Clocks, and Peripherals       MATLAB/Simulink versions 2019a – 2021b are supported for Design, Simulation, Code Generation, and Deployment of applications on i.MX RT 117x,106x, 102x & 101x Series. Other i.MX RT devices will be supported in future versions of the toolbox. Support for Software-in-Loop (SiL), Processor-in-Loop (PiL), and External Mode (classic serial, XCP Over Serial, and XCP over Ethernet). RTCESL – Real-Time Control Embedded Software Motor Control and Power Conversion Libraries (limited support designed for Motor Control applications). A future update will enhance the number of functionalities supported by Simulink.     Simulink Example library with more than 200 models to showcase various functionalities:   Integrated PMSM Motor Control Sensor/Sensor-less application for both IMXRT1060-EVK and IMXRT1170-EVK:     Target Applications with MATLAB/Simulink This release of the Model-Based Design Toolbox can be used to design, build, and test applications from multiple domains: INDUSTRIAL AC Meters Motion Control Robotics HMI SMART CITY/HOME Video Surveillance Identification Appliances Speakers   AUTOMOTIVE HVAC ECU     Target Audience This release is intended for technology demonstration, evaluation purposes, and prototyping for i.MX RT 1xxx MCUs and their corresponding Evaluation Boards: EVK-MIMXRT1170 EVK-MIMXRT1060 EVK-MIMXRT1064 EVK-MIMXRT1010 EVK-MIMXRT1024       Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt Technical by System Tools: https://web.microsoftstream.com/channel/618ab630-c8da-4fa8-ade8-5aa70a353124      
View full article
  Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K1xx – version 4.3.0 Austin, Texas, USA - September 13, 2022   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K1xx version 4.3.0. This release supports automatic code generation for S32K1xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K1xx Automotive Microprocessors. This new release adds support for RDDRONE-772B  Battery Management Systems (support for MC3377xC), Code deployment directly from Simulink via JTAG/SWD (OpenSDA, PeMicro Probe, or SEGGER JLink), SIL/PIL support for the latest MATLAB versions, new community and customer requested features (Enhanced support for SBC, FCAN Blocks, UART Blocks, I2C Blocks) and many other various new functionalities to help customers with rapid prototyping with NXP S32K1xx microcontrollers.   FlexNet Location: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   Activation link: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   Technical Support: NXP Model-Based Design Toolbox for S32K1xx issues are tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content Automatic C code generation based on S32K SDK 4.0.0 RTM drivers from MATLAB® for NXP all S32K1xx derivatives: S32K142W MCU Packages with 48/64 LQFP (*updated) S32K144W MCU Packages with 48/64 LQFP (*updated) S32K116 MCU Packages with 32QFN and 48LQFP (*updated) S32K118 MCU Packages with 48/64 LQFP (*updated) S32K142 MCU Packages with 48/64/100LQFP (*updated) S32K144 MCU Packages with 48/64/100LQFP and 100BGA (*updated) S32K146 MCU Packages with 64/100/144LQFP and 100BGA (*updated) S32K148 MCU Packages with 144/176LQFP and 100BGA/QFP (*updated) Multiple options for packages and clock frequencies are available via Model-Based Design Toolbox S32K Simulink Main Configuration Block       Added Support for RDDRONE-BMS772         We added examples for the RDDRONE-BMS772. This is a standalone BMS reference design suitable for mobile robotics such as drones and rovers, supporting 3 to 6-cell batteries. MBDT examples cover applications like BMS, LCD, CAN and SBC.       Battery Management System (BMS) support for MC3377xC – examples, documentation and FreeMASTER UI are available Special Simulink Blocks have been added to simplify the way a user can initialize such a controller, read vital parameters (like cell voltage, stack voltage, temperature, current), and manage the whole system. The entire suite of blocks is easily integrated within the new Battery Management Toolbox from Mathworks, so users can leverage these algorithms on top of our blocks.       Enhanced FCAN Support We improved the FCAN communication support by addressing the following: FCAN communication is now fully functional when external SBC is configured (for both UJA113x and UJA1169) The user is able to retrieve the ‘Error Status’ of an ongoing transfer and abort it in case something is wrong. The ‘Receive’ and ‘Send’ blocks for FCAN now allow the user to specify when the initialization for the message buffers should be executed (during Model Initialization, at each execution of the block, or none). If the ‘NONE’ option is selected, a newly added block ‘FCAN_MBConfig’ can be used to configure the message buffer. The FCAN messages ID can also be provided via an input port for both ‘Send’ and ‘Receive’ operations.   Multiple S32K1xx peripheral support. The peripheral coverage for each of the S32K1xx derivatives is shown below:   S32K116 S32K118       S32K142   S32K144         S32K146 S32K148       Added support for JTAG deployment directly from Simulink We added support for deployment over JTAG directly from Simulink. In the main Config block, under Target Connection, the JTAG option must be selected. Following this action, the JTAG Interface selection becomes active. Here is the following selection: OpenSDA Embedded Debug – the EVB Embedded Debugger is used. USB Multilink PEmicro – an external PEmicro probe is used. SEGGER JLink – this action requires the external selection of the SEGGER JLink     Extended support for MATLAB versions We extended support for our toolbox to cover a wider range of MATLAB releases – starting from R2016a and going up to R2022a. This way we want to avoid locking out users that have constraints regarding MATLAB versions.   New community-requested features In our efforts to make  NXP’s Model-Based Design Toolbox for S32K1xx version 4.3.0 fit the needs of the users, we have added the following requested features/updates: Added OSIF Time Delay Block Added Code Size Report Added NONE option for the SPI SIN/SOUT pins Enabled support for more than one ADC Interleave Block Updated Profiler functionality Updated FCAN Blocks Updated I2C Blocks Updated LPUART Blocks Fixed Registers dropdowns not displaying options on some machines   100% S32K1xx supported peripheral coverage with examples. Approximately 300 examples are available as part of the toolbox that exercises all the functionalities supported.     For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K1xx MCUs and evaluation boards solutions out-of-the-box with: NXP Support Package for S32K1xx Online Installer Guide Add-on allows users to install the NXP solution directly from the MathWorks website or directly from MATLAB IDE. The Support Package provides a step-by-step guide for installation and verification. NXP Model-Based Design Toolbox for S32K1xx version 4.3.0 is fully integrated with MATLAB® environment in terms of installation, documentation, help and examples:       Target Audience This release (4.3.0) is intended for technology demonstration, evaluation purposes, and prototyping for S32K116, S32K118, S32K142, S32K144, S32K146, S32K148, S32K142W, and S32K144W MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt      
View full article
General Tip of the day Tip of the day  Licensing MBDT license missing error  Toolbox functionality Registers, Linkers not displaying options  Profiler/Execution S32k144 Simulation Time and Profiler  Peripherals How to put MCU into sleep? Apps Motor Control
View full article
Get to know NXP Model-Based Design Toolbox™—a connection between MathWorks and NXP ecosystems that allows rapid prototyping of complex embedded designs on NXP microcontrollers. In this presentation, @Irina_Costachescu and @mariuslucianand  will highlight the main features of the NXP Model-Based Design Toolbox. They will demonstrate how to design a BMS application, covering the main development phases from an idea to a running on target prototype. Register here: https://www.matlabexpo.com/online/2022.html 
View full article
This page summarizes all Model-Based Design Toolbox topics related to the DSC Product Family. Model-Based Design Toolbox for DSC- Release Notes: Rev 1.0.0 - NXP Model-Based Design Toolbox for DSC MC56F8x MCUs - version 1.0.0 
View full article
    Product Release Announcement EDGE PROCESSING NXP Model-Based Design Toolbox for DSC MC56F8x MCUs - version 1.0.0 Bucharest, Romania  December 15th , 2021   The Edge Processing Tools Team at NXP Semiconductors is pleased to announce the release of the Model-Based Design Toolbox for DSC MC56F8x Series version 1.0.0. This release supports automatic code generation for peripherals and applications prototyping from MATLAB/Simulink for NXP’s DSC MC56F81xxx and MC56F83xxx Series of MCUs based on DSP568000E core. NXP Download Location https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX MATHWORKS Download Location https://www.mathworks.com/matlabcentral/fileexchange/103600-nxp-support-package-dsc  Version 1.0.0 Release Content Automatic C code generation based on MCUXpresso SDK 2.7.3 drivers and MCUXpresso Configuration Tools 10.0 initializations from MATLAB®/Simulink® for:   MC56F81xxx        MC56F81868VLH, MC56F81646VLF, MC56F81648VLH, MC56F81663VLC,      MC56F81666VLF, MC56F81668VLH, MC56F81743VLC, MC56F81746VLF,      MC56F81748VLH, MC56F81763VLC, MC56F81766VLF, MC56F81768VLH,             MC56F81866VLF, MC56F81643VLC                                     MC56F83xxx     MC56F83789VLL, MC56F83683VLH, MC56F83686VLL, MC56F83689VLL,     MC56F83763VLH, MC56F83766VLK, MC56F83769VLL, MC56F83783VLH,     MC56F83786VLK, MC56F83663VLH   Multiple options for configuration of MCU packages, Build Toolchain and embedded Target Connections are available via Simulink Model Configuration UI     Multiple MCU peripherals and Drivers supported. The following subsystems highlighted in red as supported in Simulink environments in various forms: blocks, files, options MC56F81xxx derivatives MC56F83xxx derivatives   Basic and Advanced Simulink Block configuration modes via MCUXpresso Configuration Tools 10.0 UIs for Pins, Clocks, and Peripherals   MATLAB/Simulink versions 2020a – 2021b are supported for Design, Simulation, Code Generation, and Deployment of applications on MC56F81xxx and MC56F83xxx Series. Other MC56F8x devices will be supported in future versions of the toolbox. Support for Software-in-Loop (SiL), Processor-in-Loop (PiL); RTCESL – Real-Time Control Embedded Software Motor Control and Power Conversion Libraries for DSP568000E core.     Simulink Example library with more than 100 models to showcase various functionalities:   Integrated PMSM Motor Control Sensor/Sensor-less application for MC56F83000-EVK: Integrated application that uses the on board FXOS8700CQ accelerometer and magnetometer sensor for both MC56F81000-EVK and MC56F83000-EVK.    Target Applications with MATLAB/Simulink This release of the Model-Based Design Toolbox can be used to design, build, and test applications from multiple domains: INDUSTRIAL AC Meters Motion Control Robotics HMI       Target Audience This release is intended for technology demonstration, evaluation purposes, and prototyping for DSC MC56F8x MCUs and their corresponding Evaluation Boards: EVK-MC56F81000 EVK-MC56F83000 Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt    
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to DSC MCUs Product Family.
View full article
This page summarizes all Model-Based Design Toolbox videos related to DSC MCUs Product Family.
View full article
General Tip of the day Tip of the day  Model Reference Model referencing in i.MX RT Toolbox  Peripherals FLEXCAN How to set i.MX RT FlexCAN receive message buffer Mask for range of IDs ?   LPI2C How to use LPI2C in transfer mode in i.MX RT  LPUART Questions about i.MX RT LPUART driver  Apps
View full article
        Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for HCP – version 1.1.0 RFP       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for HCP version 1.1.0. This release supports automatic code generation from MATLAB/Simulink for S32G2xx, S32S2xx, and S32R41 MPUs. This new product adds support for running Processor-in-Loop and Software-in-Loop simulation on S32R41 (ARM Cortex-A53).   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/product?child_plneID=683951   Technical Support: NXP Model-Based Design Toolbox for HCP issues will be tracked through NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32G2xx derivatives: S32G274A Automatic C code generation from MATLAB® for NXP S32S2xx derivatives: S32S247TV Automatic C code generation from MATLAB® for NXP S32R4x derivatives: S32R41 Supported Evaluation Boards GoldBox Development Platform (S32G-VNP-RDB2 Reference Design Board) GreenBox II Development Platform X-S32R41-EVB Development Board Support for MATLAB versions: R2020a R2020b R2021a R2021b Simulation mode: We provide support for Software-in-Loop (SIL) and Processor-in-Loop (PIL) simulation mode with code execution profiling:   Includes the HEV demo (S32G2xx, S32S2xx):   Includes the RADAR demo - MFSK Radar Range and Speed Estimation on Multiple Targets (S32R41), in collaboration with Gamax Laboratory Solutions Kft.:   Includes an Example library with 16 examples that cover: Software-in-Loop (SIL), Processor-in-Loop (PIL)   GUI to help you setup the toolbox and the evaluation board :     For more details, features and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32G2xx, S32S2xx, and S32R41  processors and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for HCP version 1.1.0 (RFP) is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.1.0 RFP) is intended for technology demonstration, evaluation purposes and prototyping S32G2xx, S32S2xx, and S32R41 and Evaluation Boards.   Useful Resources Examples, Trainings and Support: https://community.nxp.com/community/mbdt    
View full article
          Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.1.0 RTM     Austin, Texas, USA December 20, 2021 The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.1.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K344 and S32K312 MCUs and part of their peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, UART, GPT). To enable BMS applications development, we have added support for MC33775A battery cell controller (& MC33664PHY). In this release, we have also added 2 new motor control applications (for both PMSM and BLDC), as well as updated FreeMASTER, AMMCLib, and GCC compiler to the latest versions. The product comes with over 100 examples, covering everything that is supported, including demos for battery cell controllers (BCC) and motor control.   Target audience: This product is part of the Automotive SW – S32K3 Standard Software Package.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=12920897   Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K344 S32K312   Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI UART GPT DIO   Support for MC33775A battery cell controller & MC33664PHY The toolbox provides support for the MC33775A and MC33664. The MC33775A is a lithium-ion battery cell controller IC designed for automotive applications which perform ADC conversions of the differential cell voltages and battery temperatures, while the MC33664 is a transceiver physical layer transformer driver, designed to interface the microcontroller with the battery cell controllers through a high speed isolated communication network. The ready-to-run example provided with the MBDT for S32K3 shows how to communicate between the S32K344 and the MC33775A via the MC33664 transceiver. The MCU configures the battery cell controller to perform Primary and Secondary chains conversion, reads the cell voltages conversion results from the MC33775A, and displays the values to the user over the FreeMaster.     Added new motor control examples The toolbox provides examples for both 3-shunt PMSM and BLDC motor control applications. Each of them has a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization.     Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the configuration for it once. After it is saved as a custom default project, it can be used for every model that is being developed.     Support for AUTOSAR blockset (SW-C deployment) Updated to the latest version of RTD (v1.0.0) and GCC(v10.2) Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.26: All functions in the Automotive Math and Motor Control Functions Library v1.1.26 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2020a R2020b R2021a R2021b   S32Design Studio Integration We provide a simple mechanism to let users the opportunity to export the code generated from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project or for debugging purposes.     Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode     Examples for every peripheral/function supported: We have added over 100 examples, including: Motor control applications (PMSM and BLDC) Communication (SPI, CAN, UART) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode   For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.1.0 is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.1.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt    
View full article
Introduction The aim of this article is to help any user of Model-Based Design to enjoy his/her own custom C libraries or to call any C drivers or components that are not yet supported by NXP's toolbox. This uses the Matlab Coder and requires to include only a MATLAB function block in which the model will call a C function. For more details, you can have a look on the Mathworks Help Center at Integrate C Code Using the MATLAB Function Block- MATLAB & Simulink.   BMS System In my opinion, the greatest way to learn something is "learning-by-doing". So in this tutorial, we will add support for the BMS System in Model-Based Design for S32K. You are already familiar with our toolbox supported boards so let's talk a bit about this BMS system. NXP has a great cell controller IC designed for automotive and industrial applications, more details can be found here MC33772B | 6-Channel Li-ion Battery Cell Controller IC | NXP. For this tutorial, we will use the FRDM33772BSPIEVB | MC33772 SPI EVB | NXP  board, which handles up to 6 battery cells and connects to many NXP controllers via SPI. This is also compatible with the S32K family with some minor jumpers adjustments, but all the instructions can be found on the product page.  So the goal of this project is to be able to read the cell voltages from an MBDT Simulink model. Main Steps In order to include custom code, the user should follow these steps: 1. Add the directory path from which the Simulink will include the directories under Settings > Code Generation > Custom code > Include directories. 2. Insert a Matlab Function block in the Simulink model. This will be used for initialization. The goal here is to include the c headers in the generated code files. This requires to declare coder constant using the coder.const function. That has to be updated in the Build info using coder.updateBuildInfo . Here, the headers and the sources has to be included following this template: %% Adding  header information to the generated code coder.cinclude('driver.h'); %% Adding source files to MakeFile coder.updateBuildInfo( 'addSourceFiles', 'driver.c' ); This operation has to be performed only once. 3. When the user needs to call a custom function from the Simulink, the user must add a Matlab Function block, declare the inputs and outputs as required. Inside the Matlab Function code, the coder.ceval function must be called using the parameters provided as inputs. For example, if the user needs to call a C function called BMS_Init with no parameters, the following line of code will perform that: %% Initializing the BMS driver coder.ceval('BMS_Init'); If the user needs to provide an input parameter, then it will be provided either directly, either using coder.ref  as an argument or using coder.rref if the reference to that value has to be passed. function BMS_Init(parameter)    if( coder.target( 'Rtw' ) )          coder.ceval('BCC_Init', parameter);          coder.ceval('BCC_Init', coder.ref(parameter));     end end This will generate the following code: BCC_Init(true); BCC_Init(&parameter); But if the code is more complex, the easiest way is to declare a wrapper function and to call the wrapper using the coder.ceval. BMS Support This scenario fits on most of our users requirements: to use a piece of code unsupported yet on MBDT. For this IC, NXP already provides the KIT3377x_DRV driver together with an example in S32DS which measures cell voltages and displays it using FreeMaster.   We created an S32K project for the S32K144 board, added the FreeMaster block and an LPSPI Instance according to the settings and the pin requirements by the MC33772 board. The Initialize variable will only be used to call the initialization sequence for the BMS. Now, as we described in the previous chapter, we declared a folder "bcc" that contains the required drivers and some wrappers, also inserted in the Configuration parameters. The initialize function contains a Matlab Call Function. This one includes all the steps described at the second point. What should be noticed here is the check from line 7. All that cinclude code will be called only when the coder.target is Rtw. If the user adds an else condition, that code will be called only when simulate. Now, MBD_MCC_Init is wrapper designed to perform all the initialization steps from the driver. It was easier like this. The MC33772 has been initialized so whenever the user needs the values, he/she must add a Matlab Function block that will provide the values to the model.   The code behind this block has been attached in the next image. The output values from the getCellMeasurements are provided as outputs and inside the get_cellVoltages, it will call the C updateMeasurements function using the coder.wref function. Running BMS Now, after we solved some bugs during code generation   and had successfully built the code, we can run the generated code on the board. The following screenshot represents the Voltages and a variable Current measurement converted by the MC33772.   Conclusions In this article, we presented a method of getting the needed C libraries/drivers/code in the Simulink model using custom code and Matlab Coder. We provided a short step list and a more detailed tutorial for an actual application, a Battery Management System, using NXP hardware. This approach can be successfully achieved either if we use the S32K or MPC Toolboxes. Later edit (1): As requested, I attached the model and the FreeMaster project for achieving the measurements from the MC3377xB (FRDM3377xBSPIEVB) with the S32K144 board using Model-Based Design and custom code. In order to run it, you must follow the steps: 1. Download and unzip the archive there is a bcc folder inside, next to the s32k_mc3377x.mdl. 2. Download the SDK (Embedded SW: MC33771/MC33772 SW Driver | NXP )  BCC SW Driver package for MC33771B/MC33772B (Lite version) and from the SDK folder bcc copy all the files to the bcc folder of the model.  I can not add the SDK driver in the archive since for the BCC SDK there is an agreement that you must read before download. 3. Open the s32k_mc3377x model, go to the BMS_Init function and replace the line 4 string with the full path of the model bcc location folder. 4. After this, the code should be generated and run successfully. Later edit (2): If you are interested to get the solution alongside the instruction on how to connect the MC3377xB and the MPC5744P via Model-Based Design Toolbox, please have a look at this question here: MPC5744P &MC33771B Configuration Later edit (3): As many of you requested, we've added the example code for the S32K144 & FRDMDUALMC33664 to communicate with the MC33771C. See the attached archive. bms_s32k_frdm2_771c_tpl_cc. The bcc driver for the MC33771C is different than the one for the MC33771B and you have to download the missing files from here.   Happy hacking! Marius
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to HCP Product Family.   S32G2 Hybrid Electrical Vehicle (HEV) demo on S32G2 
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to S32K3xx Product Family.
View full article
    Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.0.0 RTM       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.0.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K344 MCU and part of its peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, GPT). It also adds support for FreeMASTER, AMMCLib, and Simulink simulation modes – Software-in-Loop, Processor-in-Loop, and External mode. Moreover, this release adds the option to configure everything (pins/peripherals/clock) via an external configuration tool - S32 Configuration Tools or EB Tresos. The product comes with over 70 examples, covering everything that is supported, including a motor control application demo. FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=12747097 Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K344 Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI GPT DIO Support for profiling execution times Support for register R\W and memory R\W operations Provides 2 modes of operation: Basic User Mode – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced User Mode – using S32Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.24 for: All functions in the Automotive Math and Motor Control Functions Library v1.1.24 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2020a R2020b R2021a S32Design Studio Integration We added a simple mechanism to provide users the opportunity to export the generated code from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project, as well as for debugging purposes.   Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode   Examples for every peripheral/function supported: We have added over 70 new examples, including: Motor control application Communication (SPI, CAN) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.0.0 is fully integrated with MATLAB® environment in terms of installation: Target Audience This release (1.0.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.    Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt    
View full article