NFC Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Knowledge Base

Discussions

Sort by:
MIFARE DESFire Light read and write demonstration
View full article
This document show the detail steps of following the Personalization example in AN12196. Tool : Pegoda3 and RFIDDiscover.    
View full article
The video shows how to read the NDEF message under password protection. For more details , please kindly refer to https://community.nxp.com/docs/DOC-347622 
View full article
LPCD (Low Power Card Detection) works on the principle that the I and Q values are extracted from the RF signal captured on the RX pins. These values are then compared with the I and Q data obtained using LPCD calibration. If the difference is greater than the chosen I and Q threshold, the load is detected and the IC wakes up.  1// LPCD Way of working  Run LPCD Calibration  It is recommended to use an external power supply to supply the EVK board. If the USB supply is used, the value can fluctuate because of the transition effects.  Run "Single LPCD" and check the performance  Adjust the I and Q thresholds  Low value -> Better detection range, more false wake-ups  High value -> Worse detection range, fewer false wake-ups  The number of samples, RSSI, and VDDPA parameters typically remain at their default values.  Tomas_Parizek_0-1758116172644.png 2// Auto LPCD  When the "Auto LPCD" is used, the LPCD algorithm always performs LPCD Calibration before entering the LPCD. Tomas_Parizek_2-1758117682336.png 3//Semi-autonomous LPCD mode (PN5190 only)   The user can evaluate the I and Q values behaviour under loaded/unloaded conditions. Based on that, the LPCD threshold can be properly selected.  Use the same "Register" RSSI Target and Hysteresis as for "EEPROM" Calibrate LPCD Run "Endless I/Q read"  Check how the I and Q values change With no card/object in the antenna proximity  with a NFC card/object in the antenna proximity Tomas_Parizek_3-1758117823769.png
View full article
This article describes how to evaluate ULPCD feature together with PN7642 EVK (OM27642EVK) and NFC Cockpit.  1// Disable DC-DC in EEPROM  OM27642EVK does not required any HW changes for ULPCD (**). User is only required to change the following settings in EEPROM  (disable DC-DC converter). Address: 0x0000 (Secure_Lib_Config) Value: 0x21  Reset the board after writing the value.  Tomas_Parizek_0-1745904468298.png **Note: To ensure an accurate and reliable ULPCD evaluation—particularly for ULPCD current measurements. We strongly recommend implementing the following hardware modifications on the OM27642EVK. PN7642_MB.png Note: New revision of the board already have R4=DNP, R8=0Ω. Kindly check this on your board. 2//Set required ULPCD settings in EEPROM  ULPCD VDDPA -> Typically 1.5V. If the HF attenuator is 0x00, increase e.g. to 1.8V. Since the detection range does not significantly depend on the power level, there is no need to set VDDPA above 2 V. Higher VDDPA results in increased current consumption in ULPCD, but does not significantly improve detection performance. RF On Guard time -> This value can be reduced to the minimum -> 5.2 us RSSI Guard time -> Recommended value is 25 RSSI Threshold -> Typically 4~6 Number of RSSI samples -> Typically -> 0 (4 rounds) PN7642_EEPROM_ULPCD.png 3// Perform "Reads HF Attenuator"  Once the required ULPCD settings is set (Guard times, Threshold....). Then User has to perform "Reads HF Attenuator". Make sure that the "HF Attenuator" option is checked.  As written above, the value must not be 0x00. If so, increase VDDPA. 4// Perform ULPCD Calibration and check RSSI Value  For OM27642EVK, the RSSI value for unloaded antenna is typically around 1400dec - 1600dec. 5//Enter ULPCD mode  User can enter the ULPCD mode. The board will again be connected once the load change is detected (e.g. NFC card or smartphone in the antenna proximity). 6// Typical detection performance for 65 mm x 65 mm Antenna tuned to 35Ω.   Tomas_Parizek_0-1782466647959.png MIFARE DESFire EV3: Class 1 Antenna  ICODE SLIX: Class 1 Antenna  ICODE 3: Class 6 Antenna 
View full article
https://community.nxp.com/docs/DOC-340244 
View full article
RF power regulation is a critical factor in the development of NFC devices, as it directly influences performance, reliability, and compliance with industry standards. There are three main reasons for this:  If the PN7642 VUP current exceeds the limit given by the product Data sheet, the PN7642 can be damaged. If too high RF power is radiated from the antenna, there exists a risk for NFC Cards. Too high RF power might lead to exceeding a given RF limit (NFC Forum, ISO, EMVCo). NXP provides comprehensive documentation on Dynamic Power Control for the PN7642 and PN5190. Designers are expected to adhere to these guidelines, especially when aiming for compliance with standards such as EMVCo. PN5190 Dynamic Power Control Quick Calibration and TxShaping Demo Automatic DPC Calibration for PN7642 and PN5190 However, if the user's design is intended for infrastructure applications, such as a smart lock. At a minimum, Dynamic Power Control (DPC) should be enabled to serve as a current limiter. The evaluation can be done with the help of NFC Cockpit.  1// Start DPC Calibration  "Press" Start DPC Calibration  "Press" Load protocol  Make sure that the DPC is "Enabled" Tomas_Parizek_0-1760618955468.png 2// Adjust current reduction table  Set all entries to "0" Write into EEPROM Tomas_Parizek_0-1760618870172.png   3// Set the "Target" current Use approx. the same current as "TxLDO Values"  The limit may be set higher, e.g., to 300 mA, if the purpose is solely to provide overcurrent protection for the IC. Save to EEPROM Restart the board (Close port -> Press VEN->Open port) Tomas_Parizek_0-1760618702129.png   4// Check the power regulation  Start DPC Calibration  Place a card or any metal object in the antenna's proximity  Observe VDDPA and "TxLDO" current  The current should stay around the given target  The VDDPA will drop once the antenna is loaded  Tomas_Parizek_2-1760619391451.png 5// Set a minimum VDDPA in DPC  In the case that the current is still too high, a user can define a minimum VDDPA that is used for the DPC regulation. By default, this value is set to 2.2V. The user can decrease it up to 1.5V.  In that case, NXP also recommends disabling the RDOn control.  Tomas_Parizek_1-1761307899864.png Note: The User has to consider the "DPC_TXLDO_MAX_DROPOUT" parameter, which defines the maximum voltage drop on TXLDO. By default, it is set to 3.6 V. That means if the user wants to use the minimum VDDPA 1.5 V, then the maximum TXLDO input shall not exceed 5.1 V. This feature protects the TXLDO from overheating.    Once the evaluation is done, the customer shall program the following EEPROM entries in their application. For more info, see PN7642 Product Data sheet.  DPC_CONFIG (Address: 0x0068) -> example: enabled -> 0x01 DPC_TARGET_CURRENT (Address: 0x0069) -> example: 229 mA -> 0xE5 DPC_TXLDO_MAX_DROPOUT (Addresses: 0x0073 - 0x0074) -> example: 3.6 V -> 0x10,0x0E DPC_TXLDOVDDPALow (Address: 0x006F) -> example: 1.5 V -> 0x00 DPC_HYSTERESIS_LOADING (Address: 0x006B) -> example: 20 mA -> 0x14 DPC_HYSTERESIS_UNLOADING (Address: 0x006E) -> example: 10 mA - 0x0A DPC lookup table entries (Addresses: 0x007D - 0x0125) -> example: for current limitation only -> all 0x00 If a user does not want to use a maximum range of VDDPA during DPC (5.7V), e.g., their system uses a 3.3V supply domain. Then, the maximum VDDPA in DPC can be limited by the following EEPROM settings:  TXLDO_VDDPA_MAX_RDR (Address: 0x0007)-> example: 3.0 V -> 0x0F Note: TXLDO has approx. 0.3V voltage drop. Always set this parameter 0.3V lower. Once this is done, the user has to check the "TxLDO" current and adjust the target current accordingly. In this case, to approximately 150 mA. If you don´t change it, the DPC starts to limit the power around 229 mA, as has been set in a previous step.  Tomas_Parizek_0-1761307791719.png
View full article
The NXPNCI-KDS_Example for the PN7120/PN7150 Arduino interface boards available in NXP webpage at the time of publishing this document includes a project compatible with KSDK v2.0 for FRDM-K64F platform. With the latest KSDK v2.1 some changes in the drivers along with the later FreeRTOS v9.0.0 make the build process fail when following the instructions in the application note AN11845 NXP NCI KDS Example due to incompatibilities. Meanwhile until the project in NXP webpage is updated there is a temporary project attached to this document fixed to work with KSDK v2.1. The steps to build this project are the same as explained in the appnote, summarized below: - Download and install KSDK v2.1 for FRDM-K64F using MCUXpresso SDK online builder: Welcome to MCUXpresso | MCUXpresso Config Tools  Create a new workspace in KDS IDE. Import the "NXPNCI-KDS_Example_KSDK2.1" project from the archive file. Update the PROJECT_KSDK_PATH build variable according to the installation path of KSDK v2.1. Build the project. For more details please refer to the application note AN11845. Regards! Jorge Gonzalez
View full article
A user can evaluate the current consumption of PN7642 in low power modes with the help of the PN7642 Evaluation Board (OM27642) and:  MCUXpresso SKD example (LPCD)  NFC Cockpit or MCUXpresso SKD example (ULPCD) NXP defines the current consumption in ULPCD/LPCD as VBAT current + VDDIO current for the LPCD/ULPCD cycle time of 330 ms. Make sure that DC/DC is disabled (for ULPCD).  Where:  VBAT current = VBAT_Current + VBATPWR_Current + VUP_Current See the snapshot from the PN7642 Datasheet below:  Tomas_Parizek_3-1753772522698.png   See where to measure the currents on PN7642 EVK: J63 and J64 are used for enabling/disabling the LEDs that are connected to PN7642 GPIOs. They must be disabled for a proper VDDIO current measurement.  A modification of R69 and R70 is necessary to perform the current measurement on VDDIO in LPCD mode. Tomas_Parizek_1-1759325994089.png   1. ULPCD current consumption evaluation For the ULPCD evaluation, the NFC Cockpit or SDK example can be used. In this article, we will focus on evaluation using the NFC Cockpit.  See the used ULPCD configuration:  Tomas_Parizek_0-1778131034323.png Note: The current should be measured as an average over, e.g., 30 seconds.  1.1 Overall ULPCD current measurement  To measure all currents together on PN7642 EVK, a user can create a measurement fixture as shown below:  Tomas_Parizek_0-1759471417973.png Real setup :  Tomas_Parizek_1-1759414417352.png Then the overall results look as follows: Tomas_Parizek_1-1778131365857.png Note: The Antenna is tuned to approx. 35 Ohms  In this case, the ULPCD current is approximately 21 μA. This current can be further optimized, for more details, see -> AN14518(Start-up optimization in ULPCD (PN5190/PN7642/PN76AC)) 2. LPCD current consumption evaluation The user has to import the example (pnev7642fama_nfc_low_power_mode_Pub) from the PN7642 SDK.  Before building it, the following change in the code has to be made:  -> Comment line 84 Tomas_Parizek_0-1753279011326.png   A user can adjust the LPCD cycle time as shown below: Tomas_Parizek_0-1753781089650.png   1.1 VBAT Current measurement  Tomas_Parizek_0-1754311084128.png   In this case, the VBAT current is approximately 123 μA. 1.2 VBATPWR current measurement  Tomas_Parizek_1-1759218118702.png In this case, the VBAT_PWR current is approximately 91,8 μA. 1.3 VUP Current measurement  Tomas_Parizek_0-1759217512751.png In this case, the VBAT_PWR current is approximately 32,8 μA.  Note: This current depends on the LPCD VDPPA settings + Antenna Impedance tuning  1.4 VDDIO Current measurement Note: Before VDDIO measurement, place jumpers J63 and J64 on PN7642 EVK. This will disable LEDs that are connected to PN7642 GPIOs.  The VDDIO current measurement requires the following steps:  Run the "pnev7642fama_nfc_low_power_mode_Pub" example  Once the example is running, disconnect the debugger (J-link, LPC-Link...) from J21 (NFC Debug connector)    Remove R70  Populate a 10K resistor on the R69 position (it disables the SWD interface) Once the measurement is done, change it back to the default state (R70=0R, R69=Open). Note: It is recommended to prepare the board with the option to easily populate or remove R70 and R69 when the LPCD example is running. E.g., with the help of jumpers/pin headers as shown below.   Tomas_Parizek_2-1754383701294.png Only then will the correct VDDIO be measured on PN7642 EVK.  See the VDDIO current measurement below:  Tomas_Parizek_0-1754382925680.png   In this case, the VDDIO current is approximately 5,48 μA.  Then the overall current comsumption in LPCD is I_VBAT + I_VDDIO= (123 + 91,8 + 32,8 + 5,48) = 253,08 μA Note: For this measurement, the NFC Cockpit is not suitable because the IC does not go into standby mode between LPCD RF pings. Meaning LPCD works normally, but a user can measure higher current consumption. Used Ampere meter -> Power Profiler Kit II Measurement has been performed with FW 2.6  Board supply (jumpers J1, J2 and J4) -> 3.3V Please note that this measurement is indication only! 
View full article
In the case, the Reader output power cannot be further reduced with the help of the tuning and TXLDO settings (e.g. EMI reasons)  Then further reduction can be done using DPC settings. The idea is to use just one DPC entry and adjust the GSN value as shown below: DPC Settings:  Tomas_Parizek_1-1718095662620.png   The DPC Entries (1-19) have been deactivated (Index Activate ->0), and only Entry 00 stays active.  Tomas_Parizek_0-1718095428668.png   An example (RF Field measured using a scope probe): No DPC, TXLDO 5V  image (1).png   NO DPC, TXLDO 2.7V image (2).png   DPC Activated, One Entry, GSN-> 0x05 image (3).png   DPC Activated, One Entry, GSN-> 0x01 image (4).png   Please consider that the reading performance will be impacted. 
View full article
https://community.nxp.com/docs/DOC-340389 
View full article
The latest NXP-NCI example is rev 1.6, and when you run this demo with the lpc11xx board, for example, lpc1115 rev A, and the OM5577, you may meet the following issue: The problem is due to two aspects: one is hardware and the other is software. For hardware solution, besides following what is described in AN11658 section 2.4 LPC11xx, you have to do one more thing: a) The I2C lines are not pulled-up: LPC11xx doesn't offer internal pull-up setting of the I2C lines so external pull-up resistors must be added. For software solution, the function of Sleep()( in tool.c) was optimized too much, and it didn't meet the timing requirement of OM5577, so we should let the IDE ignore it. The solution I use is as below: __attribute__((optimize("O0"))) void my_func() { blah } You may check the attachment for details. The result is shown as below: Original Attachment has been moved to: tool.c.zip
View full article
The PN7642 includes a USB interface, which allows USB communication with the PC.  Once the PN7642 USB communication is established, the NFC Cockpit tool can be used for RF debugging.  Note: This also requires flashing the NFC Cockpit application with the help of the mass storage mode or SWD interface.  Basically, the user has to connect a USB cable/Connector to the following PN7642 pins.  USB Signal  PN7642 Pin  5V  USB_VBUS Data - ATX_D Data + ATX_C GND GND   See an example below. This is a very basic connection (for evaluation or debugging only) where the USB cable is directly connected to the PN7642 pads.  This situation may arise during debugging on customer hardware where the USB interface is not yet implemented on the PCB. But a user wants to debug with the help of NFC Cockpit.  Tomas_Parizek_0-1758200945725.png   Please note that the proper USB interface might require special layout rules, such as impedance, overvoltage protection, etc.. For more info, see the PN7642 EVK reference schematic or USB PCB design guide. 
View full article
This article provides information on the expected NFC communication range for NXP products (Connected tags) when used with various mobile phones and the CLRC663 reader.   1// NFC Antenna 54 mm vs 27 mm (NTAG 5 Boost Antenna 10 mm vs 10 mm)    1.1// Used antenna Tomas_Parizek_1-1746003714114.png   1.2// Results  Tomas_Parizek_0-1746003481812.png Note: NTAG5 Link - Energy harvesting is disabled      2// NFC Antenna 25 mm vs 18 mm    2.1// Used antenna Tomas_Parizek_3-1746004068255.png   2.2// Results Tomas_Parizek_2-1746004001048.png Note: NTAG5 Link - Energy harvesting is disabled      3//NFC Antenna 25 mm vs 18 mm with "filling"    3.1// Used antenna  Tomas_Parizek_4-1746004293186.png   3.2// Results  Tomas_Parizek_0-1746004511921.png   Note: NTAG5 Link - Energy harvesting is disabled 
View full article
This porting guide is for FRDM-K82F, and it can also be used for any other platform supported by KSDK 2.2. The released NXPNCI-KDS_Example_KSDK2.2 is based on FRDM-K64F, so before porting, we need to configure and download KSDK 2.2 for FRDM-K82F. Please make sure you have selected Kinetis Design Studio before downloading. After downloading, extract the package to some folder like below: and change PROJECT_KSDK_PATH to this folder: Change project settings as below: Remove all files in the folder of drivers, and import new source files as below: and similar procedure for "startup" folder and "utilities" folder: Replace the source files in board folder with the files from some ksdk demo like hello_world: FRDM-K82F uses PTC3 for NCI_IRQ pin, PTC9 for NCI_VEN pin, and PTA1 and PTA2(I2C3) as the I2C interface. so add definition in board.c and modify BOARD_InitPins() as below: Change linker settings: -Build -Debug settings -Test Result:
View full article
Prerequities:  PN7642 design-in recommendations   1// Impedance tuning  PN76 family antenna design guide The target impedance is chosen based on the target application. If full power is required (e.g., POS terminals). The target impedance of 15-17 Ω is recommended. For lower power applications using ULPCD, the higher impedance is typically preferred, 30-50 Ω (symmetrical tuning).   2// Dynamic power control  PN7642 - Basic RF power limitation using DPC   3// H-Field check  There are given limits, especially for the maximum H-field radiated by the reader. Exceeding these limits might lead to destroying the NFC Card/NFC Tag.   The H-Field can be measured with the help of test equipment, as  ISO 10373-6 Test PICC EMVCo 3.0 Test PICC  For indication only, the customers can use "smart" Field Strength Probes as shown below :      Tomas_Parizek_0-1764148815270.jpeg   Note: The most critical position occurs when the card is placed directly on the NFC antenna . In this case, if the H-field exceeds the maximum allowed level, the output power must be reduced using DPC settings. 4// HF Attenuator value  Turn on the RF Field with the DPC set and enabled from the previous step  Read the CLIF_RXCTRL_STATUS register and check the HF_ATT_VAL as shown below.  Tomas_Parizek_1-1764147827990.png   The value for the "unloaded" condition with full power shall be approximately 35-45dec.  If the value is out of this range, the customer is required to adjust the Rx resistors to reach this value.  5// Receiver settings  Check the "Power" range and Communication Range with the default settings provided by NXP.  Power Range -> The distance at which the NFC Tag can still generate its answer, but the NFC Reader does not see it  Communication Range -> The distance at which the NFC Tag can still communitate with the NFC Reader  Ideally, Power Range ≈ Communication Range Also, the NFC Reader should not generate any false communications as e.g., "HAL COLLISION ERROR".  The optimisation of the receiver can be done in the following way:  Enter DPC Calibration  Go to the "ARC" menu and "disable" the ARC algorithm   Tomas_Parizek_0-1764153827503.png   This will force the IC to use the RX settings from the following Register/EEPROM SIGPRO_RM_TECH_REG DGRM_RSSI_REG   5.1// SIGPRO_RM_TECH_REG (RM_MF_GAIN parameter) This parameter basically defines the gain of the input amplifier.  Select SIGPRO_RM_TECH_REG  Switch "operation" to EEPROM and choose the required technology  Increase the RM_MF_GAIN to 0x02 (it depends on the setup).   Tomas_Parizek_0-1764154133976.png   5.2// DGRM_RSSI_REG (DGRM_SIGNAL_DETECT_TH_OVR_VAL parameter) This parameter defines a threshold from which the internal logic starts to decode the incoming signal.  If the threshold is too low or very close to the noise floor, the system can detect the noise as an NFC Communication.  It is therefore,  Threshold + margin > noise floor The best routine is to perform "Signal Detection Threshold" analysis. This can be done with the help of the NFC Cockpit (described in PN7642 design-in recommendations) As a result, the user can obtain the mean value of the "Noise," and suggested "DGRM_SIGNAL_DETECT_TH_OVR_VAL" threshold based on the inserted "Margin."  Maring (m) + Noise mean value (μ) = Threshold  6+16=23 Then this value shall be written in "DGRM_RSSI_REG" EEPROM as shown below.    Tomas_Parizek_0-1764155707250.png   6// ULPCD Settings  We recommend the following ULPCD Settings as a starting point.  ULPCD VDDPA should be chosen in such a way that the HF Attenuator value is not 0x00! The typical value for HF Attenuator in ULPCD is around 0x05-0x0B.   6.1// RSSI Threshold evaluation  For a proper RSSI Threshold selection, it is recommended to perform the ULPCD Calibration, e.g., 20 times, and check the "jitter" of the RSSI signal for your device.  Tomas_Parizek_1-1782466350613.png   If you see that the RSSI value is jittering, e.g., 1 unit as shown above. The absolute minimum threshold for this case is 2. However, it is always recommended to include adequate margin (To prevent false wake-ups).   Generally, the margin of 2 units is sufficient. So in this case, the optimum threshold will be 4. 
View full article
Prerequisites:  PN5190 instruction layer-> https://www.nxp.com/docs/en/user-manual/UM11942.pdf NFC Cockpit -> https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-cockpit-configuration-tool-for-nfc-ics:NFC-COCKPIT   In case of PN5190, the NFC cockpit can only show a generic error messages. More detailed error description has to be decoded from the received "FrontEnd Packets" 1. See an example of the error returned after ULPCD calibration    Tomas_Parizek_1-1744177946726.png 2.  The Errors description is descibred in  PN5190 instruction layer UM. However, the error has to be "decoded"  →> Take the received packets before the error ntf. in NFC Cockpit → 80 00 0C 02 02 00 00 BB 07 00 00 23 00 00 00 Where:  2.1. Decode the "Event" 02 02 (Little endian format) → General_Error_Event + LPCD_Calibration_Done_Event Tomas_Parizek_2-1744178043076.png Tomas_Parizek_3-1744178057014.png   2.2 Check LPCD_CALIBRATION_DONE_EVENT  07 BB (Little endian format) → Measured RSSI Value  Tomas_Parizek_4-1744178146251.png Tomas_Parizek_5-1744178162257.png   2.3. Check the GENERAL_ERROR_EVENT  00 23 (Little endian format) → Definition of the general error event → Error is : GPADC_ERROR, CLOCK_ERROR and XTAL_START_ERROR Tomas_Parizek_6-1744178213520.png Tomas_Parizek_7-1744178224958.png  
View full article
Step 1:  Disable the DCDC in settings (Valid for PNEV5190B and OM27642EVK) Write 0x21 into EEPROM PWR_CONFIG (address: 0x0000) This disables the DCDC. & selects that the VUP must be supplied with the same supply voltage as VBAT = VBATPWR. Do not enable RF afterwards, before the hardware is modified properly! Enabling the RF without supplying the VUP might kill the PN5190/PN7642! Step 2: Supply VUP = VBATPWR  Connect jumper J13 positions: 1-2: This supplies the VUP with VBATPWR = 3.3V Tomas_Parizek_0-1739277256705.png PN5190 EVK: Please note that for a final application using ULPCD, the "DC-DC" inductor (L2) has to be replaced by a zero resistor/short.  Tomas_Parizek_0-1752585917991.png   PN7642 EVK:  The OM27642EVK does not require any jumper settings (DC-DC is not used by default), the User must only disable DC-DC in EEPROM (address 0x0000, value 0x21) Then you can turn-on RF and perform ULPCD Tomas_Parizek_0-1752586235231.png   Please note that for a final application using ULPCD, the "DC-DC" inductor (L2) has to be replaced by a zero resistor/short.  Also, R8 shall be placed   
View full article
This might be convenient if the user wants to use NFC Cockpit on their device.  See the photo of PNEV5190BP EVK with the instructions.      Tomas_Parizek_2-1758172713000.png    1. Place R5 and R7, keep R6 open    2. Place R20, keep R19 open Note: This step depends on the voltage domain used in the external hardware. If R19 is placed -> 1.8V domain, if R20 is placed -> 3.3V domain.    3. Remove VBAT, VBAT_PWR, and VUP jumpers to disconnect the "internal" PN5190 located on the EVK    4. Connect the following SPI lines to external PN5190 (e.g., customer HW) SPI_CLK SPI_MOSI SPI_MISO SPI_CS NFC_IRQ GND Note: It is also necessary to disconnect the external PN5190 from the customer MCU. 5. Connect VEN to the external PN5190  NFC_VEN   Now, the external PN5190 HW should communitate with the MCU located in PNEV5190BP, and the NFC Cockpit can be used. The user should see that the blue LED is on. If the red LED is blinking, there is an issue, and the user should check the connections/supply. 
View full article
The PN7642/PN5190/PN7220 requires a calibration before the RF field is switched on for the first time with unloaded condition. "Unloaded" means: Without any additional metal in proximity of the antenna, except for the NFC reader components itself. During development of new readers, this calibration shall be done each time the antenna design, antenna matching, or EMC filter is modified. See a workflow of the Initial calibration for PN7642 done in NFC Cockpit.  PN7642_Initial_Calibration.png During this procedure, the RF Field is switched on for approx. 11 ms, and the calibration data is saved in the memory. Note: Please note that the registers and EEPROM addresses might differ for a different products. Always check the Datasheet for the used product. 
View full article