Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
LPC5536 MCAN RF0F 中断 你好 如果 IE:RF0FE 设置为 0,为什么会出现中断 (IR:RF0F)? 我正试图通过监控 IE 寄存器来解决这个问题,它正在从 0x3800000 变为 0x3800001,但第 3 位在任何时候都没有被设置。 顺祝商祺! 克里斯蒂亚诺-罗德里格斯 Re: LPC5536 MCAN RF0F Interrupt 你好@microcris kMCAN_RxFifo0FullFlag 的作用是避免 Rx FIFO 溢出。 谢谢! 爱丽丝 Re: LPC5536 MCAN RF0F Interrupt 你好,@Alice_Yang! 谢谢您的回答。 IE 注册器一切正常。我只是说没有设置 IE: RF0FE(它是位数 2 而不是位数 3),而且还有 IR: RF0F 被触发信号。如果是硬件问题,那就没关系。 每次接收到信息时,都会出现结果设置为 kMCAN_RxFifo0FullFlag 的 kStatus_MCAN_TxIdle 和 kStatus_MCAN_UnHandled,这实在有点恼人。 Re: LPC5536 MCAN RF0F Interrupt 你好@microcris 感谢您的提问。 标志 (IR:RF0F) 由硬件自动设置,与中断使能寄存器 IE:RF0FE 无关。IE 寄存器通知 CPU 执行中断处理程序。关于将 IE 第 0 位从 0 改为 1 的问题,请调试代码以检查该位被修改的位置。 谢谢! BR 爱丽丝
View full article
refresh policy problem S32K142 EVB I open project from file system then get this warning. How to Fix this warning???? Description Resource Path Location Type In Debug_FLASH configuration the refresh policy S32K142_EVB_JumpStart_Firmware does not match the project name S32K142_EVB_JumpStart_Firmware S32K142_EVB_JumpStart_Firmware S32K142_EVB_JumpStart_Firmware Refresh Policy Problem. Re: refresh policy problem S32K142 EVB A few years to late but i can confirm that for me, doing the last step only then cleaning and compiled fixed it all. I just got into the .cproject, searched all references to the old project name and changed them for the new project name. Then it compiled without these warnings.  I guess removing the warnings does the same as cleaning.  Re: refresh policy problem S32K142 EVB Hello, My colleague @BlackNight has an excellent blog on this topic. Please check it out for your solution! MCU on Eclipse | Eclipse Project ‘Refresh Policy’: Broken Incremental Build with External Make? Best regards, Mike Re: refresh policy problem S32K142 EVB Following the previous solution, I tried but did not solve the problem Re: refresh policy problem S32K142 EVB pointless Re: refresh policy problem S32K142 EVB I had the same problem after I copied an existing build configuration in S32DS 2018.R1 and delete the configuration gain in S32DS. The problem is that S32DS does not completely delete the reference to the configuration but only deletes its properties: Working configuration: <configuration configurationName="Release"> <resource resourceType="PROJECT" workspacePath="/Project_Name"/> configuration>‍‍‍‍‍‍‍‍‍ Deleted Configuration: <configuration configurationName="Debug_Release"/>‍ So what I did to solve the warnings is: Right click and delete all warnings in the console after opening the project Close the project Delete the unused configuration tag shown above in the .cproject file located in the project root folder This was of course after I had already deleted the built configuration in S32DS itself. Re: refresh policy problem S32K142 EVB As you say Xu zhao, this issue is not resolved in S32 Studio. When you duplicate a project S32 Studio fails to rename certain files and configurations. You have to review all Debug Configurations for your project (right click on project > Debug As > Debug Configuration) You will also have to review the Refresh Policy in each of your C/C++ Build configurations. Delete the wrong resources and add the proper ones Re: refresh policy problem S32K142 EVB hi, my IDE is S32 Design Studio for ARM Version: 2018.R1 Build id: 180815 also have this bad problem. always warning in problem console. I had check the prj names, it is sure correct. still not solved.... Re: refresh policy problem S32K142 EVB fix by S32DS ARM 2.0 version. thanks~ Re: refresh policy problem S32K142 EVB Hi,  there are different names for .launch xml files - located in project root -> Project_Settings\Debugger. Just rename these files  to met the project name:   On screenshot I already renamed the first two files. In my case there was extra _OOBE_ in filename.  Hope it helps.  Jiri 
View full article
VR5510 OTP設定の変更 こんにちは、 VR5510を使用してOTP設定を変更する際に問題が発生しました。テストモードに入ることができず、ご助力いただけないでしょうか。 手順は次のとおりです。 文書 AN13182 に従ってテストします。 5.1 デバッグモード/テストモードに入るに従って、VDDOTP電圧を設定すると、FS_STATES(0x18h)データは0x20、0x03として読み取られます。 表 1.FS_STATES によると、DBG_MODE ビットは 1 であり、デバッグ モードに正常に入ったことを示しています。 • デバッグモードに入った後、テストモードに入るには、I2C経由でテストモードキーのセットを送信する必要があります。これは、OTPレジスタにアクセスし、必要な設定に変更するために必要です。テストモードキーが受け入れられるまで、VDDOTPピンはハイレベルに保持する必要があります。 • 同じテストモードキーセットを、メインテストモードエントリレジスタ(M_TM_ENTRY、0x1Fh)とセキュリティテストモードエントリレジスタ(FS_TM_ENTRY、0x26h)の両方に同時に書き込む必要があります。以下のキーは、各レジスタに順番に書き込む必要があります。 – キー1: 11010101_10100111 – キー2: 10111000_11101110 – キー3: 00001111_00110111 3つのキーを16進数データに変換すると、次のようになります: key1: 0xD5, 0xA7 – キー2: 0xB8、0xEE – キー3: 0x0F、0x37 CRCはルックアップテーブル方式を用いて計算を行います。以下にCRCテーブルとルックアップテーブル関数を示します。 静的const uint8_t crc8_lookup[256] = { 0x00,0x1D,0x3A,0x27,0x74,0x69,0x4E,0x53,0xE8,0xF5,0xD2,0xCF,0x9C,0x81,0xA6,0xBB, 0xCD、0xD0、0xF7、0xEA、0xB9、0xA4、0x83、0x9E、0x25、0x38、0x1F、0x02、0x51、0x4C、0x6B、0x76、 0x87,0x9A,0xBD,0xA0,0xF3,0xEE,0xC9,0xD4,0x6F,0x72,0x55,0x48,0x1B,0x06,0x21,0x3C, 0x4A,0x57,0x70,0x6D,0x3E,0x23,0x04,0x19,0xA2,0xBF,0x98,0x85,0xD6,0xCB,0xEC,0xF1, 0x13,0x0E,0x29,0x34,0x67,0x7A,0x5D,0x40,0xFB,0xE6,0xC1,0xDC,0x8F,0x92,0xB5,0xA8, 0xDE,0xC3,0xE4,0xF9,0xAA,0xB7,0x90,0x8D,0x36,0x2B,0x0C,0x11,0x42,0x5F,0x78,0x65, 0x94,0x89,0xAE,0xB3,0xE0,0xFD,0xDA,0xC7,0x7C,0x61,0x46,0x5B,0x08,0x15,0x32,0x2F, 0x59,0x44,0x63,0x7E,0x2D,0x30,0x17,0x0A,0xB1,0xAC,0x8B,0x96,0xC5,0xD8,0xFF,0xE2, 0x26,0x3B,0x1C,0x01,0x52,0x4F,0x68,0x75,0xCE,0xD3,0xF4,0xE9,0xBA,0xA7,0x80,0x9D, 0xEB、0xF6、0xD1、0xCC、0x9F、0x82、0xA5、0xB8、0x03、0x1E、0x39、0x24、0x77、0x6A、0x4D、0x50、 0xA1,0xBC,0x9B,0x86,0xD5,0xC8,0xEF,0xF2,0x49,0x54,0x73,0x6E,0x3D,0x20,0x07,0x1A, 0x6C,0x71,0x56,0x4B,0x18,0x05,0x22,0x3F,0x84,0x99,0xBE,0xA3,0xF0,0xED,0xCA,0xD7, 0x35,0x28,0x0F,0x12,0x41,0x5C,0x7B,0x66,0xDD,0xC0,0xE7,0xFA,0xA9,0xB4,0x93,0x8E, 0xF8,0xE5,0xC2,0xDF,0x8C,0x91,0xB6,0xAB,0x10,0x0D,0x2A,0x37,0x64,0x79,0x5E,0x43, 0xB2,0xAF,0x88,0x95,0xC6,0xDB,0xFC,0xE1,0x5A,0x47,0x60,0x7D,0x2E,0x33,0x14,0x09, 0x7F,0x62,0x45,0x58,0x0B,0x16,0x31,0x2C,0x97,0x8A,0xAD,0xB0,0xE3,0xFE,0xD9,0xC4 }; uint8_t crc8_table(const uint8_t *データ, uint32_t 長さ) { uint8_t crc = 0xFF; while(len--) { crc = crc8_lookup[crc ^ *data++]; } crc を返します。 } データシート 23.I2C のデータ形式に従って、データと CRC チェック結果を配列にカプセル化します。 uint8_t key20_1[5] = {0x40, 0x1F, 0xD5, 0xA7, 0xA8}; uint8_t key21_1[5] = {0x42, 0x26, 0xD5, 0xA7, 0x24}; uint8_t key20_2[5] = {0x40, 0x1F, 0xB8, 0xEE, 0xEA}; uint8_t key21_2[5] = {0x42, 0x26, 0xB8, 0xEE, 0x66}; uint8_t key20_3[5] = {0x40, 0x1F, 0x0F, 0x37, 0x16}; uint8_t key21_3[5] = {0x42, 0x26, 0x0F, 0x37, 0x9A}; 3 つのキーをそれぞれ 2 つのレジスタに書き込みます。 VR5510_Write(key20_1);// W:0x20, 0x1F, (0xD5, 0xA7) VR5510_Write(key21_1);// W:0x21, 0x26, (0xD5, 0xA7) VR5510_Write(key20_2);// W:0x20, 0x1F, (0xB8, 0xEE) VR5510_Write(key21_2);// W:0x21, 0x26, (0xB8, 0xEE) VR5510_Write(key20_3);// W:0x20, 0x1F, (0x0F, 0x37) VR5510_Write(key21_3);// W:0x21, 0x26, (0x0F, 0x37) • テストモードエントリキーの送信に成功した後、M_TM_STATUS1(0x25h)レジスタのビット6とFS_STATES(0x18h)レジスタのビット15を読み出してテストモードステータスを確認します。両方のビットが1に設定されている場合、テストモードエントリ操作は成功です。 さらに2つのレジスタからデータを読み取る VR5510_Read(state_buf1, データ);// R:0x20, 0x25, (0x00, 0x0C) VR5510_Read(state_buf2, データ);// R:0x21, 0x18, (0x20, 0x03) FS_STATES(0x18h)のデータは0x20、0x03です。(表1に基づく)FS_STATES チェックでは、15 番目のビットが 0 であることが示されています。 M_TM_STATUS1(0x25h)のデータは0x00、0x0Cです。表2によると、M_TM_STATUS1の6番目のビットは0です。 テストモードに入ることができませんでした。 入力に失敗した場合、「5.2 デバッグモードでプログラム済みOTPを変更する」の手順に従ってOTP設定を変更しようとしました。まずレジスタを読み取り、次に新しいデータを書き込み、最後に再度読み取りました。しかし、データは変更されず、変更は失敗しました。 VR5510_書き込み(OTP1_R1_W); VR5510_Read(OTP1_R2_R、データ); VR5510_書き込み(OTP2_W1_W); VR5510_書き込み(OTP2_W2_W); VR5510_書き込み(OTP3_R1_W); VR5510_Read(OTP3_R2_R、データ); テスト モードに入ることができなかったのはなぜですか? また、どうすれば修正できますか? Re: VR5510 OTP 修改配置 ご質問がございましたら、以下のリンクからチケットを送信してください。このリンクはあなただけに表示されます。 家 Re: VR5510 OTP 修改配置 電話番号を残す Re: VR5510 OTP 修改配置 現在のチップはもう変更できないのでしょうか?AN13182ドキュメントに従ってテストと設定ができるのは空のチップだけです。テスト後、テスト時に使用した設定に従ってOTPが実行されます。OTP後は、それ以上の変更はできないということですか? Re: VR5510 OTP 修改配置 OTP がすでに実行されている場合、この出力は OTP 中に決定され、電源投入後に IIC 経由でレジスタを変更することはできません (これは無駄になります)。 OTPを自分で再作成するには、ソケットボードから空のチップ(A0バージョン)を取り出すしかありません。これが最も効果的な方法です。そうでなければ、非常に面倒な作業になります。 Re: VR5510 OTP 修改配置 購入したチップ(モデル:MVR5510AMDAHES)には、OTPが既にプログラムされています。BUCK3の電圧を変更する必要があります。I2Cを使って設定を変更することは可能ですか? Re: VR5510 OTP 修改配置 こんにちは: VR5510 用に独自の OTP を作成する予定ですか? こんにちは。現在お持ちの VR5510 の具体的なモデルを教えていただけますか? KITVR5510SKTEVM | VR5510 PMICプログラミングボード | NXPセミコンダクターズ 上記はOTPソケット用に特別に設計されたVR5510ボードです。これをOTPに使用すると便利だと思いますか?
View full article
K32L2A SWD 引脚 - 除非连接调试器,否则 MCU 无法正常运行 我有一个使用 K32L2A 的新设计,这是旧 Coldfirev1 MCF51QE32 部件的未分级设计。使用原型 PCB,软件在连接 PEMicro Cyclone 的情况下按预期运行,即使不使用该设备进行调试,只需启动设备,MCU 即可按预期运行我们的软件。 然而,当 Cyclone 与电路板断开连接时,MCU 似乎会短暂启动,然后自行关闭(不会按预期运行我们的软件,不确定它是否只是停止,或者是什么,因为我无法将 Cyclone 连接到调试,因为这会立即修复它!)。我们的设计在 SWDIO/SWCLK 线路上没有外部电阻,因为数据表提到这些电阻是由 K32L2A 内部提供的(MCF51QE 在 PCB 上有 10K 上拉电阻)。 尝试过的事情: - 在这两条线路上添加 10K 上拉电阻 - 问题仍然存在 - 将一根电线从 PCB 上取下,这样我就可以将导线接触到引脚,这样就可以解决问题,也就是说,当我用手指捏住连接到 SWDIO 引脚的导线并启动电路板时,MCU 可以正确启动并且我们的软件可以运行。它会一直运行,直到我移开手指。这与任一 SWD 引脚均可兼容。电容?我不知道!?! 在这些行上加一个小写字母似乎是一种黑客行为,显然我忽略了一些东西。 复位线上也没有外部电阻(疏忽)但这似乎不是问题,因为当我握住其中一个 SWD 引脚时 MCU 就会运行,而当我离开一个引脚时 MCU 就会失败。 想法、希望还是抱负?欢迎大家 🙂 干杯! 回复:K32L2A SWD 引脚 - 除非连接调试器,否则 MCU 无法正常运行 “在两条线路上都添加 10K 上拉电阻 - 问题仍然存在” SWD_DIO 具有内部上拉电阻。SWD_CLK 具有内部下拉。 猜测,重置时将两者都拉高可能看起来像是调试器时钟脉冲。手指等会拉下足够长的时间。 内部电阻相当高 Z 并且随温度而变化(20k 至 50k)。 我通常会添加自己的低 Z。 来自 K32L2A 的电气数据表: “虽然不需要上拉或下拉电阻 (SWD_DIO 具有内部上拉电阻,SWD_CLK 具有内部下拉电阻),建议使用外部 10 kΩ 上拉电阻以确保系统稳健性。这 还必须考虑上面提到的 RESET_b 引脚建议。”
View full article
MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Greetings! I am using the MPC5746C on a custom PCB with PEmicro Debugger. I am attempting to run an example SPI program provided by NXP, located at C:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.0\examples\MPC5746C\driver_examples\communication\spi_pal inside my local file system.  The pin assignments/connections on my custom board are inspired from the MPC5748G-LCEVB evaluation kit, but not exact. Hence, I changed the pin_mux and spi1/2 component configurations to be aligned with what our board supports and generated the Processor Expert code. The program builds. I also followed the instructions at the following webpage and modified the physical connections to align with our board: S32 SDK: SPI PAL MPC5746C When I run the program, inside main() the code calls SPI_MasterInit(): Inside SPI_MasterInit() the code calls DSPI_MasterInit(): Inside DSPI_MasterInit() the code calls DSPI_Set_MCR_Halt(): Finally, inside DSPI_Set_MCR_Halt(), when the program attempts to execute the first line inside the function, a Machine Check Interrupt (IVOR1) is raised. At this point the execution is paused in an infinite loop.  The cause of this issue is puzzling and my efforts to track it down have been unsuccessful. Is there any guidance that you can offer me to assist me solving this issue? When I run the equivalent example on the MPC5748G-LCEVB, it works fine. If it's helpful, here is what my MCSR register looks like: Thanks for your time. Kind Regards, Paul Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Thanks David. The issue was incorrectly configured clocks, which was not allowing the mode entry sequence to complete. Once I got that right I ended up just using the clock_manager inside Processor Expert to configure everything and initialized by calling the two functions below, which I learned about through some of the examples in the S32 SDK (the functions are in clock_MPC57xx.c). Just using the CLOCK_DRV_Init() processor expert function was not enough. Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Yes, the component configures ME setup, so it is it properly configured, it could be enough. Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Follow-up question: Instead of manually coding the Mode Entry module, can I just use the clock_manager component in Processor Expert? Isn't that the point of it, to do the Mode Entry leg-work? Or no? Thanks. Paul Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Hi David, I followed your advice and read up on the Mode Entry module in the reference manual. I have added some code in the Initialize_Components(void) function within main.c to enable the clocks and peripherals, aiming to transition the chip to RUN0 mode. The primary issue I'm encountering now is that when I write to the MC_ME_MCTL register to transition to RUN0 mode (with the KEY and then again with the inverted KEY), the program hangs after the second write to MC_ME_MCTL. I have attached my latest project for your reference and testing. I would appreciate any insights or suggestions you might have regarding this issue. Thank you very much for your help.  Below is a summary of changes I made to my project (and other observations) in light of the current state of the situation: I transitioned my configuration from the MPC5746_256 package to the MPC5746C_100 package, as the 100-pin package is what I'm using on my custom board The ADC1 MCR/MSR registers continue to show a value of 0x0 (I am not aiming to use ADC0, just FYI) I added a Power Manager configuration to my project, initializing it for DRUN mode, which appears to be the controller's default mode after RESET. My objective is to operate in RUN0 mode if possible, although the manual suggests the ADC should be operational in either DRUN or RUN0 mode I've also adjusted the clock settings, slowing down the FIRC to 8MHz and further dividing it to 1MHz for the FS80_CLK, which the ADC1 module uses. My concern was that a high clock speed might be contributing to the issue, so I reduced the clock speed to potentially increase the likelihood of proper functionality without adverse effects As an aside: I was able to successfully run the ADC and SPI examples on the MPC5748G-LCEVB without needing to manually configure the Mode Entry module. Any idea why this might be the case? - Paul Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code If I run this code on my board it goes to IVOR1 as well because ADC registers are not available because Mode Entry transition didn't happen and device is not clocked according the setting. Pay attention to Mode Entry module. Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Hi David, I am not sure what is going on but I have tried running multiple NXP example projects using the built-in function from the processor expert, and among all of them what I am seeing in common is when a function tries to access a module register (like MCR) it triggers the IVOR1 exception handler and won't return to finish executing the rest of the code. Here's an example function:  When the controller tries to execute the REG_BIT_SET32(&(base->MCR), ADC_MCR_PWDN(1u));, this is where the IVOR1 is raised and it won't execute. I still haven't figured out the issue with the SPI module from before, so I tried moving on to other modules but I'm facing the same obstacle. I've also tried commenting out the IVOR1 segments inside the startup files but instead of IVOR1, it just sends it up the chain to a different IVORn handler and the result is ultimately the same. Would it be possible for you to view my project or attempt to execute it on your end and see if the issue  persists (I've atttached a .zip)? I would greatly appreciate any additional insights you can offer. Thank You. Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code I see your point regarding a potential mismatch. However, inside the PE generated function "SPI_MasterInit()", it uses "DSPI_MasterInit()" so I am not sure how to disassociate the two... Additionally, I am encountering the same problem with the IVOR1 exception even when I change the module from SPI_2 to a DSPI module. I also tried using the DSPI peripheral driver component rather than the spi_pal component...same result. Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code OK, it does make sense now. Bus error during reading from SPI_2. I guess there is some mismatch between SPI_2 and DSPI_2 as these are different modules. Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Hi David, I ran the program again and realized that in the original screenshot I didn't capture the MCSRR0 register at the moment the exception is raised. Here is an updated screenshot taken at the proper time and including the MCAR register you requested. Thank you. Re: MPC5746C Machine Check Exception (IVOR1) w/ SPI Example Code Could you screenshot also MCAR register? Interesting value is stored in MCSRR0 register as it should be address of instruction causing an IVOR1 exception (machine check) and you have 0xFFFF_C000 what's reserved region within PBRIDGE_A memory space.
View full article
SPC5604 - How can I JTAG password lock ? Hello. I looking for some examples or documents for JTAG password lock in SPC5604. How can I JTAG password lock in SPC5604B ? Best Regards, SEAN SUNG Re: SPC5604 - How can I JTAG password lock ? Hello, Not sure here. I never tried it using CW. @stanish could you have a look at this? best regards, Peter Re: SPC5604 - How can I JTAG password lock ? Hello, Not sure what you mean. But if you are asking if SW can write to the shadow flash, then yes. Shadow flash is same as any other flash block, but used for configuration of device. Best regards, Peter Re: SPC5604 - How can I JTAG password lock ? Sorry, but there's another question. Can I directly inject the required configuration into the corresponding NVSCC0-1 and NVPWD0-1 register of censorship shadow flash through software injection? Re: SPC5604 - How can I JTAG password lock ? Hello, I am now encountering a problem, I am in the system initialization unlock erase and reprogram shadow flash (using the demo provided by your company), the startup process is Flash memory boot, censorship control register's config is SC == 55AA,CW !=55AA and I set a private password. Now the problem is that when the initialization is completed, when I enter the configured private password when debugging with CW 10.6, the following error will be reported, please help me answer the question of whether I should not directly operate the shadow flash during initialization. I hope you can help with this answer. Re: SPC5604 - How can I JTAG password lock ? Hello, You simply program censorship registers as described in reference manual: You will use common flash programming procedure as for any other flash. Best regards, Peter 回复: SPC5604 - How can I JTAG password lock ? How to write to the register NVPWD0 and NVPWD1 and NVSCI0 and NVSCI1? 回复: SPC5604 - How can I JTAG password lock ? https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5604B-Shadow- Flash-Reprogramming/ta-p/1119903, this answers can write shadow block success
View full article
S32M LIN スタックのコンパイル エラー S32DS 3.5 と S32M24 RTD 2.0.0 を使用しており、S32K1_S32M24X_LINSTACK_RTM_1_0_2_D2308_updatesite.zipをインストールしています。 マスターとスレーブの例をインポートし、mexファイルのバックスラッシュの問題を修正しました( )、そして、設定コードを生成しました。 どちらのプロジェクトもビルドされません。 スレーブコードに次のエラーがあります。 説明 Resource Path Location Type 'LinIf_Channel_State' undeclared (この関数で最初に使用) lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 520 行目 C/C++ の問題 'LINIF_IDLE' 未宣言 (この関数で最初に使用)。「LINIF_CODE」のことだったの?lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 520 行目 C/C++ の問題 フィールド 'lin_baudrate_adjusted_flg' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 199 行目 セマンティックエラー フィールド 'lin_max_frame_res_timeout_val' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 193 行目 セマンティックエラー フィールド 'lin_protocol_state' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 172 行目 セマンティックエラー フィールド 'lin_protocol_state' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 438 行目 セマンティックエラー フィールド 'lin_protocol_state' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 443 行目 セマンティックエラー フィールド 'lin_protocol_state' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 488 行目 セマンティックエラー フィールド 'lin_virtual_interface' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 128 行目 セマンティックエラー フィールド 'lin_virtual_interface' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 146 行目 セマンティックエラー フィールド 'lin_virtual_interface' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 176 行目 セマンティックエラー フィールド 'lin_virtual_interface' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 181 行目 セマンティックエラー フィールド 'lin_virtual_interface' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 302 行目 セマンティックエラー フィールド 'lin_virtual_interface' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 411 行目 セマンティックエラー フィールド 'lin_virtual_interface' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 489 行目 セマンティックエラー フィールド 'max_idle_timeout_cnt' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 528 行目 セマンティックエラー フィールド 'response_buffer_ptr' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 443 行目 セマンティックエラー フィールド 'response_length' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 438 行目 セマンティックエラー 関数 'OsIf_ResumeAllInterrupts' の暗黙宣言 [-Werror=暗黙の関数宣言] lin_commontl_proto.c/Lin_Master_S32M244_Example_DS/stacks/lin/src 1241 行目 C/C++ の問題 関数 'OsIf_ResumeAllInterrupts' の暗黙宣言 [-Werror=暗黙の関数宣言] lin_commontl_proto.c/Lin_Slave_S32M244_Example_DS/stacks/lin/src 1241 行目 C/C++ の問題 関数 'OsIf_SuspendAllInterrupts' の暗黙宣言 [-Werror=暗黙の関数宣言] lin_commontl_proto.c/Lin_Master_S32M244_Example_DS/stacks/lin/src 1172 行目 C/C++ の問題 関数 'OsIf_SuspendAllInterrupts' の暗黙宣言 [-Werror=暗黙の関数宣言] lin_commontl_proto.c/Lin_Slave_S32M244_Example_DS/stacks/lin/src 1172 行目 C/C++ の問題 make: *** [stacks/lin/lin_dal/src/subdir.mk:20:stacks/lin/lin_dal/src/lin_dal.o]エラー 1 Lin_Slave_S32M244_Example_DS C/C++ の問題 make: *** [stacks/lin/src/subdir.mk:36: stacks/lin/src/lin_commontl_proto.o]エラー 1 Lin_Master_S32M244_Example_DS C/C++ の問題 make: *** [stacks/lin/src/subdir.mk:36: stacks/lin/src/lin_commontl_proto.o]エラー 1 Lin_Slave_S32M244_Example_DS C/C++ の問題 make: *** 未完成の仕事を待っています...。Lin_Master_S32M244_Example_DS C/C++ の問題 make: *** 未完成の仕事を待っています...。Lin_Slave_S32M244_Example_DS C/C++ の問題 シンボル 'LinIf_Channel_State' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 520 行目 セマンティックエラー シンボル 'LINIF_IDLE' を解決できませんでした lin_dal.c/Lin_Slave_S32M244_Example_DS/stacks/lin/lin_dal/src 520 行目 セマンティックエラー マスター・コードのエラーは少なくなります。 説明 Resource Path Location Type 関数 'OsIf_ResumeAllInterrupts' の暗黙宣言 [-Werror=暗黙の関数宣言] lin_commontl_proto.c/Lin_Master_S32M244_Example_DS/stacks/lin/src 1241 行目 C/C++ の問題 関数 'OsIf_SuspendAllInterrupts' の暗黙宣言 [-Werror=暗黙の関数宣言] lin_commontl_proto.c/Lin_Master_S32M244_Example_DS/stacks/lin/src 1172 行目 C/C++ の問題 これらのエラーはどのように解決できますか? Re: S32M LIN スタックのコンパイル エラー ワークスペースから両方のプロジェクトを完全に削除してから、Lin_SlaveプロジェクトとLin_Masterプロジェクトを再インポートしました。コンフィギュレーターを開く前に、元の投稿で説明したLDFソース行のバックスラッシュの問題を修正しました。 その後、コンフィギュレーターを開き、コードを更新して、無事にビルドすることができました。 コンフィギュレーターのこの行が、このコードのすべてのバージョンで一貫して壊れているのはなぜですか?S32K118の実装でも同じ問題があります。 Re: S32M LIN スタックのコンパイル エラー マスターコードとスレーブコードのためにlin_commontl_proto.cにインクルードを追加する必要がありました。 #include 「OsIf_Internal.h」 マスターコードはビルドされますが、スレーブコードにはまだエラーがあります。 1. LINIF_IDLEが定義されていない 2. stacks/lin/lin_dal/src/lin_dal.c:520:23:エラー: 'LinIf_Channel_State' 未宣言
View full article
S32K3 RTD 5.0.0 - LPUART - 当指示“结束传输”时区分 TX 和 RX? 我正在为 S32K344 处理器编写一些板支持软件,与 S32K3 RTD 5.0.0 配合使用,特别是使用 Lpuart_Uart_Ip 进行全双工异步(中断驱动)发送和接收操作。 问题:当接收到带有事件 LPUART_UART_IP_EVENT_END_TRANSFER 的回调时,似乎没有直接的方法来区分该回调是与未完成的 TX 还是未完成的 RX 操作相关联。(此事件由两者共同产生。) 检查 Lpuart_Uart_Ip.c 后实施时,我已确定了一种在我的用例中消除歧义的有点复杂的方法。具体来说: 我会跟踪我是否期待即将发生的 RX‘结束传输’事件。我预计在以下情况下 RX‘结束传输’事件即将发生: 1) 我收到了LPUART_UART_IP_EVENT_RX_FULL事件的回调,并且 2) 我没有在该回调中将接收缓冲区重置为非零大小,例如通过 Lpuart_Uart_Ip_SetRxBuffer()。 3) 我尚未收到指示“结束传输”事件的预期回调。 当我预期即将发生 RX“结束传输”事件时,我假设回调是针对未完成的 RX 操作。 当我在其他条件下收到“结束传输”回调时,我假设该回调是针对未完成的 TX 操作。 也许我遗漏了一些东西——有没有更好的方法来消除歧义?其他 RTD 实现有单独的 RX 和 TX 回调,但这里的情况并非如此。我的建议是为 RX 和 TX 设置单独的“结束传输”事件类型枚举值,但我意识到对 API 的这种更改不会向后兼容,并且可能无法在下一个主要 RTD 版本之前实施(例如6.0.0)
View full article
S32K312 PLL_LOL 问题 你好,恩智浦、 我们发现 S32K312 将在进行 (ESD) 空气放电 ±15kV 测试时 RESET。我们发现 RESET 的原因是 PLL_LOL。然后我们使用恩智浦 S32K312EVB-Q172 进行同样的测试,它也会 RESET。 我们尝试更改 GM_SET 寄存器以提高晶体分歧强度,但没有任何改善。而且我们尝试将 DCMRWP3 [9] 设置为 1,当 PLL_LOL 时 S32K 不会 RESET,但是 mcu 会停止,只有 RESET 才能恢复。 在进行 ESD 测试时,我们需要 S32K3 保持运行。CPU 时钟能否在 PLL_LOL 时切换到 FIRC?您能给我一些建议吗? Re: S32K312 PLL_LOL Problem 嗨,丹尼尔 谢谢,禁用自动液位控制器可以解决这个问题。 Re: S32K312 PLL_LOL Problem 更大功率振荡器是什么意思? 您是否禁用了自动电平控制器(FXOSC_CTRL[ALC_D] = 1)? BR,丹尼尔 Re: S32K312 PLL_LOL Problem 你好,我是@danielmartynek、 感谢您的答复。CMU 已禁用,我确信 RESET 原因是 PLL 失锁。当 PLL LOL 时,MCU 将 RESET。当将 DCMRWP3 [9] 设置为 1 时,mcu 不会 RESET,而 PLL 哈哈但是 mcu 会停止运行。因此,当 PLL 哈哈时,我们无法将系统时钟改回 FIRC。我们尝试用更高功率的晶振取代晶振,看起来更好。 Re: S32K312 PLL_LOL Problem 你好@郑建飞1、 您确定 FXOSC 是导致 PLL 失锁的原因吗?你启用了 FXOSC 时钟监测吗? 可能只是 PLL 的问题。最后一英里调节器是否启用? 您可以尝试在中断中将系统时钟改回 FIRC。 mux_0_csc[safe_sw] = 1 此致, 丹尼尔
View full article
周期中断定时器 我正在使用时钟频率为 40MHz 的 PIT,而我正在使用那个 PIT 来发送其他函数 abc () 的触发信号,它必须在 400kHz 时触发,但是当我尝试将频率设置为 80kHz 以上时,PIT 的回调没有收到触发信号,最终函数 abc () 没有收到触发信号。 我的问题是,那是有极限的,我们使用 PIT 不能超过 80kHz 左右,还是我需要激活微控制器中的某些东西才能超过 80khz 的触发信号或其他东西? 微控制器:- S32K344 T-172 谢谢! Re: Periodic Interrupt Timer 您好, 我想现在我不会再提供任何意见了。你有两个外设,都会产生中断。在每个中断回调中,都会执行一些计算。我怀疑是中断优先级、延迟和持续时间导致了您所观察到的问题。 例如,尝试使用引脚拨动测量每个中断的持续时间。此外,还要检查中断的优先级。如果两者设置为相同级别,请记住 eMIOS 的 IRQ 编号低于 BCTU,因此优先级更高。再加上频率较高,ISR 执行时间可能较长,这可能导致 BCTU 中断延迟甚至错过。 BR, Petr Re: Periodic Interrupt Timer Namste@PetrS 是的,我明白你的意思。 但是 好吧,让我再试一次。 我正在使用Emios_Gpt触发信号算法中的一个计算,而BCTU用于触发信号同一算法中的另一项计算。 现在,当我想以 20kHz 的频率 (50uSec) 运行 BCTU 回调触发信号时,我能做到,但是当我以 114kHz 或更低的频率触发 Emios_Gpt 时。 但是当我尝试以更高的频率触发 Emios_Gpt 的回调时,BCTU 接收触发信号的频率较低。 当我将 Emios_Gpt 的频率提高到 80kHz 以上时,PIT 也发生了同样的情况。 我不明白的原因是,如果它们是单独的外设,为什么会相互干扰。 谢谢  petrS Re: Periodic Interrupt Timer 您好, 我不太清楚您的应用程序设计。如何使用外围设备,在何处使用软件或硬件触发信号。BCTU 可以由 emiOS 中的硬件触发,因此不应丢失触发信号。PIT 没有输入触发信号,可以由 SW 启动/停止。因此,如果您使用 SW 启动,那么 SW 延迟也同样适用。 BR, Petr Re: Periodic Interrupt Timer Namste @PetrS 感谢您的答复和建议。 在这里,我尝试使用Emios_Gpt来解决这个问题,我可以在其中以更高的频率触发信号abc()函数。 但是我遇到了一个新问题:-当我以更高的频率触发 Emios_Gpt 模块时,可用的 BCTU 和 PIT 模块没有收到触发信号。 但当 EMIOS_Gpt 频率较低时,BCTU 和 PIT 都能正常工作。 这里的 BCTU 和 PIT 使用了 EMIOS_0。 EMIOS_1 已用于 EMIOS_Gpt 模块。 在这里,我更改了优先级,但仍然没有效果。 有没有什么办法可以让我把它短路? Re: Periodic Interrupt Timer 您好, 看来这可能是由于 CPU 或中断处理的限制造成的,而不是 PIT 本身。在高频情况下,CPU 可能跟不上中断速率。 频率为 80 kHz 时,中断周期为 12.5μs. 这样 CPU 就有更多时间处理中断。在 400 kHz(2.5 µs)的频率下,CPU 可能会不堪重负,尤其是在 ISR 没有优化的情况下, 。 以下是一些建议: - 优化 ISR(保持简短)。 -如果可能,使用硬件触发信号(如 DMA 或计时器输出)来实现功能。 - 检查中断优先级。 - 尝试为项目设置更高的代码优化级别 BR, Petr
View full article
S32K146 - MBDT - 运行时数据存储& 在电源循环期间保留。 亲爱的恩智浦支持团队 希望这条信息能找到您,祝您一切安好。 我目前正在做一个涉及 S32K146 MCU 的项目,我正在使用 Simulink 来处理 EEPROM 操作。我在数据保留方面遇到了一些问题,一直无法解决,非常希望得到您的指导。 在我的设置中,我试图使用"Flash_EEEWrite" 块将数值存储到 EEPROM 中。我正在轮换重复序列块中的值,并在初始化"Flash_Config" 后写入这些值。为确保正确初始化,我还在执行任何写入操作前添加了 100 毫秒的延迟。 不过,在电源循环后,我写入的值不会被保留。以下是我的观察结果: 当 FLASH_EEEWrite 块的数据类型设置为 uint32_t 时,读回的值始终为 7fff(十六进制)。 当设置为 uint8_t 时,返回值为 82(十六进制)。 无论输入什么,这些值都是恒定的,并不反映我编写的值。 我不确定问题是出在 EEPROM 的配置上,还是出在我使用 Simulink 模块的方式上,又或者是对 FLASH_EEEWrite 模块在这种情况下如何工作的误解上。 我附上了我正在使用的 Simulink 模型,以帮助更清楚地说明设置。 您能否深入了解可能出现的问题,或者我应该遵循的任何建议步骤,以确保在电源循环期间可靠地进行EEPROM写入和保留? 非常感谢你们的时间和支持。如果您能提供任何帮助或建议,我将不胜感激。
View full article
IMX8M MiniのMIPI-CSIプレスリリース、製品ニュースパイプラインが動作しない こんにちは、チームの皆さん メディア パイプラインを構成しようとしたときに、どうしても /dev/media0 ノードをユーザー空間に表示できません。私たちのユース CASEでは、Yoctoビルドを備えたカスタム統合ボードで Compulab IMX8M Mini SOM を使用しています。Allied ビジョン カメラを同社の Alvium CSI2 ドライバと統合しようとしています。 主な基本的な質問: カーネルとデバイス ツリーが正しく設定されていれば、パイプラインが正しく構成されていれば /dev/media0 ノードは引き続き表示されますか?または、パイプラインを正常に開始するには、ドライバをロードする必要がありますか?いずれにしても、何をしても media0 ノードは表示されCANません。 起動時には、ボードのセットアップによりカメラがまだ使用可能になっていません。ユーザー空間に入ったら(電源レギュレータが設定され、カメラの準備が整った後)、ドライバをこの出力に再バインドします。 root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# ./RebindCamera.sh AVT カメラ ドライバを再バインドしています... ./RebindCamera.sh:7行目: echo: 書き込みエラー: そのようなデバイスはありません [ 43.335322] avt_csi2 0-003c: avt_probe[5107]: /usr/src/debug/avt-csi2/1.2.0+git/avt-csi2.c [ 43.344799] avt_csi2 0-003c: avt_probe[5147]: パワーダウンGPIOが定義されていません [ 43.351676] avt_csi2 0-003c: avt_probe[5164]: devm_gpiod_get_optional(dev, "reset-gpios" が成功しました [ 43.360713] avt_csi2 0-003c: avt_probe[5171]: fwnode_property_present が mipi_csi を見つけられませんでした [ 43.369373] avt_csi2 0-003c: avt_probe[5188]: bcrm_wait_timeoutが見つかりません。デフォルト値を使用してください [ 43.377842] avt_csi2 0-003c: avt_probe[5191]: bcrm_wait_timeout が 3000ms に設定されました [ 43.385046] avt_csi2 0-003c: avt_csi2_check_mipicfg[4586]: ep_cfg.bus.mipi_csi2.num_data_lanes1 [ 43.393965] avt_csi2 0-003c: avt_csi2_check_mipicfg[4588]: v4l2_fwnode_ep.nr_of_link_frequencies2 [ 43.402965] avt_csi2 0-003c: avt_csi2_check_mipicfg[4593]: v4l2_fwnode_ep.link-frequencies0 値 445500000 [ 43.412824] avt_csi2 0-003c: avt_csi2_check_mipicfg[4593]: v4l2_fwnode_ep.link-frequencies 1 値 891000000 [ 43.422688] avt_csi2 0-003c: avt_probe[5213]: powerdown-gpios powerdownが定義されていません [ 43.430332] avt_csi2 0-003c: avt_probe[5228]: reset-gpios が定義されていません [ 43.436726] avt_csi2 0-003c: avt_reset[2080] [ 43.443043] avt_csi2 0-003c: wait_camera_available[2025]: カメラのシャットダウンを待機しています... [ 44.648643] avt_csi2 0-003c: wait_camera_available[2033]: カメラがI2C転送に応答するのを待っています... [ 45.269281] kauditd_printk_skb: 15 個のコールバックが抑制されました [ 45.269292] 監査: タイプ=1334 監査(1723754849.880:26):プログラムID=21 オペレーション=UNLOAD [ 46.664540] avt_csi2 0-003c: wait_camera_available[2054]: ハートビートがサポートされています。ハートビートがアクティブになるのを待っています。 [ 49.878985] avt_csi2 0-003c: wait_camera_available[2064]: ハートビートがアクティブ [ 49.949573] avt_csi2 0-003c: read_cci_registers[748]: regmap_bulk_read(camera->regmap8, cci_cmd_tbl[CCI_REGISTER_LAYOUT_VERSION ].アドレス ret 540 [ 49.969505] avt_csi2 0-003c: cciレイアウトバージョンb: 0x00000100 [ 49.975362] avt_csi2 0-003c: cciレイアウトバージョンa: 0x00010000 [ 49.981170] avt_csi2 0-003c: avt_probe[5285]: read_cci_registers が成功しました [ 49.989267] avt_csi2 0-003c: avt_probe[5302]: bcrm_version_check が成功しました [ 49.996951] avt_csi2 0-003c: bcrm_get_write_handshake_availibility[704]: BCRM書き込みハンドシェイクがサポートされました! [ 49.996975] avt_csi2 0-003c: カメラALVIUM 1500 C-501c NIRを発見 [ 50.014014] avt_csi2 0-003c: avt_probe[5315]: ファームウェアバージョン: 0.6.0.8c98 ret = 0 [ 50.024773] avt_csi2 0-003c: gcprmのバージョンを修正 [ 50.029887] avt_csi2 0-003c: avt_probe[5353]: INIT_WORK(&camera->bcrm_wrhs_work, bcrm_wrhs_work_func); [ 50.046953] avt_csi2 0-003c: avt_get_sensor_capabilities[4409]: csiクロック [ 50.046953] カメラ範囲: 40000000:750000000 Hz [ 50.046953] dts リンク周波数数 2 [ 50.046953] dts link_frequencies[0] 445500000 Hz [ 50.103673] avt_csi2 0-003c: avt_get_sensor_capabilities[4450]: カメラから読み取ったCSIクロック: 443750000 Hz [ 50.113207] avt_csi2 0-003c: avt_get_sensor_capabilities[4454]: 最小解像度と最大解像度を取得する [ 50.128752] avt_csi2 0-003c: avt_init_avail_formats[1840]: MEDIA_BUS_FMT_UYVY8_2X8/V4L2_PIX_FMT_UYVY/MIPI_CSI2_DT_YUV422_8Bを追加 利用可能な形式のリスト -1 - 1 [ 50.152546] avt_csi2 0-003c: avt_init_avail_formats[1841]: MEDIA_BUS_FMT_UYVY8_1X16/V4L2_PIX_FMT_UYVY/MIPI_CSI2_DT_YUV422_8を追加 B 利用可能な形式のリスト -1 - 1 [ 50.167322] avt_csi2 0-003c: avt_init_avail_formats[1842]: MEDIA_BUS_FMT_YUYV8_1X16/V4L2_PIX_FMT_YUV422P/MIPI_CSI2_DT_YUV42を追加 2_8B 利用可能な形式のリスト -1 - 1 [ 50.182333] avt_csi2 0-003c: avt_init_avail_formats[1843]: MEDIA_BUS_FMT_YUYV8_2X8/V4L2_PIX_FMT_YUYV/MIPI_CSI2_DT_YUV422_8Bを追加 利用可能な形式のリスト -1 - 1 [ 50.197003] avt_csi2 0-003c: avt_init_avail_formats[1844]: MEDIA_BUS_FMT_VYUY8_2X8/V4L2_PIX_FMT_VYUY/MIPI_CSI2_DT_YUV422_8Bを追加 利用可能な形式のリスト -1 - 1 [ 50.211670] avt_csi2 0-003c: avt_init_avail_formats[1849]: MEDIA_BUS_FMT_RGB888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.226343] avt_csi2 0-003c: avt_init_avail_formats[1850]: MEDIA_BUS_FMT_RBG888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.241008] avt_csi2 0-003c: avt_init_avail_formats[1851]: MEDIA_BUS_FMT_BGR888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.255682] avt_csi2 0-003c: avt_init_avail_formats[1852]: MEDIA_BUS_FMT_RGB888_3X8/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.270271] avt_csi2 0-003c: avt_init_avail_formats[1856]: MEDIA_BUS_FMT_SGRBG8_1X8/V4L2_PIX_FMT_SGRBG8/MIPI_CSI2_DT_RAW8 t を追加 o 利用可能な形式のリスト 1 - 1 [ 50.284685] avt_csi2 0-003c: avt_init_avail_formats[1863]: MEDIA_BUS_FMT_SGRBG10_1X10/V4L2_PIX_FMT_SGRBG10/MIPI_CSI2_DT_RAWを追加 10 利用可能な形式のリスト 1 - 1 [ 50.320636] avt_csi2 0-003c: avt_init_controls[3359]: コントラストコントロール (0x980901) はカメラでサポートされていません [ 50.357183] avt_csi2 0-003c: avt_init_controls[3359]: シャープネスコントロール (0x98091b) はカメラでサポートされていません [ 50.367712] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.369213] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.378025] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.412857] mxc_mipi-csi 32e30000.mipi_csi:登録されたセンササブデバイス: avt_csi2 0-003c [ 50.429900] avt_csi2 0-003c: カメラ avt_csi2 0-003c が登録されました [ 50.435940] avt_csi2 0-003c: -> avt_probe[5420]: sysfsグループが作成されました!(0) [ 50.446676] avt_csi2 0-003c: avt_probe[5442]: プローブ成功! [ 50.378025] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.412857] mxc_mipi-csi 32e30000.mipi_csi:登録されたセンササブデバイス: avt_csi2 0-003c [ 50.429900] avt_csi2 0-003c: カメラ avt_csi2 0-003c が登録されました [ 50.435940] avt_csi2 0-003c: -> avt_probe[5420]: sysfsグループが作成されました!(0) [ 50.446676] avt_csi2 0-003c: avt_probe[5442]: プローブ成功! root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# この時点では、カメラはセットアップされ、ストリーミングの準備ができていると想定されますが、フレームやデータをユーザー空間に取り込むことはできません。添付の TestStream.sh スクリプトを使用します。 root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# ./TestStream.sh ./TestStream.sh:1行目: amera: コマンドが見つかりません === カメラストリーミングコントロール === 1. 現在のカメラの状態を確認します。 [ 76.502724] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 ビデオキャプチャのフォーマット:[ 76.511315] mxc_mipi-csi 32e30000.mipi_csi:フォーマットが一致しません 幅/高さ: 0/0 [ 76.519017] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ピクセル形式: '' 分野: 任意 1行あたりのバイト数: 0 画像サイズ: 0 カラースペース: デフォルト Tra[ 76.537857] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 nsfer関数: デフォルト([76.548706] avt_csi2 0-003cにマップ: avt_core_ops_s_power[2156]+: on 0、camera->power_count 1 記録。709) YCbCr/HSVエンコーディング: デフォルト(ITU-R 601にマップ) 量子化: デフォルト (フルレンジにマップ) フラグ: 2. 利用可能なco[ 76.570719] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0をリストします コントロール: 3. 利用可能なフォームをリストします[ 76.581151] mxc_mipi-csi 32e30000.mipi_csi:フォーマットが一致しません ats: ioctl: VIDIOC_ENUM_FMT Ty[ 76.589396] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 pe: ビデオキャプチャ 4. 基本的なフォーマットを設定する: [ 76.611180] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.619262] mxc_mipi-csi 32e30000.mipi_csi:フォーマットが一致しません ピクセルフォーマット「UYVY」が無効です[76.625042] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0、camera->power_count 1 5. ストリーミング コントロールがあるかどうかを確認します。 [ 76.647122] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.655283] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 6. ストリーミングを有効にしてみます(コントロールが存在する場合)。 [ 76.672441] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.682040] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ストリーミング V4L2 コントロールが見つかりません [ 76.699454] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.708214] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 stream_enable コントロールが見つかりません 7. 取得開始を試みます(AVT 固有): [ 76.724226] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.733618] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 取得開始コントロールが見つかりません 8. 露出とゲインをチェックします(適切であることを確認します)。 [ 76.749702] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.759271] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 露出制御なし [ 76.775975] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.784748] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ゲインコントロールなし 9. コントロールが存在する場合は、適切な露出/ゲインを設定します。 [ 76.801835] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.810768] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 露出を設定できません [ 76.827415] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.837494] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ゲインを設定できません 10. 設定後にフレームをキャプチャしてみます。 ./TestStream.sh:47行目: タイムアウト: コマンドが見つかりません ❌ ストリーミング設定後もデータがありません 11. カーネル メッセージでストリーミング ステータスを確認します。 [ 76.784748] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 [ 76.801835] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.810768] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 [ 76.827415] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.837494] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# 現在、フォーマットが一致しないため、/dev/media0 ノードのプレスリリース、製品ニュース-ctl を介してリセットして変更するつもりです。しかし、それは表示されません。 以下は、DTS の関連する中核部分です。 // I2Cバス上でカメラを定義する &i2c1 { /* * I2C アドレス 0x21 に PCAL6416A GPIO エクスパンダーを定義します。 * 参照できるように、「gpio_expander」というラベルを付けます。 */ gpio_expander: pcal6416a@21 { 互換性 = "nxp、pcal6416"; <0x21> レジスタ <2> = !; gpio コントローラ; #gpioセル =; }; アルビウム: アルビウム@3c { 互換性 = "alliedvision、avt_csi2"; レジスタ =<0x3c> �; ステータス = "正常"; pinctrl-names = "デフォルト"; pinctrl-0 = <&pinctrl_alvium_clk>、<&pinctrl_alvium_gpio>; // Attollo デイカメラ用ハードウェア設定 電源 = <&dayCam_step2>; リセットgpios = <&gpio1 15 GPIO_ACTIVE_LOW>; クロック = <&clk IMX8MM_CLK_CLKO1>; クロック名 = "csi_mclk"; 割り当てられたクロック = <&clk IMX8MM_CLK_CLKO1>; 割り当てられたクロックの親 = <&clk IMX8MM_CLK_24M>; 割り当てられたクロックレート = <24000000>; ポート { レジスタ = <0>; alvium_mipi_ep: エンドポイント { リモートエンドポイント = <&mipi1_sensor_ep>; データレーン = <2>; リンク周波数 = /ビット/ 64 <445500000 891000000>; mipi-csi; }; }; }; }; &mipi_csi_1 { ステータス = "正常"; /delete-node/ ポート; ポート { mipi1_sensor_ep: エンドポイント@1 { レジスタ = <1>; リモートエンドポイント = <&alvium_mipi_ep>; データレーン = <2>; csis-hs-settle = <13>; csis-clk-settle = <2>; csis-wclk; }; csi1_mipi_ep: エンドポイント@2 { レジスタ = <2>; リモートエンドポイント = <&csi1_bridge_in>; }; }; }; &csi1_bridge { ステータス = "正常"; fsl、mipi モード; /delete-node/ ポート; ポート { csi1_bridge_in: エンドポイント { リモートエンドポイント = <&csi1_mipi_ep>; }; }; }; / { dayCam_step1: camPowerEnable { compatible = "レギュレータ固定"; レギュレータ名 = "dayCam-Power-Enable"; gpio = <&gpio_expander 5 GPIO_ACTIVE_HIGH>; アクティブハイを有効にする; レギュレータ常時オン; }; dayCam_step2: dayCamI2cEnable { compatible = "レギュレータ固定"; レギュレータ名 = "dayCam-i2c-Power-Enable"; vin-supply = <&dayCam_step1>; gpio = <&gpio4 26 GPIO_ACTIVE_HIGH>; アクティブハイを有効にする; レギュレータ常時オン; // startup-delay-us = <2600000>; // 100ms待つ }; }; ご協力やアイデアをいただければ大変助かります。
View full article
MPC5744P& Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 各位专家好, 我安装了 AUTOSAR MCAL 代码包 MPC574XP_MCAL4_0_RTM_2_0_2,但它无法在 MPC5744P 上运行。为了隔离这个问题,我注释掉了 main() 中的所有应用程序代码,代之以一个最小的测试用例: BoardInit(); GPIOInit(); CANInit(); 该测试代码(使用硬编码寄存器值,仅初始化寄存器地址)值得信赖--它已在多个 MPC5744P S32 项目中运行。然而,在 AUTOSAR 项目中,虽然调试器确认寄存器设置正确,但 CAN 外设仍无法运行。 问题 尽管有共同的品牌,MPC574XP_MCAL 代码包是否会与 MPC5744P 不兼容? 为什么测试代码在 AUTOSAR 环境下会失败,而在其他环境下却能正常工作? AUTOSAR 启动代码(如时钟初始化、MPU 配置或异常处理)是否会与 MCAL 或硬件冲突? 预先表示感谢。 Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 你好 以下是 SW 团队的反馈意见: 这个问题似乎是在启动时出现的,可能是存储 Can_ControllerStatuses、缓存等内容的内存区域出了问题。我看到这个例子附在这个代码包,软件包里,他们可以尝试运行它并与他们的启动进行比较。 请运行示例并与您的代码进行比较。 顺祝商祺! 皮特 Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 你好, Diab 版本是: Can_FlexCan_InitVariables 函数中的 Can_ControllerStatuses 值: Can_FlexCan_ChangeBaudrate 函数中的 Can_ControllerStatuses 值: 在设置 CTRL1 值之前,Can_ControllerStatuses的值相同 谢谢 Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 你好 以下是 SW 团队的反馈意见: 请按照发行说明进行操作,请确保此版本支持的 diab 版本是: 能否读取 Can_ControllerStatuses 并显示该结构中所有元素在某些点的值,如下所示: 像这样: 如 RM 所述,CTRL1 中的某些位可以在冻结模式下写入: 因此,在设置 CTRL1 值之前,请确保 CAN 控制器处于冻结模式,您可以通过寄存器 MCR 来检查这一点。 该设置和检查在函数 Can_FlexCan_ChangeBaudrate( 中进行。) 顺祝商祺! Peter Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 你好 我已将您的问题转给 SW 团队,因为我不熟悉 CAN 驱动程序。 一旦得到答复,我将向您提供最新信息。 顺祝商祺! Peter Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 我尝试了直接写入;成功了,我注意到问题出在名为"Can_ControllerStatuses[CAN_MAXCTRL_CONFIGURED]的全局结构数组" 中,直接写入该结构的任何成员都不会影响该数组,因为该数组应该保存各个 FlexCAN 控制器的当前状态/运行时配置、 在 Can_Flexcan.c 中的 Can_FlexCan_InitVariables 函数中初始化所有控制器的全局变量/状态、 该截图显示了向该结构成员写入 0 后的 1111 值! 为什么会这样?我使用 diab 编译器和 S32,这是我的项目附件,如果您能提供任何解决方案,请给予帮助。 Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 你好 对 CTRL1 寄存器的访问没有限制: 切换到汇编调试,检查内核上的指令执行情况,查看寄存器是否真的会被修改。还可以尝试通过调试器直接写入。 我相信,这里没有 HW 的问题。 要么是外设没有时钟而你试图写入,要么是 SW 根本没有执行对寄存器地址的写入。 该外设是否存在任何错误? 所有问题都在勘误表中有所说明。但我不认为问题出在 UC 上。我怀疑你是社工。 只需尝试通过调试器写入寄存器... 顺祝商祺! Peter Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 谢谢 Peter 的回答, 首先:我的开发板是 https://www.nxp.com/design/design-center/development-boards-and-designs/DEVKIT-MPC5744P 我下载了这些代码包:Autosar 版本 4.0.3 第二:我需要测试使用 CAN0 的 CAN 任务,它无法正常工作,因此我使用 EB tresos 生成了另一个配置文件; 查看生成配置的这一部分:Can_PBcfg.c文件: 配置 FlexCan 控制器 CTRL1 寄存器不受更改配置的影响, 截图中的情况 - 例如 - PSEG1 =2 PSEG2 =2 PROPSEG =5 RJW =2 ,但 CTRL1 寄存器中的值是 1(在 Can_Init 函数之后 - 在 Can.c 中 - 返回)。 在 Can_FlexCan_ChangeBaudrate 函数 - 在 Can_Flexcan.c 中的这一部分之后填充的数值- 在 Can_Init 函数中调用。 该外设是否存在任何错误? 是否有任何使用这些软件包操作CAN外设的解决方案? 先行致谢。     Re: MPC5744P & Autosar (MPC574XP_MCAL4_0_RTM_2_0_2) 你好 尽管有共同的品牌,MPC574XP_MCAL 代码包是否会与 MPC5744P 不兼容? 不。它完全兼容,并在 mpc574xp 设备上进行了测试。 AUTOSAR 启动代码(如时钟初始化、MPU 配置或异常处理)是否会与 MCAL 或硬件冲突? 不会,因为 MCAL 符合 AUTOSAR 标准。(根据 autosar 标准制定)。 为什么测试代码在 AUTOSAR 环境下会失败,而在其他环境下却能正常工作? 不确定。示例代码应在导入后立即运行。 尽管有共同的品牌,MPC574XP_MCAL 代码包是否会与 MPC5744P 不兼容? 请务必参阅代码包的版本说明。 因此,您可能使用的是 4.0 以外的 autosar。 顺祝商祺! Peter
View full article
#Cannot 使用 s32k396 评估板控制 fs26 pmic gpio1,2 你好,我目前正在使用 fs26 pmic 和 s32k396 评估板。 要知道,fs26 使用 spi 通信来控制多个状态或引脚,如 gpio、trk1,2 等。 我想激活 gpio 1 密码所以我发送寄存器命令 " sbc_fs26_WriteRegister(FALSE、0x11、0x0318);"-我使用的是 s32ds 实时驱动程序。 (我激活了 gpio1、gpio2、trk1、trk2) 我读取了 M_STATUS 寄存器,从中可以了解 fs26 引脚的状态。 但 gpio 1 引脚没有激活。 此外,我停用了"Sbc_fs26_WriteRegister(FALSE, 0x12, 0x0318);" - 停用所有引脚 但 gpio2 引脚没有停用。 因此,我想知道的是,我们不能使用 spi 通信改变 gpio1、gpio2 的状态吗? 根据数据手册,VCORE_PGOOD 信号与 GPIO2 有关。 最初制造 PMIC 设备时,此配置是否设置为默认配置? 除非使用 otp 配置,否则我们不能改变状态吗?(在 s32ds fs26 示例代码中没有改变状态的寄存器地址[除了 gpio 高、低电平],如 gpio 下拉、上拉)。 谢谢。 顺祝商祺! Re: #Cannot control fs26 pmic gpio1,2 with using s32k396 evaluation board 亲爱的 Hyun 欢迎您祝您愉快 致以最崇高的敬意 约瑟夫 Re: #Cannot control fs26 pmic gpio1,2 with using s32k396 evaluation board 感谢您抽出时间回答我的问题。致以最崇高的敬意 上帝保佑你 Re: #Cannot control fs26 pmic gpio1,2 with using s32k396 evaluation board 亲爱的 Hyun 感谢您提供产品编号。根据原理图,FS2633AMDE4AD 已填充。 根据所附的 FS2633AMDE4AD OTP 配置报告,GPIO 引脚被设置为输入。 请查看 S32K396 MCU 的附加软件。 https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER?currentTab=0&selectedDevices=S32K396 如需在 OTP 模式下启用 FS26,请参阅 FS26 完整数据表中的第 21 节。请下载FS26 产品页面的 "安全 "部分。 请注意,您需要与恩智浦签订有效的 NDA(保密协议),才能下载 FS26 数据表和其他机密文件。 如果您还没有保密协议但想签署一份保密协议,请在此处创建一张新票,恩智浦代表将指导您完成整个流程。 致以最崇高的敬意 约瑟夫 Re: #Cannot control fs26 pmic gpio1,2 with using s32k396 evaluation board 我使用的是 s32k396-bga-dc1 评估板。 可以用 s32 design studio 进行 otp 设置吗? 在下面的示例代码中,我看不到任何 otp 寄存器地址 是否有任何软件可以使用 otp 设置? Re: #Cannot control fs26 pmic gpio1,2 with using s32k396 evaluation board 亲爱的 Hyun 请分享完整的评估板产品编号或评估板的链接,这样我就可以查看你在开发板上使用的是哪个 FS26 版本。OTP 寄存器一旦刻录就不能更改。只有将 FS26 设置为 OTP 模式,才能测试 OTP 寄存器设置。 致以最崇高的敬意 约瑟夫
View full article
S32K144ボード間SPI通信における異常な動作 こんにちは、S32K144 ボードで SPI 割り込み通信を設定するときに問題が発生しています。このプロジェクトは PC33771B デバイスとの通信を目的としていますが、現時点では 33664EVB によって提供される一種のループバックになっています。 大部分は機能しているように見えますが、データが実際にバッファー内に保存される方法は奇妙です。5 バイトのメッセージがあり、一般的に次の順序に従います。 B5 0 0 0 B1 B2 B3 B4 LPSPI は単語単位で動作するので、これは正しいはずだと私は思います。しかし、何らかの理由で、常にその順序になるわけではありません。ボードを開始するとき、順序は次のようになる場合があります。 B1 B2 B3 B4 B5 0 0 0 そして時にはそれはただ: B1 B2 B3 B4 0 0 0 0 5番目のバイトが完全に失われます。 CAN を使用してデバッグできるように、小さなテスト コードを作成しました。必要なメッセージを SPI_1 に送信し、SPI_0 のバッファで終わるメッセージを受信します。何が起こっているかを確認するためにロジック アナライザーも使用しています。 最初のメッセージ: まず、 spi メッセージは S32K144 規則に従っているSO、5 番目のバイトは CRC になります。また、cmd で 4 番目のバイトにステップインしているので、都合よく 4 に設定しました。SPI_0 が再び準備完了するまで待っても、常にゼロが返されます。これは最初の場合にのみ発生します。 2番目のメッセージ: 最後のバイトはまったく表示されません。何らかの理由で失われたのかもしれませんが、その場合でも、MSB 順に並べられている場合、他の 4 バイトは最初のワードには含まれないはずです。 3番目のメッセージ: これは意図したとおりに機能しているようで、すべてのデータが取得され、予想どおりの順序で実行されます。落ち着いた後にすべてのメッセージで一貫して受け取るものなので、これは予想される順序だと思います。 これに関する問題は、必ずしも 3 番目のメッセージが適切であるとは限らず、5 番目または 6 番目のメッセージが適切である場合もあれば、5 番目のバイトがまったく表示されない場合や、2 番目のワードに表示される場合もあることです。一度正しく実行し始めると、一貫して動作します。この問題の原因について何かアイデアはありますか?コードと構成は以下の通りです。 void response420 ( zc_can_packet * パケット){ zc_spi_transfer(&spi_rx, &spi_to_can_packet); transfer_E2E_spi_packet(&E2E_spi, & can_to_spi_packet , &packet-> temp_data [0]); memcpy (&can_response. temp_data , spi_to_can_packet. rx_buffer , 8); zc_can_send(&can, &can_response, MAILBOX_0); } void zc_spi_transfer ( zc_spi_hw * hw_config, zc_spi_packet * パケット){ hw_config->転送されたパケット= パケット; hw_config-> hw_mode == MASTER の場合{ SPI_MasterTransfer (hw_config-> inst 、packet-> tx_buffer 、packet-> rx_buffer 、(packet-> message_bytes_length *NUMBER_OF_BITS_IN_BYTE)/hw_config-> master_config -> frameSize ); }それ以外{ SPI_SlaveTransfer (hw_config-> inst 、packet-> tx_buffer 、packet-> rx_buffer 、(packet-> message_bytes_length *NUMBER_OF_BITS_IN_BYTE)/hw_config-> slave_config -> frameSize ); } } void transfer_E2E_spi_packet ( E2E_spi_handler * E2E_spi, E2E_spi_packet * パケット, uint8_t * データ){ E2E_spi-> protector_handler -> protect_package (E2E_spi-> protector_handler 、データ、パケット-> packet_data . data_length_bytes 、 &(packet-> raw_spi_packet . tx_buffer [0]), packet-> packet_data . E2E_packet_id , packet-> packet_data . counter ); zc_spi_transfer(E2E_spi-> spi_handler 、&(packet-> raw_spi_packet )); packet-> packet_data . counter ++; //これは実際にはこのCRC形式では使用されませんが、この関数は複数のCRC形式で動作します if (packet-> packet_data . counter > E2E_spi-> protector_handler -> counter_overflow_number ){packet-> packet_data . counter = 0;} } response420 関数は、CAN コールバック自体によってフラグが立てられたときにメイン内部で呼び出される、CAN パケットを受信するための「コールバック」です。CAN 部分はそれほど重要ではありません。このバグは CAN がなくても発生するため、デバッガーでこのバグが表示された後、より多くの入力をテストできるように CAN を試しました。 一般的に、SPI_SlaveTransfer および SPI_Master 転送関数に見られるように、私は PAL を使用しています。これは PAL 構成です: SPI_1 設定: { .ボーレート = 2000000U、 .frameSize = 40U、 .bitOrder = SPI_TRANSFER_MSB_FIRST 、 .clockPolarity = SPI_ACTIVE_HIGH 、 .ssPolarity = SPI_ACTIVE_LOW 、 .clockPhase = READ_ON_EVEN_EDGE 、 .ssPin = 0, .transferType = SPI_USING_INTERRUPTS 、 .rxDMAChannel = 0U、 .txDMAチャネル = 0U、 .callback = NULL、 .callbackParam = NULL、 .拡張子 = NULL } SPI_0 設定: { .frameSize = 40U、 .bitOrder = SPI_TRANSFER_MSB_FIRST 、 .clockPolarity = SPI_ACTIVE_HIGH 、 .ssPolarity = SPI_ACTIVE_LOW 、 .clockPhase = READ_ON_EVEN_EDGE 、 .transferType = SPI_USING_INTERRUPTS 、 .rxDMAChannel = 0U、 .txDMAチャネル = 0U、 .callback = NULL、 .callbackParam = NULL、 .拡張子 = NULL } 同様の問題を発見した人はいますか? Re: Weird behavior in S32K144 board to board SPI communication わかりました。それはよかったです。@danielmartynekさん、本当にありがとう! Re: Weird behavior in S32K144 board to board SPI communication 素晴らしい。今は期待通りに動作しているようです。 HW はバイトスワッピングをサポートしていますが、SDK ドライバはサポートしていません。 Re: Weird behavior in S32K144 board to board SPI communication さて、コードを最大限に簡略化しました。 uint8_t送信データ[8] = {0x1, 0x2, 0x3, 0x4, 0x5, 0x6, 0x7, 0x8}; uint8_t受信データ[8]; lpspi_state_t lpspiState; int main (){ zc_clock_init(); zc_start_scheduler(); const clock_names_tクロック名[LPSPI_INSTANCE_COUNT] = FEATURE_LPSPI_CLOCKS_NAMES; clock_names_tクロック名 = クロック名[1]; lpspi_master_config_t spiConfig = { .bitcount = 8U、 .bitsPerSec = 20000000, .callback = NULL、 .callbackParam = NULL、 .clkPhase = 1, .clkPolarity = 0, .isPcsContinuous = true 、 .lpspiSrcClk = クロック名、 .lsbFirst = false、 .pcsPolarity = 0, .rxDMAチャネル = 0, .transferType = LPSPI_USING_INTERRUPTS、 .txDMAチャネル = 0, .whichPcs = 0, }; LPSPI_DRV_MasterInit(1, &lpspiState, &spiConfig); config_spi_pinout(spi_pinoutconfigs[1] .pinout ); 一方、 (1){ LPSPI_DRV_MasterTransfer(1, &送信データ[0], &受信データ[0], 8); zc_delay_milliseconds(1000); } 0を返します。 } これを実行してビットカウントを 8 にすると、結果は次のようになります。 間隔が問題だが、少なくともほぼ期待通りに動作する。 ビットカウント32の場合も同様です。 各ワード内のバイトは逆順にされます... 最後に、bitcount 64 で同じことを実行して何が起こるかを確認します。 同じことです。 これを uint8_t 配列ではなく word 配列に配置するとどうなるでしょうか? uint32_t送信データ[2] = {0x01020304, 0x05060708}; uint8_t受信データ[8]; lpspi_state_t lpspiState; int main (){ zc_clock_init(); zc_start_scheduler(); const clock_names_tクロック名[LPSPI_INSTANCE_COUNT] = FEATURE_LPSPI_CLOCKS_NAMES; clock_names_tクロック名 = クロック名[1]; lpspi_master_config_t spiConfig = { .bitcount = 64U、 .bitsPerSec = 20000000, .callback = NULL、 .callbackParam = NULL、 .clkPhase = 1, .clkPolarity = 0, .isPcsContinuous = true、 .lpspiSrcClk = クロック名、 .lsbFirst = false、 .pcsPolarity = 0, .rxDMAチャネル = 0, .transferType = LPSPI_USING_INTERRUPTS、 .txDMAチャネル = 0, .whichPcs = 0, }; LPSPI_DRV_MasterInit(1, &lpspiState, &spiConfig); config_spi_pinout(spi_pinoutconfigs[1] .pinout ); 一方、 (1){ LPSPI_DRV_MasterTransfer(1, ( uint8_t *) &送信データ[0], &受信データ[0], 8); zc_delay_milliseconds(1000); } 0を返します。 } 実際に動作します... SO、フレーム サイズ 8 で作業していない場合は、リトルエンディアンのワード単位で送信されるようです。エンディアンを変更する方法はありますか? Re: Weird behavior in S32K144 board to board SPI communication こんにちは@danielmartynek 私はすでにuint8_t配列を使用しています Re: Weird behavior in S32K144 board to board SPI communication こんにちは@rchust 、 tx_buffer をどのように定義しますか? ドライバは、8 ビット配列への 8 ビット ポインターを必要とします (LPSPI_DRV_MasterTransfer() 内)。 SO、CANそこに単語を渡す代わりにuint8_t[5] tx_bufferを使用できますか? よろしくお願い申し上げます。 Re: Weird behavior in S32K144 board to board SPI communication こんにちは@danielmartynek 、 8 ビット フレームでテストしたところ、バイトを順番に送信して正常に動作しました。しかし、問題が 2 つあります。 1 つ目は、8 ビット フレームの場合、ハードウェアがデータをバイト単位で分割することです。これはフレームの定義なので当然のことですが、FUTURE に問題が発生する可能性があります。PC33771 がそのような間隔のメッセージを受け入れるかどうかはまだテストしていません。そうなるはずですが、期待通りのものではありません。 2 番目 (まだ PC33771 でテストしていない理由) は、PAL ライブラリでは連続モードを true に設定できないことです。PAL ライブラリの「方法」Master_init は、それをLPSPI_DRV_MasterInit に渡す前に、これを false に設定します。 status_t SPI_MasterInit ( const spi_instance_t * constインスタンス、 const spi_master_t *config) { status_tステータス = STATUS_ERROR ; uint8_tインデックス = 0; /* LPSPI 上で SPI PAL を定義する */ #if (定義済み (SPI_OVER_LPSPI)) /*! @brief LPSPIのクロック名 */ const clock_names_t g_lpspiClock[LPSPI_INSTANCE_COUNT] = FEATURE_LPSPI_CLOCKS_NAMES if (インスタンス-> instType == SPI_INST_TYPE_LPSPI ) { lpspi_master_config_t lpspiConfig; lpspiConfig. bitsPerSec = config-> baudRate ; lpspiConfig.whichPcs = ( lpspi_which_pcs_t )config-> ssPin ; lpspiConfig. pcsPolarity = ( lpspi_signal_polarity_t )(!(bool)(config-> ssPolarity )); lpspiConfig. bitcount = config-> frameSize ; ( void )CLOCK_SYS_GetFreq(g_lpspiClock[( uint32_t )instance-> instIdx ] ,&lpspiConfig.lpspiSrcClk ) ; lpspiConfig. clkPhase = ( lpspi_clock_phase_t )config-> clockPhase ; lpspiConfig. clkPolarity = ( lpspi_sck_polarity_t )config-> clockPolarity ; lpspiConfig. lsbFirst = config-> bitOrder ; lpspiConfig. transferType = ( lpspi_transfer_type )config-> transferType ; lpspiConfig. rxDMAChannel = config-> rxDMAChannel ; lpspiConfig. txDMAChannel = config-> txDMAChannel ; lpspiConfig.callback = config- > callback ; lpspiConfig. callbackParam = config-> callbackParam ; lpspiConfig.isPcsContinuous = false ; /* このインスタンスにLPSPI状態構造体の1つを割り当てます */ インデックス = SpiAllocateState (LpspiStateIsAllocated、LpspiStateInstanceMapping、インスタンス-> instIdx 、NO_OF_LPSPI_INSTS_FOR_SPI); ステータス = LPSPI_DRV_MasterInit(インスタンス-> instIdx 、( lpspi_state_t *)(&LpspiState[index])、&lpspiConfig); } そうでない場合、 #endif 連続モードでテストする前に、すべてのライブラリを変更して、PAL の使用を停止し、DRV の方法の使用を開始する必要があります。SOて結果を更新しますが、8 ビット フレームで正しい順序で送信されるようです。ただし、40 ビット フレームではそれが実現されないのはまだイライラします。 Re: Weird behavior in S32K144 board to board SPI communication こんにちは@rchust 、 更新ありがとうございます。 tx_buffer に 8 ビット配列を CAN 使用しますか? Re: Weird behavior in S32K144 board to board SPI communication はい、いくつかテストした後、問題の根本を見つけることができました。 どうやら、CAN を使用していないときでもピンを設定していたようで、1 つのピンがマスターの CS と衝突したようです。どうして 1 つのことが別のことに終わるのかはわかりませんが、CAN 構成を削除した後、ほとんどの問題は解消されましたが、1 つだけ問題がありました。 何らかの理由で、8 ビットを超えるフレームでデータを送信すると、各ワード内のバイトが入れ替わります。0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 というデータを含む 64 ビット フレームを配置すると、0x04 0x03 0x02 0x01 0x8 0x07 0x06 0x05 になります。これは、SPI が内部的にワードで動作し、データをバイトごとに入力しているためと思われます。あるいはそれはパルライブラリかもしれません。 Re: Weird behavior in S32K144 board to board SPI communication こんにちは@danielmartynek 、 まずおっしゃる通り、私の IDE バージョン、SDK は 4.0.2 です。申し訳ありません。 私が示しているコードは CAN コールバックであり、CAN データを SPI バッファにコピーします。このコードは、カスタム ライブラリに組み込もうとしているためこのようになっていますが、実際には、CAN から読み取った内容を SPI (SPI1) に送信し、スレーブ (SPI0) が読み取った内容を CAN に送信するだけです。 CAN は 4 バイトを送信し、次に保護によって CRC である最後のバイトが追加されます。SO SPI は 5 を送信し、次に 5 を読み取り、その後 CAN はバッファの最初の 8 バイト内にあるものをそのまま送信します。バッファ自体は実際にはもっと大きいのですが、 SPI_MasterTransfer はバッファの最初の 5 バイトだけを送信します。 デバッグモードで確認したところ、 SPI_MasterTransfer 内では送信中の SPI は常に期待通りの順序で、ギャップなくバイトが送信されています。常に正しく(少なくとも一貫性を持って)送信されているように見える、SO 問題はスレーブの受信にあるようです。 マスター ブロッキングでも同じ問題が発生するようです。スレーブをブロックするとマスターの送信がブロックされるため、スレーブをブロックして確認することはできません。また、マスターとスレーブの両方のクロック極性を低く設定すると、多くの上位ビットが失われることもわかりましたが、まずは最初のメッセージの受信が機能しない問題に取り組みましょう。 Re: Weird behavior in S32K144 board to board SPI communication こんにちは@rchust 、 SDKs ではなく IDEs (3.6.2) を指定したようです。 リリース番号がわかれば、報告されたバグを確認CANます。 非ブロッキング方法を使用しているようですが、ブロッキング転送関数でテストできますか? コードはあまり読みやすくありません。 伝達関数の引数としてどのような値を置きますか? バッファをどうやって埋めるのですか? SPI 通信で観察されるギャップは、ドライバのオーバーヘッドによって発生します。ドライバは送信 FIFO に十分な速さでデータを入れることができません。8 ビット モードでは、ドライバは FIFO にデータを 1 バイトずつ書き込むため、連続した書き込みの間にレイテンシが発生します。この遅延は、SPI クロック速度が高くなると顕著になります。この問題を軽減するには、DMA を使用することをお勧めします。 よろしくお願いいたします。 ダニエル Re: Weird behavior in S32K144 board to board SPI communication こんにちは、ダニエル。 私のSDKは3.6.2です。私は 33664EVB ボードとその TPL を介して SPI を使用しており、チップ セレクトは使用していません。チャネルはそれぞれ SPI1_clock、SPI1_tx、TPL1_data、TPL1_clock です。混乱を避けるために、FUTUREの画像では名前を付けます。後者の 2 つを SPI0_rx と SPI0_clock に直接入力してテストしたところ、同じ結果が示されたことを指摘しておきます。 8 ビット モードでテストしたところ、次の結果が得られました。 最初のメッセージ: 4番目のメッセージ: 最初に気づくのは、最初の単語と 2 番目の単語の間にある大きなギャップです。より大きなメッセージでもテストしましたが、8 ビットを使用すると各単語間にギャップが生じます。周波数を下げてみると、ギャップは減少し、500kHz あたりで消えます。それでも、33664EVB および 3771 のアプリケーション ノートでは 2MHz の使用が推奨されており、一般的に速度が低いことは望ましくありません。 まったく同じではありませんが、問題は依然として似ています。最初は最後のバイトはまったく表示されませんが、次にそれが最初に表示され、その後に他のバイトが正しい順序で表示されます。また、8 ビットではデータが入力した順序で送信されますが、40 ビット モードでは信号内のデータが交換され、その後スレーブによって再度交換されることも指摘しておく価値があります。 ワード間の大きなギャップがなければ 8 ビットの方が望ましいのですが、それでも問題は発生します。8ビット500kHzの場合: 最初のメッセージ: 2番目のメッセージ: 3 番目のメッセージSO: これは 2 つの問題を示しています。1 つ目は私が言及しているスレーブによって読み取られたデータの不一致に関する問題であり、次に TPL のクロックを見ると 2 つ目の問題がわかります。TPL はパルス幅を 2MHz のように維持します。それがそのスピードが必要な理由の一つです。 Re: Weird behavior in S32K144 board to board SPI communication こんにちは@rchust 、 ドライバのバージョンを指定できますか? どのようなプロトコルを使用していますか?チップセレクト信号を使用していますか? ロジック アナライザのキャプチャでチャネルにラベルを付けることはできますか? LPSPI ハードウェアは 8 ビット フレームの連続送信をサポートしており、当社のソフトウェア ドライバーはこれと互換性があります。 8 ビットのデータを FIFO に配置することで、40 ビットのフレームを連続モードで送信CAN。 また、タイミングや信号の整合性に関連する潜在的な問題を排除するために、より低いボー レートで SPI 通信をテストしてみてください。 よろしくお願いいたします。 ダニエル
View full article
S32k146との1線式通信 こんにちは、 私がコーディングにS32k14x EAR SDK v08.6を使用していることをお知らせします モジュール(ステアリングロック)を持っています。これは、単線通信プロトコルで動作します。 そのため、モジュールとS32k146間の通信を有効にする方法を理解するのに苦労しています。以下は私のクエリです。 1.配線接続: 以上がモジュールの配線詳細です。したがって、信号フィードバックワイヤー(緑)、S32k146のどのピンにこれを接続でき、電流に基づいてその信号を埋め込み条件でどのように有効にできますか。 2.コミュニケーションの確立。 フォウリングは、ロックベンダーが提供する例です。どうすればこれを達成できますか 例: ホスト:コントローラー スレーブ:ステアリングロック ロック:スレーブが受信したときに、ホストはデータを送信します:0xAAAA(2バイト) 称賛します、それはステアリングロックをロックするためにロック舌を伸ばし、次にそれに応答します 現在のステータス。 オープン:ホストはデータを送信します:0x5555(2バイト)スレーブが受信したとき 称賛します、それはステアリングロックを開くためにロックタングを引っ張り、次にそれに応答します 現在のステータス。 奴隷が他の賞賛を受けた場合、それを無視し、何もしません。 誰かがこれについて私を助けることができますか。それは私にとって大きな助けになるでしょう。よろしくお願いいたします 日時:S32k146とのワンワイヤー通信 ご意見ありがとうございます。私はそのエラーを見落としていました。
View full article
S32K312 UART データの送信に失敗する こんにちは、uart + dma経由でデータを送信したいのですが、プログラムはRTD2.0.3で正常に動作します。しかし、RTD 4.0.0に転送すると、uartはデータを正常に受信することしかできず、常に転送側で「00」を送信しました。アップロードしたテストプログラムは、データを受信して送信し、0~16のような正しい修正データを受け取ることができますが、16個のゼロを送信できます。プログラムを確認するのを手伝ってください、ありがとう。
View full article
RW612漫游设置 亲爱的社区,我对漫游设置有几个疑问。我正在运行 wifi-wpa-supplicant 示例,并在连接到网络时启用漫游(wlan_set_roaming(1, 70))。我注意到,当 rssi 降至 70 以下时,它会触发低 rssi 事件并启动常规扫描而不是后台扫描。但是,如果我禁用 wpa_supplicant,它会执行后台扫描而不是常规扫描。为什么会有区别? WPA_supplicant 支持后台扫描(CONFIG_BGSCAN),但它(bgscan.c)似乎已从示例程序中删除。这有什么原因吗? 在我当前的设置中,仅当 RSSI 降至特定阈值以下时才会启动漫游。如何设置计划扫描以便在发现更强的接入点时启动漫游? 非常感谢并致以问候 回复:RW612漫游设置 SDK版本为24_12_00
View full article
MIMXRT1170-EVKB スレーブリンクサーバーのデバッグタイムアウト MIMXRT1170-EVKBのM4でスレーブセッションのデバッグセッションを実行する際に問題が発生しています。 マスター/スレーブプロジェクトのいくつかのサンプルは問題なく動作するので、。必要な設定がいくつか足りないと思います。 マルチコアプロジェクトのセカンダリプロジェクトの自動デバッグを有効にするチェックが入っています。 MCUXpresso IDEユーザーガイドで説明されているように、cm7 と cm4 用にSDKから2つの新しいCプロジェクトを生成しました。スレーブプロジェクトのフラッシュメモリマッピングを削除しました。スレーブプロジェクトのローンチの LinkServer Debugger セクションに " Attach only " を設定しました。 デバッグを実行すると、LinkServerがマスタープロセスを開始し、localhost:10989に接続して実行させ、LinkServerが2番目のターゲットを検出しますが、localhost:10990で毎回タイムアウトします。 最終起動シーケンスのエラー: MIコマンドを実行できませんでした: -target-select extended-remote localhost: 10990デバッガーバックエンドからのエラーメッセージ :localhost:10990 :接続がタイムアウトしました。 MIコマンドを実行できませんでした: -target-select extended-remote localhost: 10990デバッガーバックエンドからのエラーメッセージ :localhost:10990 :接続がタイムアウトしました。 注意: で boot_multicore_slave () を呼び出しています   IDEによって生成されたプロジェクト。 マルチコアのサンプルアプリケーションではこの呼び出しは見られません。時代遅れのAPIですか? 代わりにMCMGR_を使う必要がありますか? Re: MIMXRT1170-EVKB スレーブリンクサーバーのデバッグタイムアウト こんにちは、私の名前はパベルです。あなたのケースを支持しますが、解決策が見つかったと思います。コミュニティにあなたのステップを共有してくれてありがとう。 よろしくお願いいたします パベル
View full article
An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project Hi nxp, 我正在使用 S32 Design Studio for S32 Platform 3.5 编译“IPCF_Example_multi_instance_S32G274_M7_0” 例程,出现报错如下: 14:35:25 **** Incremental Build of configuration Debug_RAM for project IPCF_Example_multi_instance_S32G274_M7_1 **** make -j20 all Building file: ../generate/src/OsIf_Cfg.c Building file: ../src/main.c Building file: ../board/Siul2_Port_Ip_Cfg.c Building file: ../src/sample.c Building file: ../generate/src/Mpu_M7_Ip_Cfg.c Invoking: Standard S32DS C Compiler Invoking: Standard S32DS C Compiler arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c" Invoking: Standard S32DS C Compiler Invoking: Standard S32DS C Compiler arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/sample.d" -MT"src/sample.o" -o "src/sample.o" "../src/sample.c" arm-none-eabi-gcc "@generate/src/Mpu_M7_Ip_Cfg.args" -MMD -MP -MF"generate/src/OsIf_Cfg.d" -MT"generate/src/OsIf_Cfg.o" -o "generate/src/OsIf_Cfg.o" "../generate/src/OsIf_Cfg.c" Invoking: Standard S32DS C Compiler arm-none-eabi-gcc "@board/Siul2_Port_Ip_Cfg.args" -MMD -MP -MF"board/Siul2_Port_Ip_Cfg.d" -MT"board/Siul2_Port_Ip_Cfg.o" -o "board/Siul2_Port_Ip_Cfg.o" "../board/Siul2_Port_Ip_Cfg.c" arm-none-eabi-gcc "@generate/src/Mpu_M7_Ip_Cfg.args" -MMD -MP -MF"generate/src/Mpu_M7_Ip_Cfg.d" -MT"generate/src/Mpu_M7_Ip_Cfg.o" -o "generate/src/Mpu_M7_Ip_Cfg.o" "../generate/src/Mpu_M7_Ip_Cfg.c" ../src/main.c:20:10: fatal error: Clock_Ip.h: No such file or directory 20 | #include "Clock_Ip.h" | ^~~~~~~~~~~~ compilation terminated. In file included from ../generate/src/Mpu_M7_Ip_Cfg.c:46: D:/nxp/workspaceS32DS.3.5/IPCF_Example_multi_instance_S32G274_M7_1/generate/include/Mpu_M7_Ip_Cfg.h:39:10: fatal error: Mpu_M7_Ip_Types.h: No such file or directory 39 | #include "Mpu_M7_Ip_Types.h" | ^~~~~~~~~~~~~~~~~~~ compilation terminated. In file included from ../board/Siul2_Port_Ip_Cfg.c:43: ../board/Siul2_Port_Ip_Cfg.h:47:10: fatal error: Siul2_Port_Ip_Types.h: No such file or directory 47 | #include "Siul2_Port_Ip_Types.h" | ^~~~~~~~~~~~~~~~~~~~~~~ compilation terminated. ../src/sample.c:24:10: fatal error: ipcf_Ip_Cfg.h: No such file or directory 24 | #include "ipcf_Ip_Cfg.h" | ^~~~~~~~~~~~~~~ In file included from ../generate/src/OsIf_Cfg.c:44: D:/nxp/S32DS.3.5/S32DS/software/PlatformSDK_S32XX_2022_03/SW32_RTD_4_4_3_0_2_D2203/Base_TS_T40D11M30I2R0/include/OsIf_Cfg_TypesDef.h:87:6: error: #error "Software Version Numbers of OsIf_Cfg_TypesDef.h and OsIf_Cfg.h are different" 87 | #error "Software Version Numbers of OsIf_Cfg_TypesDef.h and OsIf_Cfg.h are different" | ^~~~~ compilation terminated. ../generate/src/OsIf_Cfg.c:93:6: error: #error "Software Version Numbers of OsIf_Cfg.c and OsIf_Cfg_TypesDef.h are different" 93 | #error "Software Version Numbers of OsIf_Cfg.c and OsIf_Cfg_TypesDef.h are different" | ^~~~~ make: *** [generate/src/subdir.mk:23: generate/src/Mpu_M7_Ip_Cfg.o] Error 1 make: *** Waiting for unfinished jobs.... make: *** [src/subdir.mk:23: src/sample.o] Error 1 make: *** [board/subdir.mk:20: board/Siul2_Port_Ip_Cfg.o] Error 1 make: *** [src/subdir.mk:23: src/main.o] Error 1 make: *** [generate/src/subdir.mk:23: generate/src/OsIf_Cfg.o] Error 1 "make -j20 all" terminated with exit code 2. Build might be incomplete. 14:35:26 Build Failed. 12 errors, 0 warnings. (took 552ms) 打开 Peripherals 配置出现问题显示如下: 已安装软件包如下: 麻烦可以帮忙看看什么原因不?谢谢! Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project Hi @Celeste_Liu  好的,我参考一下,谢谢! Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project Hello , 很高兴听到你的问题解决了。目前没有关于 S32G3 的双核启动的类似 AN13750.pdf 的文档,并且也没有发布此类文档的计划。这是因为 S32G3 的 GoldVIP 里面已经有双核启动了。我认为 AN13750 对你仍具有一定的参考价值,因为思路是一致的。以下这个案例可能会对你有所帮助:Solved: S32G399A-RDB3-Multi-core-boot-failed-following-AN13750 。 BR, Celeste Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project Hi @Celeste_Liu  貌似是我装多一个 RTD 包导致的,我重装软件后就可以了,谢谢!问下,是否有关于 S32G-VNP-RDB3 类似 AN13750.pdf 的文档?就是能在  S32G-VNP-RDB3 上实现 A 核和 M 核同时工作的状态? Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project Hello @DRAVE , 感谢你的提问。在编译项目之前,你似乎没有使用配置工具生成代码。请点击标记处的绿色按钮”更新源代码“,它会向项目中添加缺失的模块以使其正常工作。我们建议再次导入示例(删除之前的)并使用配置工具生成代码。 Best Regards, Celeste
View full article