Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
BFU660F 的 Spice 型号 您好, 能否提供 BFU660F 的香料型号? 谢谢! 约翰 Re: Spice Model for BFU660F 您好, ,我试图将此模型用于 Orcad PSpice,但似乎无法识别某些参数(例如:...M参数......),软件就会出错。请提供可在 orcad PSpice 中导入的 BFU660F 模型, ,谢谢您的支持 ,致以最诚挚的问候 Jonata Re: Spice Model for BFU660F 亲爱的艾丽卡 我想在 LTSPICE 中使用 2 发射器模型。 请发布 BFU660F 的 4 针型号。 顺祝商祺! 诹访仁 Re: Spice Model for BFU660F 嗨,艾丽卡、 谢谢你的香料模型。 您可以关闭此主题。 顺祝商祺! 约翰 Re: Spice Model for BFU660F 您好。 SPICE 模型附后。 希望对你有所帮助。 此致问候
View full article
IMX8MM With MEMS Oscillators Hello, I am trying to design a board using the IMX8M Mini, the design requires the use of MEMS oscillators. The datasheets are not very clear for this arrangement. IMX8MMIEC: 3.1.4 states that the RTC_XTALI is connected to an external oscillator and RTC_XTALO is connected to VDD_SNVS_0P8. There is then a statement about the XTALI pin (assumed to be 24M_XTALI) with no description of what to do with the XTALO pin, is this left unconnected? There are high/low thresholds given for the RTC clock but nothing given for the 24MHz clock, what are these thresholds? IMX8MMHDG: 4.4 mentions CLK1_P/N I cannot find any other reference to this pad in any other document. There is also a mention of CLKIN_1/2, the use of these pads is rather unclear with the only reference I can find is in the register definitions. I found this post (https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007077) from 2020 with NXP stating it can bypass the XTALI pad and apologising that it is poorly documented, It still isn't very clear. Should the 24MHz MEMS oscillator be connected to 24M_XTALI or CLKIN_1? If no crystals are used should "VDD_24M_XTAL_1P8" still be powered as this is omitted from section 2.1 in IMX8MMIEC? Thanks, Chris Re: IMX8MM With MEMS Oscillators @user1092  Happy to help, and thank you for your patience. Best regards, Salas. Re: IMX8MM With MEMS Oscillators Hi Salas, Thank you for clarifying and for your assistance. Chris. Re: IMX8MM With MEMS Oscillators Hello @user1092  Yes, I can confirm that the user's guide is correct, in that case you must tie RTC_XTALO to VDD_SNVS_0P8. This is from an internal discussion: Best regards, Salas. Re: IMX8MM With MEMS Oscillators Hi Salas, Thank you for the response, this is good news. Could you also please confirm the data sheet is correct in regards to the RTC. With RTC_XTALO being tied directly to VDD_SNVS_0P8, this sounds like a strange arangement and I would like to just confirm it is the correct arrangement. Thank you, Chris Re: IMX8MM With MEMS Oscillators Hello @user1092  Following up on your inquiry, we have reviewed the RTL and datasheet of the PAD provided by the IP vendor. Based on this review, we can confirm that the PAD supports the use of an external 24MHz reference clock. As per the IP datasheet: "In the case of external clock without physical crystal, a differential signal must be applied between PADI and PADO." This means that the external 24MHz clock must be a differential (complementary) signal applied to the XTALI and XTALO pins. Specifically: The signal should swing between 0V and 1.8V. When XTALI is at 0V, XTALO should be at 1.8V, and vice versa. To achieve this, you have two options: Use an oscillator that provides complementary differential outputs. Use a single-ended oscillator along with an external inverter to generate the complementary signal. Best regards, Salas. Re: IMX8MM With MEMS Oscillators Thank you @user1092  I will update to internal team and wait for their answer. Best regards, Salas. Re: IMX8MM With MEMS Oscillators Attached file after failed post removed it. Re: IMX8MM With MEMS Oscillators Hi Salas, "It sounds like a MEMS resonator on one instance (uses both XTAL pins) and an MEMS clock generator in the other (single ended input, only one). As far as using a resonator to replace a crystal, no one has asked this to my knowledge (been covering i.MX since around 2008). Will need to do some research on this." I'm unsure as to what they are referring here, but a MEMS resonator will not be used by us. To be honest, I had not heard of them and they don't seem too readily available. We will be using a single ended clock source. "Have to dig on using an external, single ended clock generator since some parts are not able to work with an external oscillator. I don’t recall off hand which one it was so I need to dig on that too." Please that would be appreciated. "Do you have any part numbers/dara sheets?" The part will most likely be DSC6001HI2B-024.0000, See attached for datasheet. Thanks, Chris. Re: IMX8MM With MEMS Oscillators Hello @user1092  From internal team: It sounds like a MEMS resonator on one instance (uses both XTAL pins) and an MEMS clock generator in the other (single ended input, only one). As far as using a resonator to replace a crystal, no one has asked this to my knowledge (been covering i.MX since around 2008). Will need to do some research on this. Have to dig on using an external, single ended clock generator since some parts are not able to work with an external oscillator. I don’t recall off hand which one it was so I need to dig on that too. Do you have any part numbers/dara sheets? Best regards, Salas. Re: IMX8MM With MEMS Oscillators Hello @user1092  Sure, I am waiting for an answer from internal team. I will let you know when any update. Best regards, Salas. Re: IMX8MM With MEMS Oscillators Hello Salas, After re-reading the datasheet there is a section (3.1.4) stating the XTALI can be fed from an external oscillator: This chip was chosen based on this statement. The documentation seems to be a bit of a mess, as it also states in this section that the RTC can only be connected to an external oscillator. However, section 3.4.2 discusses how to use the RTC with a crystal oscillator. You never answered the question about the CLKIN pins and whether these pins can be used if the XTALI pin cannot be driven from an external oscillator. I have spent almost a year developing this product, I do not want my time to have been wasted. The datasheet states XTALI can be driven from from an external oscillator. Please could you help, as I need a solution as soon as possible. Regards, Chris Re: IMX8MM With MEMS Oscillators Hello Salas, The design cannot use a crystal oscillator as it is used in a pressurised environment. You say the only recommended/validated way is with a crystal, this suggests it is possible but not tested. Could you provide information on if it is possible and if it is possible, how? Could you please provide some information on the purpose of the CLKIN_1/2 as there is little to no documentation about these pins. https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007077 suggests the pins can be used to feed the main clock instead of the crystal. Is this correct? Thanks Chris. Re: IMX8MM With MEMS Oscillators Hello @user1092  I hope you are doing very well. It is Only recommended and validated option - use crystal as recommended in official NXP document - Hardware Guide, sect.Table 12. Oscillator/Crystal recommendations. Best regards, Salas.
View full article
rt685 HiFi4、MCUからロードされたときの不安定なDSPコードの動作 こんにちは、 私は R685-AUD-EVK で実行されるオーディオ プロセッシング デモに取り組んでいます。私は入門リソースに従いました。MCU と DSP FW は主に SDKs の「audio_demo_bm」に基づいています。 MCU FW は、シンプルなユーザーインターフェースのために GPIOS の基本的な初期化のみを実行します。 DSP FW はオーディオ入出力用の I2S と DMA を初期化し、NXP アプリケーション ノートの 1 つで提案されている「トリプル バッファ」アプローチを使用してデータをバッファリングします。 実際のオーディオ プロセッシング関数は、1msのオーディオデータ(つまり、左48個、右48個のサンプルが受信されました。 オーディオ データのプロセッシングには、natureDSP ライブラリ関数が使用されます。 これまでのところ、MCU FW と DSP FW がビルドされ、デバッグ モードで実行されるとすべてが期待どおりに実行されますが、DSP FW が MCU からロードされるときに問題が発生しています (リリース ビルド、 DSP_IMAGE_COPY_TO_RAM = 1)。 オーディオ プロセッシング関数(ISRから呼び出される)が「.iram0.text」に配置されている場合(命令 TCM メモリ) DSP FW で例外が発生します。 xt-ocd プリント: エラー: 例外の詳細: exccause:0x0、excvaddr:0xff0042、epc:0x240205bc、epcdbg:20e022 関数が TCM 以外のメモリに配置されている場合、または DSP FW がデバッグ モードでロードされている場合、この問題は発生しません。 観察された問題を説明するために探すべきものはありますか? これはメモリの配置に関係しているのでしょうか? i.MX RT600 Re: rt685 HiFi4, erratic DSP code bahaviour when loaded from MCU @Omar_Anguiano返信ありがとうございます。 post_buildスクリプトは「.iram0.text」をコピーしないことがわかりました。セクションは MCU コードに含まれるバイナリ ファイルに含まれていたSO、実際の機能コードはメモリ内に存在しませんでした。 現時点では「デバッグ」モードで作業を継続CANため、アライメントの問題についてはこれ以上調べていません。 BRウィタリ Re: rt685 HiFi4, erratic DSP code bahaviour when loaded from MCU アライメントの問題が潜在的な問題となる可能性がありますが、デバッグ用にビルドされている場合はこの問題は発生しないことがわかります。 リリース用にビルディングする場合、コンパイラによっていくつかの最適化レベルが追加されるCANがあり、それが例の動作に影響を与える可能性があります。 MCUが.iram0.textを適切にコピーしない場合または整列させないと、DSP は無効な命令をフェッチし、結果として 0x0 (不正な命令) が発生する可能性があります。 よろしくお願いします、 オマール
View full article
Android 11 OS 上の iMX8M Mini のバックライト制御 こんにちは、NXP チームの皆様、 Android 11 OS 上の iMX8M Mini に取り組んでいます。 LVDS ディスプレイのバックライト制御用に、pwm バックライト ドライバ (pwm-bl.c) をコードに統合しました。 バックライトは pwm ノード ( /sys/class/backlight/backlight_grp/brightness) から適切に制御されますが、 Android UI バックライト スライダー経由では制御できません。 カーネルの変更: バックライト: backlight_grp { 互換性 = "pwm-backlight"; pwms = <&pwm3 0 50000>; /*デューティサイクル(ナノ秒)*/ enable-gpios = <&gpio1 0 GPIO_ACTIVE_HIGH>; /*LCD_SHUTDWN*/ 明るさレベル = <0 4 8 16 32 64 128 255>; デフォルトの明るさレベル = <7>; ポストPWMオン遅延ms = <10>; pwmオフ遅延ms = <10>; ステータス = "正常"; }; init.rc の変更点: setprop vendor.hw.backlight.dev "backlight_grp" chown システム システム /sys/class/backlight/backlight_grp/brightness chmod 0660 /sys/class/backlight/backlight_grp/明るさ この問題の解決にご協力いただけませんか。 ありがとうございます リティック Android グラフィックスとディスプレイ i.MX 8M | i.MX 8M ミニ | i.MX 8M ナノ Re: Backlight control on iMX8M Mini on Android 11 OS 何か変化はありますか? 私も同じ問題を抱えています Re: Backlight control on iMX8M Mini on Android 11 OS こんにちは。私も同じ問題を抱えています。問題は解決しましたか?
View full article
ASR、TTS、Transformerに関する推奨事項 こんにちは。i.MX 93 EVK でアプリケーションを開発しています。デバイス上で実行する際に比較的低いコンピューティング要件を持つ以下のものについて推奨事項をいただければ幸いです。私はi.MX 93 デュアルコア 1.7GHz を使用しています。 私は以下の推奨事項を探しています デバイス上で実行しながら適度な精度を備えた ASR エンジン。例: ささやく小さな TTSモデル Llama 3Bなどのデバイス上のトランスフォーマーモデル パフォーマンスの比較や推奨事項などの情報をいただければ幸いです。ありがとう Re: Recommendations for ASR, TTS and Transformer Laurent_P さん、Whisper tiny.en TFLite モデルを i.MX93 の NPU にどのように実装したか教えていただけますか?私は長い間これを探していましたが、これは開発に本当に役立つでしょう。モデルを TFLite INT8 に変換することはできましたが、NPU はすべての Whisper 操作を完全にサポートしていないSO、CPU では float32 モデルを使用する必要があります。それを変換して NPU で使用することは可能ですか? ありがとう Re: Recommendations for ASR, TTS and Transformer こんにちは@QuantumPath i.MX93 では、Whisper ASR (tiny、base、small) と Moonshine ASR (tiny と base) が有効になっています。 まず、7 月中旬までに Whisper ASR を GStreamer 経由で音声プラグインとして提供します。 TTS については、ViTS TTS を有効にしました。LLM の場合、Danube 0.5B のような小さな LLM を実行 CAN。 並行して、i.MX95 上で実行される完全な eIQ Gen Al フロー パイプライン (ウェイク ワード、ASR、LLM、RAG、TTS) がここにあります: https://github.com/nxp-appcodehub/dm-eiq-genai-flow-demonstrator?tab=readme-ov-file
View full article
S32K312 EVBデバッグ こんにちは: 本当に愚かなミスを犯してしまいました。S32K31XEVB-Q100 のデバッグ ポートを通常の GPIO として構成したため、デバッグ ポート経由でプログラムをダウンロードできなくなりました。この問題の解決策があるかどうか教えていただけますか? さらに、搭載 OPEN-SDA の代わりに外部デバッガーを使用しています。 Re: S32K312 EVB DEBUG こんにちは@PINKMAN 、 Segger 社はこの問題を修正しており、11 月 12 日にリリース予定のバージョン V8.88 に変更が組み込まれる予定です。 よろしくお願いいたします。 ダニエル Re: S32K312 EVB DEBUG こんにちは@PINKMAN 、 SEGGER お問い合わせにお問い合わせしたところ、アルゴリズムにバグがあることが確認されました。 現在、修正に取り組んでいます。利用可能になったら、それに応じてThreadを更新します。 よろしくお願いいたします。 ダニエル Re: S32K312 EVB DEBUG S32K31XEVB-Q100をお持ちの場合、PTA4(JTAG_TMS_SWD_DIO)をCMP_OUTとして設定し、jlinkコマンドを使用してロック解除を試みることができますか? Re: S32K312 EVB DEBUG 2つのモードすべてを試しましたが、まだ機能しません Re: S32K312 EVB DEBUG JTAG プロトコルも試していただけますか? よろしくお願い申し上げます。 Re: S32K312 EVB DEBUG あなたの提案によると、それは機能しません。写真は私の手順です。何が起こったのか教えていただけますか。私のデバッグはSWDモードです。ありがとうございます Re: S32K312 EVB DEBUG この解決策を試していただけますか? https://community.nxp.com/t5/S32-SDK/dap-after-program-s32k312-with-pll0-equal/td-p/1609010 の電源投入に失敗しました ありがとうございました。 BR、ダニエル Re: S32K312 EVB DEBUG PTA4 (JTAG_TMS_SWD_DIO) のみを CMP_OUT として設定し、他のデバッグ ピンは設定しませんでした。使用するデバッガーは JLINK です。この問題を解決する方法があれば教えていただけますか? Re: S32K312 EVB DEBUG こんにちは@PINKMAN 、 デバッグを成功させるには、ピンが再構成される前に、MCU をリセットし、デバッガーがコアを接続して短時間内に停止する必要があります。 reset_b ピンも再構成しましたか? SO、MCU をリセットする唯一の信頼できる方法は、パワーオン リセット (POR) を使用することです。 どのデバッガーを使用していますか? たとえば、Lauterbach を使用している場合は、次のようなスクリプトをCAN。 SYStem.CPU S32K312-M7 SYStem.config.core 1. 1. SYStem.config.debugporttype JTAG System.JTAGclock 10MHz sys.Option DUALPORT ON wait state.power() sys.up if RUN() break MCU に電源が投入されるまで待機します。 よろしくお願いいたします。 ダニエル
View full article
NOR フラッシュに UBI を接続すると、U-Boot「ubi0: レイアウト ボリュームが見つかりません」というエラーが発生します。 「私は、256 MiB NOR フラッシュ (GD55B02g2) を搭載した i.MX ベースのボードで U-Boot 2024.04 を使用しています。」 U-Boot はフラッシュとパーティションを正しく検出します。 mtdparts=21e0000.qspi:448k(U-Boot),64k(U-BootEnv),-(ubi パーティション) しかし、U-Boot が UBI パーティションを接続しようとすると失敗します。 SPIFlashから環境をロード中... SF: ページサイズ256バイト、消去サイズ64 KiB、合計256 MiBのGD55B02g2を検出しました *** 警告 - CRC が不正です。デフォルトの環境を使用しています UBI から環境をロードしています... ubi0: mtd3 を接続 ubi0: スキャンが完了しました ubi0 エラー: ubi_read_volume_table: レイアウトボリュームが見つかりませんでした ubi0 エラー: ubi_attach_mtd_dev: mtd3 の接続に失敗しました、エラー -22 UBIエラー: mtd3をアタッチできません UBI エラー: UBI を初期化できません、エラー -22 UBI初期化エラー22 正しい MTD パーティションが使用されているかどうか (サイズが十分大きいか) を確認してください。 ** mtdパーティション「ubi-partition」が見つかりません mtdparts と mtd list はパーティションが有効であることを示します。 sf プローブは正常に動作します。 U-Boot が正常に接続できるように、この ubi パーティションを適切に初期化またはフォーマットするにはどうすればよいですか? => mtdパーツ デバイス nor0 <21e0000.qspi>、部品数 = 3 #: 名前 サイズ オフセット mask_flags 0: U-Boot 0x00070000 0x00000000 0 1: U-BootEnv 0x00010000 0x00070000 0 2: ubiパーティション 0x0ff80000 0x00080000 0 アクティブパーティション: nor0,0 - (U-Boot) 0x00070000 @ 0x00000000 デフォルト: mtdids: nor0=21e0000.qspi mtdparts: mtdparts=21e0000.qspi:448k(U-Boot),64k(U-BootEnv),-(ubi-partition) => mtdリスト MTD デバイスのリスト: * ノル0 - デバイス: flash@0 - 親: spi@21e0000 - ドライバ: jedec_spi_nor - パス: /soc/bus@2100000/spi@21e0000/flash@0 - タイプ: NORフラッシュ - ブロックサイズ: 0x10000 バイト - 最小I/O: 0x1バイト - 0x000000000000-0x000010000000 : "nor0" - 0x000000000000-0x000000070000 : 「U-Boot」 - 0x000000070000-0x000000080000 : 「U-BootEnv」 - 0x000000080000-0x000010000000 : 「ubiパーティション」 次を使用して、U-Boot で UBI パーティションをアタッチしてみました。 => sfプローブ => ubi パート ubi パーティション U-Boot が UBI デバイスを正常に接続し、利用可能なボリュームを一覧表示することを期待していました。 しかし、次の理由で失敗しました: ubi0 エラー: ubi_read_volume_table: レイアウトボリュームが見つかりませんでした ubi0 エラー: ubi_attach_mtd_dev: mtd3 の接続に失敗しました、エラー -22 また、パーティション レイアウトが正しいことと、フラッシュが適切に検出されたことを確認するために、mtdparts と mtd list も実行しました。これで有効な UBI パーティションが確認されると思っていましたが、有効な UBI ヘッダーがまだないようです。 Re: U-Boot "ubi0: the layout volume was not found" error when attaching UBI on NOR flash. こんにちは@LoKi 返信が遅くなり申し訳ありません。まずは ubi パーティションをフォーマットして、有効な UBI パーティションにする必要があります。 BR
View full article
Android vendor_boot img で imx95 evk ボードのスターティングブロックを作成する imx95 android 15コードをダウンロードし、イメージを正常にビルドしてuuu_imx_android_flash.shでフラッシュしました。デフォルトで avb をサポートしており、フラッシュ プロセスは成功し、ブートローダは正常に動作しますが、boot_jump_linux 関数 armv8_switch_to_el2 を実行すると、ブロックされます。これらの vendor_boot.img と vbmeta-imx95.img を公式にビルドされた img に置き換えてみたところ、うまくいきました。そして、vendor_boot.img を単独で置き換え、uboot でパッケージ チェックを閉じると、カーネルも起動できるSO、ブロックの原因は私が構築した vendor_boot イメージであることがわかりました。vendor_boot イメージを解凍して、公式のものでコンパイルしてみましたが、bootconfig と dtb の違いは見つかりませんでした。 なぜ vendor_boot がカーネル実行問題を解決できないのか疑問に思います。私は vendor_boot のソースを変更していません。ブートローダと DDR タイミングのみを変更した場合、起動の問題の根本原因を見つけるにはどうすればよいですか。 回复: Android vendor_boot img make imx95 evk board starting block テストのためにこれらのイメージを置き換えようとしましたが、ブートローダーとspl /uboot init_boot vendor_boot vbmeta super dtboとパーティションテーブルが置き換えられ、最後にvendor_bootを置き換える必要があることが判明し、起動できるようになりました。つまり、カーネルの起動時にブロックされなくなり、カーネルの起動メッセージ「物理 CPU で Linux を起動しています...」が出力されます。
View full article
读/写 DDR 时,DRAM_ADDR10 变为 "1"(i.MX7D) 你好。 该电路基于 i.mx7D-Sabre 板。 如果我写入地址 0x80000000,同样的值也会写入地址 0x80000100。 当我用示波器检查时,确认 DDR_ADDR10 设置为 "1"。 我还确认 DDR_ADDR10 在刷新时序(3.5uSec)设置为 "1"。 除了刷新定时外,DDR_ADDR10 变为 "1 "是否有其他原因? 顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好,pengyong_zhang。 有你们的支持,我做得很好。 我按照"图 9-4 进行了设置。系统地址到物理地址的映射". 我将 BANK 和 ROW 向下移动了 1 位,并启用了 ROW_B15。 我已禁用 COL_B9。 我认为参考手册是矛盾的。 例如,COL_B2。 全总线宽度模式:-----位 2 半总线宽度模式:-----位 3 四分之一总线宽度模式:-----位 4 正确 全总线宽度模式:-----位 2 半总线宽度模式:-----位 1 四分之一总线宽度模式:-----位 3 这与"图 9-4 相对应。系统地址到物理地址的映射". 顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好@塔莫津 您可以通过 RPA 表更改总线宽度,如下图所示: B.R Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好,pengyong_zhang。 写入 DDR 的值与读取的值一致。 原理图中的错误是整个总线宽度变成了总线宽度的一半。 你能告诉我如何将地址映射寄存器设置为半总线宽度吗? 例如,我不明白为什么地址映射寄存器 2 中的 COL_B5 会从第 5 位变为第 6 位。 第 2194-2195 页上的解释仅适用于总线全宽。 顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好@塔莫津 请使用 md mw 命令读取数据并写入 DDR 地址测试,看看写入值是否与您的写入值相同。我已经在我的 imx7D 板上测试过了,我写入和读取值时没有问题。 你在 DDR 设计中犯了什么错误?我不明白您在原理图文件中提到的错误。 B.R Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好,pengyong_zhang。 我重读了参考手册并注意到了地址映射寄存器设置。 我发现全总线和半总线之间的列地址有所不同。 当我看到图 9-4 时,我以为 "全屏 "和 "半屏 "是相同的设置。 我以为 HIF 地址没有区别,但我错了吗? 当前设置如下: DDRC_ADDRMAP0 : 0x0000001F DDRC_ADDRMAP1 : 0x00080808 DDRC_ADDRMAP2 : 0x00000000 DDRC_ADDRMAP3 : 0x00000000 DDRC_ADDRMAP4 : 0x00000F0F DDRC_ADDRMAP5 : 0x07070707 DDRC_ADDRMAP6 : 0x0F070707 请指出任何错误。 顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好,pengyong_zhang。 现附上 Kyoto Microcomputer 的调试器 Jetset3 显示的内容。 顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好,pengyong_zhang。 谢谢! DDR 原理图附后。 主寄存器为 0x01041001。 u-启动 重定位的源代码如下: ENTRY(重新定位代码) adr r3, relocate_code ldr r1, _image_copy_start_ofs add r1, r3 /* r1<- 运行&__image_copy_start */ subs r4, r0, r1 /* r4<- 运行以复制偏移量 */ beq relocate_done /* 跳过重新定位 */ ldr r1, _image_copy_start_ofs add r1, r3 /* r1<- 运行&__image_copy_start */ ldr r2, _image_copy_end_ofs add r2, r3 /* r2<- 运行&__image_copy_end */ 复制循环: ldmia r1!, {r10-r11} /* 从源地址 [r1] 复制 */ stmia r0!, {r10-r11} /* 复制到目标地址 [r0] */ cmp r1, r2 /* 直到源端地址 [r2] */ blo copy_loop   在 DDR 中,或非-FLASH 中 0x28080000 的值被复制到 0x9FF93000。 但在 DDR 中,相同的值被复制到 0x9FF93800。 原因是 DRAM_ADDR10 复制到 0x9FF93000 时会变为 "1"。 我想知道 DRAM_ADDR10 为什么会变成 "1",以便解决这个问题。   顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) HI@tamotsu 你提到在 DDR 设计中犯了一个错误,什么是错误?如何更改 MR 寄存器? 能否提供有关问题描述的更多细节?测试代码和完整的日志文件。 B.R Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 我会补充更多信息。 我在 DDR 设计中犯了一个错误,将主寄存器的 DATA_BUS_WIDTH 设置为 Half DQ。 顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好,pengyong_zhang。 调试器发出的命令 我是通过在 u-boot 中使用 relocate.S 的过程找到的。 命令是 ldmia 和 stmia。 我试着将自动刷新改为自刷新,但效果并不明显。 顺祝商祺! Re: DRAM_ADDR10 becomes '1' when reading/writing DDR (i.MX7D) 你好@塔莫津 你在写什么命令? B.R
View full article
MIMXRT1180-EVK U10 (FlexSPI1_B) からの起動方法 おはよう、 FlexSPI1_B 経由で U10 NOR フラッシュからプログラムおよびブートするにはどうすればよいでしょうか? 1. 完了: プロジェクト構成で適切なドライバを使用する: MIMXRT1180_SFDP_FlexSPI1_B_QSPI.cfx 2. 方法: OTP をプログラミングする (OTP をプログラミングするにはどうすれば CAN 良いでしょうか?)どのようなツールを使う必要がありますか? 3. 完了: J59を1-2に移動して、U12が有効になっていないことを確認します。 SO、他にやるべきことがない場合、変更する OTP が何であるか、どのようにであるかを正確に知る必要があります。 サポートありがとうございます! Re: MIMXRT1180-EVK How to boot from U10 (FlexSPI1_B) ヒューズは xSPI_NOR_CONNECTION_SEL と呼ばれ、ヒューズ ワード 25 にあります。 BR、 オマール Re: MIMXRT1180-EVK How to boot from U10 (FlexSPI1_B) @Omar_Anguiano FLASH_CONNECTION_SEL が見つかりません。U10 から起動するために otp をどのように融合すればよいか教えていただけますか? どうもありがとうございます! Re: MIMXRT1180-EVK How to boot from U10 (FlexSPI1_B) @Omar_Anguianoさん、返信ありがとうございます。 私のニーズに合わせてヒューズを正しく焼き切るために、正確なポイントと書き込む必要のある値のスクリーンショットを送っていただけますか? Re: MIMXRT1180-EVK How to boot from U10 (FlexSPI1_B) Secure Provisioning Tool を使用してヒューズを焼き、他のピン グループを起動に使用することができます。 イメージのヘッダーもパッド構成と一致する必要があります。 BR、 オマール Re: MIMXRT1180-EVK How to boot from U10 (FlexSPI1_B) FLASH_CONNECTION_SEL ヒューズを交換するにはどうすればよいですか? よろしくお願い申し上げます。
View full article
swd構成デバイスが検出されません こんばんは、 残念ながら、フラッシュを誤ってプログラミングした後、ターゲットを見つけることがCANません。 .launchを削除してみましたファイル; カードが存在することはCAN認識しますが、もう見つかりません。 外部デバッガーがありません。ターゲットを修復するにはどうすればいいですか? よろしくお願いいたします。 Re: swd configuration no device detected こんにちは、パブロさん。 RT1062-EVKB ボードを使用していますが、プログラムもできません。MCUXpresso IDE は CMSIS-DAP デバッガーを検出しますが、デバッグ セッションを起動すると、SWD が検出されないというメッセージが表示されます。セキュア プロビジョニング ツールで提案されたことを実行しようとしましたが、チップの検出にも失敗しました。SO、CMD を使用して強制しようとしましたが、何も機能しませんでした。何か提案はありますか? Re: swd configuration no device detected おはようございます、パブロさん。 どうぞよろしくお願いいたします。なんとか修理でき、カードは動作するようになりました。 なぜこのようなことが起こったのか教えていただけますか? 改めて感謝申し上げます。 Re: swd configuration no device detected こんにちは@Transidico 、 フラッシュメモリが保護されている可能性があります。メモリが保護されているかどうか確認してもらえますか? これは、MCUXpresso Secure Provisioning Toolを使用して実行 CAN。 UART ボタン (赤) をクリックします。これにより、「ターゲット プロセッサとの接続」ウィンドウが開きます。 MCU-Link USB (J13) を介してボードを接続し、テスト接続ボタン (緑) を使用して UART 接続をテストします。 フラッシュが図のように固定されている場合は、次の操作を試してください。 コマンドラインインターフェース (青) を開き、次のコマンドを実行します。 blhost -p COM37,57600 -- フラッシュ消去すべて非セキュア 注: COM ポートは設定によって異なる場合があります。 よろしくお願いします、 パブロ Re: swd configuration no device detected 一括消去コンソール: フラッシュ操作「消去」を実行しています (フラッシュ消去) - Wed Sep 10 10:16:37 CEST 2025 MCU 情報を確認しています... ターゲットをスキャンしています... フラッシュアクションを実行しています... MCUXpresso IDE RedlinkMulti ドライバ v24.9 (2024年9月19日 19:34:05 - crt_emu_cm_redlink.exe ビルド 802) ( 0) リモート構成の読み取り Wc(03)。キャッシュはサポートされていません。 C:/ユーザー/transidico/Desktop/workspace2/TB1585/Debug\MCXC242.xml にチップ XML ファイルが見つかりました (5)リモート設定完了 既存の LinkServer プロセスに再接続しました。 ============= スクリプト: MCXC_connect.scp ============== MCXC 接続スクリプト プローブインデックス = 1 に接続しています このプローブ = 1 このTAP = 0 このコア = 0 DPID = 0BC11477 NRESETをアサートする リセットピンの状態: 00 パワーアップデバッグ MDM-AP APID: 0x001C0020 MDM-AP システムリセット/ホールドリセット/デバッグ要求 MDM-AP制御: 0x00000008 MDM-AP ステータス (フラッシュ準備完了): 0x00000036 部品は固定されています 一括消去が必要です ============= スクリプト終了 ============================ プローブファームウェア: MCU-LINK FRDM-MCXC242 (r0E7) CMSIS-DAP V3.160 (NXP Semiconductors) シリアル番号: D3RQLYWOEAOJ0 VID:PID: 1FC9:0143 USBパス: 0001:000d:00 適切なコアを検索した後、コア0のメモリを使用する redlink サーバー クライアント - 2000 ミリ秒後にサーバーからの応答 (op 62 へ) を受信できませんでした - タイムアウトしました (rc 138) 接続に失敗しました - EE(47): デバッグメールボックス要求が失敗しました...再試行しています redlink サーバー クライアント - 2000 ミリ秒後にサーバーからの応答 (op 12 へ) を受信できませんでした - タイムアウトしました (rc 138) プローブ 1 TAP 0 は TAP ID の読み取りに失敗しました - Ee(FF)。Redlink インターフェース エラー 255。 接続に失敗しました: Ee(FF)。Redlink インターフェース エラー 255。 接続してリセットしました。以前は: 未接続でした。DpID: 0BC11477。CPUID: 00000000。情報: 最後のスタブエラー0: OK 最後のスティッキーエラー: 0x0 AIndex: 0 デバッグバスが選択されました: MemAp 0 DAP 速度テストが実行されなかったか失敗しました デバッグ プロトコル: SWD。RTCK: 無効。ベクターキャッチ: 無効。 (100)ターゲット操作に失敗しました redlink サーバー クライアント - 警告 - サーバーからの予期しないデータ 28 バイト デバッグセッションの終了時にエラーが発生しました - Nn(05)。DAP アクセスにおける Wire ACK 障害 操作を実行できません! コマンドは終了コード 1 で失敗しました Re: swd configuration no device detected おはようございます、パブロさん。 LPC55s69のプログラミングを試みましたが、うまくいきませんでした。フラッシュメモリの一括消去も試みましたが、やはりうまくいきませんでした。 .launchファイルを削除した場合デバイスが見えます しかし、充電しようとするとデバイスが認識されません。 本当にどうすればいいのか分からない。 ありがとうございます。よろしくお願いいたします。 Re: swd configuration no device detected この新しいファームウェアが何と関係があるのか分かりません。フラッシュを間違ってプログラムした場合、フラッシュを一括消去すると問題が解決すると思います。コンソールからの変数を使用してフラッシュをプログラムし、コンソールが突然シャットダウンした場合、フラッシュを誤ってプログラムしたことになります。一括消去でこの問題が解決するかどうか教えていただけますか? ご返信ありがとうございます。 Re: swd configuration no device detected こんにちは@Transidico 、 CAN LPC55S69 のファームウェアを更新することで問題が解決するかどうかをテストするのを手伝ってもらえますか? 次の投稿に記載されている手順に従ってください。 MCX-NとMCX-Aのデバッガーを更新する方法 - NXPコミュニティ FRDM-MCXC242 で EVK を DFU モードに設定するには、ジャンパー JP1 を閉じる必要があります。 よろしくお願いします、 パブロ Re: swd configuration no device detected 何が起こったのか説明しましょう。私は統合された mcxpresso コンソールを備えた frdm-mcxc242 ボードを使用しています。コンソールから挿入してフラッシュ ドライブに変数を保存する、非常にシンプルなプログラムを作成してみたいと思いました。変数をフラッシュ ドライブに 3 回または 4 回保存して読み取った後、ある時点で、前述の画面 (SWD にデバイスが利用できません) が表示されました。 外部デバッガーは使用していませんが、ボードを回復する必要があります。リセットボタンを押してPCを再起動してみたのですが、効果はありませんでした。 ボードは紛失しましたか?
View full article
ベーシックセキュアブート HSE S32K344 ADKP こんにちは、みんな、 ベースセキュアブートでADKPをプログラムする方法を知りたいです S32K344-WB #HSE#ベースセキュアブート よろしくお願いします。 Re: Basic Secure Boot HSE S32K344 ADKP こんにちは、みんな、 私はS32K312EVB-Q172ボードを使用しており、 HSE デモ例をテストしたいと考えています。 ファイルS32K3_HSE_DemoExamples_1_0_0.zipにアクセスすることは可能でしょうか? 私はS32 プラットフォーム用の S32 Design Studio をPEMicro デバッガーと一緒に使用しています。 ご協力をよろしくお願いいたします! よろしくお願いします、 ダビデ Re: Basic Secure Boot HSE S32K344 ADKP こんにちは@silvia_zandoli2 発生している問題に関連している可能性があるので、次のThreadを確認することをお勧めします。 S32K344 セキュアブート HSE_VerifyBootImage の問題 Re: Basic Secure Boot HSE S32K344 ADKP こんにちは、 ブートローダーが正常に起動し (HSE_SignBootImage OK)、検証に合格すると、システムの LED が短時間青色に点滅します (セキュア ブートが成功したことを示します)。しかし、再起動または2回目のデバッグ時にシステムがクラッシュし、/* 生成されたタグがAPPBLに対して有効であることを確認する*/が合格しません。 #if VERIFY_TAG srvResponse = HSE_VerifyBootImage(pAppBL); ASSERT(HSE_SRV_RSP_OK == srvResponse); 問題は上書きにあると思われます。修正方法をご存知ですか? どうもありがとうございます。 Re: Basic Secure Boot HSE S32K344 ADKP こんにちは@silvia_zandoli2 HSE サービス応答 0x55A5AA33 は HSE_SRV_RSP_OK に対応します。 ただし、HSE_SignBootImage() 関数の呼び出し時に問題が発生する場合は、次のThreadを確認することをお勧めします。発生している問題に関連している可能性があります。 HSE_VerifyBootImage は HSE_SRV_RSP_VERIFY_FAILED を返します 問題が解決しない場合、またはThreadが特定のCASEに対応していない場合は、お知らせください。 Re: Basic Secure Boot HSE S32K344 ADKP S32K3_HSE_DemoExamples_1_0_0、S32K344デバイスを持っています ADKP は正常にプログラムされています (check_debug_password_programmed_status() が TRUE を返します)。 しかし、関数HSE_SignBootImage()は呼び出し直後に失敗し続け、エラーコード0x55a5aa33を返します。 基本的なセキュアブートのメインではアサートをパスしません /* 生成されたタグがAPPBLに対して有効であることを確認します */ #if VERIFY_TAG srvResponse = HSE_VerifyBootImage(pAppBL); ASSERT(HSE_SRV_RSP_OK == srvResponse); #endif S32K344_SecureBootBlinky.bin を生成し、C:\NXP に配置します。SecureBootBlinky と Basic_SecureBoot は C:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Secure_Boot にあります。 ベーシックセキュアブートのリンカーファイル「S32K344_flash.ld」に、 _adkp_key :  {  . = ALIGN(4);  キープ(*(_adkp_key))  . = ALIGN(4);  } > フラッシュ そのファイルを変更する必要がありますか?あなたに添付します /***************************************************************************** * * Copyright 2020-2022 NXP * All Rights Reserved * ***************************************************************************** * * このソフトウェアはNXPによって「現状のまま」提供され、明示的または黙示的を問わず、 * 黙示の保証(ただし、これに限定されません) * 商品性および特定目的への適合性については保証されません。 * いかなる場合においても、NXPまたはその貢献者は、いかなる直接的、間接的、偶発的、特別、懲罰的、または結果的な損害に対しても責任を負わないものとします。 * (代替品の調達を含むが、これに限定されません) * サービス、使用、データ、利益の喪失、または事業の中断) * いかなる原因であっても、また契約上の責任理論に基づいても、 * 厳格責任、または不法行為(過失その他を含む)から生じる * いかなる場合においても、このソフトウェアの使用から生じるいかなる損害についても、 * 当該損害の可能性。 * ********************************************************************************/ __STACK_SIZE = 0x00001000; __HEAP_SIZE = 0x00001000; /* メモリ領域を構成するリンカー スクリプト。Aggiungi PFLASH_SECURE は、地域の鳩を見て、チアビの批判を受け入れます*/ メモリ { ITCM (RWX) : 原点 = 0x00000000、長さ = 0x10000 PFLASH (RX) : 原点 = 0x400000、長さ = 0x3f4000 DFLASH (RX) : 原点 = 0x10000000、長さ = 0x20000 DTCM (RW) : 原点 = 0x20000000、長さ = 0x20000 SRAM0_STDBY (RW) : 原点 = 0x20400000、長さ = 0x8000 SRAM (RW) : 原点 = 0x20408000、長さ = 0x48000 } /* セクションとシンボル値を配置するためのリンカー スクリプト。一緒に使用する必要があります * メモリ領域 FLASH および RAM を定義する他のリンカー スクリプトを使用します。 * 次のシンボルを参照します。これらはコード内で定義する必要があります。 * Reset_Handler: リセットハンドラのエントリ * * 次のシンボルを定義します。コードでは定義しなくても使用できます。 * __exidx_start * __exidx_end * __ecc_table_start __ * __ ecc_table_end __ * __電子テキスト * __data_start __ * __事前初期化配列開始 * __preinit_array_end * __init_array_start * __init_array_end * __fini_array_start * __fini_array_end * __data_end __ * __ bss_start __ * __ bss_end __ * __ end __ * end * __ヒープ制限 * __StackLimit * __スタックトップ * __スタック */ ENTRY(リセットハンドラー) セクション { 。文章: { KEEP(*(.vectors)) *(。文章*) KEEP(*(.init)) KEEP(*(.fini)) /* .ctors*/ *crtbegin.o(.ctors) *crtbegin?.o(.ctors) *(EXCLUDE_FILE(*crtend?.o *crtend.o).ctors) *(SORT(.ctors.*)) *(.ctors) /* .dtors*/ *crtbegin.o(.dtors) *crtbegin?.o(.dtors) *(EXCLUDE_FILE(*crtend?.o *crtend.o).dtors) *(SORT(.dtors.*)) *(.dtors) *(.rodata*) 保持(*(.eh_frame*)) } > フラッシュ .ARM.extab: { *(.ARM.extab*.gnu.linkonce.armextab.*) } > フラッシュ __exidx_start = .; .ARM.exidx : { *(.ARM.exidx*.gnu.linkonce.armexidx.*) } > フラッシュ __exidx_end = .; .ecc.テーブル: { 。= 整列(4); __ecc_table_start__ = .; QUAD (__data_start __) QUAD ((__ data_end __ - __ data_start__) / 😎 クアッド (__bss_start __) QUAD ((__ bss_end __ - __ bss_start__) / 😎 QUAD ( __HeapTop) QUAD ((__ヒープ制限 - __ヒープトップ) / 😎 QUAD ( __StackLimit) QUAD ((__スタックトップ - __StackLimit) / 😎 クワッド(原点(ITCM)) クワッド(長さ(ITCM)/ 😎 クアッド(原点(DTCM)) クワッド(長さ(DTCM)/ 😎 __ecc_table_end__ = .; } > フラッシュ .copy.table : { 。= 整列(4); __copy_table_start__ = .; LONG ( __etext) LONG (__データ開始__) LONG ((__データ終了__ - __データ開始__) / 4) /* ここに各追加データセクションを追加します */ /* LONG ( __etext2) LONG (__ data2_start __) LONG ((__ data2_end __ - __ data2_start __) / 4) */ __ copy_table_end__ = .; } > フラッシュ .zero.table : { 。= 整列(4); __zero_table_start __ = .; /* Add each additional bss section here */ /* LONG (__ bss2_start __) LONG ((__ bss2_end __ - __ bss2_start __) / 4) */ __ zero_table_end__ = .; } > フラッシュ __etext = ALIGN(8); .boot_header: { KEEP(*(.boot_header)) } > Dフラッシュ .standby_ram: { *(.スタンバイ_ram) } > SRAM0_STDBY /* ECC初期化シーケンス __data_start __ and __ data_end __ should be aligned on 8 bytes */ .data : AT (__ etext) { 。= 整列(8); __data_start__ = .; *(vテーブル) *(。データ) *(。データ。*) . = ALIGN(4); /* 事前初期化データ */ PROVIDE_HIDDEN (__preinit_array_start = .); KEEP(*(.preinit_array)) PROVIDE_HIDDEN (__preinit_array_end = .); . = ALIGN(4); /* 初期化データ */ PROVIDE_HIDDEN (__init_array_start = .); KEEP(*(SORT(.init_array.*))) KEEP(*(.init_array)) PROVIDE_HIDDEN (__init_array_end = .); . = ALIGN(4); /* 有限データ */ PROVIDE_HIDDEN (__fini_array_start = .); KEEP(*(SORT(.fini_array.*))) KEEP(*(.fini_array)) PROVIDE_HIDDEN (__fini_array_end = .); 保持(*(.jcr*)) 。= 整列(8); /* 全データ終了 */ __data_end__ = .; } > SRAM /* ECC 初期化シーケンスのため __bss_start __ and __ bss_end __ should be aligned on 8 bytes */ .bss : { . = ALIGN(8); __ bss_start __ = .; *(.bss) *(.bss.*) *(COMMON) . = ALIGN(8); __ bss_end__ = .; } > SRAM /* ECC初期化シーケンスのため__HeapTop and __ HeapLimitは8バイトに揃える必要があります */ 。ヒープ(コピー): { 。= 整列(8); __HeapTop = .; __終了__ = .; _end = .; PROVIDE(終了 = .); 。= .+ __HEAP_SIZE; 。= 整列(8); __ヒープ制限 = .; } > SRAM /* ECC初期化シーケンスのため__StackLimit and __ StackTopは8バイトに揃える必要があります */ 。スタック(ORIGIN(SRAM) + LENGTH(SRAM) - __STACK_SIZE) (コピー) : { 。= 整列(8); __StackLimit = .; . = . + __スタックサイズ; 。= 整列(8); __StackTop = .; } > SRAM PROVIDE(__スタック = __StackTop); /* データ + ヒープ + スタックが RAM 制限を超えていないか確認します */ ASSERT( __StackLimit >= __ HeapLimit、「領域 RAM がスタックでオーバーフローしました」) CM7_START_ADDRESS = ORIGIN(PFLASH); __STDBYRAM_START = ORIGIN(SRAM0_STDBY); __STDBYRAM_SIZE = 長さ(SRAM0_STDBY); } S32K344-WB Re: Basic Secure Boot HSE S32K344 ADKP こんにちは@silvia_zandoli2 次のThreadを参照してください。このトピックに関連する情報が含まれており、役立つ可能性があります。 [S32K3] HSE使用時にパスワードでデバッグアクセスを制限する さらに、汎用 HSE デモ例および/または HSE_DEMOAPP 用の S32K3 MCUで提供されている関数 ProgramADKPService()、Advance_LifeCycle_Service()、および attributeProgrammingService() の実装を確認することをお勧めします。 BR、ヴェインB
View full article
NXP iMX95 EVK - NPU TensorFlow Lite モデル こんにちは、 NPU で eIQ TensorFlow Lite サンプルモデルを実行しましたが、次のエラーが発生して失敗しました。 情報: モデル mobilenet_v1_1.0_224_quant.tflite がロードされました 情報: 解決済み報告者 情報: EXTERNAL デリゲートが作成されました。 remoteproc remoteproc0: FWイメージNeutronFirmware.elfを起動しています remoteproc remoteproc0: リモートプロセッサ neutron-rproc が起動しました 情報: NeutronDelegate デリゲート: 1 つのパーティションを持つ 31 ノードのうち 29 ノードが委任されました。 INFO: EXTERNAL デリゲートを適用しました。 情報: CPU 用の TensorFlow Lite XNNPACK デリゲートを作成しました。 Neutron 4ab00004.imx95-Neutron: 無効な ioctl。コマンド=1075577096、引数=549719032088 Neutron推論ジョブの作成に失敗しました エラー: コンポーネント='Neutron ドライバ'、カテゴリ='内部障害'、コード=442 エラー: ノード番号 31 (NeutronDelegate) の呼び出しに失敗しました。 エラー: tflite の呼び出しに失敗しました。 例は次のパッケージを使用して構築されました。 # AI/ML IMAGE_INSTALL:append = "tensorflow-lite-neutron-delegate" 現在、リモート プロセッサはオフラインとして表示されます。 root@toradex-smarc-imx95-12593622:/sys/class/remoteproc/remoteproc0# 猫の状態 オフライン リモート プロセッサを手動で起動しようとすると、権限エラーが発生します。 root@toradex-smarc-imx95-12593622:~# echo rproc-neutron-rproc-fw > /sys/class/remoteproc/remoteproc0/firmware -sh: /sys/class/remoteproc/remoteproc0/firmware: 権限が拒否されました root@toradex-smarc-imx95-12593622:~# echo start > /sys/class/remoteproc/remoteproc0/state -sh: /sys/class/remoteproc/remoteproc0/state: 権限が拒否されました 現在、IMX_ML_User_Guide を参照して、NPU 上で eIQ Toolkit TensorFlow Lite の例を実行する作業を行っていますが、マイクロコードの不一致エラーが発生しました。 私たちのセットアップでは、BSPバージョンscarthgap-6.6.36-2.1.0を使用しています。eIQ ツールキット バージョン 1.16.0。TensorFlow Liteモデルを.tfliteに変換しましたeIQ ツールキットを使用して NPU 最適化モデルに変換しましたが、実行中に次のエラーが発生します。 トラブルシューティングのために、複数のBSPとeIQツールキットのバージョンの組み合わせ(BSP 6.6.52_2.2.0、6.12.34_2.1.0)をテストしました。、lf-6.6.3_1.0.0 6.6.23_2.0.0 および 6.6.36_2.1.0eIQ 1.16.0では、1.15.1、および 1.14.0)。ただし、マイクロコードのバージョンはいずれも、予想されるバージョンと一致しません。 予想されるマイクロコードバイナリ(NeutromFirmware.elf)を提供してください変更の実行やアドバイスのため。 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 BSP バージョンが 6.12.20 から 6.12.34 にアップグレードされ、eIQ ツールキットのデフォルトの例が実行されました。添付のスクリーンショットは結果を示しています。この例は正常に実行され、NXP i.MX95 EVK でデフォルトの画像分類出力が生成されました。ただし、実行中に 31 個のノードのいずれも委任されませんでした。 .tfliteを変換しました最新の eIQ Toolkit バージョン 17 を使用したモデル。ただし、TensorFlow Lite バージョン 17 で例を実行すると、画像分類の結果が表示されません。この問題を示すスクリーンショットを添付しました。 上記の両方のCASEは、NXP i.MX95 EVK で実行されました。 ただし、私たちの主な目的は、これらの例を Toradex SMARC i.MX95 EVK で実行することです。 Toradex ボードの BSP バージョン アップグレードはまだ不安定で、Toradex i.MX95 EVK にバージョン 6.12.34 の安定した BSP リリースがまだないため、NPU で AI ワークロードを実行すると複数のエラーが発生します。 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 モデルを次のように変換する必要があります。 /opt/nxp/eIQ_Toolkit_v1.17.0/bin/neutron-converter/MCU_SDK_25.09.00+Linux_6.12.34_2.1.0/neutron-converter \ --input you_model_quant.tflite \ --output your_model_neutron.tflite \ --target imx95 \ --convert-inputs-uint8-to-int8 \ --convert-outputs-uint8-to-int8 YOLOv11 Nano を 27 FPS で実行できました。バージョン不一致の警告はまだ表示されますが、問題は発生していません。警告を受けるのは楽しいことではありませんが、今となってはそれについてCANことはあまりありません。 お役に立てれば幸いです。 乾杯! Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 最新バージョン (6.12.34) では、さらに多くのノードとオペレーターを変換することができました。変換された演算子が 3% から 62 ドルに増加しました。これは、YOLOv11 ベースのモデルとしては非常に良好です。 今度はバージョンの不一致もあります。しかし、それは私のボードのバージョンによるものです。SO、6.12.20 から 6.12.34 にアップデートしようとしています。お持ちのバージョンと変換に使用したバージョンをご確認ください。 乾杯! Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 このエラーについては分かりませんが、おそらく NXP の誰かが介入するはずです。 私もガイドに従って、カスタム 1 ステージ検出器 (CNN ベース) を変換することができました。残念ながら、デリゲートにロードされるノードは 1 つだけです (残りは、CPU 用の XNNPACK のままです)。 ====== V4L2ENC: 1.26.0 build on May 7 2025 08:46:20. ====== INFO: NeutronDelegate delegate: 1 nodes delegated out of 697 nodes with 1 partitions. INFO: Neutron delegate version: v1.0.0-a5d640e6, zerocp enabled. INFO: Created TensorFlow Lite XNNPACK delegate for CPU. これはおそらく、変換後に 697 個の Neutron Graph のうち 1 個だけ作成されるためです。変換された演算子は 27 個のみです。笑 Conversion statistics: Number of operators after import = 678 Number of operators after optimize = 723 Number of operators converted = 27 Number of operators NOT converted = 696 Number of operators after extract = 697 Number of Neutron graphs = 1 Number of operators NOT converted = 696 Operator conversion ratio = 27 / 723 = 0.0373444 Operators converted = 1,2,3,4,5,6,7,8,9,10,11,12,13,14,15,16,17,18,19,20,21,22,23,24,25,26,27, Variscite のサポートに再度お問い合わせし、何かアイデアが得られるか確認してみました。NXP がここで実際に返答しないのは残念です。 解決策が見つかることを願っています。引き続き調査を続け、何か見つかったらお知らせします。 乾杯! Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 サポートありがとうございます。共有していただいたリンクを確認し、提供された手順に従いましたが、マイクロコード不一致エラーがまだ発生します。参考までにスクリーンショットを添付しました。 これを確認して問題解決にご協力いただけますでしょうか? Re: NXP iMX95 EVK - NPU TensorFlow Lite Model NXP のサポートは非常に悪く、ドキュメントには必要なものがすべて記載されていません。また、Neutron 準拠モデルが付属していないイメージについては言うまでもありません (変換されずにイメージに追加されなかったためです)。 私は、NXP iMX 95 が統合されたボードを提供しているNXPについてである Variscite に連絡し、支援してもらいました。これを動作させるには、NPX の例であっても、自分でモデルを変換する必要があります。次の手順に従ってください: https://dev.variscite.com/dart-mx95/mx95-yocto-walnascar-6.12.20_2.0.0-v1.2/machine-learning/ 他の作業で忙しいので、まだ変換は行っていません。 お役に立てれば幸いです。 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 最新の BSP リリースに更新しましたが、問題は依然として解決しません。この問題の解決にご協力いただけませんか? Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 私も同じ問題に直面しており、CAN回避できません。 以下の例のように、画像に付属するサンプル コードをテストしました。NeutroDelegate がノードを適切に委任しないという同じ問題が発生します。私たちの検出モデルで試してみましたが、予想どおり同じ結果でした。 ====== V4L2ENC: 1.26.0 build on May 7 2025 08:46:20. ====== INFO: NeutronDelegate delegate: 0 nodes delegated out of 678 nodes with 0 partitions. Error in cpuinfo: prctl(PR_SVE_GET_VL) failed INFO: Created TensorFlow Lite XNNPACK delegate for CPU. これを実行しようとすると、 echo start > /sys/class/remoteproc/remoteproc0/state 結果としてアクセスが拒否されました。 多くの画像で試してみました: 6.12.20_2.0.0-v1.1:動作し、起動しますが、デリゲートが適切に割り当てられません。 6.6.52_2.2.0-v1.1:動作しません。起動すらしません。 6.6.23_2.0.0-v1.1:動作しません。起動すらしません。 6.6.1_1.0.0-v1..00: 動作しません - 起動すらしません。 Variscite DART DM95 に付属する NXP i.MX 95 をテスト中です (またはテストしようとしています)。画像は彼らのサイトからダウンロードされました。最新の NXP リリースでも試してみましたが、これも機能しませんでした。 この許可が拒否された理由は何でしょうか?特定の動作する画像をお持ちの場合は、それをダウンロードするためのリンクを共有していただけますか? サポートをよろしくお願いいたします。 乾杯! Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは。 それは奇妙です。SO、最新の BSP を使用していることを確認し、ボードの Linux を消去して再度書き込んでください。ここでは問題なく動作しているので、これ以上言うことはCANません。 よろしくお願いします。 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 ご提案のとおり、以下のコマンドを試しましたが、依然としてアクセスが拒否されるなどのエラーが発生しました。ルートおよび sudo でもコマンドを試していますが、依然としてアクセス拒否の問題が発生しています。参考までにスクリーンショットを追加しました。 1.エコー停止 > /sys/class/remoteproc/remoteproc0/state 2.cat /sys/class/remoteproc/remoteproc0/state 3.ls /lib/ファームウェア 4.echo NeutronFirmware.elf > /sys/class/remoteproc/remoteproc0/firmware Re: NXP iMX95 EVK - NPU TensorFlow Lite Model こんにちは、 エラー メッセージによると、RemoteProc 権限の問題と NPU デリゲートの失敗の両方が発生しています。これらを段階的に解決するお手伝いをさせていただきます。 1. RemoteProc の権限の問題 リモート プロセッサを手動で制御しようとしたときに表示される権限エラーはよくあるものです。RemoteProc のドキュメントによると、変更を加える前にリモート プロセッサが正しい状態であることを確認する必要があります。 # cat /sys/class/remoteproc/remoteproc0/state 権限が拒否されたエラーが発生した場合は、まずリモート プロセッサを停止してみてください。 # エコー停止 > /sys/class/remoteproc/remoteproc0/state ( 次に、オフラインであることを確認します。 # cat /sys/class/remoteproc/remoteproc0/state オフライン 2. ファームウェアのロードプロセス ファームウェアをロードする場合、RemoteProc フレームワークはデフォルトで /lib/firmware 内に格納されている *.elf ファームウェアを検索します(1) 。ファームウェアを次の場所にコピーCAN: $ scp hello_world.elf root@ :/lib/firmware ファームウェアが他の場所に保存されている場合は、ファームウェア パスを更新CAN。 # echo -n new_path > /sys/module/firmware_class/parameters/path 3. リモートプロセッサのロードと起動 ファームウェアをロードするには、ファームウェア ファイルにその名前を書き込みます。 # echo.elf > /sys/class/remoteproc/remoteproc0/ファームウェア 重要: 必ず *.elf ファームウェアを実行してください。そうしないと動作しません。 新しいファームウェアでリモート プロセッサを起動するには: # エコー開始 > /sys/class/remoteproc/remoteproc0/state 次のような出力が表示されます。 [12594.692880] remoteproc remoteproc0: imx-rproc を起動しています [12594.698629]remoteproc remoteproc0: FWイメージhello_world.elfを起動しています。サイズ 240736 [12594.706192]remoteproc remoteproc0: dtb rsrc-table がありません [12594.761474]remoteproc remoteproc0: リモートプロセッサ imx-rproc が起動しました 4. NPU構成要件 コミュニティの議論に基づいて、NPU の設定にはいくつかの重要な考慮事項があります。 NPU サポートの確認: ハードウェアが NPU 実行をサポートしていること、および使用している TensorFlow Lite バージョンが NPU アクセラレーションと互換性があることを確認します。 NPUドライバのインストール: NPUドライバが正しくインストールされ、設定されていることを確認します 正しい TensorFlow Lite デリゲートを使用する: NPU 実行に適切なデリゲートを使用していることを確認します。 5. トラブルシューティングの手順 ハードウェアサポートの確認: ハードウェア構成がNPUデリゲートをサポートしていることを確認します。 ファームウェアの検証: 正しいNPUファームウェアがロードされていることを確認します ドライバステータス: Neutronドライバが正しくロードされ、アクセス可能かどうかを確認します デリゲート構成: TensorFlow Lite デリゲートが特定のハードウェアに対して正しく構成されていることを確認します。 6. 代替アプローチ 問題が引き続き発生する場合は、まず CPU のみの推論でテストして、問題が NPU アクセラレーションに特有のものかどうかを特定することを検討してください。ハードウェアアクセラレーションを一時的に無効にするには、 USE_HW_ACCELERATED_INFERENCE=0 よろしくお願いします。  
View full article
恩智浦 iMX95 EVK - NPU TensorFlow Lite 模型 你好、 我们在 NPU 上运行了 eIQ TensorFlow Lite 示例模型,但却出现了以下错误: 信息:加载模型 mobilenet_v1_1.0_224_quant.tflite INFO: 解决了记者问题 INFO:已创建外部代表。 remoteproc remoteproc 0:正在启动几个镜像 neutronFirmware.elf remoteproc remoteproc0:远程处理器 neutron-rproc 已启动 INFO:NeutronDelegate 委托:31 个节点中已委托 29 个节点,1 个分区。 信息:应用了外部委托。 信息:为 CPU 创建了 TensorFlow Lite XNNPACK 代理。 中子 4ab00004.imx95-neutron:ioctl 无效。cmd=1075577096,arg=549719032088 无法创建中子推理任务 错误:元器件="Neutron Driver",category="内部故障",代码=442 错误:节点编号 31(NeutronDelegate)无法调用。 错误:调用 tflite 失败! 这些示例是使用以下代码包构建的: # AI/ML IMAGE_INSTALL:append =" tensorflow-lite-neutron-delegate" 目前,远程处理器显示为脱机: root@toradex-smarc-imx95-12593622:/sys/class/remoteproc/remoteproc0# cat state 脱机 在尝试手动启动远程处理器时,我遇到了权限错误: root@toradex-smarc-imx95-12593622:~# echo rproc-neutron-rproc-fw> /sys/class/remoteproc/remoteproc0/firmware -sh:/sys/class/remoteproc/remoteproc0/firmware:权限被拒绝 root@toradex-smarc-imx95-12593622:~# echo start> /sys/class/remoteproc/remoteproc0/state -sh:/sys/class/remoteproc/remoteproc0/state:权限被拒绝 我们目前正在参照 IMX_ML_User_Guide,在 NPU 上运行 eIQ Toolkit TensorFlow Lite 示例,但遇到了微码不匹配错误。 我们的设置使用 电路板支持包 版本 scarthgap-6.6.36-2.1.0和 eIQ 工具包 1.16.0 版。我们将 TensorFlow Lite 模型 .tflite但在执行过程中,出现了以下错误: 为了排除故障,我们测试了多个电路板支持包和 eIQ Toolkit 版本组合(电路板支持包 6.6.52_2.2.0、6.12.34_2.1.0、6.12.34_2.1.0), lf-6.6.3_1.0.0 6.6.23_2.0.0 和 6.6.36_2.1.0使用 eIQ 1.16.0、1.15.1 和 1.14.0)。但是,任何微码版本都与预期版本不符。 请提供预期的微码二进制文件 (NeutromFirmware.elf)执行或提出任何修改意见。 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 你好, 电路板支持包 版本从 6.12.20 升级到 6.12.34,并执行了 eIQ 工具包中的默认示例。所附截图显示了结果--示例成功运行,并在恩智浦 i.MX95 EVK 上生成了默认图像分类输出。然而,在执行过程中,31 个节点中没有一个被委托。 我转换了我的 .tflite该模型使用最新的 eIQ 工具包第 17 版。但是,当我使用 TensorFlow Lite 17 版本运行该示例时,却没有显示图像分类结果。我附上了显示此问题的截图。 上述两个案例都是在恩智浦 i.MX95 EVK 上执行的。 不过,我们的主要目标是在 Toradex SMARC i.MX95 EVK 上运行这些示例。 由于Toradex i.MX95 EVK尚未发布6.12.34版本的稳定电路板支持包,因此Toradex主板上的电路板支持包升级仍然不稳定,导致在NPU上运行人工智能工作负载时出现多个错误。 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 又见面了 你应该这样转换你的模型: /opt/nxp/eIQ_Toolkit_v1.17.0/bin/neutron-converter/MCU_SDK_25.09.00+Linux_6.12.34_2.1.0/neutron-converter \ --input you_model_quant.tflite \ --output your_model_neutron.tflite \ --target imx95 \ --convert-inputs-uint8-to-int8 \ --convert-outputs-uint8-to-int8 我让 YOLOv11 Nano 以 27 FPS 的速度运行。我仍然收到版本不匹配警告,但这些都不会造成问题。有警告并不好玩,但现在也无能为力。 希望对您有所帮助。 干杯 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 又见面了 我设法用最新版本(6.12.34)转换了更多的节点和操作符。从 3% 到 62 美元的运营商转换,这对于基于 YOLOv11 的机型来说真是不错。 现在我也遇到了版本不匹配的问题。但这是我主板上的版本造成的。因此,我试图将它从 6.12.20 升级到 6.12.34。请检查您拥有的版本和用于转换的版本。 干杯 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 您好, 我不知道这个错误,也许恩智浦公司的人可以插话。 我也按照指南,成功转换了我的定制单级探测器(基于 CNN)。遗憾的是,只有 1 个节点被加载到委托中(其余节点仍由 CPU XNNPACK 处理): ====== V4L2ENC: 1.26.0 build on May 7 2025 08:46:20. ====== INFO: NeutronDelegate delegate: 1 nodes delegated out of 697 nodes with 1 partitions. INFO: Neutron delegate version: v1.0.0-a5d640e6, zerocp enabled. INFO: Created TensorFlow Lite XNNPACK delegate for CPU. 这可能是因为转换后,697 个中子图中只创建了 1 个。只有 27 名操作员进行了转换。lol Conversion statistics: Number of operators after import = 678 Number of operators after optimize = 723 Number of operators converted = 27 Number of operators NOT converted = 696 Number of operators after extract = 697 Number of Neutron graphs = 1 Number of operators NOT converted = 696 Operator conversion ratio = 27 / 723 = 0.0373444 Operators converted = 1,2,3,4,5,6,7,8,9,10,11,12,13,14,15,16,17,18,19,20,21,22,23,24,25,26,27, 我再次联系了 Variscite 的支持人员,看看他们是否有什么好主意。很遗憾恩智浦没有真正回复。 希望你能找到解决办法。我会继续调查,如果有什么发现,我会告诉你。 干杯 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 您好, 感谢您的支持。我查看了您分享的链接,并按照提供的步骤进行了操作,但还是遇到了微码不匹配错误。我附上了一张屏幕截图供你参考。 能否请您检查一下并帮助我们解决问题? Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 恩智浦的支持真的很糟糕,他们的文档也没有提供我们所需要的一切,更不用说那些不带 Neutron 兼容模型的映像了--因为他们没有将其转换并添加到映像中。 我联系了Variscite,该公司提供了集成恩智浦iMX 95的板,他们为我提供了帮助。即使是使用 NPX 示例,也必须自己转换模型才能正常工作。请按此处说明操作: https://dev.variscite.com/dart-mx95/mx95-yocto-walnascar-6.12.20_2.0.0-v1.2/machine-learning/ 我还没有进行转换,因为忙于其他事情。 希望对你有所帮助。 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 我们已经更新到最新的电路板支持包版本,但问题仍然存在。您能帮助我们解决这个问题吗? Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 您好, 我面临着同样的问题,却无法解决。 我测试了图片附带的示例代码 - 在示例下。我也遇到了同样的问题,NeutroDelegate 无法正确委托节点。我用我们的检测模型试了试,结果和预想的一样。 ====== V4L2ENC: 1.26.0 build on May 7 2025 08:46:20. ====== INFO: NeutronDelegate delegate: 0 nodes delegated out of 678 nodes with 0 partitions. Error in cpuinfo: prctl(PR_SVE_GET_VL) failed INFO: Created TensorFlow Lite XNNPACK delegate for CPU. 任何这样的尝试: echo start > /sys/class/remoteproc/remoteproc0/state 结果是拒绝许可。 我试过很多图片: 6.12.20_2.0.0-v1.1:可以工作,可以启动,但委托没有得到正确分配。 6.6.52_2.2.0-v1.1:不起作用-甚至无法启动。 6.6.23_2.0.0-v1.1:不起作用-甚至无法启动。 6.6.1_1.0.0-v1.. 00:不起作用-甚至无法启动。 我们正在测试或试图测试 Variscite DART DM95 附带的 NXP i.MX 95。图片是从他们的网站上下载的。我也尝试过最新的恩智浦版本,但这也行不通。 您知道权限被拒绝的原因是什么吗?如果您有特定的工作图像,能否分享下载链接? 提前感谢您的支持。 干杯 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 你好。 这很奇怪,所以请确保你有最新的电路板支持包,擦掉板上的 linux 再烧掉,我不能再说了,因为它在这里运行良好。 此致 Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 你好, 我们按照你的建议尝试了下面的命令,但仍然遇到了权限被拒绝等错误。我们也在尝试使用 root 和 sudo 命令,但仍然面临权限被拒绝的问题。已添加屏幕截图供您参考。 1.echo stop> /sys/class/remoteproc/remoteproc0/state 2.cat /sys/class/remoteproc/remoteproc0/state 3.ls /lib/firmware 4.echo NeutronFirmware.elf> /sys/class/remoteproc/remoteproc0/firmware Re: NXP iMX95 EVK - NPU TensorFlow Lite Model 你好 根据你的错误信息,你同时遇到了 RemoteProc 权限问题和 NPU 委托失败。让我来帮你逐步解决这些问题。 1.RemoteProc 权限问题 您在尝试手动控制远程处理器时看到的权限错误很常见。根据 RemoteProc 文档,在进行更改之前,需要确保远程处理器处于正确状态。 # cat /sys/class/remoteproc/remoteproc0/state 如果出现权限拒绝错误,请先尝试停止远程处理器: # echo stop> /sys/class/remoteproc/remoteproc0/state ( 然后验证是否脱机: # cat /sys/class/remoteproc/remoteproc0/state offline 2.固件加载过程 在加载固件时,RemoteProc 框架默认会查找存储在 /lib/firmware 内的 *.elf 固件(1)。您可以将固件复制到该位置: $ scp hello_world.elf root@ :/lib/firmware 如果固件存储在其他地方,可以更新固件路径: # echo -n new_path> /sys/module/firmware_class/parameters/path 3.加载和启动远程处理器 要加载固件,请将其名称写入固件文件: # echo .elf> /sys/class/remoteproc/remoteproc0/firmware 重要: 确保运行 *.elf 固件,否则将无法运行 使用新固件启动远程处理器: # echo start> /sys/class/remoteproc/remoteproc0/state 您应该会看到类似的输出结果: [12594.692880] remoteproc remoteproc0:启动 imx-rproc [12594.698629]remoteproc remoteproc 0:正在启动 fw 图片 hello_world.elf,size 240736 [12594.706192]remoteproc remoteproc0: no dtb rsrc-table [12594.761474]remoteproc remoteproc0:远程处理器 imx-rproc 已启动 4.NPU 配置要求 根据社区讨论,设置 NPU 有几个重要的考虑因素: 验证 NPU 支持:确保您的硬件支持 NPU 执行,且您使用的 TensorFlow Lite 版本与 NPU 加速兼容 安装 NPU 驱动程序:确保正确安装和配置 NPU 驱动程序 使用正确的 TensorFlow Lite 委托:确保使用合适的委托执行 NPU 5.故障排除步骤 检查硬件支持:验证硬件配置是否支持 NPU 代理 固件验证:确保已加载正确的 NPU 固件 驱动程序状态:检查中子驱动程序是否已正确加载并可访问 委托配置:验证 TensorFlow Lite 委托是否针对特定硬件进行了正确配置 6.替代方法 如果继续遇到问题,请考虑先使用纯 CPU 推理进行测试,以确定问题是否与 NPU 加速有关。您可以使用 USE_HW_ACCELERATED_INFERENCE=0 此致  
View full article
i.MX RT1062 的最新 SDK 25_09 中缺少 flexio_mculcd 驱动程序 您好,NXP团队, 我注意到,在以前的 SDK 版本中可用的 flexio_mculcd 驱动程序在最新的 SDK 25_09 中似乎不见了。 我目前正在使用 i.MX RT1062 处理器,并计划在显示器上使用 8080 接口。请说明该驱动程序是否已被弃用或迁移,或者在最新的 SDK 中是否有推荐的替代方法? 如能得到任何指导,将不胜感激。 非常感谢, Hoa Re: Missing flexio_mculcd Driver in Latest SDK 25_09 for i.MX RT1062 flexio_mculcd 驱动程序并没有被弃用;但是,i.MX RT1060 的当前 SDK 2.5.09 版本中并不包含该驱动程序。 要访问和使用该驱动程序,我们建议参考较早的 SDK 版本,在该版本中,驱动程序和相关示例仍然可用。 这种方法允许您继续使用 8080 接口进行开发,同时保持与现有驱动程序支持的兼容性。 BR, Omar
View full article
LINFlexD UART Rx FIFO 软复位 你好 我正在尝试使用 TX 和 RX FIFO 缓冲器将 LINFlexD_9 设置为 UART 模式。TX FIFO 工作正常,但是当我启用 RX FIFO 退出初始化模式(LINCR1 [INIT] = 0)时,会导致软复位。 这些是将 LINCR1[INIT] 设置为 0 之前的寄存器值。 您知道发生了什么事吗? Re: LINFlexD UART Rx FIFO sofreset 你好@smp9、 对不起,我的回复晚了。您只需选择Watch 寄存器中的所有寄存器,然后以逗号分隔数据的形式复制即可。不过,由于 LIN 的登记册很少,您可以通过以下方法进行比较: 在进入正常模式之前,我在这里对程序进行了加密: 调用堆栈如下 登记情况如下 UARTCR 0x00000027 LINSR 0x00002000 LINOCR 0x0000 FFFF UARTPTO 0x00000FFF BDRL 0x00000000 DMARXE 0x00000000 LINTOCR 0x00000E2C LINFBRR 0x0000000B LINCR1 0x00000080 BDRM 0x00000000 LINESR 0x00000000 LINCR2 0x00006000 UARTCTO 0x000009FE UARTSR 0x00000048 LINCFR 0x00000000 BIDR 0x00000000 DMATXE 0x00000000 LINTCSR 0x00000200 GCR 0x00000000 里纳 0x00000000 LINIBRR 0x00000015 如果您发现任何重大差异,请告诉我 Re: LINFlexD UART Rx FIFO sofreset 你好@alejandro_e、 我尝试同时写入 SLEEP 和 WRITE 位,但问题依然存在。 我附上了使用 "监视寄存器"> "导出 "转储的寄存器值,因为 "内存"> "导出 "对这些地址不起作用。 谢谢。 Re: LINFlexD UART Rx FIFO sofreset 你好@smp9、 感谢您再次与我们联系。我猜你还在使用 S32E2。我查看了 RTD 的操作方法,似乎需要同时写入 SLEEP 和 INIT 位: 您是以这种方式进行配置的吗? 如果问题不在于此,您能否共享在向 LINCR1[INIT] 写 0 之前对 LLCE 寄存器的完整转储?地址范围 0x42980000 - 0x4298005C 因此,我可以举例说明。 谢谢  Re: LINFlexD UART Rx FIFO sofreset 你要退出启动 ROM 了吗?我在启动 S32E 评估板时遇到了这个问题。如果无法启动其他启动源,HSE 处理器中的启动 ROM 将进入串行启动模式,它会访问 LINFLEX 9 尝试从 UART 加载启动序列。这种行为似乎与尝试初始化 RX FIFO 相冲突并导致软复位。一旦你退出启动 ROM(通过启动有效的启动源,如 EMMC 或 QSPI),启动 ROM 就不会尝试持续访问 LINFLEX 9,启用 RX FIFO 也不会再导致这种软复位。
View full article
ex_ecc with -DPTMW_SE05X_Auth=ECKey_PlatfSCP03 I'm using Plug & Trust middleware (v04.05.03) from  github plug-and-trust. Built ex_ecc with CMake flags: -DPTMW_Applet=SE05X_C -DPTMW_HostCrypto=OPENSSL -DPTMW_SE05X_Auth=ECKey_PlatfSCP03 Configured /tmp/SE05X/plain_scp.txt: Running ./ex_ecc /dev/i2c-0 fails with: SE ECDSA Public Key is not Provisioned!!! and sss_session_open failed. Full log: App :INFO :PlugAndTrust_v04.05.03_20240502 App :INFO :Running //tmp/ex_ecc App :INFO :Using PortName='/dev/i2c-0' (CLI) ... App :WARN :Using SCP03 keys from:'/tmp/SE05X/plain_scp.txt' App :ERROR:Unknown key type ... sss :INFO :atr (Len=35) ... sss :INFO :Newer version of Applet Found sss :INFO :Compiled for 0x70200. Got newer 0x70216 ... sss :ERROR:SE ECDSA Public Key is not Provisioned!!! App :ERROR:sss_session_open failed ... How do I provision the ECDSA public key for ECKey_PlatfSCP03 auth? Smart Cards Re: ex_ecc with -DPTMW_SE05X_Auth=ECKey_PlatfSCP03 Hi @carlos_o  Thanks for the previous guidance. I resolved the "SE ECDSA Public Key is not Provisioned" issue with the following steps on SE052F: Set default session login to SSS_HAVE_SE05X_AUTH_PLATFSCP03. Run the se05x_Delete_and_test_provision example to perform AddAttestationKeys and ReInitializeTestSample (all succeeded with kSE05x_Result_SUCCESS). Switch default session login to SSS_HAVE_SE05X_AUTH_ECKEY_PLATFSCP03. After this, ex_sss_boot_open succeeds, and ./ex_ecc /dev/i2c-0 runs without errors. Can you confirm if this workflow:SSS_HAVE_SE05X_AUTH_PLATFSCP03 -->provision --> SSS_HAVE_SE05X_AUTH_ECKEY_PLATFSCP03 is correct and recommended? Re: ex_ecc with -DPTMW_SE05X_Auth=ECKey_PlatfSCP03 Hi @KiteJLKo  Could you try to update to SE-PLUG-TRUST-MW_04.07.01?  Re: ex_ecc with -DPTMW_SE05X_Auth=ECKey_PlatfSCP03 Hi @carlos_o , My Env: yocto Linux  Re: ex_ecc with -DPTMW_SE05X_Auth=ECKey_PlatfSCP03 Hi @KiteJLKo  Could you please provide in which environment are you building the code? (Windows, linux, specific microcontroller)
View full article
RT1051 PWM Capture Counter Stop Hello, recently when I was doing a project about FlexPWM capture on RT1051, I encountered a problem that the timer could not start properly, when I remove the crossover code or set it to 1 crossover frequency, Counter can run normally, but when I set it to 2 crossover frequency or higher crossover frequency Counter stops, what is the reason for this? void Capture_config(void) { pwm_input_capture_param_t pwm_input_capture; gpio_pin_config_t PWM_pin_config; //初始化输入捕获管脚 IOMUXC_SetPinMux(PWM2_PWMA03_IOMUXC, 0U); //设置外部引脚的复用功能 IOMUXC_SetPinConfig(PWM2_PWMA03_IOMUXC, PWMC_INPUT_PAD_CONFIG_DATA); //设置引脚的 pad 属性 PWM_pin_config.direction = kGPIO_DigitalInput; PWM_pin_config.interruptMode = kGPIO_NoIntmode; GPIO_PinInit(PWM2_PWMA03_GPIO, PWM2_PWMA03_GPIO_PIN, &PWM_pin_config); //初始化输入捕获配置参数 pwm_input_capture.captureInputSel = false; pwm_input_capture.edge0 = kPWM_RisingEdge; //pwm_input_capture.edge1 = kPWM_FallingEdge; pwm_input_capture.enableOneShotCapture = false; //pwm_input_capture.edgeCompareValue = 10; //当captureInputSel为FALSE时,此处设值无意义 pwm_input_capture.fifoWatermark = 0; PWM_SetupInputCapture(PI_PWM_BASEADDR, kPWM_Module_3, kPWM_PwmA, &pwm_input_capture); //开启捕获中断 //set_IRQn_Priority(PWM2_3_IRQn,Group4_PreemptPriority_0, Group4_SubPriority_0);//设置中断优先级 //PWM_EnableInterrupts(PI_PWM_BASEADDR, kPWM_Module_3, kPWM_CaptureA0InterruptEnable| kPWM_CaptureA1InterruptEnable ); PWM_EnableInterrupts(PI_PWM_BASEADDR, kPWM_Module_3, kPWM_CaptureA0InterruptEnable ); EnableIRQ(PWM2_3_IRQn); } /** * @brief 初始化 PWM 配置参数 * @retval 无 */ void PWM_config(void) { pwm_config_t pwmConfig;//定义pwm 配置结构体 PWM_Deinit(PI_PWM_BASEADDR, kPWM_Module_3); /*设置AHB总线时钟和IP总线时钟*/ CLOCK_SetDiv(kCLOCK_IpgDiv, 0x3); /* Set IPG PODF to 3, divede by 4 */ /*设置pwm 错误输入为高电平,表示没有错误,只有当pwm 没有错误输入或者禁止错误检测才能正常输出pwm波*/ XBARA_Init(XBARA1); XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputLogicHigh, kXBARA1_OutputFlexpwm1Fault0); XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputLogicHigh, kXBARA1_OutputFlexpwm1Fault1); XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputLogicHigh, kXBARA1_OutputFlexpwm1234Fault2); XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputLogicHigh, kXBARA1_OutputFlexpwm1234Fault3); PWM_GetDefaultConfig(&pwmConfig); pwmConfig.reloadLogic = kPWM_ReloadPwmFullCycle; //新值在上一个pwm周期输出结束之后加载到缓冲寄存器中 pwmConfig.pairOperation = kPWM_Independent; // 工作在独立模式 pwmConfig.clockSource = kPWM_BusClock; pwmConfig.enableDebugMode = true; // 使能DebugMode pwmConfig.prescale = kPWM_Prescale_Divide_128; //1320000000/128/65535=16Hz=PWM最小频率 //初始化 PWM 并且判断初始化是否成功 if (PWM_Init(PI_PWM_BASEADDR, kPWM_Module_3, &pwmConfig) == kStatus_Fail) { PRINTF("PWM initialization failed\n"); } Capture_config(); PWM_SetPwmLdok(PI_PWM_BASEADDR,kPWM_Control_Module_3 , true); PWM_StartTimer(PI_PWM_BASEADDR, kPWM_Control_Module_3 ); } i.MXRT 105x Re: RT1051 PWM Capture Counter Stop Hi @coderick , Thanks for your interest in NXP MIMXRT series! Did you set BOARD_PWM_BASEADDR->SM[3].VAL1 & INIT in your project? If VAL1 is still 0, it will cause a problem. Best regards, Gavin
View full article
GHS マルチデバッガ - マイクロコントローラの POR 後に再開しない こんにちは。私は Renasas E1 デバッガーと GHS マルチ デバッガーを使用しています。マイクロコントローラの電源をオフにして再びオンにすると、デバッガー ウィンドウが停止します。デバッグのために再開する必要があります。これに対する解決策を提供してください。セッションを再開するためにソフトウェアを再度フラッシュせずにこれを行うことは可能ですか。 Re: GHS Multi debugger - Not resuming after Microcontroller POR こんにちは@danielmartynek 、 私はルネサスRH850 - RH850/C1M-A2を使用しています よろしくお願い申し上げます。 Re: GHS Multi debugger - Not resuming after Microcontroller POR こんにちは@Lokesh_0109さん、 MCU部分を指定してください。 よろしくお願い申し上げます。
View full article
用于 mcxn947 的 flexio qspi 恩智浦你好, 我需要使用 flexio 来模拟 qspi 接口才能使用或非 flash。我想知道是否有任何方法可以直接对闪光灯进行编程,类似于 ISP 模式的工作方式。 我已经简要地阅读了参考手册,看来MCX无法在flexio上与qspi进行直接交互,只能与可以支持此功能的flexspi进行直接交互。 nxp 提供的现有工具中是否有可以实现此功能的工具? 我还查看了关于使用 flexio 仿真 qspi 的 AN14175。 我想问一下,中断模式的 flexio qspi 和 edma 模式的 flexio qspi 有什么区别?它们各自的性能如何,每种模式的用例又是什么。 启动 ROM | 启动配置 | 闪存 通信& 控制(I3C | I2C | SPI | FlexCAN | 以太网 | FlexIO) 核心与内存 MCX N Re: flexio qspi for mcxn947 你好@TomC818 我可以像 ISP 使用 FlexsPI 一样通过 Flexio-QSPI 对 NOR Flash 进行编程吗? 不,不是直接。 ISP 仅通过 FlexSPI 而非 FlexIO 仿真 QSPI 支持外部闪存编程。 MCX 中的 ROM 引导加载程序 (ISP) 无法识别或支持 FlexIO 作为可编程接口。   BR 哈利
View full article