Let´s start with KSDK! What is it KSDK? = Kinetis Software Development Kit Kinetis SDK v2 is a collection of comprehensive software enablement for NXP Kinetis Microcontrollers that includes: •system startup •peripheral drivers •USB and connectivity stacks •Middleware •Real-time operating system (RTOS) kernels. Documents – Release Note, API Reference Manual, Getting Started with KSDK, for USB – User Guide, USB Composite Device Guide, USB Device Reference Manual and USB Host Reference Manual. All these documents is possible to find at Software Development Kit for Kinetis MCUs|NXP or \SDK_2.0_selected_device\docs KSDK Structure Diagram KSDK Features •ARM® and DSP standard libraries, and CMSIS-compliant device header files which provide direct access to the peripheral registers •Open-source peripheral drivers •Open-source RTOS wrapper driver •Real time operation systems (RTOS) including FreeRTOS OS, μC/OS-II, and μC/OS-III •Stacks and middleware in source or object formats including: − CMSIS-DSP - a suite of common signal processing functions − FatFs - a FatFile System for small embedded systems − mmCAU - Memory-Mapped Cryptographic Acceleration Unit − SDMMC - software component supporting SD Cards and eMMC − DMA Manager - software component used for managing on-chip DMA channel resources − mbedTLS and WolfSSL - cryptographic SSL/TLS libraries − lwIP and USB Stack - a light-weight TCP/IP stack KSDK Evolution KSDK v1/v2 – what new features KSDK 2.0 brings •MQX Kernel removed from KSDK -> focus on FreeRTOS •MQX RTCS Ethernet and MFS File System Stacks -> lwIP and FatFS •OSA, Power Manager and Clock Manager -> no longer required by the drivers •USB Stack re-write -> BSD licensed solution •No platform library -> single project with all needed files •Mbed TLS now included as part of the accelerated cryptography drivers •Eliminates separate HAL and Peripheral Driver -> single driver for each peripheral •Processor Expert -> Kinetis Expert Tool •Updates for KDS -> via online update tool •Installation of KSDK -> KEX Tool (smaller download & sizes) •KEX Tool -> pin muxing selection & generation, clock configuration, low power estimation Simplified folder structure KSDK highlights & benefits •Collection of software enablement offered by free •KSDK is fully supported in these IDE: − Atollic® TrueSTUDIO® − GNU toolchain for ARM® Cortex® -M with CMake build system − IAR Embedded Workbench − Keil™ MDK-ARM − Kinetis Design Studio IDE •KSDK supports most of Kinetis MCUs •Created examples for drivers, USB, RTOS, demo applications •Start with development without device register knowledge Support & download Official support of KSDK: Kinetis Software Development Kit Create new SR according to: How to submit a new question for NXP Support More about KSDK... KSDK Official Website www.nxp.com/ksdk Introducing Kinetis SDK v2 https://community.freescale.com/docs/DOC-329783 Kinetis SDK 2.0 Transition Guide Kinetis SDK 2.0 Transition Guide KSDK Community https://community.freescale.com/community/kinetis/kinetis-software-development-kit Let´s continue in reading! See Let´s start with FreeMASTER!
View full article