Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
For MMA685x Accelerometer, what is the maximum junction temperature Tj? For MMA685x Accelerometer, what is the maximum junction temperature Tj?  The datasheet lists a Storage Temperature Range of -40C to +125C, but Max Tj is not provided. Accelerometers Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Hi Gerard, I just got an answer from our apps/design team, the maximum junction temperature Tj is 85 °C. Regards, Tomas Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Hi Gerard, OK, I need to check on this. I have emailed our apps/design team and will update this thread once I have their answer. Regards, Tomas Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Thank you Tomas for the quick response. I do not anticipate the device exceeding the Max Tj in our application; the worst case hot operating temperature is around 70°C. However, the Reliability Report I am compiling requires documentation of the manufacturer’s Max Tj for all semiconductor devices and microcircuits in the design. Since the Max Storage Temperature is listed as 125°C, is it a reasonable to also use this as Freescale’s rating for the Max Tj? If not, can Freescale provide a value for the Max Tj rating? Regards, Gerry Seipelt L-3 Communications O: 513.943.2226 Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Hi Gerard, I do not have an exact number, but the very low power consumption leads to a negligable increase of the junction temperature (<< 1 °C). Regards, Tomas
查看全文
MPX2010DPは空気の流れを計算します <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 拝啓、 以下の条件で空気流量(kg/s)を計算するにはどうすればよいでしょうか?ぜひお勧めください。ありがとうございます 1. パイプ径:6mm 2. オリフィス径:5mm 3. 圧力差(MPX2010DP圧力センサから取得):0.5 psi 圧力センサ Re: MPX2010DP calculate air flow <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるヨゼフへ 迅速なサポートをありがとうございます。 Re: MPX2010DP calculate air flow <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ジェフ様 空気の流量を計算する方法と計算式が記載されたリンクを見つけました。こちらのリンクをご覧ください: https://allsensors.com/engineering-resources/white-papers/pressure-point-11-calculating-flow-rate-from-pressure-measurem… こちらもご覧ください:低速はダクト内の空気の流れに悪影響を及ぼしますか? | Energy Vanguard あなたにとっても役立つかもしれません。 敬具、 ヨゼフ
查看全文
压力传感器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,我想在我的项目中使用压力传感器 MPX2100A 1- 我读到 110kpa 是什么意思(大气压力 +100 kpa ) 2- 是否可以将 arduino 与该压力传感器配合使用? Re: pressure sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,努里、 1.MPX2100A 是一种绝对压力传感器,这意味着设备输出是指施加在表面上的单位面积力的绝对值。因此,绝对压力是某一点的压力与绝对零度压力或完全真空之间的差值。 在这种情况下,您读取的不是大气压力,而是施加在 P1 上的压力。 2.事实上,您可以将 MPX2100A 与 Arduino 一起使用。 请注意,MPX2100A 是一种补偿压力传感器,这意味着给定输出已经过内部温度补偿,因此只需在外部添加放大电路,然后将传感器信号发送到MCU 的 ADC。 您可以参考以下放大电路: 希望这些信息对你有用。 如果我误解了你的问题,请随时告诉我。 我很乐意提供帮助。 祝您有美好的一天。 戴维-迪亚兹 注:如果本帖回答了您的问题,请点击 "正确答案 "按钮。谢谢!
查看全文
FXTH87 Evaluation Module or Development Kit Hi. I'm studing on TPMS and looking for the FXTH87 Family DVK to implement the system. According to "Xtrinsic FXTH87 Evaluation Design Reference Manual", It seem that the DVK or EVM are exist. But I was not able to find the web-site that sales the device. How can i get it ? And I also need to a device that can receive the sensing data from FXTH87. Thank you for your interesting. Pressure Sensors Sensing Platforms Re: FXTH87 Evaluation Module or Development Kit Hi. I don't receive any answer from Pascal Bernard. So, i try to contact with Freescale Korea Inc, and request the any help. At the result, I got the FXTH87 Module from Freescale Korea Inc. If you want to get the FXTH87 evaluation board, i advise you to try to contact with branch office of your location. I hope that this answer is helpful. Regards. Re: FXTH87 Evaluation Module or Development Kit Hi! Only Pascal Bernard can help with FXTH87 Development kit and evaluation board? I wrote to him, but didn't receive any answer... We working on prototype of commercial TPMS. With plans begin to produce it in Russia at 2016 Thank you! Re: FXTH87 Evaluation Module or Development Kit Hi Sol, New FXTH87 family evaluation boards are available in a limited quantity, please email directly MBW108 with your contact information and application description. Meanwhile, you might find useful the Xtrinsic FXTH87 Family Evaluation Design Reference Manual including the schematic, BOM and other useful information. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.
查看全文
センサタイプ MPXH6300A <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> センサータイプ MPXH6300A には、より媒体耐性のあるゲルのオプションはありますか?現在のデバイスにはフロロシリコーンタイプのゲルが使用されています 圧力センサ Re: sensor type MPXH6300A <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> トーマスさん、「受け取ったままの」状態では、同じリールに曇ったゲルと透明なゲルが混在しています...曇った外観はパフォーマンスに影響しますか、それともこれは許容できる状態ですか? Re: sensor type MPXH6300A <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、フィル。 いいえ、ありません。メディア耐性ゲルを備えたシリーズは、 MPXHZ6250AおよびMPXHZ6400Aシリーズのみです。 よろしくお願いいたします。 トーマス 追伸: 私の回答が質問の解決に役立った場合は、「正解」とマークしてください。ありがとう。
查看全文
FXPS7140P4 un-programmed default PSI5 communication Hi Can I communicate with FXPS7140P4 sensor with default setting? or it has to be programmed through PSI5 first in order to receive sensor data from it? If I can communicate with default setting then what is the default mode? asynchronous, synchronous, 10bit/16bit data, parity or CRC ? Regards, J Pressure Sensors Re: FXPS7140P4 un-programmed default PSI5 communication Hi Joe, Yes, but it can be shared under NDA only. If you have not signed the NDA with NXP yet, please create a standard case for my colleagues who are in charge of the NDA process and can eventually help you with that. Best regards, Tomas Re: FXPS7140P4 un-programmed default PSI5 communication Hi @TomasVaverka : Hope you are doing good. Is the official datasheet for FXPS7140P4 released yet ? We are waiting for it. You mentioned about the release date is around end of January 2022.  Best Regards, Joe Re: FXPS7140P4 un-programmed default PSI5 communication Hi Thomas, I got one more question for you. Can I set value 0x1A to register $25. Especially, the DATA_EXT bit, it allows us to read data range between -480 to +480 LSB according to the draft document(negative 16% to positive 16% for relative pressure). I have tried writing value 0x8A to register $25, it is working fine but again according to the draft document, it only allows us to read -102 to +307 LSB (which I can only read 3% of negative pressure change and 10% of positive pressure change ). Regards, Joe Re: FXPS7140P4 un-programmed default PSI5 communication Hi Tomas, Thank you for the detailed explanation and the pressure range again. With your word, I can rest assured that there is not thing bad happening during the programming. It was me changing the value in register $40 which resulted in OTP MEM fault. Although I have broken some samples here, you save me some samples that I was going to test. Thank you. I will look forward to the release of the document for this pressure sensor. Best Regards, Joe Re: FXPS7140P4 un-programmed default PSI5 communication Hi Joe, The pressure range cannot be changed in this device otherwise it will set the errors. The intension initially was to be able to change the range if a large opportunity presented itself and this can be evaluated on a case by case bases. With this said $40, range has been revised to "Reserved". This will be updated in a future release of the datasheet which I am guessing should be ready in the end of January 22. The datasheet will have the following for this register: The pressure range should be 40 kPa to 140 kPa. Best regards, Tomas Re: FXPS7140P4 un-programmed default PSI5 communication Hi Thomas,  We got a few samples here from local NXP, I cannot seem to understand the register 0x40. Whenever I set USER RANGE[1:0] bit to 0x01, and programed the chip with the rest of register setting indicated by programming manual. It resulted in MEMTEMP_ERR and U_OTP_ERR, which I cannot read sensor value. (would always read 0x1EB). However, if we set the USER RANGE[1:0] to 0x00 with the same setting of the other registers (again specified by programming manual and not modifying the 0x16 COMM bit), it would read pressure value just fine, and there is no MEMTEMP_ERR & U_OTP_ERR bits set. (the voltage setting and sync pulse width all conform to the sensor manual ) As our manual dose not elaborate on USER RANGE bit, we just want to confirm that the setting of 0x00 for register 0x40 can read the range as document specified 50kPA to 126 kPA for sensor FXPS7140P4. Regards, Joe Re: FXPS7140P4 un-programmed default PSI5 communication Hi Tomas, Thanks for your reply Regards, Joe Re: FXPS7140P4 un-programmed default PSI5 communication Hi Joe, All registers are set to 0 for any PSI5 configuration. So register 25 is 00 (PSI5_CFG). If you have a PSI5 device (FXPS7140P4), then you have to use PSI5 to use/comm to the device. With this said, the COMMTYPE bit field is set to 1 in register 16. If you try to changes this, it will produce an error so caution must be taken if you want do any over writes to the UF2 region in that this should be masked. Best regards, Tomas
查看全文
Regarding the accuracy performance of MPX5700AP I am not sure if the accuracy of my MPX5700AP meets the standards, and if there are any better suggestions for my testing circuit (has my current circuit had a negative impact on my testing     accuracy?) .I have connected the necessary capacitors as required. Thank you very much for answering my question. Pressure Sensors Re: Regarding the accuracy performance of MPX5700AP Ok, the samples I will move to the PCB board to measure. Thank you for your reply. Re: Regarding the accuracy performance of MPX5700AP The datasheet is somewhat accurate, and your test is best done on a PCB board. Re: Regarding the accuracy performance of MPX5700AP Hello, I just want to ask about the product output error, which is not written in the specification, and whether the usage needs to be improved. The company does have some pressure sensor products that Re: Regarding the accuracy performance of MPX5700AP Future bios will use pressure-related sensors. Re: Regarding the accuracy performance of MPX5700AP No, I'm still a student and my teacher told us to study this product. Re: Regarding the accuracy performance of MPX5700AP Is your company friendly?
查看全文
FXTH87 TPMS 評価ボードはどこで入手できますか? ハイ FXTH871511を韓国で購入しました。 評価用タイヤ空気圧監視センサボードを購入したいのですが、どうすれば購入できますか? Re: Where can I get FXTH87 TPMS Evaluation Board? EOL は行末ですか? 買わないの? Re: Where can I get FXTH87 TPMS Evaluation Board? この部品はすでにEOLでした。
查看全文
移植恩智浦传感器融合库时遇到的问题 你好 我正在将恩智浦传感器融合库移植到第三方微控制器上,但遇到了一些问题,不知道如何调试。 为了让您大致了解,实际需要进行航位推算(对线性加速度进行双重积分,以得出静止位置的位移)。积分周期应该很短,大约几秒钟,精度也不是那么重要。长话短说,假设我要用 IMU 测量一个摆锤的摆幅(单位:厘米)(摆锤的枢轴是固定的)。 在我看来,这似乎是可行的,尽管众所周知,使用这些 mems 传感器进行的死循环计算存在漂移问题,您同意吗? 到目前为止,我构建了一个采集加速度中心和陀螺仪数据的系统,为了简化开发,我将恩智浦传感器融合库封装到Octave/Matlab中。一旦程序库在 MCU 上运行,同样的代码也将在 MCU 上使用。 现在,我正在进行基本测试,以了解融合器是否按预期工作,但我遇到了一些问题(见图片),也许在该领域有更多经验的人在看到结果后能建议我从哪里着手解决这个问题。 在下面的测试中,IMU 绕 Y 轴旋转(一个方向旋转 90°,另一个方向旋转 180°,然后回到起始位置)。这些是我能提取的部分图像: 原始数据(Accensitivity=0.488mg/LSB)、陀螺仪灵敏度=17.5mdps/LSB) Raw accelerometer原始加速度计 Raw gyroscope原始陀螺仪 加速度计的原始数据很容易验证,在 Z 轴上可以看到 2070 个重力计数。2070*0.488=1010 毫克。 为了验证陀螺仪的数据,我将其整合(在融合库之外),得到了这个数据: Integrated raw gyroscope集成原始陀螺仪 除了陀螺仪偏移导致的漂移(这是预料之中的,因为没有对原始数据进行校正)之外,Y 轴上90° 顺时针 - 180° 逆时针 - 90° 顺时针的旋转模式清晰可见,因此传感器本身看起来没有问题。 然而,当原始数据被输入 SV_6DOF_GY_KALMAN 算法时,得到的线性加速度和方位角为 Linear acceleration线性加速 Orientation (roll/pitch/yaw) 方向(滚动/俯仰/偏航 ) 在这里,我看到了与想象中不同的东西。首先,加速度的 Y 轴在受到刺激后需要一段时间才能恢复到 0。 那么,有没有人可以建议我可能做错了什么,或者从哪里开始调试? 我知道,由于我使用的不是恩智浦平台,答案可能是",我们不支持这个" ,但我还是试一试。 非常感谢、 达维德 加速度传感器 陀螺仪 传感器融合
查看全文
计算压力传感器的高度范围 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,我正在查看 MPX4115A 空气压力传感器。 我正在考虑将其用于无人机测量气压高度。 我想知道我能用它测量的高度范围是多少;即:0 -> ****** 米或英尺。 另外,如果有更好的传感器选项(分辨率和范围),封装尺寸和接口相似,请告诉我 谢谢! 压力传感器 Re: Calculating the altitude range for pressure sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,丹尼尔 MPX4115A 是一款具有模拟输出的绝对压力传感器。它测量其端口上相对于真空密封参考的压力。其压力范围为 15kPa 至 115kPa。根据美国标准大气层的海拔高度与气压模型,其对应的海拔高度范围为-1080 米(115 千帕)至 13503 米(15 千帕)。 关于可能的替代部件,有采用较小封装(SOP 或 SSOP)的 mpxx6115a 系列。主要特征相同。 如果你不喜欢模拟输出,MPL3115A2 将是一个不错的选择。其校准后的压力范围从 50kPa 到 110 kPa,相当于 -698 米到 5572 米的高度范围。它允许通过 I2C 接口直接读取海拔高度(几乎无需额外计算),并将海拔数据提供到 30 厘米以内(启用过采样)。如果你想了解更多,迈克尔斯斯坦利发表了三篇关于这部分的文章。 希望对您有所帮助。 此致, 托马斯
查看全文
FXAS21000 停止工作 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 大家好,我正在使用 FXAS21000,在完成了裸机示例项目之后,我得以从设备中获得一些读数。但是,问题在于,经过几次读取 (< 5),设备会停止工作。我注意到中断引脚保持低电平。由于我使用 INT2 作为外部中断来知道何时读取寄存器,所以我的代码就停止工作了。如果忽略中断引脚,只读取 OUT_X_MSB 寄存器,就能得到正确的读数。 我知道只要读取从 OUT_X_MSB 开始的 6 个数据字节就应该 RESET 中断标志(数据表:" 读取 INT_SRC_FLAG 寄存器不会 RESET 任何事件标志源位;它们可以通过读取相应的事件源寄存器 " 来 RESET),但事实似乎并非如此。数据表还指出 " ... 该寄存器 (0x0B) 的内容在从待机模式过渡到运行模式或从就绪模式过渡到运行模式 " 时 RESET,所以我决定在读取之前从 " active " 切换到 " ready " 模式,然后返回 " 处于活动状态" 读取寄存器的内容后,这似乎可以解决问题,但并不理想,因为我需要3次操作才能读取数据。 #define FXAS21000_DR_SHIFT2(x) (x << 2) #define FXAS21000_REG1_DR_MSK 0x1C void FXAS21000::init(){     writeRegister(FXAS21000_CTRL_REG1, FXAS21000_REG1_SFT_RST); // Factory default     wait(1_ms);     // Enter in standby mode     uint8_t reg = getRegister(FXAS21000_CTRL_REG1);     writeRegister(FXAS21000_CTRL_REG1, reg & ~FXAS21000_REG1_STANDBY);     // Set the Full scale mode at 800dps     // High pass filter disabled     writeRegister(FXAS21000_CTRL_REG0, 0x01);     // Enable data ready interrupts     writeRegister(FXAS21000_CTRL_REG2, (1 << 2));     // Set a low sampling rate to start with (Mode_25Hz)     reg = getRegister(FXAS21000_CTRL_REG1) & ~FXAS21000_REG1_DR_MSK;     writeRegister(FXAS21000_CTRL_REG1, reg | (FXAS21000_REG1_DR_MSK & FXAS21000_DR_SHIFT2(3)));     // Back to active mode     reg = getRegister(FXAS21000_CTRL_REG1) & ~FXAS21000_REG1_STANDBY;     int r = writeRegister(FXAS21000_CTRL_REG1, reg | FXAS21000_REG1_ACTIVE); } int FXAS21000::read(int16_t * t){     uint8_t d[7];     int r = read( FXAS21000_STATUS, d, 7);     if(r <= 0){         return r;     }     t[0] = ((d[1] * 256) + ((unsigned short) d[2]));     t[1] = ((d[3] * 256) + ((unsigned short) d[4]));     t[2] = ((d[5] * 256) + ((unsigned short) d[6])); }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 有人遇到过类似问题吗?如果能得到任何帮助,我们将不胜感激! 谢谢、 A. 陀螺仪 传感平台 Re: FXAS21000 stops working <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 已经过去一年多了,我完全忘记了这篇文章。我现在回复,是为了让这些信息对其他人有所帮助。 问题原来是竞争条件;在 IRQ 例程中,我设置了一个标志来表示陀螺仪有数据,然后在主循环中我检查了该标志以确定是否应该读取新数据,如果是,则读取数据并将标志重置回 0。正如你现在所想象的那样,问题在于,在读取轴的 i2c 交易完成和我将标志重置回 0 之间,会出现另一个 IRQ,所以我基本上忽略了最后一个中断信号,这解释了中断引脚保持低电平的原因。 有几种解决方法,但我想我最终还是保留了原样,但在主循环中,即使标志为假(没有中断出现),也要重复检查 IRQ 引脚是否为低,这样就避免了在每个循环周期中都调用引脚状态,而只在明显发生错误时(标志表明没有新数据,但中断引脚为低)才调用引脚状态。 希望能对您有所帮助。 干杯 A. Re: FXAS21000 stops working <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,托马斯,谢谢你的答复。 是的,我确实有一台逻辑分析器,但不幸的是,该设备装在组装好的板上,我很难访问总线。我知道 INT2 引脚保持低电平,因为我可以从 MCU 读取该引脚的逻辑电平,并显示为低电平(在读数停止上升后)。 我知道 ISR 的 RESET 位;我在同一块板(以及许多其他板)上还有另一个使用相同的 IRQ 处理例程的传感器工作正常。此外,如果是这样的话,仅仅改变陀螺仪的运行模式不应该让 " 修复 " 这个问题。这说明我在配置 FXAS21000 的寄存器时做了一些愚蠢的事情。 我在最初的帖子中提到,该设备最多可以运行大约 5 个读数(似乎是随机的)然后停止工作,这让我想知道读取一定数量后是否应该清除 FIFO 缓冲区? 谢谢! A. Re: FXAS21000 stops working <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,亚历山大、 你有逻辑分析仪或示波器来了解总线上发生了什么吗?没有它,可能很难进行调试。   通过读取所有 X、Y、Z 输出数据寄存器(0x01 - 0x06),SRC_DRDY 标志被清除,INTx 引脚也随之失效。还需要在 ISR 中确认 IRQ,通常是向 MCU 的特定位写入逻辑 1。如果不这样做,MCU 上的中断标志将保持激活状态,从而无法接收来自 FXAS21000 的任何其他中断。   希望对你有所帮助。 顺祝商祺! 托马斯
查看全文
MPXM2053 电源电压 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 能否使用 Vs = 5 VDC 为 MPXM2053GS 供电?所选仪器放大器 INA333 的共模电压为 2.5 V。 压力传感器 Re: MPXM2053 Supply Voltage <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 谢谢您! Re: MPXM2053 Supply Voltage <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,海科、 是的,该传感器可以在 5V 电源电压下使用,最小电压约为 3V,以获得正确的比率输出。所选仪表放大器应正常。 此致, 托马斯
查看全文
圧力センサの高度範囲の計算 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは。MPX4115A 空気圧センサを検討しています。 私は気圧高度を測定する UAV アプリケーションとしてこれを検討しています。これで測定できる高度の範囲がどの程度なのかを知りたいです。つまり、0 -> ****** メートルまたはフィートです。 また、同様のパッケージサイズとインターフェースを備えた、より優れたセンサーオプション(解像度と範囲)がある場合は、お知らせください。 よろしくお願いします。 圧力センサ Re: Calculating the altitude range for pressure sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ダニエル。 MPX4115A は、アナログ出力を備えた絶対圧力センサーです。真空密封された基準を基準としてポート上の圧力を測定します。圧力範囲は15kPa~115kPaです。高度と圧力に関する米国標準大気モデルによれば、これは -1080 メートル (115kPa) から 13503 メートル (15kPa) の高度範囲に相当します。 代替可能な部品としては、小型パッケージ(SOP または SSOP)のMPXxx6115A シリーズがあります。主な特徴は同じです。 アナログ出力を好まない場合は、 MPL3115A2が良い選択肢です。校正済みの圧力範囲は50kPa~110kPaで、高度範囲は-698m~5572mに相当します。I2Cインターフェースを介して高度を直接読み取ることができ(追加の計算はほとんど不要)、 30cm以内の高度データを提供します(オーバーサンプリング有効時)。この製品についてさらに詳しく知りたい方は、 michaelestanleyがこの製品に関する3つの記事を公開しています。 これが役に立つことを願います。 よろしくお願いいたします。 トーマス
查看全文
DPS 読み取りのためにジャイロスコープ値を統合しますか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 FXAS21002C ジャイロスコープに関する機能上の質問があります。センサからの値をリアルタイムで印刷できます。しかし、動きが止まったときにゼロに戻るのではなく、角度変位を表示してその値をその位置に保持したいと考えています。一定時間にわたって値を積分すると問題が解決するのではないかと思います。私は C の初心者なので、実装するための詳細な参考資料やサンプル コードがあれば幸いです。 よろしくお願いします。 Re: Integrating Gyroscope values for dps readings? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、Priyank Sさん 動きを止めた後にジャイロスコープの値がゼロに戻る理由は、ジャイロスコープが実際には位置ではなく、角度変位の速度を測定しているためです。あなたができることは、あなたが言ったように、一定時間にわたって値を積分して修正することです。 または、他の解決策としては、システムに加速度センサを追加して、角度変位の前後の位置を実際に測定する方法があります。 残念ながら、この特定のアプリケーションを実装するための参考資料やサンプル コードはありませんが、次のリンクで FXAS2100x ジャイロ スコープのベアメタル サンプル プロジェクトを見つけることができます: https://community.freescale.com/docs/DOC-100869 これが Freescale ジャイロスコープの使用開始に役立つことを願っています。 すてきな一日を、 ホセ・レイエス ----------------------------------------------------------------------------------------------------------------------- 注: この投稿で質問が解決した場合は、「正解」ボタンをクリックしてください。ありがとう! -----------------------------------------------------------------------------------------------------------------------
查看全文
Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello, I am using High Accuracy Low g Inertial Sensor (MMA690xKQ) in my project. I have read the specification but I am unable to find the use case of Register Pointer Read and Register Pointer Write in Table 3.4, 3.5, 3.6, 3.7. Kindly let me know how to use Register Pointer Read and Register Pointer Write and also the meaning of bits A[7:0] is the same tables. Accelerometers Re: Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello For any register reading I am getting E6 or FE response can you please help me on exact response clock is good and CS pin also ok Re: Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello register address: e       register address:14     message transmitted STATUS is 0xe0-0x00-0x00-0x00 E0 00 STATUS is 0xe0-0x00-0x00-0x00 serialNo - 0:e0 printf device status register register address:1   register address:30    message transmitted STATUS is 0xff-0xff-0x00-0x00 FF FF STATUS is 0xff-0xff-0x00-0x00 serialNo - 0:ff printf device status register register address:0   register address:20    message transmitted STATUS is 0xe6-0x00-0x00-0x00 E6 00 STATUS is 0xe6-0x00-0x00-0x00 serialNo - 0:e6 this is the response I am getting Please help me on the exact response Re: Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello Manojkumar, The SPI protocol for the MMA690x devices does not allow for transmission of both a register address and register data in the same command.  The address must be set by a previous command.  This is the purpose of the Register Pointer Write command.  The Register Pointer is the address at which data will be read from or written to when a Register Data Write or Register Data Read is executed.  So the normal sequence for a register read or a register write will take at least 2 commands:   Register Read: Send a “Register Pointer Write” command to set the pointer to the register address to be read Send a “Register Data Read” command to retrieve the data from the register pointed to Register Write: Send a “Register Pointer Write” command to set the pointer to the register address to be read Send a “Register Data Read” command to retrieve the data from the register pointed to   Note that the MISO response for each MOSI command will come on the subsequent transfer.  As shown in the image below. Here are a few examples. Read Register $10 (DEVSTAT) Register Pointer Write to $10 MOSI                    = 0x1410 Expected MISO  = 0x0800 Register Data Read MOSI                    = 0x2000 Expected MISO  = 0x1000              (assumes no flags set in DEVSTAT) Write 0x01 to Register $0E (Enable Positive Self-Test) Register Pointer Write to $0E MOSI                    = 0x140E Expected MISO  = 0x0800 Register Data Write MOSI                    = 0x3001 Expected MISO  = 0x180E              (includes address echo) Register Data Read to Confirm MOSI                    = 0x2000 Expected MISO  = 0x1401 I hope this is clear. Best regards, Tomas
查看全文
MMA8453 Detect false double tap Hi, MMA8453 is placed inside a device which a person can carry while traveling. We've enabled double tap feature which the person can use in case of emergency. The problem is we're getting false double taps when the vehicle is moving. Configuration: REG_PULSE_CFG 0x2A REG_PULSE_THSX 0x20 REG_PULSE_THSY 0x20 REG_PULSE_THSZ 0x40 REG_PULSE_TMLT 0x18 REG_PULSE_LTCY 0x28 REG_PULSE_WIND 0x3C Thanks, Prakash Re: MMA8453 Detect false double tap Hi Prakash, I have never heard of a similar problem and it is hard to provide any specific setting that would eliminate such unwanted triggers. My only recommendation is to adjust the threshold and duration values by testing it in a vehicle. Best regards, Tomas
查看全文
FXTH8709116T1 和 FXTH8709226T1 有什么区别?我在数据表中没有看到任何明显的区别,也许我遗漏了什么? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好 - 我正在查看恩智浦的 TPMS 芯片,但看不出 FXTH8709116T1 和 FXTH8709226T1 之间有什么区别? 有人能告诉我吗? 非常感谢 Peter Re: What is the difference between the FXTH8709116T1 and the FXTH8709226T1?  I don't see any obvious differences in the data sheet, perhaps I'm missing something? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,托马斯 谢谢您的帮助。 能否与我们联系 x22 固件指南的更新版本何时可用? 非常感谢 Peter Re: What is the difference between the FXTH8709116T1 and the FXTH8709226T1? I don't see any obvious differences in the data sheet, perhaps I'm missing something? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 是的,将软件从 x22 移植到 x11 非常简单。通过比较x11 固件用户指南和x22 固件用户指南,可以列出两种固件之间的区别。也可在 本网页"用户指南 "下找到 这 两份指南。 注意:当前的 x22 固件用户指南将很快更新(几周内),因为当前版本中的某些信息还不完整。 顺祝商祺! 托马斯 Re: What is the difference between the FXTH8709116T1 and the FXTH8709226T1? I don't see any obvious differences in the data sheet, perhaps I'm missing something? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,托马斯 感谢您的回复。我的问题的背景与需要将软件从 x22 移植到 x11 有关。如果软件已经在 x22 芯片中实现,我想知道需要对软件做多大改动,以及需要进行多少后续测试。我想这个问题的答案与软件的具体功能有关,这也是我寻找固件规格的原因。您认为从 x22 到 x11 的软件移植是否简单? 非常感谢 Peter Re: What is the difference between the FXTH8709116T1 and the FXTH8709226T1? I don't see any obvious differences in the data sheet, perhaps I'm missing something? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 FXTH870922 固件包含与 FXTH870911 相同的功能,只是其中一些功能没有正确实现,因此无法使用。 这意味着与 FXTH870911 相比,使用 FXTH870922 没有优势。FXTH870922 固件没有额外的功能;相反,FXTH870911 固件的功能更多,因为所有固件功能都已正确实现。 顺祝商祺! 托马斯 Re: What is the difference between the FXTH8709116T1 and the FXTH8709226T1? I don't see any obvious differences in the data sheet, perhaps I'm missing something? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,托马斯 感谢您的回复。 有什么地方能提供 FXTH870922 的固件指南吗? 我有 x11(和 x12)的指南,我想知道它们到底有什么区别。 或者更好的是,能准确描述差异(在性能或功能等方面)的东西? 非常感谢 Re: What is the difference between the FXTH8709116T1 and the FXTH8709226T1? I don't see any obvious differences in the data sheet, perhaps I'm missing something? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 唯一不同的是内部的固件,硬件是一样的。 FXTH870922 固件是为希望在先前 TPMS 设备的固件与当前 FXTH 之间兼容的客户发布的。该固件不具备FXTH870911固件的所有改进功能。因此,建议所有新客户使用FXTH870911,而不是FXTH870922。 顺祝商祺! 托马斯
查看全文
reliability data MPX4250 Hello We are using one of your components (MPX4250) in our designs. We do our calculations with data from studies of the components HTOL.May we have its reliability data (FIT, MTBF,...)? Thank you and best regards, Fernando López Bolós Indra Systems - Torrejon de Ardoz (Madrid, España) Ctra de Loeches 9 28850 +34 916271190 Pressure Sensors Re: reliability data MPX4250 Hello Fernando, Thank you very much for writing. In order to provide you the material requested, please submit a new case at the NXP web page. To submit a case, you need to log in to our NXP website and once log in, click on this link https://nxpcommunity.force.com/community/. It will redirect you to the case portal and you'll be able to submit the case. Please let me know if you have any further question. Saludos, David
查看全文
MMA8652 : 過渡割り込み閾値 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるコミュニティの皆様 過渡割り込みしきい値を考慮します。 以下のようにレジスタ値を設定する場合、 一時割り込みはいつ発生しますか? 0x1F:TRANSIENT_THSレジスタTHS[6:0]を000_0000bに設定します。 0x1D:TRANSIENT_CFG レジスタ HPF_BYP を 1 に設定します。 過渡割り込みトリガーポイント値はどれですか? 「ゼロ G 以上」か「ゼロ G より大きい」か? よろしくお願いします、 坂上公一 加速度センサ Re: MMA8652 : Transient interrupt threshold value <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 光一様 最小しきい値解像度は 0.063g (TRANSIENT_THS = 0x01) です。当社の加速度センサはどれもこれより高い解像度を提供しません。 よろしくお願いいたします。 トーマス Re: MMA8652 :  Transient interrupt threshold value <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> トーマス様 お返事ありがとうございます。 > このような設定は何の役に立つのでしょうか? 0.063g 未満の過渡現象を検出したいと思います。 よろしくお願いします、 坂上公一 Re: MMA8652 : Transient interrupt threshold value <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 光一様 このような設定は何の役に立つのでしょうか?加速度が 0g を超えると割り込みが発生します。 よろしくお願いいたします。 トーマス
查看全文
FXAS21002 显示 WHO_AM_I 为 0 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好。 我正在通过 I2C 接口查询 FXAS21002 陀螺仪的 WHO_AM_I 寄存器。以下是逻辑分析仪的屏幕截图。 在我看来有点奇怪的是,在传送第 9 位(ACK)后,SDA 在寄存器地址传送前的一段时间内没有变为高电平。这可能是我面临的问题吗? 如果没有,问题出在哪里? 非常感谢您。 陀螺仪 Re: FXAS21002 gives WHO_AM_I as 0 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,托马斯。 谢谢。你说得对。重复启动其实才是问题所在。看来 Raspberry Pi3 无法正确处理它。 此致敬礼, 埃夫西米奥斯 Re: FXAS21002 gives WHO_AM_I as 0 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,埃夫西米奥斯、 我想问题是你在第二个字节 (0x0C) 之后发送停止条件(SDA 从低到高的转换,而 SCL 为高电平),而不是发送重复的启动条件。因此,请尝试修改源代码,使 SDA 在 SCL 变为高电平之前过渡到高电平,以消除停止条件。 希望对你有所帮助。 顺祝商祺! 托马斯
查看全文